技术日 - 培训资料

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Technology Days - Training Material

Training Sessions Material



Home

Home is where the heart is..

Home Control & Security; Development Software & Tools

Automotive

Automotive

讨论

排序依据:
Ensuring that valuable IP is protected throughout the product lifecycle can help bring peace of mind and prevent loss of business revenue. This webinar will provide an overview of the security features available on the LPC5500 MCU series from NXP and how they can be leveraged as part of the manufacturing process. EPS Global, a worldwide provider of IC programming and secure provisioning services, will discuss the value these security features bring to IP protection and outline the manufacturing flows available for the LPC5500 MCU series to deliver end-to-end security throughout the product’s lifecycle, from design, and throughout the manufacturing supply chain. Presenters:  Clark Jarvis, Ecosystem Product Marketer, NXP Brian Colgan, Field Applciation Engineer, EPS Global
查看全文
Review of NXP’s current CAN portfolio and CAN functions, our support for CAN FD and an overview of the breakthrough products keeping CAN highly relevant for the new generation of vehicles.
查看全文
Presented by Taki Chow, Advantech Presented at DwF Kinetis MCUs Based on ARM® Technology Nanjing - 12 March 2015
查看全文
Presented by Cao Nan, Nanjing Normal University Presented at DwF Kinetis MCUs Based on ARM® Technology Nanjing - 12 March 2015
查看全文
With its broad portfolio, NXP is uniquely positioned to propose a full system allowing a scalability from NCAP to L4/L5 autonomous driving. To address such scalability, NXP has faced some challenging decisions about the system partitioning, performance, safety decomposition, AI Acceleration and Programming language. All these challenges will be addressed during the session.
查看全文
2019 is forecasted to be the year that voice will move beyond smart speakers to all segments of the IoT/industrial market. In this class we will give an overview of different architectures and solutions that can be implemented based on NXP processors.
查看全文
The PF81 and PF82 PMIC family is designed for high-performance processing applications such as infotainment, telematics, clusters, vehicle networking, ADAS, vision and sensor fusion. It is ideal for i.MX 8, i.MX 8X, S32V, and Networking processors in Automotive, Industrial, and Consumer applications. In this session we will offer a detailed overview of the family, its features and advantages of scalability and functional safety
查看全文
Do you need a robust MCU for high reliability and safety applications? Join this class to learn about the S32K MCU platform which offers auto grade, CAN-FD, lower power, hardware and software scalability and a minimum 15 year longevity.
查看全文
Presented by LIANG PING Presented at DwF Kinetis MCUs Based on ARM® Technology Nanjing - 12 March 2015
查看全文
S32K11x, S32K14x product and solution, migration to future S32K products.
查看全文
If you find yourself in need of using a low cost co-processor to act as a communications hub, why not consider a GPIO expander?  With the features in our latest GPIO expanders, this device can almost mimic a low cost MCU while being more cost-effective and reducing the complexity of your system. Come learn about the features and benefits, and actually see the GPIO expander in action on a simple PCB you’ll experiment with in this class.
查看全文
S32V234 vision product family introduction.
查看全文
Get to know the latest offering from the leading supplier in Automotive and Industrial controllers. This class will first give you an overview of our benchmark next-generation S32 hardware, software and tool enablement, Then go over the latest product offering of the #1 Automotive MCU S32K with its new reference design, software and tools enablement which will introduce you to the popular and powerful S32V vision processor for mass market applications including new software library enablement for AI CNN and DNN applications.
查看全文
This presentation provides an overview of the new toolchain to support the S32 platform of MCUs and application processors, this includes an IDE with new project generation, extensive collateral for ease of use and getting started as well as the next-generation Debugger tools, a new Flash tool specifically design for the S32 platform, the S32 configuration tool plus numerous software products integrated into the toolchain for ease of customer use.
查看全文
Learn about the automotive microcontrollers innovative applications.
查看全文