S32K知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K Knowledge Base

标签

讨论

排序依据:
Some customers inquire how to use FreeMASTER with S32K3. But there is no exists example projects which demonstrate usage of the FreeMASTER serial communication driver in S32K3 Real Time Drivers at the moment. So this article will introduce how to use FreeMaster SDKs in S32K3 RTD 0.9.0. Download S32DS \ S32K3 Development Package \ RTD (SDK) \ FreeMASTER Driver Login your account on NXP website, and download the S32K3 Standard software from TOOLS &SOFTWARE of S32K3 webpage. If you have already installed the S32DS3.4 \ S32K3 Development Package 3.4.0 \ RTD 0.9.0, then you can skip the following part and start directly from 4.Install FreeMASTER Driver 3.0 for S32K3 S32K3 Standard Software.png Download S32DS S32K3 Development Package RTD FreeMASTER Driver.png Install S32K3 Development Package 3.4.0 After install the S32 Design Studio v3.4, we should install S32K3 Development Package 3.4.0(SW32K3_S32DS_3.4.0_D2012.zip): go to menu "Help" -> "Install New Software" and click on "Add..." button Add Repository.png Here we uncheck S32 Design Studio S32K3 SDK (RTD S32K3 0.8.1), because we will install the newer version S32K3 RTD 0.9.0 later. Install New Software SW32K3_S32DS_3.4.0_D2012.png Install S32K3 Real Time Drivers Version 0.9.0 S32K3 Real Time Drivers Version 0.9.0 can be installed by refer the Offline Package Installation Setup of S32DS Extensions & Updates: Explanation and How To Use. Offline Package Installation Setup S32K3 Real Time Drivers Version 0.9.0.png S32K3 RTD AUROSAR 4.4 Version 0.9.0 selected.png Install FreeMASTER Driver 3.0 for S32K3 Offline Package Installation Setup FreeMASTER Driver 3.0 for S32K3.png FreeMASTER Driver 3.0 for S32K3 selected RTD090.png Attach FreeMASTER_S32K3 to S32K344_UART_Printf_Sample_090_34 The reason for choosing the S32K344_UART_Printf_Sample_090_34 project to demonstrate the combination of FreeMaster SDKs is that the project has already configured the LPUART of the S32K3X4EVB-Q257 development board. S32K3_EVB defined symbols.png Attach FreeMASTER_S32K3.png Select LPUART peripheral as host communication Through the description in the Requirements and Release Description chapter of FreeMASTER Driver Release Notes(FMSTRS32K3RN), we can see that currently only UART interface is supported. The S32K3 FreeMASTER 3.0 version 1.0.0 only support NXP GCC 6.3 or 9.2 for ARM at the moment, but the latest S32K3 Real Time Drivers Version 1.0.0 is based on NXP GCC 10.2.0. This is the reason why RTD 0.9.0 is selected in this article.  Requirements and Release Description FMSTRS32K3RN.png The README.txt also shows that: Current package provides FreeMASTER Communication Driver support for S32K344 over LPUART module README include_freemaster.png  LPUART13 is selected in this project for S32K3X4EVB-Q257, so we need to define the base address for FreeMASTER: #define FMSTR_LPUART_BASE           0x404A0000 define FMSTR_LPUART_BASE.pngModify the main function according to the README.txt: main.png Connect FreeMASTER3.1 to S32K3X4EVB-Q257 board Here we can see that the FreeMASTER3.1 is connected to S32K3X4EVB-Q257 board. connected.png  
查看全文
******************************************************************************** * Detailed Description: * * Example shows possible setting for PWM duty cycle update using DMA. * FTM0 ch0 is set to Edge aligned mode with 20KHz period. * Initialization trigger is routed back to HW trigger 1 using TRGMUX, so this HW * trigger can be used for CnV synchronization. * DMA on FTM0 ch0 is enabled (on ch0 CHF flag) and DMA ch0 configured to update C0V * from duty cycle variable. * NOte CHF is not set for 0% and 100% duty cycle, thus no DMA trigger is generated. * * Green LED is dimming as duty is changing. * * ------------------------------------------------------------------------------ * Test HW: S32K118EVB-Q64 * MCU: PS32K118LAMLH 0N97V * Compiler: S32DS.ARM.2.2 * SDK release: S32SDK_S32K1xx_RTM_3.0.3 * Debugger: Lauterbach, OpenSDA * Target: internal_FLASH * ******************************************************************************** Revision History: 1.0 Sep-16-2021 Petr Stancik Initial Version *******************************************************************************/
查看全文
Due to K3 hasn't been mass-produced yet, this content is moved to S32K3 Internal forum: https://community.nxp.com/t5/S32K3-Internal-Community/S32K3-Low-power-lab/ta-p/1280219 Any question, pls contact [email protected].
查看全文
********************************************************************************  Detailed Description:  Example shows FlexCAN 0 usage in RUN/VLPR modes using SDK.  CAN bitrate is set to 250bit/s.  MCU enters VLPR mode by pressing SW3 button. CAN std message is sent with data VLPRmode"  MCU exits VLPR to RUN mode when one of following happens:  - CAN std message with RX_MSG_ID is received and MCU is in VLPR  - SW2 button is pressed (PTC12 interrupt). CAN std message is sent with data "RUN mode"  Blue LED is dimming and the rate is different for each power mode due to different  system clock (48Mhz vs 4MHz)  ------------------------------------------------------------------------------  Test HW: S32K116EVB-Q48  MCU: PS32K116LAM 0N96V  Compiler: S32DS.ARM.2.2  SDK release: S32SDK_S32K1xx_RTM_3.0.3  Debugger: Lauterbach, OpenSDA  Target: internal_FLASH ********************************************************************************
查看全文
Hello everyone, SEGGER's Real Time Transfer (RTT) is the new technology for interactive user I/O in embedded applications. It combines the advantages of SWO and semihosting at very high performance. Bi-directional communication with the target application Very high transfer speed without affecting real-time behavior Uses debug channel for communication No additional hardware or pin on target required Supported by any J-Link model Supported by ARM Cortex-M0/M0+/M1/M3/M4/M7/M23/M33 and Renesas RX100/200/600 Complete implementation code providing functionality and freedom Here, I'd like to share you the SEGGER RTT porting project on S32K144 as attached. SW requirements: S32DS for ARM v2.2 IDE + S32K1xx SDK RTM 3.0 HW requirements: S32K144-EVB  + J-LINK debugger   For SEGGER RTT, you can refer to: About Real-Time Transfer: https://www.segger.com/products/debug-probes/j-link/technology/about-real-time-transfer/   RTT SEGGER Wiki: https://wiki.segger.com/RTT#SEGGER_RTT_TerminalOut.28.29;   Using Segger Real Time Terminal (RTT) with Eclipse: https://mcuoneclipse.com/2015/07/07/using-segger-real-time-terminal-rtt-with-eclipse/   Hope this project can help you, and enjoy the RTT! Best regard, Enwei Hu.
查看全文
Audio Video Bridging(AVB) is a protocol for the transport of audio and video streams over Ethernet-based networks, which makes it possible to deliver high volumes of data in real-time to multiple destinations with very low latency. This reference design board demonstrates the usage for AVB over S32K148. Alternatively, it can be an S32K148 evaluation board of 100pin version besides S32K148EVB-Q144 and S32K148EVB-Q176. Below shows the board layout, diagram, and main features. AVB RDB V2 picture.jpg Figure 1. S32K148AVB-RDB Layout   S32K148AVB-RDB Diagram(Rev B) Figure 2. S32K148AVB-RDB Diagram S32K148AVB-RDB Features Figure 3. S32K148AVB-RDB Features In terms of the software, we provide several examples to show the AVB/TSN usages and other applications. The avb_listener_talker project is the main example which implements most features and demonstrates by connecting 2 AVB boards by Ethernet cable.   AVB examples.jpg Figure 4. S32K148AVB-RDB Code Examples Below software stack and middleware are implemented. ✓ RTOS: FreeRTOS ✓ Peripherial Driver: SDK RTM 3.0 (Work with Processer Expert) ✓ AVB Stream: RTM 1.0 ✓ AVB AudioIf: RTM 1.0 ✓ gPTP Stack Version: 1.3.4 ✓ Lwip Stack Version: 2.1.2 •Note: Even though we did a lot of tests, it’s still the customer’s responsibility to ensure the total quality by themselves when it’s integrated into a real application project, all the sample codes and user guide documentation are just reference for the customer. •Note: We do not have an FCC or CE certificate for this board.   Now we have 50 pcs boards available in Chongqing, China. For applying for the board, please contact NXP sales or GPIS marketing.  Since the AVB stack is not free of use, for accessing the code please contact NXP sales or GPIS marketing. For technical discussion, please contact [email protected] or [email protected].  
查看全文
******************************************************************************************************** Detailed Description: LPUART1 echoes RX signal at 115200 bps When an 's' char is received, the MCU enters VLPS. A falling edge of the RX signal brings the MCU from VLPS via LPUART RXEDGIF interrupt. BUS_CLK can be monitored at CLKOUT PTD14. In VLPS, BUS_CLK is gated off. -------------------------------------------------------------------------------------------------------------------------- Test HW: S32K144EVB-Q100 MCU: S32K 0N57U Debugger: S32DS_ARM_2.2, OpenSDA Target: internal_FLASH ******************************************************************************************************** danielmartynek_0-1605283306283.png danielmartynek_2-1605283434147.png    
查看全文
Hi,      The draft time gap, from power-on to clock output of S32K14x, is as below. Snipaste_2020-11-09_14-10-24_Reset vs CLKOUT.jpg Snipaste_2020-11-09_14-09-54.jpg    You can take a reference. Cheers! Oliver
查看全文
NXP S32K1xx serial MCU is widely used in automotive body control and many general-purpose automotive applications, while to target some applications with special requirements such as requiring more peripherals instance than the portfolio can offer (e.g. 6x CAN-FD, 6x LIN or 4 I2C) like mid-end BCM or DCU, an on-board dual/multi MCU sync solution is proposed as an alternate solution to extend the S32K1xx MCU peripherals/memory resource and CPU process capability. The eRPC (Embedded Remote Procedure Call) is a Remote Procedure Call (RPC) system created by NXP(https://github.com/EmbeddedRPC/erpc/). An RPC is a mechanism used to invoke a software routine on a remote system using a sample local function call. eRPC software architecture Figure 1. eRPC software architecture In this project, we ported the eRPC protocol to S32K1xx platform, tested and figured out its performance. An out-of-box software package with detailed user guide (this document) is provided to simplify and accelerate users’ assessment of eRPC on S32K1xx. Two S32K144EVB boards are connected to demonstrate the usage of the eRPC protocol. One works as the client, another as the server. The client board starts an eRPC request and the server board responds to the request and executes the service. eRPC task workflow on S32K144-EVB.png Figure 2. eRPC task workflow on S32K144-EVB There are three types of MCU extensions are demonstrated in the project: MCU IO extension: Set LED; MCU peripheral extension: CAN and LIN message forwarding, LED luminance regulator; CPU process capability extension: Matrix multiply and addition math operation. Please find the attached sample projects and user guide for more details. Table of Contents in User Guide.png Figure 3. Table of Contents in User Guide •Note: Even though we did a lot of tests for the solution with the sample projects on S32K144-EVB, it’s still customer’s responsibility to ensure the total quality by themselves when it’s integrated in a real application project, all the sample codes and user guide documentation are just reference for customer. If you have any questions about this solution, please post here and we can have an open discussion. Best Regard, Enwei Hu(胡恩伟) GPIS System Apps Engineer.  
查看全文
Often we need to implement a SENT receiver in order to read the information sent by some sensors. It is useful to have the possibility of transmitting different message patterns in order to test your implementation. With this project you can transmit via a computer terminal a group of messages (up to 64). The project runs on a S32K144 EVB board, the output signal goes through J206 pin.
查看全文
*******************************************************************************************************  Detailed Description:  Configures the MCU to run system clock from XOSC.  LPUART1 is set to respond to LIN header sent from master.  Based on ID received the LPUART1 either receive frame's data and compare checksum  or publish requested data with calculated checksum. Enhanced checksum is used.  Interrupt is used for RX and TX operation and 2 versions of interrupt routine are available.  VER 1 ... during response transmission receiver disabled and transmit interrupt enabled  VER 2 ... during response transmission receiver is kept enabled  ------------------------------------------------------------------------------  Test HW: S32K116 EVB-Q048  MCU: PS32K116LAM 0N96V  Fsys: 40MHz  Debugger: Lauterbach  Target: internal_FLASH ******************************************************************************************************
查看全文
An example implementation of SENT protocol receiver with S32K118 evaluation board. The input is expected in J106, TICK duration is 2,75us. CRC is calculated and check, the decoded output is printed into terminal via UART (ASCII)
查看全文
**************************************************************************************** Detailed Description: This is a rather simple example that shows LPI2C0 in Master mode. MPL3115A2 sensor is used as a slave device. I2C bus at PTA2 SDA, PTA3 SCL (2-pin open drain mode), external pull-up resistors on BRKTSTBC-P3115 board. BRKTSTBC-P3115 supplied from P3V3 (J3.7). Baud rate 400kHz, source SIRCDIV2 8MHz. The master reads periodically MPL3115A2 status register (every 200ms) and temperature / altitude data once they are ready. ------------------------------------------------------------------------------------------------------- Test HW: S32K144EVB-Q100, BRKTSTBC-P3115 MCU: S32K144 0N57U IDE: S32DSR1, OpenSDA Target: internal_FLASH ****************************************************************************************
查看全文
Using S32k144 ISELD SDK driver and adding Touch Sensor software, a demo is created to show different light combinations when electrodes of S32K144 EVB are touched. ADK ISELED board is attached to S32K144 EVB.
查看全文
Example of usage of AIPS-lite, Protects the access to GPIO port. This example can be used with UART terminal, 115200 bps. The interface menu shows like this: AIPS example has started Please press 0 + enter to set red LED in GPIO port Please press 1 + enter to set red LED in GPIO port Please press 2: GPIO peripheral will only accept accesses from trusted master, M0 (Core) is set as untrusted when a write access, AIPS cannot longer be modified from core and a reset will occur in the next GPIO access Please press 3: GPIO access is write protected, any write access to GPIO will produce a hard fault
查看全文
Hi,     If you try to compile the sample project within S32K14X_MCAL4_2_RTM_1_0_0, you should take care of the command if you use Linaro.    After you set the environment of compiling and run the command under command window, you should enter     "launch.bat MODE=USER TOOLCHAIN=linaro"    NOT    "launch.bat MODE=USER TOOLCHAIN=LINARO"      The command is case sensitivity.   Hope you can compile the project successfully.  Cheers! Oliver
查看全文
To accelerate S32K demand creation and support urgent evaluation requriement in Great China, we build one batch boards locally. These boards will only be given out to our potential opportunities for free. The boards are made by China local partner and verified by AE and FAE team. if you have any question on this kind of board, please go to China Auto CAS or Auto MCU marketing for support. 1. Board overview   2. Pinout 3. Test point 4. Block diagram 3. The main difference between NXP official S32K EVB and this FRDM-S32K144 board are OpenSDA firmware and CAN PHY The original OpenSDA firmware in this board is from MBED which is not supported by S32DS, thus we need to change to PEmicro OpenSDA firmware, and then we can use S32DS for development.   Unplug the USB cable (if attached). Press and hold the Reset button. Plug in a USB cable from a USB Host to the OpenSDA USB port. Release the RESET/Bootloader button. A removable drive will be visible in the host file system with a volume label of BOOTLOADER. Drag/drop or copy/paste attached firmware “DEBUG-FRDM-K64F_Pemicro_v108a_for_OpenSDA_v2.0.bin” into the removable drive. Unplug the USB cable and plug it in again. The OpenSDA application should now be running. The CAN physical is different. This board used standalone CAN PHY but not CAN SBC. Please refer SCH file for debug.   Original Attachment has been moved to: dmeo2.rar
查看全文
Dear all, I'd like to share some useful tips about S32DS for ARM v2018.R1 IDE and S32K1xx development  in Chinese as below: 《S32DS使用Tips--SDK使用常见问题(FAQ)答疑》; 《S32K SDK使用详解之S32 SDK软件编程思想详解》; 《S32K SDK使用详解之S32 SDK软件架构详解》; 《 S32K1xx系列MCU使用Tips--功能介绍及软件开发和硬件设计FAQ》; 《 S32K1xx系列MCU使用Tips--Flash加密后不断复位无法连接调试器的问题解决》; 《S32DS使用Tips--S32DS for Power V1.2 链接文件和启动过程详解》; 《S32K1xx系列MCU使用Tips之SDK软件架构和使用详解》; 《S32DS使用Tips--SDK使用常见问题(FAQ)答疑》; 《S32DS IDE使用Tips--应用工程调试常见问题(FAQ)答疑》; 《 S32DS 使用Tips之S32DS for Power不同版本之间的GNU工具链差异与外设寄存器位域访问问题总结》; 《 S32DS使用Tips之S32DS for Power v1.1应用工程升级到v1.2重新编译运行程序跑飞问题解决》; 《S32DS 使用tips--S32DS for ARM v1.3工程到S32DS for ARM V2.0迁移升级方法和注意事项》; 《  S32DS 使用 tips--工程属性配置(编译选项和C编译器、汇编器及链接器设置)》; 《 S32DS使用Tips--如何编译生成和调用静态库》; 《S32DS使用Tips--如何通过创建新的编译目标(Build Target)在同一个S32DS工程中同时编译静态库和应用程序》; 《 S32DS使用Tips--如何配置和使能Attach功能定位软件程序bug和完成bootloader与应用程序工程的联合调试》; 《 CodeWarrior与S32DS IDE使用 Tips之如何在应用工程中保留定义但未使用的全局常量、变量(用于参数标定)》; 《 S32DS 使用 tips--使用Flash from file下载S19或elf文件》; 《S32DS for ARM v2018.R1安装IAR Eclipse插件调用IAR工具链开发S32K系列MCU应用程序详解》 For more contents, please follow below link: “汽车电子expert成长之路”微信公众号最新最全原创技术分享文章列表 ; Hope this can help you and have a nice day~! Best regard, Enwei Hu(胡恩伟)
查看全文
S32Kxxx   Excel configurators MPC5xxx/S32Kxx: CAN / CAN FD bit timing calculation   S32K1/S32M24x   Documents Solution for S32K14x which could be attached while couldn't be re-programmed Fault handling on S32K144 FRDM-S32K144 EVB Useful tips about S32DS for ARM v2018.R1 IDE and S32K1xx development Using S32K CMSIS-SVD Files in EmbSysRegView Eclipse Plugin FlexNVM used as code/data Flash   S32K3/S32M27x   Excel configurators S32K344 DCF Configurator   Debugger plugins Lauterbach FCCU_Utility plugin - S32K3xx    Documents Restrict the debug access with a password when HSE is not used S32K3/S32M27x – eMIOS Usage S32K3/S32M27x – eMIOS/BTCU/ADC/DMA – [RTD600] S32K3/S32M27x – eMIOS/TRGMUX/LCU – [RTD600] EMCEM DCM EIM mapping for S32K3x1 S32K3x2 S32K344 S32K324 S32K314  DOC_S32K3x1_S32K3x2_S32K3x4_eMCEM_DCM_Mapping_v1_0_SPD1.0.5_Unofficial    S32K39-37-36   Documents S32K39-37-36 – eMIOS/BTCU/SAR-ADC/DMA – [RTD600] S32K39-37-36 – eFlexPWM/TRGMUX/BCTU/SAR-ADC/DMA – [RTD600]  
查看全文
******************************************************************************** Detailed Description: Configures the FlexCAN 0 to transmit and receive a CAN message Baudrate to is set to 500kbps. In this config, RXFIFO is used to receive a messages. 16 filter elements are defined in the RXFIFO table. Both standard and extended IDs are used. DMA is enabled in component inspector to read RXFIFO. MB10 is moreover used to receive a message with given standard ID and MB11 is used to transmit a message upon button press. The callback function is installed as well and is it called each time message is received in MB10, RXFIFO or message is transmitted. Note: EVB must be powered by 12V to have SBC's CAN transceiver active * ------------------------------------------------------------------------------ * Test HW:        S32K144EVB-Q100 * MCU:            FS32K144UAVLL 0N57U * Target:         Debug_FLASH * EVB connection: PCAN-View with PCAN-USB Pro connected to CAN port J13 * Compiler:       S32DS.ARM.2018.R1 * SDK release:    S32SDK_S32K1xx_RTM_3.0.0 * Debugger:       Lauterbach Trace32 ******************************************************************************** Revision History: Ver    Date           Author          Description of Changes 0.1    Apr-04-2019    Petr Stancik    Initial version *******************************************************************************/
查看全文