S32K知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K Knowledge Base

标签

讨论

排序依据:
Hello everyone, SEGGER's Real Time Transfer (RTT) is the new technology for interactive user I/O in embedded applications. It combines the advantages of SWO and semihosting at very high performance. Bi-directional communication with the target application Very high transfer speed without affecting real-time behavior Uses debug channel for communication No additional hardware or pin on target required Supported by any J-Link model Supported by ARM Cortex-M0/M0+/M1/M3/M4/M7/M23/M33 and Renesas RX100/200/600 Complete implementation code providing functionality and freedom Here, I'd like to share you the SEGGER RTT porting project on S32K144 as attached. SW requirements: S32DS for ARM v2.2 IDE + S32K1xx SDK RTM 3.0 HW requirements: S32K144-EVB  + J-LINK debugger   For SEGGER RTT, you can refer to: About Real-Time Transfer: https://www.segger.com/products/debug-probes/j-link/technology/about-real-time-transfer/   RTT SEGGER Wiki: https://wiki.segger.com/RTT#SEGGER_RTT_TerminalOut.28.29;   Using Segger Real Time Terminal (RTT) with Eclipse: https://mcuoneclipse.com/2015/07/07/using-segger-real-time-terminal-rtt-with-eclipse/   Hope this project can help you, and enjoy the RTT! Best regard, Enwei Hu.
查看全文
Audio Video Bridging(AVB) is a protocol for the transport of audio and video streams over Ethernet-based networks, which makes it possible to deliver high volumes of data in real-time to multiple destinations with very low latency. This reference design board demonstrates the usage for AVB over S32K148. Alternatively, it can be an S32K148 evaluation board of 100pin version besides S32K148EVB-Q144 and S32K148EVB-Q176. Below shows the board layout, diagram, and main features. Figure 1. S32K148AVB-RDB Layout   S32K148AVB-RDB Diagram(Rev B) Figure 2. S32K148AVB-RDB Diagram S32K148AVB-RDB Features Figure 3. S32K148AVB-RDB Features In terms of the software, we provide several examples to show the AVB/TSN usages and other applications. The avb_listener_talker project is the main example which implements most features and demonstrates by connecting 2 AVB boards by Ethernet cable.   Figure 4. S32K148AVB-RDB Code Examples Below software stack and middleware are implemented. ✓ RTOS: FreeRTOS ✓ Peripherial Driver: SDK RTM 3.0 (Work with Processer Expert) ✓ AVB Stream: RTM 1.0 ✓ AVB AudioIf: RTM 1.0 ✓ gPTP Stack Version: 1.3.4 ✓ Lwip Stack Version: 2.1.2 •Note: Even though we did a lot of tests, it’s still the customer’s responsibility to ensure the total quality by themselves when it’s integrated into a real application project, all the sample codes and user guide documentation are just reference for the customer. •Note: We do not have an FCC or CE certificate for this board.   Now we have 50 pcs boards available in Chongqing, China. For applying for the board, please contact NXP sales or GPIS marketing.  Since the AVB stack is not free of use, for accessing the code please contact NXP sales or GPIS marketing. For technical discussion, please contact [email protected] or [email protected].  
查看全文
******************************************************************************************************** Detailed Description: LPUART1 echoes RX signal at 115200 bps When an 's' char is received, the MCU enters VLPS. A falling edge of the RX signal brings the MCU from VLPS via LPUART RXEDGIF interrupt. BUS_CLK can be monitored at CLKOUT PTD14. In VLPS, BUS_CLK is gated off. -------------------------------------------------------------------------------------------------------------------------- Test HW: S32K144EVB-Q100 MCU: S32K 0N57U Debugger: S32DS_ARM_2.2, OpenSDA Target: internal_FLASH ********************************************************************************************************    
查看全文
Hi,      The draft time gap, from power-on to clock output of S32K14x, is as below.    You can take a reference. Cheers! Oliver
查看全文
NXP S32K1xx serial MCU is widely used in automotive body control and many general-purpose automotive applications, while to target some applications with special requirements such as requiring more peripherals instance than the portfolio can offer (e.g. 6x CAN-FD, 6x LIN or 4 I2C) like mid-end BCM or DCU, an on-board dual/multi MCU sync solution is proposed as an alternate solution to extend the S32K1xx MCU peripherals/memory resource and CPU process capability. The eRPC (Embedded Remote Procedure Call) is a Remote Procedure Call (RPC) system created by NXP(https://github.com/EmbeddedRPC/erpc/). An RPC is a mechanism used to invoke a software routine on a remote system using a sample local function call. eRPC software architecture Figure 1. eRPC software architecture In this project, we ported the eRPC protocol to S32K1xx platform, tested and figured out its performance. An out-of-box software package with detailed user guide (this document) is provided to simplify and accelerate users’ assessment of eRPC on S32K1xx. Two S32K144EVB boards are connected to demonstrate the usage of the eRPC protocol. One works as the client, another as the server. The client board starts an eRPC request and the server board responds to the request and executes the service. Figure 2. eRPC task workflow on S32K144-EVB There are three types of MCU extensions are demonstrated in the project: MCU IO extension: Set LED; MCU peripheral extension: CAN and LIN message forwarding, LED luminance regulator; CPU process capability extension: Matrix multiply and addition math operation. Please find the attached sample projects and user guide for more details. Figure 3. Table of Contents in User Guide •Note: Even though we did a lot of tests for the solution with the sample projects on S32K144-EVB, it’s still customer’s responsibility to ensure the total quality by themselves when it’s integrated in a real application project, all the sample codes and user guide documentation are just reference for customer. If you have any questions about this solution, please post here and we can have an open discussion. Best Regard, Enwei Hu(胡恩伟) GPIS System Apps Engineer.  
查看全文
Often we need to implement a SENT receiver in order to read the information sent by some sensors. It is useful to have the possibility of transmitting different message patterns in order to test your implementation. With this project you can transmit via a computer terminal a group of messages (up to 64). The project runs on a S32K144 EVB board, the output signal goes through J206 pin.
查看全文
******************************************************************************** Detailed Description: This example shows SRAM ECC injection. By default, a double-bit ECC error is injected on read access of a location in SRAM_U region. This can be changed with the SRAM_U and DOUBLE_BIT macros. The errors can be detected by both the ERM and MCM modules and the corresponding interrupts can be called. Although only ERM is needed, for demonstration purposes, the MCM interrupt is enabled as well with a lower priority than the ERM interrupts. The ERM interrupts that are called first disable the injection mechanism so that subsequent errors can not be detected during a stack read access. The default S32 Design Studio start_up file copies the vector table to the SRAM_L region. To be able to inject ECC errors in this SRAM region and call the interrupts, the copying is disabled by __flash_vector_table__ symbol  declared in the start_up.h file and defined in the S32K144_64_flash linker file. -------------------------------------------------------------------------------------------- Test HW: S32K144EVB-Q100 MCU: S32K144 0N57U Debugger: S32DSR1 Target: internal_FLASH ********************************************************************************
查看全文
Hi,     I would like to share with you the follow solution for S32K14x which could be attached while couldn't be re-programmed and stopped at RAM initializing.     If you met the issue as title, please check the SIM_CHIPCTL's value in IDE with attach function. Maybe you can find that the value is 0x0, which is not as default value after reset which is 0x0030_0000.     If you check the meaning on SIM_CHIPCTL, you can find that SRAMU and SRAML are retained across resets.  To solute the issue, you should add 'WRITE_LONG=00300000/40048004/ ;' in front of it the algorithm (it's better after reset) of freescale_s32k144f512m15_pflash_dflash_eeprom.arp which is at  'C:\NXP\S32DS_ARM_v20\eclipse\plugins\com.pemicro.debug.gdbjtag.pne_3.3.3.201712132114\win32\gdi\P&E\supportFiles_ARM\NXP\S32K1xx' After that, you can download your project as normal. Cheers! Oliver
查看全文
An example implementation of SENT protocol receiver with S32K118 evaluation board. The input is expected in J106, TICK duration is 2,75us. CRC is calculated and check, the decoded output is printed into terminal via UART (ASCII)
查看全文
Using S32k144 ISELD SDK driver and adding Touch Sensor software, a demo is created to show different light combinations when electrodes of S32K144 EVB are touched. ADK ISELED board is attached to S32K144 EVB.
查看全文
Example of usage of AIPS-lite, Protects the access to GPIO port. This example can be used with UART terminal, 115200 bps. The interface menu shows like this: AIPS example has started Please press 0 + enter to set red LED in GPIO port Please press 1 + enter to set red LED in GPIO port Please press 2: GPIO peripheral will only accept accesses from trusted master, M0 (Core) is set as untrusted when a write access, AIPS cannot longer be modified from core and a reset will occur in the next GPIO access Please press 3: GPIO access is write protected, any write access to GPIO will produce a hard fault
查看全文
Hi,     If you try to compile the sample project within S32K14X_MCAL4_2_RTM_1_0_0, you should take care of the command if you use Linaro.    After you set the environment of compiling and run the command under command window, you should enter     "launch.bat MODE=USER TOOLCHAIN=linaro"    NOT    "launch.bat MODE=USER TOOLCHAIN=LINARO"      The command is case sensitivity.   Hope you can compile the project successfully.  Cheers! Oliver
查看全文
To accelerate S32K demand creation and support urgent evaluation requriement in Great China, we build one batch boards locally. These boards will only be given out to our potential opportunities for free. The boards are made by China local partner and verified by AE and FAE team. if you have any question on this kind of board, please go to China Auto CAS or Auto MCU marketing for support. 1. Board overview   2. Pinout 3. Test point 4. Block diagram 3. The main difference between NXP official S32K EVB and this FRDM-S32K144 board are OpenSDA firmware and CAN PHY The original OpenSDA firmware in this board is from MBED which is not supported by S32DS, thus we need to change to PEmicro OpenSDA firmware, and then we can use S32DS for development.   Unplug the USB cable (if attached). Press and hold the Reset button. Plug in a USB cable from a USB Host to the OpenSDA USB port. Release the RESET/Bootloader button. A removable drive will be visible in the host file system with a volume label of BOOTLOADER. Drag/drop or copy/paste attached firmware “DEBUG-FRDM-K64F_Pemicro_v108a_for_OpenSDA_v2.0.bin” into the removable drive. Unplug the USB cable and plug it in again. The OpenSDA application should now be running. The CAN physical is different. This board used standalone CAN PHY but not CAN SBC. Please refer SCH file for debug.   Original Attachment has been moved to: dmeo2.rar
查看全文
S32Kxxx   Excel configurators MPC5xxx/S32Kxx: CAN / CAN FD bit timing calculation   S32K1/S32M24x   Documents Solution for S32K14x which could be attached while couldn't be re-programmed Fault handling on S32K144 FRDM-S32K144 EVB Useful tips about S32DS for ARM v2018.R1 IDE and S32K1xx development Using S32K CMSIS-SVD Files in EmbSysRegView Eclipse Plugin FlexNVM used as code/data Flash   S32K3/S32M27x   Excel configurators S32K344 DCF Configurator   Debugger plugins Lauterbach FCCU_Utility plugin - S32K3xx    Documents Restrict the debug access with a password when HSE is not used S32K3/S32M27x – eMIOS Usage S32K3/S32M27x – eMIOS/BTCU/ADC/DMA – [RTD600] S32K3/S32M27x – eMIOS/TRGMUX/LCU – [RTD600] DOC_S32K3x1_S32K3x2_S32K3x4_EIM_Mapping_v1_0_SPD105_Unofficial  DOC_S32K3x1_S32K3x2_S32K3x4_eMCEM_DCM_Mapping_v1_0_SPD1.0.5_Unofficial    S32K39-37-36   Documents S32K39-37-36 – eMIOS/BTCU/SAR-ADC/DMA – [RTD600] S32K39-37-36 – eFlexPWM/TRGMUX/BCTU/SAR-ADC/DMA – [RTD600]  
查看全文
Welcome to the S32K Microcontrollers forum. Get expert advice from the NXP developer community. Our support team also monitors these forums to provide answers and take your feedback.   Anyone can read the discussions, but only registered NXP Community members can post questions and comments. Before you ask a question, please search the community to find if someone has already offered a solution. If you don’t see a solution, then ask the community your question. S32K Web page S32K Reference manual S32K Data sheet S32K Application notes and other documents S32K Evaluation Board S32 Design Studio IDE https://community.nxp.com/docs/DOC-334170 
查看全文
******************************************************************************** * Detailed Description: * * This example shows how to use the back-to-back mode of the PDB to trigger * sequence of ADC channels conversion. 4 PDB channel 0 pre-triggers/triggers are * generated upon single PDB SW trigger. The first trigger is started by the PDB, * no delay is used. Next 3 triggers start after corresponding acknowledgment is * received from ADC0. * * Converted data is used to change color of the EVB led based on Trimmer position. * * ------------------------------------------------------------------------------ * Test HW:         FRDM-S32K144 * MCU:             PS32K144HFVLL 0N77P * Fsys:            default * Debugger:        S32DS * Target:          internal_FLASH * ********************************************************************************
查看全文
Hi,        ARM Cortex-M have a DWT (Data Watchpoint and Trace) unit implemented, and it has a nice feature in that unit which counts the execution cycles. The DWT is usually implemented on most Cortex-M3, M4 and M7 devices, including e.g. the NXP S32K14x.      Attachment is the sample project on S32K142 to measure the running time of a function.     Password of extraction is nxp.     Enjoy the measuring!   Cheers! Oliver BTW, Measure the running time of one function on PowerPC could also be gotten through the link.
查看全文
*All of the source code placed is for example use only. Document listed is only for your information only. NXP does not accept liability for use of this code or document in the user’s application. Map: https://bra.in/3vGE9q Resource: My Brain (thebrain.com) Links Community relative for S32K S32K S32DS: S32 Design Studio S32K SDK: S32 SDK S32K Safety: SafeAssure NDA Model-based Design: NXP Model-Based Design Tools Documentation Reference Manual Rev12.1 Data Sheet Rev12 Hardware Design Guide: AN5426, Hardware Design Guidelines for S32K1xx Microcontrollers  (REV 4)  Errata Application Note Tool & Software Design & Solution  S32DS IDE for ARM S32k1: S32 Design Studio IDE for Arm® based MCUs | NXP   S32SDK for ARM S32K1: Automotive S32 SDK for Arm® devices | NXP  Embedded Software Unified Bootloader Framework Unified bootloader stack based on UDS and CAN/LIN TP protocol. AUTOSAR MCAL Tips/FAQ  Safety Process to apply access to Safety Docs and Support: Functional Safety documents AVAILABLE | Require access to the SafeAssure NDA group S32K Safety Enablement: https://community.nxp.com/t5/S32K/S32K-safety-documents-and-demo-code-with-SDK/m-p/1156735#M8231 Hard Fault Fault handling on S32K144  AN12522, S32K1xx ECC Error Handling – Application note  (REV 0) S32K1xx系列MCU的常见内核异常(Fault Exception)及处理详解(以S32K144为例介绍) [FAQ] AUTOSAR MCAL   Where can I find compiler and compiler option info for specific MCAL package? Can I use different compiler version or compiler options for specific MCAL package? Where can I download MCAL package? How to get latest MCAL HF version from your NXP website account if you have already registered and applied MCAL SW package. What does HF(Hot Fix) mean? Can we use it for production? How to calculate current (power consumption) of S32K? S32K Power Estimation Tool (PET) released Enwei Hu 公众号 "汽车电子expert成长之路"原创: 历史文章分类列表目录(点击文章标题直接跳转,截止2020年4月20日)  1. 汽车电子ECU bootloader开发系列 汽车电子ECU bootloader开发要点详解 汽车电子ECU bootloader开发之S32K1xx系列MCU NVM驱动独立安全bootloader开发详解 S32K1xx ECU bootloader开发之RAM NVM驱动(S19文件)生成与集成调用和测试详解 汽车电子ECU bootloader开发之S32K144的CAN bootloader开发详解(工程源代码开源供大家参考) 汽车电子ECU bootloader开发开发之S32K1xx系列MCU bootloader开发要点详解 汽车电子ECU BootLoader开发之基于CAN总线通信的MPC574xP系列MCU bootloader开发详解 汽车电子ECU BootLoader开发之基于CAN总线通信的S12(X) 系列MCU独立NVM驱动安全bootloader  浅谈嵌入式软件开发之Qorivva MPC57xx和S32R系列多核MCU启动配置与bootloader开发要点详解 Qorivva MPC56xx系列MCU启动过程全解析(基于CW IDE应用工程--EAB I、链接文件、启动文件和map文件) 浅谈嵌入式MCU软件开发之startup过程详解(从复位向量到main函数之前的准备工作) 浅谈嵌入式MCU软件开发之S32K1xx系列MCU启动过程及重映射代码到RAM中运行方法详解 CodeWarrior IDE使用Tips之利用prm链接文件实现储存器数据填充和代码编译结果CRC校验和自动生成详解 汽车电子ECU BootLoader开发系列相关文章链接与资源汇总; 2. 浅谈嵌入式MCU软硬件开发系列 浅谈嵌入式MCU开发中的三个常见误区 浅谈嵌入式 MCU 软件开发之应用工程的堆与栈 浅谈嵌入式MCU软件开发之中断优先级与中断嵌套 浅谈嵌入式MCU软件开发之代码风格与代码优化 深入浅出谈嵌入式MCU 内核之ARM Cortex-M系列CPU内核功能特性概述与对比(强烈推荐!!!) 浅谈嵌入式MCU软件开发之内存分配详解--链接文件与map文件中段的分配使用和使用注意事项 浅谈嵌入式MCU硬件设计之MCU最小系统电路 浅谈嵌入式MCU软件开发之startup过程详解(从复位向量到main函数之前的准备工作) 浅谈嵌入式MCU软件开发之S32K1xx系列MCU启动过程及重映射代码到RAM中运行方法详解 浅谈嵌入式MCU软件开发之S32K1xx系列MCU CPU内核性能优化方法详解 浅谈嵌入式软件开发之Qorivva MPC57xx和S32R系列多核MCU启动配置与bootloader开发要点详解 浅谈嵌入式系统软件开发之S32K1xx系列MCU的MPU配置与使用详解 浅谈嵌入式软件开发之MagniV S12Z系列MCU内核Machine Exception异常原理与恢复 浅谈嵌入式软件开发之重定向标准输入输出设备使用printf()函数格式化输出调试信息(基于S32DS IDE和MPC5744P) 浅谈嵌入式MCU软件开发之startup过程详解(在CodeWarrior 5.1 中实现RAM自定义初始化) 嵌入式软件开发之S12(X)系列MCU的far和near函数指针调用详解(S12G128 CW 5.x Project) 浅谈嵌入式MCU软件开发之S12(X)系列MCU 中断ISR在CodeWarrior 5.1 IDE 中的三种写法 浅谈嵌入式软件开发之Qorivva MPC56/57xx系列MCU的Power e200内核寄存器功能和内核调试技巧介绍 嵌入式软件开发之调试器(Debugger)使用--PEMicro Multilink功能介绍与使用FAQ 浅谈嵌入式MCU软件开发之MCU芯片内部Bandgap参考电压(带隙基准)和集成温度传感器的工作原理和使用详解 浅谈嵌入式MCU软件开发之条件断点的设置与使用详解(以S32DS IDE + U-Multink debugger为例介绍) 浅谈嵌入式软件开发之使用Srecord工具实现S19文件数据填充和CRC校验和自动计算与存储方法详解 浅谈嵌入式MCU软件开发之使用makefile脚本编译和调试NXP S32 SDK应用工程详解 3. 外设使用Tips系列 S32K1xx系列MCU使用Tips之SDK软件架构和使用详解 S12(X)系列MCU的片上存储器资源与分页访问机制详解(一) S12(X)系列MCU的片上存储器资源与分页访问机制详解(二) S12(X)系列MCU的加密(Secure)原理和解密(Unsecure)方法 Qorivva MPC56xx系列MCU的Flash加密解密原理与工程实现方法详解 使用 Cyclone 离线编程器对 S12(X)和 MagniV S12Z 系列 MCU 片上 NVM 编程  S32K1xx系列MCU使用Tips--功能介绍及软件开发和硬件设计FAQ  S32K1xx系列MCU使用Tips--Flash加密后不断复位无法连接调试器的问题解决 S32K14x系列MCU使用Tips之硬件FPU特性介绍和使用详解 外设使用Tips之Qorivva MPC56xx_57xx系列MCU内核异常(IVORx)与IRQ中断处理详解 外设使用Tips之Qorivva MPC56xx/57xx系列MCU的模式控制与切换(片上外设资源使能与功耗控制) 外设使用Tips之MCU内部集成IRC时钟工作原理、特性和trim原理及方法详解(以KEA系列MCU的ICS为例) 外设使用Tips之S12G系列MCU Startup之前的复位过程详解(COP看门狗复位和时钟监测复位中断识别与处理)  外设使用Tips之MPC57xx系列MCU C55 Flash模块详解及其SSD(标准软件驱动)使用 外设使用Tips之MSCAN接收ID滤波器设置 外设使用Tips之TIM定时器使用FAQ和使用经验 外设使用Tips之MPC574xP系列汽车级MCU的SWT看门狗定时器配置与使用 NXP汽车MCU开发详解之KEA系列汽车MCU开发指南 S32K1xx系列MCU应用指南之芯片锁死(lockup)复位原因分析与恢复方法详解 关于使用J-LINK开发S32K1xx系列MCU应用程序的使用说明和注意事项 NXP S12G_XE系列汽车MCU软件开发指南 资料分享--S12XE 系列MCU XGATE协处理器开发常见问题(Q&A) S32K1xx系列MCU应用指南之相同封装不同型号(part number)间相互替换的软件与硬件设计注意事项 4. S32K SDK使用详解系列 S32K SDK使用详解之S32 SDK软件编程思想详解 S32K SDK使用详解之S32 SDK软件架构详解 S32K SDK使用详解之Keil MDK开发S32K1xx系列MCU应用程序(使用Processor Expert配置SDK) S32K SDK使用详解之GHS Multi(Eclipse插件)开发S32K1xx系列MCU应用程序(使用PE配置SDK) 浅谈嵌入式MCU软件开发之使用makefile脚本编译和调试NXP S32 SDK应用工程详解 浅谈嵌入式MCU软件开发之S32K1xx系列MCU CPU内核性能优化方法详解 S32DS GNU GCC编译优化选项与配置方法详解及S32 SDK代码编译优化选项设置建议 S32K系列MCU应用开发详解直播ppt高清pdf版本下载与直播视频回放链接 S32DS使用Tips--SDK使用常见问题(FAQ)答疑 S32K SDK使用详解之interrupt_manager组件配置与使用详解 S32K SDK使用详解之Flash驱动组件使用(FTFC Flash控制器功能详解与使用FAQ & Tips) S32K SDK使用详解之PinSettings组件配置与使用详解(S32K1xx PORT 和GPIO模块) 5. S32K1xx应用指南系列 S32K1xx系列MCU的常见内核异常(Fault Exception)及处理详解(以S32K144为例介绍) S32K1xx系列MCU应用指南之芯片锁死(lockup)复位原因分析与恢复方法详解 S32K1xx系列MCU的EEE(Emulated EEPROM)使用详解 S32K1xx系列MCU应用指南之FlexIO和CSEc硬件加密模块的使用详解 S32K1xx系列MCU应用指南之WDOG看门狗模块使用详解 S32K1xx系列MCU应用指南之存储器ECC功能使用详解(一) S32K1xx系列MCU应用指南之存储器ECC功能使用详解(二) S32K1xx系列MCU应用指南之RTC模块使用详解 S32K1xx系列MCU应用开发指南之IAR toolchain样例工程及使用常见问题(FAQ) S32K1xx系列MCU的低功耗实现要点详解(基于S32K144 EVB-Q100x Rev C测试) 6. 细说汽车电子通信总线系列 细说汽车电子通信总线之CAN 2.0 总线协议详解 细说汽车电子通信总线之CAN-FD 总线协议详解 细说汽车电子通信总线之LIN总线协议详解 细说汽车电子通信总线之常见汽车电子串行通信总线(CAN、LIN、DSI、ISO-9141、SWCAN、J 1850)对比 7. S32DS IDE使用Tips系列 S32DS使用Tips--S32DS for Power V1.2 链接文件和启动过程详解 S32K1xx系列MCU使用Tips之SDK软件架构和使用详解 S32DS GNU GCC编译优化选项与配置方法详解及S32 SDK代码编译优化选项设置建议 S32DS IDE使用Tips--应用程序开发实战实用技巧总结与详解(工欲善其事必先利其器) S32DS使用Tips--SDK使用常见问题(FAQ)答疑 S32DS IDE使用Tips--应用工程调试常见问题(FAQ)答疑 S32DS IDE使用Tips之Classic CW(2.10)和EclipseCW(10.x和11.x)应用工程移植指南 S32DS 使用Tips之S32DS for Power不同版本之间的GNU工具链差异与外设寄存器位域访问问题总结 S32DS使用Tips之S32DS for Power v1.1应用工程升级到v1.2重新编译运行程序跑飞问题解决 S32DS 使用tips--S32DS for ARM v1.3工程到S32DS for ARM V2.0迁移升级方法和注意事项 S32DS 使用 tips--工程属性配置(编译选项和C编译器、汇编器及链接器设置) S32DS使用Tips--如何编译生成和调用静态库 S32DS使用Tips--如何通过创建新的编译目标(Build Target)在同一个S32DS工程中同时编译静态库和应用程序 S32DS使用Tips--如何配置和使能Attach功能定位软件程序bug和完成bootloader与应用程序工程的联合调试 CodeWarrior与S32DS IDE使用 Tips之如何在应用工程中保留定义但未使用的全局常量、变量(用于参数标定) S32DS 使用 tips--使用Flash from file下载S19或elf文件 S32DS for ARM v2018.R1安装IAR Eclipse插件调用IAR工具链开发S32K系列MCU应用程序详解 浅谈嵌入式MCU软件开发之条件断点的设置与使用详解(以S32DS IDE + U-Multink debugger为例介绍) S32DS IDE使用Tips之配置objcopy选项生成S3行的S19文件和指定每行S19文件的最大数据长度的方法和步骤详解 8. CodeWarrior IDE使用Tips系列 CodeWarrior IDE使用tips之bug定位绝技--hotsync与attach调试 CodeWarrior IDE使用Tips之Qorivva MPC56xx新建应用工程选项、调试高级选项及下载过程控脚本详解 CodeWarrior IDE使用tips之prm链接文件详解(自定义存储器分区以及自定义RAM数据初始化与在RAM中运行函数) CodeWarrior IDE使用Tips-Qorivva MPC56xx应用工程map文件全解析(CW 2.10/10.x ) CodeWarrior IDE使用tips之map文件详解 CodeWarrior IDE 版本选择与 License功能(feature)和价格,授权形式差异、激活方法与安装使用 答疑解惑之Win10操作系统中CodeWarrior IDE USB dongle  license安装问题解决方法详解 CodeWarrior IDE使用Tips之利用Hiwave读取S12(X)系列MCU片上NVM命令脚本(CW 5.x IDE) CodeWarrior IDE使用Tips-如何编译生成和调用静态库 CodeWarrior与S32DS IDE使用 Tips之如何在应用工程中保留定义但未使用的全局常量、变量(用于参数标定) CodeWarrior IDE使用Tips之如何通过prm文件指定汇编代码函数、全局变量和常量的储存地址 CodeWarrior IDE使用Tips之利用prm链接文件实现储存器数据填充和代码编译结果CRC校验和自动生成详解 CodeWarrior IDE使用Tips之burner工具使用详解(实现不同类型存储器地址间的转换和NVM编程格式文件的输出) CodeWarrior IDE使用Tips--使用burner将elf文件转换生成HEX和BIN文件的方法和步骤详解 CodeWarrior IDE使用Tips之利用Hiwave读取S12(X)系列MCU片上NVM命令脚本(CW 5.x IDE) S32DS IDE使用Tips之Classic CW(2.10)和EclipseCW(10.x和11.x)应用工程移植指南 9.   汽车ECU参数标定系列 汽车ECU参数标定之配置e200系列CPU内核MMU实现Qorivva MPC56xx_57xx系列MCU的参数在线实时标定 汽车ECU参数标定之配置Overlay RAM实现Qorivva MPC57xx系列MCU参数在线标定和代码重映射原理和方法详解 CodeWarrior IDE使用Tips之如何通过prm文件指定汇编代码函数、全局变量和常量的储存地址 CodeWarrior与S32DS IDE使用 Tips之如何在应用工程中保留定义但未使用的全局常量、变量(用于参数标定) CodeWarrior IDE使用tips之prm链接文件详解(自定义存储器分区以及自定义RAM数据初始化与在RAM中运行函数) CodeWarrior IDE使用tips之map文件详解 S32DS使用Tips--S32DS for Power V1.2 链接文件和启动过程详解 10.  工欲善其事必先利其器系列 工欲善其事必先利其器之NXP汽车MCU系列产品家族(Family)功能特性及应用介绍 工欲善其事必先利其器之NXP汽车MCU开发资料和开发软件获取与使用指南 11.  答疑解惑系列 疑难答疑之S12G系列MCU使用Hiwave和BDM调试器debug时无法使用逻辑地址查看和保存P-flash问题的解决 疑难答疑之S32DS IDE调试启动过程详解与调试目标复位方法和步骤详解 答疑解惑之S12(X)系列MCU的CodeWarrior 5.x应用工程下载调试过程详解以及如何保护NVM存储器不被擦除 答疑解惑之Win10操作系统中CodeWarrior IDE USB dongle  license安装问题解决方法详解 12. 产线批量Flash编程与ESD/EOS保护系列 使用 Cyclone 离线编程器对 S12(X)和 MagniV S12Z 系列 MCU 片上 NVM 编程 使用Cyclone 离线编程器对S32K1系列MCU进行NVM(P-Flash, D-Flash和EEE)编程的方法与步骤详解 13.  其他 汽车电子expert成长之路微信公众号原创技术分享文章全集-2019年度精编版 汽车电子expert成长之路微信公众号原创技术分享文章集合2017~2018年 最新最全的NXP Techday和Connect(原Freescale FTF)技术培训资料下载链接 汽车以太网(100BASE-T1)转工业以太网(100BASE-TX)转换器工作原理介绍 使用关键词回复功能找到感兴趣的公众号原创技术文章    
查看全文
********************************************************************************  Detailed Description:  Example shows how to use FlexCAN 0 Pretended networking mode to allow FlexCAN  module to wake up MCU from STOP mode using SDK.  Wake up by Timeout and wake up by Match events are enabled.  Also pin interrupt can be used to exit STOP mode.  So MCU enters STOP mode by pressing SW3 button.  MCU exits STOP mode when one of following happens:  - no CAN message comes in 8sec (CAN PN timeout event)  - message with standard ID 0x554 or 0x555 comes (CAN PN match event)  - SW2 button is pressed (PTC12 interrupt)  In run mode blue LED is dimming and the rate is different for each wakeup event  ------------------------------------------------------------------------------  Test HW: S32K116EVB-Q48  MCU: PS32K116LAM 0N96V  Compiler: S32DS.ARM.2.2  SDK release: S32SDK_S32K1xx_RTM_3.0.0  Debugger: Lauterbach, OpenSDA  Target: internal_FLASH ********************************************************************************
查看全文
Greetings, if you want to use the open source EmbSysRegView plugin in your Eclipse environment: this article describes how to add the S32K CMSIS-SVD files to it: Adding CMSIS-SVD Files to EmbSysRegView 0.2.6.r192 and Eclipse Happy SVDing 🙂 Erich
查看全文