S32K Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K Knowledge Base

Labels

Discussions

Sort by:
*********************************************************************************** * Detailed Description: * The example locks * PFC PFCBLK2_SSPELOCK REG_PROT soft lock * and PFC REG_PROT hard lock. * ------------------------------------------------------------------------- * Test HW: : S32K344EVB-Q172 * MCU: : S32K344 * Project : RTD AUTOSAR 4.7 * Platform : CORTEXM * Peripheral : S32K3XX * Dependencies : none * * Autosar Version : 4.7.0 * Autosar Revision : ASR_REL_4_7_REV_0000 * SW Version : 5.0.0 * Build Version : S32K3_RTD_5_0_0_D2408_ASR_REL_4_7_REV_0000_20241002 ***********************************************************************************
View full article
This article has been moved to a new location: https://community.nxp.com/t5/S32M-Knowledge-Base/S32M2xx-Motor-control-use-cases/ta-p/2039790
View full article
This is an example project which is created to do an internal wake up from VLPS mode using LPTMR0.   From S32KRM, it tells us that internal wakeup is achievable using LPTMR0.     What code does? ======================================= 1) LPTMR0 is configured for 5 Seconds. So for interrupt occurs for every 5 seconds 2)LPTMR0  wakes up MCU for every 5 seconds and again it goes back to sleep for next 5 seconds. This cycle repeats forever. 3) When MCU is in RUN mode, GREEN color LED will be ON and it will in OFF if it goes to VLPS.   Project Configurations: =======================================     Other Informations: ======================================= Design studio: S32DS3.4 SDK                    : RTM 4.0.2 EVB                     : S32K118EVB2Q048   Note:   Following symbols should be included if you are creating the project from scratch to properly put MCU to sleep and wakeup from POR.   Thanks & regards, Krishnakumar V
View full article
【RTD400 MCAL 3】 K312 MCU clock system configuration 1. Abstract This document is talking about how to configure the clock system in the MCU of the K3 chip MCAL. This topic was always disdainful to talk about when I was doing LLD before, because the clock system of K3 is too simple, with internal fast and slow clock sources, external fast and slow clock sources, a PLL multiplier, and then various core peripherals to share. K3's RM even made a few options to frame the rules. From the perspective of LLD, especially the perspective of S32DS CT configuration, it is even more concise and clear. Here is a CT picture to show it:   Fig 1     Fig 2 With such a clock system, you can generate code with just a few taps and pokes. However, LLD is too free, and MCAL often encounters problems. Therefore, I decided to spend some time to understand the entire clock system of this MCAL MCU. This article takes K312 as an example to explain. Other K3 series are similar. 2. Clock system theory and configuration 2.1 K312 clock system From the clock chapter of RM, you can see the whole system block diagram:     Fig 3 This block diagram clearly shows the situation of each part. There are four clock sources: Internal fast clock FIRC: 48MHz, +/-5% error, maximum startup time 25us Internal slow clock SIRC: 32KHz, +/-10% error, maximum startup time 3ms External fast clock FXOSC: 8-40MHz, startup stabilization time FXOSC_CTRL[EOCV] × 128 External slow clock SXOSC: 32.768KHz, startup stabilization time SXOSC_CTRL[EOCV] x 128 One PLL: input 8-40MHZ, VOC output 640M-1280Mhz, PLL_PHIn_CLK output 25-480MHz. MUX_0: Output CORE_CLK, AIPS_PLAT_CLK, AIPS_SLOW_CLK, HSE_CLK, DCM_CLK MUX_1: Output system timer STM0_CLK MUX_3: Output FLEXCAN0-2 clock MUX_4: Output FLEXCAN3-5 clock MUX_5: Output CLKOUT_STANDBY MUX_6: Output CLKOUT_RUN MUX_11: Output TRACE_CLK RTC_CLK: RTC clock 2.1.1 PLL From the PLL perspective, we need to know which values ​​the frequency multiplier is related to, which can be calculated using the following formula:     Fig 4 If it is an integer, the red box in the above figure is the common method, and this article will also use the above method to configure. PLL_PHI is the clock output by the final PLL, which is provided to the MC corresponding to other MUXs for selection. 2.1.2 MUX_0 System The MUX_0 system with details can be seen from RM:     Fig 5 As you can see, the clock source of MUX_0 can be two types: PLL or internal FIRC. Then the core clock can be generated later, AIPS_PLAT_CLK, AIPS_SLOW_CLK, HSE_CLK, DCM_CLK. So what is the specific frequency of the generated clock? In principle, it can meet the maximum clock corresponding to each module, but the K3 series also makes some option recommendations. For example, K312 recommends using option B mode when RUN, especially the HSE clock, which usually needs to strictly meet the option recommendation. 2.1.3 MUX_6 Clock output In order to check the corresponding clock situation in the chip, the corresponding clock can be output through the CLKOUT pin. The CLKOUT pin can correspond to the selection of multiple clock sources. The specific situation is as follows:     Fig 6 The yellow content in the figure is what K312's CLKOUT_RUN can support. After the clock is configured, the corresponding clock will be selected to test whether the output is consistent with the configuration. 2.1.4 option B Recommended Solution In this article, K312 will configure the clock of option B in EB.     Fig 7 2.2 EB configuration        First, create a new K312 EB project. For the specific creation method, please refer to the previous article: [S32K3 Tools Part] How to port RTD's existing MCAL demo to other K3 chips This article will focus on the clock configuration corresponding to the MCU module based on RTD400 MCAL. For MCU configuration, two documents need to be consulted as reference books: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Mcu_TS_T40D34M40I0R0\doc: RTD_MCU_UM.pdf and RTD_MCU_IM.pdf If you don’t know how to configure, just follow the default values ​​recommended by the document. The following figure is an overview of the MCU. The main configured modules have the following three components: General, McuClockSettingConfig, McuModeSettingConf     Fig 8 2.2.1 General configuration In addition to Figure 8, you need to turn on the internal and external fast and slow clock control and PLL control, and add the corresponding API, as well as the crystal oscillator frequency. If this is not turned on, the corresponding configuration later will not be able to be configured.     Fig 9 2.2.2 McuClockSettingConfig configuration        This is the core area of ​​MCU clock configuration, which includes clock source, PLL, and various MUX conditions. First, you need to add a clock configuration:     Fig 10 Click in and there will be detailed configuration:     Fig 11 There are 17 items in total. You can keep the default configuration for options 1 and 6. Since the board does not connect to the external slow crystal oscillator 5, it is not configured. The rest should be configured according to the actual situation. The following explains them one by one: 2.2.2.1 McuFIRC configuration    Internal fast clock, 48MHz:     Fig 12 2.2.2.2 McuSIRC configuration Internal slow clock 32Khz     Fig 13 2.2.2.3 McuFXOSC configuration External crystal oscillator 16MHZ, fill in according to the actual connection situation.     Fig 14 2.2.2.4 McuCgm0ClockMux0 configuration Mux0 configuration, here are configured core clock, AIPS_PLAT_CLK, AIPS_SLOW_CLK, HSE, DCM_CLK, is to meet the optionB requirements, and the clock comes from PLL_PHI0_CLK. When actually configuring, first configure the PLL clock to output the correct PLL_PHI0_CLK, PLL_PHI1_CLK clock.     Fig 15 2.2.2.5 McuCgm0ClockMux1 configuration     Fig 16 It can be configured according to the clock source required by the actual module. 2.2.2.6 McuCgm0ClockMux3 configuration Configure the clock source of the FLEXCAN0-2 module:     Fig 17 2.2.2.7 McuCgm0ClockMux4 configuration Configure the clock source of the FLEXCAN3-5 module:     Fig 18 2.2.2.8 McuCgm0ClockMux5 configuration Configure the clock source of the CLKOUT_STANBY module:     Fig 19 2.2.2.9 McuCgm0ClockMux6 configuration Configure the clock source of the CLKOUT_RUN module     Fig 20 2.2.2.10 McuCgm0ClockMux11 configuration Configure the clock source of the TRACE_CLK module     Fig 21 2.2.2.11 McuRtcClockSelect configuration Configure the clock source of the RTC module     Fig 22 2.2.2.12 McuPLL configuration Configure the clock source of the PLL module     Fig 23 2.2.2.13 McuClockReferencePoint configuration Configure the reference clock and the clock source selection interface of the peripheral modules.     Fig 24 At this point, the clock configuration is complete. For verification, you can use the CLKOUT_RUN output to output the corresponding clock to pin PTD10 for viewing. 2.2.3 McuModeSettingConf  configuration In Mcu's McuModeSettingConf->McuPeripheral, you need to turn on the peripherals you want to use:     Fig 25 2.2.4 PORT  configuration Because the internal clock needs to be output to CLKOUT_RUN, K312's PTD10 MSCR106 is checked, so the PORT pin is added as follows:     Fig 26 3. Test Result Next, on the S32K312-EVB board, we modify the clock source of EB's CLKOUT_RUN to test whether the clock matches the configuration. Commonly used MCU-related drivers are as follows:     Fig 27 The calling sequence of system startup MCU initialization is as follows: 1). Mcu_Init() 2). Mcu_InitClock() 3). Mcu_GetPllStatus() - Till PLL is locked. 4). Mcu_DistributePllClock() 5). Mcu_SetMode() 6). Mcu_InitRamSection() - If required The corresponding main code is as follows: #include "Mcu.h" #include "Mcu_Cfg.h" #include "Port.h" #include "Dio.h" #include "Port_Cfg.h" #include "Platform.h" void TestDelay(uint32 delay); void TestDelay(uint32 delay) { static volatile uint32 DelayTimer = 0; while(DelayTimer < delay) { DelayTimer++; } DelayTimer = 0; } /** * @brief Main function of the example * @details Initialize the used drivers and uses the Icu * and Dio drivers to toggle a LED on a push button */ int main(void) { uint8 count = 0U; uint8 u8TimeOut = 100U; /* Initialize the Mcu driver */ #if (MCU_PRECOMPILE_SUPPORT == STD_ON) Mcu_Init(NULL_PTR); #elif (MCU_PRECOMPILE_SUPPORT == STD_OFF) Mcu_Init(&Mcu_Config_VS_0); #endif /* (MCU_PRECOMPILE_SUPPORT == STD_ON) */ /* Initialize the clock tree and apply PLL as system clock */ Mcu_InitClock(McuClockSettingConfig_0); #if (MCU_NO_PLL == STD_OFF) while ( MCU_PLL_LOCKED != Mcu_GetPllStatus() ) { } Mcu_DistributePllClock(); #endif /* Apply a mode configuration */ Mcu_SetMode(McuModeSettingConf_0); /* Initialize all pins using the Port driver */ Port_Init(NULL_PTR); /* Initialize Platform driver */ Platform_Init(NULL_PTR); while (count++ < 10) { Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED_Q172, STD_HIGH); Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED_Q257, STD_HIGH); TestDelay(5000000); Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED_Q172, STD_LOW); Dio_WriteChannel(DioConf_DioChannel_Digital_Output_LED_Q257, STD_LOW); TestDelay(5000000); } // Exit_Example(TRUE); return (0U); } #ifdef __cplusplus } #endif 3.1 CLKOUT FIRC_CLK DIV2     Fig 28 It can be seen that the original 48Mhz clock of FIRC is divided by 2 and the clock waveform of 24Mhz is obtained, which is correct! 3.2 CLKOUT SIRC_CLK DIV2     Fig 29 It can be seen that the original 32Khz clock of SIRC is divided by 2 and the clock waveform of 16khz is obtained, which is correct! 3.3 CLKOUT FXOSC_CLK DIV10     Fig 30 It can be seen that the original 16Mhz clock of FXOSC is divided by 10 and the clock waveform of 1.6Mhz is obtained. 3.4 CLKOUT PLLPH0 CLK DIV10     Fig 31 It can be seen that the original 120Mhz clock of PLLPH0 is divided by 10 and the 12Mhz clock waveform is obtained, which is correct. 3.5 CLKOUT CORE CLK DIV10     Fig 32 It can be seen that the original 120Mhz clock of CORE is divided by 10 and the 12Mhz clock waveform is obtained, which is correct. 3.6 CLKOUT PLLPH1 CLK DIV4     Fig 33 It can be seen that the original 48Mhz clock of PLLPH1 is divided by 4 and the 12Mhz clock waveform is obtained. 3.7 CLKOUT HSE CLK DIV10     Fig 34 It can be seen that the original 60Mhz clock of HSE is divided by 10 and the clock waveform of 6Mhz is obtained, which is correct. 3.8 CLKOUT AIPS_PLAT CLK DIV10     Fig 35 It can be seen that the original 60Mhz clock of AIPS_PLAT_CLK is divided by 10 and the clock waveform of 6Mhz is obtained, which is correct. 3.9 CLKOUT AIPS_SLOW CLK DIV10     Fig 36 It can be seen that the original 30Mhz clock of AIPS_SLOW_CLK is divided by 10 and the clock waveform of 3Mhz is obtained, which is correct.  
View full article
Hi team, First let me explain about the code about what it does. ======================================= 1) From POR, LED  starts blinking - In this state RTC won't be initialized. 2) Once SW5 is pressed in S32K312 EVB - RTC will be initialized before MCU goes to sleep. 3) RTCCNT will be incrementing during sleep  4) Once SW6 is pressed , MCU wakes from the sleep and we could able see the updated RTC time and date. WAR(Work Around)done to keep RTC alive during sleep: ======================================= Tried to test the RTC with sleep mode, observed that RTCCNT value is getting reset once after every wakeup. So that time and date was not able to preserve the value. In order to avoid this, I have done two workarounds to solve this RTCCNT value reset issue. 1) RTC will not be initialized for if MCU wakeup from the sleep - Made the check to initialize when MCU is not from the wakeup before it goes to sleep. wake_up_event will be incremented if MCU reset reason is wakeup as shown below.   2) Updating "Rtc_Ip_u32ChState" array variable for "ticksPerSecond" member in "Rtc_Ip.c" file manually after the code generation is completed.  Note: With auto generated code the value of "ticksPerSecond "will be "0".    Any other alternatives other than this approach is highly appreciated. Thanks in advance!  
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the  LPSPI IP Driver for the S32K3xx MCU.  The example uses LPSPI2 for transmit & receive Twelve bytes using the DMA. This above mentioned operation is performed 10 times continuously MOSI MISO connected on Hardware in loopback.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** For S32K312, please use this correct clock HSE to AIPS clock should be ½. Please make these changes in the below all example code clock setting. HSE clock to 60 MHZ.     Use this MACRO to enable disable the non cacheable region variable placement :--          
View full article
******************************************************************************************** * Test HW: S32K311 EVB-Q100 * MCU: S32K311 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************************** The purpose of this demo application is to enter the standby mode and waking up from sleep using the user button. =============== How this DEMO works ========== 1) once the image is flashed, the application starts running and BLUE LED blinks for every one second during RUN mode 2) Once SW5 in EVB is pressed, MCU enters the SLEEP mode and it turns off BLUE LED & PIT 3) To Wakeup: Press SW4 in EVB 4) Once it returns to normal mode, BLUE LED and PIT starts running. Used pins: ========= PTC11 -> SW5 -> EnterStandby PTA8 -> SW4 -> WakeupFromSleep PTB8 -> D12   -> Blue led  
View full article
The purpose of this demo application is to show you the usage of the FlexCAN module configured to use CAN FD and Enhance RXFIFO using the S32 RTD API. - This demo application requires two boards, or single board connected with CAN tool. - CAN FD is enabled with bitrate 500/2000 kbps - MB0 is configured to transmit either std. or ext ID - MB1 is configured to receive ext ID 0xFACE and MB2 to receive std ID 0x1 - Enhanced RXFIFO is enabled and 3 enhanced RXFIFO filter elements (filter + mask scheme) are defined ext ID 0xABCD with mask 0x1FFFFFFF std ID 0x123 with mask 0x7FF std ID 0x456 with mask 0x7FF - DMA is used to read enhanced RXFIFO, watermark is set to 5 - Callback function is used as well to handle TX and RX process in MBs and Enhanced RXFIFO after DMA complete 5 reading of RXFIFO  ------------------------------------------------------------------------------  Test HW: S32K3444EVB-Q172  MCU: PS32K344EHVPBS 1P55A  Compiler: S32DS.ARM.3.5  SDK release: S32K3_RTD_4_0_0_D2311  Debugger: Lauterbach  Target: internal_FLASH
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the  LPSPI IP Driver for the S32K3xx MCU.  The example uses LPSPI2 for transmit & receive Twelve bytes using the SPI Interrupt Lpspi_Ip_AsyncTransmit() method . MOSI MISO connected on Hardware in loopback.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Interrupt Triggered :-- Async callback triggered at the end of transfer/reception :-- Lpspi_Ip_AsyncTransmit(&MASTER_EXTERNAL_DEVICE, txBuffer, rxBuffer, numberOfBytes, lpspi_callback_int);      
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the  LPSPI IP Driver for the S32K3xx MCU.  The example uses LPSPI2 for transmit & receive Twelve bytes using the SPI polling Lpspi_Ip_SyncTransmit() method. MOSI MISO connected on Hardware in loopback.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************    
View full article
 ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** Example MCAL S32K312 MEM_InFls  DS3.5 RTD300 :-- Example MCAL S32K312 MEM_InFls DS3.5 RTD300 - NXP Community Example MCAL S32K312 FEE DS3.5 RTD300 :-- Example MCAL S32K312 FEE DS3.5 RTD300 - NXP Community Example MCAL S32K312 FEE and MEM_InFls DS3.5 RTD300 :-- Example MCAL S32K312 FEE and MEM_InFls DS3.5 RTD300 - NXP Community Example MCAL S32K312 PWM ICU using Custom IRQ EMIOS DS3.5 RTD300 :-- Example MCAL S32K312 PWM ICU using EMIOS DS3.5 RTD300 - NXP Community Example ASR S32K312 EMIO PWM Generation & Duty capture using Interrupt DS3.5 RTD300 :-- Example ASR S32K312 EMIO PWM Generation & Duty capture using Interrupt DS3.5 RTD300 - NXP Community  Example ASR S32K312 EMIO PWM Generation & Duty capture using Polling DS3.5 RTD300 :-- Example ASR S32K312 EMIO PWM Generation & Duty capture using Polling DS3.5 RTD300 - NXP Community
View full article
******************************************************************************* The purpose of this demo application is to present a usage of the EMIOS IP Driver in Interrupt mode for the S32K3xx MCU. The example use to :-- EMIOS-1 - ch-0  --> PTC24 --> Generate the PWM EMIOS-1 - ch-1  --> PTC25 --> is the ICU channel to measure the duty Pins used :--     This example is tested for SAIC & IPWM mode both. You can change the mode by this setting in MEX file :--     Difference between SAIC & IPWM,  ICU Driver User Manual :--   These Two Macro :-- SAIC_MODE  --> this maco will enable variables to store for SAIC mode CUSTOM_IRQ  --> this MACRO will enable customized IRQ or RTD available IRQ   Result :--     Sometimes Compiling error comes, in Autogenerated RTD file.    Change the Header file name :--    ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
View full article
******************************************************************************* The purpose of this demo application is to present a usage of the EMIOS IP Driver in Polling mode for the S32K3xx MCU. The example use to :-- EMIOS-1 - ch-0  --> PTC24 --> Generate the PWM EMIOS-1 - ch-1  --> PTC25 --> is the ICU channel to measure the duty Pins used :--     This example is tested for IPWM mode .  :--       IPWM mode ,  ICU Driver User Manual :--   Result :-- Sometimes Compiling error comes, in Autogenerated RTD file.    Change the Header file name :--      ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the ICU & PWM MCAL Driver for the S32K3xx MCU. This example uses the custom IRQ. The example uses:-- EMIOS-1 - ch-0  --> PTC24 --> Generate the PWM EMIOS-1 - ch-1  --> PTC25 --> is the ICU channel to measure the duty       Result :--      ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
View full article
******************************************************************************* The purpose of this demo application is to present a usage of the EMIOS IP Driver in Polling mode for the S32K3xx MCU. The example use to :-- EMIOS-1 - ch-0  --> PTC24 --> Generate the PWM EMIOS-1 - ch-1  --> PTC25 --> is the ICU channel to measure the duty Pins used :--     This example is tested for IPWM mode .  :--       IPWM mode ,  ICU Driver User Manual :--   Result :--    ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
View full article
******************************************************************************* The purpose of this demo application is to present a usage of the EMIOS IP Driver in Interrupt mode for the S32K3xx MCU. The example use to :-- EMIOS-1 - ch-0  --> PTC24 --> Generate the PWM EMIOS-1 - ch-1  --> PTC25 --> is the ICU channel to measure the duty Pins used :--     This example is tested for SAIC & IPWM mode both. You can change the mode by this setting in MEX file :--     Difference between SAIC & IPWM,  ICU Driver User Manual :--   These Two Macro :-- SAIC_MODE  --> this maco will enable variables to store for SAIC mode CUSTOM_IRQ  --> this MACRO will enable customized IRQ or RTD available IRQ   Result :--    ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the EMIOS IP Driver for the S32K3xx MCU. This example uses the custom IRQ.  The example uses:-- EMIOS-1 - ch-0  --> PTC24 --> Generate the PWM EMIOS-1 - ch-1  --> PTC25 --> is the ICU channel to measure the duty           Result :--        ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the FEE MCAL Driver for the S32K3xx MCU. This example read & write 4 byte FEE BLock. I have renamed the FEE block using a MACRO as FOUR_BYTE_EEPROM_FEE_VARIABLE.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Driver configuration :--   Three FEE blocks are created. Each FEE block can be considered as EEPROM variables    How customer can use FEE block as EEPROM variable. Max size of FEE block :--     You can declare a MACRO for the Variable of EEPROM :-- FOUR_BYTE_EEPROM_FEE_VARIABLE How to Read and write the FEE variables :--  
View full article
  1. Abstract This article also explains the S32DS+EB configuration, RTD400. The MCAL training of other modules will be based on this structure in the future. However, this article will provide a command line version of the code. If you need the command line mode, you can directly copy one under the RTD MCAL code package and use VScode to compile it. The hardware of this article is based on K312-miniEVB, and the board situation is as follows:      Fig 1 Function: In the K312 MCAL code, the UART transceiver function is implemented using DMA. Since RTD400 does not have K312 routines, there is also a process of porting from RTD400 to K312 MCAL. Of course, the previous article has explained it very clearly, and also provided the S32DS project template. This article will be based on the previous S32DS EB project template.  2. Function Implementation 2.1 K312 MINIEVB hardware configuration For the hardware configuration, since this article only uses UART, the structure is very simple, using the pins: LPUART3_TX: PTD2 LPUART3_RX: PTD3 and an external TTL-USB tool to achieve signal communication. 2.2 EB Configuration     Here we list all the modules used in EB tresos related to this article, and focus on the modules that require specific configuration. Fig 2 2.2.1 Mcl module The Dma Logic Channel interface needs to be configured. The main purpose is to configure two DMA channels for LPUART3_TX and RX. (1)dmalogicChannel_Type_0 Fig 3 (2)dmalogicChannel_Type_2 Fig 4 The callback registered here can also be called directly in the code. 2.2.2 Mcu module Mcu->McuClockSettingConfig->McuClockReferencePoint->Lpuart3_clk Fig 5 In fact, it configures the clock source frequency of LPUART to 24Mhz, which comes from AIPS_SLOW_CLK. 2.2.3 Platform module Platform->Interrupt Controller->IntCtrlConfig,Configure 3 channels: Fig 6 Here we only need to pay attention to the LPUART3 interrupt, as well as the DMA0 channel 6 and channel 7 interrupts, because these two DMA channels are configured for UART TX and RX. FlexIO is ignored, it is just a matter of whether it is deleted in the original routine. 2.2.4 Port module Port->PortContainer, add PTD2,PTD3 pins: Fig 7 Fig 8 2.2.5 Uart module There are two places to configure: (1)uart->General Fig 9 (2)uart->uartChannel Fig 10 There are 4 points to note here: Point 1: Select the clock source configured in the mcu Point 2: Configure the baud rate to 115200 Point 3: Select the asynchronous mode as DMA Point 4: Select the two DMA channels configured in the mcl, and you need to match TX and RX to the corresponding DMA channels. 2.2.6 Rm module Rm->DMA MUX Configure 2 DMA_MUX channels: Fig 11 Fig 12 2.3 main code     #include "Mcl.h" #include "Mcu.h" #include "CDD_Uart.h" #include "CDD_Rm.h" #include "Port.h" #include "Platform.h" #include "Lpuart_Uart_Ip_Irq.h" #include "Flexio_Uart_Ip_Irq.h" //#include "check_example.h" #include <string.h> #include "Port_Cfg.h" #define UART_LPUART_INTERNAL_CHANNEL 0U #define UART_FLEXIO_TX_CHANNEL 1U #define UART_FLEXIO_RX_CHANNEL 2U /* Welcome messages displayed at the console */ #define WELCOME_MSG "MCAL UART DMA Helloworld for automotive with S32K312!\r\n" /* Error message displayed at the console, in case data is received erroneously */ #define ERROR_MSG "An error occurred! The application will stop!\r\n" /* Length of the message to be received from the console */ #define MSG_LEN 50U #define UART_BUFFER_LENGTH ((uint32)10U) Std_ReturnType T_Uart_Status; //uint8 Rx_Buffer[UART_BUFFER_LENGTH]; #define UART_START_SEC_VAR_CLEARED_UNSPECIFIED_NO_CACHEABLE #include "Uart_Memmap.h" __attribute__(( aligned(32) )) uint8 Rx_Buffer[UART_BUFFER_LENGTH]; #define UART_STOP_SEC_VAR_CLEARED_UNSPECIFIED_NO_CACHEABLE #include "Uart_Memmap.h" uint32 g_Uart_CallbackCounter = 0U; uint32 g_DmaCh16_ErrorCallbackCounter = 0U; uint32 g_DmaCh17_ErrorCallbackCounter = 0U; //void Uart_Callback (void); void Uart_Callback(const uint8 HwInstance, const Lpuart_Uart_Ip_EventType Event, void *UserData); void Mcl_DmaCh16_ErrorCallback (void); void Mcl_DmaCh17_ErrorCallback (void); void Uart_Callback(const uint8 HwInstance, const Lpuart_Uart_Ip_EventType Event, void *UserData) { if(Event == LPUART_UART_IP_EVENT_END_TRANSFER) { __asm volatile ("nop"); __asm volatile ("nop"); __asm volatile ("nop"); __asm volatile ("nop"); __asm volatile ("nop"); __asm volatile ("nop"); } else if (Event == LPUART_UART_IP_EVENT_TX_EMPTY) { __asm volatile ("nop"); __asm volatile ("nop"); } else if (Event == LPUART_UART_IP_EVENT_RX_FULL) { __asm volatile ("nop"); } else if (Event == LPUART_UART_IP_EVENT_ERROR) { __asm volatile ("nop"); } else { __asm volatile ("nop"); } } void Mcl_DmaCh6_ErrorCallback (void) { g_DmaCh16_ErrorCallbackCounter++; } void Mcl_DmaCh7_ErrorCallback (void) { g_DmaCh17_ErrorCallbackCounter++; } boolean User_Str_Cmp(const uint8 * pBuffer1, const uint8 * pBuffer2, const uint32 length) { uint32 idx = 0; for (idx = 0; idx < length; idx++) { if(pBuffer1[idx] != pBuffer2[idx]) { return FALSE; } } return TRUE; } /** * @brief Main function of the example * @details Initializez the used drivers and uses the Icu * and Dio drivers to toggle a LED on a push button */ int main(void) { Std_ReturnType UartStatus = E_NOT_OK; uint32 RemainingBytes; uint32 Timeout = 0xFFFFFF; Uart_StatusType UartReceiveStatus = UART_STATUS_TIMEOUT; Uart_StatusType UartTransmitStatus = UART_STATUS_TIMEOUT; /* Initialize the Mcu driver */ Mcu_Init(NULL_PTR); Mcu_InitClock(McuClockSettingConfig_0); Mcu_SetMode(McuModeSettingConf_0); /* Initialize Mcl module */ Mcl_Init(NULL_PTR); /* Initialize Rm driver for using DmaMux*/ Rm_Init (NULL_PTR); /* Initialize all pins using the Port driver */ Port_Init(NULL_PTR); /* Initialize IRQs */ Platform_Init(NULL_PTR); /* Initializes an UART driver*/ Uart_Init(NULL_PTR); T_Uart_Status = Uart_AsyncSend(UART_LPUART_INTERNAL_CHANNEL, (const uint8 *)WELCOME_MSG, strlen(WELCOME_MSG)); if (E_OK == T_Uart_Status) { do { /* Get transmission status */ UartTransmitStatus = Uart_GetStatus (UART_LPUART_INTERNAL_CHANNEL, &RemainingBytes, UART_SEND); } while (UART_STATUS_NO_ERROR != UartTransmitStatus && 0 < Timeout--); Timeout = 0xFFFFFF; UartTransmitStatus = UART_STATUS_TIMEOUT; } for(;;) { /* Receive data from the PC - Get 10 bytes in total */ UartStatus = Uart_AsyncReceive (UART_LPUART_INTERNAL_CHANNEL, Rx_Buffer, UART_BUFFER_LENGTH); if (E_OK == UartStatus) { do { /* Get receive status */ UartReceiveStatus = Uart_GetStatus (UART_LPUART_INTERNAL_CHANNEL, &RemainingBytes, UART_RECEIVE); } while (UART_STATUS_NO_ERROR != UartReceiveStatus && 0 < Timeout--); Timeout = 0xFFFFFF; UartReceiveStatus = UART_STATUS_TIMEOUT; } UartStatus = E_NOT_OK; /* Send data to the PC - Echo back the received data */ UartStatus = Uart_AsyncSend (UART_LPUART_INTERNAL_CHANNEL, Rx_Buffer, UART_BUFFER_LENGTH); if (E_OK == UartStatus) { do { /* Get transmission status */ UartTransmitStatus = Uart_GetStatus (UART_LPUART_INTERNAL_CHANNEL, &RemainingBytes, UART_SEND); } while (UART_STATUS_NO_ERROR != UartTransmitStatus && 0 < Timeout--); Timeout = 0xFFFFFF; UartTransmitStatus = UART_STATUS_TIMEOUT; } UartStatus = E_NOT_OK; } Uart_Deinit(); Mcl_DeInit(); // Exit_Example((T_Uart_Status1 == E_OK) && (T_Uart_Status2 == E_OK)); return (0U); }     It should be noted here that according to RTD C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Uart_TS_T40D34M40I0R0\doc的RTD_UART_IM.pdf, RTD_UART_UM.pdf. Fig 13 When doing DMA transfer, the buffer needs to be placed in the noncacheable area. That's why this article is:     #define UART_START_SEC_VAR_CLEARED_UNSPECIFIED_NO_CACHEABLE #include "Uart_Memmap.h" __attribute__(( aligned(32) )) uint8 Rx_Buffer[UART_BUFFER_LENGTH]; #define UART_STOP_SEC_VAR_CLEARED_UNSPECIFIED_NO_CACHEABLE #include "Uart_Memmap.h"     3. Test Result Use UART3, pin UART3_TX:PTD2, UART3_RX:PTD3 After the chip is reset, send first: Helloworld for automotive with S32K344! Then wait for reception. After receiving 10 bytes of data, generate uart_callback interrupt and enter LPUART_UART_IP_ENET_END_TRANSFER. You can see that the data received in RX_Buffer is consistent with the data sent. Then, the code will loop back the received data. The test situation is as follows: The figure below shows two groups of tests: PC sends: 1234567890, after MCU receives it, loop it back. PC sends: 0987654321, after MCU receives it, debug stops at the breakpoint, you can check the received buffer situation, you can see that the buffer data is correct. Fig 14 Fig 15 Attached are two code packages: (1) Uart_TS_T40D34M40I0R0_miniK312_3.zipEB MCAL command line method After unzip the code, put it in: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins, and then you can compile it directly using the command line : Fig 16 (2)Mcal_UARTDMA_S32K312_RTD400_S32DS.zip:The way to import into S32DS, of course, it already contains the EB project: Fig 17 PS: Add another code, it add the IDLE function, based on the RTD400,  Mcal_UARTDMA_IDLE_S32K312_RTD400_S32DS.zip Test result is:      
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the  ADC_SAR and BCTU IP Driver for the S32K3xx MCU. The example uses the TWO PIT0 trigger to trigger BCTU conversion list to perform parallel conversions on ADC0/ADC1. Each Trigger has one LIST associated with it in the BCTU. Conversion result for EACH list is stored in individual FIFO of the BCTU. DMA will transfer the ADC conversion result. LIST-1 ADC channels are selected to be converted on each ADC:     LIST-2 ADC channels are selected to be converted on each ADC:--      Converted results from BCTU FIFO are moved by DMA into result array.  ADC channel S10 is connected to board's potentiometer. Result :--    ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ********************************************************************************
View full article