S32K311_SleepWakeupUsingButton_RTD3p0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K311_SleepWakeupUsingButton_RTD3p0

S32K311_SleepWakeupUsingButton_RTD3p0

********************************************************************************************
* Test HW: S32K311 EVB-Q100
* MCU: S32K311
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE Micro
* Target: internal_FLASH
********************************************************************************************
The purpose of this demo application is to enter the standby mode and waking up from sleep using the user button.


=============== How this DEMO works ==========
1) once the image is flashed, the application starts running and BLUE LED blinks for every one second during
RUN mode

2) Once SW5 in EVB is pressed, MCU enters the SLEEP mode and it turns off BLUE LED & PIT

3) To Wakeup: Press SW4 in EVB

4) Once it returns to normal mode, BLUE LED and PIT starts running.

Used pins:
=========
PTC11 -> SW5 -> EnterStandby
PTA8 -> SW4 -> WakeupFromSleep
PTB8 -> D12   -> Blue led

 

Attachments
No ratings
Version history
Last update:
‎12-20-2024 05:28 AM
Updated by: