S32K Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K Knowledge Base

Labels

Discussions

Sort by:
*******************************************************************************  The purpose of this demo application is to present a usage of the Printf Semihosting for the S32K3xx MCU.  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Create New project :-- Select Semi hosting library in project Properties :-- In Debugger setting :--- Include file :-- #include <stdio.h> Output :--    
View full article
  1. Abstract This article also explains the S32DS+EB configuration, RTD400. The MCAL training of other modules will be based on this structure in the future. However, this article will provide a command line version of the code. If you need the command line mode, you can directly copy one under the RTD MCAL code package and use VScode to compile it. The hardware of this article is based on K312-miniEVB, and the board situation is as follows:      Fig 1 Function: In the K312 MCAL code, the UART transceiver function is implemented using DMA. Since RTD400 does not have K312 routines, there is also a process of porting from RTD400 to K312 MCAL. Of course, the previous article has explained it very clearly, and also provided the S32DS project template. This article will be based on the previous S32DS EB project template.  2. Function Implementation 2.1 K312 MINIEVB hardware configuration For the hardware configuration, since this article only uses UART, the structure is very simple, using the pins: LPUART3_TX: PTD2 LPUART3_RX: PTD3 and an external TTL-USB tool to achieve signal communication. 2.2 EB Configuration     Here we list all the modules used in EB tresos related to this article, and focus on the modules that require specific configuration. Fig 2 2.2.1 Mcl module The Dma Logic Channel interface needs to be configured. The main purpose is to configure two DMA channels for LPUART3_TX and RX. (1)dmalogicChannel_Type_0 Fig 3 (2)dmalogicChannel_Type_2 Fig 4 The callback registered here can also be called directly in the code. 2.2.2 Mcu module Mcu->McuClockSettingConfig->McuClockReferencePoint->Lpuart3_clk Fig 5 In fact, it configures the clock source frequency of LPUART to 24Mhz, which comes from AIPS_SLOW_CLK. 2.2.3 Platform module Platform->Interrupt Controller->IntCtrlConfig,Configure 3 channels: Fig 6 Here we only need to pay attention to the LPUART3 interrupt, as well as the DMA0 channel 6 and channel 7 interrupts, because these two DMA channels are configured for UART TX and RX. FlexIO is ignored, it is just a matter of whether it is deleted in the original routine. 2.2.4 Port module Port->PortContainer, add PTD2,PTD3 pins: Fig 7 Fig 8 2.2.5 Uart module There are two places to configure: (1)uart->General Fig 9 (2)uart->uartChannel Fig 10 There are 4 points to note here: Point 1: Select the clock source configured in the mcu Point 2: Configure the baud rate to 115200 Point 3: Select the asynchronous mode as DMA Point 4: Select the two DMA channels configured in the mcl, and you need to match TX and RX to the corresponding DMA channels. 2.2.6 Rm module Rm->DMA MUX Configure 2 DMA_MUX channels: Fig 11 Fig 12 2.3 main code     #include "Mcl.h" #include "Mcu.h" #include "CDD_Uart.h" #include "CDD_Rm.h" #include "Port.h" #include "Platform.h" #include "Lpuart_Uart_Ip_Irq.h" #include "Flexio_Uart_Ip_Irq.h" //#include "check_example.h" #include <string.h> #include "Port_Cfg.h" #define UART_LPUART_INTERNAL_CHANNEL 0U #define UART_FLEXIO_TX_CHANNEL 1U #define UART_FLEXIO_RX_CHANNEL 2U /* Welcome messages displayed at the console */ #define WELCOME_MSG "MCAL UART DMA Helloworld for automotive with S32K312!\r\n" /* Error message displayed at the console, in case data is received erroneously */ #define ERROR_MSG "An error occurred! The application will stop!\r\n" /* Length of the message to be received from the console */ #define MSG_LEN 50U #define UART_BUFFER_LENGTH ((uint32)10U) Std_ReturnType T_Uart_Status; //uint8 Rx_Buffer[UART_BUFFER_LENGTH]; #define UART_START_SEC_VAR_CLEARED_UNSPECIFIED_NO_CACHEABLE #include "Uart_Memmap.h" __attribute__(( aligned(32) )) uint8 Rx_Buffer[UART_BUFFER_LENGTH]; #define UART_STOP_SEC_VAR_CLEARED_UNSPECIFIED_NO_CACHEABLE #include "Uart_Memmap.h" uint32 g_Uart_CallbackCounter = 0U; uint32 g_DmaCh16_ErrorCallbackCounter = 0U; uint32 g_DmaCh17_ErrorCallbackCounter = 0U; //void Uart_Callback (void); void Uart_Callback(const uint8 HwInstance, const Lpuart_Uart_Ip_EventType Event, void *UserData); void Mcl_DmaCh16_ErrorCallback (void); void Mcl_DmaCh17_ErrorCallback (void); void Uart_Callback(const uint8 HwInstance, const Lpuart_Uart_Ip_EventType Event, void *UserData) { if(Event == LPUART_UART_IP_EVENT_END_TRANSFER) { __asm volatile ("nop"); __asm volatile ("nop"); __asm volatile ("nop"); __asm volatile ("nop"); __asm volatile ("nop"); __asm volatile ("nop"); } else if (Event == LPUART_UART_IP_EVENT_TX_EMPTY) { __asm volatile ("nop"); __asm volatile ("nop"); } else if (Event == LPUART_UART_IP_EVENT_RX_FULL) { __asm volatile ("nop"); } else if (Event == LPUART_UART_IP_EVENT_ERROR) { __asm volatile ("nop"); } else { __asm volatile ("nop"); } } void Mcl_DmaCh6_ErrorCallback (void) { g_DmaCh16_ErrorCallbackCounter++; } void Mcl_DmaCh7_ErrorCallback (void) { g_DmaCh17_ErrorCallbackCounter++; } boolean User_Str_Cmp(const uint8 * pBuffer1, const uint8 * pBuffer2, const uint32 length) { uint32 idx = 0; for (idx = 0; idx < length; idx++) { if(pBuffer1[idx] != pBuffer2[idx]) { return FALSE; } } return TRUE; } /** * @brief Main function of the example * @details Initializez the used drivers and uses the Icu * and Dio drivers to toggle a LED on a push button */ int main(void) { Std_ReturnType UartStatus = E_NOT_OK; uint32 RemainingBytes; uint32 Timeout = 0xFFFFFF; Uart_StatusType UartReceiveStatus = UART_STATUS_TIMEOUT; Uart_StatusType UartTransmitStatus = UART_STATUS_TIMEOUT; /* Initialize the Mcu driver */ Mcu_Init(NULL_PTR); Mcu_InitClock(McuClockSettingConfig_0); Mcu_SetMode(McuModeSettingConf_0); /* Initialize Mcl module */ Mcl_Init(NULL_PTR); /* Initialize Rm driver for using DmaMux*/ Rm_Init (NULL_PTR); /* Initialize all pins using the Port driver */ Port_Init(NULL_PTR); /* Initialize IRQs */ Platform_Init(NULL_PTR); /* Initializes an UART driver*/ Uart_Init(NULL_PTR); T_Uart_Status = Uart_AsyncSend(UART_LPUART_INTERNAL_CHANNEL, (const uint8 *)WELCOME_MSG, strlen(WELCOME_MSG)); if (E_OK == T_Uart_Status) { do { /* Get transmission status */ UartTransmitStatus = Uart_GetStatus (UART_LPUART_INTERNAL_CHANNEL, &RemainingBytes, UART_SEND); } while (UART_STATUS_NO_ERROR != UartTransmitStatus && 0 < Timeout--); Timeout = 0xFFFFFF; UartTransmitStatus = UART_STATUS_TIMEOUT; } for(;;) { /* Receive data from the PC - Get 10 bytes in total */ UartStatus = Uart_AsyncReceive (UART_LPUART_INTERNAL_CHANNEL, Rx_Buffer, UART_BUFFER_LENGTH); if (E_OK == UartStatus) { do { /* Get receive status */ UartReceiveStatus = Uart_GetStatus (UART_LPUART_INTERNAL_CHANNEL, &RemainingBytes, UART_RECEIVE); } while (UART_STATUS_NO_ERROR != UartReceiveStatus && 0 < Timeout--); Timeout = 0xFFFFFF; UartReceiveStatus = UART_STATUS_TIMEOUT; } UartStatus = E_NOT_OK; /* Send data to the PC - Echo back the received data */ UartStatus = Uart_AsyncSend (UART_LPUART_INTERNAL_CHANNEL, Rx_Buffer, UART_BUFFER_LENGTH); if (E_OK == UartStatus) { do { /* Get transmission status */ UartTransmitStatus = Uart_GetStatus (UART_LPUART_INTERNAL_CHANNEL, &RemainingBytes, UART_SEND); } while (UART_STATUS_NO_ERROR != UartTransmitStatus && 0 < Timeout--); Timeout = 0xFFFFFF; UartTransmitStatus = UART_STATUS_TIMEOUT; } UartStatus = E_NOT_OK; } Uart_Deinit(); Mcl_DeInit(); // Exit_Example((T_Uart_Status1 == E_OK) && (T_Uart_Status2 == E_OK)); return (0U); }     It should be noted here that according to RTD C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins\Uart_TS_T40D34M40I0R0\doc的RTD_UART_IM.pdf, RTD_UART_UM.pdf. Fig 13 When doing DMA transfer, the buffer needs to be placed in the noncacheable area. That's why this article is:     #define UART_START_SEC_VAR_CLEARED_UNSPECIFIED_NO_CACHEABLE #include "Uart_Memmap.h" __attribute__(( aligned(32) )) uint8 Rx_Buffer[UART_BUFFER_LENGTH]; #define UART_STOP_SEC_VAR_CLEARED_UNSPECIFIED_NO_CACHEABLE #include "Uart_Memmap.h"     3. Test Result Use UART3, pin UART3_TX:PTD2, UART3_RX:PTD3 After the chip is reset, send first: Helloworld for automotive with S32K344! Then wait for reception. After receiving 10 bytes of data, generate uart_callback interrupt and enter LPUART_UART_IP_ENET_END_TRANSFER. You can see that the data received in RX_Buffer is consistent with the data sent. Then, the code will loop back the received data. The test situation is as follows: The figure below shows two groups of tests: PC sends: 1234567890, after MCU receives it, loop it back. PC sends: 0987654321, after MCU receives it, debug stops at the breakpoint, you can check the received buffer situation, you can see that the buffer data is correct. Fig 14 Fig 15 Attached are two code packages: (1) Uart_TS_T40D34M40I0R0_miniK312_3.zipEB MCAL command line method After unzip the code, put it in: C:\NXP\SW32K3_S32M27x_RTD_R21-11_4.0.0\eclipse\plugins, and then you can compile it directly using the command line : Fig 16 (2)Mcal_UARTDMA_S32K312_RTD400_S32DS.zip:The way to import into S32DS, of course, it already contains the EB project: Fig 17 PS: Add another code, it add the IDLE function, based on the RTD400,  Mcal_UARTDMA_IDLE_S32K312_RTD400_S32DS.zip Test result is:      
View full article
Greetings, if you want to use the open source EmbSysRegView plugin in your Eclipse environment: this article describes how to add the S32K CMSIS-SVD files to it: Adding CMSIS-SVD Files to EmbSysRegView 0.2.6.r192 and Eclipse Happy SVDing 🙂 Erich
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the  FlexCAN IP Driver for the S32K3xx MCU.  The example uses FLEXCAN-0 for transmit & receive Tusing following Message buffer :-- #define RX_MB_IDX_0 10U #define RX_MB_IDX 11U #define TX_MB_IDX 12U FIFO Receive Message from range :-- 0x01 to 0x16 BAUDRATE : 500 KBPS  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************    
View full article
The purpose of this demo application is to show you the usage of the FlexCAN module configured to use CAN FD and Enhance RXFIFO using the S32 RTD API. - This demo application requires two boards, or single board connected with CAN tool. - CAN FD is enabled with bitrate 500/2000 kbps - MB0 is configured to transmit either std. or ext ID - MB1 is configured to receive ext ID 0xFACE and MB2 to receive std ID 0x1 - Enhanced RXFIFO is enabled and 3 enhanced RXFIFO filter elements (filter + mask scheme) are defined ext ID 0xABCD with mask 0x1FFFFFFF std ID 0x123 with mask 0x7FF std ID 0x456 with mask 0x7FF - DMA is used to read enhanced RXFIFO, watermark is set to 5 - Callback function is used as well to handle TX and RX process in MBs and Enhanced RXFIFO after DMA complete 5 reading of RXFIFO  ------------------------------------------------------------------------------  Test HW: S32K3444EVB-Q172  MCU: PS32K344EHVPBS 1P55A  Compiler: S32DS.ARM.3.5  SDK release: S32K3_RTD_4_0_0_D2311  Debugger: Lauterbach  Target: internal_FLASH
View full article
[S32K3 tool part]:How to flexibly debug elf files without source code  1.Doc Introduction When supporting customers with the MCU software technical issues, we often encounter situations where customers are unable to provide the source code of problematic projects due to company policies. At most, they can provide the elf files of problematic projects. This involves how to make good use of elf to achieve flexible debugging goals. Elf file is a binary file format that contains program code, data, symbol tables, segment tables, and other information. When debugging elf, you cannot see the source code, but you can see the function name corresponding to the assembly address. At this time, debugging can still relatively know the location. However, the problem is that it is not possible to freely modify and generate new files like modifying the source code. Is it feasible to make specific modifications to elf files to achieve the purpose of functional testing? This article will provide testing methods for skipping specific positions, erasing functions, replacing code, concatenating functions, etc. on an existing elf, to achieve skipping of code in certain positions of elf, or not executing it at any time, creating a new area to concatenate other functional functions, and then modifying the original call position to forcibly insert test function code. The testing platform for this article is S32K344 and RTD500.        Fig 1 2. Function implementation    Fig 1 is an elf file of the original function. The function is to call three functions after startup: Fun1, Fun2, and Fun3 Fun1: Flashing Red Light Fun2: Flashing green light Fun3: Flashing Blue Light The main functions that need to be implemented in this article are as follows: (1) Fun2 function skipped There are two types of function skipping here: When debugging, start from Fun2 and modify the PC to jump to Fun3 Do not run Fun2 even when powered on, simply erase the Fun2 value from the main as nop        Fig 2    (2)Add Fun4, modify Fun2 call in Main to jump to Fun4        This involves inserting Fun4 code into an empty flash address, modifying the jump asm code of Fun2 to jump to Fun4   Fig 3 2.1 Code and Tool preparation Hardware Platform: S32K344-EVB Software: RTD500, S32DS3.5, JFLASH, PE Multilink(built-in to EVB), Lauterbach  JFLASH tool download link:https://www.segger.com/downloads/jlink/  Create a simple led blinking project that can be based on RTD's existing Siul_2Dio_ip_Instance_S32K344 project, add three LED light pins, and construct three functions for flashing red, green, and blue lights respectively. Call the three functions sequentially in main. Generate elf backup when testing is working. 2.2 Implementation of elf modification function: Fun2 function skipped    Here is the specific implementation method for Figure 2: the PC crosses Fun2 and replaces Fun2 with asm nop 2.2.1 PC Crossing Fun2 In the Main function, call the assembly position breakpoint of Fun2, directly modify PC to the value of Fun3 address+1, and then run to skip Fun2. As shown in Figure 4, it has already been run to Fun2, but has not yet entered the function body of Fun2. Simply change the pointer entry that was originally intended to call Func2 to 0X4027B4+1, which is the function entry of Fun3. As can be seen, after modifying the PC, press enter and step into the Fun3 function body. If you modify the starting point of Fun2's function body to jump from PC to Fun3, both sides of Fun3 will run from the main function as a whole   Fig 4 Fig 5 2.2.2 Replace Fun2 with NOP The situation of directly using debug to jump to PC above bypasses Fun2. Although Fun2 can be skipped in testing, it should be noted that when downloading the code, it will actually run the code before entering debug. If some tests want to start from POR without running Fun2, then it is necessary to directly erase the location code of the original elf Fun2 call, and the commonly used method can be replaced with harmless nop instructions. The assembly hexadecimal value of the nop instruction is 00 BF, as shown in the following figure:       Fig 6 With the target modification value, the following is to find the call address of Fun2 in elf main and replace the corresponding 4 bytes with 00BF00BF. From the original elf file, we can see that the data location of the call Fun2 is 4 bytes starting from the absolute address 0X0040280E, use the JFLASH tool in the Segger JLINK driver to open the original elf file, modify the data of the 4 bytes starting address 0X0040280E from FFF7ABFF to 00BF00BF, save the modified data as an srec file, and then call the srec file in the temporary project to run the modified code. The following figure shows the modification process Fig 7 The modified debug result is as follows: Fig 8 As can be seen, the assembly that jumped from the 0X40280e area to Fun2 has now become a nop instruction. At this point, running at full speed will ignore fun2 and proceed in sequence. Whether debugging or after powering on, Fun2 calls have been completely erased from the overall runtime sequence. Of course, since manually modified elf cannot be directly saved as an elf file through JFLASH, choosing to save it as an Srec file will result in losing the symbol table when debugging again. When using elf in the early stage, remember the absolute addresses of several functions that need to be used. 2.3 Elf modification function implementation: Fun4 replaces Fun2 entrance     In the above content, we skip or insert nop directly at the main Fun2 call position, can we call another function body in the original Fun2 for testing, achieving the same area but with other functions? It's possible. There are also two types here: one is to destroy the original Fun2 function body position and directly replace the code content of the function body, of course, this is limited by the size of the original Fun2 function body. On the other hand, keep the original Fun2 for future use. You can start another function Fun4 at other blank addresses in flash, and then change the code that calls Fun2 in main to call Fun4 to achieve seamless docking of Fun1->Fun4->Fun3 operations.     This article mainly uses to create a new function at a specific absolute address in the flash blank space. Of course, attention should be paid to the original elf map situation to ensure that the blank area is sufficient for use. It is best for this new function to be self-contained and independent of other functions to avoid calling bias. If it is necessary to call other function bodies, it is necessary to set the addresses of other dependent functions in the sample project to be consistent when constructing this new function.     Here, we will create a S32DS project and allocate a flash area in the linkfile to store the newly created Fun4. The Fun4 function is to achieve alternating blink green and red led.      2.3.1 linkfile modification MEMORY { int_pflash : ORIGIN = 0x00400000, LENGTH = 0x00010000 /* 4096KB - 176KB (sBAF + HSE)*/ int_pflash_user : ORIGIN = 0x00410000, LENGTH = 0x003C4000 int_dflash : ORIGIN = 0x10000000, LENGTH = 0x00020000 /* 128KB */ int_itcm : ORIGIN = 0x00000000, LENGTH = 0x00010000 /* 64KB */ int_dtcm : ORIGIN = 0x20000000, LENGTH = 0x0001F000 /* 124KB */ int_stack_dtcm : ORIGIN = 0x2001F000, LENGTH = 0x00001000 /* 4KB */ int_sram : ORIGIN = 0x20400000, LENGTH = 0x0002FF00 /* 184KB, needs to include int_sram_fls_rsv */ int_sram_fls_rsv : ORIGIN = 0x2042FF00, LENGTH = 0x00000100 int_sram_no_cacheable : ORIGIN = 0x20430000, LENGTH = 0x0000FF00 /* 64KB, needs to include int_sram_results */ int_sram_results : ORIGIN = 0x2043FF00, LENGTH = 0x00000100 int_sram_shareable : ORIGIN = 0x20440000, LENGTH = 0x00004000 /* 16KB */ ram_rsvd2 : ORIGIN = 0x20444000, LENGTH = 0 /* End of SRAM */ } SECTIONS { .FUNC4 : { *(.func4) } > int_pflash_user … } 2.3.2 Fun4 function code The function body code is constructed as follows, purely logical, without relying on any external functions or variables. __attribute__((section (".func4"))) void Func4(void) { uint8 count1 = 0U; static volatile uint32 DelayTimer = 0; volatile uint8 *red_addr_byte = (volatile uint8 *)0x4029131e; volatile uint8 *green_addr_byte = (volatile uint8 *)0x4029131d; volatile uint8 *blue_addr_byte = (volatile uint8 *)0x4029131c; //RED: GPIO29, 0x4029131e //green: GPIO30, 0x4029131d //blue: GPIO31, 0x4029131c while (count1++ < 6) { *red_addr_byte = 1; *green_addr_byte = 0; while(DelayTimer < 4800000) { DelayTimer++; } DelayTimer = 0; *red_addr_byte = 0; *green_addr_byte = 1; while(DelayTimer < 4800000) { DelayTimer++; } DelayTimer = 0; /* Siul2_Dio_Ip_WritePin(LED_RED_PORT, LED_RED_PIN, 1U); Siul2_Dio_Ip_WritePin(LED_GREEN_PORT, LED_GREEN_PIN, 0U); while(DelayTimer < 4800000) { DelayTimer++; } DelayTimer = 0; Siul2_Dio_Ip_WritePin(LED_RED_PORT, LED_RED_PIN, 0U); Siul2_Dio_Ip_WritePin(LED_GREEN_PORT, LED_GREEN_PIN, 1U); while(DelayTimer < 4800000) { DelayTimer++; } DelayTimer = 0; */ } *red_addr_byte = 0; *green_addr_byte = 0; } Here we know, this Fun4 address starts from flash 0x00410000 and generates elf after compiling the project with the above function. 2.3.3 Separate Fun4 function body into independent files Open the elf file with newly created Fun4 using JFLASH and delete all code above 0x00410000. Method: JFLASH->Edit->Delete range:   Fig 9 After deletion, obtain a file containing only Fun4 code and save it as the ElfdebugSource_S32K344_STD500_delete.srec file. 2.3.4 Merge the Fun4 function body into the corresponding Srec of the original elf      Open the Srec corresponding to the original elf and the Fun4 Srec file that was just separated using JFLASH. Choosing to merge two files will automatically concatenate Fun4 files with different addresses into the original Srec file and save them as a separate file.   Fig 10 Fig 11 2.3.5 Modify the original Fun2 calling in main to Fun4 calling Modify code from: 0040280e: ff f7 ab ff   bl      0x402768 <Func2> To: 0040280e: 0d f0 f7 fb   bl      0x410000 Among them, 0x410000 is the absolute address of Fun4. Fig12 Modify the Srec file that has already added Fun4 to start with 0040280e with a value of 0d f0 f7 fb, then save it as a new Srec and debug it. It can be found that the running order of main has changed to Fun1->Fun4->Fun3 Skipped Fun2 while also running the newly integrated Fun4. The above image was run in the S32DS+PE Multilink environment. At this time, due to the operation of the Srec file, the symbol table information for elf was no longer included, but the functionality was successful. 2.3 Lauderbach synchronously loads the original elf symbol table Due to a series of grafting modifications on the original elf and saving it as SREC, the symbol table was lost. So if you still want to view the symbol table of unmodified areas, you can use the Laubach tool. After attaching the code, you can load the original elf file in trace32 by following the command: Data.LOAD.Elf  C:\S32DS35_RTD500\elfdebug\elftest\Debug_FLASH\Elfdebug_S32K344_RTD500.elf /nocode As can be seen, the original part with Fun2 symbol table is only missing due to modifications, but other call header symbol tables still exist. This is also convenient for code execution and reading.     Fig 13 Fig 14 Fig 15 3. Knowledge points Here we share the corresponding hexadecimal data operations for BL addr jumps. The previous one was generated directly using S32DS 0040280e: 0d f0 f7 fb   bl      0x410000 It can be known that the value corresponding to the bl 0x410000 instruction is 0d f0 f7 fb So how is the value of 0d f0 f7 fb calculated? This requires reference to ARM's architecture document: DDI0403E_d_armv7m_arm.pdf For the situation corresponding to the BL jump thumb2 instruction: Fig 16 For BL, it is a long jump, which is actually composed of two jump instructions, Thumb instructions are all 2 bytes long, and BL consists of 2 jump instructions that make up 4 bytes. The 0-11 bits represent an 11 bit address, with the following specific meanings: The 11th digit is 0, representing a high offset The 11th digit is 1, representing a low offset The calculation formula is as follows: offset = (target address- source address -4) & 0x007fffff high = offset >> 12(decimalism) low = ( offset & 0x00000fff )>>1  machineCode = ((0xF800 | low) << 16) | (0xF000 | high) Let's calculate what we use here: bl      0x410000 Offset=(Destination Address - Source Address -4)&0x007fffff = (0x410000-0x40280e-4)& 0x007fffff =D7EE High=offset>>12 (decimal)=D low = ( offset & 0x00000fff )>>1  = 3F7 machineCode = ((0xF800 | low) << 16) | (0xF000 | high) =((0xF800 | 3F7) << 16) | (0xF000 | D) =0XFBF7F00D This corresponds to a low to high: 0D 00 7F FB This is also the source of the following binary modulation instructions: 0040280e: 0d f0 f7 fb   bl      0x410000    
View full article
     In fact, this topic has been written by many people before, and it is well written. However, in actual operation, you may encounter some pitfalls, so this article will not write the article steps in detail, but will provide a real and direct operation video process. The main reference article source link is: https://www.wpgdadatong.com.cn/blog/detail/74936 The method is very useful. I have tried the existing RTD4.0.0 MCAL code and also imported it into my own configured MCAL code. The method is reliable and effective. Platform:     SW32K3_S32M27x_RTD_R21-11_4.0.0 S32DS3.5 EB tresos Studio 29.0 S32K344-EVB Attach the video directly: The main steps are as follows: STEP 1. Create a new S32DS project STEP 2. S32DS project configuration Including folder deletion, addition, filter condition addition, include files, link files, optimization conditions, macro definitions, etc. STEP 3. Create a new EB project Configure a new RTD, or copy the existing RTD configuration to avoid unnecessary problems and errors. STEP 4. Compile and download The following are some related files that need to be copied: MCAL_Plugins->Link Source Resource Filters   Fig 1 Includes   Fig 2 "${ProjDirPath}/Generate/include" "${MCAL_PLUGIN_PATH}/Adc${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Ae${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/BaseNXP${MCAL_MODULE_NAME_SUFFIX}/header" "${MCAL_PLUGIN_PATH}/BaseNXP${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Can_43_FLEXCAN${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/CanIf${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/CanTrcv_43_AE${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Crc${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/CryIf${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Crypto_43_HSE${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Csm${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Dem${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Det${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Dio${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Dpga${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/EcuM${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Eth_43_GMAC${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/EthIf${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/EthSwt${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/EthTrcv${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Fee${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Gdu${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Gpt${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/I2c${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/I2s${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Icu${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Lin_43_LPUART_FLEXIO${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/LinIf${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/LinTrcv_43_AE${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Mcl${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Mcu${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Mem_43_EEP${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Mem_43_EXFLS${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Mem_43_INFLS${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/MemAcc${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/MemIf${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Ocotp${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Ocu${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Os${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Platform${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Platform${MCAL_MODULE_NAME_SUFFIX}/startup/include" "${MCAL_PLUGIN_PATH}/Port${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Pwm${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Rm${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Rte${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Sent${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Spi${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Uart${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Wdg${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/WdgIf${MCAL_MODULE_NAME_SUFFIX}/include" "${MCAL_PLUGIN_PATH}/Zipwire${MCAL_MODULE_NAME_SUFFIX}/include"   Preprocessor   Fig  3 S32K3XX S32K344 GCC USE_SW_VECTOR_MODE D_CACHE_ENABLE I_CACHE_ENABLE ENABLE_FPU   Linker   Fig  4 "${MCAL_PLUGIN_PATH}/Platform${MCAL_MODULE_NAME_SUFFIX}/build_files/gcc/linker_flash_s32k344.ld" optimization   Fig 5 -fno-short-enums -funsigned-char -fomit-frame-pointer -fstack-usage   main.c Comment: #include "check_example.h #Exit_Example(TRUE);   Attached code: MCAL_Dio_S32K344_S32DS363_RTD600_CP.zip: RTD MCAL copy to S32DS project MCAL_Dio_S32K312_RTD600_MCUPLL.zip: S32K312 MCU with PLL, add UART printf Others attachment all link the MCAL to RTD install path.
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the  FlexCAN IP Driver for the S32K3xx MCU.  The example uses FLEXCAN-0 for transmit & receive using following Message buffer :-- #define RX_MB_IDX_0 10U #define RX_MB_IDX 11U #define TX_MB_IDX 12U BAUDRATE : 500 KBPS  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************        
View full article
********************************************************************************  Detailed Description:  Example shows how to use FlexCAN 0 Pretended networking mode to allow FlexCAN  module to wake up MCU from STOP mode using SDK.  Wake up by Timeout and wake up by Match events are enabled.  Also pin interrupt can be used to exit STOP mode.  So MCU enters STOP mode by pressing SW3 button.  MCU exits STOP mode when one of following happens:  - no CAN message comes in 8sec (CAN PN timeout event)  - message with standard ID 0x554 or 0x555 comes (CAN PN match event)  - SW2 button is pressed (PTC12 interrupt)  In run mode blue LED is dimming and the rate is different for each wakeup event  ------------------------------------------------------------------------------  Test HW: S32K116EVB-Q48  MCU: PS32K116LAM 0N96V  Compiler: S32DS.ARM.2.2  SDK release: S32SDK_S32K1xx_RTM_3.0.0  Debugger: Lauterbach, OpenSDA  Target: internal_FLASH ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * * Example shows possible setting for PWM duty cycle update using DMA. * FTM0 ch0 is set to Edge aligned mode with 20KHz period. * Initialization trigger is routed back to HW trigger 1 using TRGMUX, so this HW * trigger can be used for CnV synchronization. * DMA on FTM0 ch0 is enabled (on ch0 CHF flag) and DMA ch0 configured to update C0V * from duty cycle variable. * NOte CHF is not set for 0% and 100% duty cycle, thus no DMA trigger is generated. * * Green LED is dimming as duty is changing. * * ------------------------------------------------------------------------------ * Test HW: S32K118EVB-Q64 * MCU: PS32K118LAMLH 0N97V * Compiler: S32DS.ARM.2.2 * SDK release: S32SDK_S32K1xx_RTM_3.0.3 * Debugger: Lauterbach, OpenSDA * Target: internal_FLASH * ******************************************************************************** Revision History: 1.0 Sep-16-2021 Petr Stancik Initial Version *******************************************************************************/
View full article
******************************************************************************** The purpose of this demo application is to show you the usage of the FlexCAN module configured to use CAN FD using the S32 RTD API. - This demo application requires two boards, or single board connected with CAN tool. - CAN FD is enabled with bitrate 500/2000 kbps - It configures FlexCAN0 module and its transceiver (TJA1153). - MB0 is used to transmit CANFD std. ID - MB1 is configured to receive any std. ID - Callback function is used as well to handle TX and RX process in MBs. Received ID is echoed back. - setupCanXCVR function is called to Init TJA1153 connected to FlexCAN0 on the board. It expects transceiver in Vanilla state and set TPL to pass all std and ext ID and do not block any message coming from bus. Finally leaving configuration mode without writing to non-volatile memory nor locking the transceiver. * * ------------------------------------------------------------------------------ * Test HW: S32K3X8EVB-Q289 rev B2 * MCU: P32K358HVS 0P14E * Compiler: S32DS.ARM.3.5 * SDK release: S32K3_RTD_4.0.0_D2311 / S32K3_RTD_5_0_0_D2408 * Debugger: Lauterbach * Target: internal_FLASH * ********************************************************************************
View full article
********************************************************************************  Detailed Description:  Example shows FlexCAN 0 usage in RUN/VLPR modes using SDK.  CAN bitrate is set to 250bit/s.  MCU enters VLPR mode by pressing SW3 button. CAN std message is sent with data VLPRmode"  MCU exits VLPR to RUN mode when one of following happens:  - CAN std message with RX_MSG_ID is received and MCU is in VLPR  - SW2 button is pressed (PTC12 interrupt). CAN std message is sent with data "RUN mode"  Blue LED is dimming and the rate is different for each power mode due to different  system clock (48Mhz vs 4MHz)  ------------------------------------------------------------------------------  Test HW: S32K116EVB-Q48  MCU: PS32K116LAM 0N96V  Compiler: S32DS.ARM.2.2  SDK release: S32SDK_S32K1xx_RTM_3.0.3  Debugger: Lauterbach, OpenSDA  Target: internal_FLASH ********************************************************************************
View full article
Often we need to implement a SENT receiver in order to read the information sent by some sensors. It is useful to have the possibility of transmitting different message patterns in order to test your implementation. With this project you can transmit via a computer terminal a group of messages (up to 64). The project runs on a S32K144 EVB board, the output signal goes through J206 pin.
View full article
 ------------------------------------------------------------------------------ * Test HW: S32K3X4EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE Micro * Target: internal_FLASH ******************************************************************************** Example MCAL S32K312 MEM_InFls  DS3.5 RTD300 :-- Example MCAL S32K312 MEM_InFls DS3.5 RTD300 - NXP Community Example MCAL S32K312 FEE DS3.5 RTD300 :-- Example MCAL S32K312 FEE DS3.5 RTD300 - NXP Community Example MCAL S32K312 FEE and MEM_InFls DS3.5 RTD300 :-- Example MCAL S32K312 FEE and MEM_InFls DS3.5 RTD300 - NXP Community Example MCAL S32K312 PWM ICU using Custom IRQ EMIOS DS3.5 RTD300 :-- Example MCAL S32K312 PWM ICU using EMIOS DS3.5 RTD300 - NXP Community Example ASR S32K312 EMIO PWM Generation & Duty capture using Interrupt DS3.5 RTD300 :-- Example ASR S32K312 EMIO PWM Generation & Duty capture using Interrupt DS3.5 RTD300 - NXP Community  Example ASR S32K312 EMIO PWM Generation & Duty capture using Polling DS3.5 RTD300 :-- Example ASR S32K312 EMIO PWM Generation & Duty capture using Polling DS3.5 RTD300 - NXP Community
View full article
******************************************************************************** * File: main.c * Owner: David Tosenovjan * Version: 0.0 * Date: Mar-12-2021 * Classification: General Business Information ******************************************************************************** * Detailed Description: * Example code configures the whole 4kB FlexRAM area for SRAM use. * By default or after mass erase, S32K1 device has only address range * 0x1400_0000-0x1400_0DFF (3.5kB) accessible for SRAM use. * To enable remaining 0.5kB it is needed to perform Program Partition Command * (with the setting shown in the example), but only once with the blank new * device (or previously mass erased). It sets up address range * 0x1400_0000-0x1400_0FFF for SRAM use. * ------------------------------------------------------------------------------ * Test HW: S32K146EVB-Q144 * MCU: PS32K146UAVLQ 0N73V QAC1735D * Fsys: default * Debugger: Lauterbach Trace32, OpenSDA * Target: Debug_RAM * Terminal: none * EVB connection: default ********************************************************************************
View full article
************************************************************************************************ * Detailed Description: * The example shows how to skip an instruction * that causes uncorrectable ECC fault exception during C40_Ip_Read(). * ----------------------------------------------------------------------------------------------- * Test HW: S32312EVB-Q172 * MCU: S32K312 * Debugger: S32DS 3.4, PEMicro Multilink * Target: internal_FLASH *************************************************************************************************
View full article
******************************************************************************** * Detailed Description: * The example adds DTCM_1 backdoor access for CM7_0. * int_dtcm_1_bd memory region and section dtcm1_bd_data added to the linker file. * DTCM1 ECC initialized in startup_cm7.s * MPU on DTMC1 enabled in system.c * Global variables decleared with __attribute__ ((section(".dtcm1_bd_data"))) in main.c * ------------------------------------------------------------------------------ * Test HW: S32K314EVB-Q172 * MCU: S32K314 * Debugger: S32DS_ARM_3.4 * Target: internal_FLASH ********************************************************************************
View full article
******************************************************************************** * Detailed Description: * The purpose of this example is show how to keep data in SRAM memory over SW * reset. SW reset is triggered by pressing the SW3 button on the S32K118EVB. * Reset is delayed for 514 LPO cycles. In the RCM interrupt, SRAMU_RETEN is * cleared allowing to retain SRAM data during the reset. After SW reset, * SRAMU_RETEN is set to allow accesses to SRAM. * File startup_S32K116.S in modified to skip ECC RAM initialization for SW reset * source. To check whether stored data stayed unmodified in the SRAM, specified * address is read and the LED lights up. * ------------------------------------------------------------------------------ * Test HW: S32K118EVB-Q064 * MCU: S32K118 LAMLH 0N97V QTZE1802B * Fsys: fsys = 48MHz * Debugger: Lauterbach Trace32 * Target: Debug * Terminal: 19200-8-no parity-1 stop bit-no flow control * EVB connection: default ******************************************************************************** Revision History: Ver Date Author Description of Changes 0.0 May-17-2023 David Tosenovjan Initial version *******************************************************************************/
View full article
*******************************************************************************  The purpose of this demo application is to present a usage of the HSE IP Driver for the S32K3xx MCU. This DEMO make use of SHE based keys & the RAM keys.  Step-1> Uncomment this MACRO to program the MASTER_ECU_KEY & BOOT_MAC_KEY #define FORMAT_HSE_KEY_CATALOG (1U) Step-2> Then comment the above mentioned MACRO to test the demo. Step-3> End of the DEMO in Switch case HSE_ERASE : keys are erased. HSE_EraseKeys(); SHE based secured boot :-- This demo uses the SHE based secured boot. You can test this after performing step-1. Once SHE is enabled code will be stuck at this point, after this issue an RESET.    ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ********************************************************************************
View full article
******************************************************************************************************* * Detailed Description: The purpose of these demo applications is to present a usage of the LPSPI Driver together with DMA Driver (IP and MCAL) for the S32K3xx MCU. The applications uses the LPSPI driver to transfer data between LPSPI2 (master, no DMA) and LPSPI0 (slave, with DMA) physical units. * Connections * Test HW: S32K3X4EVB-T172 * MCU: S32K344 * Debugger: S32DS 3.5, PEMicro Multilink Universal FX rev.B * Target: internal_FLASH *******************************************************************************************************
View full article