------------------------------------------------------------------------------
* Test HW: S32K3X4EVB-Q172
* MCU: S32K312
* Compiler: S32DS3.5
* SDK release: RTD 3.0.0
* Debugger: PE Micro
* Target: internal_FLASH
********************************************************************************
For S32K312, please use this correct clock HSE to AIPS clock should be ½.
Please make these changes in the below all example code clock setting.
HSE clock to 60 MHZ.
S32K312 PIT BTCU ADC-1 BCTU_ADC_DATA_REG DMA :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-PIT-BTCU-ADC-1-BCTU-ADC-DATA-REG-DM...
S32K312 UART Transmit & Receive Using DMA :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-UART-Transmit-amp-Receive-Using-DMA...
S32K312 EIRQ Interrupt :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-EIRQ-Interrupt-DS3-5-RTD300/ta-p/17...
S32K312 SPI Transmit & Receive Using DMA :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-SPI-Transmit-amp-Receive-Using-DMA-...
S32K312 CAN Transmit & Receive Using Polling mode :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-CAN-Transmit-amp-Receive-Using-Poll...
S32K312 CAN Transmit & Receive Using MB & FIFO DMA :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-CAN-Transmit-amp-Receive-Using-MB-a...
S32K312 ADC :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-ADC-DS3-5-RTD300/ta-p/1789282
S32K312 Switch Debouncing :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Switch-Debouncing-DS3-5-RTD300/ta-p...
S32K312 UART Freemaster :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-UART-Freemaster-DS3-5-RTD300/ta-p/1...
S32K312 PIT BTCU parallel ADC FIFO DMA :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-PIT-BTCU-parallel-ADC-FIFO-DMA-DS3-...
S32K312 placing variables in DCTM & code in ICTM :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-placing-variables-in-DCTM-amp-code-...
Example S32K312 Standby mode & Standby RAM and PAD keeping DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Standby-mode-amp-Standby-RAM-and-PA...
Example S32K312 SWT DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-SWT-DS3-5-RTD300/ta-p/1800559
Example S32K312 Printf Semihosting DS3.5 RTD300 :---
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Printf-Semihosting-DS3-5-RTD300/ta-...
Example S32K312 I2C Transmit & Receive Using DMA DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-I2C-Transmit-amp-Receive-Using-DMA-...
Example S32K312 HARDFAULT Handling Interrupt DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-HARDFAULT-Handling-Interrupt-DS3-5-...
Example S32K312 Bootloader to Application Jump DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-Bootloader-to-Application-Jump-DS3-...
Example S32K312 PIT timer Toggle LED DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-PIT-timer-Toggle-LED-DS3-5-RTD300/t...
Example S32K312 HARDFAULT Interrupt Handling using a script DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-HARDFAULT-Interrupt-Handling-using-...
Example S32K312 UART Transmit & Receive Using Interrupt DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-UART-Transmit-amp-Receive-Using-Int...
Example S32K312 CAN Transmit & Receive Using MB Interrupt DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-CAN-Transmit-amp-Receive-Using-MB-I...
Example S32K312 STANDBY wake up using CAN-0-RX and GPIO Switch DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-STANDBY-wake-up-using-CAN-0-RX-and-...
Example S32K312 STANDBY wake up using RTC DS3.5 RTD300 :--
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-STANDBY-wake-up-using-RTC-DS3-5-RTD...