S32 Design Studio知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32 Design Studio Knowledge Base

讨论

排序依据:
This document contains the instructions how to download separate elf/srec/hex file to the microcontroller using S32 Design Studio and USB PE Micro Universal Multilink/OpenSDA debug probes. This could be used in case you get an executable/binary image file only without any project or source code. There are basically three ways: flash programming support in IDE. This is only useful for programming the device. (it is available in S32DS ARM v1.3+, S32DS Power v1.2+) Create a new configuration, adjust its name and browse for elf/srec/hex file: Select MCU and specific core you are targeting: Select where the Flash Configuration should be saved into - workspace metadata (local file) or as a specific file e.g. part of an existing project (shared file). This way the config could be e.g.transferred with this project. Click on "Flash" button to proceed to programming. As soon as the device is programmed it's disconnected. 2. Executable file importer. Go to menu File -> Import -> Select "Executable File Importer"  this starts the wizard. This is for programming and debugging an executable elf object file only. Select the MCU/core you are targeting and browse for the .elf file Adjust the project name and create a debug/launch configuration (PEMicro GDB server example). If the .elf file is built on another machine and the source files are available but located in a different folder the source path could be adjusted. Source-level debugging is then possible. Finish the wizard and new "container" project for your elf is created. Its debug configuration opens automatically. "Debug" button starts the load/debug of the selected elf file. 3. reuse an existing project debug configuration or create a new dummy project for loading .elf/srec/hex Create new project which will provide basic debug settings Compile the project Copy the required .elf file to the created project Debug folder Open new project Debug configuration Choose correct project and set the correct .elf/srec/hex you want to download Click Apply button and then Debug button. The debug window with correct .elf file will be opened. Program is downloaded and you are able to debug or run it.
查看全文
This document explains how to change the package of a processor expert project, for example, from S32K144 100LQFP to S32K144 64LQFP.  It does NOT explain how to change processor derivatives (e.g. S32K144 to S32K142). 1. Assuming that the project is opened and active, go to Components Library View and click on Processors     2. Expand the repository folders and double click on your processor (e.g. S32K144) 3. Select new package (e.g.S32K144_64) and click on finish. Now the new variant will be added to your project 4. Go to PinSettings component and click on Switch Configuration. This action will change the pins configuration for new package and will discard the original pin configuration.
查看全文
Sometimes you need an output file other than the standard ELF, like a FLASH image. This instruction shows how to setup the selected build type to generate an additional output from the supported file types.   Go to Project Properties Right click on the Project name in Project Explorer -> Properties, OR Select the Project name in Project Explorer, select from pulldown menu Project -> Properties image.png Navigate to C/C++ Build -> Settings -> Cross Settings, check the box for ‘Create flash image’. Be sure to take note that the build configuration set in the Configuration field is correct one. The change you make here will only apply to the selected configuration. image.png Scroll the window down until you can see the ‘Apply’ button, then click on it. image.png You can specify output in newly appeared option Standard S32DS Create flash image image.png Build the project. The new output file is generated. image.png image.png
查看全文
S32 Design Studio is free-of-charge software that just requires to be activated. The activation process is incorporated into the S32DS installer. Before you proceed to the installation you always need to get an activation code. The activation code is typically sent automatically to your email registered on nxp.com account when you proceed to downloading of S32DS installer. The example of notification email is below:     There are two types of activation you can choose from - online and offline. If your machine is connected to the Internet then in most cases you just select online activation and S32DS gets activated automatically without any additional steps required.   Anyway if the computer that you are installing S32 Design Studio into has no internet access or there are some firewall/antivirus/infrastructure restrictions that voids the online activation you can select offline activation type instead. This document describes the offline activation process step-by-step:   Step 1. S32 Design studio for Arm/Power/Vision installer pops up the "S32DS Activation" dialog  where you first enter your activation ID and select activation type as offline Step 2. The Offline process will require to save an activation request file -"request.xml". Please save this file into a local folder or an USB drive. Step 3. Software will then require an activation response. To get this file move to a station with the Internet connection. We will get back here once we have activation response file ready. Step 4. Look for the Internet connection and take the "request.xml" file with you. Go to https://www.nxp.com/security/login  click on Apps and Services >  "Software Licensing and Support > Click on View Accounts chrome_2022-09-20_10-32-23.png jiri_kral_0-1663663175551.png Step 5. In product information page look for the "Offline Activation" option on the left menu. Step 6. Click on "Choose File" and select the "request.xml" file generated in Step 2.  Press "Process" button to get the "activation.xml" file. This file will be downloaded.   Step 7. Save "activation.xml" file and take it to the original offline station, go back to the Activation response dialog described by Step 3. Step 8.  Load file and installation will be finished. S32 design studio will be activated with your activation ID.
查看全文
Hello, the new release of S32DS for ARM v1.3 is available now in the download section of S32DS web page: http://www.nxp.com/s32ds   The Activation code is required to install the product. The activation code is different to previous versions (v1.1/1.2). You should get the appropriate Activation Code by a notification email which is send automatically when you proceed to the downloading: What is new?  New device supported: S32K144 v2.0 ARM64: Linaro GCC 4.9-2015.05 Fully integrated S32 SDK for S32K144 EAR release v0.8.2. including PinMuxing and Processor Expert configuration. FreeMASTER Serial Communication driver for S32K144 family  Highly Assembly Optimized version of Automotive Math and Motor Control Libraries for KEA and S32K devices v1.1.6  IAR debugger support by new project wizard Updated SEGGER and P&E debug plugins to the latest and greatest versions Reset functionality added with P&E debugger for single core projects (KEA, S32K devices) and A5 core for MAC57D54H Flash configuration supported for S32V234 Header files for KEA and MAC57D54H updated Advanced FreeRTOS kernel aware debug support Bug fixes Project Explorer updated to correctly show active build configuration resources     Note: The plugins to support GreenHills, IAR, iSystem, Lauterbach are not included and have to be installed from corresponding update site or installation.
查看全文
Function printf is C library function, which sends formatted output to stdout. Because microcontroller does not contain stdout, it it necessary to redirect it to a different type of output. One of the possible way is using UART. All MPC57xx has LinFlexD module, which supports UART mode.   For proper use the LinFlexD module, it is necessary to initialize it and also create simple functions for transmit and receive data. You can create your own file or use the file uart.c in the attachment. If you want to create your own file, please do not forget to implement the methods, which are called by MW MSL libraries to perform console IO (please look at the attached file uart.c).   In uart.h file, you will find correct function prototypes for functions used in uart.c and also some important enum data types.   Third important file is uart_console_io.c which you find in folder, where S32DS was installed. Open the folder and choose path: S32DS/e200_ewl2/EWL_C/src/sys. This file contains routines which implement low-level console IO routines.   Now, we have all basic files which help us to use printf function. So lets create new project and test printf. Example project is created for MPC5744P.   Create new project, choose EWL library and finish project wizard. Include stdio.h to the file, where you want to call printf function.   Now add uart.c and uart_console_io.c files to the project folder src. Add uart.h file to project folder include.   Initialize system clock and clock for peripherals (look at the attached project). In uart.c file, there are settings for GPIO pins, LinFlex initialization for UART mode and also baud rate calculation (please look at the uart.c file in the attachment).   Now it is possible to use printf function. Important point is, that \n character triggers the data sending. Also, if you do not use this \n character, you will get compile error, but I will explain this further in this tutorial.   Run some terminal emulation, for example Putty and use the following settings:   Now open terminal and  run the code in the microcontroller. This should be the result:   /*************************************************************************************************************************************************************************************/ /*************************************************************************************************************************************************************************************/ /*************************************************************************************************************************************************************************************/   This was the easiest way, how to use printf function. But printf also provides some format characters for printing decimals, floating points, etc. All options you can find in ewl_c_reference.pdf document which is place in S32DS installation folder S32DS/help/pdf.   When you want to use some of the characters mentioned above, you get the following compile error:   When you do not use any format characters in printf argument, function _EWL_CDECL puts(const char_t * s) from puts.c file is called on background. But when you use format characters in printf argument, function int_t _EWL_CDECL printf(const char_t * _EWL_RESTRICT format, ...) from printf.c file is called instead of puts.   Variable result saves value, which function __pformatter returns. But function __pformatter is not implemented. Instead of __pformatter, function __pformatterFP (placed in __printformat.c file) is implemented.   So there are two possible workarounds.   First workaround is place the following code to the Linker flags in project properties: -Xlinker --undefined=__pformatterFP -Xlinker --defsym=__pformatter=__pformatterFP   The code says that there is undefined symbol __pformatterFP (part -Xlinker --undefined=__pformatterFP) and define symbol alias __pformatter=__pformatterFP (-Xlinker --defsym=__pformatter=__pformatterFP ). So from my point of view, symbol __pformatter is replaced by __pformatterFP. Now the correct function is called and the project could be successfully built.     Second workaround is add the printf.c file from S32DS installation folder S32DS/e200_ewl2/EWL_C/src/stdio to the project src folder and exchange __pformatter for __pformaterFP. Clean project and recompile.       I hope this document helps you while implementing printf function in your projects.   Regards, Martin
查看全文
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM 2018.R1         February 6, 2017 NXP Semiconductors is pleased to announce the release of the S32 Design Studio for ARM 2018.R1 for Automotive and Ultra-Reliable MCUs. The S32 Design Studio is based on the Eclipse open development platform and integrates the Eclipse IDE, GNU Compiler Collection (GCC), GNU Debugger (GDB), and other open-source software to offer designers a straightforward development tool with no code-size limitations. Red highlighted items below are new/updated features in comparison to previous releases/updates. Release content (What is new?) Eclipse Neon 4.6 Framework GNU Tools for ARM® Embedded Processors (Launchpad) build (4.9.3 20150529) ARM64: Linaro GCC 4.9-2015.05 GNU Tools for ARM® Embedded Processors build (6.3.1 20170824) - supported by New Project Wizard for S32K1xx device. See the complete GNU ARM 6.3.1 release notes attached below. GCC Source code package is available here. Libraries included: newlib, newlib-nano and ewl2 (ewl and ewlnano). GDB 7.12.1 with Python P&E Multilink/Cyclone/OpenSDA (with P&E GDB Server) - updated (v3.3.5.201801101746) SEGGER J-Link (with SEGGER GDB Server) - updated (V6.22e_B180108) New Project wizard to create application and library projects for supported devices Fully integrated S32 SDK for S32K14x EAR release v.0.8.6. For the details on the feature set of SDK please refer to SDK Release notes and Reference Manuals. S32 SDK Release notes attached.Please note that S32K SDK has Early Access Release status, that means that there could be some limitations and issues. The S32K SDK is available for Windows host only. There is limitation on the supported GreenHills compiler version – the SDK released with GreenHills v2014.4, but due to GreenHills plugin limitation support for GreenHills compiler v2017.1 integrated, so new project wizard would not provide possibility to create SDK project with GreenHills compiler. SDK management included Sample Drivers for KEA family (Evaluation grade) FreeMASTER Serial Communication driver for KEA and S32K families Automotive Math and Motor Control Libraries for KEA,S32K and S32V234 devices supporting the ARM Cortex-M4 core v1.1.11 (the particular version availability for a device could be limited by supported compiler versions) Import projects from CodeWarrior for MCU v.10.6 and Kinetis Design Studio for respective supported processors IAR v7.x and v8.11.2 compiler support by new project wizard GreenHills v2017.1.4 compiler support by new project wizard iSystem, Lauterbach and IAR debuggers support by new project wizard. Kernel Aware debugging for FreeRTOS, OSEK. MQX 4.2 for MAC57D54H with possibility to create project from example Devices supported SKEAZN8, SKEAZN16, SKEAZN32, SKEAZN64, SKEAZ128, SKEAZ64 S32K144 v2.0, S32K142, S32K146, S32K148 S32V234 MAC57D54 Getting started page to allow the centralized access to documentation and additional materials Bug Fixes Updated header and register description files to fix issues and synchronize with latest Ref Manual versions [S32DS-4629] Clean rule doesn't work after particular user actions in "C/C++ Build -> Behavior" [S32DS-301] After some debugging work (using BP, Stepping, Resume...) Disassembly view content disappears. [S32DS-1093] Debugging session hangs when "c" step over is done on a loop statement that has its entire block in a single line. [S32DS-273] Can not suspend after set condition of breakpoint = 0 and resume [S32DS-61] Breakpoint properties disappeared after right-click into breakpoint [S32DS-6072] Unable to export S32K144 SDK project into ProjectInfo.xml The complete S32 Design Studio for ARM 2018.R1 release notes are attached below. Installation Notes Please visit the S32DS for ARM product page - download section to download the installer. The installer requires the NEW Activation ID to be entered during the installation. You should receive an email that includes your Activation ID after starting the download. Technical Support S32 Design Studio issues are tracked through the S32DS Public NXP Community space: https://community.nxp.com/community/s32/s32ds    
查看全文
Dear S32DS users, S32 Design Studio for Power v1.1 Update 1 has been released.  The Offline update package could be downloaded here:   https://www.nxp.com/webapp/Download?colCode=S32DS_PA_v1.1_UP1&appType=license&location=null&Parent_nodeId=14320533561557…    For online installation please select predefined NXP repository "Help" -> "lnstall New Software..." dialog:  ${p2.metadata.repo.name} - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_1_1/com.freescale.s32power.updatesite       The list of changes:  new compiler build 1.1.3 – see details in compiler release notes (attached) MS Visual C++ 2010 Redistributable x86 included for SPT tools for Windows 10 Updated SPT tools: ENGR00381373 - Error build after Generate SPT Fixed ADD, SUB, CMP when destination register is different from src1 ENGR00380758 64 bits operands are not supported for spt2 on windows  Updated Examples  New SPT1 example for MPC5775K o SingleElf_MPC5748G launch files updated with GDB command "set architecture powerpc:vle" Graph Tools ENGR00380255 [SPT] default graph should be created with standard includes Bug fixes: ENGR00375995 MPC5746C Embsys register definitons are missing SPI register set ENGR00379744 SPT assembler shall have initialized 'Include paths (-I) options after MPC577xK or S32R274 project creation ENGR00380796 Linker files section .spt should be corrected for SPT1/SPT2
查看全文
Bare-metal project migration from an older version of S32DS into a newer one is typically pretty straightforward. Despite of that the migration into S32DS Power v1.2+ requires more attention due the fact it includes a new version of GCC compiler + GCC binutils (see the GCC release notes - here). This version of GCC is now fully EABI VLE compliant  (in contrast to previous versions of S32DS Power  v1.0 and v1.1) and it has several consequences for the project migration object code/libraries are not backward compatible - if you have an object code/library built by a previous version of S32DS Power v1.x you have to rebuild it in new S32DS v1.2+ compiler. default compiler setup has changed - bitfield access is not volatile anymore. This may have a impact on a peripheral registers access via standard header file bitfield structures. Such access may require a specific load/store instruction e.g. "stw" but if compiler is allowed to optimize the access (e.g. use "stb" instead of "stw") an exception may occur. Therefore it is recommended to add  -fstrict-volatile-bitfields  flag into your project GCC compiler settings: linker script file (*.ld) requires some additional linker sections - Linker script file in S32DS Power v1.2+ must contain the sections below: •  KEEP for .init and .fini sections • .ctors and .dtors sections • .preinit array .init array and .fini array sections If the linker script file is not updated and the linker warnings are ignored you may experience an exception at the runtime - typically when __init routine is executed. Missing .init section causes that an invalid instructions is fetched and causes the core IVOR exception. There is an easy way how to automatically fix the linker script file issue directly in IDE. If you import and build an older project in S32DS Power v1.2 the linker issues these linker script related warnings: Right click on the warning and select Quick Fix: Select "Add missed section in linker script"  + "Select All" and press "Finish". Repeat these steps until all the linker script warnings disappears. If you don't use IDE project you have to add the sections below into your linker script manually: .text_vle : { INPUT_SECTION_FLAGS (SHF_PPC_VLE) *(.text.startup) *(.text) *(.text.*) KEEP (*(.init)) KEEP (*(.fini)) . = ALIGN(16); } > m_text /* that will force pick VLE .text sections */ .ctors : { __CTOR_LIST__ = .; /* gcc uses crtbegin.o to find the start of the constructors, so we make sure it is first. Because this is a wildcard, it doesn't matter if the user does not actually link against crtbegin.o; the linker won't look for a file to match a wildcard. The wildcard also means that it doesn't matter which directory crtbegin.o is in. */ KEEP (*crtbegin.o(.ctors)) KEEP (*crtbegin?.o(.ctors)) /* We don't want to include the .ctor section from from the crtend.o file until after the sorted ctors. The .ctor section from the crtend file contains the end of ctors marker and it must be last */ KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .ctors)) KEEP (*(SORT(.ctors.*))) KEEP (*(.ctors)) __CTOR_END__ = .; } > m_text .dtors : { __DTOR_LIST__ = .; KEEP (*crtbegin.o(.dtors)) KEEP (*crtbegin?.o(.dtors)) KEEP (*(EXCLUDE_FILE(*crtend?.o *crtend.o) .dtors)) KEEP (*(SORT(.dtors.*))) KEEP (*(.dtors)) __DTOR_END__ = .; } > m_text .preinit_array : { PROVIDE_HIDDEN (__preinit_array_start = .); KEEP (*(.preinit_array*)) PROVIDE_HIDDEN (__preinit_array_end = .); } > m_text .init_array : { PROVIDE_HIDDEN (__init_array_start = .); KEEP (*(SORT(.init_array.*))) KEEP (*(.init_array*)) PROVIDE_HIDDEN (__init_array_end = .); } > m_text .fini_array : { PROVIDE_HIDDEN (__fini_array_start = .); KEEP (*(SORT(.fini_array.*))) KEEP (*(.fini_array*)) PROVIDE_HIDDEN (__fini_array_end = .); } > m_text‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍‍ This may help you to avoid time consuming debugging to figure out the root cause of the core exception. 
查看全文
******************************************************************************** * Detailed Description: * This example shows, how to use printf function in project. * Files uart_console_io.c, uart.c and uart.h was added. These files contain * necessary functions for correct printf() functionality * * * Test HW:         FRDMPK144-Q100 * MCU:             PS32K144HFVLL 0N77P * Terminal:        9600-8-no parity-1 stop bit-no flow control on LPUART1 * Fsys:            160 MHz * Debugger:        Lauterbach Trace32 *                  PeMicro USB-ML-PPCNEXUS *                  OpenSDA embedded debug * Target:          internal_FLASH, internal RAM * EVB connection:  default
查看全文
Hello,   The new official release of S32DS for ARM v1.2 is available in the download section of S32DS web page: http://www.nxp.com/s32ds       To  install the product the Activation Code is needed. You can Find it under "License keys" tab.   S32 Design Studio is based on Eclipse open development platform and integrates the Eclipse IDE, GNU Compiler Collection (GCC), GNU Debugger (GDB), and other open-source software. This release supports Windows 7/8/8.1/10 (32/64 bit) and Linux versions as well.   S32DS ARM v1.2 main features Free of charge tool with no code size limitation (no license file required) Eclipse Luna 4.4 Framework GNU Tools for ARM embedded processors (launchpad, based on gcc 4.9.3) and ARM64: 4.9.3 20141031 Linaro Libraries included: newlib, newlib-nano and Freescale EWL2 (ewl and ewl-nano) SEGGER J-Link (with SEGGER GDB Server), P&E Multilink (with P&E GDB Server) Fully integrated S32 SDK for S32K144 EAR release v.0.8.1 SDK management included (KEA drivers, FreeMASTER for KEA, AMMCLIB for KEA and S32K) CodeWarrior/KDS project importer GreenHills/IAR compiler support by the new Project Wizard iSystem/Lauterbach debuggers support by the new Project Wizard Kernel Aware Debugging FreeRTOS, OSEK. Devices supported SKEAZN8, SKEAZN16, SKEAZN32, SKEAZN64, SKEAZ128, SKEAZ64 S32K144 S32V234 MAC57D54H   Technical Support S32 Design Studio is supported by NXP community - https://community.freescale.com/community/s32/s32ds/ For more details see the attached release notes.     * Red items are the new features   Regards, Stanislav  
查看全文
This short video discuss the main features introduced with the S32 Design Studio 3.6.0 A comparison between S32DS 3.5 and 3.6 in regards to the product architecture & release changes is shown, followed by a quick overview of the main features introduced that impact everyone using the new version of the toolset
查看全文
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Updates 5 and 6          What is new? S32 SDK for Power Architecture 1.0.0 RTM supporting MPC574xx.  Service Pack supporting MPC5775 B/E This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4 ). Installation instructions The update is available for online (via S32DS Eclipse Updater) or offline installation (direct download link) online installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use  direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
查看全文
This Example demonstrates an alternative way to multi-core projects. This is basically a single eclipse project that generates the single elf file for dual core MCU (MPC5777C) See the project structure below where the sources for each core are separated into a core specific source folder: Main core0 [e200z7_0] performs basic initialization (Clocks, ports..) Each core initializes the interrupt controller in order to service interrupts generated by PIT (Periodic Interrupt Timer): Core 0 (e200z7_0) services PIT channel 0 interrupts generated once per second. Core 1 (e200z7_1) services PIT channel 2 interrupts generated once per two seconds.
查看全文
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1 Update 8          What is new? S32 SDK for Power Architecture 1.8.0 EAR supporting MPC5777C, MPC5775B, MPC5775E, MPC5746R, MPC5745R, MPC5743R This is a cumulative update - it includes all of the content of previous updates (Update 1, Update 2, Update 3, Update 4, Updates 5 and 6, Update 7 ). Installation instructions The update is available for  (via S32DS Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_2017.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for Power product page -> Downloads section or use direct link to download the update archive zip file  Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive zip file you downloaded in the previous step Select all available items and click "Next" button.   This will start the update installation process.
查看全文
Installation & Activation HOWTO: Activate S32 Design Studio  HOWTO: Install Lauterbach TRACE32 debugger plug-in into S32 Design Studio  Create a New Project  HOWTO: Create APEX2 Project From Example in S32DS for Vision  HOWTO: Create An ISP Project From Example in S32DS for Vision  HOWTO: Create A53 Linux Project in S32DS for Vision  HOWTO: Create An ISP Project From Existing VSDK Graph in S32DS for Vision  HOWTO: Create A New Makefile Project With Existing Code From NXP Vision SDK Example Project   HOWTO: Build a Project and Setup a Debug Configuration for debugging in S32 Design Studio  HOWTO: Create A53 APEX2 and/or ISP Linux Project in S32DS for Vision DDR Configuration & Validation and Stress Test Tools HOWTO: Use DDR Configuration and Validation Tool  HOWTO: Use DDR Stress Test Tool  Hardware Setup HOWTO: Setup S32V234 EVB for debugging with S32DS for Vision and Linux BSP HOWTO: Prepare and boot S32V234 EVB from eMMC  HOWTO: Setup static IP address for S32 debug probe  Debugging HOWTO: Setup S32V234 EVB for debugging with S32DS for Vision and Linux BSP  HOWTO: S32V234-EVB debugging with Linux and gdbserver on target machine  HOWTO: Start Debug on an ISP Application Project with S32 Debugger and S32 Debug Probe  HOWTO: Start Debug on an APEX2 Application Project with S32 Debugger and S32 Debug Probe  Debugging the Startup Code with Eclipse and GDB | MCU on Eclipse   VSDK HOWTO: Change Vision SDK root in S32DS for Vision  HOWTO: Create A New Makefile Project With Existing Code From NXP Vision SDK Example Project  HOWTO: Prepare A SD Card For Linux Boot Of S32V234-EVB Using BSP From VSDK  Linux HOWTO: S32V234 EVB Linux - Static IP address configuration  HOWTO: S32V234 EVB Linux - DHCP IP address setup  HOWTO: Prepare A SD Card For Linux Boot Of S32V234-EVB Using BSP From VSDK  HOWTO: Access Linux BSP file system on S32V234-EVB from S32DS for Vision HOWTO: Setup A Remote Linux Connection in S32DS for Vision  General Usage HOWTO: S32 Design Studio Command Line Interface  HOWTO: Add user example into S32DS  HOWTO: Generate S-Record/Intel HEX/Binary file  HOWTO: Update S32 Design Studio  Troubleshooting Help! I just relaunched S32DS for Vision and my visual graph is collapsed!  Help! I just updated to new version of S32DS and now my projects have errors and I can't build!  Troubleshooting: PEmicro Debug Connection: Target Communication Speed  Troubleshooting: Indexer errors on header file  S32 Design Studio Offline activation issue hot fix  https://community.nxp.com/docs/DOC-345238 
查看全文
The FreeMASTER serial communication driver is a piece of code that enables an embedded application to communicate with the FreeMASTER PC application. Please note: The FreeMASTER_S32xx does not support all Toolchains and not all versions of supported Toolchains. The available SDKs will vary depending upon the toolchain which is selected. It is independent of the S32/MPC SDKs. In most cases, it is not integrated with the S32/MPC SDKs, although this could change in the future. When creating a new S32DS Application Project, you may have noticed the FreeMASTER_S32xx SDK option in the Select SDK menu. To add the FreeMASTER SDK to your project, simply add it in the New Project Wizard (as pictured above) or add it later through the project properties menu, SDKs: Select the desired SDK from the list, then click 'Attach/Detach...' Click in the column for each build configuration for which you wish to have the SDK attached. You can remove SDKs by clicking the '+', making it disappear. It should also be noted that there exists example projects which demonstrate usage of the FreeMASTER serial communication driver, though these do not use the FreeMASTER SDK, the driver was added manually. When working in your project, you can use the SDK Explorer to drag and drop macros and function calls into your code. To add the SDK Explorer to your perspective, there are at least 2 methods: 1) Menu method a) Window -> Show View -> Other... OR Alt + Shift + Q, Q b) Filter on 'SDK' c) Select 'SDK Explorer' d) Click OK 2) Quick Access method a) Type 'SDK' b) Select 'SDK Explorer' To access the macros and function calls from the SDK Explorer: 1) Go to the Project Explorer and select your project to make it active. 2) Go to SDK Explorer and all of the SDKs you included in the project will be listed. 3) For the SDK you wish to access, expand the folders and files until you can see the function you wish to add. You can set some filters to hide unwanted content. 4) Simply drag and drop the macro/function call into your source file. The #include statement for the associated header file will be automatically added near the top of your source file. Happy FreeMASTER serial communicating!
查看全文
        Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for Power Architecture 2017.R1         The Automotive Microcontrollers and Processors’ Embedded Tools Team at NXP Semiconductors, is pleased to announce the release of the S32 Design Studio for Power Architecture version 2017.R1. It is the successor of S32 Design Studio for Power v1.2. - the versioning scheme has changed. Release content (What is new?) Eclipse Neon 4.6 Framework GNU Build Tools for e200 processors (support VLE and BookE ISA, based on gcc 4.9.4 [7.October 2017], binutils 2.28 and gdb 7.8.2) - see the complete GCC release notes Libraries included: newlib, newlib-nano and Freescale EWL2 P&E Multilink/Cyclone/OpenSDA (with P&E GDB Server) - updated (v1.7.2.201709281658) New Project wizard to create application and library projects for supported devices Peripherals Register and Special Purpose Registers View Fully integrated MPC5748G/MPC5746C SDK EAR v.0.8.1. For the details on the feature set of SDK please refer to SDK Release notes attached and Reference Manuals (Please note that SDK has Early Access Release status, which means that there could be some limitations and/or issues. Also note, the SDK is available for Windows host only). SDK management included: o FreeMASTER Serial Communication driver (v2.0 August 31th 2016) o Automotive Math and Motor Control Libraries(v1.1.9) Windriver Diab compiler support by new project wizard Lauterbach, iSystem, and PLS debuggers support by new project wizard (The plugins to support Diab, iSystem, Lauterbach are not included and have to be installed from the corresponding update site or installation. The current version of the GreenHills plugin is not compatible with Eclipse Neon version, so it should not be used with this release) Kernel Aware debugging for FreeRTOS, eCOS, OSEK Devices supported: S32R274 S32R372 MPC5775K, MPC5774K MPC5746R, MPC5745R, MPC5743R MPC5777M MPC5777C MPC5748G, MPC5747G, MPC5746G MPC5744B, MPC5745B, MPC5746B, MPC5744C, MPC5745C, MPC5746C MPC5744P, MPC5743P, MPC5742P, MPC5741P MPC5601P, MPC5602P, MPC5603P, MPC5604P MPC5644B, MPC5644C, MPC5645B, MPC5645C, MPC5646B, MPC5646C MPC5601D, MPC5602B, MPC5602C, MPC5602D, MPC5603B, MPC5603C, MPC5604B, MPC5604C, MPC5605B, MPC5606B, MPC5607B MPC5606S MPC5604E MPC5644A, MPC5642A MPC5643L MPC5676R MPC5632M, MPC5633M, MPC5634M MPC5674F MPC5673K, MPC5674K, MPC5675K Collateral Getting Started page Bug Fixes C preprocessor tool added for C++ projects configuration The makefile generation is updated to fix and issue with building a project on the Korean version of Windows - Code page switch command cannot be executed. The Rename Project functionality is improved to cover referenced projects and launch configurations Complete S32 Design Studio for Power Architecture 2017.R1 release notes are available here Installation Notes To download the installer please visit the S32DS for Power Architecture product page: downloads section. The installer requires the the NEW Activation ID to be entered during the installation. You should receive an email that includes your Activation ID after starting the installer downloading process: Technical Support S32 Design Studio issues are tracked through the S32DS Public NXP Community space: https://community.nxp.com/community/s32/s32ds    
查看全文
      Product Release Announcement Automotive Microcontrollers and Processors S32 Design Studio for ARM® 2018.R1  Update 7          What is new? S32K1xx SDK BETA 2.9.0 supporting S32K116, S32K118, S32K142, S32K144, S32K146, and S32K148.  Also included is AMMCLIB 1.1.13 for S32K11x and S32K14x. This is a cumulative update - it includes all the content of previous updates (Update 1, Update 2, Update 3, Update 4, Update 5, Update 6) Installation instructions The update is available for  (via Eclipse Updater) or offline installation (direct download link)  installation:  go to menu "Help" -> "Install New Software..." dialog  select predefined update site "S32DesignStudio - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_ARM_2018.R1/updatesite" select all available items and click "Next" button   offline installation:   go to S32 Design Studio for ARM product page -> Downloads section or use direct link to download the update archive zip file Start S32DS and go to "Help" -> "Install New Software..." Add a new "Archive" repository and browse to select the downloaded update archive .zip file you downloaded in the previous step Select all available items and click "Next" button.   This will starts the update installation process.
查看全文
S32DS ARM2.2 K144xx fPic Example description. Provided example demonstrate possibility of creation Position Independent Code using  standard  S32DS ARM 2.2 tools.  Example code blink RGB LED using svc interrupt handler. Output  picExample.bin should be loaded via restore gdb command only into existing K144 RAM area(0x1fff8000 – 20007000 for EVB board), then pc set to startup value.(see picExample_Debug_RAM_PNE_fpic  Debug configuration). Note: restore gdb command needs absolute path to *.bin file. Example is based on standard K144 application. Changes: -fPIC option should be set(Project->Properties->C/C++ Build ->Settings->Standard S32DS Compiler->Miscalenous->Position Independent Code). Create flash image checkbox should bes set.( Project->Properties->Cross Settings -> Create flash image). Flash Image output file format  should be set to Raw binary(Project->Properties->C/C++ Build ->Settings->Standard S32DS Create Flash Image ) Add -nostdlib linker option(Project->Properties->C/C++ Build ->Settings->Standard S32DS Linker->General ->No startup or default libs). Existing S was modified(stack pointer was corrected, bl instead of blx for function calls was used. Standard linker script was modified(see example) Interrupts vector table was moved to data area. Due to this vector addresses are corrected on startup by FixGot routine(see SystemInit()c) Common RAM area was declared starting from 0. __got_start and __got_end were declared in Global Offset Table   For an in-depth analysis and step-by-step guide on the topic of implementing position-independent code, please see the following blog at mcuoneclipse.com: Position-Independent Code With GCC for arm Cortex M 
查看全文