NFC Knowledge Base

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC Knowledge Base

Discussions

Sort by:
This post provides guidance on how to port the example projects from the NXP NCI 2.0 NFC library to the MCXW71 Wireless MCU using SPI interface to communicate with PN7160 SPI EVK. To follow this guide, please use the following environment: MCUXpresso IDE 25.06.136. FRDM-MCXW71 SDK v25.12.00 (last available for MCUXpresso IDE). FRDM-MCXW71. OM27160B1 (PN7160 SPI EVK). Hardware Setup. The MCXW71 complies with the Arduino header standard as the OM27160B1 board, therefore you can connect directly the shield over the FRDM-MCXW71 as the pin connection match among both, allowing an easy connection between the devices. Take into consideration that this setup forces us to use the LPSPI1 instance of the MCXW71, it is possible to use another instance, but we would not be able to connect the boards directly, rather we would need to do the connections with jumpers. RomanVR_2-1776964886314.png Downloading base projects and adapting for MCXW71 port. To start with the porting work, download the NXP-NCI example project from this page. This compressed file contains the base project for different boards that will allow us to do the required modifications to add support for the MCXW71. Once downloaded, extract the SW6705 file into a known path (e.g. the Downloads folder) to later import the project to the IDE. The extracted folder should contain a .zip file with the examples that we will later import to the IDE. RomanVR_3-1776965056204.png Download the FRDM-MCXW71's SDK from the SDK Builder page, make sure to select the 25.12.00 version, as it is the latest SDK available to use along the MCUXpresso IDE. RomanVR_5-1776965144996.png Now we have to import the NXP-NCI2.0_MCUXpresso_examples.zip file we previously extracted to the IDE's workspace, to do so, click on the Import project(s) from file system and in the Project archive (zip) tab, browse for the extracted file of step 1 (NXP-NCI2.0_MCUXpresso_examples.zip) and click on Next >. NOTE: Don’t worry if the IDE shows an error message for not having the SDKs of the default boards (iMXRT1170, LPC55S6x, LPC82x) or having a different version, close the warning message, we only need these examples to copy the NCI library and example files. RomanVR_6-1776965251263.png RomanVR_7-1776965305716.png Your workspace should now look like the following image: RomanVR_8-1776965374185.png Import the hello_world example from the FRDM-MCXW71 SDK: RomanVR_9-1776965452594.png RomanVR_0-1777063242176.png Add the SPI drivers to the imported project by right clicking over the project, hover the cursor over the SDK Management option and select the option Manage SDK Components: RomanVR_11-1776966112046.png Select the driver, click Ok and if you are asked to refresh files accept it, after this you should be able to see the driver in the "drivers" folder of the project. RomanVR_12-1776966161256.png Copy the contents of the source folder of the iMXRT1170 project, as well as the NfcLibrary folder and paste them into the imported hello_world project: RomanVR_13-1776966215404.png         RomanVR_14-1776966224634.png Make sure to delete the hello_world.c and hello_word.mex files as we won't need it again. RomanVR_15-1776966329391.png            RomanVR_16-1776966350734.png After this process your project should look like the following image: RomanVR_17-1776966416175.png To avoid compiling issues, exclude from the build the files nfc_example_P2P.c and nfc_example_RW.c, to do so right click on the file, go to Resource Configurations and select Exclude from Build… and select for all configurations. Do this for each file. RomanVR_18-1776966481521.png Add the preprocessor macro: BOARD_NXPNCI_INTERFACE_SPI, as this is used by the example to select the interface with the board. To do this, right-click on the project and select Properties, then drop-down the C/C++ Build option and go to the Settings tab. Here, add the macro in the Preprocessor option, click on Apply and accept the index rebuild. RomanVR_19-1776966571549.png Add the root folder in C/C++ General > Paths and Symbols > Source Location tab, click on Ok and then Apply: RomanVR_20-1776966631332.png Still in Paths and Symbols, go to the Includes tab and add the source, TML and tool folders from workspace, click Ok and Apply. Make sure to add them one by one. RomanVR_21-1776966724329.png Now, go to C/C++ Build > Settings > Includes and add the following folders from Workspace. You can select all of them and add them at the same time or also do it one by one. Once done, click on Apply and Apply and Close. If you are asked to rebuild the index, do it. "${workspace_loc:/${ProjName}/source/TML}" "${workspace_loc:/${ProjName}/source/tool}" "${workspace_loc:/${ProjName}/NfcLibrary}" "${workspace_loc:/${ProjName}/NfcLibrary/inc}" "${workspace_loc:/${ProjName}/NfcLibrary/NdefLibrary}" "${workspace_loc:/${ProjName}/NfcLibrary/NdefLibrary/inc}" "${workspace_loc:/${ProjName}/NfcLibrary/NdefLibrary/src}" "${workspace_loc:/${ProjName}/NfcLibrary/NxpNci20}" "${workspace_loc:/${ProjName}/NfcLibrary/NxpNci20/inc}" "${workspace_loc:/${ProjName}/NfcLibrary/NxpNci20/src}" RomanVR_22-1776966780932.png Source Code Changes. In the board folder, open the board.h file and add the following definitions to refer to the peripherals and clocks to be used. Please notice that you may change the LPSPI instance, however you would need to connect jumpers instead of connecting directly the shield over the FRDM. #ifdef BOARD_NXPNCI_INTERFACE_SPI #define BOARD_NXPNCI_SPI_CLOCK (CLOCK_GetIpFreq(kCLOCK_Lpspi1)) #define BOARD_NXPNCI_SPI_INSTANCE (LPSPI1) #define BOARD_NXPNCI_SPI_BAUDRATE (400000) #endif #define BOARD_NXPNCI_IRQ_PORT (GPIOC) // J2.10 - GPIO0 [PN7160] - IRQ -> J2.10 GPIOC0 [MCXW71] #define BOARD_NXPNCI_VEN_PORT (GPIOA) // J4.1 - GPIO1 [PN7160] - VEN -> J1.8 GPIOA21 [MCXW71] #define BOARD_NXPNCI_DWL_PORT (GPIOA) // J4.2 - GPIO2 [PN7160] - REQ -> J1.7 GPIOA20 [MCXW71] #define BOARD_NXPNCI_IRQ_PIN (0U) #define BOARD_NXPNCI_VEN_PIN (21U) #define BOARD_NXPNCI_DWL_PIN (20U)   Now we need to add the required clock, peripheral and pin initialization for our board. To do this, go to the hardware_init.c file inside the board folder, and overwrite the BOARD_InitHardware function with the following: void BOARD_InitHardware(void) { BOARD_InitPins(); BOARD_BootClockRUN(); BOARD_InitDebugConsole(); CLOCK_SetIpSrc(kCLOCK_Lpspi1, kCLOCK_IpSrcFro192M); CLOCK_SetIpSrcDiv(kCLOCK_Lpspi1, kSCG_SysClkDivBy16); }   To add the correct pin multiplexing and configuration for our SPI and GPIO pins, go to the pin_mux.c file (also in the board folder) and overwrite the BOARD_InitPins function with the following: void BOARD_InitPins(void) { /* Clock Configuration: Peripheral clocks are enabled; module does not stall low power mode entry */ CLOCK_EnableClock(kCLOCK_GpioA); CLOCK_EnableClock(kCLOCK_GpioC); CLOCK_EnableClock(kCLOCK_PortA); CLOCK_EnableClock(kCLOCK_PortB); CLOCK_EnableClock(kCLOCK_PortC); /*IF SHORTING SH11, SH12, SH13, SH14 needed for LPSPI1*/ const port_pin_config_t portb0_pin46_config = {/* Internal pull-up resistor is enabled */ (uint16_t)kPORT_PullUp, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPSPI0_PCS0 */ (uint16_t)kPORT_MuxAlt2, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTB0 (pin 46) is configured as LPSPI1_PCS0 */ PORT_SetPinConfig(PORTB, 0U, &portb0_pin46_config); const port_pin_config_t portb1_pin47_config = {/* Internal pull-up resistor is enabled */ (uint16_t)kPORT_PullUp, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPSPI0_SIN */ (uint16_t)kPORT_MuxAlt2, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTB1 (pin 47) is configured as LPSPI1_SIN */ PORT_SetPinConfig(PORTB, 1U, &portb1_pin47_config); const port_pin_config_t portb3_pin1_config = {/* Internal pull-up resistor is enabled */ (uint16_t)kPORT_PullUp, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPSPI0_SOUT */ (uint16_t)kPORT_MuxAlt2, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTB3 (pin 1) is configured as LPSPI1_SOUT */ PORT_SetPinConfig(PORTB, 3U, &portb3_pin1_config); const port_pin_config_t portb2_pin48_config = {/* Internal pull-up resistor is enabled */ (uint16_t)kPORT_PullUp, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPSPI0_SCK */ (uint16_t)kPORT_MuxAlt2, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTA19 (pin 14) is configured as LPSPI1_SCK */ PORT_SetPinConfig(PORTB, 2U, &portb2_pin48_config); /*IF SHORTING SH11, SH12, SH13, SH14 needed for LPSPI1*/ const port_pin_config_t irq_pin = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullUp, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as PTC0 */ (uint16_t)kPORT_MuxAsGpio, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTC0 (pin 37) is configured as PTC0 */ PORT_SetPinConfig(PORTC, 0U, &irq_pin); const port_pin_config_t ven_pin = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullDisable, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as PTA20 */ (uint16_t)kPORT_MuxAsGpio, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTA20 (pin 17) is configured as PTA20 */ PORT_SetPinConfig(PORTA, 20U, &ven_pin); const port_pin_config_t req_pin = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullDisable, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as PTA21 */ (uint16_t)kPORT_MuxAsGpio, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTA21 (pin 18) is configured as PTA21 */ PORT_SetPinConfig(PORTA, 21U, &req_pin); const port_pin_config_t portc2_pin39_config = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullDisable, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPUART1_RX */ (uint16_t)kPORT_MuxAlt3, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTC2 (pin 39) is configured as LPUART1_RX */ PORT_SetPinConfig(PORTC, 2U, &portc2_pin39_config); const port_pin_config_t portc3_pin40_config = {/* Internal pull-up/down resistor is disabled */ (uint16_t)kPORT_PullDisable, /* Low internal pull resistor value is selected. */ (uint16_t)kPORT_LowPullResistor, /* Fast slew rate is configured */ (uint16_t)kPORT_FastSlewRate, /* Passive input filter is disabled */ (uint16_t)kPORT_PassiveFilterDisable, /* Open drain output is disabled */ (uint16_t)kPORT_OpenDrainDisable, /* Low drive strength is configured */ (uint16_t)kPORT_LowDriveStrength, /* Normal drive strength is configured */ (uint16_t)kPORT_NormalDriveStrength, /* Pin is configured as LPUART1_TX */ (uint16_t)kPORT_MuxAlt3, /* Pin Control Register fields [15:0] are not locked */ (uint16_t)kPORT_UnlockRegister}; /* PORTC3 (pin 40) is configured as LPUART1_TX */ PORT_SetPinConfig(PORTC, 3U, &portc3_pin40_config); }   To add the required interfacing APIs specific of our chip, we need to modify the tml.c file from the TML folder, in this file overwrite the functions: INTF_INIT, INTF_WRITE and INTF_READ with the following: static void INTF_INIT(void) { lpspi_master_config_t userConfig; uint32_t srcFreq = 0; /*SPI configuration*/ LPSPI_MasterGetDefaultConfig(&userConfig); userConfig.baudRate = BOARD_NXPNCI_SPI_BAUDRATE; srcFreq = BOARD_NXPNCI_SPI_CLOCK; userConfig.whichPcs = (lpspi_which_pcs_t)kLPSPI_Pcs0; userConfig.pcsActiveHighOrLow = (lpspi_pcs_polarity_config_t)kLPSPI_PcsActiveLow; /*Initialize SPI*/ LPSPI_MasterInit(BOARD_NXPNCI_SPI_INSTANCE, &userConfig, srcFreq); } static status_t INTF_WRITE(uint8_t *pBuff, uint16_t buffLen) { uint8_t temp[1000]; temp[0] = 0x7F; memcpy(temp+1, pBuff, buffLen); masterXfer.txData = temp; masterXfer.rxData = NULL; masterXfer.dataSize = buffLen+1; masterXfer.configFlags = kLPSPI_MasterPcs0 | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;; return LPSPI_MasterTransferBlocking(BOARD_NXPNCI_SPI_INSTANCE, &masterXfer); } static status_t INTF_READ(uint8_t *pBuff, uint16_t buffLen) { status_t status; uint8_t temp[257]; temp[0] = 0xFF; masterXfer.txData = temp; masterXfer.rxData = temp; masterXfer.dataSize = buffLen+1; masterXfer.configFlags = kLPSPI_MasterPcs0 | kLPSPI_MasterPcsContinuous | kLPSPI_MasterByteSwap;; status = LPSPI_MasterTransferBlocking(BOARD_NXPNCI_SPI_INSTANCE, &masterXfer); if(status == kStatus_Success) memcpy(pBuff, temp+1, buffLen); SDK_DelayAtLeastUs(10, SDK_DEVICE_MAXIMUM_CPU_CLOCK_FREQUENCY); return status; } #endif   We also need to overwrite the functions: tml_Init, tml_DeInit and tml_Reset to adapt them to use the specific APIs for the GPIOs of our board. static Status tml_Init(void) { gpio_pin_config_t in_config = {kGPIO_DigitalInput, 0}; gpio_pin_config_t out_config = {kGPIO_DigitalOutput, 0}; GPIO_PinInit(BOARD_NXPNCI_IRQ_PORT, BOARD_NXPNCI_IRQ_PIN, &in_config); GPIO_PinInit(BOARD_NXPNCI_VEN_PORT, BOARD_NXPNCI_VEN_PIN, &out_config); GPIO_PinInit(BOARD_NXPNCI_DWL_PORT, BOARD_NXPNCI_DWL_PIN, &out_config); INTF_INIT(); return SUCCESS; } static Status tml_DeInit(void) { GPIO_PortClear(BOARD_NXPNCI_VEN_PORT, 1U << BOARD_NXPNCI_VEN_PIN); return SUCCESS; } static Status tml_Reset(void) { /* Set DWL_REQ low for NCI protocol */ GPIO_PortClear(BOARD_NXPNCI_DWL_PORT, 1U << BOARD_NXPNCI_DWL_PIN); GPIO_PortClear(BOARD_NXPNCI_VEN_PORT, 1U << BOARD_NXPNCI_VEN_PIN); Sleep(10); GPIO_PortSet(BOARD_NXPNCI_VEN_PORT, 1U << BOARD_NXPNCI_VEN_PIN); Sleep(10); return SUCCESS; }   Finally, modify the main file so it uses the APIs to initialize our board clocks and pins: #include <stdio.h> #include <string.h> #include "app.h" #include "board.h" #include "pin_mux.h" #include "fsl_debug_console.h" extern void nfc_example (void); int main(void) { BOARD_InitHardware(); #ifdef BOARD_NXPNCI_INTERFACE_I2C PRINTF("\nRunning the NXP-NCI2.0 example (I2C interface)\n"); #else PRINTF("\nRunning the NXP-NCI2.0 example (SPI interface)\n"); #endif nfc_example(); } Testing the example. At this point we have everything set to build and flash our example with SPI interface, you may proceed to build and debug/flash the example by pressing the blue beetle button: RomanVR_23-1776969017743.png Once the example is flashed, open a serial terminal such as Teraterm with the following settings: Baudrate: 115200. Data: 8 bits. Parity: None. Stop bits: 1 bit. No flow control. While running, the example should output the following logs to the terminal: RomanVR_24-1776969098939.png When a tag is placed near the antenna, the example should print the tag information in the terminal as shown: RomanVR_25-1776969122735.png  
View full article
RF power regulation is a critical factor in the development of NFC devices, as it directly influences performance, reliability, and compliance with industry standards. There are three main reasons for this:  If the PN7642 VUP current exceeds the limit given by the product Data sheet, the PN7642 can be damaged. If too high RF power is radiated from the antenna, there exists a risk for NFC Cards. Too high RF power might lead to exceeding a given RF limit (NFC Forum, ISO, EMVCo). NXP provides comprehensive documentation on Dynamic Power Control for the PN7642 and PN5190. Designers are expected to adhere to these guidelines, especially when aiming for compliance with standards such as EMVCo. PN5190 Dynamic Power Control Quick Calibration and TxShaping Demo Automatic DPC Calibration for PN7642 and PN5190 However, if the user's design is intended for infrastructure applications, such as a smart lock. At a minimum, Dynamic Power Control (DPC) should be enabled to serve as a current limiter. The evaluation can be done with the help of NFC Cockpit.  1// Start DPC Calibration  "Press" Start DPC Calibration  "Press" Load protocol  Make sure that the DPC is "Enabled" Tomas_Parizek_0-1760618955468.png 2// Adjust current reduction table  Set all entries to "0" Write into EEPROM Tomas_Parizek_0-1760618870172.png   3// Set the "Target" current Use approx. the same current as "TxLDO Values"  The limit may be set higher, e.g., to 300 mA, if the purpose is solely to provide overcurrent protection for the IC. Save to EEPROM Restart the board (Close port -> Press VEN->Open port) Tomas_Parizek_0-1760618702129.png   4// Check the power regulation  Start DPC Calibration  Place a card or any metal object in the antenna's proximity  Observe VDDPA and "TxLDO" current  The current should stay around the given target  The VDDPA will drop once the antenna is loaded  Tomas_Parizek_2-1760619391451.png 5// Set a minimum VDDPA in DPC  In the case that the current is still too high, a user can define a minimum VDDPA that is used for the DPC regulation. By default, this value is set to 2.2V. The user can decrease it up to 1.5V.  In that case, NXP also recommends disabling the RDOn control.  Tomas_Parizek_1-1761307899864.png Note: The User has to consider the "DPC_TXLDO_MAX_DROPOUT" parameter, which defines the maximum voltage drop on TXLDO. By default, it is set to 3.6 V. That means if the user wants to use the minimum VDDPA 1.5 V, then the maximum TXLDO input shall not exceed 5.1 V. This feature protects the TXLDO from overheating.    Once the evaluation is done, the customer shall program the following EEPROM entries in their application. For more info, see PN7642 Product Data sheet.  DPC_CONFIG (Address: 0x0068) -> example: enabled -> 0x01 DPC_TARGET_CURRENT (Address: 0x0069) -> example: 229 mA -> 0xE5 DPC_TXLDO_MAX_DROPOUT (Addresses: 0x0073 - 0x0074) -> example: 3.6 V -> 0x10,0x0E DPC_TXLDOVDDPALow (Address: 0x006F) -> example: 1.5 V -> 0x00 DPC_HYSTERESIS_LOADING (Address: 0x006B) -> example: 20 mA -> 0x14 DPC_HYSTERESIS_UNLOADING (Address: 0x006E) -> example: 10 mA - 0x0A DPC lookup table entries (Addresses: 0x007D - 0x0125) -> example: for current limitation only -> all 0x00 If a user does not want to use a maximum range of VDDPA during DPC (5.7V), e.g., their system uses a 3.3V supply domain. Then, the maximum VDDPA in DPC can be limited by the following EEPROM settings:  TXLDO_VDDPA_MAX_RDR (Address: 0x0007)-> example: 3.0 V -> 0x0F Note: TXLDO has approx. 0.3V voltage drop. Always set this parameter 0.3V lower. Once this is done, the user has to check the "TxLDO" current and adjust the target current accordingly. In this case, to approximately 150 mA. If you don´t change it, the DPC starts to limit the power around 229 mA, as has been set in a previous step.  Tomas_Parizek_0-1761307791719.png
View full article
this is a step by step guider to port PN7160 to Android 14 on i.MX 8M Nano board
View full article
The Raspberry Pi Foundation released the Raspberry Pi 5 in October 2023, Raspberry Pi 5 features the Broadcom BCM2712 quad-core Arm Cortex A76 processor @2.4GHz, making it up to three times fast than Raspberry Pi 4.   The latest version of Raspberry Pi OS is Bookworm. However, some customers found the PN7160 is not detected over I2C/SPI on the Raspberry Pi 5. Running "i2cdetect -y 1" produces a blank table, and running "nfcDemoApp poll" results in an "nfcservice init fail" message. The incompatibility appears to be between the PN7160 and the new Raspberry Pi OS—Bookworm.  This reason is Raspberry Pi OS received a major update in Linux Kernel 6.6,  the classic way of GIPO handling no long work.   In step 6, a new GPIO interface is introduced to resolve the incompatibility issue. This article is a step-by-step guide to port PN7160 NCI2 stack to Raspberry Pi OS--Bookworm.   Hardware setup: For detail information about Raspberry Pi 5, please refer to below link.  https://www.raspberrypi.com/products/ danielchen_0-1729324169624.png   The PN7160 EVK board must be connected to Raspberry Pi using the following instructions:   Raspberry Pi 5 board pin NFC controller board signal #1 3.3V PWR VDD (PAD) +5V VBAT and VDD (UP) #16 GPIO23 IRQ #18 GPIO24 VEN #22 DWL_REQ #6 GND #5 I2C_SCL #3 I2C_SDA   danielchen_1-1729324214785.png   This matches the Raspberry Pi version of OM27160A1EVK (I2C variant).  The kit can then be plugged on Raspberry Pi 5 board to run the example. First of all, assemble the PN7160 NFC controller board (OM27160A1HN or OM27160B1HN) with the Raspberry Pi interface board (OM29110RPI)   danielchen_2-1729324261302.png    Then stacked together the boards with the Raspberry Pi board. danielchen_3-1729324294665.png     Software Setup: 1    Install Rasp 5 OS -Bookworm We use Raspberry Pi Imager tool to install Raspberry Pi OS (64bit, Bookworm). Click choose device and select Raspberry Pi 5, next click choose OS and select an operating system –Raspberry Pi OS (64-bit) , and select Micro SD card. Next we can write the Image to the Micro SD card. danielchen_4-1729324360355.png   2 Enable i2c interface 1). Run command:     sudo raspi-config   danielchen_5-1729324408868.png   2). Use the down arrow to select "Interface Options" danielchen_0-1729324525908.png   3). Arrow down to "I5 I2C"   danielchen_1-1729324564799.png   4). Select "yes" when it asks you to enable I2C 5). Use the right arrow to select the <Finish> button To verify the i2c interface is enabled, enter the following command: $ ls /dev/i2c* The Pi should respond with “ /dev/i2c-1” which represents the user-mode i2c interface to which is connected the PN7160 danielchen_2-1729324627935.png    3 Install necessary tools   We need to use APT commands to install , update software package in Raspberry Pi OS, please refer to  below link. https://www.raspberrypi.com/documentation/computers/os.html Libtool needs to be installed to run the NCI stack.    4 Clone Linux libnfc-nci library repository NFC NCI library is available from the following repository: https://github.com/NXPNFCLinux/linux_libnfc-nci $ git clone https://github.com/NXPNFCLinux/linux_libnfc-nci.git -b NCI2.0_PN7160   danielchen_3-1729324690006.png   5 Apply 64bit patch To install on 64bit OS, we need to apply 64bit patch.  It is under folder linux_libnfc-nci/64bit_patch/ROOT_src.patch   6 Modifications for GPIO Raspberry Pi OS (Bookworm) received a major update which includes the Linux kernel 6.6.   In the new OS update, the classic way of interfacing with GPIO has been deprecated.  Unfortunately our PN7160 NCI stack still interact with GPIO using /sys/class/gpio pseudo-filesystem,  low level control of GPIOs no longer work with Bookworm.  So we need to use the new GPIO interface on the Raspberry PI: libgpiod.  At this point Raspberry OS with a kernel 6.6 both libgpiod and gpiod are not pre-packaged and we need to install them.   6.1  Installation of gpiod tools danielchen_4-1729324839785.png We can look more into what is installed danielchen_5-1729324942850.png   The output of gpioinfo reports all of the available GPIO lines, by default for all chips. 6.2 Installation of the gpio libraries If we want to install libraries for development we need to do the following danielchen_6-1729325031223.png   Here is the info on libgpiod-dev danielchen_7-1729325104084.png   danielchen_8-1729325127909.png   The development package installs the C libraries and header files for us to use. Namely, the /usr/include/gpiod.h C header file and the /usr/lib/arm-linux-gnueabihf/libgpiod.so Shared Library.   6.3 Modifications in PN7160 NCI2 library. In source code, we need to add the gpiod library support 6.3.1 Makefile.am  danielchen_9-1729325179442.png   6.3.2 src/nfcandroid_nfc_hidlimpl/halimpl/tml/transport/NfccAltTransport.cc danielchen_10-1729325241358.png    ...... danielchen_11-1729325277575.png danielchen_12-1729325305421.png     and src/nfcandroid_nfc_hidlimpl/halimpl/tml/transport/NfccAltTransport.h danielchen_13-1729325356759.png   If you need the modified source code files, please let me know. I can send the source code changes to you.    7 Configure the library danielchen_14-1729325396498.png   danielchen_15-1729325419517.png     8 Set the library to map i2c interface danielchen_16-1729325461585.png   9 Build and install the library   $ make $ sudo make install $ export LD_LIBRARY_PATH=/usr/local/lib   10 Run & Verify the NFC functionality   danielchen_17-1729325515743.png   This demo works as expected.   Summary: Porting PN7160 NCI2 stack to Raspberry Pi 5, we need to follow PN7160 Linux porting guide and update the classic GPIO interface to gpiod libraries.   Happy porting 😊
View full article
https://community.nxp.com/docs/DOC-340244 
View full article
This post contains a step by step guide of how to use PN7150 with i.MX RT1060. This document is structured as follows: Overview of PN7150 PN7150 is a Plug-and-Play all-in-one NFC solution for easy integration into any OS environment like Linux and Android, reducing Bill of Material (BoM) size and cost. The embedded Arm® Cortex®-M0 microcontroller core is loaded with the integrated firmware, simplifying the implementation as all the NFC real-time constraints, protocols and the device discovery (polling loop) are processed internally. In few NCI commands, the host SW can configure the PN7150 to notify for card or peer detection and start communicating with them. It has the following salient features: Full NFC forum compliancy with small form factor antenna Embedded NFC firmware providing all NFC protocols as pre-integrated feature Direct connection to the main host or microcontroller, by I2C-bus physical and NCI protocol Ultra-low power consumption in polling loop mode Highly efficient integrated power management unit (PMU) allowing direct supply from a Battery Hardware Requirements      1. OM5578/PN7150ARD      2. i.MX RT1060 EVK Evaluation Board + usb micro cable        Using PN7150 with i.MX RT1060 Hardware Connections The hardware connections are simple. Both the EVKB-IMXRT1060 board and OM5578/PN7150ARD board have an Arduino interface. So, mount the PN7150ARD board with male Arduino connector onto the female Arduino connector of the EVKB-IMXRT1060 board.  Running the Demo If this is the first time you’re using EVK-MIMXRT1060 board, follow the getting started guide first: i.MX RT1060 Evaluation Kit | NXP . Make sure to install the SDK package for EVK-MIMXRT1060 board which is required for the project to run.   Download the ‘evkbimxrt1060_PN7150’ package which you will find attached to this post. Drag and drop the downloaded package to the “Project Explorer” tab of your MCUXpresso IDE workspace (If you don’t have MCUXpresso, it can be downloaded for free from here: https://www.nxp.com/support/developer-resources/software-development-tools/mcuxpresso-software-and-tools/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE Now that the package has been imported to the MCUXpresso IDE (via drag and drop), click on Debug icon from the Quickstart panel to begin a debug session. Once the debug session has started, click on the run icon to run the code: After step 3, the project should be running now. The project contains basic discovery loop functionality. Here is how the output looks in the console tab on MCUXpresso: Bring any NFC card near the PN7150 board’s antenna and the output console will show the detection and type of the card. For example, in the picture below, we can see that type 4 card was detected: Available Resources AN11990 NXP-NCI MCUXpresso example document. (https://www.nxp.com/docs/en/application-note/AN11990.pdf) The example project explained in this project was ported to i.MX RT1060 using section 5.3 and 6 of the above mentioned document. PN7150 datasheet (https://www.nxp.com/docs/en/data-sheet/PN7150.pdf) PN7150 User Manual (https://www.nxp.com/docs/en/user-guide/UM10936.pdf) PN7150 NFC Controller SBC Kit User Manual  (https://www.nxp.com/docs/en/user-guide/UM10935.pdf)
View full article
This page contains information about the supported NXP MCU/MPU and NXP NFC product combinations which have ready to use packages. These can be used as a reference. The table below contains link to where you can find the projects as well.    MCU ↓   NFC IC →  NTAG I²C  plus NTAG 5 PN7150 CLRC663 plus family* PN5180 i.MX RT1050 i.MX RT1050 + NTAG I²C plus i.MX RT1050 + CLRC663 plus   Video: Using i.MX RT1050 with CLRC663 plus family and the NFC Reader Library | NXP  i.MX RT1060 i.MX RT1060 + NTAG I²C plus  i.MX RT1060 + PN7150 i.MX 8M Mini i.MX 8M Mini + PN7150 (Andriod) i.MX 8M Mini + PN7150 (linux-yocto) i.MX 7 Dual Sabre i.MX7 Dual Sabre + PN5180 LPC1769 LPC1769 + CLRC663 plus LPC1769 + PN5180 LPC55S69 LPC55S69 + NTAG I²C plus LPC55S69 + NTAG 5 LPC55S69 + PN7150 LPC55S69 + CLRC663 plus LPC55S69 + CLRC663 plus + SE050 (smart lock) LPC11u37h LPC11u37 + PN7150 LPC11u37h + CLRC663 plus LPC11u68 LPC11u68 + PN7150 LPC82X LPC82X + PN7150 LPC845 LPC845 + CLRC663 plus Kinetis K82F K82F + CLRC663 plus K82F + PN5180 Kinetis K64F K64F + PN7150 K64F + CLRC663 plus Kinetis K63 K63 + PN7150 Kinetis K24 K24 + PN7150 KW41Z KW41Z + NTAG I²C plus KW41Z + NTAG 5 KW41Z + PN7150 *CLRC663 plus family: CLRC663 plus, MFRC630 plus, MFRC631 plus, SLRC610 plus For more information on the NFC products, please visit https://www.nxp.com/nfc
View full article
Introduction The secure firmware download example "DownloadLibEx1" from LPC55S16 Host Software demonstrates how the user can update the PN7642 NXP secure firmware via the Host Interface. This post describes how to enable the download via UART. Resources needed to follow this guide LPC55S16 Host Software Version 02.02.00 LPCXpresso55S16 Development Board OM27642: Development Kit for PN7642 Secure Compact NFC Controller Hardware Connections On the PN7642 there are various shifters and multiplexers in between the host and the actual PN7642 inputs. In order to bypass them quickly, we will interconnect the boards as follows. UART Tx and Rx: Locate J68 on the PNEV7642A board. These 4 jumpers are the host interface connectors (ATX_A, ATX_B, ATX_C, ATX_D). Take the jumpers off as we are going to directly connect to this pin-header. EduardoZamora_0-1781124699804.png LPC55S16-EVK   PNEV7642A Eval Board Pin Signal (LPC)   Pin Signal (PNEV) J12-14 UART Tx → J68-2 UART Rx J12-16 UART Rx ← J68-8 UART Tx JP12-17 GND ↔ J47-6 GND IRQ, VEN and DWL_REQ connection Note: In this case, please do not remove the jumpers of J45 and J20 on the PNEV7642A, we are going to attach the jumpers directly onto those headers. EduardoZamora_0-1785967035261.png Also, please remove the jumper on J25.   IRQ VEN DWL_REQ LPC55S16-EVK J13-1 J12-12 J13-3 PNEV7642A J45 J20 J25-2 In order to select the UART Host Interface in the PNEV7642A, we need to set the HIF switches (SW5-SW7) as indicated: EduardoZamora_0-1784052280049.png Software Prior to the following steps, please follow section 8 of the PN76 family evaluation board quick start guide. To run the example in UART mode, first we need to compile the following libraries: EduardoZamora_1-1784052475173.png EduardoZamora_2-1784052493978.png Please compile the main example the exact same way after this. EduardoZamora_6-1784053460818.png Code Modifications: In lpc55S16Board.c (LPC55S16_Lib/source) In the “lpc55S16Board_Init” function we need to add the following lines in order to enable one the ports and the clock for the USART of the Flexcomm2 peripheral. EduardoZamora_8-1784053796090.png GPIO_PortInit(GPIO, 1); CLOCK_AttachClk(kFRO12M_to_FLEXCOMM2); In pin_mux.c (LPC55S16_Lib/board) In the “BOARD_InitPins” functions we need to add the following line to enable GPIO 1’s clock. EduardoZamora_9-1784053928400.png CLOCK_EnableClock(kCLOCK_Gpio1); In phHdll_Lib.c (Hdll_Lib/comps/phHdllLib/src) In this file we are going to include the following library: EduardoZamora_10-1784054328036.png #include "fsl_usart.h" In the “phHdll_Lib_HalHwExchange” function we are going to add the following lines right after performing the UART transmission of the command. EduardoZamora_11-1784054370469.png while(USART2->FIFOSTAT & 0x40) { USART_ReadByte(USART2); } This is done to empty the RX FIFO of the UART before performing a reception, in order to prevent reading errors. In fsl_usart.c (LPC55S16_Lib/drivers) In the “USART_ReadBlocking” function please copy the line 625 and paste it again after clearing the reception flags. EduardoZamora_12-1784054430177.png This is done in order to avoid erroneous interpretation of the RX frame. In DownloadLibEx1.c Lastly, we need to change the path of the ESFWU files to the local path where the files will be located. Please visit PN7642 Product Page, Software section to download the Firmware file. EduardoZamora_13-1784054476381.png Final Build: Now we need to rebuild the main example, and we should be able to flash and debug after this. EduardoZamora_0-1786041828193.png
View full article
The PN7642/PN5190/PN7220 requires a calibration before the RF field is switched on for the first time with unloaded condition. "Unloaded" means: Without any additional metal in proximity of the antenna, except for the NFC reader components itself. During development of new readers, this calibration shall be done each time the antenna design, antenna matching, or EMC filter is modified. See a workflow of the Initial calibration for PN7642 done in NFC Cockpit.  PN7642_Initial_Calibration.png During this procedure, the RF Field is switched on for approx. 11 ms, and the calibration data is saved in the memory. Note: Please note that the registers and EEPROM addresses might differ for a different products. Always check the Datasheet for the used product. 
View full article
The PN7642 includes a USB interface, which allows USB communication with the PC.  Once the PN7642 USB communication is established, the NFC Cockpit tool can be used for RF debugging.  Note: This also requires flashing the NFC Cockpit application with the help of the mass storage mode or SWD interface.  Basically, the user has to connect a USB cable/Connector to the following PN7642 pins.  USB Signal  PN7642 Pin  5V  USB_VBUS Data - ATX_D Data + ATX_C GND GND   See an example below. This is a very basic connection (for evaluation or debugging only) where the USB cable is directly connected to the PN7642 pads.  This situation may arise during debugging on customer hardware where the USB interface is not yet implemented on the PCB. But a user wants to debug with the help of NFC Cockpit.  Tomas_Parizek_0-1758200945725.png   Please note that the proper USB interface might require special layout rules, such as impedance, overvoltage protection, etc.. For more info, see the PN7642 EVK reference schematic or USB PCB design guide. 
View full article
This might be convenient if the user wants to use NFC Cockpit on their device.  See the photo of PNEV5190BP EVK with the instructions.      Tomas_Parizek_2-1758172713000.png    1. Place R5 and R7, keep R6 open    2. Place R20, keep R19 open Note: This step depends on the voltage domain used in the external hardware. If R19 is placed -> 1.8V domain, if R20 is placed -> 3.3V domain.    3. Remove VBAT, VBAT_PWR, and VUP jumpers to disconnect the "internal" PN5190 located on the EVK    4. Connect the following SPI lines to external PN5190 (e.g., customer HW) SPI_CLK SPI_MOSI SPI_MISO SPI_CS NFC_IRQ GND Note: It is also necessary to disconnect the external PN5190 from the customer MCU. 5. Connect VEN to the external PN5190  NFC_VEN   Now, the external PN5190 HW should communitate with the MCU located in PNEV5190BP, and the NFC Cockpit can be used. The user should see that the blue LED is on. If the red LED is blinking, there is an issue, and the user should check the connections/supply. 
View full article
A user can evaluate the current consumption of PN7642 in low power modes with the help of the PN7642 Evaluation Board (OM27642) and:  MCUXpresso SKD example (LPCD)  NFC Cockpit or MCUXpresso SKD example (ULPCD) NXP defines the current consumption in ULPCD/LPCD as VBAT current + VDDIO current for the LPCD/ULPCD cycle time of 330 ms. Make sure that DC/DC is disabled (for ULPCD).  Where:  VBAT current = VBAT_Current + VBATPWR_Current + VUP_Current See the snapshot from the PN7642 Datasheet below:  Tomas_Parizek_3-1753772522698.png   See where to measure the currents on PN7642 EVK: J63 and J64 are used for enabling/disabling the LEDs that are connected to PN7642 GPIOs. They must be disabled for a proper VDDIO current measurement.  A modification of R69 and R70 is necessary to perform the current measurement on VDDIO in LPCD mode. Tomas_Parizek_1-1759325994089.png   1. ULPCD current consumption evaluation For the ULPCD evaluation, the NFC Cockpit or SDK example can be used. In this article, we will focus on evaluation using the NFC Cockpit.  See the used ULPCD configuration:  Tomas_Parizek_0-1778131034323.png Note: The current should be measured as an average over, e.g., 30 seconds.  1.1 Overall ULPCD current measurement  To measure all currents together on PN7642 EVK, a user can create a measurement fixture as shown below:  Tomas_Parizek_0-1759471417973.png Real setup :  Tomas_Parizek_1-1759414417352.png Then the overall results look as follows: Tomas_Parizek_1-1778131365857.png Note: The Antenna is tuned to approx. 35 Ohms  In this case, the ULPCD current is approximately 21 μA. This current can be further optimized, for more details, see -> AN14518(Start-up optimization in ULPCD (PN5190/PN7642/PN76AC)) 2. LPCD current consumption evaluation The user has to import the example (pnev7642fama_nfc_low_power_mode_Pub) from the PN7642 SDK.  Before building it, the following change in the code has to be made:  -> Comment line 84 Tomas_Parizek_0-1753279011326.png   A user can adjust the LPCD cycle time as shown below: Tomas_Parizek_0-1753781089650.png   1.1 VBAT Current measurement  Tomas_Parizek_0-1754311084128.png   In this case, the VBAT current is approximately 123 μA. 1.2 VBATPWR current measurement  Tomas_Parizek_1-1759218118702.png In this case, the VBAT_PWR current is approximately 91,8 μA. 1.3 VUP Current measurement  Tomas_Parizek_0-1759217512751.png In this case, the VBAT_PWR current is approximately 32,8 μA.  Note: This current depends on the LPCD VDPPA settings + Antenna Impedance tuning  1.4 VDDIO Current measurement Note: Before VDDIO measurement, place jumpers J63 and J64 on PN7642 EVK. This will disable LEDs that are connected to PN7642 GPIOs.  The VDDIO current measurement requires the following steps:  Run the "pnev7642fama_nfc_low_power_mode_Pub" example  Once the example is running, disconnect the debugger (J-link, LPC-Link...) from J21 (NFC Debug connector)    Remove R70  Populate a 10K resistor on the R69 position (it disables the SWD interface) Once the measurement is done, change it back to the default state (R70=0R, R69=Open). Note: It is recommended to prepare the board with the option to easily populate or remove R70 and R69 when the LPCD example is running. E.g., with the help of jumpers/pin headers as shown below.   Tomas_Parizek_2-1754383701294.png Only then will the correct VDDIO be measured on PN7642 EVK.  See the VDDIO current measurement below:  Tomas_Parizek_0-1754382925680.png   In this case, the VDDIO current is approximately 5,48 μA.  Then the overall current comsumption in LPCD is I_VBAT + I_VDDIO= (123 + 91,8 + 32,8 + 5,48) = 253,08 μA Note: For this measurement, the NFC Cockpit is not suitable because the IC does not go into standby mode between LPCD RF pings. Meaning LPCD works normally, but a user can measure higher current consumption. Used Ampere meter -> Power Profiler Kit II Measurement has been performed with FW 2.6  Board supply (jumpers J1, J2 and J4) -> 3.3V Please note that this measurement is indication only! 
View full article
This article describes how to evaluate ULPCD feature together with PN7642 EVK (OM27642EVK) and NFC Cockpit.  1// Disable DC-DC in EEPROM  OM27642EVK does not required any HW changes for ULPCD (**). User is only required to change the following settings in EEPROM  (disable DC-DC converter). Address: 0x0000 (Secure_Lib_Config) Value: 0x21  Reset the board after writing the value.  Tomas_Parizek_0-1745904468298.png **Note: To ensure an accurate and reliable ULPCD evaluation—particularly for ULPCD current measurements. We strongly recommend implementing the following hardware modifications on the OM27642EVK. PN7642_MB.png Note: New revision of the board already have R4=DNP, R8=0Ω. Kindly check this on your board. 2//Set required ULPCD settings in EEPROM  ULPCD VDDPA -> Typically 1.5V. If the HF attenuator is 0x00, increase e.g. to 1.8V. Since the detection range does not significantly depend on the power level, there is no need to set VDDPA above 2 V. Higher VDDPA results in increased current consumption in ULPCD, but does not significantly improve detection performance. RF On Guard time -> This value can be reduced to the minimum -> 5.2 us RSSI Guard time -> Recommended value is 25 RSSI Threshold -> Typically 4~6 Number of RSSI samples -> Typically -> 0 (4 rounds) PN7642_EEPROM_ULPCD.png 3// Perform "Reads HF Attenuator"  Once the required ULPCD settings is set (Guard times, Threshold....). Then User has to perform "Reads HF Attenuator". Make sure that the "HF Attenuator" option is checked.  As written above, the value must not be 0x00. If so, increase VDDPA. 4// Perform ULPCD Calibration and check RSSI Value  For OM27642EVK, the RSSI value for unloaded antenna is typically around 1400dec - 1600dec. 5//Enter ULPCD mode  User can enter the ULPCD mode. The board will again be connected once the load change is detected (e.g. NFC card or smartphone in the antenna proximity). 6// Typical detection performance for 65 mm x 65 mm Antenna tuned to 35Ω.   Tomas_Parizek_0-1782466647959.png MIFARE DESFire EV3: Class 1 Antenna  ICODE SLIX: Class 1 Antenna  ICODE 3: Class 6 Antenna 
View full article
  Some customers are trying to update the user firmware on PN7642 through host interface and using “DownloadLibEx1” demo,  and they are using SFWUMaker to create .esfwu file from .bin followed the readme file but failed to do a firmware update. Here is a step-by-step guide to do it. I will use the SDK led blinky demo,  and generate an Esfwu file , and program it into PN7642 board with LPC5516 host.  Led blinky demo is in PN7642_MCUXpresso_SDK_02-15-00_PUB.  You can download it from PN7642 product page.  Single-Chip Solution with High-Performance NFC Reader, Customizable MCU and Security Toolbox | NXP Semiconductors Step 1: compile pnev7642fama_led_blinky demo Please make sure the flash size is 180KB.  By default,  the output flash size is 180KB with MCUXpresso IDE. danielchen_0-1727969697151.png     Step 2: Bin file generation The binary (.bin) file is not generated by default, we can do it manually by doing following: Build your target application Open the debug/release folder in MCUXpresso Right-click on the *.axf file Choose 'Binary Utilities' → 'Create binary' in the menu The .bin should appear danielchen_1-1727969750247.png   Step 3: Make an ESFWU file To convert a bin file to an ESFWU file, we can use the ESFWU Maker Utility (sw810311). It can be downloaded from PN7642 product page. It is a secure file, and you need to have an active NDA to get it.  To run this utility, the toml file is very important.  You need to change the output name and binary name according to your project ,  and  you need to use the correct aes_root_key. For other parameters, we left them unchanged.   3.1   change the output name and binary name danielchen_2-1727969831738.png   3.2 set the correct aes_root_key The application flashed via SWD is a bin file and NOT encrypted neither is it flashed with our bootloader. The .esfwu file via host interface is encrypted and flashed by our own bootloader.  The keys have to be valid, else the bootloader will not be able to decrypt the received file. Please make sure we are using the right keys to create the user application firmware.  This is crucial and without it, it won’t work anyways. The default keys are mentioned in the datasheet as transport keys. See below picture.  But it is highly recommended to provision your own keys!  Please have a look at the secure key mode application note for further information on that.   danielchen_3-1727969857833.png   danielchen_4-1727969899780.png    If you are not sure whether you have provisioned the root key or not, you can check the SKM state by running SKM demo. if the root key is provisioned, please use the provisioned root key.  From below picture, I can see that the app_root_key is  not provisioned, so I use the default transport key. danielchen_5-1727969952354.png     3.3  use the EsfwuMaker command to generate the Esfwu file.   danielchen_6-1727969995698.png   After this command, we can get the esfwu file.   danielchen_7-1727970036883.png     Step 4: Secure firmware download   We use the firmware download example to update the PN7642 firmware.  It is in the host software package, it  holds examples to be used with LPC55S16 and MCUXpresso, to interact with the PN7642. The LPC55S16 Host Software can be download from PN7642 product page. LPC55S16 Host Software Version 02.01.00 (nxp.com) To run the demo, we need to edit the firmware location.  In file DownloadLibEx1.c,  about line 60.   danielchen_8-1727970075699.png     Please set the correct hardware settings as below.  we have to stack the PNEV7642A Rev-B development board on top of the LPC55S16-EVK board. Align Pin.1 of J36 of the PNEV7642A Rev-B development board with Pin.1 of J9 of the LPC55 board. The last 4 pins, 17 - 20, of J12 of the LPC board are not connected. As well as pin 1-4 of J10 stay unconnected, as below picture shows.   danielchen_9-1727970111317.png     Run the firmware download Demo with LPC55s16,  see the log output below.  Choose option “6” to update your application firmware. The update may take a while.  At the end, a successful update is indicated by the prompt of “Successful firmware upload ”.     danielchen_10-1727970154067.png     To verify it is successful, we can run this demo, please keep J65 open.  you will see the D7 (RED LED) blinky (0.5 HZ rate). If you need the pnev7642fama_led_blinky.esfwu, please let me know.    
View full article
Using an alternative clock source to set up PN7462's contact interface clock , so that we have more options of the clock frequency.
View full article
Example sends Wi-Fi credentials from phone to IoT device, so it can join the Wi-Fi network.  Using: iOS and Android phone with NXP's TagWriter app PN7462 NFC Reader device on PNEV7462B eval board, part of kit OM27462CDK Host Card Emulation mode example based on NfcrdlibEx8_HCE_T4T example from NFC Reader Library Example will also print out other NDEF messages received.  NDEF formats include: Contacts / Business Cards URL link Wi-Fi network and credentials Bluetooth MAC address for pairing Email address Phone number Geo location Launch application on host OS Plain text SMS (sorry the audio is horrible)
View full article
https://community.nxp.com/docs/DOC-340389 
View full article
The NXP-NCI example is based on NXP-NCI lib and LPCopen lib, and due to the good consistency, the porting is mainly focus on LPCopen lib switching.   Software setup download lpcopen package via http://www.nxp.com/assets/downloads/data/en/software/lpcopen_3_01_lpcxpresso_nxp_lpcxpresso_11u68.zip  download SW3241 via https://www.nxp.com/webapp/Download?colCode=SW3241&amp;appType=license&amp;location=null&fsrch=1&sr=3&pageNum=1&Parent_n…  import NXP-NCI_LPC11Uxx_example by LPCXpresso v8.1.4.   LPCopen porting remove *.h and *.c in the folder of LPC11Uxx/inc and LPC11Uxx/src. 2.import header files and c files from lpc_chip_11u6x/inc and lpc_chip_11u6x/src to LPC11Uxx/inc and LPC11Uxx/src 3. repeat step 2 , import source files and header files from lpc_board_nxp_lpcxpresso_11u68/inc and lpc_board_nxp_lpcxpresso_11u68/src to Drivers/inc and Drivers/src. 4.Change MCU settings 5.Change project settings. 6.compiling error fixes: 6.1 solution: replace with i2c_11u6x.h 6.2 solution: 6.3 solution: create a template project for LPC11U6x and import the source file of "cr_startup_lpc11u6x.c"   Porting Result   This porting guide is for LPC11U68 Xpresso v2 Rev C, and can also be used a reference when you try to port NXP-NCI examples to other lpcxpresso boards.   Please kindly refer to the attachment for details. Original Attachment has been moved to: NXP-NCI_LPC11Uxx_example.zip
View full article
Environments & Devices --Hardware 1、PN7462 DEMO Board(PNEV7642B) --Software 1、Ubuntu 16.04 desktop 2、Test tools ---libusb ---pcsc-lite ---ccid driver ---opensc          Before testing, please install above test tools to Ubuntu 16.04 according to document on the link https://community.nxp.com/docs/DOC-334952 !          Then follow steps below to begin testing PN7462 DEMO board by above test tools. 1、Update firmware of PN7462 DEMO board          Please update firmware of PN7462 DEMO board according to UM10915.pdf, then test it on windows, ensuring PN7462 DEMO board can normally work at CCID protocol on window platform. 2、Connecting PN7462 DEMO Board to PC USB via USB OTG Cable.          On PENV7462B side, X3 connector should be used for USB OTG cable. 3、Using lsusb to list USB devices weidong@ubuntu:~$ lsusb Bus 002 Device 002: ID 0e0f:0003 VMware, Inc. Virtual Mouse Bus 002 Device 003: ID 0e0f:0002 VMware, Inc. Virtual USB Hub Bus 001 Device 001: ID 1d6b:0002 Linux Foundation 2.0 root hub Bus 002 Device 001: ID 1d6b:0001 Linux Foundation 1.1 root hub Bus 002 Device 004: ID 0e0f:0008 VMware, Inc. Bus 002 Device 005: ID 1fc9:0117 NXP Semiconductors          Last line is PN7472 DEMO board. 4、Open 2 terminals at the same time on Ubuntu desktop (1) One terminal is used to run “pcsc” command weidong@ubuntu:~$ sudo /usr/local/sbin/pcscd -adf [sudo] password for weidong: 00000000 pcscdaemon.c:345:main() pcscd set to foreground with debug send to stdout 00012288 configfile.l:361:DBGetReaderList() Parsing conf file: /usr/local/etc/reader.conf.d 00000037 pcscdaemon.c:658:main() pcsc-lite 1.8.22 daemon ready. 00023126 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x1D6B, PID: 0x0001, path: /dev/bus/usb/002/001 00000101 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x1D6B, PID: 0x0001, path: /dev/bus/usb/002/001 00000113 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x0E0F, PID: 0x0003, path: /dev/bus/usb/002/002 00000112 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x1D6B, PID: 0x0001, path: /dev/bus/usb/002/001 00000160 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x0E0F, PID: 0x0002, path: /dev/bus/usb/002/003 00000152 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x0E0F, PID: 0x0008, path: /dev/bus/usb/002/004 00000115 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x0E0F, PID: 0x0008, path: /dev/bus/usb/002/004 00000165 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x0E0F, PID: 0x0002, path: /dev/bus/usb/002/003 00000263 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x1D6B, PID: 0x0002, path: /dev/bus/usb/001/001 ^V56546837 hotplug_libudev.c:651:HPEstablishUSBNotifications() USB Device add 00000101 hotplug_libudev.c:297:get_driver() Looking for a driver for VID: 0x1FC9, PID: 0x0117, path: /dev/bus/usb/002/006 00000007 hotplug_libudev.c:436:HPAddDevice() Adding USB device: PN7462 USB Reader 00000045 readerfactory.c:1074:RFInitializeReader() Attempting startup of PN7462 USB Reader (1.00) 00 00 using /usr/local/lib/pcsc/drivers/ifd-ccid.bundle/Contents/Linux/libccid.so 00127887 readerfactory.c:949:RFBindFunctions() Loading IFD Handler 3.0 00000236 ifdhandler.c:1965:init_driver() Driver version: 1.4.27 00000477 ifdhandler.c:1982:init_driver() LogLevel: 0x0003 00000004 ifdhandler.c:1993:init_driver() DriverOptions: 0x0000 00000165 ifdhandler.c:111:CreateChannelByNameOrChannel() Lun: 0, device: usb:1fc9/0117:libudev:0:/dev/bus/usb/002/006 00000021 ccid_usb.c:302:OpenUSBByName() Using: /usr/local/lib/pcsc/drivers/ifd-ccid.bundle/Contents/Info.plist 00000727 ccid_usb.c:320:OpenUSBByName() ifdManufacturerString: Ludovic Rousseau ([email protected]) 00000016 ccid_usb.c:321:OpenUSBByName() ifdProductString: Generic CCID driver 00000004 ccid_usb.c:322:OpenUSBByName() Copyright: This driver is protected by terms of the GNU Lesser General Public License version 2.1, or (at your option) any later version. 00000433 ccid_usb.c:656:OpenUSBByName() Found Vendor/Product: 1FC9/0117 (PN7462 USB Reader) 00000005 ccid_usb.c:658:OpenUSBByName() Using USB bus/device: 2/6 00000021 ccid_usb.c:717:OpenUSBByName() bNumDataRatesSupported is 0 00128471 ifdhandler.c:382:IFDHGetCapabilities() tag: 0xFB3, usb:1fc9/0117:libudev:0:/dev/bus/usb/002/006 (lun: 0) 00000027 readerfactory.c:396:RFAddReader() Using the reader polling thread 00004709 ifdhandler.c:382:IFDHGetCapabilities() tag: 0xFAE, usb:1fc9/0117:libudev:0:/dev/bus/usb/002/006 (lun: 0) 00000023 ifdhandler.c:477:IFDHGetCapabilities() Reader supports 1 slot(s) (2)The other terminal is used to run “"testpcsc " in pcsc-lite/src source code weidong@ubuntu:~/ccid/pcsc-lite-1.8.22/src$ ./testpcsc   MUSCLE PC/SC Lite unitary test Program   THIS PROGRAM IS NOT DESIGNED AS A TESTING TOOL FOR END USERS! Do NOT use it unless you really know what you do.   Testing SCardEstablishContext        : Command successful. Testing SCardIsValidContext   : Command successful. Testing SCardIsValidContext   : Invalid handle. (don't panic) Testing SCardListReaderGroups      : Command successful. Group 01: SCard$DefaultReaders Testing SCardFreeMemory               : Command successful. Testing SCardListReaders        : Command successful. Testing SCardListReaders        : Command successful. Reader 01: PN7462 USB Reader (1.00) 00 00 Waiting for card insertion        :          2 screenshots for above 2 terminals: 5、Test cards (All cards are contactless) (1) MIFARE Plus x 4K card Re move it: (2) MIFARE Nano card          Note: testpcsc should be run again. Remove it: (3) MIFARE EV1 card Remove it: 6、Using Opensc-tool to Test cards            Open a new terminal for running the command, please! (1)No cards (2) MIFARE Plus x 4K card (close to antenna , then run opensc-tool) (3) MIFARE Nano card (4) MIFARE EV1 card    TIC Weidong Sun 2018-07-09
View full article
The latest NXP-NCI example is rev 1.6, and when you run this demo with the lpc11xx board, for example, lpc1115 rev A, and the OM5577, you may meet the following issue: The problem is due to two aspects: one is hardware and the other is software. For hardware solution, besides following what is described in AN11658 section 2.4 LPC11xx, you have to do one more thing: a) The I2C lines are not pulled-up: LPC11xx doesn't offer internal pull-up setting of the I2C lines so external pull-up resistors must be added. For software solution, the function of Sleep()( in tool.c) was optimized too much, and it didn't meet the timing requirement of OM5577, so we should let the IDE ignore it. The solution I use is as below: __attribute__((optimize("O0"))) void my_func() { blah } You may check the attachment for details. The result is shown as below: Original Attachment has been moved to: tool.c.zip
View full article