Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
imx95 sai1 SAI1_MCLK Hi, The SAI1_MCLK and UART2_RXD of IMX95 are multiplexed. However, UART2 also uses the debug port of M33. My codec is connected to the sai1 interface. How can the PAD_UART2_RXD pin be reused as SAI1_MCLK I tried as follows: pinctrl_sai1: sai1grp { fsl,pins = < IMX95_PAD_UART2_RXD__AONMIX_TOP_SAI1_MCLK 0x31e IMX95_PAD_SAI1_RXD0__AONMIX_TOP_SAI1_RX_DATA_BIT0 0x31e IMX95_PAD_SAI1_TXC__AONMIX_TOP_SAI1_TX_BCLK 0x31e IMX95_PAD_SAI1_TXFS__AONMIX_TOP_SAI1_TX_SYNC 0x31e IMX95_PAD_SAI1_TXD0__AONMIX_TOP_SAI1_TX_DATA_BIT0 0x31e >; }; However, the following error will be reported: [2.079005] scmi-pinctrl-imx scmi_dev.8: Error set config-13 [2.084536] scmi-pinctrl-imx scmi_dev.8: pin_config_set op failed for pin 118
View full article
MCXW23はAOA(到来角)機能をサポートしていますか? こんにちは、NXPさん。 MCXW23はAOA(BLEによる到来角)機能に対応していますか? この機能を使って場所を特定する必要があります。 ありがとうございました。 通信および制御(I3C | I2C | SPI | FlexCAN | イーサネット | FlexIO) Re: Can MCXW23 support AOA (angle-of-arrival) function ? こんにちは、アナさん。 わかった。どうもありがとうございました。 しかし、お客様は位置情報機能を備えたBLEを必要としているため、MCXW72は評価対象となる選択肢の一つです。 再度、感謝します。 Re: Can MCXW23 support AOA (angle-of-arrival) function ? こんにちは、 あなたの調子が良いといいのですが!   MCXW23ではAOA(到来角)はサポートされていません。位置特定アプリケーションにおいては、このデバイスはUWBトラッキングタグおよび位置特定ソリューションのコンパニオンチップとして機能することを目的としています。UWBサポートの詳細については、NXP SemiconductorsのTrimension ® 超広帯域無線(UWB: Ultra-Wideband)ページをご覧ください。 あるいは、MCXW72ファミリはチャネルサウンディングによる位置特定にも対応しています。詳細については、アプリケーションノートAN14865「KW47およびMCXW72のチャネルサウンディングの基礎」を参照してください。   よろしくお願いします、 アナ・ソフィア。 Re: Can MCXW23 support AOA (angle-of-arrival) function ? こんにちは。NXP製品にご関心をお寄せいただきありがとうございます。 MCX W72を潜在的な解決策としてご検討ください。開発を支援するための評価ボードも用意されており、その中にはチャネルサウンディング**アプリケーション**向けに特別に設計されたMCXW72-LOCも含まれています。 他に質問があれば、遠慮なくお尋ねください! よろしくお願いします、 アナ・ソフィア。
View full article
TypeA Layer3 Card Detection on PN7642 Hello All, I'm using the demo pnev7642fama_Nfcrdlib_SimplifiedAPI_ISO_Freertos_Pub for card detection, there are E_PH_NFCLIB_MIFARE_CLASSIC_1K and E_PH_NFCLIB_TYPEA_LAYER4  application cases, and it works well. But there is no application for E_PH_NFCLIB_TYPEA_LAYER3, I tried to implement the application based on the card datasheet, but  there was no response, the status of phNfcLib_Transmit() was always 0x20000. The card used are FM1208-10 and FM1216. I couldn't find the reason.  I have no idea why there is no application case for E_PH_NFCLIB_TYPEA_LAYER3, Is there any references for this card type?  Thanks. Re: TypeA Layer3 Card Detection on PN7642 Hello @wangea, Hope you are doing well. Layer 3 covers anti-collision, UID selection and card activation, while ISO 14443 layer 4 presents a set of standardized commands for data exchange. Basic Tags/Cards stop after Layer 3 and use proprietary memory-read/write commands instead of Layer 4. As you mentioned, you could try to implement the proprietary command set for your device. Please refer to NxpNfcRdlib -> types -> ph_Status.h for the Status Code definitions. Regards, Eduardo.
View full article
Edgelock RW612 Zephyr Hello, I would like to store cetificates and private key in the edge lock secure enclave of the RW612. My application is developed using zephyr and I need to be able to provision those certificates and read them at run time. Is this supported ? Could you provide documents / guides on how to do that. I am currently using upstream Zephyr 4.2.0 Thanks. Re: Edgelock RW612 Zephyr Hello @benjaminaxiles, hope you are doing well. Would you please provide more details on your expected application functionality to provision the certificates/private key? Are you expecting the provisioning to be done with an specific transport? In the meantime, I suggest referring to the examples "zephyr/samples/tfm_integration/psa_crypto" and "modules/lib/nxp_iot_agent/zephyr/samples/el2go_agent", as these implement different approaches to key storage and provisioning, in particular, the "el2go_agent" example is meant to demonstrate how to use the Edgelock 2GO service to provision keys and certificates. As a side note, I would suggest migrating to latest Zephyr downstream/upstream versions, as the support for RW612's security features has been modified since version 4.2.0. Please let me know if this information is helpful.
View full article
S32K344 MDIO MDC support >2.5 MHz? The S32K344 EMAC peripheral MAC_MDIO_Address.CR field supports CSR clock dividers down to /4, for up to a 20 MHz MDC (with 80 MHz AIPS_PLAT_CLK). Many PHYs and other MDIO devices support MDC >2.5 MHz, and this can be very helpful for reducing transaction runtimes. Experimentally, we have been able to configure the S32K344 MDIO bus for this higher speed and interface with an external PHY.  However, we noticed the S32K344 datasheet ("MDIO Timing Specifications") publishes a max supported MDC frequency of just 2.5 MHz. A faster MDC would be helpful for our application; despite the datasheet specification, does the S32K344 provide any official support for running MDC >2.5 MHz? Re: S32K344 MDIO MDC support >2.5 MHz? Thank you! Re: S32K344 MDIO MDC support >2.5 MHz? Hello @andye , The EMAC register interface may allow divider settings that would nominally generate an MDC frequency above 2.5 MHz. However, for S32K344 the officially supported maximum MDC frequency is the value published in the datasheet, i.e. 2.5 MHz. Therefore, operation above this limit cannot be considered officially supported. Even if communication appears to work at a higher MDC frequency in a specific setup, this would be outside the published specification and should be treated as application-specific experimental behavior. In practice, increasing MDC reduces the available timing margin for MDIO setup/hold and output valid timing, and it also makes the interface more sensitive to the RC time constant of the MDIO line (for example due to pull-up resistance, bus capacitance, routing, and the number of attached devices).  Best regards, Pavel
View full article
S32K3 I2S Audio Output Example? Is there an S32K3 example that demonstrates playing (or recording) audio over an I2S based CODEC such as the SGTL5000? Re: S32K3 I2S Audio Output Example? Hello @hns80, Could you please enter an internal case (support ticket) instead?  There are some materials which can be shared, but under NDA. You can submit one through Support Tickets. Best regards, Julián
View full article
ESFWU Maker Utility Hi All, I'm trying to flash a FW in a PN7642 via I2C. I've the correct HW setup (LPC EVK board and PN7642 EVK connected), and I can flash supplied firmwares. My problem now is I cannot find the ESFWU Maker Utility (sw810311) mentioned to create suitable binaries myself. Step by Step Guide to update user firmware through host interface for PN7642  Cannot find it in secure resources for PN7642. Regards, Re: ESFWU Maker Utility Hi Eduardo, I found it under other name. HOST CRYPTO SCRIPTS. I'm pending my NDA reactivation. Thanks and Regards, Re: ESFWU Maker Utility Hello @V_Palacio, Hope you are doing well. I apologize for the inconvenience, this software is secured under NDA (Non-Disclosure Agreement) and must be requested through the Secure Access Rights. For further information on how to request Secure Resources, I would recommend checking the Secure Access Rights FAQs | NXP Semiconductors. Regards, Eduardo.
View full article
errors with S32M24xEVB I have tried example codes for this kit and the S32M24xEVB_BLDC_6Step_Sensorless is the only one working. What am I doing wrong? The hall gives theese errors (missing headers): ....Building file: ../generate/src/Dpga_Ip_BOARD_INITPERIPHERALS_PBcfg.c C:/Users/nitro/workspaceS32DS.3.5_DP_V10/S32M24xEVB_BLDC_6Step_Hall/generate/include/Adc_Ip_BOARD_INITPERIPHERALS_PBcfg.h:44:10: fatal error: Adc_Ip_Types.h: No such file or directory Building file: ../generate/src/Ftm_Gpt_Ip_BOARD_INITPERIPHERALS_PBcfg.c 44 | #include "Adc_Ip_Types.h" | ^~~~~~~~~~~~~~~~ compilation terminated. ../generate/src/Aec_Ip_Cfg.c:41:10: fatal error: Aec_Ip_Types.h: No such file or directory Invoking: Standard S32DS C Compiler 41 | #include "Aec_Ip_Types.h" | ^~~~~~~~~~~~~~~~ compilation terminated. make: *** [generate/src/subdir.mk:78: generate/src/Adc_Ip_BOARD_INITPERIPHERALS_PBcfg.o] Error 1 make: *** Waiting for unfinished jobs.... make: *** [generate/src/subdir.mk:78: generate/src/Aec_Ip_Cfg.o] Error 1 ../generate/src/Aec_Ip_Sa_BOARD_INITPERIPHERALS_PBcfg.c:42:10: fatal error: Aec_Ip_Types.h: No such file or directory Building file: ../generate/src/Ftm_Pwm_Ip_BOARD_INITPERIPHERALS_PBcfg.c 42 | #include "Aec_Ip_Types.h" arm-none-eabi-gcc "@generate/src/Adc_Ip_BOARD_INITPERIPHERALS_PBcfg.args" -MMD -MP -MF"generate/src/Dpga_Ip_BOARD_INITPERIPHERALS_PBcfg.d" -MT"generate/src/Dpga_Ip_BOARD_INITPERIPHERALS_PBcfg.o" -o "generate/src/Dpga_Ip_BOARD_INITPERIPHERALS_PBcfg.o" "../generate/src/Dpga_Ip_BOARD_INITPERIPHERALS_PBcfg.c" | ^~~~~~~~~~~~~~~~ Invoking: Standard S32DS C Compiler compilation terminated. Invoking: Standard S32DS C Compiler make: *** [generate/src/subdir.mk:79: generate/src/Aec_Ip_Sa_BOARD_INITPERIPHERALS_PBcfg.o] Error 1 arm-none-eabi-gcc "@generate/src/Adc_Ip_BOARD_INITPERIPHERALS_PBcfg.args" -MMD -MP -MF"generate/src/Ftm_Pwm_Ip_BOARD_INITPERIPHERALS_PBcfg.d" -MT"generate/src/Ftm_Pwm_Ip_BOARD_INITPERIPHERALS_PBcfg.o" -o "generate/src/Ftm_Pwm_Ip_BOARD_INITPERIPHERALS_PBcfg.o" "../generate/src/Ftm_Pwm_Ip_BOARD_INITPERIPHERALS_PBcfg.c" In file included from ../generate/src/CDD_Gdu_BOARD_INITPERIPHERALS_PBcfg.c:43: arm-none-eabi-gcc "@generate/src/Adc_Ip_BOARD_INITPERIPHERALS_PBcfg.args" -MMD -MP -MF"generate/src/Ftm_Gpt_Ip_BOARD_INITPERIPHERALS_PBcfg.d" -MT"generate/src/Ftm_Gpt_Ip_BOARD_INITPERIPHERALS_PBcfg.o" -o "generate/src/Ftm_Gpt_Ip_BOARD_INITPERIPHERALS_PBcfg.o" "../generate/src/Ftm_Gpt_Ip_BOARD_INITPERIPHERALS_PBcfg.c" C:/Users/nitro/workspaceS32DS.3.5_DP_V10/S32M24xEVB_BLDC_6Step_Hall/generate/include/Gdu_Ip_BOARD_INITPERIPHERALS_PBcfg.h:46:10: fatal error: Gdu_Ip_Types.h: No such file or directory 46 | #include "Gdu_Ip_Types.h" | ^~~~~~~~~~~~~~~~ compilation terminated. make: *** [generate/src/subdir.mk:80: generate/src/CDD_Gdu_BOARD_INITPERIPHERALS_PBcfg.o] Error 1 In file included from ../generate/src/Dpga_Ip_BOARD_INITPERIPHERALS_PBcfg.c:41: C:/Users/nitro/workspaceS32DS.3.5_DP_V10/S32M24xEVB_BLDC_6Step_Hall/generate/include/Dpga_Ip_BOARD_INITPERIPHERALS_PBcfg.h:43:10: fatal error: Dpga_Ip_Types.h: No such file or directory 43 | #include "Dpga_Ip_Types.h" | ^~~~~~~~~~~~~~~~~ compilation terminated. make: *** [generate/src/subdir.mk:80: generate/src/Dpga_Ip_BOARD_INITPERIPHERALS_PBcfg.o] Error 1 In file included from C:/Users/nitro/workspaceS32DS.3.5_DP_V10/S32M24xEVB_BLDC_6Step_Hall/generate/include/Ftm_Pwm_Ip_Cfg.h:54, from ../generate/src/Ftm_Pwm_Ip_BOARD_INITPERIPHERALS_PBcfg.c:41: C:/Users/nitro/workspaceS32DS.3.5_DP_V10/S32M24xEVB_BLDC_6Step_Hall/generate/include/Ftm_Pwm_Ip_BOARD_INITPERIPHERALS_PBcfg.h:45:10: fatal error: Ftm_Pwm_Ip_Types.h: No such file or directory 45 | #include "Ftm_Pwm_Ip_Types.h" | ^~~~~~~~~~~~~~~~~~~~ compilation terminated. In file included from ../generate/src/Ftm_Gpt_Ip_BOARD_INITPERIPHERALS_PBcfg.c:47: C:/Users/nitro/workspaceS32DS.3.5_DP_V10/S32M24xEVB_BLDC_6Step_Hall/generate/include/Ftm_Gpt_Ip_BOARD_INITPERIPHERALS_PBcfg.h:46:10: fatal error: Ftm_Gpt_Ip_Types.h: No such file or directory 46 | #include "Ftm_Gpt_Ip_Types.h" | ^~~~~~~~~~~~~~~~~~~~ compilation terminated. make: *** [generate/src/subdir.mk:80: generate/src/Ftm_Pwm_Ip_BOARD_INITPERIPHERALS_PBcfg.o] Error 1 make: *** [generate/src/subdir.mk:80: generate/src/Ftm_Gpt_Ip_BOARD_INITPERIPHERALS_PBcfg.o] Error 1 "make -j8 all" terminated with exit code 2. Build might be incomplete. The PMSM_FOC is like incomplete: -j8 all Cannot run program "": Launching failed Error: Program "" not found in PATH Re: errors with S32M24xEVB Hi Did you click click on "Update Code" button for generating configuration files by refer to 4.2 Use Configuration Tool? Did you install SW32K1_S32M24x_RTD_4.4_R21-11_2.0.0_D2308_DS_Updatesite.zip and SW32K1_S32M24x_RTD_R21-11_2.0.0_P04_D2404_DS_updatesite.zip by refer to 2. Get Software of S32M24X Board Setup Guides? I am able to build the those three projects without error. C:\NXP\MC_DevKits\S32M24xEVB\sw\S32M24xEVB_BLDC_6Step_Sensorless and S32M24xEVB_BLDC_6Step_Hall and S32M24xEVB_PMSM_FOC_1Sh   Did you download S32 Design Studio - Releases & Updates here? And don't forget to install NXP GCC for Arm Embedded Processors v10.2 build 1728 by S32DS Extensions and Updates Best Regards, Robin ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. -------------------------------------------------------------------------------
View full article
CAN MCAL Hi, I am trying to implement CAN communication using the AUTOSAR MCAL layer on the S32K144 MCU. I am able to transmit data successfully, but I am not able to receive any data. I am using the polling method (not interrupts), and currently calling the following API periodically: Can_MainFunction_Read();   Is this API sufficient for receiving CAN messages in polling mode? Do I need to use any other API along with it to receive messages properly? Could you please share an example or reference code to implement CAN reception using AUTOSAR MCAL (polling mode) on S32K144? Re: CAN MCAL Hello, I've encountered the same problem as you. Could you please share how you solved it? Re: CAN MCAL Thank you. I have figured out the solution. Re: CAN MCAL Hi, you can check within debugger if message is really received. Inspect used MB area, MB flag. Also be sure no error is detected during reception, otherwise message is not moved-in and no MB flag will be set, check ECR/ESR1 registers. BR, Petr Re: CAN MCAL When I try to debug my code, it’s not entering the Rx callback function. It gets stuck in the Can_Ipw_MainFunction_Read() function, where the Message Buffer (MB) state is not IDLE. How can I resolve this issue? Re: CAN MCAL Hi, yes, it is enough to call MainFunction_Read periodically. Upon reception you should get CanIf_RxIndication callback. Refer e.g to RTD200 demo example, which is using polling mode for both TX and RX. BR, Petr Re: CAN MCAL How to configure and use interrupt to receive CAN messages
View full article
Guiderソフトウェア内のGuiderテーブルコントロールで、各セルの幅を調整するにはどうすればよいですか? テーブルコントロールを使用している際に、ガイドインターフェースに各セルの幅を調整するためのボタンや入力ボックスが見つかりませんでした。デザイン時にセルの幅を調整するにはどうすればよいでしょうか? Re: 请问guider的table控件怎样在guider软件里调整每个单元格的宽度? こんにちは、 @alen-liao こんにちは。このパラメータを変更してみてください。 BR ハリー
View full article
KW45 Secure Boot with no private key Hello, is there a method for authenticating images signed by external PKI? Let me explain better my question. I would like to enable secure boot by burning fuse CUST_PROD_OEMFW_AUTH_PUK with sha-256 of public key. I have the certificate with the public key provided by the OEM but I don't have the related private key because I am not the signer. I can only sign my plain test by external portal with a dedicated PKI and obtain ECDSA signature. I was referring to the following image but, assuming that i can obtain the signature, how can I know the exact tbs? in particular the data contained in the vector table? I hope I have explained my question in a good way. Thank you, Alessandro Re: KW45 Secure Boot with no private key AN14670 EdgeLock 2GO Provisioning via SPSDK for MCUs AN14624 EdgeLock 2GO Provisioning via Secure Provisioning Tool (SEC) for MCUs AN14109 KW45 and K32W148 Secure Boot Using the SEC Tool Re: KW45 Secure Boot with no private key Hi @alereale  It is possible to configure external signature provider. It is documented here: Signature provider - Generic workflows — Secure Provisioning Tool 26.03 Short story: You need to implement custom HTTP server providing the API for signing the application, the sample implementation of the server is provided as a source code. Re: KW45 Secure Boot with no private key Hi @marek-trmac Thank you for your reply. I was wondering if that is the only solution? In this way, I need to "force" the OEM to implement such a custom HTTP server. I say that because the OEM already has a server where I can upload my binary file for signing it. In general, can you confirm that the only way to enable Secure Boot in KW45 is to go through Secure Provisioning Tool? Thank you very much. Regards, Alessandro
View full article
PN7462 I2CM configuration Hi team, I am using PN7462 controller and the following I2CM initialization and EEPROM read implementation, which works correctly in the PN7462AU_ex_phExHif demo project: phStatus_t I2C_Init(void) { phStatus_t status; uint8_t bBaudRate; bBaudRate = (uint8_t) ((PH_EXHIF_HW_CRYSTAL_CLK / 100000UL) - PH_EXHIF_HW_CRYSTAL_CLK_MHZ); status = phhalI2CM_Init( PH_EXHIF_HW_I2CM_TX_FIFO_THRES, PH_EXHIF_HW_I2CM_RX_FIFO_THRES, PH_EXHIF_HW_I2CM_TIMEOUT, PH_EXHIF_HW_I2CM_RETRY_CNT); if(status != PH_ERR_SUCCESS) { return status; } status = phhalI2CM_Config( 0x40, 0x09, E_I2CM_7BIT_ADDR_MODE); return status; } #define EEPROM_ADDR (0x50U) #define EEPROM_MFG_ADDR (0xFAU) #define EEPROM_DEV_ADDR (0xFBU) #define EEPROM_UID_ADDR (0xFCU) phStatus_t EEPROM_ReadUID(uint8_t uid[4]) { return EEPROM_Read( EEPROM_UID_ADDR, uid, 4); } static phStatus_t EEPROM_Read(uint8_t memAddr, uint8_t *pData, uint16_t length) { phStatus_t status; uint32_t txBuf[4]; uint32_t rxBuf[64] = {0}; txBuf[0] = memAddr; status = phhalI2CM_Transmit( EEPROM_ADDR, 1, txBuf); if(status != PH_ERR_SUCCESS) { return status; } status = phhalI2CM_Receive( EEPROM_ADDR, length, rxBuf); if(status != PH_ERR_SUCCESS) { return status; } memcpy(pData, (uint8_t *)rxBuf, length); return PH_ERR_SUCCESS; } int main(void) { /* Boot initialization */ phFlashBoot_Main(); /* LED init */ phLED_Init(); /* UART init */ UART_Init(); I2C_Init(); EEPROM_WriteRead_Test(); while(1) { /* Everything handled in callbacks */ } } This exact code works in the PN7462AU_ex_phExHif demo. However, when integrated into my application and also phExMain example, it causes a HardFault. is there any additional configuration required in phExMain and on my application for I2CM operation? Re: PN7462 I2CM configuration Hi @EduardoZamora  I investigated the issue further and found a difference between the HIF demo and our application. The HIF demo is running with the NULL OS implementation, whereas our application is running with FreeRTOS. After starting the I2C transaction, the driver waits for an event to be posted from the I2C ISR when the transfer completes. In our application, the I2C ISR eventually calls: phStatus_t phOsal_EventPost(phOsal_Event_t * eventHandle, phOsal_EventOpt_t options, phOsal_EventBits_t FlagsToPost, phOsal_EventBits_t *pCurrFlags) { BaseType_t HigherPriorityTaskWoken; phOsal_EventBits_t CurrentFlags; if((eventHandle == NULL) || ((*eventHandle) == NULL)) { return (PH_OSAL_ERROR | PH_COMP_OSAL); } HigherPriorityTaskWoken = pdFALSE; if (xPortIsInsideInterrupt() == pdTRUE) { CurrentFlags = xEventGroupSetBitsFromISR( *eventHandle, FlagsToPost, &HigherPriorityTaskWoken); if(CurrentFlags == pdPASS) { portYIELD_FROM_ISR(HigherPriorityTaskWoken); } } else { CurrentFlags = xEventGroupSetBits( *eventHandle, FlagsToPost); } if (pCurrFlags != NULL) { *pCurrFlags = CurrentFlags; } return PH_OSAL_SUCCESS; } While debugging, the execution flow is: I2C ISR -> phOsal_EventPost() -> xEventGroupSetBitsFromISR() -> xTimerPendFunctionCallFromISR() -> xQueueSendFromISR() Inside FreeRTOS: BaseType_t xTimerPendFunctionCallFromISR( PendedFunction_t xFunctionToPend, void * pvParameter1, uint32_t ulParameter2, BaseType_t * pxHigherPriorityTaskWoken ) { DaemonTaskMessage_t xMessage; BaseType_t xReturn = pdPASS; xMessage.xMessageID = tmrCOMMAND_EXECUTE_CALLBACK_FROM_ISR; xMessage.u.xCallbackParameters.pxCallbackFunction = xFunctionToPend; xMessage.u.xCallbackParameters.pvParameter1 = pvParameter1; xMessage.u.xCallbackParameters.ulParameter2 = ulParameter2; xReturn = xQueueSendFromISR( xTimerQueue, &xMessage, pxHigherPriorityTaskWoken ); return xReturn; } At this point, xTimerQueue is NULL. xQueueSendFromISR() checks the queue handle using: configASSERT(pxQueue); and our assert is defined as: #define configASSERT(x) \ if((x) == 0) \ { \ taskDISABLE_INTERRUPTS(); \ for(;;); \ } Since xTimerQueue is NULL, the code enters the infinite loop. When running normally, it eventually results in a HardFault. For comparison, the NULL OS implementation of phOsal_EventPost() is: phStatus_t phOsal_EventPost( phOsal_Event_t * eventHandle, phOsal_EventOpt_t options, phOsal_EventBits_t FlagsToPost, phOsal_EventBits_t *pCurrFlags) { if((eventHandle == NULL) || ((*eventHandle) == NULL)) { return PH_OSAL_ADD_COMPCODE(PH_OSAL_ERROR, PH_COMP_OSAL); } phOsal_EnterCriticalSection(); (*((uint32_t *)(*eventHandle))) |= FlagsToPost; if (pCurrFlags != NULL) { *pCurrFlags = (*((uint32_t *)(*eventHandle))); } phOsal_ExitCriticalSection(); phOsal_WakeUp(); return PH_OSAL_SUCCESS; } This implementation does not use Event Groups, Timer Service Tasks, or Timer Queues, so it works correctly in the HIF demo. Could you please advise whether additional FreeRTOS timer service initialization is required before using the I2C/HIF drivers, or if there is a recommended FreeRTOS configuration for this use case? Thanks. Re: PN7462 I2CM configuration Hello @uday_gowda Could you please confirm what is the instruction that triggers the HardFault? Please consider that some demo projects, such as phExMain, may use a large amount of memory, and adding functionality may exceed the available space. I will recommend you scaling down the project to the minimal functionality required by your application. Regards, Eduardo.
View full article
FRDM-RT1186:The flash loader program reported an error. The debug log may contain more details Every time I modify the code and click download for the first time, it throws an error (a popup prompts "The flash loader program reported an error", and the debug log shows "Processor did not stop on hardware reset"). However, if I do nothing after the error and simply click download again, it successfully flashes the code and enters normal debugging. Could anyone explain what causes this? How should I configure IAR or the debugger settings to avoid this issue? Thanks! i.MXRT Windows Re: FRDM-RT1186:The flash loader program reported an error. The debug log may contain more details Dear guogai, When I changed the configuration to flexspi_nor_debug, I was able to reproduce the issue you reported. I am currently investigating the root cause and working on a solution. I will keep you updated on the progress. Re: FRDM-RT1186:The flash loader program reported an error. The debug log may contain more details Dear Shelly, Thanks for your reply. Regarding your suggestion to switch to FlashIMXRT1186-FRDM_FlexSPI_M33.board, I have two questions: Missing File: My IAR version is relatively old, so I do not have the FlashIMXRT1186-FRDM_FlexSPI_M33.board file in my current environment. Could you please kindly provide this single .board file for me? Hardware Mismatch: The target flash memory on my board is physically connected to the FlexSPI2 interface. If I switch the loader to FlexSPI (which usually targets SPI1), will it still be able to flash and program successfully? Thank you for your support! Re: FRDM-RT1186:The flash loader program reported an error. The debug log may contain more details Dear guogai, The current latest version is SDK_26_03_00_FRDM-IMXRT1186, please use the latest SDK. In addition, please check whether the flash loader is  $TOOLKIT_DIR$/config/flashloader/NXP/FlashIMXRT1186-FRDM_FlexSPI_M33.board .  If not, please modify it to this file.  Re: FRDM-RT1186:The flash loader program reported an error. The debug log may contain more details Hi @guogai  The hardware version currently I am using is SCH-95302 Rev A3, and the IAR version is 9.70.4.This setup has already been tested on my side, and there are no issues. We recommend using our official free MCUXpresso IDE.    Best Regards, Shelly
View full article
MIMXRT1170 芯片评估 亲爱的恩智浦支持团队 我们正在评估用于关键任务嵌入式应用的 i.MX RT1170 / MIMXRT1170-EVK 或 EVKB。处理器启动架构、固件更新策略、回滚能力和实时操作系统支持直接影响我们的系统可靠性,因此我们希望在进一步讨论之前与恩智浦验证我们的理解。 在现阶段,我们寻求的是广泛的供应商指导,而不是详细的实施步骤。 能否请您帮助我们澄清以下方面? 1.本机引导 ROM 功能 i.MX RT1170 bootROM 原生支持哪些启动功能? 特别是,使用该处理器的量产设计是否有任何主要限制、限制或推荐的启动源? 2。原生双映像/冗余启动 i.MX RT1170 bootROM 是否提供任何原生双镜像或冗余映像启动机制? 如果是,能否请您详细说明一下: 这是真正的 BootROM 管理双镜像功能吗? 它是否基于图像版本、图像偏移、熔丝配置或其他元数据? 这种本地机制的主要局限性是什么? 是用于生产固件冗余,还是仅用于有限的恢复? 3.OTA / 现场固件更新 i.MX RT1170 的 BootROM 是否支持本机 OTA 或现场固件更新? 如果没有,恩智浦推荐的实施架构是什么: * A/B 固件更新 * 签名图像验证 * 图像确认 * 回滚 * 更新失败后的恢复 * 签名图像、A/B 更新和回滚可以一起使用吗? 应该使用 MCUboot、恩智浦 SDK 引导加载程序示例还是自定义辅助引导加载程序来实现? 4.支持实时操作系统:Zephyr 据我们了解,Zephyr 的板支持 MIMXRT1170-EVK/EVKB。 请您澄清一下: * i.MX RT1170 提供什么级别的 Zephyr 支持? * 恩智浦是否验证了该主板上的 Zephyr 与 McuBoot 的集成? * 在 i.MX RT1170 上通过 Zephyr/MCUboot 是否支持 A/B 更新、签名映像、映像确认和回滚? * 应将哪个 NXP 或 Zephyr 官方版本库/示例用作基线? 5.支持 RTOS:RTEMS 我们还在评估 RTEMS 在飞行软件方面的应用,因为 RTEMS 具有航天和国防传统。 请您澄清一下: * 恩智浦是否提供或验证了对 i.MX RT1170 的 RTEMS 支持? * 是否有 MIMXRT1170-EVK/EVKB 的 RTEMS 电路板支持包? * 如果不是,从现有 RTEMS i.MXRT 电路板支持包 系列中移植在技术上是否可行? * 在 i.MX RT1170 上从 MCUboot 或自定义引导加载程序启动 RTEMS 映像时,是否存在已知问题? 6.建议的结构 对于强大的更新和恢复设计,恩智浦建议 i.MX RT1170 采用以下哪种架构选项? * BootROM 直接引导 RTOS 应用程序 * BootROM 引导 MCUboot,然后 MCUboot 引导 RTOS 应用程序 * BootROM 引导自定义二级引导加载器,然后引导加载器选择映像 A /映像 B /恢复映像 * 仅有 BootROM 本地双映像机制,无 MCUboot 我们正试图确定哪些功能是处理器的原生功能,哪些功能由恩智浦软件示例支持,哪些功能由 RTOS 生态系统提供,哪些功能必须由我们的应用程序或自定义引导加载程序来实现。 您可以向我们提供的任何官方文档、应用笔记、SDK 示例或存储库都将非常有帮助。 很抱歉提出了这么多问题,但这些都是对任务至关重要的参数,我们希望在继续进行之前验证我们的理解。 致以最诚挚的问候, Ruthvik R Re: MIMXRT1170 Chip Evaluation 你好 Gavin_Jia, 感谢您快速而翔实的回复。 我将与我的团队讨论这个问题,并给您回复。 谢谢! 此致, Ruthvik R Re: MIMXRT1170 Chip Evaluation 你好@ruthvik_1、 感谢您的详细提问。 I.MX RT1170 bootROM 应被视为不可变的第一阶段启动代码。它可以处理早期启动、启动媒体选择、启动映像解释以及与安全启动相关的原语。参考手册摘录还记录了一种 PERSIST_SECONDARY_BOOT/次映像表机制,在该机制中,bootROM 可以从该表指定的次映像位置启动。 但是,不应将此机制解释为完整的**产品级** A/B OTA 或回滚管理器。经审查的 BootRom 证据未显示应用程序运行状况检查、映像确认、试用启动策略或自动回滚。恩智浦的FOTA参考架构在辅助引导加载程序级别实现这些功能,例如通过SBL/SFW或基于Mcuboot的设计,使用插槽、图像签名、图像确认、还原/回滚状态和恢复处理。 对于 Zephyr 而言,上游 Zephyr 文档将 mimxrt1170_evk 列为维护板,并指出 Zephyr 支持最初的 MIMXRT1170-EVK 版本以及 EVKB。客户可以试用 Zephyr 中提供的 MCUboot,但我们不能保证它是功能完备的实现。有些机制可能需要由客户制定。同时,MCUXpresso SDK还包括McuBoot OTA的示例项目供您参考。 对于 RTEMS 来说,它包括 i.mxRT 电路板支持包 系列,但经过审查的公开文件显示了 imxrt1052 和 imxrt1166-cm7-saltshaker 等变体;我没有找到专用的 MIMXRT1170-EVK/EVKB RTEMS 电路板支持包 或恩智浦在 RT1170 上对 RTEMS 进行验证的公开证据。因此,RT1170 上的 RTEMS 应被视为移植和集成活动。 对于关键任务设计,建议评估的架构是 BootROM + 可信的辅助引导加载程序,如 NXP SBL、MCUboot 或客户控制的引导加载程序,并在系统级实施和验证 A/B 插槽、签名映像验证、映像确认、回滚和恢复策略。 希望对你有所帮助! 致以最诚挚的问候, Gavin
View full article
PowerPCハードウェアプラットフォーム(Yoctoビルドシステム使用時)でSPIドライバが期待どおりに動作しない みなさん、こんにちは。 私はカーネルが組み込まれた古いビルドシステム(2.6.73.x)を使用していますが、私のアプリケーションは正常にコンパイルされ、PowerPCアーキテクチャに基づいたカスタムLinuxボード上で問題なく動作しています。 最新のカーネル(6.xx)が搭載されているYOCTOビルドシステムに移行しました。以前のビルドシステムでは正常に動作していたSPIデバイスが、期待どおりに動作しなくなっていることに気づきました。 カーネルバージョンの大幅な変更(ひいてはSPIドライバの変更)に伴い、多くの動特性やパラメータが変わることは承知しています。変更モードと制御チップセレクトAPIに遅延を追加してみましたが、多少改善はしたものの、成功には至りませんでした。 SPIコントローラのパラメータを変更するために様々な実験を試みましたが、成功しませんでした。インターネットでいくつか情報を得ましたが、問題は解決していません。私見では、これはタイミングの問題だと思います。しかし、どこを修理すればいいのか正確にはわかりません。 ですから、もしあなたがこのような、あるいは似たような課題に直面したことがあるなら、リーダーシップを発揮したり、支援したりすることができます。どんなご提案、修正方法、ご助言、ご指示でも歓迎いたします。 ありがとう バラト Re: SPI driver not working as expected on powerpc hardware platform (with yocto build system) 何かご提案があれば、ぜひご返信ください。大変参考になります。
View full article
请求支持 Windows ARM64(LinkServer/MCUXpresso) 这也要求开始发布 Windows ARM64 版本的 LinkServer 和 MCUXpresso 安装程序。我最近看到越来越多的学生使用这些基于ARM的Windows笔记本电脑。 开发板 MCXA MCX N Re: Windows ARM64 support request (LinkServer/MCUXpresso) 你好 感谢您的建议,我将向通讯员团队提出意见、 关于 MCUXpresso 的使用,您能否帮助我们尝试使用 Visual Studio Code 扩展?然后与我们联系你的发现? 有关该工具安装和使用的更多信息,请参阅 MCUXpresso for VS Code 文档 - MCUXpresso for VS Code 26.05 文档 适用于 Visual Studio Code 的 MCUXpresso | NXP 半导体 最诚挚的问候,路易斯 Re: Windows ARM64 support request (LinkServer/MCUXpresso) 谢谢您的答复。 vscode 扩展正常工作。mcu-link 驱动程序基于 WinUSB,微软对其进行了完美移植。 我在测试系统上没有管理员权限,但我可以将 linkserver 复制到系统上并调试项目。我不知道 LinkServer 安装中的其他驱动程序,但它们需要签名的 arm 版本。 不幸的是," mcuxpresso 安装程序 " 安装的所有工具都是 x64,因此所有工具都通过 Prism 转换层运行。git、python、ninja、cmake 等应该已经发布了 arm 版本这样就可以打包了。只有 arm-none-eabi 工具链尚未发布 arm64 版本,但可以构建。特别是对于 mcu-link 开发板来说,它主要与 ARM64 Windows 版本的性能有关。 Re: Windows ARM64 support request (LinkServer/MCUXpresso) 你好! 很高兴听到它对您来说运行正常。至于该主题的最新进展,很遗憾,我们不会为 MCUXpresso IDE 开发 ARM64 版本,因为我们现在只对该平台进行维护,我们仍然建议使用 VS Code 扩展来支持 MCUXpresso。 最诚挚的问候,路易斯 Re: Windows ARM64 support request (LinkServer/MCUXpresso) MCUXpresso 安装程序由 VSCode 扩展使用,这就是我之前提到的: https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-installer :MCUXPRESSO-INSTALLER 和https://mcuxpresso.nxp.com/mcux-vscode/latest/html/MCUXpresso-Installer.html 。此版本适用于 macOS x64/arm64 和 linux/windows x64,但不适用于 arm64。此软件包包含链接服务器,该服务器已发布,适用于 macOS x64/arm64、linux x64/arm64 以及 windows x64。我希望这些应用程序能够发布适用于 Windows arm64 的版本。我知道 mcuxpresso 安装程序会安装很多东西,其中大部分东西在 Windows arm64 上已经可用了。我教的学生都拥有这些新的 Windows arm64 笔记本电脑,现在我必须帮助他们找到解决方法才能让程序正常运行。
View full article
モバイルオンラインバカラアカウントの登録およびお問い合わせは、15708835568までお電話ください。
View full article
关于 S32K3 EMIOS 的几个问题 亲爱的支持团队 我有几个关于 eMIOS 的技术问题。 1.X 通道和 G 通道都有一个 CNT 寄存器。为什么两个通道都支持 OPWFMB,而只有 G 通道支持 OPWMCB? 2.我将 Emios0_Ch3 配置为 DOAC 模式,"标志事件仅在 B 匹配时发生"。 在这个频道的中断回调函数中,我改变了占空比。 但是,输出是 5 个波形,占空比为 500,然后是 4 个循环占空比为 1000 的波形。 我在第 133 行将占空比设置为 1000,在第 137 行将占空比设置为 500,但行为保持不变。 当我将占空比更改为其他值时,模式似乎是: 占空比较大的波形出现的时间少了一次(只有 4 次,而不是预期的 5 次),而占空比较小的波形出现的时间是预期的 5 倍。 OPWMT 和 OPWMB 模式下不会出现此问题。 3.MCR 寄存器中的 GPRE 对 OPWFMB 模式下的波形频率没有影响吗? 在其他条件不变的情况下,当我修改 Emios_Mcl 中的这一参数时,OPWFMB 模式(Emios0_Ch0)下的输出频率不会发生变化。 4. 根据参考手册: "为什么 OPWFMB 频率不受 GPRE 影响? Cn[UCPRE] 的功能是什么? 如果您能回答上述问题,我将不胜感激。 顺祝商祺! Re: several questions about S32K3 EMIOS 你好@Jason22 1.虽然两种通道类型都包含一个内部计数器,但这并不意味着它们具有相同的内部结构。以下是总体比较: G 型(7 个通道):功能齐全。它包括一个内部计数器,但该计数器不能与其他通道共享。 X 型(15 个通道):包括一个内部计数器,其 MC/MCB 计数器总线可由其他通道共享和使用。 2.请参阅《S32M27x/S32K3 - eMIOS 使用》中提供的 DAOC 示例项目。该示例包括有关驱动程序限制的信息,并就正确使用提供了有用的指导。 3.时钟分频器值充当预分频器,用于分频eMIOS实例的输入时钟频率。这实际上决定了该实例中所有通道使用的基本时间分辨率。 较高的分频器值 → 降低时钟频率 → 增加计时器周期 → 导致输出信号频率降低。 较低的分频器值 → 增加时钟频率 → 缩短计时器周期 → 导致更高的输出信号频率。 BR、VaneB Re: several questions about S32K3 EMIOS 你好@VaneB 非常感谢你回答我的问题。 我仍然对"eMIOS 的 GCP 输出信号除以 UC CP(Cn [UCPRE]+1)以产生 UC 内部计数器" 的时钟使能有一些疑问。在实际测试中,我发现如果 C2_n [UCPRECLK] 为 0,预刻度时钟的频率等于 GCP 除以 (C2_n [UCEXTPRE]+1) 而不是 (Cn [UCPRE]+1),我在 Emios_Pwm_Ip_HwAccess 中找到了这句话。h (RTD700):"未使用位文件 UCPRE。取而代之的是使用 C2" 中的 UCEXTPRE 来控制数值。参考手册指出 " C2_n [UCEXTPRE] 的两个最低有效位镜像 UCPRE。"。我已经看到UCPRE在参考手册中多次出现,但我似乎看不出驱动程序代码中使用了UCPRE。 能否请您解释一下 UCPRE 的用途? 致以最诚挚的问候 Re: several questions about S32K3 EMIOS 你好@Jason22 请参阅下面的相关主题,也许会有所帮助。 PWM 捕获时钟的分频问题
View full article
LS1046A FEC support Hello, I'm interested is it FEC (Firecode FEC used in 10GBASE-KR) supported on LS1046A platform and how to enable it? I saw that in Linux kernel 6.12.49 there is 10GBASE-KR support, but only for Auto Negotiation and Link Training. Also I wanted to use USDPAA device tree to be able to use DPDK + VPP, so are there some blockers to make FEC work in that setup? Is it possible also to avoid running Auto negotiation and Link training and to run FEC only? Thanks in advance, Nenad Re: LS1046A FEC support Auto-negotiation is a necessary step in the current driver flow. If auto-negotiation fails, the process will not proceed further. So  the current backplane driver does not support FEC, and auto-negotiation is an integral part of the workflow. If you want to remove auto-negotiation, you will need to modify the driver by yourselves, and we do not recommend doing so. If link training itself has issues, there is no point in proceeding with other configurations. To enable FEC, an additional PMD register needs to be programmed. Re: LS1046A FEC support FEC is not supported in current backplane driver. Auto-negitation is necessary step in the backplane driver, I suggest customer modify backplane driver to set XFI_10GR_FEC_CTL[FEC_ENAB] to enable FEC Re: LS1046A FEC support I successfully enabled FEC and I am not using AN/LT (its disabled). I am basically including "-kr.dtsi" files for mac9 and mac10 to be able to access registers to write FEC_ENAB. When I say throughput in the next lines for example 4gbps I mean on 2x 4gbps is generated from network tester to board. BERT test is running (L2 traffic test termination). And when I start VPP so that mac9 and mac10 are bridged I see that errors are smaller, on one port there is 0 errors and on other port there is no errors when throughput is smaller (<4gbps) and when there is throughput >4gbps errors are around BER ratio 2E-08 and smaller (E-09). But those measurements are when the system is idle (not using console at all). But when I do something, for example start top program, press Enter multiple times, errors are increasing (BER ratio E-07, E-06). So I made a script that is doing memcpy fast (to put pressure on ddr) and I saw that I got a lot of bit errors (BER ratio is going up to E-04 for throughputs bigger than 7gbps) on MTS5800 network tester. My setup is like this: DPDK + VPP (main core 1, workers 2 and 3), isolcpus=1-3, nohz_full=1-3, rcu_nocbs=1-3, iommu_passthrough=1, hugepagessz=2m, number of hugepages 512. Is there maybe DDR bandwidth bottleneck in higher network throughputs?
View full article
如何在 i.mx8M Mini 的 eMMC 分区 (boot1) 中刷新 u-boot 您好, 我们希望使用 i.MX8M MINI 主板从 eMMC 的 boot0 和 boot1 分区进行闪存和启动。 你能为我提供任何必要的内核修改和 uuu 文件更改以将镜像闪存到主板上吗? 此致, 达米克 Re: How to flash u-boot in eMMC partition(boot1) in i.MX8M Mini 您好, 是的,请参阅 UUU github 获取此任务的示例脚本,有关修改,请参阅文档: https://github.com/nxp-imx/mfgtools/wiki/Sample-scripts#burn-yocto-image-to-emmc-by-linux-kernel 文件: https://github.com/nxp-imx/mfgtools/releases/download/uuu_1.5.243/UUU.pdf 致以最崇高的敬意/问候, Aldo。 Re: How to flash u-boot in eMMC partition(boot1) in i.MX8M Mini 您可以阅读文档: i.MX8QXP eMMC 二级启动并更改为 8 毫米 https://community.nxp.com/t5/NXP-Tech-Blog/i-MX8QXP-eMMC-Secondary-Boot/ba-p/1257704#M45https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX8MM-SDCARD-Secondary-Boot-Demo/ta-p/1500011 i.MX8QXP_emmc_boot_part_secondary_boot.uuu 向 boot2 段写入你想要的内容。 # Secondary boot FB: ucmd setenv part 2 FB: ucmd if test ${part} != 7; then mmc dev ${emmc_dev} ${part}; else mmc dev ${emmc_dev}; fi #FB: download -f imx-boot-imx8qxpc0mek-sd.bin-flash-L5.4.47-2.2.0 FB: download -f imx-boot-imx8qxpc0mek-sd.bin-flash-L5.4.70-2.3.0 FB: ucmd echo ${fastboot_bytes} FB: ucmd setexpr blks ${fastboot_bytes} / 0x200; setexpr blks ${blks} + 1 FB: ucmd mmc write ${loadaddr} ${boot_offset} ${blks} 完整剧本 uuu_version 1.2.39 SDPS: boot -f imx-boot-imx8qxpc0mek-sd.bin-flash-L5.4.70-2.3.0 SDPV: delay 1000 SDPV: write -f imx-boot-imx8qxpc0mek-sd.bin-flash-L5.4.70-2.3.0 -skipspl SDPV: jump #FB: ucmd setenv emmc_dev 1 FB: ucmd setenv part 1 FB: ucmd setenv boot_offset 0x0 FB: ucmd setenv fastboot_dev mmc FB: ucmd setenv mmcdev ${emmc_dev} FB: ucmd if test ${part} != 7; then mmc dev ${emmc_dev} ${part}; else mmc dev ${emmc_dev}; fi FB: ucmd setenv fastboot_buffer ${loadaddr} FB: download -f imx-boot-imx8qxpc0mek-sd.bin-flash-L5.4.47-2.2.0 #FB: download -f imx-boot-imx8qxpc0mek-sd.bin-flash-L5.4.70-2.3.0 FB: ucmd echo ${fastboot_bytes} FB: ucmd setexpr blks ${fastboot_bytes} / 0x200; setexpr blks ${blks} + 1 FB: ucmd mmc write ${loadaddr} ${boot_offset} ${blks} # Secondary boot FB: ucmd setenv part 2 FB: ucmd if test ${part} != 7; then mmc dev ${emmc_dev} ${part}; else mmc dev ${emmc_dev}; fi #FB: download -f imx-boot-imx8qxpc0mek-sd.bin-flash-L5.4.47-2.2.0 FB: download -f imx-boot-imx8qxpc0mek-sd.bin-flash-L5.4.70-2.3.0 FB: ucmd echo ${fastboot_bytes} FB: ucmd setexpr blks ${fastboot_bytes} / 0x200; setexpr blks ${blks} + 1 FB: ucmd mmc write ${loadaddr} ${boot_offset} ${blks} FB: ucmd setenv part 1 FB: ucmd if env exists emmc_ack; then ; else setenv emmc_ack 0; fi; FB: ucmd mmc partconf ${emmc_dev} ${emmc_ack} ${part} 0 FB: done https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/iMX-secondary-boot-collection/ta-p/1916915
View full article