2120432_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2120432_en-US

2120432_en-US

CAN MCAL

Hi,

I am trying to implement CAN communication using the AUTOSAR MCAL layer on the S32K144 MCU. I am able to transmit data successfully, but I am not able to receive any data.

I am using the polling method (not interrupts), and currently calling the following API periodically:

Can_MainFunction_Read();
 
  • Is this API sufficient for receiving CAN messages in polling mode?

  • Do I need to use any other API along with it to receive messages properly?

  • Could you please share an example or reference code to implement CAN reception using AUTOSAR MCAL (polling mode) on S32K144?

Re: CAN MCALHello, I've encountered the same problem as you. Could you please share how you solved it?Re: CAN MCALThank you. I have figured out the solution.Re: CAN MCAL

Hi,

you can check within debugger if message is really received. Inspect used MB area, MB flag.
Also be sure no error is detected during reception, otherwise message is not moved-in and no MB flag will be set, check ECR/ESR1 registers.

BR, Petr

Re: CAN MCALWhen I try to debug my code, it’s not entering the Rx callback function. It gets stuck in the Can_Ipw_MainFunction_Read() function, where the Message Buffer (MB) state is not IDLE.
How can I resolve this issue?
Re: CAN MCAL

Hi,

yes, it is enough to call MainFunction_Read periodically. Upon reception you should get CanIf_RxIndication callback.
Refer e.g to RTD200 demo example, which is using polling mode for both TX and RX.

BR, Petr

Re: CAN MCAL

How to configure and use interrupt to receive CAN messages

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎06-16-2026 03:27 AM
更新者: