2379659_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2379659_en-US

2379659_en-US

errors with S32M24xEVB

I have tried example codes for this kit and the S32M24xEVB_BLDC_6Step_Sensorless is the only one working. What am I doing wrong? The hall gives theese errors (missing headers):

....Building file: ../generate/src/Dpga_Ip_BOARD_INITPERIPHERALS_PBcfg.c
C:/Users/nitro/workspaceS32DS.3.5_DP_V10/S32M24xEVB_BLDC_6Step_Hall/generate/include/Adc_Ip_BOARD_INITPERIPHERALS_PBcfg.h:44:10: fatal error: Adc_Ip_Types.h: No such file or directory
Building file: ../generate/src/Ftm_Gpt_Ip_BOARD_INITPERIPHERALS_PBcfg.c
44 | #include "Adc_Ip_Types.h"
| ^~~~~~~~~~~~~~~~
compilation terminated.
../generate/src/Aec_Ip_Cfg.c:41:10: fatal error: Aec_Ip_Types.h: No such file or directory
Invoking: Standard S32DS C Compiler
41 | #include "Aec_Ip_Types.h"
| ^~~~~~~~~~~~~~~~
compilation terminated.
make: *** [generate/src/subdir.mk:78: generate/src/Adc_Ip_BOARD_INITPERIPHERALS_PBcfg.o] Error 1
make: *** Waiting for unfinished jobs....
make: *** [generate/src/subdir.mk:78: generate/src/Aec_Ip_Cfg.o] Error 1
../generate/src/Aec_Ip_Sa_BOARD_INITPERIPHERALS_PBcfg.c:42:10: fatal error: Aec_Ip_Types.h: No such file or directory
Building file: ../generate/src/Ftm_Pwm_Ip_BOARD_INITPERIPHERALS_PBcfg.c
42 | #include "Aec_Ip_Types.h"
arm-none-eabi-gcc "@generate/src/Adc_Ip_BOARD_INITPERIPHERALS_PBcfg.args" -MMD -MP -MF"generate/src/Dpga_Ip_BOARD_INITPERIPHERALS_PBcfg.d" -MT"generate/src/Dpga_Ip_BOARD_INITPERIPHERALS_PBcfg.o" -o "generate/src/Dpga_Ip_BOARD_INITPERIPHERALS_PBcfg.o" "../generate/src/Dpga_Ip_BOARD_INITPERIPHERALS_PBcfg.c"
| ^~~~~~~~~~~~~~~~
Invoking: Standard S32DS C Compiler
compilation terminated.
Invoking: Standard S32DS C Compiler
make: *** [generate/src/subdir.mk:79: generate/src/Aec_Ip_Sa_BOARD_INITPERIPHERALS_PBcfg.o] Error 1
arm-none-eabi-gcc "@generate/src/Adc_Ip_BOARD_INITPERIPHERALS_PBcfg.args" -MMD -MP -MF"generate/src/Ftm_Pwm_Ip_BOARD_INITPERIPHERALS_PBcfg.d" -MT"generate/src/Ftm_Pwm_Ip_BOARD_INITPERIPHERALS_PBcfg.o" -o "generate/src/Ftm_Pwm_Ip_BOARD_INITPERIPHERALS_PBcfg.o" "../generate/src/Ftm_Pwm_Ip_BOARD_INITPERIPHERALS_PBcfg.c"
In file included from ../generate/src/CDD_Gdu_BOARD_INITPERIPHERALS_PBcfg.c:43:
arm-none-eabi-gcc "@generate/src/Adc_Ip_BOARD_INITPERIPHERALS_PBcfg.args" -MMD -MP -MF"generate/src/Ftm_Gpt_Ip_BOARD_INITPERIPHERALS_PBcfg.d" -MT"generate/src/Ftm_Gpt_Ip_BOARD_INITPERIPHERALS_PBcfg.o" -o "generate/src/Ftm_Gpt_Ip_BOARD_INITPERIPHERALS_PBcfg.o" "../generate/src/Ftm_Gpt_Ip_BOARD_INITPERIPHERALS_PBcfg.c"
C:/Users/nitro/workspaceS32DS.3.5_DP_V10/S32M24xEVB_BLDC_6Step_Hall/generate/include/Gdu_Ip_BOARD_INITPERIPHERALS_PBcfg.h:46:10: fatal error: Gdu_Ip_Types.h: No such file or directory
46 | #include "Gdu_Ip_Types.h"
| ^~~~~~~~~~~~~~~~
compilation terminated.
make: *** [generate/src/subdir.mk:80: generate/src/CDD_Gdu_BOARD_INITPERIPHERALS_PBcfg.o] Error 1
In file included from ../generate/src/Dpga_Ip_BOARD_INITPERIPHERALS_PBcfg.c:41:
C:/Users/nitro/workspaceS32DS.3.5_DP_V10/S32M24xEVB_BLDC_6Step_Hall/generate/include/Dpga_Ip_BOARD_INITPERIPHERALS_PBcfg.h:43:10: fatal error: Dpga_Ip_Types.h: No such file or directory
43 | #include "Dpga_Ip_Types.h"
| ^~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [generate/src/subdir.mk:80: generate/src/Dpga_Ip_BOARD_INITPERIPHERALS_PBcfg.o] Error 1
In file included from C:/Users/nitro/workspaceS32DS.3.5_DP_V10/S32M24xEVB_BLDC_6Step_Hall/generate/include/Ftm_Pwm_Ip_Cfg.h:54,
from ../generate/src/Ftm_Pwm_Ip_BOARD_INITPERIPHERALS_PBcfg.c:41:
C:/Users/nitro/workspaceS32DS.3.5_DP_V10/S32M24xEVB_BLDC_6Step_Hall/generate/include/Ftm_Pwm_Ip_BOARD_INITPERIPHERALS_PBcfg.h:45:10: fatal error: Ftm_Pwm_Ip_Types.h: No such file or directory
45 | #include "Ftm_Pwm_Ip_Types.h"
| ^~~~~~~~~~~~~~~~~~~~
compilation terminated.
In file included from ../generate/src/Ftm_Gpt_Ip_BOARD_INITPERIPHERALS_PBcfg.c:47:
C:/Users/nitro/workspaceS32DS.3.5_DP_V10/S32M24xEVB_BLDC_6Step_Hall/generate/include/Ftm_Gpt_Ip_BOARD_INITPERIPHERALS_PBcfg.h:46:10: fatal error: Ftm_Gpt_Ip_Types.h: No such file or directory
46 | #include "Ftm_Gpt_Ip_Types.h"
| ^~~~~~~~~~~~~~~~~~~~
compilation terminated.
make: *** [generate/src/subdir.mk:80: generate/src/Ftm_Pwm_Ip_BOARD_INITPERIPHERALS_PBcfg.o] Error 1
make: *** [generate/src/subdir.mk:80: generate/src/Ftm_Gpt_Ip_BOARD_INITPERIPHERALS_PBcfg.o] Error 1
"make -j8 all" terminated with exit code 2. Build might be incomplete.


The PMSM_FOC is like incomplete:

-j8 all
Cannot run program "": Launching failed

Error: Program "" not found in PATH

Re: errors with S32M24xEVB

Hi

Did you click click on "Update Code" button for generating configuration files by refer to 4.2 Use Configuration Tool?
Did you install SW32K1_S32M24x_RTD_4.4_R21-11_2.0.0_D2308_DS_Updatesite.zip and SW32K1_S32M24x_RTD_R21-11_2.0.0_P04_D2404_DS_updatesite.zip by refer to 2. Get Software of S32M24X Board Setup Guides?
I am able to build the those three projects without error.
C:\NXP\MC_DevKits\S32M24xEVB\sw\S32M24xEVB_BLDC_6Step_Sensorless and S32M24xEVB_BLDC_6Step_Hall and S32M24xEVB_PMSM_FOC_1Sh
 

Did you download S32 Design Studio - Releases & Updates here?

And don't forget to install NXP GCC for Arm Embedded Processors v10.2 build 1728 by S32DS Extensions and Updates


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-------------------------------------------------------------------------------

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎06-11-2026 02:31 AM
更新者: