RT1052's DCD file SDRAMCR0 and SEMC_DBICR0 registers are configured in contradiction to each other. Dear NXP. Hello! In the RT1052 development board SDK (D:\SDK_2_14_0_MIMXRT1052xxxxB\boards\evkbimxrt1050\lvgl_examples\lvgl_demo_widgets\mdk), in the dcd.c file, there are two registers configured: ① /* #1.104, command: write_value, address: SEMC_SDRAMCR0, value: 0xF07, size: 4 */ 0x40, 0x2F, 0x00, 0x40, 0x00, 0x00, 0x0F, 0x07, COL:11b - 9 bit 9-8 COL Column address bit number 00b - 12 bit 01b - 11 bit 10b - 10 bit 11b - 9 bit This register configures the Column address bit number to 9 bits. ② /* #1.108, command: write_value, address: SEMC_DBICR0, value: 0x21, size: 4 */ 0x40, 0x2f, 0x00, 0x80, 0x00, 0x00, 0x00, 0x21. COL:0000b - 12 Bits 15-12 COL Column Address bit width 0000b - 12 Bits 0001b - 11 Bits 0010b - 10 Bits 0011b - 9 Bits 0100b - 8 Bits 0101b - 7 Bits 0110b - 6 Bits 0111b - 5 Bits 1000b - 4 Bits 1001b - 3 Bits 1010b - 2 Bits 1011b - 12 Bits 1100b - 12 Bits 1101b - 12 Bits 1110b - 12 Bits 1111b - 12 Bits Column Address bit width is set to 12bit. Are these two register configurations contradictory? Or is there something wrong with my understanding? (used at the end of a letter introduce a polite salutation) Salute! Re: RT1052的DCD文件SDRAMCR0与SEMC_DBICR0两个寄存器配置矛盾 Hi @FromCH0,
Thank you for your interest in the NXP RT product line and we are pleased to be of service to you.
Q: Are these two register configurations contradictory? Or is my understanding wrong?
A: These two settings do not contradict each other.
1: SEMC_SDRAMCR0 is used for SDRAM address multiplexing/mapping, determines the organization of address bits such as Column, Bank, etc., and acts as the Row address setting.
2: SEMC_DBICR0 is the DBI-B control register of SEMC, which belongs to Display Bus Interface control function and does not participate in SDRAM address mapping, so the two registers will not conflict.
I hope the above helps you
Best Regards
May Liu Re: RT1052的DCD文件SDRAMCR0与SEMC_DBICR0两个寄存器配置矛盾 The reliably identified core purpose of the RT1052's SEMC_DBICR0 is currently to configure the SEMC's DBI-B/8080 display bus bitwidth (for example: 8-bit or 16-bit), which is not involved in SDRAM mapping, and the timing details should be configured primarily in DBICR1. Re: RT1052的DCD文件SDRAMCR0与SEMC_DBICR0两个寄存器配置矛盾 I probably understand what you mean. However, SEMC_DBICR0 is to configure the Display Bus Interface control function, how to configure this register, there is not much description about this register in the RT1052 reference manual, SEMC_SDRAMCR0 is easy to understand, look up the DATASHEET of the SDRAM, and the corresponding register is The configuration of SEMC_SDRAMCR0 is easy to understand. Re: RT1052的DCD文件SDRAMCR0与SEMC_DBICR0两个寄存器配置矛盾 You are also an employee of NXP. You can't get the details of SEMC_DBICR0 register? Yesterday, I attended one of your meetings, and your technical engineers from NXP's China team would also find it difficult to master the RT series MCUs?
記事全体を表示