2352748_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2352748_en-US

2352748_en-US

RT1052's DCD file SDRAMCR0 and SEMC_DBICR0 registers are configured in contradiction to each other.

Dear NXP.

Hello!

In the RT1052 development board SDK (D:\SDK_2_14_0_MIMXRT1052xxxxB\boards\evkbimxrt1050\lvgl_examples\lvgl_demo_widgets\mdk), in the dcd.c file, there are two registers configured:

/* #1.104, command: write_value, address: SEMC_SDRAMCR0, value: 0xF07, size: 4 */
0x40, 0x2F, 0x00, 0x40, 0x00, 0x00, 0x0F, 0x07,

COL:11b - 9 bit
9-8
COL
Column address bit number
00b - 12 bit
01b - 11 bit
10b - 10 bit
11b - 9 bit

This register configures the Column address bit number to 9 bits.

/* #1.108, command: write_value, address: SEMC_DBICR0, value: 0x21, size: 4 */

0x40, 0x2f, 0x00, 0x80, 0x00, 0x00, 0x00, 0x21.

COL:0000b - 12 Bits
15-12
COL
Column Address bit width
0000b - 12 Bits
0001b - 11 Bits
0010b - 10 Bits
0011b - 9 Bits
0100b - 8 Bits
0101b - 7 Bits
0110b - 6 Bits
0111b - 5 Bits
1000b - 4 Bits
1001b - 3 Bits
1010b - 2 Bits
1011b - 12 Bits
1100b - 12 Bits
1101b - 12 Bits
1110b - 12 Bits
1111b - 12 Bits

Column Address bit width is set to 12bit.

Are these two register configurations contradictory? Or is there something wrong with my understanding?

(used at the end of a letter introduce a polite salutation)

Salute!


Re: RT1052的DCD文件SDRAMCR0与SEMC_DBICR0两个寄存器配置矛盾

Hi @FromCH0,

Thank you for your interest in the NXP RT product line and we are pleased to be of service to you.

Q: Are these two register configurations contradictory? Or is my understanding wrong?

A: These two settings do not contradict each other.

1: SEMC_SDRAMCR0 is used for SDRAM address multiplexing/mapping, determines the organization of address bits such as Column, Bank, etc., and acts as the Row address setting.

2: SEMC_DBICR0 is the DBI-B control register of SEMC, which belongs to Display Bus Interface control function and does not participate in SDRAM address mapping, so the two registers will not conflict.

 
I hope the above helps you
Best Regards
May Liu
Re: RT1052的DCD文件SDRAMCR0与SEMC_DBICR0两个寄存器配置矛盾

The reliably identified core purpose of the RT1052's SEMC_DBICR0 is currently to configure the SEMC's DBI-B/8080 display bus bitwidth (for example: 8-bit or 16-bit), which is not involved in SDRAM mapping, and the timing details should be configured primarily in DBICR1.

Re: RT1052的DCD文件SDRAMCR0与SEMC_DBICR0两个寄存器配置矛盾

I probably understand what you mean. However, SEMC_DBICR0 is to configure the Display Bus Interface control function, how to configure this register, there is not much description about this register in the RT1052 reference manual, SEMC_SDRAMCR0 is easy to understand, look up the DATASHEET of the SDRAM, and the corresponding register is The configuration of SEMC_SDRAMCR0 is easy to understand.

Re: RT1052的DCD文件SDRAMCR0与SEMC_DBICR0两个寄存器配置矛盾You are also an employee of NXP. You can't get the details of SEMC_DBICR0 register? Yesterday, I attended one of your meetings, and your technical engineers from NXP's China team would also find it difficult to master the RT series MCUs?
Tags (1)
No ratings
Version history
Last update:
‎05-10-2026 04:31 AM
Updated by: