Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
HDMI Audio Setting 1. Set up HDMI 2. Test raw audio 3. Make HDMI audio the default output 4. Encoded audio 1. Set up HDMI Set up your kernel to use HDMI adding the following code to bootargs on u-boot: video=mxcfb0:dev=hdmi,1920x1080M@60,if=RGB24 2. Test raw audio In order to test only raw audio, use the following command: aplay -D hw:1,0 Kaleidoscope.wav 3. Make HDMI audio the default output In order to configure audio output over HDMI, please, replace content of file ~/.asoundrc to the following one pcm.dmix_48000{      type dmix      ipc_key 5678293      ipc_key_add_uid yes      slave{           pcm "hw:1,0"           period_time 0           period_size 2048           buffer_size 24576           format S16_LE           rate 48000      } } pcm.!dsnoop_44100{      type dsnoop      ipc_key 5778293      ipc_key_add_uid yes      slave{           pcm "hw:0,0"           period_time 0           period_size 2048           buffer_size 24576           format S16_LE           rate 44100      } } pcm.!dsnoop_48000{      type dsnoop      ipc_key 5778293      ipc_key_add_uid yes      slave{           pcm "hw:1,0"           period_time 0           period_size 2048           buffer_size 24576           format S16_LE           rate 48000      } } pcm.asymed{      type asym      playback.pcm "dmix_48000"      capture.pcm "dsnoop_44100" } pcm.dsp0{      type plug      slave.pcm "asymed" } pcm.!default{      type plug      route_policy "average"      slave.pcm "asymed" } ctl.mixer0{      type hw      card 0 } This will configure alsa to use sound card hw:1,0. Please, pay attention to use the proper audio card name for your device. In order to see available sound cards on board: root@imx53qsb:~# aplay -l **** List of PLAYBACK Hardware Devices **** card 0: imx3stack [imx-3stack], device 0: SGTL5000 SGTL5000-0 []   Subdevices: 1/1   Subdevice #0: subdevice #0 card 1: imx3stackspdif [imx-3stack-spdif], device 0: IMX SPDIF mxc spdif-0 []   Subdevices: 1/1   Subdevice #0: subdevice #0 For detail on how to create asound.conf, please see alsa-lib configuration introduction. 4. Encoded audio For encoded (i.e. AC3, DTS) audio, you can use, for example, ac3dec, an utility provided by alsa-tools with the following command line: ac3dec -D hw:1,0 -C test.ac3 This would work for both HDMI audio and SPDIF audio. Double check your hardware and/or schematic in order to know which one to use. i.MX53 Multimedia Re: HDMI Audio Setting Dear Daiane Angolini, I created a new ticket through SR. Please check the below case from SR. [Case:00198948] How to configure the HDMI Audio as 24bit in i.MX6Q / Linux 3.14.52 Best Regards, Eric. Re: HDMI Audio Setting Could you, please, create a new ticket? Otherwise it might get off the radar Re: HDMI Audio Setting Dear Daiane Angolini, I want to know how to configure the HDMI Audio as 24bit in i.MX6Q / Linux 3.14.52. Please let me know how to do that. It's very helpful to me if you tell me how to confirm that in i.MX6Q Evaluation board. Actually I could confirm the below contents in the some documents. - HDMI Audio 24bit is supported in the i.MX6Q Reaference Manual   . Table 33-6. Data Arrangement in System Memory for L-PCM (24 bits) in Chapter 33   . - HDMI Audio 24bit is NOT supported in the i.MX6 Linux Reference Manual for Linux 3.14.52   . Chapter 15 On-Chip High Definition Multimedia Interface (HDMI) Driver   . Best Regards, Eric. Re: HDMI Audio Setting look for some pulseaudio conf file. Create a bbappend on your meta layer in order to add this by default on your image. (sorry, i don't know pulseaudio ) Re: HDMI Audio Setting i think the pulseaduio detect the output of audio, sometime is HDMI and sometime is the other, so i need to specify the HDMI as the default output, how to do ? Re: HDMI Audio Setting it looks like bad, i also stat up the daemon like what i said in mail list, i restart again with command "pulseaudio -D", the output of audio is not from HDMI except the "card 0: wm8962audio [wm8962-audio], device 0: HiFi wm8962-0 []" it's really strange, help... Re: HDMI Audio Setting Well, I think you make it work (by your comment on meta-freescale) Re: HDMI Audio Setting Hi,      There is not the command "pacmd", just "pactl". BTW, i use the YOCTO project of FSL community to build all, what is my next step about for your ask ? Re: HDMI Audio Setting ohhhhhhhhhhhh you´re right! the way to configure pulseaudio is different.... From my old emails, I got this command line: pacmd set-default-sink 1 Could you, please, give it a try and let us know the results? Re: HDMI Audio Setting good, it really works if i use the native app to play audio in IMX6QSD but there is no audio output from HDMI with the pulse audio server. the output of audio just is from the "wm8962audio" as bellow in my IMX6QSD, any advices about this ? i want to use pulse audio server to output in HDMI interface. root@imx6qsabresd:~# aplay -l **** List of PLAYBACK Hardware Devices **** card 0: wm8962audio [wm8962-audio], device 0: HiFi wm8962-0 []   Subdevices: 1/1   Subdevice #0: subdevice #0 card 1: imxhdmisoc [imx-hdmi-soc], device 0: IMX HDMI TX mxc-hdmi-soc-0 []   Subdevices: 0/1   Subdevice #0: subdevice #0 Re: HDMI Audio Setting Hello, Very beautiful guide, how to set default SPDIF audio card on Android ? Thanks
View full article
Example MCAL S32K312 MEM_InFls DS3.5 RTD300 *******************************************************************************  The purpose of this demo application is to present a usage of the MEM_InFls MCAL Driver for the S32K3xx MCU.  The example uses MEM_InFls driver to write 128 bytes to FLASH memory address  0x50_0000 .  ------------------------------------------------------------------------------ * Test HW: S32K3X2EVB-Q172 * MCU: S32K312 * Compiler: S32DS3.5 * SDK release: RTD 3.0.0 * Debugger: PE micro * Target: internal_FLASH ******************************************************************************** Dinesh_Guleria_0-1715852390344.png Results :-- Dinesh_Guleria_1-1715852435648.png Ram location where FLASH writing erase code is placed :-- I placed the code at 256 byte below the MAX address of the RAM size 0x20417DAA = 541162922 Dinesh_Guleria_4-1715852864835.png Dinesh_Guleria_3-1715852777286.png Size of RAM need to save the flashing routine, as per the MAP & linker file :-- 0x00407e64 - 0x00407e38 = 44 bytes Dinesh_Guleria_2-1715852737622.png Dinesh_Guleria_5-1715852986217.png  S32K3 FLASH Memory Terminology :-- Dinesh_Guleria_0-1715853503848.png Dinesh_Guleria_2-1715853660788.png Dinesh_Guleria_3-1715853699814.png  
View full article
How to Update eIQ Projects with the Latest eIQ Neutron SDK Libraries eIQ Neutron SDK is a new software package that includes the Neutron Compiler tool and eIQ Neutron libraries to run Neutron converted neural network models on devices that have an eIQ Neutron NPU like MCX N, i.MX RT700, or i.MX95 Previously the Neutron Compiler tool was part of eIQ Toolkit. However going forward, new versions of the Neutron Compiler tool will be released as part of the eIQ Neutron SDK. This change will allow for more frequent updates to provide better performance and additional operator support. The Neutron Compiler tool was previously named the Neutron Converter tool, but the name was changed in August 2026 with the release of eIQ Neutron SDK 3.2.1. The functionality is the same, just the name changed.  MCUXpresso SDK and Linux BSP use Neutron libraries as part of the eIQ examples included in those software releases. However to use the latest Neutron Compiler, an eIQ project will need to be updated to use the latest Neutron software libraries. This post walks through where to place the updated Neutron libraries and header files.  If the version of the Neutron Compiler tool that was used to convert a model does not match the Neutron libraries used by the eIQ project, then during inference you will see the following error(s) printed on the serial terminal and may get incorrect results: Microcode version mismatch Or Internal Neutron NPU driver error 281b in model prepare Or Incompatible Neutron NPU microcode and driver versions The version of the Neutron Compiler tool that was used to convert a model can be found by either viewing the converted model in Netron or by looking at the generated header file:   header.png netron.png Here is a table showing where you can find the matching version of the Neutron Compiler tool for the default Neutron libraries found in different versions of MCUXpresso SDK: MCUXpresso SDK Default Neutron Library Version in MCUXpresso SDK Default Compatible Neutron Compiler/Converter Can Be Found In 24.12 1.2.0+0x6f710a6d eIQ Toolkit 1.17 25.03 1.2.0+0X1b86b19d eIQ Toolkit 1.17 25.06 2.0.2 eIQ Toolkit 1.17 25.09 2.1.3 eIQ Toolkit 1.17 25.12 2.2.2 eIQ Neutron SDK 2.2.2 26.03 3.0.0 eIQ Neutron SDK 3.0.0 26.06 3.1.1 eIQ Neutron SDK 3.1.1 Manually Update SDK Libraries To Use Latest Version eIQ Neutron SDK 3.2.1 It is highly recommend to always use the latest Neutron Compiler tool and to update the libraries in your eIQ project to match the latest Neutron Compiler tool. The libraries can be updated by overwriting the original files. You may wish to make a backup first though as the default eIQ examples in that SDK will use models that were converted to match those original Neutron libraries. The Neutron file structure in eIQ Neutron SDK and MCUXpresso SDK are now the same so that the entire Neutron folder can be overwritten directly.  Updating Neutron Libraries in MCUXpresso SDK 25.12 and later: File Source Directory in eIQ Neutron SDK Target Directory in MCUXpresso SDK libNeutronDriver.a target\imxrt700\ rt700\cm33\ \middleware\eiq\neutron\rt700\cm33\ libNeutronFirmware.a target\imxrt700\ rt700\cm33\ \middleware\eiq\neutron\rt700\cm33\ NeutronDriver.h target\imxrt700\ driver\include\ \middleware\eiq\neutron\driver\include\ NeutronErrors.h target\imxrt700\ common\include\ \middleware\eiq\neutron\common\include\ Note: The target\imxrt700\driver\include\NeutronEnvConfig.h and the libraries in target\imxrt700\cmodel are used by the ExecuTorch inference engine and so are not needed for TFLM eIQ projects.  Note: In MCUXpresso SDK 26.03 there are two sets of Neutron libraries in imported projects. It's the files in the /middleware/eiq folder that need to be updated.  anthony_huereca_0-1776090421844.png Updating Neutron Libraries in MCUXpresso SDK 25.09 or before: File Source Directory in eIQ Neutron SDK Target Directory in MCUXpresso SDK libNeutronDriver.a target\imxrt700\ rt700\cm33\ \middleware\eiq\tensorflow-lite\third_party\neutron\rt700\ libNeutronFirmware.a target\imxrt700\ rt700\cm33\ \middleware\eiq\tensorflow-lite\third_party\neutron\rt700\ NeutronDriver.h target\imxrt700\ driver\include\ \middleware\eiq\tensorflow-lite\third_party\neutron\driver\include\ NeutronErrors.h target\imxrt700\ common\include\ \middleware\eiq\tensorflow-lite\third_party\neutron\common\include\ Updating Neutron Libraries for MCUXpresso SDK 2.16 or before: Replace the entire middleware\eiq directory from MCUXpresso SDK 26.03 into your project, and then the Neutron libraries can be updated per the instructions above. In these older MCUXpresso SDK releases there were additional eIQ changes beyond just the four files above, so the easiest method to update those older projects is just to replace the entire eIQ middleware directory.  Updating Neutron Libraries for i.MX devices: To update the neutron runtime on a target device, upload the files to their designated directories, as follows: File Target Directory NeutronFirmware.elf /lib/firmware libNeutronDriver.so /lib/ libneutron_delegate.so /lib/
View full article
ウェビナー:今すぐ登録して、i.MX RT1170で魅力的なIoTエクスペリエンスを作成する方法を学びましょう いつ: 9月14日火曜日の午前11時(東部標準時) 今すぐ登録するには、ここをクリックしてください。 ディスカッションのトピック 民生機器から産業機器へ、すでにパラダイムシフトが始まっています。スマートフォンでの日常的な体験は、私たちが使用する組み込み製品の基盤として、より高いパフォーマンス、より多くの接続性、および優れたユーザーエクスペリエンスに対する需要を後押ししています。 しかし、どうすれば製品を次のレベルに簡単に引き上げることができますか? NXPとCrank Softwareに参加して、NXP I.MX RT1170クロスオーバーMCUが作成に適した組み込みハードウェアであり、開発リスクの低減に役立つ理由と、魅力的なユーザーエクスペリエンスの開発が開発ワークフローの一部になることがどのように簡単になるかを学びます。 このセッションでは、次のことを学びます。 i.MX RT [1170] クロスオーバー・マイコンによる電力と性能の最適化について エンベデッドGUI開発が、開発とデザインの間のコラボレーション・エクスペリエンスになる仕組み Storyboardのラピッドデザインとイテレーションテクノロジーが開発中のUIデザインの変更をどのように受け入れるか ハードウェアの可能性を最大限に引き出すためにどのような統合機能が役立つか ストーリーボードのライブデモによるGUIアプリの開発のしやすさ
View full article
带 DMA 的 S32K358 RTD ICU 示例 德拉支持、 我的客户 Aptiv 正在寻找基于 DMA 的 ICU 处理。根据传入的上升沿,应在 mcl 驱动程序中配置 DMA 交易。在我们的 RTD ICU 用户手册中,自某些版本发布以来,我们发现了同样的说法: 3.6.1 带有 DMA 功能的 Icu 有关此功能 的提示将在下一版本中添加。 它在 RTD5.00 / 6.0.0 和 7.0.0 中 我们是否有工作示例向 Aptiv 演示如何使用该功能? 最好是 S32K358 RTD6.0.0,但如果有其他版本也可以。 顺祝商祺! 维克托 优先级:高 RTD 资料来源直接客户 Re: S32K358 RTD ICU Example with DMA 你好@viktorfellinger、 该功能有一些注意事项: - DMA 只支持 IcuMeasurementMode 为 ICU_MODE_SIGNAL_MEASUREMENT 或 ICU_MODE_TIMESTAMP。 - DMA 功能仅支持 eMios SAIC 模式下的 ICU_MODE_SIGNAL_MEASUREMENT。 - 只有部分 Emios 通道支持 DMA,您可以通过所附的 excel 找到这一点:RM 中的 S32K3xx_DMAMUX_map,就像这样: 在我的例子中,我使用 Emios_0,通道 1 来测量信号。 在 Icu: 在 Mcl 中,使用 DMA_TCD0 在 Rm: 在平台上: 我在这里附上了我在软件包中使用所附示例 (RTM600) 的示例,然后添加了这个功能。 我还创建了票证:ARTDCT1-637,以便 SW 团队可以在下一个版本中更新本章。 顺祝商祺! Nhi
View full article
PN7160 PN7220 Android 15 移植到 i.MX8MN-EVK 简介 我们有一份官方的PN7160/PN7220 Android 15移植指南(PN7160/PN7220 – Android 15 移植指南)。但这些补丁仅适用于Android 15 AOSP r1(android-15.0.0_r1)。如果用户想移植到较新版本的AOSP,在源代码编译过程中会出现很多错误。本文件供客户参考,以便逐一解决错误。 注意:所有修改仅供参考。它们不是 NXP 官方针对 AOSP 新版本移植提供的补丁。因此,这些修改可能并非最佳解决方案。请客户根据自身需求修改 AOSP 源代码。 硬件板: i.MX8MN EVK PN7160 EVK PN7220 EVK 为 i.MX8MN EVK 构建 Android 我使用的 i.MX Android BSP 是 Android 15.0.0_2.0.0 (L6.12.20_2.0.0 BSP),可从此处下载:用于 i.MX 应用处理器的 Android 操作系统 | NXP 半导体。 1. 下载"文档"和"安装代码包"。 2. 首先按照 Android BSP 为 i.MX8MN EVK 构建 Android BSP。 根据 android_build/.repo/manifests/aosp-android-15.0.0_2.0.0.xml,您将看到 AOSP 版本是 android-15.0.0_r32。 现在,请按照 PN7160/PN7220 – Android 15 移植指南,将 NFC 移植到 i.MX Android BSP。 1. 内核驱动程序: 为了与 PN7220 或 PN7160 建立连接,Android 协议栈使用 nxpnfc 内核驱动。您可以从下面的 GitHub 链接下载驱动程序: nfcandroid_platform_drivers/drivers at br_ar_16_comm_infra_dev · nxp-nfc-infra/nfcandroid_platform_drivers · GitHub git clone "https://github.com/nxp-nfc-infra/nfcandroid_platform_drivers.git"-b br_ar_16_comm_infra_dev 驱动程序适用于 Kernel 6.6 和 6.12。因此,请下载适合您移植的正确版本。例如,i.MX Android BSP Android 15.0.0_2.0.0 中的 Kernel 版本为 6.12。因此,我将使用针对 6.12 的驱动程序进行移植。 在移植过程中,请确保 Makefile 和 Kconfig 文件中的 PATH 设置正确。 例如在我的移植中: android_build/vendor/nxp-opensource/kernel_imx/drivers/nfc$ tree . ├── Kconfig ├── Makefile └── pn7160 ├── common.c ├── common.h        ├── i2c_drv.c        ├── i2c_drv.h        ├── Kbuild         ├── Kconfig         ├── Makefile         ├── spi_drv.c        └── spi_drv.h 1 个目录,11 个文件 android_build/vendor/nxp-opensource/kernel_imx/drivers/nfc$ cat Makefile # # 内核NFC设备驱动程序的Makefile。 # obj-y += pn7160/ android_build/vendor/nxp-opensource/kernel_imx/drivers/nfc$ cat Kconfig source "drivers/nfc/pn7160/Kconfig" 2. 将 “nxpnfc” 添加到 i.MX8MN EVK 设备树文件中。 在板上显示连接表。 显示图片 &i2c3 { clock-frequency = <100000>; pinctrl-names = "default", "gpio"; pinctrl-0 = <&pinctrl_i2c3>; pinctrl-1 = <&pinctrl_i2c3_gpio>; scl-gpios = <&gpio5 18 GPIO_ACTIVE_HIGH>; sda-gpios = <&gpio5 19 GPIO_ACTIVE_HIGH>; status = "okay"; nxpnfc@28{ compatible = "nxp,nxpnfc"; reg = <0x28>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_nfc>; nxp,nxpnfc-irq = <&gpio3 22 0>; nxp,nxpnfc-ven = <&gpio3 20 0>; nxp,nxpnfc-fw-dwnld = <&gpio3 21 0>; }; &iomuxc {         pinctrl_nfc: nfcgrp {                 fsl,pins = <                         MX8MN_IOMUX_SAI5_RXC_GPIO3_IO20                 0X19  // VEN MX8MN_IOMUX_SAI5_RXD0_GPIO3_IO21 0X19 // FW-DWNLD MX8MN_IOMUX_SAI5_RXD1_GPIO3_IO22 0X19 // IRQ                 >;         }; 显示示意图。 3. 修改 imx8mn_gki.fragment nano vendor/nxp-opensource/kernel_imx/arch/arm64/configs/imx8mn_gki.fragment 添加 CONFIG_NXP_NFC_I2C=m 4. 转到设备 device/nxp/imx8m/evk_8mn/ 修改 BoardConfig.mk。 # selinux permissive +BOARD_KERNEL_CMDLINE += androidboot.selinux=permissive BOARD_SEPOLICY_DIRS := \ $(CONFIG_REPO_PATH)/imx8m/sepolicy \        $(IMX_DEVICE_PATH)/sepolicy  \ +       vendor/nxp/nfc/sepolicy \ + vendor/nxp/nfc/sepolicy/nfc ShareBoardConfig.mk     $(KERNEL_OUT)/drivers/net/phy/realtek.ko \ $(KERNEL_OUT)/drivers/pps/pps_core.ko \     $(KERNEL_OUT)/drivers/ptp/ptp.ko \ $(KERNEL_OUT)/drivers/net/ethernet/freescale/fec.ko + $(KERNEL_OUT)/drivers/nfc/nfc/nxpnfc-i2c.ko endif     $(KERNEL_OUT)/drivers/trusty/trusty-core.ko \     $(KERNEL_OUT)/drivers/trusty/trusty-log.ko \     $(KERNEL_OUT)/drivers/trusty/trusty-ipc.ko \     $(KERNEL_OUT)/drivers/trusty/trusty-virtio.ko \ + $(KERNEL_OUT)/drivers/nfc/nfc/nxpnfc-i2c.ko else BOARD_VENDOR_RAMDISK_KERNEL_MODULES += \     $(KERNEL_OUT)/drivers/input/touchscreen/goodix_ts.ko \     $(KERNEL_OUT)/drivers/input/touchscreen/synaptics_dsx/synaptics_dsx_i2c.ko endif Compatibility_matrix.xml         netutils-wrapper 1.0     android.hardware.emvco 1         IEmvco default     device_framework_matrix.xml nxp.hardware.secureime 1 ISecureIME default     nxp.hardware.imx_dek_extractor 1 IDek_Extractor default     vendor.nxp.nxpnfc 2.0 INxpNfc default     android.hardware.emvco 1 IEmvco default     evk_8mn.mk # -------@block_bluetooth------- # Bluetooth HAL PRODUCT_PACKAGES += \     android.hardware.bluetooth \     android.hardware.bluetooth-service.default.nxp # NXP 8987 蓝牙厂商配置 PRODUCT_PACKAGES += \ bt_vendor.conf # ------nfc------- $(call inherit-product, vendor/nxp/nfc/device-nfc.mk) $(call inherit-product, vendor/nxp/emvco/device-emvco.mk) PRODUCT_PACKAGES += \ android.hardware.nfc-service.nxp PRODUCT_PACKAGES += \         com.nxp.emvco \         com.nxp.nfc \ nfc_nci_nxp_pn72xx # -------@block_usb------- Init.rc 在 post-fs && property:vendor.skip.charger_not_need=0     # 一次只交换一页     写入 /proc/sys/vm/page-cluster 0 # 授予获取 statsd 的 available_pages 信息的权限 chown system system /proc/pagetypeinfo     chmod 0440 /proc/pagetypeinfo     exec u:r:vendor_modprobe:s0 -- /vendor/bin/modprobe -a -d \ /vendor/lib/modules nxpnfc_i2c 写入 /sys/power/wake_lock nosleep 在 post-fs-data && property:vendor.skip.charger_not_need=0 setprop vold.post_fs_data_done 1 ueventd.nxp.rc /sys/devices/virtual/thermal/thermal_zone* trip_point_0_hyst 0660 系统 系统 /sys/devices/virtual/thermal/thermal_zone* trip_point_1_hyst 0660 系统 系统 /dev/dmabuf_imx           0664   系统     系统 /sys/class/backlight/* 亮度 0660 系统 系统 /dev/ttymxc1              0666   nfc   nfc /dev/ttymxc2 0666 nfc nfc /dev/nxpnfc 0666 nfc nfc # 用于 libcamera /dev/media* 0660 system camera /dev/v4l-subdev* 0660 系统摄像头 5. hardware/interfaces/compatibility_matrices/compatibility_matrix.202404.xml android.hardware.wifi.hostapd 1 IHostapd default     android.hardware.wifi.supplicant 2 ISupplicant default     nxp.hardware.imx_dek_extractor 1 IDek_Extractor default     vendor.nxp.nxpnfc 2.0 INxpNfc default     vendor.nxp.emvco 1 INxpEmvco default     6.  android_build/vendor/nxp/nfc/device-nfc.mk android_build/vendor/nxp/emvco/device-emvco.mk 两种方法。 1. 将 NXP NFC 补丁应用到 Android AOSP,然后进行构建。如果 Android 版本过新,将会出现大量错误。 2. 先将 R1 文件复制到 R30,然后应用 NXP NFC 补丁。然后构建。 我使用第二种方法。 下载 AOSP R1 源代码。 将 R1 复制并替换以下文件夹。 应用补丁。 版本代码。 以下是错误列表及参考解决方案。
View full article
【新手指南】如何构建 Yocto Linux BSP - i.MX FRDM 开发板版(日语博客) 本指南将向您展示如何使用 i.MX FRDM 板作为基础构建 Yocto Linux。 本文以 FRDM-IMX93 为例,但同样的步骤也可用于在其他 i.MX FRDM 板上进行构建。 本文以“Linux 6.12.49_2.2.0 ( Yocto 5.2 “Walnascar” )”为例,描述了 Yocto Linux BSP。 问:i.MX FRDM 板是什么? 答:i.MX FRDM 开发板是一款价格更实惠、体积更小的开发板,相比恩智浦功能齐全的 EVK 开发板,它的功能有所减少。其目的是方便用户进行基本的评估和原型设计。 1. 环境与准备 1.1.环境 大项目 小项目 内容 备注 文档 - IMX_YOCTO_PROJECT_USERS_GUIDE.pdf (这是主要方法。它描述了构建 BSP 的步骤。) i.MX Linux ®发行说明 (您可以查看支持功能列表。) i.MX 移植指南 (实际实施时需要注意的要点总结) 点击此处下载Yocto Linux 通用文档。 硬件 FRDM板 FRDM-IMX8MPLUS FRDM-IMX91S FRDM-IMX91 FRDM-IMX93 FRDM-IMX95 本章将以 FRDM-IMX93 为基础进行解释。 主机 PC Ubuntu 环境 ・VMware/Virtual Box 等(在 Windows 上) ・Native Linux 以下选项之一 推荐版本:Ubuntu 22.04 或更高版本 SD卡+读卡器/写入器 建议使用 16GB 或更多内存   硬件 (选项) MIPI 摄像头 (选项) 兼容BSP的MIPI相机 (参见 i.MX Linux ®发行说明) USB摄像头也可以替代(可能会出现延迟) 显示 (选项) 展示   USB 设备 (选项) USB鼠标、USB存储器   耳机 (选项) 3.5mm 耳机 带麦克风的耳机(例如老款 iPhone 附带的耳机)更好。 软件 Yocto 环境 Linux BSP (这次我们使用了 Linux 6.12.49_2.2.0( Yocto 5.2 “Walnascar” )) 本文将介绍安装过程,包括安装方法。 1.2.图例 命令提示符图例 =>           u-bootプロンプト $            BSPがインストールされているLinux PCのプロンプト 2. 主机 推荐使用 Ubuntu 22.04 桌面版。为了获得较为流畅的使用体验,建议使用至少配备 8 个线程和 16GB 内存的主机。所需的存储空间会根据具体项目而有所不同,小型项目大约需要 50GB,大型项目则需要 500GB。 2.1。Yocto 所需的软件包 请按照以下步骤安装所需的软件包。 $ sudo apt-get install build-essential chrpath cpio debianutils diffstat file gawk gcc git iputils-ping libacl1 liblz4-tool locales python3 python3-git python3- jinja2 python3-pexpect python3-pip python3-subunit socat texinfo unzip wget xzutils zstd efitools curl 注意:除了 IMX_YOCTO_PROJECT_USERS_GUIDE.pdf 中的信息外,还添加了curl 。 2.2. 设置交换文件 以下是设置 32GB 交换文件的示例。 $ sudo fallocate -l 32G /swapfile $ sudo chmod 600 /swapfile $ sudo mkswap /swapfile $ sudo swapon /swapfile 注意:如果/swapfile 目录已存在,则第一行命令将失败。如果要更改其大小,请执行以下命令,然后再运行上面的命令。 $ sudo swapoff /swapfile $ sudo rm /swapfile 要在主机启动时自动挂载交换文件,请将以下行添加到/etc/fstab文件中: /swapfile none swap sw 0 0 3. Yocto Linux BSP 从 nxp.jp 网站的“i.MX 应用处理器的嵌入式 Linux”部分,选择所需的 Linux BSP 版本,并获取 i.MX Yocto 项目用户指南。 Yocto User Guide.jpg 按照 i.MX Yocto 项目用户指南 (IMXLXYOCTOUG) 中的“4 Yocto 项目设置”部分的步骤创建映像。 本文档假设使用以下设置生成图像。 发行版 = fsl-imx-xwayland 机器 = imx93-11x11-lpddr4x-frdm 3.1. 设置和构建 Yocto BSP 有关主机设置,请参阅 2. 主机。 3.1.1.安装仓库实用程序 $ mkdir ~/bin $ curl https://storage.googleapis.com/git-repo-downloads/repo > ~/bin/repo $ chmod a+x ~/bin/repo 3.1.2. 将存储库添加到您的 PATH 环境变量中 将以下行添加到$HOME/.bashrc文件中: export PATH=~/bin:$PATH 3.1.3.Git 设置 $ git config --global user.name "Your Name" $ git config --global user.email "Your Email" $ git config --list 3.1.4.Yocto BSP 设置 $ mkdir imx-yocto-bsp $ cd imx-yocto-bsp $ repo init -u https://github.com/nxp-imx/imx-manifest -b imx-linux-walnascar -m imx-6.12.49-2.2.0.xml $ repo sync 3.1.5.设置构建目标,构建 $ MACHINE=imx93-11x11-lpddr4x-frdm DISTRO=fsl-imx-xwayland source ./imx-setup-release.sh -b build $ bitbake imx-image-full *构建完成后,将生成一个 Linux 镜像。 * 有关如何写入生成的映像的说明,请参阅您的特定 FRDM 板的入门指南中的步骤 1 和 2。 FRDM-IMX8MPLUS 入门指南 FRDM-IMX91 入门指南 FRDM-IMX91S 入门指南 FRDM-IMX93 入门指南 FRDM-IMX95 入门指南 注意:如果您想为其他 FRDM 板构建 Linux BSP,请将上述命令中的“ MACHINE= ”部分替换为以下名称。 imx8mp-lpddr4-frdm (FRDM-IMX8MPLUS) imx91-11x11-lpddr4-frdm (FRDM-IMX91) imx91-11x11-lpddr4-frdm-imx91s (FRDM-IMX91S) imx93-11x11-lpddr4x-frdm (FRDM-IMX93) imx95-15x15-lpddr4x-frdm (FRDM-IMX95) 注意:对于图形功能,您还可以使用上述命令中的“ DISTRO = ”部分选择发行版。 fsl-imx-wayland (Wayland) fsl-imx-xwayland (与使用 Wayland 和 X11 *EGL 的 X11 应用程序不兼容) 注意:每个项目只能使用imx-setup-release.sh脚本进行一次设置。如果对现有项目执行此操作,将会生成诸如conf/local.conf之类的新文件,并且您之前的设置将会丢失。如果您希望重用现有项目……3.3.1.请参阅“从现有构建目录恢复工作”。 注意:根据主机配置的不同,构建过程可能需要数十小时。此外,预计会占用 400-500GB 的存储空间。 注意:在多核多线程主机上构建时,如果内存不足以支持所有线程,则会发生内存交换。限制线程数的方法将在 3.4.2 节中介绍。请参阅“限制构建过程中运行的线程数”。 注意:Ubuntu 22.04 初始状态下可能未配置交换分区,这会导致系统运行极其缓慢甚至崩溃。交换分区文件配置如下:2.2.请参阅有关配置交换文件的章节。 以下信息仅供参考。 3.2 构建和安装工具链 您可以构建和安装交叉编译器等工具链。通过使用此处生成的脚本,您可以避免交叉编译过程中经常出现的问题,例如找不到要链接的包含文件或库。 3.2.1.工具链的构建 $ bitbake imx-image-full -c populate_sdk 3.2.2.安装 $ tmp/deploy/sdk/fsl-imx-xwayland-glibc-x86_64-imx-image-full-armv8a-imx93-11x11-lpddr4x-pf0900-evk-toolchain-6.12-walnascar.sh 这里我们就不解释如何使用该工具链了。 3.3.常用的 Yocto bitbake 命令和设置 3.3.1.从现有构建目录继续工作。 $ cd /path/to/imx-yocto-bsp $ source ./setup-environment build 注意:这里提到的路径和目录来自 3.1.4 节。Yocto BSP 设置,3.1.5。构建目标设置在构建过程中已配置。 下面我们将以 linux-imx 为例,给出一些命令示例。您可以将“ linux-imx ”替换为其他软件包名称,对每个软件包执行相同的操作。 3.3.2. 软件包的重新构建 $ bitbake -c compile linux-imx -f $ bitbake -c install linux-imx $ bitbake -c deploy linux-imx 如果不添加注释-f ,则可以跳过这些步骤。 注意 - 某些软件包在使用 `-c deploy` 进行部署时可能会显示错误,但在大多数情况下,这仅仅是因为 `do_deploy` 命令不可用,因此您可以忽略该错误。 3.3.3 删除软件包 如果某个软件包出现不应发生的错误,请尝试使用以下命令删除该软件包,然后重试。这或许可以解决错误。(这是因为软件包可能在下载过程中损坏,或者如果构建过程过早终止,则可能残留一些垃圾数据。) $ bitbake -c cleansstate linux-imx 注意:提取出的所有源代码都将被删除,因此如果您正在编辑任何文件,请务必小心。 3.3.4. 软件包提取 如果您只想提取软件包而不想编译它 $ bitbake -c patch linux-imx 3.3.5. 将更改应用到配置文件 如果您想更改配置文件(例如arch/arm64/configs/imx_v8_defconfig )并希望这些更改生效: $ bitbake -c configure linux-imx $ bitbake -c compile linux-imx -f 3.3.6. 运行 linux-imx menuconfig 更改 Linux 内核的构建选项时 $ bitbake -c menuconfig linux-imx 此时会弹出一个类似这样的窗口,请进行必要的更改并保存(使用十字光标键选择所需项目,然后按空格键确认)。 有关建造方面的技巧,请参考以下文章。 Yocto Linux BSP 构建技巧 - i.MX 8M Plus 版 ========================= 即使您在本文的“评论”栏留言,我们目前也无法回复。 给您带来不便,我们深感抱歉。请在询问时参阅“NXP技术问题-联系方式(日本博客)”。 (如果您已经是NXP的代理商或与其有合作关系,可以直接向负责人咨询。) 本指南将向您展示如何使用 FRDM(Freedom)板构建 Linux BSP,使您能够以紧凑且经济实惠的方式开始使用嵌入式 Linux。 本文以 FRDM-IMX93 为例,但同样的步骤也可用于在其他 i.MX FRDM 板上进行构建。 本文以“Linux 6.12.49_2.2.0 (Yocto 5.0.4)”为例,对 Yocto Linux BSP 进行了描述。 i.MX 处理器 SW | 下载 日本博客
View full article
扩展你的 Android 应用显示 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 许多用户询问过但仍在为 Android 开发中的功能之一是扩展桌面功能。目前,Android 允许您在两个显示器上镜像您的桌面,但您仍然无法像使用 Linux 或 Windows 等任何其他操作系统那样扩展您的桌面。 本教程旨在向您展示如何使用特殊对象来控制辅助或外部显示器上显示的内容,从而取代屏幕镜像。 那么我们该怎么做呢? 演示文稿是在外部显示器上以视图层次结构的形式显示用户界面的容器。这非常类似于对话框,因为它显示与其活动分开的 UI,但不同之处在于演示文稿显示在外部显示器上,而对话框将其显示在主屏幕上。现在,由于这个原因,外部显示器上的 UI 要使用的资源与主屏幕上使用的资源不同,演示的上下文不是活动。 我们如何选择将此演示文稿发送到哪里? 最简单的方法是使用 MediaRouter API。mediarouter 的作用是跟踪系统上可用的音频和视频路由。无论何时选择或取消选择路线,MediaRouter 都会发送通知。应用程序可以简单地监视这些通知并自动在首选演示显示屏上显示或关闭演示。 首选演示显示器是媒体路由器建议应用程序在想要在辅助显示器上显示内容时使用的显示器。如果没有首选的演示显示,则应用程序应该在本地显示其内容而不使用演示。 使用 Mediarouter MediaRouter 是通过调用 getSystemService() 并请求 MEDIA_ROUTER_SERVICE 获得的系统服务。 我们应该使用 mediarouter 在首选的演示显示器上创建和显示演示文稿: MediaRouter mediaRouter = ( MediaRouter ) context . getSystemService ( Context . MEDIA_ROUTER_SERVICE ); MediaRouter.RouteInfo route = mediaRouter.getSelectedRoute ( ) ;​​ 如果(路线!= null ) { 显示presentationDisplay =路由.getPresentationDisplay () ; 如果( presentationDisplay != null ) { 演示文稿=新MyPresentation (上下文, presentationDisplay ) ; 演示.展示(); } } 为了在您的应用中使用此框架,您需要获取 MediaRouter 框架对象的一个实例并附加一个 MediaRouter.Callback 对象来监听可用媒体路由中的事件。 实现媒体路由器 API 的 Android 应用程序需要包含一个 Cast 按钮,以允许用户选择媒体路由在辅助输出设备上播放媒体。实现 Cast 按钮的推荐方法是从 ActionBarActivity() 扩展您的活动并使用 onCreateOptionMenu() 方法添加选项菜单。Cast 按钮必须使用 MediaRouteActionProvider 类作为其操作: xml 版本= "1.0"编码= "utf-8" ?> <菜单xmlns:android = " http://schemas.android.com/apk/res/android " xmlns:app = " http://schemas.android.com/apk/res-auto " > <项目机器人:ID = “@ + id / media_route_menu_item” 机器人:标题= “@string/media_route_menu_title” 应用程序:actionProviderClass = “android.support.v7.app.MediaRouteActionProvider” app:showAsAction = “总是” /> 媒体路由器框架通过附加到媒体路由器框架对象的回调对象与应用程序进行通信。有必要扩展回调对象以便在媒体路由连接时接收消息。 一旦为媒体路由器定义了回调,您就需要将其附加到媒体路由器对象。下面的示例演示了如何使用生命周期方法来适当地添加和删除应用程序的媒体路由器回调对象。您需要添加和删除它,因为无论何时关闭应用程序或将其放在后台,它都需要是空闲的,以便其他应用程序在必要时使用它。 公共类MediaRouterPlaybackActivity扩展了ActionBarActivity { 私人MediaRouter mMediaRouter ; 私人MediaRouteSelector mSelector ; 私人回调mMediaRouterCallback ; // 您的应用程序可以使用它们,以便框架可以发现它们。 @Override 受保护的void onCreate ( Bundle savedInstanceState ) { 超级. onCreate ( savedInstanceState ); 设置ContentView ( R.layout.activity_main ) ;​​ // 获取媒体路由器服务。 mMediaRouter = MediaRouter.getInstance ( this ) ;​ ... } // 在启动时添加回调来告诉媒体路由器有哪些类型的路由 // 您的应用程序可以使用它们,以便框架可以发现它们。 @Override 公共无效的onStart () { mMediaRouter.addCallback ( mSelector , mMediaRouterCallback ,​​ 媒体路由器.回调标志位 请求发现); 超级. onStart (); } // 停止时删除选择器,告诉媒体路由器它不再 // 需要发现您的应用的路线。 @Override 公共无效onStop () { mMediaRouter.removeCallback ( mMediaRouterCallback ) ;​ 超级. onStop (); } ... } 远程回放 这种方法将控制命令发送到辅助设备以启动播放并控制正在进行的播放(播放、停止、快进、倒带等)。当您的应用支持这种类型的媒体路由时,您必须使用通过应用的 MediaRouter.Callback 对象接收的远程播放 MediaRoute.RouteInfo 对象创建一个 RemotePlaybackClient 对象。 下面的示例代码演示了一个控制器方法,该方法创建一个新的远程播放客户端并向其发送视频进行播放。 私人无效更新远程播放器( RouteInfo路线) { // 改变路线:拆除之前的客户端 如果( mRoute != null && mRemotePlaybackClient != null ) { mRemotePlaybackClient .释放(); mRemotePlaybackClient =空; } // 保存新路线 mRoute =路线; // 附加新的播放客户端 mRemotePlaybackClient =新的RemotePlaybackClient ( this , mRoute ) ; // 发送文件进行播放 mRemotePlaybackClient.play ( Uri .​​解析( “ http://archive.org/download/Sintel/sintel-2048-stereo_512kb.mp4 ” ) “video/mp4” , null , 0 , null , new ItemActionCallback () { @Override public void onResult (捆绑数据,字符串sessionId , MediaSessionStatus会话状态, 字符串itemId , MediaItemStatus itemStatus ) { logStatus ( "播放:项目成功" + itemId ); } @Override public void onError (字符串错误, int代码, Bundle数据) { logStatus ( "播放:失败 - 错误:" + code + " - " + error ); } }); } } 有关如何使用媒体路由器的更多信息,请访问developer.android.com
View full article
i.MX6 での高保証ブート (HAB) <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 要約 セキュリティは、私たちが日常生活で耳にする避けられない言葉です。セキュリティのないテクノロジーは、多くの人にとって「信頼」のないテクノロジーです。私たちは皆、職場からソーシャルチャットまで、セキュリティが私たちの生活でどのように重要な役割を果たしているかを知っています。組み込みシステムであっても、機密データへの不正なアクセスを防ぐためのセキュリティを実装する必要があります。i.MX6 プラットフォームが認証されたイメージでのみ起動できるようにするには、どうすればよいですか。High Assurance Booting(HAB)という名前のクールなものを見てみましょう。これにより、ブートイメージが安全でシンプルになります。 紹介 デジタルセキュリティは、その誕生以来、私たちの生活の避けられない部分となっています。このケースは、特に機密データを扱う場合、どの組み込みシステムでも変わりません。銀行取引、防衛、医療、産業、自動車に使用されている多くの組み込みデバイスは、セキュリティを厳格に実装しています。 ほとんどすべての組み込みシステムは、フラッシュされた画像を通じて与えられる特定の命令に基づいて動作しています。ハッカーが自分の命令を組み込みデバイスにフラッシュできるとしたら、そのデバイスで何をする必要があるかを完全に制御できると想像してみてください。デバイスが銀行の目的で使用している場合、ハッカーはパスワードを含むすべての詳細を取得します。このシナリオは、デバイスが防衛または医療分野で使用されている場合、さらに悪化します。どうすればこのケースを防ぐことができますか?まあ、答えはそれほど簡単ではありません! 組み込みシステムOSイメージは、MMC、SDカード、SATA、イーサネットなどのさまざまなメディアからフラッシュできます。SDカードなどのメディアは簡単に交換できるため、メディアにセキュリティチェックを実装することは困難です。さらに、これらのメディアにフラッシュした後、OSイメージを変更できます。したがって、イメージをフラッシュする前だけにセキュリティチェックを実装するだけでは、この問題に対処するには不十分です。では、OSイメージが十分に安全であることを確認するためのセキュリティチェックをどのように実装できますか?その答えはHAB(High Assurance Boot)です。 フリースケールは、i.MX6Qプロセッサのオプション機能としてHABv4 (最新のHABバージョン4) を提供しました。HABはフリースケールのセキュリティブロックの一部であり、CAAMやTrustZoneなどの他のセキュリティ機能と連携できます。 HAB を使用する利点には、次のものが含まれますが、これらに限定されません。 HABv4 は、一度融合すると変更できないブート ROM レベルのセキュリティを実装しています。 効率的。 イメージがシステムを制御する前のセキュリティチェック。 複数のルート キーを許可します。 デジタル署名を利用する - OSイメージを保護する最も効率的な方法。 OSイメージの機能に影響を与えずに、セキュリティをOSイメージに直接追加します。 OS イメージの検証によるプロセッサ レベルのチェックにより、セキュア ブートが完全に保証されます。 HABの仕組みは? デジタル署名の原則に基づくHAB。デジタル署名は、コンテンツコンテキストに署名することにより、コンテンツを安全に保ちます。この署名プロセスには、最終的な結果を強化するために、複数のセキュリティ アルゴリズムを組み込む必要があります。 HAB デジタル署名は、open-ssl 認証、MD5 ハッシュ、RSA-AES-DES の公開鍵と秘密鍵のチェックを組み合わせたものです。 HAB は、ブートローダー (u-boot) と OS イメージ (uImage) の両方を署名付きイメージにすることでセキュリティを確保します。これらの署名付きイメージには、通常のイメージ コンテンツとセキュリティ手順が含まれています。これらのイメージには、公開鍵と秘密鍵も含まれています。HAB プロセス中、組み合わせから派生した公開鍵ハッシュ・コードは、i.MX6 プロセッサーのブート ROM コードに融合します。この融合により、プラットフォームの安全性が向上し、後で変更することはできません。 ブート時間中、ブートプロセスの初期パラメータは、フラッシュメディア(SDカードなど)からブートROMコードを取り込む必要があります。次に、HAB 命令は、ブート ROM と署名付きイメージの内部に存在するハッシュ値を調べます。これら 2 つのハッシュ値が一致すると、HAB プロセスにより、プラットフォームはイメージを起動できます。それ以外の場合、システムはすべてのプロセスを停止し、許可されたイメージを待ちます。 このようにして、システムは、後の段階で誰かが署名されたイメージを変更した場合でも、許可されていないアクセスから保護する必要があります(これにより、最終的にイメージのハッシュ値が変更されるため、ランタイムチェック中に失敗します)。 iWaveは、 i.MX6Q iW-RainboW-G15D-Q7 Linuxプラットフォーム にHABを成功裏に実装し、HABを検証してプラットフォームを保護する方法を確認しました。ただし、HAB は、開発プラットフォームの購入またはモジュールの購入の一部として提供される標準 BSP の一部ではありません。これは特別なリクエストがある場合にのみ利用できます。 結論 HABは、OSイメージへの不正アクセスを防ぐための最良のソリューションの1つです。機密データ(バンキング、防衛など)を扱う組み込みシステムは、外部ソースによってシステム全体を制御されないように、企業内にHABを配置する必要があります。HAB は i.MX6 プラットフォームのオプション機能ですが、ブート プロセスの安全性を高めるために実装することをお勧めします。 参考: AN4581_HAB_Application_Note.pdf - i.MX50、i.MX53、および i.MX53 および HABv4 を使用した i.MX 6 シリーズでのセキュア ブート アプリケーション ノート i.MX_6_Linux_High_Assurance_Boot_(HAB)_User's_Guide.pdf - i.MX 6 Linux High Assurance Boot (HAB) ユーザーズガイド 全般
View full article
FS27 RTDとBMS GEN2 RTDの互換性に関するコンサルティング こんにちは、専門家の皆様 顧客の新しい BMS プロジェクトでは、 S32K358 + FS27 + BMS GEN2 SDK を使用したいと考えています。 BMS チームから次のことを学びました。 BMS GEN2 SDK AUTOSAR 4.4 R21-11 バージョン0.9.1 CD05および BMS GEN2 SL SDK AUTOSAR 4.4 R21-11 バージョン0.9.1 CD05は来週リリース予定です。S32K3 RTD 6.0.0 との統合をサポートします。 BMS GEN2 SDK は、2026 年第 1 四半期中に BMS リリースv1.0.0でS32K3 RTD 6.0.0に移行される予定です。 つまり、 BMS GEN2 SDK は近い将来S32K3 RTD 6.0.0と互換性を持つようになります。 顧客は 24V プラットフォームを必要としているため、FS26 ではなく FS27 を使用したいと考えています。オートモーティブ SW - SBC/PMIC - リアルタイム・ドライバから、次の 2 つのバージョンの FS27 を見つけました。 S32K3xx SBC FS27 R21-11 0.8.0 ( S32K3 RTD 5.0.0ベース) S32K3 RTD 7.0.0 ベースの SBC FS27 R23-11 1.0.0 Q1.顧客は、S32K3 RTD のバージョンが一貫していないため、FS27 と BMS GEN2 SDK のドライバに互換性がないのではないかと懸念しています。BMS GEN2 SDKでS32K3 RTD 6.0.0 を選択した場合、お客様がS32K3xx SBC FS27 R21-11 0.8.0またはSBC FS27 R23-11 1.0.0を使用すると問題が発生しますか? Q2. FS27にはS32K3 RTD 6.0.0に基づくドライバーがありますか? 助けていただけませんか?ご協力をよろしくお願いします! よろしくお願いいたします ロビン お客様情報は次のとおりです: お問い合わせ名 TengHsaing Wen メール(お問い合わせ)[email protected] 会社名:XINGMOBILITY AA SW - 外部デバイス 優先度: 中 出典: 直接顧客 Re: Consulting on the compatibility of FS27 RTD and BMS GEN2 RTD こんにちは、ヴィクトルさん。 情報をいただきありがとうございます。 S32K3 RTD 6.0.0 に基づく「BMS GEN2 SDK AUTOSAR 4.4 R21-11 バージョン 0.9.1 CD05」はまだダウンロードできません。 ダウンロードできるようになったら、少なくとも正常にコンパイルできるかどうかをテストします。 よろしくお願いいたします ロビン Re: Consulting on the compatibility of FS27 RTD and BMS GEN2 RTD こんにちは、ロビン。 RTD 6.0.0専用のリリースはありませんが、最新バージョン(FS27 1.0.0)下位互換性があるはずです。何か問題がございましたら、お知らせください。 よろしくお願いいたします、ヴィクトル Re: Consulting on the compatibility of FS27 RTD and BMS GEN2 RTD このトピックは調査するためにチームにリダイレクトされました。 連絡先: Razvan Tilimpea / Cristian Durla または Viktor Obr Re: Consulting on the compatibility of FS27 RTD and BMS GEN2 RTD こんにちは、ヴィクトルさん。 「BMS GEN2 SDK AUTOSAR 4.4 R21-11 バージョン 0.9.1 CD05」がダウンロード可能になりました。 お客様は、2 つのドライバ(R23-11とR21-11 ) の AUTOSAR バージョンが大幅に異なり、 SBC FS27 R23-11 1.0.0と組み合わせた場合に互換性の問題が発生するのではないかと疑問を呈していました。 よろしくお願いいたします ロビン Re: Consulting on the compatibility of FS27 RTD and BMS GEN2 RTD こんにちは、ロビン。 異なる AUTOSAR バージョン間の互換性は難しいため、統合しようとしている両方のコンポーネントで使用されるすべてのドライバを比較する必要がありますが、私は BMS SDK に 100% 精通しているわけではありません。FS27 のバージョンとそれが使用するドライバに関しては、R21-11 と R23-11 の間で大きな変更は見られませんでしたが、1 つのプロジェクトでコンポーネントを組み合わせるとすぐにわかる小さな違いがいくつかある可能性があります (バージョン固有のマクロなど)。ただし、機能的な観点からは、同じように動作するはずです。 よろしくお願いいたします。 ヴィクトル Re: Consulting on the compatibility of FS27 RTD and BMS GEN2 RTD こんにちは@viktorobr 、 「BMS GEN2 SDK AUTOSAR 4.4 R21-11バージョン 0.9.1 CD06 」がダウンロード可能になりました。 お客様は、2 つのドライバ(R23-11とR21-11) の AUTOSAR バージョンが大幅に異なり、SBC FS27 R23-11 1.0.0と組み合わせた場合に互換性の問題が発生するのではないかと疑問を呈していました。 よろしくお願いいたします ロビン
View full article
PN7160 PN7220 Android 15のi.MX8MN EVKへの移植 はじめに 当社では、PN7160/PN7220 Android 15公式ポーティングガイド(PN7160/PN7220 – Android 15ポーティングガイド)をご用意しております。ただし、パッチはAndroid 15 AOSP r1(android-15.0.0_r1)専用です。AOSP最新版へのポーティングを希望する場合、ソースコードのコンパイル中でエラーが頻発します。このドキュメントを参考に、エラーを一つずつ解決してください。 注:変更はすべて参考目的で提供されており、AOSP最新版へのポーティング向けのNXP公式パッチではありません。変更が最善の解決策ではない可能性がありますので、AOSPソースコードを自社のニーズに基づいて変更してください。これは製品向けではありません。ポーティング後は、お客様側で引き続き完全なテストを実施する必要があります。 ハードウェアボード: i.MX8MN EVK (i.MX 8M Nano評価キット | NXP Semiconductors) 8mnevk.jpg PN7160 EVK (OM27160|PN7160 プラグアンドプレイ NFC コントローラ用開発キット|NXP Semiconductors) pn7160.jpg bothevk.jpg i.MX8MN EVKとPN7160 OM29110ARD-Bの接続 i.MX8M ナノ EVK ピン PN7160 ピン 3.3V J1003-1 VDD(3.3V) J1-4 5V J1003-2 VBAT(5V) J1-5 I2C3 SDA J1003-3 SDA J2-2 I2C3 SCL J1003-5 SCL J2-1 GPIO3_22 J1003-37 IRQ J2-10 GPIO3_21 J1003-38 REQ J4-2 GND J1003-39 GND J1-6 GPIO3_20 J1003-40 N/A J4-1 i.MX8MN EVK向けAndroidの構築 ここで使用したi.MX Android BSPはAndroid 15.0.0_2.0.0(L6.12.20_2.0.0 BSP)で、こちらからダウンロードしていただけます:i.MX アプリケーション・プロセッサ向けAndroid OS | NXP Semiconductors 1. 「ドキュメント」と「インストールソースパッケージ」をダウンロードします。 2. まず、Androidユーザーガイドの手順に従って、i.MX8MN EVK用のAndroid BSPをビルドします。  android_build/.repo/manifests/aosp-android-15.0.0_2.0.0.xmlによると、表示されるAOSPバージョンはandroid-15.0.0_r32です。 ポーティングに関する参考文献: PN7160/PN7220 – Android 15 移植ガイド  i.MX8M NanoボードでPN7160をAndroid 14に移植 さて、移植を始めましょう。  1. カーネル・ドライバ PN7220またはPN7160との接続を確立するために、Androidスタックはnxpnfcカーネルドライバを使用します。以下のGitHubからドライバをダウンロードできます: br_ar_16_comm_infra_dev · nxp-nfc-infra/nfcandroid_platform_d... の br_ar_16_comm_infra_dev の nfcandroid_platform_drivers/drivers コマンドは次のとおりです。 git clone "https://github.com/nxp-nfc-infra/nfcandroid_platform_drivers.git" -b br_ar_16_comm_infra_dev カーネル6.6および6.12用のドライバがありますので、ポーティングに適したドライバをダウンロードしてください。例えば、i.MX Android BSP Android 15.0.0_2.0.0のカーネルは6.12ですので、ポーティングには6.12ドライバを使用します。 ポーティングする際は、MakefileとKconfigファイルのパスが正しく設定されていることを確認してください。 例えば、ここでは以下のようにポーティングします。 . ├── Kconfig ├── Makefile └── pn7160 ├── common.c ├── common.h ├── i2c_drv.c ├── i2c_drv.h ├── Kbuild ├── Kconfig ├── Makefile ├── spi_drv.c └── spi_drv.h すべてを簡素化するため、I2Cのみをサポートし、SPIはサポートしません。ドライバ/nfc/pn7160/Makefile のデフォルトコードを以下のコードに置き換えてください(理解しやすくするため)。 nxpnfc-i2c-objs = i2c_drv.o common.o obj-$(CONFIG_NXP_NFC_I2C) += nxpnfc_i2c.o ドライバ/nfc/Kconfig の内容。PN7160を以下のように追加してください。 source "drivers/nfc/pn7160/Kconfig" source "drivers/nfc/fdp/Kconfig" source "drivers/nfc/pn544/Kconfig" source "drivers/nfc/pn533/Kconfig" source "drivers/nfc/microread/Kconfig" source "drivers/nfc/nfcmrvl/Kconfig" source "drivers/nfc/st21nfca/Kconfig" source "drivers/nfc/st-nci/Kconfig" source "drivers/nfc/nxp-nci/Kconfig" source "drivers/nfc/s3fwrn5/Kconfig" source "drivers/nfc/st95hf/Kconfig" endmenu The contents of ドライバ/nfc/Makefile. Add the PN7160 like below: # SPDX-License-Identifier: GPL-2.0 # # Makefile for nfc devices # obj-$(CONFIG_NXP_NFC_I2C) += pn7160/ obj-$(CONFIG_NFC_FDP) += fdp/ obj-$(CONFIG_NFC_PN544) += pn544/ obj-$(CONFIG_NFC_MICROREAD) += microread/ obj-$(CONFIG_NFC_PN533) += pn533/ obj-$(CONFIG_NFC_MEI_PHY) += mei_phy.o obj-$(CONFIG_NFC_SIM) += nfcsim.o obj-$(CONFIG_NFC_PORT100) += port100.o obj-$(CONFIG_NFC_MRVL) += nfcmrvl/ obj-$(CONFIG_NFC_TRF7970A) += trf7970a.o obj-$(CONFIG_NFC_ST21NFCA) += st21nfca/ obj-$(CONFIG_NFC_ST_NCI) += st-nci/ obj-$(CONFIG_NFC_NXP_NCI) += nxp-nci/ obj-$(CONFIG_NFC_S3FWRN5) += s3fwrn5/ obj-$(CONFIG_NFC_ST95HF) += st95hf/ obj-$(CONFIG_NFC_VIRTUAL_NCI) += virtual_ncidev.o 2. i.MX8MN EVKデバイスツリーファイルに「nxpnfc」を追加します。 &i2c3 { clock-frequency = <100000>; pinctrl-names = "default", "gpio"; pinctrl-0 = <&pinctrl_i2c3>; pinctrl-1 = <&pinctrl_i2c3_gpio>; scl-gpios = <&gpio5 18 GPIO_ACTIVE_HIGH>; sda-gpios = <&gpio5 19 GPIO_ACTIVE_HIGH>; status = "okay"; nxpnfc@28{ compatible = "nxp,nxpnfc"; reg = <0x28>; pinctrl-names = "default"; pinctrl-0 = <&pinctrl_nfc>; nxp,nxpnfc-irq = <&gpio3 22 0>; nxp,nxpnfc-ven = <&gpio3 20 0>; nxp,nxpnfc-fw-dwnld = <&gpio3 21 0>; }; The GPIO settings in the IOMUXC: &iomuxc { pinctrl_nfc: nfcgrp { fsl,pins = < MX8MN_IOMUXC_SAI5_RXC_GPIO3_IO20 0X19 // VEN MX8MN_IOMUXC_SAI5_RXD0_GPIO3_IO21 0X19 // FW-DWNLD MX8MN_IOMUXC_SAI5_RXD1_GPIO3_IO22 0X19 // IRQ >; }; 3.  imx8mn_gki.fragmentを変更します。 ファイル:android_build/vendor/nxp-opensource/kernel_imx/arch/arm64/configs/imx8mn_gki.fragment "CONFIG_NXP_NFC_I2C=m" を  imx8mn_gki.fragment に追加します。 4. Androidの対応するボード設定ファイルに設定を追加してください。 - android_build/device/nxp/imx8m/evk_8mn/ に移動してください  BoardConfig.mkを修正します。 # selinux permissive + BOARD_KERNEL_CMDLINE += androidboot.selinux=permissive BOARD_SEPOLICY_DIRS := \ $(CONFIG_REPO_PATH)/imx8m/sepolicy \ $(IMX_DEVICE_PATH)/sepolicy \ + vendor/nxp/nfc/sepolicy \ + vendor/nxp/nfc/sepolicy/nfc + include vendor/nxp/nfc/BoardConfigNfc.mk - ShareBoardConfig.mkに”nxpnfc_i2c.ko”を追加します。パスとファイル名が正しいか確認します。 $(KERNEL_OUT)/drivers/net/phy/realtek.ko \ $(KERNEL_OUT)/drivers/pps/pps_core.ko \ $(KERNEL_OUT)/drivers/ptp/ptp.ko \ $(KERNEL_OUT)/drivers/net/ethernet/freescale/fec.ko + $(KERNEL_OUT)/drivers/nfc/pn7160/nxpnfc_i2c.ko endif $(KERNEL_OUT)/drivers/trusty/trusty-core.ko \ $(KERNEL_OUT)/drivers/trusty/trusty-log.ko \ $(KERNEL_OUT)/drivers/trusty/trusty-ipc.ko \ $(KERNEL_OUT)/drivers/trusty/trusty-virtio.ko \ + $(KERNEL_OUT)/drivers/nfc/pn7160/nxpnfc_i2c.ko else BOARD_VENDOR_RAMDISK_KERNEL_MODULES += \ $(KERNEL_OUT)/drivers/input/touchscreen/goodix_ts.ko \ $(KERNEL_OUT)/drivers/input/touchscreen/synaptics_dsx/synaptics_dsx_i2c.ko Endif - Compatibility_matrix.xmlに以下を追加します netutils-wrapper 1.0 android.hardware.emvco 1 IEmvco default -  device_framework_matrix.xmlに以下を追加します。 nxp.hardware.secureime 1 ISecureIME default nxp.hardware.imx_dek_extractor 1 IDek_Extractor default vendor.nxp.nxpnfc 2 INxpNfc default android.hardware.emvco 1 IEmvco default - evk_8mn.mkに以下を追加します。 # ------nfc------- $(call inherit-product, vendor/nxp/nfc/device-nfc.mk) $(call inherit-product, vendor/nxp/emvco/device-emvco.mk) PRODUCT_PACKAGES += \ android.hardware.nfc-service.nxp PRODUCT_PACKAGES += \ com.nxp.emvco \ com.nxp.nfc \ nfc_nci_nxp_pn72xx - init.rcにnxpnfc_i2cを追加します。 # Grant permission for fetching available_pages info of statsd chown system system /proc/pagetypeinfo chmod 0440 /proc/pagetypeinfo exec u:r:vendor_modprobe:s0 -- /vendor/bin/modprobe -a -d \ /vendor/lib/modules nxpnfc_i2c write /sys/power/wake_lock nosleep on post-fs-data && property:vendor.skip.charger_not_need=0 setprop vold.post_fs_data_done 1 - ueventd.nxp.rc に nxpnfc を追加します。 /sys/devices/virtual/thermal/thermal_zone* trip_point_0_hyst 0660 system system /sys/devices/virtual/thermal/thermal_zone* trip_point_1_hyst 0660 system system /dev/dmabuf_imx 0664 system system /sys/class/backlight/* brightness 0660 system system /dev/ttymxc1 0666 nfc nfc /dev/ttymxc2 0666 nfc nfc /dev/nxpnfc 0666 nfc nfc # for libcamera /dev/media* 0660 system camera /dev/v4l-subdev* 0660 system camera 5. NXP AOSPパッチの適用 NXP公式のNFCパッチはAOSP android-15.0.0_r1のみで、 android-15.0.0_r1と android-15.0.0_r32では大きな違いがあります。このため、パッチを適用する前に、Android-15.0.0_r1からNFCフォルダをコピーして、Android-15.0.0_r32のNFCフォルダを置き換えます。 まず、GitHubからAOSP android-15.0.0_r1をダウンロードしてください。 $ mkdir android-15.0.0_r1 $ cd android-15.0.0_r1 $ repo init -u https://android.googlesource.com/platform/manifest -b android-15.0.0_r1 $ repo sync 次に、以下のフォルダをandroid-15.0.0_r32から削除します。そして、Android-15.0.0_r1から次のNFCフォルダをコピーして、Android-15.0.0_r32の同じフォルダを置き換えます。 パッケージ/apps/Nfc frameworks/base/nfc frameworks/base/nfc-extras システム/NFC 以下にその例をご紹介します。 $ rm -rf android_build/packages/apps/Nfc $ cp -ra android-15.0.0_r1/packages/apps/Nfc android_build/packages/apps/ 私はGitHubからパッチをダウンロードするスクリプトを作成します。お客様は以下のスクリプトを、android_buildと同じディレクトリに配置できます。 AOSP_adaptation.sh # nxp_nci_hal_nfc git clone "https://github.com/nxp-nfc-infra/nxp_nci_hal_nfc.git" cd nxp_nci_hal_nfc git checkout br_ar_15_comm_infra_dev cp -rf * ../android_build/packages/apps/Nfc/ cd .. # nxp_nci_hal_libnfc-nci git clone "https://github.com/nxp-nfc-infra/nxp_nci_hal_libnfc-nci.git" cd nxp_nci_hal_libnfc-nci git checkout br_ar_15_comm_infra_dev cp -rf * ../android_build/system/nfc/ cd .. # nfcandroid_nfc_hidlimpl git clone "https://github.com/nxp-nfc-infra/nfcandroid_nfc_hidlimpl.git" cd nfcandroid_nfc_hidlimpl git checkout br_ar_15_comm_infra_dev cp -rf * ../android_build/hardware/nxp/nfc cd .. # nfcandroid_frameworks git clone "https://github.com/nxp-nfc-infra/nfcandroid_frameworks.git" cd nfcandroid_frameworks git checkout br_ar_15_comm_infra_dev mkdir ../android_build/vendor/nxp/frameworks cp -rf * ../android_build/vendor/nxp/frameworks cd .. # nfcandroid_emvco_aidlimpl git clone "https://github.com/nxp-nfc-infra/nfcandroid_emvco_aidlimpl.git" cd nfcandroid_emvco_aidlimpl git checkout br_ar_15_comm_infra_dev mkdir ../android_build/hardware/nxp/emvco cp -rf * ../android_build/hardware/nxp/emvco cd .. # nfcandroid_platform_reference git clone "https://github.com/nxp-nfc-infra/nfcandroid_platform_reference.git" cd nfcandroid_platform_reference git checkout br_ar_15_comm_infra_dev cp -rf vendor/nxp/* ../android_build/vendor/nxp/ cd .. # nfcandroid_infra_test_apps git clone https://github.com/nxp-nfc-infra/nfcandroid_infra_test_apps.git cd nfcandroid_infra_test_apps/ git checkout br_ar_15_comm_infra_dev cd test_apps/ cp -rf SMCU_Switch/ ../../android_build/packages/apps/ cp -rf EMVCoModeSwitchApp/ ../../android_build/packages/apps/Nfc/ cp -rf load_unload/ ../../android_build/hardware/nxp/nfc/ cp -rf SelfTestAidl/ ../../android_build/hardware/nxp/nfc/ cd ../.. # nfcandroid_infra_comm_libs git clone "https://github.com/nxp-nfc-infra/nfcandroid_infra_comm_libs.git" cd nfcandroid_infra_comm_libs git checkout br_ar_15_comm_infra_dev cp -rf nfc_tda/ ../android_build/system/ cp -rf emvco_tda/ emvco_tda_test/ ../android_build/hardware/nxp/emvco/ cp -rf NfcTdaTestApp/ ../android_build/packages/apps/Nfc/ cd .. Apply_patches.sh cd android_build/build/bazel/ patch -p1 < ../../../nfcandroid_platform_reference/build_cfg/build_pf_patches/AROOT_build_bazel.patch cd ../release patch -p1 < ../../../nfcandroid_platform_reference/build_cfg/build_pf_patches/AROOT_build_release.patch cd ../../external/libchrome patch -p1 < ../../../nfcandroid_platform_reference/build_cfg/build_pf_patches/AROOT_external_libchrome.patch cd ../../frameworks/base patch -p1 < ../../../nfcandroid_platform_reference/build_cfg/build_pf_patches/AROOT_frameworks_base.patch cd ../../system/logging patch -p1 < ../../../nfcandroid_platform_reference/build_cfg/build_pf_patches/AROOT_system_logging.patch このため、 AOSP_adaptation.shを実行し、その後、 Apply_patches.shを実行します。 6. hardware/interfaces/compatibility_matrices に変更を加えます Androidのバージョンごとに互換性マトリックスが異なります。 ファイル: android_build/hardware/interfaces/compatibility_matrices/compatibility_matrix.202404.xml android.hardware.audio.effect 1-2 IFactory default + + nxp.hardware.imx_dek_extractor + 1 + + IDek_Extractor + default + + + + vendor.nxp.nxpnfc + 2 + + INxpNfc + default + + + + vendor.nxp.emvco + 1 + + INxpEmvco + default + + android.hardware.audio.sounddose 1-3 7. デバイス固有の .mk を変更 pn7160の場合、 NXP_NFC_HWはpn7160と等しくなる必要があります。 pn7220の場合、 NXP_NFC_HWはpn7220_i2csと等しくなる必要があります。 File : android_build/vendor/nxp/nfc/device-nfc.mk ##### ##### NXP NFC Device Configuration makefile ###### NXP_NFC_HOST := $(TARGET_PRODUCT) ifndef TARGET_NXP_NFC_HW NXP_NFC_HW := pn7160 else NXP_NFC_HW := $(TARGET_NXP_NFC_HW) endif NXP_NFC_PLATFORM := pn54x NXP_VENDOR_DIR := nxp NXP_I2CM_S := $(TARGET_NXP_I2C_M_S) ファイル: android_build/vendor/nxp/emvco/device-emvco.mk NXP_VENDOR_DIR := nxp NXP_NFC_HW := $(TARGET_NXP_NFC_HW) ifeq ($(strip $(TARGET_NXP_NFC_HW)),) NXP_NFC_HW := pn7160 endif # Nfc service has dependency with EMVCo JAR PRODUCT_PACKAGES += \ com.nxp.emvco 8. これで、Android BSPの構築を始めることができます。 i.MX8MN EVKの場合、  $ source build/envsetup.sh $ lunch evk_8mn-nxp_stable-userdebug $ export TARGET_RELEASE=nxp_stable $ build_build_var_cache $ ./imx-make.sh -j4 2>&1 | tee build-log.txt BSPをビルディングする際には、ビルド中に多くのエラーが発生します。以下にいくつかの誤りと参考解決策を挙げておきます。  エラー リファレンス・ソリューション nfc_aconifg_flagsについて苦情を申し上げます。 packages/apps/Nfc/flags/Android.bp aconfig_declarations { // name: "nfc_aconfig_flags", name: "com.android.nfc.flags-aconfig", package: "com.android.nfc.flags", container: "system", srcs: ["nfc_flags.aconfig"], } java_aconfig_library { // name: "nfc_aconfig_flags_lib", // aconfig_declarations: "nfc_aconfig_flags", name: "com.android.nfc.flags-aconfig-java", aconfig_declarations: "com.android.nfc.flags-aconfig", min_sdk_version: "33", apex_available: [ "//apex_available:platform", "com.android.nfcservices", ], } java_library { name: "nfc_flags_lib", sdk_version: "system_current", min_sdk_version: "33", srcs: [ "lib/**/*.java", ], static_libs: [ "com.android.nfc.flags-aconfig-java", ],  android.hardware.nfc-V2-ndk に関して苦情を伝える ファイル: hardware/interfaces/nfc/aidl/vts/functional/Android.bp android.hardware.nfc-V2-ndk を変更しますandroid.hardware.nfc-V1-ndkへ platform_testing/build/tasks/tests/native_test_list.mk: error: continuous_native_tests:モジュール 'libnfc-nci-jni-tests' のインストールされたファイルが不明です。 'libnfc-nci-jni-tests' を削除します。  native_test_list.mk error: パッケージ/apps/Nfc/tests/instrumentation/Android.bp:6:1:モジュール「NfcNciInstrumentationTests」バリアント「Android_common」は、java_sdk_library「android.test.runner」に直接依存することはできません。「android.test.runner.stubs」に頼ってみて、「android.test.runner.stubs.system」「android.test.runner.stubs.test」または「android.test.runner.impl」その代わり ヒントはエラーメッセージに記載されています。 "android.test.runner" を  "android.test.runner.stubs"、"android.test.runner.stubs.system""android.test.runner.stubs.test"または"android.test.runner.impl"に変更します。 エラー: vendor/nxp/frameworks/nfc/Android.bp:12:1:モジュール "com.nxp.nfc"バリアント"android_common"は、このモジュールから見えない //frameworks/base/nfc:framework-nfc.impl に依存しています。 "//vendor/nxp/frameworks/nfc"を可視性に追加する必要があるかもしれません。 ファイル: frameworks/base/nfc/Android.bp permitted_packages: [ "android.nfc", "com.android.nfc", ], impl_library_visibility: [ "//frameworks/base:__subpackages__", "//cts/hostsidetests/multidevices/nfc:__subpackages__", "//cts/tests/tests/nfc", "//vendor:__subpackages__", "//packages/apps/Nfc:__subpackages__", ], packages/apps/Nfc/nci/src/com/android/nfc/dhimpl/NativeT4tNfceeManager.java:20: エラー:重複クラス:com.android.nfc.dhimpl.nativet4tnfceemanager ファイルを編集してください。 パッケージ/apps/Nfc/nci/src/com/Android/nfc/dhimpl/NativeT4tNfceeManager.java そして重複したクラスをコメントアウトします。 android/R.java:12483:エラー: フィールド FLAG_NFC_ASSOCIATED_ROLE_SERVICES を解決できません     @android.注釈。FlaggedApi(android.nfc.Flags.FLAG_NFC_ASSOCIATED_ROLE_SERVICES) 編集 frameworks/base/nfc/java/android/nfc/flags.aconfig 下のフラグを追加してください。 flag { name: "nfc_associated_role_services" is_exported: true namespace: "nfc" description: "Share wallet role routing priority with associated services" bug: "366243361" } 失敗: platform_testing/build/tasks/tests/native_test_list.mk: エラー: continuous_native_tests: モジュール 'libnfc-nci-tests'のインストールされたファイルが不明です。  native_test_list.mkのlibnfc-nci-testを削除します。 prebuilts/clang/host/linux-x86/clang-r536225/include/c++/v1/string:780:43: error: implicit instantiation of undefined template 'std::char_traits '   780 |   static_assert((is_same<_CharT, typename traits_type::char_type>::value)、       |                                           ^ packages/apps/Nfc/nci/jni/NativeNfcTda.cpp:32:35: note: ここで要求されるテンプレートクラス「std::basic_string 」のインスタンス化    32 | 静的 std::basic_string sRxTdaDataBuff;       |                                   ^ パッケージ/アプリ/Nfc/nci/jni/NativeNfcTda.cppを編集してください using android::base::StringPrintf; extern bool nfc_debug_enabled; SyncEvent sCtLibSyncEvt; //static std::basic_string sRxTdaDataBuff; static std::basic_string sRxTdaDataBuff; packages/apps/Nfc/nci/jni/NativeT4tNfcee.cpp:493:21: エラー: 'append'への呼び出しに一致するメンバー関数がありません。  493 |      sRxDataBuffer.append(data.p_data,data.len);       |       ~~~~~~~~~~~~~~^~~~~~ パッケージ/アプリ/Nfc/nci/jni/NativeT4tNfcee.cppを編集してください void NativeT4tNfcee::t4tReadComplete(tNFA_STATUS status, tNFA_RX_DATA data) { mT4tOpStatus = status; if (status == NFA_STATUS_OK) { if (data.len > 0) { sRxDataBuffer.insert(sRxDataBuffer.end(), data.p_data, data.p_data + data.len); LOG(DEBUG) << StringPrintf("%s: Read Data len new: %d ", __func__, data.len); } } SyncEventGuard g(mT4tNfcEeRWCEvent); mT4tNfcEeRWCEvent.notifyOne(); } frameworks/base/core/java/android/provider/Settings.java:2351: エラー: フィールド FLAG_NFC_ACTION_MANAGE_SERVICES_SETTINGS を解決できませんでした @FlaggedApi(android.nfc.Flags.FLAG_NFC_ACTION_MANAGE_SERVICES_SETTINGS) ファイル: frameworks/base/nfc/java/android/nfc/flags.aconfig flags.aconfig に以下を追加します flag { name: "nfc_action_manage_services_settings" is_exported: true namespace: "nfc" description: "Add Settings.ACTION_MANAGE_OTHER_NFC_SERVICES_SETTINGS" bug: "358129872" } エラーメッセージには、エラーを修正するためのヒントがいくつか含まれているため、表に記載されていないエラーもあります。お客様はヒントに従い、ニーズに応じてソースコードを変更することができます。 時々、お客様はr1とr32のソースコードを比較できます。こちらは AOSP ソースコード android-15.0.0_r32 と android-15.0.0_r1です。 9. 画像をi.MX8MN EVKボードにダウンロードします - 8MN EVKボード上でダウンロードモードに切り替えます evk_switch.png - まず、Android BSP WebページからAndroid 15 BSP i.MX8MN EVKデモイメージをダウンロードします。UUUスクリプトと必要なイメージファイルはすでにデモイメージパッケージに入っているためです。  - ここから UUU をダウンロードします: リリース · nxp-imx/mfgtools - UUU実行ファイルをデモイメージフォルダに配置します。 uuu_imx_android_flash.batが同じフォルダに配置されているスクリプトです。 - ビルドに成功した後、画像をデモイメージのフォルダにコピーします。画像は、android_build/out/target/product/evk_8mn/ に位置しています - UUUスクリプトを実行して、画像をEVKボードにダウンロードします。 uuu.jpg nxp.png 参考情報: Yocto Linux + PN7160を実行しているi.MX6ULL EVK i.MX8M NanoボードでPN7160をAndroid 14に移植 i.MXアプリケーション・プロセッサ用Android OS | NXP Semiconductors PN7160/PN7220 – Android 15 移植ガイド プラグ・アンド・プレイNFCフロントエンド、統合ファームウェア搭載 | NXP Semiconductors
View full article
Flash layout for new boot flow with TF-A Please note that the LSDK memory layout for TF-A boot flow explained in this topic is only applicable for LSDK 18.12 and newer releases.  The following table shows the memory layout of various firmware stored in NOR/NAND/QSPI flash device or SD card on all QorIQ Reference Design Boards. When the board boots from NOR flash, the NOR bank from which the board boots is considered as the "current bank" and the other bank is considered as the "alternate bank". For example, if LS1043ARDB boots from NOR bank 4, to update an image on NOR bank 0, you need to use the "alternate bank" address range,0x64000000 - 0x64F00000. Firmware Definition MaxSize Flash Offset (QSPI/NAND flash) Absolute address (NOR bank 0 on LS1043ARDB, LS1021ATWR) Absolute address  (NOR bank 4 LS1043ARDB, LS1021ATWR) Absolute address (NOR bank 0 on LS2088ARDB) Absolute address (NOR bank 4 on LS2088ARDB) SD Start Block No. RCW + PBI + BL2 (bl2.pbl) 1 MiB 0x00000000 0x60000000 0x64000000 0x580000000 0x584000000 0x00008 ATF FIP Image (fip.bin) BL31 + BL32 + BL33 4 MiB 0x00100000 0x60100000 0x64100000 0x580100000 0x584100000 0x00800 Boot firmware environment 1 MiB 0x00500000 0x60500000 0x64500000 0x580500000 0x584500000 0x02800 Secure boot headers 2 MiB 0x00600000 0x60600000 0x64600000 0x580600000 0x584600000 0x03000 Secure header or DDR PHY FW 512 KiB 0x00800000 0x60800000 0x64800000 0x580800000 0x584800000 0x04000 Fuse provisioning header 512 KiB 0x00880000 0x60880000 0x64880000 0x580880000 0x584880000 0x04400 DPAA1 FMAN ucode 256 KiB 0x00900000 0x60900000 0x64900000 0x580900000 0x584900000 0x04800 QE/uQE firmware 256 KiB 0x00940000 0x60940000 0x64940000 0x580940000 0x584940000 0x04A00 Ethernet PHY firmware 256 KiB 0x00980000 0x60980000 0x64980000 0x580980000 0x584980000 0x04C00 Script for flashing image 256 KiB 0x009C0000 0x609C0000 0x649C0000 0x5809C0000 0x5849C0000 0x04E00 DPAA2-MC or PFE firmware 3 MiB 0x00A00000 0x60A00000 0x64A00000 0x580A00000 0x584A00000 0x05000 DPAA2 DPL 1 MiB 0x00D00000 0x60D00000 0x64D00000 0x580D00000 0x584D00000 0x06800 DPAA2 DPC 1 MiB 0x00E00000 0x60E00000 0x64E00000 0x580E00000 0x584E00000 0x07000 Device tree(needed by uefi) 1 MiB 0x00F00000 0x60F00000 0x64F00000 0x580F00000 0x584F00000 0x07800 Kernel lsdk_linux.itb 16 MiB 0x01000000 NA NA NA NA 0x08000 Ramdisk rfs 32 MiB 0x02000000 NA NA NA NA 0x10000 The following figures highlight the changes in the flash layout for previous boot flow (with PPA) and flash layout for TF-A boot flow. Flash layout for previous boot flow (with PPA) Changed flash layout for TF-A boot flow QorIQ LS1 Devices QorIQ LS2 Devices
View full article
Zephyr培训资源 以下是一些资源,帮助您更好地了解Zephyr: 本篇 恩智浦 Zephyr 入门教程将通过 MCUXpresso for VS Code 和 MCUXpresso Installer 向您介绍所有 Zephyr 环境设置步骤,帮助您构建并运行第一个 Zephyr 应用程序。 本分步实验室指南(来自恩智浦技术日培训)从 " Hello,World " 开始,然后引导您完成有关 Kconfig、设备树和调试方法的有用教程: 实践研讨会:在 Visual Studio Code 中使用 Zephyr™ 操作系统进行开发 本教程展示了 Zephyr 强大的便携性。演示了将 FRDM-MCXN947 的 LVGL 演示移植到 FRDM-RW612 的简单步骤: 恩智浦 Zephyr 显示器便携性演示 想了解更多?访问我们 Zephyr 登录页面的 “培训” 部分,查找恩智浦在线研讨会和在线培训 ——只需点击页面顶部的 “培训” 选项卡即可 返回 Zephyr 知识中心
View full article
KW38 - 使用 OTAP 客户端软件对 KW38 设备进行重新编程 简介 空中编程(OTAP)是NXP提供的一项基于蓝牙低功耗(Bluetooth LE)的定制服务,提供升级微控制器中运行的软件的解决方案。本文件指导用户通过空中编程(OTAP)Bluetooth LE服务,将新的软件镜像加载到KW38设备中。。 软件要求 MCUXpresso IDE 或 IAR Embedded Workbench IDE。 FRDM-KW38 SDK。 IoT Toolbox 应用程序,适用于 Android 和 iOS 系统。你也可以从以下帖子下载 IoT Toolbox 应用程序的 APK 文件:Android 版 IoT Toolbox 硬件要求 FRDM-KW38板。 带有 IoT Toolbox 应用程序的智能手机。 OTAP 客户端软件在更新过程中使用的 KW38 闪存 默认情况下,512KB KW38 闪存被分区为: 一个 256KB 的程序闪存阵列 (P-Flash),分为 2KB 的扇区,闪存地址范围从 0x0000_0000 到 0x0003_FFFF。 一个256KB的FlexNVM数组,分为2KB的扇区,地址范围从0x1000_0000到0x1003_FFFF。 别名内存 (Alias memory),地址范围从 0x0004_0000 到 0x0007_FFFF。对别名内存的写入或读取操作分别会修改或返回 FlexNVM 的内容。换句话说,别名内存是使用不同地址来访问 FlexNVM 内存的另一种方式。 Untitled.png 以下几点将简化说明 OTAP 服务的工作原理:   OTAP 应用程序由两个独立的部分组成,即 OTAP 引导加载程序和 OTAP 客户端。OTAP 引导加载程序会验证 OTAP 客户端中是否有可用的新镜像,以对设备进行重新编程。另一方面,OTAP 客户端软件提供了所需的蓝牙低功耗自定义服务,使 OTAP 客户端设备(待重新编程的设备)能够与 OTAP 服务器设备(包含用于重新编程 OTAP 客户端设备的镜像的设备)进行通信。因此,首次准备软件时,需要对 OTAP 客户端设备进行两次编程,首先是 OTAP 引导加载程序,然后是 OTAP 客户端软件。使两个不同的软件能够在同一设备中共存的机制是将它们分别存储在不同的内存区域。这是通过在链接器文件中为每个软件指定不同的内存区域来实现的。对于 KW38 设备,OTAP 引导加载程序预留了一个从 0x0000_0000 到 0x0000_1FFF 的 8KB 存储空间,因此,内存的其余部分除其他用途外,由 OTAP 客户端软件预留。   Untitled.png   为 OTAP 客户端设备生成新的镜像文件时,我们需要在链接器文件中指定代码将以 8KB 的偏移量进行放置(就像 OTAP 客户端软件所做的那样),因为必须保留这些地址范围以避免覆盖 OTAP 引导加载程序。新应用程序还应在相应的地址包含引导加载程序标志,以确保其正常工作(稍后我们将回到这一点)。   Untitled.png   当 OTAP 客户端设备和 OTAP 服务器设备连接且正在进行下载时,OTAP 服务器设备通过蓝牙低功耗将镜像数据包(称为块)发送到 OTAP 客户端设备。OTAP 客户端设备可以将这些块存储在外部 SPI 闪存(FRDM-KW38 开发板上已预装)或片上 FlexNVM 区域中。这些块的存储目的地可在 OTAP 客户端软件中选择(本文将提供修改存储目的地的说明)。   Untitled.png   当镜像传输完成且所有块都已从 OTAP 服务器设备发送到 OTAP 客户端设备后,OTAP 客户端软件会将诸如软件更新源(外部闪存或 FlexNVM)之类的信息写入称为引导加载程序标志的内存部分。然后,OTAP 客户端对微控制器(MCU)执行软件复位,以执行 OTAP 引导加载程序代码。接着,OTAP 引导加载程序代码读取引导加载程序标志,以获取使用新应用程序对设备进行重新编程所需的信息。请参见以下流程图,该图解释了这两个应用程序的流程。   Untitled.png 由于新应用程序是按 8KB 的偏移量构建的,因此 OTAP 引导加载程序从 0x0000_2000 地址开始对设备进行编程,因此,OTAP 客户端应用程序会被新镜像覆盖。然后,OTAP 引导加载程序转移应用程序的流程,开始执行新代码。   Untitled.png   实际上,如第 3 点所述,当启用 FlexNVM 存储时,OTAP 客户端软件和软件更新之间的边界并非恰好位于 P-Flash 和 FlexNVM 内存区域的边界上,此外,这些值可能会根据你的链接器设置而变化。要了解边界的位置,你应该检查项目中的实际内存地址。       在 IAR Embedded Workbench IDE 中配置和编程 OTAP 客户端软件 如最后一节所述,要完成 OTAP 实现所需的软件,需要在 FRDM-KW38 开发板上编程两个软件,即 OTAP 引导加载程序和 OTAP 客户端。本节将指导你使用 IAR Embedded Workbench IDE 进行编程,并配置设置以在外部存储和内部存储之间进行选择。 1- 第一步是在 KW38 中编程 OTAP 引导加载程序。解压 SDK,然后在以下路径中找到 OTAP 引导加载程序软件: \boards\frdmkw38\wireless_examples\framework\bootloader_otap\bm\iar\bootloader_otap.eww 2- 点击 “Download and Debug” 图标 (Ctrl + D),在开发板上编程 OTAP 引导加载程序项目。 Untitled.pngKW38 编程完成并开始调试会话后,中止会话 (Ctrl + Caps Lock + D) Untitled.png,以安全地停止 MCU。 3- 此时,您已将OTAP引导程序编程到您的KW38中。接下来是编程和配置 OTAP 客户端软件。请在以下路径找到 OTAP 客户端软件: FreeRTOS项目版本: \boards\frdmkw38\wireless_examples\bluetooth\otac_att\freertos\iar\otap_client_att_freertos.eww 裸机 (Baremetal) 项目版本: \boards\frdmkw38\wireless_examples\bluetooth\otac_att\bm\iar\otap_client_att_bm.eww 4- 然后,配置 OTAP 客户端以选择外部存储或内部存储。 要选择外部存储,请按照以下步骤操作(这是 SDK 项目中的默认配置): 4.1- 在工作区的源文件夹中找到 “app_preinclude.h” 头文件。搜索 “gEepromType_d” 定义,并将其值设置为 “gEepromDevice_AT45DB041E_c”。 /* Specifies the type of EEPROM available on the target board */ #define gEepromType_d gEepromDevice_AT45DB041E_c 4.2- 打开项目选项窗口 (Alt + F7)。在 “Linker->Config” 窗口中,设置 “gUseInternalStorageLink_d=0”。 Untitled.png   要选择内部存储,请按照以下步骤操作: 4.1 - 在工作区的源文件夹中找到 “app_preinclude.h” 头文件。搜索 “gEepromType_d” 定义,并将其值设置为 “gEepromDevice_InternalFlash_c”。 /* Specifies the type of EEPROM available on the target board */ #define gEepromType_d gEepromDevice_InternalFlash_c 4.2- 打开项目选项窗口 (Alt + F7)。在 “Linker->Config” 窗口中,设置 “gUseInternalStorageLink_d=1”。 Untitled.png   5- 配置好存储设置后,保存项目中的更改。然后点击 “Download and Debug” 图标(Ctrl + D) Untitled.png,在开发板上编程软件。KW38 编程完成并开始调试会话后,中止会话 (Ctrl + Caps Lock + D) Untitled.png,以安全地停止 MCU。 在 IAR Embedded Workbench IDE 中创建用于更新 OTAP 客户端软件的 SREC 镜像 本节将展示如何以无线示例为起点,创建与 OTAP 兼容的镜像,以使用 IAR Embedded Workbench IDE 对 KW38 OTAP 客户端进行重新编程。 1- 从 SDK 包的 Bluetooth 文件夹中选择任意示例,使用 IAR IDE 打开。Bluetooth 示例位于以下路径: \boards\frdmkw38\wireless_examples\bluetooth  在本示例中,我们将使用葡萄糖传感器项目: \boards\frdmkw38\wireless_examples\bluetooth\glucose_s\freertos\iar\glucose_sensor_freertos.eww 2- 打开 IAR 中的项目选项窗口 (Alt + F7)。在 “Linker->Config” 窗口中,编辑选项以包含 “gUseBootloaderLink_d=1” 标志,并更新 “gEraseNVMLink_d=0” 标志。当 gUseBootloaderLink_d 标志为 true 时,它向链接器文件指示镜像必须在第一个闪存扇区之后寻址,以避免覆盖 OTAP 引导加载程序软件(如我们之前所述)。另一方面,gEraseNVMLink_d 符号用于用 0xFF 模式填充未使用的 NVM 闪存区域。禁用此标志后,我们的软件镜像将不包含此模式,因此,镜像的总大小会减小,并提高 OTAP 下载速度和内存使用率。 Untitled.png 3- 进入 “Output Converter” 窗口。取消选中 “Override default” 复选框,然后展开 “Output format” 下拉框,选择 “Motorola S-records” 格式。点击 “OK” 按钮完成设置。 Untitled.png 4- 构建项目。 5- 在以下路径中找到 S-Record 文件 (.srec),并将其保存到智能手机上的已知位置。 \boards\frdmkw38\wireless_examples\bluetooth\glucose_s\freertos\iar\debug\glucose_sensor_freertos.srec 在 MCUXpresso IDE 中配置和编程 OTAP 客户端软件 如前文所述,为了完成OTAP实现,您需要在FRDM-KW38上编写两个软件:OTAP引导加载程序和OTAP客户端。本节将指导您使用MCUXpresso IDE对设置进行编程和配置,以选择外部存储或内部存储。 1- 打开 MCUXpresso IDE。在"快速入门面板"中点击"导入SDK示例"。 Untitled.png 2- 选择 FRDM-KW38 图标,然后点击 “Next>”。 Untitled.png 3- 导入 OTAP 引导加载程序项目。它位于 “wireless_examples -> framework -> bootloader_otap -> bm -> bootloader_otap”。点击 “Finish” 按钮。 Untitled.png 4- 点击 “Debug” 图标 Untitled.png,在开发板上编程 OTAP 引导加载程序项目。KW38 编程完成并开始调试会话后,中止会话 Untitled.png (Ctrl + F2),以安全地停止 MCU。 5- 重复步骤 1 到 3,在 MCUXpresso IDE 中导入 OTAP 客户端软件。对于 FreeRTOS 版本,它位于 “wireless_examples -> bluetooth -> otac_att -> freertos -> otap_client_att_freertos”;如果你更喜欢裸机版本,则位于 “wireless_examples -> bluetooth -> otac_att -> bm -> otap_client_bm_freertos”。。 6- 然后,配置 OTAP 客户端以选择外部存储或内部存储。 要选择外部存储,请按照以下步骤操作(这是 SDK 项目中的默认配置): 6.1- 在工作区的源文件夹下找到 “app_preinclude.h” 文件。搜索 “gEepromType_d” 定义,并将其值设置为 “gEepromDevice_AT45DB041E_c”。 /* Specifies the type of EEPROM available on the target board */ #define gEepromType_d gEepromDevice_AT45DB041E_c 6.2- 导航至 “Project -> Properties -> C/C++ Build -> MCU settings -> Memory details”。按照下图所示编辑 Flash 字段,保持 RAM 不变。 Untitled.png 要选择内部存储,请按照以下步骤操作: 6.1- 在工作区的源文件夹下找到 “app_preinclude.h” 文件。搜索 “gEepromType_d” 定义,并将其值设置为 “gEepromDevice_InternalFlash_c”。 /* Specifies the type of EEPROM available on the target board */ #define gEepromType_d gEepromDevice_InternalFlash_c 6.2- 导航至 “Project -> Properties -> C/C++ Build -> MCU settings -> Memory details”。按照下图所示编辑 Flash 字段,保持 RAM 不变。 Untitled.png 7- 配置好存储设置后,保存项目中的更改。然后点击 “Debug” 图标 Untitled.png,在开发板上编程软件。KW38 编程完成并开始调试会话后,中止会话 Untitled.png (Ctrl + F2),以安全地停止 MCU。 在 MCUXpresso IDE 中创建 SREC 镜像以更新 OTAP 客户端中的软件 本节将展示如何以无线示例为起点,创建与 OTAP 兼容的镜像,以使用 MCUXpresso IDE 对 KW38 OTAP 客户端进行重新编程。 1- 如前所述,从 SDK 包的 Bluetooth 文件夹中导入任意示例。在 SDK 导入向导中,Bluetooth 示例位于 “wireless_examples -> bluetooth” 文件夹中。本示例将使用 “wireless_examples -> bluetooth -> glucose_s -> freertos -> glucose_sensor_freertos” 中的葡萄糖传感器项目。见下图。 Untitled.png 2- 导航至 “Project -> Properties -> C/C++ Build -> MCU settings -> Memory details”。按照下图所示编辑 Flash 字段,保持 RAM 不变。最后几个字段向链接器文件指示镜像必须在第一个闪存扇区之后寻址,以避免覆盖 OTAP 引导加载程序软件,如我们在本文简介中所述。 Untitled.png 3- 解压 KW38 SDK 包。将 “main_text_section.ldt” 链接脚本从以下路径拖放到工作区的 “linkscripts” 文件夹中。结果应与下图类似。 \middleware\wireless\framework\Common\devices\MKW38A4\mcux\linkscript_bootloader\main_text_section.ldt Untitled.png 4- 在 MCUXpresso IDE 中打开位于 linkscripts 文件夹中的 “end_text.ldt” 链接脚本文件。找到下图所示的部分,并删除 “FILL” 和 “BYTE” 语句。BYTE 和 FILL 行用于用 0xFF 模式填充未使用的 NVM 闪存区域。删除此代码后,我们的软件镜像将不包含此模式,因此,镜像的总大小会减小,并提高 OTAP 下载速度和内存使用率。 Untitled.png 5- 打开 “app_preinclude.h” 文件,将 “gEepromType_d” 定义为内部存储。这是一个必要的虚拟定义,用于将引导加载程序标志放置在正确的地址,因此,这不会影响你之前在 MCU 中编程 OTAP 客户端和 OTAP 引导加载程序软件时选择的存储方法。 /* Specifies the type of EEPROM available on the target board */ #define gEepromType_d gEepromDevice_InternalFlash_c 6- 在项目的 “framework” 文件夹中包含 “OtaSupport” 文件夹及其文件。同时在项目的 “framework -> Flash” 文件夹中包含 “External” 文件夹及其文件。“OtaSupport” 和 “External” 文件夹可在 SDK 中找到。你可以轻松地从 SDK 下载路径中拖动这些文件夹并将其放入 MCUXpresso 的工作区中。“OtaSupport” 和 “External” 文件夹位于: OtaSupport middleware\wireless\framework\OtaSupport External 中间件\无线\框架\Flash\External 结果应如以下图所示:  Untitled.png 7- 依次进入 “Project -> Properties -> C/C++ Build -> Settings -> Tool Settings -> MCU C Compiler -> Includes”。点击 “Include paths” 旁边的图标(见下图)。会弹出一个新窗口,然后点击 “Workspace” 按钮。 Untitled.png 8- 在 “Folder selection” 窗口中展开项目目录,然后选择 “framework -> Flash -> External -> interface”(框架 -> 闪存 -> 外部 -> 接口)和 “framework -> OtaSupport -> interface” 文件夹。点击 “OK”按钮保存更改。 Untitled.png 9- 确保 “OtaSupport” 和 “External” 文件夹已导入 “Include paths” 窗口中。然后点击 “Apply and Close” 按钮保存更改。 Untitled.png 10- 点击此图标 Untitled.png保存并构建项目。然后,展开项目中的 “Binaries” 图标。右键点击 “.axf” 文件,选择 “Binary Utilities -> Create S-Record” 选项。生成的 S 记录文件将以 “.s19” 为扩展名保存在工作区的 Debug 文件夹中。将该 S 记录文件保存到智能手机上的已知位置。 Untitled.png 使用 IoT Toolbox 应用程序测试 OTAP 客户端 本节介绍如何使用 IoT Toolbox 应用测试 OTAP 客户端软件。 1- 在你的智能手机上打开 IoT Toolbox 应用。选择 OTAP,然后点击 “SCAN” 以开始扫描合适的 OTAP 客户端设备。 Untitled.png  2- 按下 FRDM-KW38 开发板上的 ADV 按钮 (SW2) 以开始广播。 3- 当你的智能手机找到 FRDM-KW38 开发板后,该设备将显示为 “NXP_OTAA”。将你的智能手机与此设备连接。随后,智能手机上会显示一个新窗口。 Untitled.png  4- 点击 “Open” 按钮,查找 SREC 软件更新文件。 5- 点击 “Upload” 开始传输。等待下载完成。更新成功后,会显示确认消息。 Untitled.png  6- 等待几秒钟,直到软件更新被编程到你的 MCU 中。新代码将自动开始运行。 如果对本主题有任何问题,请告知我。 BLE软件 千瓦 回复:KW38 - 使用 OTAP 客户端软件对 KW38 设备进行重新编程 嗨,EdgarLomeli   很多人无法使用 Google 应用商店,你能提供 IoT Toolbox 的最新 apk 安装包吗?  非常感谢。
View full article
Unable to debug i.MXRT1064 custom board. Hi,       I'm getting "Break at address "0x20d102" with no debug information available" message while trying to run my code in debug mode.       I'm using i.MXRT1064 custom board and programming it using, LinkServer LPC-Link2.       This board was working earlier without issue but now all of a sudden, this message appears.        I'm tried Release mode. I can successfully flash my board with the release code but then it seems the program doesn't run. I don't see any output, either from serial terminal or from display.       I also tried programming this board using Secure Provisioning Tool but it still doesn't work.         Can anyone help on where to focus or any leads for this issue? Re: Unable to debug i.MXRT1064 custom board. Hi MayLiu,        Thanks for your response.         Earlier, I did try that setting as suggested by you, but the IDE prompted an error (Failed to execute MI command: -target-download) when try to debug. I have attached a snapshot of that error for your reference.         Going back to the previous message, I wish to add that when I checked the address of where the current program is executing, it was showing that the code is in ROM region (address 0x20E35A). So somehow the code is unable to reach/start application code and is struck in ROM. Is my assumption correct? Can there be such a scenario? Re: Unable to debug i.MXRT1064 custom board. Hi @nxpsachve , Thank you so much for your interest in our products and for using our community. 1: Please try select Link application to RAM, then debug again. mayliu1_1-1768964548758.png If your application can run successfully from RAM, please set the board as Serial Downloader mode, and then use the Secure Provisioning Tool to program your board by UART1 or USB1.   If your application  fails to run, I suggest you using an oscilloscope to check your board the power‑on sequence.   Wish it helps you. Best Regards MayLiu Re: Unable to debug i.MXRT1064 custom board. Hi @nxpsachve , I do not think MCUXpresso IDE  change BOOT configuration,  Boot behavior on NXP RT is determined by hardware boot config and boot mode pins.  Since the target can be detected in Serial Downloader mode, this indicates that the ROM is still running correctly. As a next step, you could: Perform a full chip erase, Switch the board to Internal Boot mode, and Try reconnecting with MCUXpresso IDE for debugging. Alternatively, you may also use the MCUXpresso Secure Provisioning Tool to program the application image. Best Regards MayLiu Re: Unable to debug i.MXRT1064 custom board. Hi MayLiu, Thanks for your suggestion. I would like to check if there are any such setting/configuration within MCUXpresso that can alter or impact the BOOT Conf? Just to rule out the IDE. The link server is able to detect the target when in serial download mode. Re: Unable to debug i.MXRT1064 custom board. Hi @nxpsachve , Thanks for your updated information. Based on the information you provided, it is possible that the CPU is currently executing code from the Boot ROM rather than your application code.   I would suggest checking the BOOT CFG and BOOT mode pin settings, ensuring that the device is configured to boot from user flash.   You may also try to set your board as serial downloader mode and then connecting via J-Link to confirm whether the debugger can  detect and communicate with the target.   Best Regards MatLiu
View full article
KSDKの例のリスト <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 現在のKSDK 1.3の例は、C:\Freescale\KSDK_1.3.0\examplesにあります。 C:\Freescale\KSDK_1.3.0\middleware の下にあるミドルウェア (tcpip、ファイルシステム) の例   他にも作成された例があります。   KSDK 1.3 (英語) KSDK 1.3 で FTM PWM を使用したレインボーカラー KDS3.0 + KSDK1.3でprintf()を使用して文字列をUARTに出力する方法 KSDKドライバーを使用した16x2 LCDの駆動 NFCコントローラーライブラリとKSDKの統合 KL43ZによるsLCDおよびKDS3.0 + KSDK1.3.0 +プロセッサエキスパートによるタッチセンスのサポート   KSDK 1.2 (英語) DMAを使用したKSDKによるADCフレキシブルスキャンモードのエミュレーション 初めてのKSDK1.2を書くKDS3.0 でのアプリケーション - Hello World と GPIO 割り込み付きトグル LED KSDKによるDCモータの速度制御とサーボモータの位置制御 [FTM + GPIO] KSDK搭載ラインスキャンカメラ [ADC + PIT + GPIO] フリースケール・カップ・スマート・レースのトラックの中心を検出する簡単な方法 Kinetis Design StudioのKSDKを使用したFatFs + SDHCデータロガー KSDKのセグメントLCDの例 KSDK GPIOドライバーとProcessor Expertの DAC Sinus Demo(PEx + KSDK 1.2 + KDS 3.0を使用) KSDKデモコードに基づいてカスタマイズされたKSDKプロジェクトを開始する方法   KSDK 1.1 (英語) SDKとCMSISを使用したKV31へのFIR機能実装のサンプルプロジェクト KDS 2.0 と KSDK 1.1.0 で LED を切り替える方法およびプロセッサエキスパート KSDK SPIマスタースレーブ(FRDM-K64F付き) Kinetisソフトウェア開発キット(KSDK)による超音波トランスデューサによる距離測定の設定(英語) Kinetis SDK 1.1.0用のUSB HID双方向汎用デバイスのデモ・プロジェクト 赤外線 (IR) センサで距離を測定するためのKinetisソフトウェア開発キット (SDK) の構成 KDSで初めてのKSDKアプリケーションの作成-Hello WorldとGPIO割り込み   KSDK 1.0 (英語) FRMD-K64F + KDS 1.1.0を使用した最初のトグルLEDアプリケーションの作成+ KSDK 1.0.0非プロセッサエキスパート SDKを使用した低消費電力アプリケーション KSDK I2C EEPROM の例 全般 Re:KSDKの例のリスト <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> これらの例はKSDK 2.0用に更新されますか - これらの例は廃止されたKSDKバージョン用です。 また、Processor Expertは明らかに時代遅れで、これ以上開発されることはないのでしょうか? 感謝 よろしくお願いします、デイブ
View full article
Example S32K144 FlexCAN Pretended Networking STOP mode test S32DS.ARM.2.2 ********************************************************************************  Detailed Description:  Example shows how to use FlexCAN 0 Pretended networking mode to allow FlexCAN  module to wake up MCU from STOP mode.  Wake up by Timeout and wake up by Match events are enabled.  Also pin interrupt can be used to exit STOP mode.  So MCU enters STOP mode by pressing SW3 button.  MCU exits STOP mode when one of following happens:  - no CAN message comes in 8sec (CAN PN timeout event)  - message with standard ID 0x554 or 0x555 comes (CAN PN match event)  - SW2 button is pressed (PTC12 interrupt)  In run mode blue LED is dimming and the rate is different for each wakeup event  ------------------------------------------------------------------------------  Test HW: S32K144 EVB-Q100  MCU: FS32K144UAVLL 0N57U  Fsys: 160MHz  Debugger: Lauterbach, OpenSDA  Target: internal_FLASH ******************************************************************************** General
View full article
CAN FDとCAN(動作していません) NXPコミュニティの皆様、こんにちは。 現在、CAN 構成に関する問題が発生しています。CAN 通信には基本設定を使用していますが、 PEAK CAN ViewerでCAN-FD モードを使用する場合にのみ機能します。ただし、標準のClassical CAN (非 FD) を試しても、応答がありません。 参考までに私のプロジェクトを添付しました。どなたか親切にレビューして、不足している構成や設定が見落とされているかどうか教えていただけませんか? 要約すると: CAN-FD + PEAK CAN Viewer :期待通りに動作 標準CAN + PEAK CANビューア:ボードからの応答なし ご提案やご指導をいただければ幸いです。 お手数ですが、よろしくお願いいたします。 よろしくお願いします、 ガネーシュ・バグワット Re: CAN FD and CAN(not Working) こんにちは、ジュリアン ご返信ありがとうございます。 最初はソフトウェアの構成の問題を疑ったので、ここに投稿しました。しかし、それは TJA1443 トランシーバ接続に関するハードウェア関連の問題であることが判明しました。フローティング ピンのため、通常の CAN では CAN メッセージを受信または送信できませんでしたが、FD ではなぜ動作していたのかはわかりません。 ハードウェアの問題を解決した後、すべてが期待どおりに動作するようになりました。 ご返信いただき、また、役に立つコミュニティ投稿を紹介していただき、改めて感謝申し上げます。 よろしくお願いします、 ガネーシャ Re: CAN FD and CAN(not Working) こんにちは@GaneshBhagwat PCAN-View ツールは、モード、ボーレート、サンプリング ポイントに対して正しく構成されていますか? バス上で表示されている内容を共有することは可能ですか?(ロジックアナライザまたはオシロスコープを使用して)フレームが正しく送信されているかどうかを確認するだけです。また、「機能していない」とはどういう意味か詳しく説明してください。受付時にコールバックを入力できますか?問題があるのはトランスミッションだけですか? CANInit 関数で、ID 0x80000 が受け入れ用に設定されていることがわかります。これが CAN アナライザーでも設定されているかどうかを確認してください。 このコミュニティ投稿を CAN 構成のガイダンスとして使用できます:例: S32K358 FlexCAN TXRX ISR S32DS35 RTD400/500 - NXPコミュニティ。 よろしくお願いします、 ジュリアン
View full article
AR1335 相机传感器驱动程序 @kerryzhou 我想知道您是否使用过这种摄像头传感器:AR1335 与任何恩智浦 MCU 配合使用。如果是,请与我分享驱动程序源代码。 此致, 法里德 Re: AR1335 camera sensor driver 你好,法比奥, ,我正在使用 yocto。 您可以在此处找到最新的 ar1335 传感器内核驱动程序: https://github.com/nxp-imx/isp-vvcam/tree/lf-5.15.y_2.0.0/vvcam/v4l2/sensor/ar1335 如果使用 Yocto,除了上述isp-vvcam之外,还需要 isp-imx: 如果对源代码感兴趣,可以在 Ubuntu 主机上下载并执行 bin 文件获取: https://www.nxp.com/lgfiles/NMG/MAD/YOCTO/isp-imx-4.2.2.20.0.bin 用你在电路板支持包中使用的版本替换版本(这里我们使用 v20) 以下是如何为另一个传感器部署驱动程序的示例:https://www.nxp.com/docs/en/application-note/AN13712.pdf Re: AR1335 camera sensor driver 你好,谢谢。我是新手,所以我的问题可能很愚蠢。 您使用的是 Debian 还是 Yocto?能否提供股票驱动程序的链接? Re: AR1335 camera sensor driver 你好,法比奥, 是的,我可以使用原版驱动程序。 到目前为止,我使用的是高清 1080p 分辨率。 计划过几天还将尝试 4K 及以上的分辨率。 Re: AR1335 camera sensor driver 您好。 我想知道你们是否成功地将 AR1335 摄像机与 Mx8 plus 相连接。 请 法比奥 Re: AR1335 camera sensor driver 嗨,迈克尔、 >>我已经使用恩智浦 iMX8M Mini SoC 运行了这个传感器 我对此非常感兴趣。你有可能提供源代码和设备树文件吗? 我正试图让iMX8M-plus 也能这样做,因为它与 iMX8M-plus 非常相似。 谢谢 MC Re: AR1335 camera sensor driver 嗨,迈克-帕特黑、 已经请我们的内部专家进行了仔细检查,并在您的新帖中给您回复。 如有任何新问题,请关注该新帖。 顺祝商祺! kerry Re: AR1335 camera sensor driver 谢谢你,凯瑞!我开设了一个新主题来讨论这个问题: https://community.nxp.com/t5/i-MX-RT/RT1170-Using-MIPI-CSI-with-grayscale-or-raw-image-sensors/m-p/1270310#M14031 Re: AR1335 camera sensor driver 嗨,迈克-帕特黑、 从 AE 的内部描述来看,是芯片 MIPI CSI 无法支持,而不是 SDK 的问题。 因此,参考手册将来会添加相关描述。 但如果要使用原始数据,则需要使用并行 CSI 接口,而不是 mipi-csi。 很抱歉给您带来不便。 顺祝商祺! kerry Re: AR1335 camera sensor driver 嗨,凯瑞、 这是否意味着 RT1176(准确地说是 OV9281,数据格式为 RAW8)无法使用 8 位单色灰度图像传感器?这是硬件的基本限制,还是 SDK 的问题,将来会得到修复? 我已经使用恩智浦 iMX8M Mini SoC 运行了这个传感器,它似乎使用了类似的 MIPI CSI 外设,但需要移植到 RT1176。 贝斯特,迈克尔 Re: AR1335 camera sensor driver 适用于 Jetson nano 的 AR1335 Linux 设备驱动程序: https://www.arducam.com/docs/camera-for-jetson-nano/mipi-camera-modules-for-jetson-nano/driver-installation/ Re: AR1335 camera sensor driver 你好,fmabrouk、 很抱歉迟迟没有回复。 只要得到内部的 AE 回复,这对你来说确实是一个悲惨的故事:由于 VIDEO_MUX 错误,MIPI-CSI2 无法支持原始数据,这些信息将添加到 RT1170 参考手册中。 因此,请检查外部 AR1335 是否可以配置为支持,例如RGB? 现在是 10bit 原始数据,确实没有解决方法。 很抱歉回复晚了,非常感谢你们的努力。 顺祝商祺! kerry Re: AR1335 camera sensor driver 论坛其他成员或恩智浦团队对我的问题是否有任何反馈。我真的没时间了,需要解决这个问题!如果可以,请提供帮助。 Re: AR1335 camera sensor driver @kerryzhou 我希望你一切都好!我只是想跟进一下,看看你们是否对我的问题有任何更新。 我再次需要帮助配置 CSI 驱动程序,这样我才能捕获每个输出像素数据的 10 位原始数据。捕获数据后,我可以使用自己的软件将数据转换为 RGB 888 格式。 谢谢! Re: AR1335 camera sensor driver 你好,凯瑞、 还有一件事我想告诉你,相机传感器的输出格式是 RAW10(10 位):RAW10(10 位),而在当前的恩智浦 CSI/相机驱动程序中,我没有看到支持这种格式。我只看到这些: /*!@brief 像素格式定义。*/ typedef enum _video_pixel_format { /* RGB */ kVIDEO_PixelFormatXRGB8888 = FSL_VIDEO_FOURCC('X','R','2','4'),/*!< 32 位 XRGB8888。*/ kVIDEO_PixelFormatRGBX8888 = FSL_VIDEO_FOURCC('R','X','2','4'),/*!< 32 位 RGBX8888。*/ kVIDEO_PixelFormatXBGR8888 = FSL_VIDEO_FOURCC('X','B','2','4'),/*!< 32 位 XBGR8888。*/ kVIDEO_PixelFormatBGRX8888 = FSL_VIDEO_FOURCC('B','X','2','4'),/*!< 32 位 BGRX8888。*/ kVIDEO_PixelFormatRGB888 = FSL_VIDEO_FOURCC('R','G','2','4'),/*!< 24 位 RGB888。*/ kVIDEO_PixelFormatBGR888 = FSL_VIDEO_FOURCC('B','G','2','4'),/*!< 24 位 BGR888。*/ kVIDEO_PixelFormatRGB565 = FSL_VIDEO_FOURCC('R','G','1','6'),/*!< 16 位 RGB565。*/ kVIDEO_PixelFormatBGR565 = FSL_VIDEO_FOURCC('B', 'G', '1', '6'), /*!< 16 位 BGR565。*/ kVIDEO_PixelFormatXRGB1555 = FSL_VIDEO_FOURCC('X','R','1','5'),/*!< 16 位 XRGB1555。*/ kVIDEO_PixelFormatRGBX5551 = FSL_VIDEO_FOURCC('R','X','1','5'),/*!< 16 位 RGBX5551。*/ kVIDEO_PixelFormatXBGR1555 = FSL_VIDEO_FOURCC('X','B','1','5'),/*!< 16 位 XBGR1555。*/ kVIDEO_PixelFormatBGRX5551 = FSL_VIDEO_FOURCC('B','X','1','5'),/*!< 16 位 BGRX5551。*/ kVIDEO_PixelFormatXRGB4444 = FSL_VIDEO_FOURCC('X','R','1','2'),/*!< 16 位 XRGB4444。*/ kVIDEO_PixelFormatRGBX4444 = FSL_VIDEO_FOURCC('R','X','1','2'),/*!< 16 位 RGBX4444。*/ kVIDEO_PixelFormatXBGR4444 = FSL_VIDEO_FOURCC('X','B','1','2'),/*!< 16 位 XBGR4444。*/ kVIDEO_PixelFormatBGRX4444 = FSL_VIDEO_FOURCC('B','X','1','2'),/*!< 16 位 BGRX4444。*/ /* YUV。*/ kVIDEO_PixelFormatYUYV = FSL_VIDEO_FOURCC('Y', 'U', 'Y', 'V'), /*!< YUV422, Y-U-Y-V.*/ kVIDEO_PixelFormatYVYU = FSL_VIDEO_FOURCC('Y','V','Y','U'),/*!< YUV422, Y-V-Y-U.*/ kVIDEO_PixelFormatUYVY = FSL_VIDEO_FOURCC('U','Y','V','Y'),/*!< YUV422, U-Y-V-Y.*/ kVIDEO_PixelFormatVYUY = FSL_VIDEO_FOURCC('V','Y','U','Y'),/*!< YUV422, V-Y-U-Y.*/ kVIDEO_PixelFormatXYUV = FSL_VIDEO_FOURCC('X', 'Y', 'U', 'V'), /*!< YUV444, X-YU-V.*/ kVIDEO_PixelFormatXYVU = FSL_VIDEO_FOURCC('X','Y','V','U'),/*!< YUV444, X-Y-V-U.*/ } video_pixel_format_t; 能否在应用程序代码中将 Raw10 转换为 RGB888? 我附上了一些数据表供你参考。 Re: AR1335 camera sensor driver 你好,fmabrouk、 感谢您提供的信息。 请耐心等待,我将检查您的代码的更多细节,并与我们内部的 CSI 专家核实。 在我得到任何有价值的信息后,我会尽快通知你们。 请再给我一些时间,非常感谢! 顺祝商祺! kerry Re: AR1335 camera sensor driver @kerryzhou @jingpan 我用示波器验证了相机传感器正在流式传输数据;在调试代码时我能够捕获 CSI 读取寄存器:请参阅随附的屏幕截图。但是,我无法获得全帧缓冲区 CSI 中断。这还是与我初始化 MIPI CSI 的方式有关,你或其他人能否根据我在上一封邮件中说明的图像要求,帮我正确设置一下? 干杯 Re: AR1335 camera sensor driver @kerryzhou 以下是我感兴趣的图像参数摘要:; [PLL 参数] ;目标 Vt 像素频率:220 MHz ;输入时钟频率:24 MHz;实际 Vt 像素时钟:220 MHz ;实际操作像素时钟:110 MHz ;pll_multiplier(M 值)= 55 ;pll_clk_div2(N 值)= 2 ;pll_multiplier2(M2 值)= 55;pll_clk_div2(N2 值)= 55 ;pll_clk_div2(N2 值)= 55 2 ;Fpfd = 12 MHz;Fvco = 660 MHz;Fvco2 = 660 MHz;Vt 系统分频器 = 1 ;Vt Pix 分频器 = 3 ;运算系统分频器 = 1;运算像素分频器 = 6 ;;[图像参数];每个请求的帧数 第二:30 ;输出列:640;输出行数:480 ;使用 Y 求和:未选中 ;仅限 X 的分箱:未选中 ;允许跳过:选中 ;空白计算:HB 最大,然后 VB ;;最大帧时间:33.3333 毫秒 ;最大帧时钟:7333333.3 clocks ; 读出模式:1,YSum:无,XBin: ; Horiz clks: 640 active + 1688 blank = 2328 total ; Vert rows:480 活动 + 2674 空白 = 总计 3154 ; 输出列:640 ; 输出行:480 ; FOV Cols:640 ; FOV 行:480 ; 实际帧时钟:7342512 个时钟 ; 行时间:10.582 usec / 2328 个时钟 ; 积分时间:33 毫秒。 ;帧时间:33.375055 毫秒 ;允许的最大帧速率:191.739fps ;每秒帧数:29.962 fps Re: AR1335 camera sensor driver @kerryzhou 我在 imx RT1170 上使用 mipi CSI2 演示代码从 AR1335 获取 480x640 图像。 我发现该相机传感器的输出格式为:10 位。我需要在 CSI 驱动程序中进行哪些更改才能捕获我需要的图像。 我使用制造商的工具生成了配置文件,但由于错误配置了 CSI 驱动程序,我还远远没有获得图像。 你能否建议需要在演示代码 CSI 驱动程序中修改哪些内容才能从 AR1335 捕获图像。 此致敬礼, Re: AR1335 camera sensor driver 你好,fmabrouk、 到目前为止,我们还没有关于导入其他相机传感器的直接文件。 据我所知,照相机传感器也应该有配置工具,可以进行配置并生成代码。 您的 AR1335 是否已经从自己的公司获得了相关驱动程序? 我还检查了内部,直到现在才找到 AR1335 RT 的相关驱动程序。 顺祝商祺! kerry Re: AR1335 camera sensor driver @kerryzhou 我正在使用这个摄像头传感器:imX RT1170 板上的 AR1335 而不是 OV5640。AR1335 只发送 10 位图像。我相信 OV5640 像素数据总线是 16 位。 如何修改恩智浦 SDK 随附的 mipi csi 演示代码,以便用该传感器获取图像? 我希望能有一些文档,指导如何将另一个相机传感器导入该演示代码。 非常感谢!   Re: AR1335 camera sensor driver 你好,fmabrouk、 关于你提到的时钟,你可以从 RT1170 参考手册中找到: kerryzhou_0-1615519963656.png kerryzhou_1-1615519969817.png kerryzhou_2-1615520019886.png 希望它能帮到你! 顺祝商祺! kerry Re: AR1335 camera sensor driver @kerryzhou @jingpan 除了我上面提出的问题外,如果我需要将像素时钟设置为 80MHz。在 imx RT1170 的 CSI2 mipi 演示代码中,我应该更改哪些寄存器? 谢谢! Re: AR1335 camera sensor driver @jingpan @kerryzhou 我仍在尝试将 AR1335 摄像头驱动程序移植到 ImX RT1170 CCI2 mipi 演示代码中。 在 CS2 mipi 代码中,我发现了这些时钟: CLOCK_SetRootClock(kCLOCK_Root_Csi2,&csi2CClockConfig); CLOCK_SetRootClock(kCLOCK_Root_Csi2_Esc,&csi2EscClockConfig); CLOCK_SetRootClock(kCLOCK_Root_Csi2_Ui,&csi2UiClockConfig); 谁能解释一下这些钟是用来做什么的? 谢谢! Re: AR1335 camera sensor driver 你好,fmabrouk、 到目前为止,我还没有找到有关 AR1335 的 RT 芯片驱动程序,我也在内部搜索过,但没有找到。 也许您可以从互联网上搜索,某些第三方可能有 AR1335 驱动程序。 Nxp 官方那边没有找到,直到现在,RT 主要使用 MT9M114 或 OV7725 摄像头模块。 很抱歉给您带来不便,并感谢您的理解。 顺祝商祺! kerry
View full article
S32M2xx - MOSFET switching adjustment for Motor control examples This article is applicable to all motor control application SWs as described in the following article. S32M2xx - Motor control use cases - NXP Community It has been found that on some of S32M24xEVBs an overheating of the power MOSFETs may occur. This will be addressed in the new release of the Motor control example SW and will be carried out in Motor control example SW for S32M24xEVB, S32M27xEVB and S32M276SFFRD. As a solution in the current release, the following settings are recommended. Extend deadtime: For S32M24xEVB, for FTM3, set Dead Time to 50 (corresponds to 625 nanoseconds): JoJa_3-1763040265098.png For S32M27xEVB and S32M276SFFRD, for LCU outputs channels 0 - 5, set LUT rise filter to 75 (corresponds to 625 nanoseconds): JoJa_0-1763039392742.png Set faster slew rates: Common for all EVBs: JoJa_2-1763040220621.png
View full article