1101224_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

1101224_en-US

1101224_en-US

Example S32K144 FlexCAN Pretended Networking STOP mode test S32DS.ARM.2.2

********************************************************************************
 Detailed Description:

 Example shows how to use FlexCAN 0 Pretended networking mode to allow FlexCAN
 module to wake up MCU from STOP mode.
 Wake up by Timeout and wake up by Match events are enabled.
 Also pin interrupt can be used to exit STOP mode.

 So MCU enters STOP mode by pressing SW3 button.
 MCU exits STOP mode when one of following happens:
 - no CAN message comes in 8sec (CAN PN timeout event)
 - message with standard ID 0x554 or 0x555 comes (CAN PN match event)
 - SW2 button is pressed (PTC12 interrupt)

 In run mode blue LED is dimming and the rate is different for each wakeup event

 ------------------------------------------------------------------------------
 Test HW: S32K144 EVB-Q100
 MCU: FS32K144UAVLL 0N57U
 Fsys: 160MHz
 Debugger: Lauterbach, OpenSDA
 Target: internal_FLASH

********************************************************************************

General
タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-18-2025 05:29 AM
更新者: