Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Pressure sensors for low pressure (negative differential pressure/ underpressure) ? I am looking for a suitable pressure sensor for a project involving a gripping system for composites. With the help of a compressed air flow and the Coanda Effect a small vacuum is generated inside the gripper chamber. Therefore, a pressure sensor that is able to operate in the pressure range from -50kPa to 0( negative differential pressure), is needed. Along the Freescale line of products I was able to find the sensors MP3V5050V and MPXV5050VC6T1. The main difference between these two models that I was able to notice is the output range, is there any other differences that I should be aware of? However, I would like to have information about other suitable options. The two previous mentioned sensor are of the type gauge, are there any suitable ones of the type differential? Would you recommend gauge over differential? What are the main benefits of each type? Other features that the sensor should have are: -Temperature compensated - Conditioned output Signal ( Amplified Analog Output in Vdc or digital) -Operating Temperature Range of 0 to 50 C or above I thank you in advance for your time and support Pressure Sensors Re: Pressure sensors for low pressure (negative differential pressure/ underpressure) ? Hello Nicole, Thanks for using our community. The type of pressure sensor (gauge or differential) depends on the application. They’re basically the same device, both reads differential pressure. Differential pressure sensor measures the differential pressure between two pressurized chambers, that’s why those sensors had two hose connection ports (P1 & P2). Gauge pressure sensors measure the differential pressure between a pressurized chamber and atmospheric pressure. This kind of sensor only has one hose connection port (P1) and the second port (P2) is underneath the sensor, exposed to the atmospheric pressure. As per the description you wrote, I think you’d need a gauge pressure sensor, so that you can measure the generated vacuum inside the pressurized chamber using the atmospheric pressure as a reference. Please notice that differential pressure sensors can also be used as gauge pressure sensors by connecting the pressurized chamber into P1 and leave P2 exposed to the atmospheric pressure (when measuring positive pressure). In your case, since you’d measure _negative_ pressure you should connect P2 to the pressurized chamber and leave P1 open to the atmospheric pressure (P1 should ALWAYS be greater than P2). Hence, you’d have plenty of options here. You could use the sensor you mentioned or any differential pressure sensor that can measure 50kPa or more. There are no other differences between the devices you mentioned but the operating voltage, both of them are temperature compensated (0 to 80°C) and signal conditioned. Hope it helps! Regards, Josh
View full article
MPX5050 可以在海水中使用吗? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我正计划制造一个在海水中使用的皮托管式流体动态速度传感器。 我想了解一下你们的传感器系列: "MPX5050 Rev 11, 03/2010" 数据表中写道 "MPX5050/MPXV5050G可以在任何地方使用。 压力传感器 运行特性、内部可靠性和 鉴定测试使用干燥空气作为压力 媒体。干燥空气以外的介质可能会对以下设备产生不利影响 传感器性能和长期可靠性。联系 工厂了解有关 媒体兼容性 应用"。 因此,我的问题是:它在海水中能起作用吗? 压力传感器 Re: Can I use the MPX5050 in sea water? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,埃里克、 MPX5100DP 可用于您的应用,但请考虑以下信息。 一般来说,我们的压力传感器只能在清洁干燥的空气中使用。我们的媒体兼容性免责声明表明,我们的客户有责任确定其他环境中的媒体兼容性。我们敦促客户进行自己的内部评估和特性分析,以确定我们的设备是否适合在非清洁干燥空气环境中使用。 我们提供了一些应用笔记,为在液体环境中使用这些设备提供了一些想法: + AN1516 发布在此 URL 上,讨论液位控制:http://www.freescale.com/files/sensors/doc/app_note/AN1516.pdf + AN1950 发布在此 URL 上,讨论水位监测:http://www.freescale.com/files/sensors/doc/app_note/AN1950.pdf 模具上的凝胶涂层不应与湿气接触,因为潮湿时凝胶会膨胀,导致读数不可靠。凝胶必须保持完好无损,因为它可以保护模具的活性表面和线键不被氧化。 有些客户使用 P2 侧并抽真空,而不是在与非洁净干燥空气连接时对 P1 施加正压。P2 不包括凝胶,因此减少了一些媒体关注的问题,但并没有消除。一些客户使用的另一种方法是在 P1 表面填充硅脂,以保护模具和胶衣。还可以在传感器和介质之间设置物理屏障,以隔离传感器。 注油是在真空状态下进行的,以避免产生气泡。通常情况下,需要进行偏移校准,因为润滑脂会产生一些机械应力,可能会使偏移值发生偏移。 我们可以建议Gelest作为硅油脂的供应商: Gelest, Inc. 钢铁东路 11 号 宾夕法尼亚州莫里斯维尔 19067 (215)5 47-1015 http://www.gelest.com 同样,在任何不清洁的干燥空气环境中使用该设备都将导致保修失效。 通过添加硅油脂来修改设备时也是如此。 媒体兼容性免责声明: " 飞思卡尔已在选定的解决方案或环境中测试了介质容忍传感器设备,测试结果基于飞思卡尔选择的特定条件和程序。请客户注意,实际服务条件下的结果可能会有所不同。提醒客户,他们有责任确定传感器设备在其应用程序中的媒体兼容性以及可预见的应用程序的使用和滥用。" 祝您愉快, 何塞-雷耶斯 ----------------------------------------------------------------------------------------------------------------------- 注:如果本帖回答了您的问题,请点击正确答案按钮。Thank you! -----------------------------------------------------------------------------------------------------------------------
View full article
Using SEN-SPI-BOX + SEN-DSI3-ADAPTER to Validate DSI3 Slave – Is It Possible? Hello, I am currently preparing to validate a DSI3 slave device. Since the DSI3 protocol requires a master device for communication, I would like to confirm whether the following product combination can be used to act as a DSI3 master: SEN-SPI-BOX SEN-DSI3-ADAPTER Can this setup be used to validate a DSI3-compliant slave device? Also, I could not find a datasheet or detailed documentation for the SEN-DSI3-ADAPTER. Is there any official documentation or user guide available for this module? Thank you. SEN-SPI-BOX  Re: Using SEN-SPI-BOX + SEN-DSI3-ADAPTER to Validate DSI3 Slave – Is It Possible? Hello Choi, yes, the SEN-SPI-BOX + SEN-DSI3-ADAPTER combination is possible. Please refer to the UM11524.  I have attached the SEN-DSI3-ADAPTER schematic. Unfortunately we do not have any document for the SEN-DSI3-ADAPTER.  I apologize for inconvenience.  With Best Regards, Jozef
View full article
FXO8700 または FXAS21002 センサの両方を同じ PCB に配置すると、奇妙な問題が発生しました。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 当社の製品は正常に動作しますが、製品のライト部分をデバイスの底部に置いた瞬間に動作が停止します。 スプリングアクションライトのクリック音が、センサの 1 つまたは両方を混乱させることが判明しました。クリックの強さはボールポイントのクリックと同様です。これらのセンサが搭載された PCB がそのようなクリックにさらされた瞬間、センサから出力されるデータは完全に破損し、破損したままになります。 強いクリック音がしないようにスプリングを曲げると、センサーは正常に動作し続けるため、小さなクリック音であることが確実です。 この現象はコミュニティの他のユーザーに知られていますか? このようなクリックの G フォース スパイクが何らかの形でセンサ内部のレジスタを混乱させる可能性はありますか? その他の条件では、両方のセンサは問題なく完璧に動作します。 よろしくお願いいたします。 ルード 加速度センサ ジャイロスコープ Re: We got a perculiar problem with a FXO8700 or FXAS21002 sensor both placed on the same PCB. <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、ルードさん。 あなたがおっしゃったように、これは非常に特殊な問題であり、これまで同様の問題を抱えている人から聞いたことはありません。 問題はクリックによるものであると確信しているとおっしゃっていますが、追加テストとして、センサをオンにする前にライトをクリックしてテストすることは可能ですか? または、点灯した部分をクリックした瞬間(通常のクリック)に、ショートなどの事象が発生する可能性はありますか? ちなみに、「点灯している部分をクリックする」とおっしゃっていましたが、何が起こっているのかよく分かりません。可能であれば、アプリケーションと問題を視覚化するために、画像や写真をいくつかいただけると助かります。 すてきな一日を、 ホセ ----------------------------------------------------------------------------------------------------------------------- 注: この投稿で質問が解決した場合は、「正解」ボタンをクリックしてください。ありがとう! -----------------------------------------------------------------------------------------------------------------------
View full article
MMA8452Q I2C Read Single Byte problem Hi, I'm having a problem with the MMA8452Q when attempting to read the WHO_AM_I register over I2C. We are using an iMX28 based platform running Linux 2.6.35. The device driver reads a value of 0 instead of the expected value of 0x2A. I've seen that on the I2C bus the controller sends a Stop Condition after writing the register it wants to read before starting to read the actual value. It does not use a repeated start. The MMA8452Q data sheet states "....The MM8452Q expects repeated starts to be used to randomly read from specific registers". It also states (under Single Byte Read) "The Master (or MCU) transmits a repeated start condition (SR) and the addresses the MMA8452Q ($1D) with the R/W bit set to "1" for a read from the previously selected register. Does this mean we MUST use a repeated start when reading random register values and that the MMA8452 does NOT support using a Stop condition after writing the register address before another Start/Stop to read the actual value? Thanks, Bruno Accelerometers Sensing Platforms Re: MMA8452Q I2C Read Single Byte problem Thanks Tomas, It's what I thought but I just wanted it confirmed. Bruno Re: MMA8452Q I2C Read Single Byte problem Hi Bruno, Yes, the MMA8452Q uses a combined I 2 C data transfer format and requires a repeated start condition after the second byte (register address). A single byte read from the WHO_AM_I register 0x0D looks like this (note that it is for the MMA8652FC I have on my desk): Please let me know if you have any other questions. Regards, Tomas PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.
View full article
CRTOUCH can not work with 5-wire TP? Hi dears:    I start work with CRTOUCH, and found some problem with CRTOCH and 5-wire TP.  I use "Xtrinsic CRTouch Capacitive and Resistive Touch-Sensing Platform Evaluation Board" The 5-wire TP can work under mouse emulation tab.  And I successed calibration. But when I change to Gestures tab and start test, it shows: "Multi-touch points NOT calibrated. Please calibrate first at the 'Calibration' tab." Pls take a look at the following image: The calibrationg is ok. But here, it show calibration is not ok. The data from IC looks ok. When I use a 4-wire TP, it will work, but 5-wire TP not. Anybody who met this problem before? Thanks a lot! Pressure Sensors Sensing Platforms Touch Sensors Re: CRTOUCH can not work with 5-wire TP? Dear Jose: Thanks for your explanation. Now I'm fully understand. Thank you & best regards! 2014-05-28 ldqmoon From: Jose Alberto Reyes Morales Date: 2014-05-27 23:32 To: Luo Deqiang Subject: Re: - CRTOUCH can not work with 5-wire TP? CRTOUCH can not work with 5-wire TP? reply from Jose Alberto Reyes Morales in Sensors - View the full discussion Hi Luo Deqiang Unfortunately, dual touch gesture recognition is only supported for 4-wire resistive touch and unfortunately there is no other solution that we can offer to work with gesture recognition dual-touch with 5-wire. Basically, this is not a technical issue, but it is the way the algorithm is implemented for the CRTOUCH, this algorithm consider the impedance distribution of a 4-wire screen (connections, signal polarization) and therefore, the impedance distribution are different for the 5-wire screen panels. So, unfortunately , it is not possible to detect double touch gesture detection with the 5-wire CRTOUCH, 5-wire CRTOUCH only support single touch detection. Have a great day, Jose Reyes Re: CRTOUCH can not work with 5-wire TP? Hi Luo Deqiang Unfortunately, dual touch gesture recognition is only supported for 4-wire resistive touch and unfortunately there is no other solution that we can offer to work with gesture recognition dual-touch with 5-wire. Basically, this is not a technical issue, but it is the way the algorithm is implemented for the CRTOUCH, this algorithm consider the impedance distribution of a 4-wire screen (connections, signal polarization) and therefore, the impedance distribution are different for the 5-wire screen panels. So, unfortunately , it is not possible to detect double touch gesture detection with the 5-wire CRTOUCH, 5-wire CRTOUCH only support single touch detection. Have a great day, Jose Reyes ----------------------------------------------------------------------------------------------------------------------- Note: If this post answers your question, please click the Correct Answer button. Thank you! -----------------------------------------------------------------------------------------------------------------------
View full article
MMA8451Q で SA0 が未接続のままになっているとどうなりますか? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 最新のボードに誤って MMA8451Q の SA0 を残してしまいました。どのような行動が予想されますか?デフォルトで 1 つのアドレス (0x1C または 0x1D) に設定されるか、起動時にアドレスが決定される (つまり、ランダムに 1 つのアドレスを選択するが、電源がある限りそのアドレスが維持される) か、またはアドレス間を継続的に移動するかのいずれかだと思います。 最初のシナリオと 2 番目のシナリオはソフトウェアで簡単に処理できますが、3 番目のシナリオは面倒になります。 ありがとうございます 編集: AN4077 には、「ピン 7 (SA0: アドレス ピン)、... はすべてプルアップ/プルダウン抵抗を使用してピンの状態を維持する必要があります。」と記載されているため、未接続のままにしておくのは良くない選択だったと思います。 メッセージは osed によって編集されました 加速度センサ Re: What happens if SA0 is left unconnected on MMA8451Q? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、オスカー。 はい、SA0 ピンには内部プルアップ抵抗またはプルダウン抵抗がないため、フローティング状態のままにした場合、ピンの値がどうなるかを知る方法はありません。SA0 ピンを VDDIO (7 ビット アドレス = 0x1D) または GND (7 ビット アドレス = 0x1C) に接続する必要があります。 よろしくお願いいたします。 トーマス 追伸: 私の回答が質問の解決に役立った場合は、「正解」とマークしてください。ありがとう。
View full article
How to detect the Direction and Angle using XZ-accelerometer Sensor Dear All, I am using FXTH8719xxxx Family XZ axis Accelerometer Sensor. I need to find the direction as well how much angle turned by using X-axis ans Z Axis data. If any one can help me the possibility? Each sensor Z-Axis have the different offset values, help me how to calibrate the Z-axis with the new sensor. Accelerometers Re: How to detect the Direction and Angle using XZ-accelerometer Sensor hi Anthony, I have one points to clarify, what is the values for Z0 - Z base values, How to find the Z base values? Thanks, Sakthivel K Re: How to detect the Direction and Angle using XZ-accelerometer Sensor Dear Anthony, Thanks for your response. Your points are very helpful i'm collecting z-x axis data so i will apply your method if any points to clarify i get back to you. Regards, Sakthivel K Re: How to detect the Direction and Angle using XZ-accelerometer Sensor Hi Hulandaivel, There are several methods to calibrate sensor offsets. The big limitation with an accelerometer is you need to do the calibration phase with quasi-static data. I mean: if you move the FXTH8719xxxx , you will add an acceleration vector on both axis (Z & X) and this will degrade/pervert the calibration... So you have to take care of the sensor rotation by doing very smooth motion (external acceleration should be very small compared to the 1g-force). About calibration algorithms: 1. You can collect data/measurements around the circle in a buffer. When the full revolution is done, you compute the Z offset with an optimization method to minimize the standard deviation of the 1g vector on all measurements. 2. You can calculate the circle center with 3 points only. (Basic equations & resolution) ------ The final angle can be calulated with the following equation: -Z0 the Z bias - Z current / X current  are the actual measurements. Note that these equations are only valid in a static model and are using the 1g gravitational force as reference. I hope it helps. Thanks, Anthony
View full article
磁力計と磁気回転センサー <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Melexis MLX90316 に似た磁気回転センサが必要です。 ただし、SPI インターフェースを備え、最低 0.1 度の精度を持つ低電力 3.3V センサが必要です。 Freescale MAG3110 はこのような構成で動作しますか? MAG3110 のアナログ部分のゲインは非常に高いので、大きな磁場 (つまり、感知するシャフト上の磁石に隣接する磁場) があれば飽和してしまうのではないかと思います。 接触せずに角度の位置を感知する他の方法はありますか?また、機械的にも堅牢でなければなりません。 ありがとうございます ロブ。 磁気センサ Re: Magnetometer vs. Magnetic Rotary Sensor <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ロブ、 それは確かにチェックしてみる価値のあるものです。通常、当社のハード/ソフトアイアン補正ルーチンが使用されるときは、温度の影響についてはあまり心配しません。これらの計算は 1 秒間に複数回実行され、温度スケール/オフセットの問題はこれらの計算の副次的な効果として修正されるはずです。 Mike Re: Magnetometer vs. Magnetic Rotary Sensor <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ご意見ありがとうございます、マイクさん。 私がホセに述べたように、このデザインは磁気角度センサを必要としないところまで進化しました。 しかし、以前の投稿(あなただったと思います)で、MAG3110 にも厄介な温度ドリフトがあり、定期的に補正する必要があると書かれていたことに気付きました。MLX の部分ではこれに気づきませんでした。この問題はこのテクノロジーに共通するものでしょうか?このようなニーズに再度遭遇した場合、誰の部品を見ているかに関係なく、温度に対する安定性を考慮に入れる必要がありますか? それでは。 ロブ。 Re: Magnetometer vs. Magnetic Rotary Sensor <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ご返信ありがとうございます、ホセ。 この設計を進めていくうちに、角度位置の検出に磁気センサを使用する必要がなくなりました。磁場強度マネジメントに関するご提案は理解できました。このアプリケーションでは、FXOS8700 のわずかに高い範囲は、追加コストを正当化するのに十分ではない可能性があります。加速度センサは必要ですが、さまざまな理由から、磁力計を配置する必要がある場所に加速度センサを配置するのは不適切です。 サポートとご関心をいただきありがとうございます。 それでは。 ロブ。 Re: Magnetometer vs. Magnetic Rotary Sensor <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 皆様、 参考までに、FXOS8700CQ には mag と accel の両方が含まれており、MMA8451Q とピン互換性があると思います。しかし、以前の投稿で述べたように、最大磁場には注意を払う必要があります。センサの最大値は +/- 1200 マイクロテスラです。 Mike Re: Magnetometer vs. Magnetic Rotary Sensor <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、ロブ。 まず、MAG3110 はホール センサではないことに注意することが重要だと考えます。 また、デバイスのフルスケール範囲 (FSR) はそれほど大きなスケールではないため (+/-1000uT)、飽和についても考慮する必要があると思います。 アプリケーション内でフィールドがどの程度強力になるかは不明のため、これに関する質問に答えるのは困難です。Melexis 部品の標準的な磁場強度は 50mT であり、これは MAG3110 の FSR の 50 倍であることがわかります。SO、あなたが送ってくれた情報に基づく私の見解によれば、飽和は起こり得ると思いますが、より弱い磁石を使用するか、センサーから遠ざけることでこれを回避できる可能性があります。 飽和問題が解決されると、理論的には、MAG3110 の x 軸と y 軸のみを使用して、センサ上面と共面の磁気ベクトルを計算することが可能になります。1 度未満の精度が必要な場合は、おそらく硬鉄/軟鉄のキャリブレーションを実行する必要があります。また、このキャリブレーションを使用しても、他のさまざまな要因に依存するため、これを達成できることを保証することはできません。 代わりに、FXOS8700 をご覧になることをお勧めします。FSR がわずかに高く、温度性能も優れています: http://cache.freescale.com/files/sensors/doc/data_sheet/FXOS8700CQ.pdf Re: Magnetometer vs. Magnetic Rotary Sensor <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 返信ありがとうございます、ホセ。 実際、この設計では、傾き検知に Freescale MMA8451Q を使用します。 磁気回転センサーはシャフトの回転を感知するためのものです (したがって、傾き感知は適切なソリューションではありません)。 MAG3110 の使用を試みる際の懸念は、ホール センサの下流のアンプがこのアプリケーションの強力な磁場によって飽和してしまうのではないかということです。これは起こらないと言っているのですか?そうではないことがわかるような、この種のアプリケーションで MAG3110 を使用した経験はありますか? デザインで I2C を使用することについては、あまり心配していません。速度の点では SPI の方が好みです (I2C は非常に遅くなることがあり、これはバッテリー駆動のデバイスです)。 再度、感謝します。 ロブ。 Re: Magnetometer vs. Magnetic Rotary Sensor <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、ロブ。 Freescale Magnetometer MAG3110 は、Melexis MLX90316 を搭載した専用の回転位置センサではありませんが、磁力計に加えて加速度センサを使用してさらに精度を上げることで作業を実行できます。ただし、MAG3110 には SPI 通信インターフェースがありません (I2C のみを使用)。 お客様のアプリケーションに適したもう 1 つのソリューションとして、3 軸加速度センサを使用した傾き測定が挙げられます。この方法については、次のアプリケーションノートをご覧ください: http://cache.freescale.com/files/sensors/doc/app_note/AN3461.pdf ただし、現時点では、新しいデザインに推奨される SPI インターフェースを備えた加速度センサはありません。 よろしくお願いいたします。 ホセ
View full article
MPR121のマトリックスPCBレイアウト設計オプション <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> AN4600 以外に、MPR121 でサポートされているマトリックス PCB レイアウトの列と行の構成にはどのようなものがありますか? つまり、4 列 (ELE0-ELE3)、8 行 (ELE4-ELE11) を設計できるのでしょうか? AN4600 ではブロック サイズ 3.5 - 4.00 mm を推奨します。それはブロックの側面寸法ですか? センサのカバーの最大厚さはどれくらいですか? カバーは PCB に接着する必要がありますか? PCB とカバーの間に隙間があってもよいですか? タッチ・センサ Re: Matrix PCB layout design options for MPR121 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、ジェームズ。 当コミュニティをご利用いただきありがとうございます。MPR121 には「サポートされている構成」はありません。アプリケーションに適した構成を使用できます。変更されるのは補間アルゴリズムのみであり、これはマトリックス配列に完全に依存します。 電極の推奨最小面積は 3 x 3 mm です。 すべての質問に対する回答は、次のアプリケーションノートに記載されています。 http://cache.freescale.com/files/sensors/doc/app_note/AN3863.pdf お役に立てれば幸いです。 -ジョシュ
View full article
MPXV7002 - sensitive to position? Or a faulty part? I'm trying to use an MPXV7002 in a handheld mobile connected device. It appears the baseline shifts when I pick up the device. Is the MPXV7002 sensitive to position (effect of gravity on the membrane)? Or should it remain the same reading no matter how I hold the transducer? Thanks, Jerry Pressure Sensors Re: MPXV7002 - sensitive to position? Or a faulty part? Hi Jerry, Yes, a small change in offset voltage (typically a few mV) due to a change in position is common for such highly sensitive pressure sensors. This is because the the diaphragm and gel of the sensor have mass and because the mass to diaphragm thickness ratio increases as the pressure range decreases, the sensitivity to position increases as the pressure range decreases. Regards, Tomas PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.
View full article
動かないデバイスのMAG3110キャリブレーション <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 電源を入れても動かないデバイスがあるのですが、どの方向を向いているのか知りたいです。MAG3110 磁力計のキャリブレーション手順では、デバイスを移動して (図 8 または類似の図)、結果として得られる測定範囲にソリューションを適合させます。少量の PCB/デバイスのサンプルの硬鉄と軟鉄の較正を決定し、それを同じレイアウトの他のすべてに使用できると想定するのはどの程度合理的でしょうか? 磁気センサ Re: MAG3110 calibration of devices that don't move <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> トーマスの返答を確認してください。 mag3110からのデータを処理する方法 私があなたに提供する追加情報があれば、その方法を理解できるはずです。Hardiron キャリブレーションを使用し、次に arctan(Y/Z) を適用します。全てのピースが揃っているので、それを全て結合するだけです。 アンソニー Re: MAG3110 calibration of devices that don't move <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 水平と水平の間の角度を計算したいだけの場合はどうすればいいでしょうか? 発信したiPhone Re: MAG3110 calibration of devices that don't move <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> はい、調整する必要があります。そうしないと、不正確な結果になります。 Re: MAG3110 calibration of devices that don't move <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 水平に対する角度を知りたいだけです。mag3110で何ができるでしょうか?調整が必要ですか?詳しいやり方を教えてください 発信したiPhone Re: MAG3110 calibration of devices that don't move <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、マンディさん。 このソフトウェア機能は、HardIron (ボードと磁力計によってもたらされるオフセット) をキャリブレーションするためのものです。ただし、これは 1 つの重要な条件を満たせば機能します。キャリブレーションの実行中にボード/MAG31110 を 3 軸で回転させる必要があるということです。 下のグラフを見てください(ここではボードは一定速度で回転していますが、そうする必要はありません) 磁力計を回転させると、磁場(コンパスのように地球によって誘導される)が変化します。最小値と最大値をキャプチャすることで、MAG3110 のオフセットを計算できるようになります。これらの値を OFF_axis_xSB レジスタに書き込むことで、MAG3110 はこのハードアイアン ベクトル補正を生の測定値に適用できるようになります。これがキャリブレーションです。 これがお役に立てば幸いです。 アンソニー Re: MAG3110 calibration of devices that don't move <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは。 デモを参考にキャリブレーション方法を使用します。しかし、私が間違っている場合、なぜこの方法で調整できるのかわかりません。mag3110 組み込みオフセットをどのように使用すればよいですか? スクリーンショットは私の調整方法です Re: MAG3110 calibration of devices that don't move <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、ベン。 MAG3110 組み込みオフセット キャリブレーションを使用しましたか、それとも実際の磁気外部キャリブレーションを使用しましたか?自動キャリブレーションの場合は、1、2、または3軸で動作します。 「静的(非動的)キャリブレーション」を実行することがどの程度合理的であるかを判断することは困難です。最終的なアプリケーションに応じて異なりますが、合理的ではないと言えます。それについてさらに詳しく教えていただけますか? ありがとうございました。 アンソニー
View full article
关于接收 NTM88 示例的问题 要配置我的 RF 接收器,我需要 NTM88 示例代码中的设置,例如:载波频率 (434MHz?会不会是 433.92MHz?)、传输速率(最大 19200 波特?),但主要是偏差。另一个问题是,发送的 CRC 是将所有值都设为 1 还是 0? Re: Questions for receiving the NTM88 example 亲爱的以色列 请看下面应用工程师的回答。 说明 寄存器的默认值见用户手册。参见寄存器描述中的 “RESET” 行:它包含开启射频模块时不同位的值。 致以最崇高的敬意 约瑟夫 Re: Questions for receiving the NTM88 example 感谢约瑟夫帮我解决问题!阅读代码,查看是否有以下说明:"434.0083 - 433.9131 = +/- 47.6kHz" 这就是中心频率的推导率吗?还是与 BFREQ/AFREQ = 3.17 kHz 有关? Re: Questions for receiving the NTM88 example 亲爱的以色列 下面是我联系的一位应用工程师的回答。 说明 射频模块在 main.c 中的 u8InitRf() 函数中初始化。 这里配置了控制频率、波特率、频率偏差......的寄存器。 如需了解寄存器值与频率、波特率......之间的对应关系,请参阅用户手册,其中详细介绍了所有寄存器: https://www.nxp.com/webapp/Download?colCode=UM11227&appType=license 致以最崇高的敬意 约瑟夫 Re: Questions for receiving the NTM88 example 感谢您的回答!我已经有了代码示例,我正在查找 NTM88 的默认射频设置,特别是 CRC 发送 0 还是 1,以及 433mhz 时的导出值。 Re: Questions for receiving the NTM88 example 亲爱的以色列 有关 NTM88 的代码示例,请参阅NTM88 产品页面。代码示例位于软件部分。 致以最崇高的敬意 约瑟夫
View full article
0.2g 未満の加速度を測定するのに最適な加速度センサはどれですか? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 0.2g 未満の加速度での Z 軸の動きを測定したいです。どの加速度センサを調べるべきでしょうか? 加速度センサ センシング・プラットフォーム Re: Optimal accelerometer for measure accelerations less than 0.2g? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、プラヴィーンさん。 MMA8451Qは、マーケットで最も低ノイズのデジタル部品と言えるでしょう。優れた温度特性と14ビットの分解能を備えており、このようなアプリケーションに最適です。可能な限り低いODRを選択し、±2gのレンジを設定し、低ノイズ(LNOISEビット = 1)モードと高解像度(SMODS = 1)モードの両方を使用することで、最高のノイズ性能が得られます。また、傾き誤差を補正するために、内蔵ハイパスフィルタの使用も推奨されます。 お役に立てれば幸いです。 よろしくお願いいたします。 トーマス Re: Optimal accelerometer for measure accelerations less than 0.2g? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ありがとう、トーマス。私のアプリケーションに関する詳細は以下のとおりです。 加速度センサは直線に沿って約 1 メートル移動します。最大加速度はおそらく 0.5g 以下、平均は 0.1g 以下です。加速度センサはしばらく加速し、その後減速して停止し、その後後退します。 この動きが行われるたびに加速度と移動距離が変化するため、毎回正確に測定したいと思います。 私はプロトタイプを構築しており、最初は加速度センサからデジタル出力を取得したいと考えています。この加速度センサをRasPiに接続しています。 データシートを確認したところ、MMA8451Q が試してみる価値があるようです。距離を測定するのは大きな課題であることは承知していますが、私が説明したような制約のある環境では、それが可能だと思いますか。RasPi でいくつかのプロセッシングアルゴリズムを実行できます。検討すべき後プロセッシングアルゴリズムについて何か提案はありますか? よろしくお願いします。 プラヴィーン Re: Optimal accelerometer for measure accelerations less than 0.2g? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、プラヴィーンさん。 アプリケーションと要件についてもう少し詳しく説明していただけますか? 信号調整された電圧出力を備えた 低GのZ軸加速度センサをお探しなら 、 MMA1270KEG(R2) をご検討ください。この製品は、±2.5gのフルスケール範囲と750mV/gの感度で加速度を測定します。 また、低消費電力で高感度を実現する新しい 3 軸アナログ加速度センサFXLN83xxQファミリも検討することをお勧めします。この製品およびその他の(デジタル)デバイス( MMA8451Q 、 FXLS8471Q 、 MMA8491Q )の詳細については、ファクトシートを参照してください。 よろしくお願いいたします。 トーマス 追伸: 私の回答がご質問の解決に役立った場合は、「正解」または「役に立った」と評価してください。ありがとうございます。
View full article
I'm looking for the right processor for a MMA865... Dear members, i'm a newbie in this chat. But i hope you can help me. Our company is looking for the right processor for using an MMA865 accelerometer. We want to detect the deceleration and the tilt of a vehicle. It is necessary that  the detection is very fast and the current consumption as low as possible because we want to use Energy Harvesting. Thank you for your answers. Accelerometers Re: I'm looking for the right processor for a MMA865... Hi Christopher, Several options for you and others probably have good advice too. The Freedom boards for the Kinetis L Series of MCU's (KL02/KL03/KL05) are low power and have an accelerometer (MMA8451Q 14-bit rather than 10-bit you are looking at) on board too. Kinetis L series MCUs FRDM-KL02Z for Kinetis KL02 MCUs FRDM-KL03Z for Kinetis KL03 MCUs FRDM-KL05Z for Kinetis KL05Z and KL04Z MCUs The LPC812 is ultra low power and has reference design with energy harvesting: Smartphone Quick-Jack solution | www.LPCware.com Other information on it: - OM13069 Smartphone Quick-Jack solution|NXP - http://www.nxp.com/documents/application_note/AN11552.pdf Regards, David
View full article
UAV飛行姿勢記録 ドローンの3軸の方位角、加速度、速度を記録したいです。 高さも記録できればさらに良いでしょう。 ただし、記録されたデータはリアルタイムで地上のコンピューターに送信する必要があります。 Re: 无人机飞行姿态记录 以下から選択できます。 製品セレクタ | NXPセミコンダクターズ
View full article
For MMA685x Accelerometer, what is the maximum junction temperature Tj? For MMA685x Accelerometer, what is the maximum junction temperature Tj?  The datasheet lists a Storage Temperature Range of -40C to +125C, but Max Tj is not provided. Accelerometers Re: For MMA685x Accelerometer, what is the maximum junction temperature Tj? Hi Gerard, I just got an answer from our apps/design team, the maximum junction temperature Tj is 85 °C. Regards, Tomas Re: For MMA685x Accelerometer, what is the maximum junction temperature Tj? Hi Gerard, OK, I need to check on this. I have emailed our apps/design team and will update this thread once I have their answer. Regards, Tomas Re: For MMA685x Accelerometer, what is the maximum junction temperature Tj? Thank you Tomas for the quick response. I do not anticipate the device exceeding the Max Tj in our application; the worst case hot operating temperature is around 70°C. However, the Reliability Report I am compiling requires documentation of the manufacturer’s Max Tj for all semiconductor devices and microcircuits in the design. Since the Max Storage Temperature is listed as 125°C, is it a reasonable to also use this as Freescale’s rating for the Max Tj? If not, can Freescale provide a value for the Max Tj rating? Regards, Gerry Seipelt L-3 Communications O: 513.943.2226 Re: For MMA685x Accelerometer, what is the maximum junction temperature Tj? Hi Gerard, I do not have an exact number, but the very low power consumption leads to a negligable increase of the junction temperature (<< 1 °C). Regards, Tomas
View full article
MPX2010DPは空気の流れを計算します <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 拝啓、 以下の条件で空気流量(kg/s)を計算するにはどうすればよいでしょうか?ぜひお勧めください。ありがとうございます 1. パイプ径:6mm 2. オリフィス径:5mm 3. 圧力差(MPX2010DP圧力センサから取得):0.5 psi 圧力センサ Re: MPX2010DP calculate air flow <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 親愛なるヨゼフへ 迅速なサポートをありがとうございます。 Re: MPX2010DP calculate air flow <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ジェフ様 空気の流量を計算する方法と計算式が記載されたリンクを見つけました。こちらのリンクをご覧ください: https://allsensors.com/engineering-resources/white-papers/pressure-point-11-calculating-flow-rate-from-pressure-measurem… こちらもご覧ください:低速はダクト内の空気の流れに悪影響を及ぼしますか? | Energy Vanguard あなたにとっても役立つかもしれません。 敬具、 ヨゼフ
View full article
压力传感器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,我想在我的项目中使用压力传感器 MPX2100A 1- 我读到 110kpa 是什么意思(大气压力 +100 kpa ) 2- 是否可以将 arduino 与该压力传感器配合使用? Re: pressure sensor <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,努里、 1.MPX2100A 是一种绝对压力传感器,这意味着设备输出是指施加在表面上的单位面积力的绝对值。因此,绝对压力是某一点的压力与绝对零度压力或完全真空之间的差值。 在这种情况下,您读取的不是大气压力,而是施加在 P1 上的压力。 2.事实上,您可以将 MPX2100A 与 Arduino 一起使用。 请注意,MPX2100A 是一种补偿压力传感器,这意味着给定输出已经过内部温度补偿,因此只需在外部添加放大电路,然后将传感器信号发送到MCU 的 ADC。 您可以参考以下放大电路: 希望这些信息对你有用。 如果我误解了你的问题,请随时告诉我。 我很乐意提供帮助。 祝您有美好的一天。 戴维-迪亚兹 注:如果本帖回答了您的问题,请点击 "正确答案 "按钮。谢谢!
View full article
FXTH87 Evaluation Module or Development Kit Hi. I'm studing on TPMS and looking for the FXTH87 Family DVK to implement the system. According to "Xtrinsic FXTH87 Evaluation Design Reference Manual", It seem that the DVK or EVM are exist. But I was not able to find the web-site that sales the device. How can i get it ? And I also need to a device that can receive the sensing data from FXTH87. Thank you for your interesting. Pressure Sensors Sensing Platforms Re: FXTH87 Evaluation Module or Development Kit Hi. I don't receive any answer from Pascal Bernard. So, i try to contact with Freescale Korea Inc, and request the any help. At the result, I got the FXTH87 Module from Freescale Korea Inc. If you want to get the FXTH87 evaluation board, i advise you to try to contact with branch office of your location. I hope that this answer is helpful. Regards. Re: FXTH87 Evaluation Module or Development Kit Hi! Only Pascal Bernard can help with FXTH87 Development kit and evaluation board? I wrote to him, but didn't receive any answer... We working on prototype of commercial TPMS. With plans begin to produce it in Russia at 2016 Thank you! Re: FXTH87 Evaluation Module or Development Kit Hi Sol, New FXTH87 family evaluation boards are available in a limited quantity, please email directly MBW108 with your contact information and application description. Meanwhile, you might find useful the Xtrinsic FXTH87 Family Evaluation Design Reference Manual including the schematic, BOM and other useful information. Regards, Tomas PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.
View full article