Hello,
I am currently preparing to validate a DSI3 slave device.
Since the DSI3 protocol requires a master device for communication, I would like to confirm whether the following product combination can be used to act as a DSI3 master:
SEN-SPI-BOX
SEN-DSI3-ADAPTER
Can this setup be used to validate a DSI3-compliant slave device?
Also, I could not find a datasheet or detailed documentation for the SEN-DSI3-ADAPTER.
Is there any official documentation or user guide available for this module?
Thank you.
Hello Choi,
yes, the SEN-SPI-BOX + SEN-DSI3-ADAPTER combination is possible. Please refer to the UM11524.
JozefKozon_0-1748411079001.png
JozefKozon_1-1748411127320.png
I have attached the SEN-DSI3-ADAPTER schematic. Unfortunately we do not have any document for the SEN-DSI3-ADAPTER.
I apologize for inconvenience.
With Best Regards,
Jozef