Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Usage of register pointer read and write in G-Sensor (MMA690xKQ) Hello, I am using High Accuracy Low g Inertial Sensor (MMA690xKQ) in my project. I have read the specification but I am unable to find the use case of Register Pointer Read and Register Pointer Write in Table 3.4, 3.5, 3.6, 3.7. Kindly let me know how to use Register Pointer Read and Register Pointer Write and also the meaning of bits A[7:0] is the same tables. Accelerometers Re: Usage of register pointer read and write in G-Sensor (MMA690xKQ) Hello For any register reading I am getting E6 or FE response can you please help me on exact response clock is good and CS pin also ok Re: Usage of register pointer read and write in G-Sensor (MMA690xKQ) Hello register address: e       register address:14     message transmitted STATUS is 0xe0-0x00-0x00-0x00 E0 00 STATUS is 0xe0-0x00-0x00-0x00 serialNo - 0:e0 printf device status register register address:1   register address:30    message transmitted STATUS is 0xff-0xff-0x00-0x00 FF FF STATUS is 0xff-0xff-0x00-0x00 serialNo - 0:ff printf device status register register address:0   register address:20    message transmitted STATUS is 0xe6-0x00-0x00-0x00 E6 00 STATUS is 0xe6-0x00-0x00-0x00 serialNo - 0:e6 this is the response I am getting Please help me on the exact response Re: Usage of register pointer read and write in G-Sensor (MMA690xKQ) Hello Manojkumar, The SPI protocol for the MMA690x devices does not allow for transmission of both a register address and register data in the same command.  The address must be set by a previous command.  This is the purpose of the Register Pointer Write command.  The Register Pointer is the address at which data will be read from or written to when a Register Data Write or Register Data Read is executed.  So the normal sequence for a register read or a register write will take at least 2 commands:   Register Read: Send a “Register Pointer Write” command to set the pointer to the register address to be read Send a “Register Data Read” command to retrieve the data from the register pointed to Register Write: Send a “Register Pointer Write” command to set the pointer to the register address to be read Send a “Register Data Read” command to retrieve the data from the register pointed to   Note that the MISO response for each MOSI command will come on the subsequent transfer.  As shown in the image below. Here are a few examples. Read Register $10 (DEVSTAT) Register Pointer Write to $10 MOSI                    = 0x1410 Expected MISO  = 0x0800 Register Data Read MOSI                    = 0x2000 Expected MISO  = 0x1000              (assumes no flags set in DEVSTAT) Write 0x01 to Register $0E (Enable Positive Self-Test) Register Pointer Write to $0E MOSI                    = 0x140E Expected MISO  = 0x0800 Register Data Write MOSI                    = 0x3001 Expected MISO  = 0x180E              (includes address echo) Register Data Read to Confirm MOSI                    = 0x2000 Expected MISO  = 0x1401 I hope this is clear. Best regards, Tomas
View full article
Using a MMA8451 FIFO Interrupt I am using the 8451 in the following configuration. - ODR 800 Hz 4G scale - I2C at 400kHz rate - Sleep modes disabled. always in active mode -FIFO in Circular Buffer mode. -The only interrupt configured is "FIFO full" vectored to the Int1 pin. That is No watermarks or pulse/landscape/freefall detection enabled. - On the interrupt I flush the FIFO 14 bit data...192 bytes. - For speed of operation and hence current consumption I do not read either:    (a)The status register at 0x00. as I can guarantee I will service the interrupt and read out some data before the next sample is done 1.25mS later.    (b) The Interrupt source register at 0x0C as I only have one interrupt source. This appears to works OK. The interrupt on INT1 pin goes high approximately half way through the 5.2mS FIFO flush However it is not clear from the datasheet that for correct operation you must  read the interrupt source register to clear it. Question: Must I clear the interrupt source register by reading it for correct operation regards John Campbell Re: Using a MMA8451 FIFO Interrupt Tomas, Thanks very much for your prompt response to this and my other question. This is a relief as I release my software on Wednesday for a major production run for an automotive client. Best regards and thanks again Johnc Re: Using a MMA8451 FIFO Interrupt Hi John, Yes, there is no need to read the INT_SOURCE register (0x0C), the SRC_FIFO bit is cleared and consequently the INT1 pin deasserted by reading all the X, Y, Z output data registers (0x01 – 0x06). Best regards, Tomas
View full article
FXAS21002(ジャイロ)状態図問題 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> これは愚かな論理的行き詰まりのように聞こえるかもしれませんが、それでも私は尋ねます。 FXAS21002 データシート (Rev2.0、2015年2月号では、23ページの図15に遷移図を示しています。 図によると、センサがアクティブ モードのときに、CTRL_REG1 に特定のビットを書き込むことによって、センサを準備モードまたはスタンバイ モードに切り替えることができます。第 6 章.15 の 42 ページのレジスタの説明には、CTRL_REG1 への書き込みはアクティブ モードではなく、スタンバイ モードまたは準備完了モードでのみ許可されることが明記されています。これは実際には、出力データが破損している可能性があるものの、いずれにせよ準備完了またはスタンバイへの移行が行われる、つまりモードが変更されることを意味しますか? よろしくお願いいたします(帯域幅を使用して申し訳ありません) ハリ・ヴァンハラ ジャイロスコープ Re: FXAS21002 (gyro) state diagram problem <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、ハリー。 第 6 章.15 の注記は、実際には、出力データ レート (DR[2:0] ビット) を変更するには、FXAS21002 をスタンバイ モードまたは準備完了モードにする必要があることを意味しています。そうしないと、出力データの正確さは保証されません。したがって、次のようなものを使用することをお勧めします。 // 準備モード IIC_RegWrite(CTRL_REG1, IIC_RegRead(CTRL_REG1) & 0b11111101); // ODRを変更する IIC_RegWrite(CTRL_REG1, IIC_RegRead(CTRL_REG1) | 0b000xxx01); // 再びアクティブモード IIC_RegWrite(CTRL_REG1, IIC_RegRead(CTRL_REG1) | 0b00000011); よろしくお願いいたします。 トーマス 追伸: 私の回答が質問の解決に役立った場合は、「正解」とマークしてください。ありがとう。
View full article
FRDM-KL25Zを使用した転倒検知と歩数カウント <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> さて、私は Freescale FRDM-KL25Z 開発プラットフォームに取り組んでいますが、次のサンプル コードを入手できません。 - 落下時にLEDを点滅させる方法(基本的には落下検出) - 人体に装着して歩数を数える方法。 誰かこの件について助けてくれませんか?本当に緊急なんです… よろしくお願いします。 センサ・フュージョン Re: Fall Detection and Step Count using FRDM-KL25Z <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、メーガンさん。 FRDM-KL25Z は、MMA8451 加速度センサを搭載したマイクロコントローラ ボードです。 自由落下のようなイベントをキャプチャするには、自由落下を検出し、MCU にイベントを通知する割り込みを生成するように、レジスタに設定を書き込むことによって、I2C 経由で加速度計をプログラムする必要があります。その後、MCU はオンボード LED をオンにして表示することができます。以下の手順に従って例を構築します。 さて、歩数を検出するには、加速度センサのデータを読み取って歩数を計算できる歩数計アルゴリズムが必要になります。歩数検出には、以下に示す例を使用できます。 https://mcuxpresso.nxp.com/をご覧ください--> ボードの選択 --> ボード --> Kinetis --> FRDM-KL25Z --> MCUXpresso SDK のビルド --> ソフトウェア コンポーネント ISSDK を追加し、SDK アーカイブをビルドしてダウンロードします。 自由落下検出の場合、サンプル boards\frdmkl25z\issdk_examples\センサ\mma8451q\mma845x_interrupt を開始点として使用し、アプリケーションノートAN4070.pdfに従って自由落下検出サンプルを作成します。 歩数計の場合、サンプル boards\frdmkl25z\issdk_examples\algorithms\pedometer\pedometer_mma8451 が目的にかなうはずです。
View full article
NTM88 | SPI が期待通りに動作しない 親愛なるチームの皆様、 お客様は当社の NTM88 センサを使用していますが、SPI 経由で MCU と通信する際に問題が発生しています。 お客様によると、当社のすべての文書を概観しているときに、いくつかの情報が一致していないことに気づいたそうです。 たとえば、NTM88 ファームウェア ライブラリ ユーザー ガイド ( UM11145) では、センサが CLK と DATA に PTA0 と PTA1 を使用すると説明されていますが、NTM88+KW38 サンプル ガイドのサンプル コードでは、ピンの異なる設定が示されており、混乱を招きます。 SO、顧客はコードのベースラインとして NTM88+KW38 BLE ビーコンのサンプル コードを搭載したスティックを選択し、セットアップは以下の NTM88+Silab (BLE) になります。 お客様の質問は、SPI 通信が機能しない理由を理解することです。お客様は、KBI 割り込みは機能しているものの、センサからのデータが表示されないことに気づきました。 何が問題なのか教えてください。 親切なフィードバックをお待ちしております。よろしくお願いいたします。 よろしくお願いいたします。 シャイ 加速度センサ 圧力センサ センサ・フュージョン Re: NTM88 | SPI Not working as expected こんにちは、シャイさん。 すべてが順調であることを願っています。NXP コミュニティをご利用いただきありがとうございます。 メールで送信するファイルを確認してください。GPIO と SPI/I2C 機能間のマッピングの構成を図 4 に示します。 この情報がお役に立てれば幸いです。 よろしくお願いいたします。 デビッド
View full article
FXAS21002 gives WHO_AM_I as 0 Hello. I am querying the FXAS21002 gyro via I2C interface for the WHO_AM_I register. I don't seem to get any result other than 0. Following is a screen shot from the logic analyzer. What seems to me slightly strange is that after the 9th bit (the ACK) get transmitted, the SDA doesn't go high for some period of time before the address of the register gets transmitted. Is it possible that this is the problem I am facing? If not, what might be the problem? Thank you very much in advance. Gyroscope Re: FXAS21002 gives WHO_AM_I as 0 Hi Tomas. Thanks. You are right. The repeated start is actually the issue. It seems that Raspberry Pi3 can not handle it correctly. Kind regards, Efthymios Re: FXAS21002 gives WHO_AM_I as 0 Hi Efthymios, I guess the problem is that you are sending the stop condition (a LOW to HIGH transition of SDA while SCL is HIGH) after the second byte (0x0C) instead of sending the repeated start condition. So try to modify your source code so that SDA transitiones to HIGH before the SCL goes HIGH in order to eliminate the stop condition. Hope it helps. Best regards, Tomas
View full article
MMA8652 : 過渡割り込み閾値 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 親愛なるコミュニティの皆様 過渡割り込みしきい値を考慮します。 以下のようにレジスタ値を設定する場合、 一時割り込みはいつ発生しますか? 0x1F:TRANSIENT_THSレジスタTHS[6:0]を000_0000bに設定します。 0x1D:TRANSIENT_CFG レジスタ HPF_BYP を 1 に設定します。 過渡割り込みトリガーポイント値はどれですか? 「ゼロ G 以上」か「ゼロ G より大きい」か? よろしくお願いします、 坂上公一 加速度センサ Re: MMA8652 : Transient interrupt threshold value <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 光一様 最小しきい値解像度は 0.063g (TRANSIENT_THS = 0x01) です。当社の加速度センサはどれもこれより高い解像度を提供しません。 よろしくお願いいたします。 トーマス Re: MMA8652 :  Transient interrupt threshold value <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> トーマス様 お返事ありがとうございます。 > このような設定は何の役に立つのでしょうか? 0.063g 未満の過渡現象を検出したいと思います。 よろしくお願いします、 坂上公一 Re: MMA8652 : Transient interrupt threshold value <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 光一様 このような設定は何の役に立つのでしょうか?加速度が 0g を超えると割り込みが発生します。 よろしくお願いいたします。 トーマス
View full article
What is the MMA7456L WHO_AM_I register value? The data sheet doesn't describe this register. Thanks! Accelerometers Re: What is the MMA7456L WHO_AM_I register value? Hi Martin, Let me explain the history of the MMA745xL. Seven years ago, the original MMA7455L was improved resulting in tighter offset specification tolerances and better TCO and TCS performance (see PCN13436). This improved version got a new number - MMA7456L. However, our marketing department decided to cancel this part number and maintain the MMA7455L. All MMA7455L products shipped from Oct 30, 2008 and later are the improved versions. Let me know if you have any other questions. Regards, Tomas Re: What is the MMA7456L WHO_AM_I register value? So that's the same as for MMA7455L. What's the difference between the two? Thanks a lot! Re: What is the MMA7456L WHO_AM_I register value? Hi Martin, The content of the Who_Am_I register (0x0F) is 0x55. Regards, Tomas PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.
View full article
MMA7456L WHO_AM_I レジスタ値は何ですか? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> データシートではこのレジスタについては説明されていません。ありがとう! 加速度センサ Re: What is the MMA7456L WHO_AM_I register value? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、マーティン。 MMA745xLの歴史についてご説明いたします。7 年前、オリジナルの MMA7455L が改良され、オフセット仕様の許容範囲が狭くなり、TCO と TCS のパフォーマンスが向上しました ( PCN13436 を参照)。この改良バージョンには新しい番号 MMA7456L が付けられました。しかし、当社のマーケティング部門はこの部品番号をキャンセルし、MMA7455L を維持することを決定しました。2008年10月30日以降に出荷されたMMA7455L製品はすべて改良版です。 他にご質問がございましたらお知らせください。 よろしくお願いいたします。 トーマス Re: What is the MMA7456L WHO_AM_I register value? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> つまり、MMA7455L の場合と同じです。この2つの違いは何でしょうか?どうもありがとう! Re: What is the MMA7456L WHO_AM_I register value? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、マーティン。 Who_Am_Iレジスタ(0x0F)の内容は0x55です。 よろしくお願いいたします。 トーマス 追伸: 私の回答が質問の解決に役立った場合は、「正解」とマークしてください。ありがとう。
View full article
RFなしでFRDM-KW01評価ボードを使用してFXTH87からデータを取得しますか? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは。私は MCU プログラミングの初心者ですが、RF なしで FRDM-KW019032 を搭載した FXTH87 評価ボードからデータを取得できるかどうかを知りたいです。可能であれば、従うべき文書はありますか?どうすれば管理できますか?すべての例は、RF を使用してデータを取得することについてです。 アテシュ Re: Get data from FXTH87 with FRDM-KW01 evaluation board without RF? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、アテシュさん FXTH87 にはハードウェア SPI または C ブロックがないため、FXTH87 はソフトウェア SPI またはソフトウェア IIC を使用して別の MCU に情報を転送できます。 圧力/温度測定と SPI/IIC 転送をトリガーする方法はいくつかあります。たとえば、FXTH PWU ブロックを使用して定期的なウェイクアップによってトリガーしたり、FXTH GPIO の割り込みをトリガーする外部信号 (FXTH87 の KBI ブロックを使用) によってトリガーしたりできます。ただし、現在これを説明するコード例やドキュメントは存在しません。 よろしくお願いいたします。 トーマス
View full article
MPX5700 安装时的最高温度 关于 MPX5700 传感器在焊炉中能承受的最高温度是多少? 我想将一块印刷电路板在 240°C 下烘烤 60 分钟。 这会损坏传感器吗? 数据表显示,它支持最高 125°C 的工作温度,我只是想在高温下焊接它,但使用温度不会太高。 Re: MPX5700 maximum temperature for mounting 谢谢 Tomas! Re: MPX5700 maximum temperature for mounting 你好,若昂、 正如您在本网站或AN3150 中看到的,MPX5700 在高于 220°C 的温度下暴露的时间不应超过 30 秒。 顺祝商祺! 托马斯
View full article
MPL3115 altitude accuracy over temperature Hi, I'm planning to use the MPL3115A2 in a low temperature environment(-20~30 degrees C) and wanted to know the accuracy of the altimeter under such conditions. Is the 0.3m accuracy still valid? Any caveats I should be aware of? Pressure Sensors Re: MPL3115 altitude accuracy over temperature Hi Sree, Please distinguish between accuracy and resolution. 0.3m is resolution the MPL3115A2 can achieve when using maximum oversampling (OS[2:0] = 0b111). This is valid over the whole operating temp range. However, accuracy will likely be worse than the one specified in the datasheet (±0.4kPa).  Best regards, Tomas
View full article
MPX2300DT1 的保质期 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好。我们使用的是 MPX2300DT1。是否知道保质期(限制)?尤其是凝胶涂层是否容易老化?预先表示感谢。 压力传感器 Re: shelf life of MPX2300DT1 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,马蒂斯、 恩智浦无法承诺其压力传感器的使用寿命,而使用寿命与传感器的工作环境和使用情况有关。 我们不建议所有传感器直接接触任何种类的液体物质或腐蚀性气体,否则会损坏凝胶体并导致传感器超出规格。 应变片和用于校准和补偿的电子电路受氮化物层保护,但为了使粘接可行,在引线框和应变片之间提供电气连接的铝粘合焊盘没有受到保护。整个模具还受到硅胶的保护。虽然我们在新型压力传感器中使用了更好的凝胶体,但这种凝胶体并非完全密封,水或任何其他流体都可以穿透凝胶体到达模具。 例如,当传感器芯片与水接触时,传感器一偏置,Al/Al3+ 和水之间就开始发生氧还原反应。经过几个小时甚至几天的工作后,电源引脚的铝垫肯定会被破坏,这样 Vcc 引脚上就会出现开路。这是一种铝腐蚀现象。但关闭传感器电源电压后,腐蚀现象就会停止。还有一些其他故障原因,如电偶腐蚀,但这些其他原因造成的平均故障时间(MTTF)比 Vcc 焊盘电腐蚀造成的平均故障时间(MTTF)要长得多。因此,电腐蚀是主要的故障原因,而且是永久性的。 然而,正如您可能知道的那样,我们的产品用于洗衣机,这将使凝胶暴露在潮湿的环境中。在这些应用中,该设备位于测量管的顶部,因此水位是通过将捕获的气柱推向传感器的水来间接测量的。如图所示,传感器与水没有直接接触,而是被空气柱隔开。 如果它们对你有用,我想参考以下应用笔记: AN1950:水位监测 AN1516:使用压力传感器进行液位控制 我们还有关于媒体兼容性的应用笔记: AN3728:IPS PRT 压力传感器的介质兼容性 希望这些信息对你有用。 如果我误解了你的问题,请随时告诉我。 我很乐意提供帮助。 祝您有美好的一天。 戴维-迪亚兹 PS:如果我的回答有助于解决您的问题,请标记为"正确" 。谢谢。
View full article
MPX2300DT1の保管寿命 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは。MPX2300DT1を使用しています。保存期間(制限)について何か分かっていますか?特にゲルコーティングは経年劣化しやすいのでしょうか?前もって感謝します。 圧力センサ Re: shelf life of MPX2300DT1 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、マティスさん。 NXP は、圧力センサの寿命について確約することはできません。寿命は、センサの動作環境と使用方法に関係します。 当社のセンサは、ゲルを損傷し、センサの仕様外となる可能性があるため、いかなる種類の液体物質や腐食性ガスとも直接接触することは推奨しません。 ひずみゲージと較正および補正用の電子回路は窒化物層で保護されていますが、リードフレームとゲージ間の電気的接続を提供するアルミニウム接合パッドは、接合を可能にするために保護されていません。完成したダイもシリコンゲルで保護されています。このゲルは完全に密閉されているわけではありません。新しいタイプの圧力センサにはより高品質なゲルを使用していますが、水やその他の液体がゲルを浸透してダイに到達する可能性があります。 たとえば、センサーダイが水と接触すると、センサーにバイアスが加わるとすぐに、Al/Al3+ と水の間の酸化還元反応が始まります。数時間または数日の作業後、電源ピンのアルミニウム パッドが確実に破壊され、Vcc ピンにオープン サーキットが発生します。これはアルミニウムの腐食現象です。しかし、センサーの供給電圧をオフにすると腐食現象は停止します。ガルバニック腐食など、他の故障原因もありますが、これらの他の原因による平均故障時間 (MTTF) は、Vcc パッドの電気腐食による MTTF よりもはるかに長くなります。したがって、電気腐食が主な故障原因であり、その故障は永久的です。 しかし、ご存知のとおり、当社の製品は洗濯機アプリケーションに使用され、ジェルが湿気の多い環境にさらされることになります。これらのアプリケーションでは、デバイスは測定チューブの上部に配置されているため、閉じ込められた空気柱をセンサーまで押し上げる水を通じて水位が間接的に測定されます。ご覧のとおり、センサーは水と直接接触せず、空気柱によって分離されています。 ご参考になれば幸いです。以下のアプリケーションノートをご参照ください。 AN1950: 水位監視 AN1516: 圧力センサを使用した液面制御 メディアの互換性に関するアプリケーションノートも用意しています。 AN3728: IPS PRT圧力センサーのメディア互換性 この情報が皆様のお役に立てれば幸いです。 ご質問を誤解していた場合は、遠慮なくお知らせください。喜んでお手伝いさせていただきます。 素晴らしい一日をお過ごしください。 デビッド・ディアス。 追伸: 私の回答が質問の解決に役立った場合は、「正解」とマークしてください。ありがとう。
View full article
MPX4250用ゴム配管サイズ こんにちは。MPX4250に適したゴム配管のサイズを教えてください。 Re: Rubber piping size for MPX4250 こんにちは、ヨゼフ わかりました。ありがとうございます。 Re: Rubber piping size for MPX4250 こんにちは、ジェリー。 ホースのサイズと推奨材質については、 AN936の「利用可能なパッケージ」セクションを参照してください。 敬具、 ヨゼフ
View full article
如何使用 FRDM-K-22F 的板载加速度计? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我使用的是 FRDM-K22-F .it有板载加速度计 FXOS8700CQ。我想用它来读取我的应用程序中的 x、y、z 轴信息。如果有人做过请帮我... 加速度传感器 传感平台 Re: How to use on-board Accelerometer of FRDM-K-22F ? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,贾吉尔 请查看 FRDM-K22F-QSP 快速入门软件包示例,该示例可在以下网址找到: frdm-k22f|自由开发板|Kinetis|飞思卡尔 此致, 戴维
View full article
MPXV7025圧力トランスデューサーを使用します。ダイをより良く保護するために、ダイの圧力側と通気側の両方にシリコンゲルを塗布することはできますか? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> MPXV7025圧力トランスデューサーを使用します。ダイをより良く保護するために、ダイの圧力側と通気側の両方にシリコンゲルを塗布することはできますか? Re: We use the MPXV7025 pressure transducer. Can we get silicone gell on both the pressure and vent side fo the die for better protection of the die? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、 はい、デバイスの圧力側と通気側の両方にシリコンゲルを追加して、保護を強化することができます。圧力ポート (ポート P1) にはすでにジェル (デバイスのバージョンに応じてフルオロシリコーン ジェルまたは「耐媒体ジェル」) が含まれていますが、通気側 (ポート P2) にはジェルが含まれていないことに注意してください。 シリコングリースの充填は気泡を避けるために真空状態で行われます。通常、グリースによって機械的ストレスが生じ、オフセット値が変化する可能性があるため、オフセット調整が必要になります。 シリコングリースのサプライヤーとして Gelest をお勧めします。 ゲレスト株式会社 イースト・スティール・ロード11番地 ペンシルベニア州モリスビル 19067 (215)5 47-1015 http://www.gelest.com 代わりに MPXV7025DP 圧力センサを使用することをお勧めします。このデバイスは同じファミリの一部であり、このファミリの他の圧力センサとまったく同じように動作しますが、大きな違いは両方のポートがすでに「フルオロシリコーン ゲル」で満たされていることです。そのため、湿度の高い環境で使用しない場合は、このバージョンのデバイスを使用しても変更は必要ありません。 NXP 圧力センサは、クリーンでない乾燥空気環境で使用することは推奨されません。使用すると保証が無効になります。 すてきな一日を、 ホセ ----------------------------------------------------------------------------------------------------------------------- 注: この投稿で質問が解決した場合は、「正解」ボタンをクリックしてください。ありがとう! -----------------------------------------------------------------------------------------------------------------------
View full article
压差传感器适用于柴油还是石油燃料介质? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我正试图开发一个油位监测数据采集系统,因此我选择了 MPX2053 和类似的传感器,用于测量油箱中最多 4 米的油位高度。 我想知道的是,这些压差传感器是否适用于柴油和/或石油燃料? 如果没有,您能否建议我在应用中可以使用哪些替代传感器或方法? 一种选择是使用基于不锈钢的差压发射器(4 至 20 mA 输出)并将其连接到我的系统。这是一个现成的解决方案,但与基于离散传感器的系统相比,成本非常高。因此,我更倾向于使用恩智浦/飞思卡尔的传感器,因为我以前在不同的应用中使用过同样的传感器。 谢谢! 此致, Zeeshan 压力传感器 Re: Are the differential pressure sensors suited to be used with diesel or petro fuel mediums ? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,齐斯汉 请注意,对于所有恩智浦标准压力传感器产品,除干燥空气外的任何环境都会对产品的可靠性和使用寿命产生一定影响。恩智浦硅压力传感器与油、气、汽油、水或水蒸汽或化学品不兼容。 必须确定这种影响是否可以接受。这就意味着不能将我们的压力传感器用于可能与上述介质直接接触的应用中。工作一段时间后,设备可能会出现故障。 除了提供的信息和解决方案外,我想参考以下值得考虑的**应用笔记**: 1.AN3728:IPS PRT 压力传感器的介质兼容性 2.AN1516:使用压力传感器进行液位控制 3.AN1950:水位监测 希望这些信息对你有用。 如果我误解了你的问题,请随时告诉我。 我很乐意提供帮助。 祝您有美好的一天。 戴维-迪亚兹 PS:如果我的回答有助于解决您的问题,请标记为"正确" 。谢谢。
View full article
用于 MPX4250 的橡胶管尺寸 您好,我想问一下 MPX4250 适合哪种尺寸的橡胶管? Re: Rubber piping size for MPX4250 hi Jozef 好的,谢谢。 Re: Rubber piping size for MPX4250 嗨,杰瑞、 有关软管尺寸和推荐材料,请参阅 AN936 中的 " 可用包装 " 部分。 致以最崇高的敬意 约瑟夫
View full article
Rubber piping size for MPX4250 hi  , i want to ask  which  rubber piping size  is suitable for   MPX4250 Re: Rubber piping size for MPX4250 hi Jozef            All right  ,thanks. Re: Rubber piping size for MPX4250 Hi Jerry, for the hose size and recommended material, please refer to the section "Available Packages" in the AN936. With Best Regards, Jozef
View full article