Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
RFID Tag wrong datasheet We want to use SL3S1013FTB0,115 tag in our product. However, when we click to open the data sheet, it opens SL3S1003_1013's datasheet. It's so confusing, and I wasted a lot of time with this confusion. My question is whether SL3S1013FTB0 and SL3S1003_1013 are the same? If yes, why have two different part numbers for a single part? It's really frustrating and a waste of time for us. i Re: RFID Tag wrong datasheet The IC type is different. In the Chapter 4 Ordering Information,  you can see the SL3S1013 is G2iM+. The SL3S1003 is G2iM. Re: RFID Tag wrong datasheet We want to use SL3S1013FTB0,115 tag in our product. However, when we click to open the data sheet, it opens SL3S1003_1013's datasheet.  You are the different part and ask me to refer to 4. So what is the difference between SL3S1013FTB0,115 and SL3S1003_1013? Only packaging?  Re: RFID Tag wrong datasheet SL3S1003_1013 is the name of the datasheet. It means it is the datasheet of  SL3S1003 and  SL3S1013.  The SL3S1013 is G2iM+. The SL3S1003 is G2iM.  The UCODE G2iM+ offers on top of the UCODE G2iM features an integrated tag tamper alarm, digital switch, external supply mode, data transfer mode and real read range reduction. A special feature is the conditional, automatic real read range reduction, where the activation condition can be defined by the user, is newly introduced in the UCODE G2iM+. When connected to a power supply, the READ as well as the WRITE range can be boosted to a sensitivity of -27 dBm. The UCODE G2iM+ also allows the segmentation of the 640 bit User Memory in up to three segments (open, protected, private) with different access levels (Access- and User Password). For applications which require a longer EPC number the UCODE G2iM+ offers the possibility of up to 448 bit. Re: RFID Tag wrong datasheet My questions are as follows: Your comment: A special feature is the conditional, automatic real read range reduction, where the activation condition can be defined by the user, is newly introduced in the UCODE G2iM+. My question: How can we reduce the UCODE G2iM+ read range? I’m asking this because there are no serial communication lines available to connect to the MCU, so I don’t know how we can control the read range. Your comment: When connected to a power supply, the READ as well as the WRITE range can be boosted to a sensitivity of -27 dBm. My question: I have attached the pinouts and connections of UCODE G2iM+. How this read and write is done? Is it through the RFID connection? The UCODE G2iM+ offers on top of the UCODE G2iM features an integrated tag tamper alarm, digital switch, external supply mode, data transfer mode and real read range reduction. My question: can you please explain integrated tag tamper alarm, digital switch, external supply mode, data transfer mode, and real read range reduction modes? The reason is that I would like to see how I can utilize those features in my product. My question: Please see the attached picture. The self-powered RFID transponder connection. Please let me know if this connection will result in 2V to 5V Vout from RFID energy harvesting. Re: RFID Tag wrong datasheet im still waiting for an answer. NXP should know how to use their product, and that's what I want to know. I have two more questions. 1) In a self-power RFID transponder, what is the voltage range at the OUT?  2) In an external-power RFID transponder, what is the voltage range at the OUT?  Re: RFID Tag wrong datasheet im still waiting for an answer. NXP should know how to use their product, and that's what I want to know. i have two more questions. 1) In a self-power RFID transponder, what is the voltage range at the OUT?  2) In an external-power RFID transponder, what is the voltage range at the OUT? 
查看全文
Iterfacing HDMI-CSI convertor module TC358743 with i.MX8MP- FRDM board I am trying to interface HDMI to CSI2 convertor module from waveshare based on Toshiba IC TC358743. I am using yocto project to build image $ DISTRO=fsl-imx-wayland MACHINE=imx8mp-lpddr4-frdm source imx-setup-release.sh -b frdm_sources_whinlatter and i have selected the driver using this command bitbake -c menuconfig /virtual/kernel and it is reflecting in the .config file also CONFIG_VIDEO_TC358743=y CONFIG_VIDEO_TC358743_CEC=y and i have modified the dts file accordingly here i am attaching the dts file for your reference. But i couldnt able to communicate with the IC even for i2cdetect -y 1 it is not locking (UU) to 0x0F address. but i can able to see the device address in i2c1. What i am missing in dts file or in driver selection? Linux Multimedia Yocto Project Re: Iterfacing HDMI-CSI convertor module TC358743 with i.MX8MP- FRDM board we don't have official verified code for this, the link I sent to you shared the dts settings, you can compare with your own, to check if you miss something Re: Iterfacing HDMI-CSI convertor module TC358743 with i.MX8MP- FRDM board Getting page not found error for the solution mentioned in this query. Is there any official support page to resolve this query? Re: Iterfacing HDMI-CSI convertor module TC358743 with i.MX8MP- FRDM board pls refer to the link as below, to check if you set correctly or not https://community.nxp.com/t5/i-MX-Processors/i-MX8MP-%E7%A7%BB%E6%A4%8Dtc358743%E5%88%86%E8%BE%A8%E7%8E%87%E8%B0%83%E6%95%B4%E9%97%AE%E9%A2%98/m-p/1631189 Re: Iterfacing HDMI-CSI convertor module TC358743 with i.MX8MP- FRDM board This Issue is resolved but i am facing one more regarding video pipeline from CSI2 to HDMI using Gstremer, i couldnt able to understand whether its the dts issue or something else. here i am attaching response log from the device for your reference. and the dts file, root@imx8mp-lpddr4-frdm:~# i2cdetect -y 1 0 1 2 3 4 5 6 7 8 9 a b c d e f 00: -- -- -- -- -- -- -- UU 10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- 50: -- -- -- UU -- -- -- -- -- -- -- -- -- -- -- -- 60: -- -- -- -- -- -- -- -- 68 -- -- -- -- -- -- -- 70: -- -- -- -- -- -- -- -- root@imx8mp-lpddr4-frdm:~# v4l2-ctl --list-devices (): /dev/v4l-subdev0 FSL Capture Media Device (platform:32c00000.bus:camera): /dev/media0 mxc-isi_v1 (platform:32e00000.isi:cap_devic): /dev/video3 mxc-isi-m2m_v1 (platform:32e00000.isi:m2m_devic): /dev/video2 vsi_v4l2dec (platform:vsi_v4l2dec): /dev/video1 vsi_v4l2enc (platform:vsi_v4l2enc): /dev/video0 root@imx8mp-lpddr4-frdm:~# v4l2-ctl -d /dev/v4l-subdev1 --query-dv-timings Active width: 1280 Active height: 720 Total width: 1650 Total height: 750 Frame format: progressive Polarities: -vsync -hsync Pixelclock: 74250000 Hz (60.00 frames per second) Horizontal frontporch: 0 Horizontal sync: 370 Horizontal backporch: 0 Vertical frontporch: 0 Vertical sync: 30 Vertical backporch: 0 Standards: Flags: root@imx8mp-lpddr4-frdm:~# v4l2-ctl -d /dev/v4l-subdev1 --set-dv-bt-timings query BT timings set root@imx8mp-lpddr4-frdm:~# media-ctl -p Media controller API version 6.18.2 Media device information ------------------------ driver mxc-md model FSL Capture Media Device serial bus info platform:32c00000.bus:camera hw revision 0x0 driver version 6.18.2 Device topology - entity 1: mxc_isi.0 (16 pads, 2 links, 0 routes) type V4L2 subdev subtype Unknown flags 0 pad0: SINK <- "mxc-mipi-csi2.0":4 [ENABLED] pad1: SINK pad2: SINK pad3: SINK pad4: SINK pad5: SINK pad6: SINK pad7: SINK pad8: SINK pad9: SINK pad10: SINK pad11: SINK pad12: SOURCE -> "mxc_isi.0.capture":0 [ENABLED] pad13: SOURCE pad14: SOURCE pad15: SINK - entity 18: mxc_isi.0.capture (1 pad, 1 link) type Node subtype V4L flags 0 device node name /dev/video3 pad0: SINK <- "mxc_isi.0":12 [ENABLED] - entity 22: mxc-mipi-csi2.0 (8 pads, 2 links) type Node subtype V4L flags 0 device node name /dev/v4l-subdev0 pad0: SINK <- "tc358743 1-000f":0 [ENABLED,IMMUTABLE] pad1: SINK pad2: SINK pad3: SINK pad4: SOURCE -> "mxc_isi.0":0 [ENABLED] pad5: SOURCE pad6: SOURCE pad7: SOURCE - entity 31: tc358743 1-000f (1 pad, 1 link, 0 routes) type V4L2 subdev subtype Unknown flags 0 device node name /dev/v4l-subdev1 pad0: SOURCE [stream:0 fmt:RGB888_1X24/1280x720 field:none colorspace:srgb] [dv.caps:BT.656/1120 min:640x350@13000000 max:1920x1200@165000000 stds:CEA-861,DMT,CVT,GTF caps:progressive,reduced- blanking,custom] [dv.detect:BT.656/1120 1280x720p60 (1650x750) stds: flags:] [dv.current:BT.656/1120 1280x720p60 (1650x750) stds: flags:] -> "mxc-mipi-csi2.0":0 [ENABLED,IMMUTABLE] root@imx8mp-lpddr4-frdm:~# gst-launch-1.0 v4l2src device=/dev/video3 num-buffers=10 ! \ > video/x-raw,format=YUY2,width=1920,height=1080,framerate=60/1 ! \ > fakesink Setting pipeline to PAUSED ... Pipeline is live and does not need PREROLL ... Pipeline is PREROLLED ... Setting pipeline to PLAYING ... New clock: GstSystemClock ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Failed to allocate required memory. Additional debug info: /usr/src/debug/gstreamer1.0-plugins-good/1.26.6.imx/sys/v4l2/gstv4l2src.c(957): gst_v4l2src_decide_allocation (): /GstPipeline:pipel ine0/GstV4l2Src:v4l2src0: Buffer pool activation failed Execution ended after 0:00:00.025120625 Setting pipeline to NULL ... ERROR: from element /GstPipeline:pipeline0/GstV4l2Src:v4l2src0: Internal data stream error. Additional debug info: /usr/src/debug/gstreamer1.0/1.26.6.imx/libs/gst/base/gstbasesrc.c(3187): gst_base_src_loop (): /GstPipeline:pipeline0/GstV4l2Src:v4l 2src0: streaming stopped, reason not-negotiated (-4) Freeing pipeline ... and i am not seeing anything on external display also (Connected over HDMI) Re: Iterfacing HDMI-CSI convertor module TC358743 with i.MX8MP- FRDM board pls refer to the chapter 7.3.9 Camera preview of linux user guide, you need to use media-ctl to create a connection https://www.nxp.com/docs/en/user-guide/UG10163.pdf
查看全文
PN7462 GPIO出力読み取りの問題(phhalPcr_GetGpioVal()使用時) チームの皆さん、こんにちは。 私はPN7462を使用しており、phhalPcr_GetGpioVal()を使用して出力として構成されたLED GPIOピンを読み取ろうとしています。 uint8_t val = 0; phhalPcr_GetGpioVal(LED_RED, &val); しかし、LED出力がHIGHの場合でも、APIは常に0を返します。 phhalPcr_GetGpioVal() は入力パッドの状態を読み取るだけの関数ですか? PN7462の出力GPIOピンの状態や出力ラッチ値を読み取るための他のAPIはありますか? よろしくお願いいたします。 開発ボード Re: PN7462 GPIO Output Read Issue Using phhalPcr_GetGpioVal() こんにちは、 @uday_gowda さん PN7642_MCUXpresso_SDK_02-15-006_PUB\boards\pnev7642fama\driver_examples\gpt の例を参照してください。そこにあなたが求めている答えがあります。 Re: PN7462 GPIO Output Read Issue Using phhalPcr_GetGpioVal() 参考資料をありがとうございます。 私はSDK NxpNfcRdLib_PN7462_v07.14.00_Pubを使用してPN7462AUを使用しています。 提示されたサンプル領域を確認しましたが、そこにもLEDに対するGPIO書き込み操作しかなく、GPIO出力読み出し操作は見当たりませんでした。 PN7462の出力GPIOの状態を読み取るためのAPIが存在するかどうか確認していただけますか? Re: PN7462 GPIO Output Read Issue Using phhalPcr_GetGpioVal() こんにちは、 @uday_gowda さん 次のような方法を試してみてはいかがでしょうか。
查看全文
RDDRONE-BMS772开发板 我想知道如果利用这个板子进行电池的测试实验时,能不能设计电池的充放电工况,比如恒流恒压充电或者HPPC、UDDS等动态工况。 Re: RDDRONE-BMS772开发板 那个是charger里面检测设置的不是BMS这边的功能
查看全文
MCXW236BIHNARチップ電源設計 こんにちは、NXPさん。 MCXW236BIHNARの電源設計回路図を添付しました。設計が適切で、チップが正常に動作するのに十分かどうか、ご確認いただけますでしょうか? よろしくお願いします、 シャキール・サラム ボード設計
查看全文
バカラで本当に勝者は多いのでしょうか?カスタマーサービス(15708835568)までお問い合わせください。
查看全文
AI音声認識とオンデバイスLLMは、組み込みシステムにおける次の大きな変革となるのか? 近年のデバイス内AIやリアルタイム音声インターフェースへの取り組みの高まりにより、私たちは生成型AIの新たな段階、つまりクラウドへの依存度が低く、エッジネイティブな段階に入りつつあるように感じられます。 最近私が気づいたいくつかの傾向: デバイス内LLM(プライバシー保護と低レイテンシ)への需要の高まり AI音声エージェントの台頭により、従来のUIフローが置き換えられつつある。 組み込みハードウェア向け効率的なモデル最適化(量子化、蒸留)への注力 インダストリアルおよびオートモーティブ用途向けのオフライン対応AIシステムへの関心の高まり これは興味深い疑問を提起する。 👉 私たちは、APIに頼るのではなく、すべてのデバイスが独自の「ローカルAIブレイン」を持つ未来に向かっているのだろうか? 開発の観点から見ると、この変化は些細なことではない。これには以下が含まれます。 パフォーマンスを損なうことなくモデルを圧縮する ハードウェアを考慮したAIアーキテクチャ設計 エッジとクラウドのインテリジェンスのシームレスな統合 私は生成型AI開発サービス、特に実世界での展開(デモだけでなく)に最適化されたカスタムAIモデルの構築に深く携わってきましたが、私が考える最大の課題はモデルを構築することではなく、それを本番環境で使いやすく、効率的で、拡張性のあるものにすることです。 このコミュニティの皆さんの意見を聞きたいです。 デバイス上のLLMやエッジAIを試していますか? これまでで最大のボトルネックは何でしたか?パフォーマンス、コスト、それともシステム統合でしょうか? クラウドベースのGenAIが今後も主流であり続けると思いますか、それともエッジコンピューティングが取って代わると思いますか? ぜひ意見交換や実体験を共有したいです。
查看全文
IPTVGreatが2026年最高のIPTVである理由とは? 2026年最高のIPTVをお探しですか?IPTVGreatは、14万以上のライブTVチャネルと10万以上の映画やシリーズを素晴らしい4K品質で提供するプレミアムな選択肢として際立っています。7年以上にわたる信頼の実績を持つこの製品は、高度なフリーズ防止技術によって、スムーズでバッファリングのないストリーミング体験を提供します。 ライブスポーツやPPVイベントから、Netflixスタイルの番組、70カ国以上からの国際チャンネルまで、IPTVGreatは手頃な価格のサブスクリプションで全てを提供します。スマートテレビ、Android、iOS、Firestick、PCなど、あらゆるデバイスで動作します。 信頼性、豊富なコンテンツ、そして最高のパフォーマンスを求めるなら、IPTVGreatは2026年のベストIPTVの有力候補です。 アクセス先: https://iptvgreat.store/ Re: Why is IPTVGreat the Best IPTV 2026? IPTVGreatは、 14万以上のライブチャネル、 10万以上の4K映画とシリーズ、そして7年以上の信頼できるサービスを提供し、 2026年のベストIPTVとして有力な選択肢です。凍結防止テクノロジにより、スマートテレビ、Firestick、Android、iOS、PCなど、あらゆるデバイスでスムーズでバッファリングのないストリーミングを実現します。スポーツ、映画、そして世界のエンターテイメントを一つのサブスクリプションで楽しめる、確かな選択肢です。 👉 IPTVGreat をご覧ください Re: Why is IPTVGreat the Best IPTV 2026? 🚀 2026年最高のIPTVをお探しですか?IPTVGreatは、14万以上のライブTVチャンネル、10万以上の映画やシリーズ、そしてパワフルな4K画質で、素晴らしいストリーミング体験を提供します。ライブスポーツやPPVイベントから国際的なエンターテイメントまで、すべてが手頃な価格のIPTVサブスクリプションで利用可能です。 バッファリングが一切なく、あらゆるデバイスにサポートしているIPTVGreatは、世界中のIPTVユーザーにとって人気の選択肢になりつつあります。 🔥📺 🌐 アクセス先: https://iptvgreat.store/ Re: Why is IPTVGreat the Best IPTV 2026? 🔥 IPTVGreatは、2026年のベストIPTVの有力候補の一つであることは間違いありません!14万以上のライブチャネル、10万以上の映画やシリーズ、そして非常にスムーズな4Kストリーミングを備えたこのサービスは、世界中のスポーツファンやエンターテイメント愛好家にとって最適な選択肢です。 ⚽📺 バッファリングが全く発生しないパフォーマンスと膨大な国際コンテンツライブラリにより、IPTVGreatは他のIPTVプロバイダーとは一線を画しています。2026年にプレミアムIPTVサービスを探している人にとって、間違いなくチェックする価値のあるサービスです。 🌐 今すぐアクセス: https://iptvgreat.store/
查看全文
ライノス - 発売日は? こんにちは、Yoctoの新しいリリースが間もなく登場しますが、wrynoseをサポートするmeta-qoriq BSPはいつ頃リリースされる予定ですか?コードベースを凍結する前に、新しいリリースに切り替えられるかどうかを計画する必要があります。 Re: Wrynose - relase date? こんにちは、 NXPは 現在、 yocto - sdk マニフェスト での meta-qoriqの 使用 を含め 、 Layerscape/QorIQ ワークフロー 向けの Kirkstone 、 Mickledore 、 Scarthgap などの リリース を 文書化/サポートしています 。 NXPは 、 一部 のコンポーネントの アップグレード に関して 、 リリース 予定日 が 確定し た 際に、 その 旨 を 公表すること があり ます 。例えば 、 meta-qoriq の ATF アップデートは 6.12.20-2.0.0-25Q2 に 予定されて いる と 記載され ています 。 したがって、 計画 に関する 回答 は 、 meta-qoriq BSP の Wrynose サポート に関する 検証済みの 公開 スケジュール は あり ませ ん 。コード凍結の 決定が その サポート の 実装 に 依存する 場合 、 入手可能な ドキュメント では 、 それが 予定通り に 利用可能 に なる と想定すること は でき ません。 よろしくお願いします。   よろしくお願いします。
查看全文
ThriveCartクーポンコード(44%オフ)$550生涯割引 Thrivecartの割引で44%オフをゲットしよう ThriveCartの 購入をお得にするため の有効なクーポンコードをお探しですか ?まさにぴったりの場所です。ThriveCartは、 生涯利用権 を提供する数少ないSaaSツールの1つです。 つまり、一度購入すれば、月額料金なしで永久に利用できます。 ThriveCart Proの永久ライセンスが75%オフ! ThriveCart Proプランが75%オフ!しかも永久アクセス権付き。他のプラットフォームで月額料金を払い続けるよりも、このお得なプランなら初期費用を大幅に節約できます。アフィリエイトトラッキング、アップセル、バンプオファー、カスタムチェックアウトページといった高度な機能を、月額料金なしで永久にご利用いただけます。 ThriveCartの500ドル割引プロモーションコード 新規ユーザーは、このオファーを利用することで、ThriveCartのスタンダードパッケージを500ドル割引で利用できます。このプランでは、モバイルフレンドリーなペイメント機能や30種類以上のペイメントシステムとの連携機能を維持しつつ、初期費用を大幅に削減できます。 ThriveCartの50%オフクーポンコード(プロアカウント限定) ThriveCart Proアカウントを50%割引で入手し、月額料金なしで生涯アクセス権を一度支払うだけで、無制限の商品、無制限の取引、ワンクリックアップセル、オーダーバンプ、アフィリエイトトラッキング、詳細な売上レポートなどの強力な機能を利用できます。年間料金を請求するプラットフォームと比較して、数百ドルも節約できます。 ThriveCart生涯クーポンコード(プロプラン)(690ドル節約) ThriveCartの生涯クーポンコードを使ってProプランを契約すると、690ドル節約でき、Standardプランのすべての機能に加え、本格的な販売者向けの高度なツールも利用できます。これには、アフィリエイト管理、購読者維持機能、高度な自動化機能、顧客ポータル、そしてコースのホスティングと販売のためのThriveCart Learn+へのフルアクセスが含まれます。これらすべては、一度限りのペイメントで済み、継続的な費用は一切かかりません。これにより、コンバージョン率を高め、プラットフォームのコストを削減し、より多くの利益を確保できます。 ThriveCartプロモーションコード - 495ドル割引 ThriveCartのプロモーションコード(495ドル割引) を利用すれば 、スタンダードプランを1回限りの支払いで入手でき、月額料金が永久に無料になります。このプランには、無制限の商品、販売ファネル、チェックアウトページ、そして生涯無料のアップデートが含まれており、オンライン販売者は通常の価格のほんの一部でフル機能を利用でき、継続的な費用をかけずにビジネスを成長させることができます。 ThriveCartのブラックフライデークーポンで250ドル割引 ThriveCartのブラックフライデー・フラッシュセール期間中は、250ドルの割引が適用され、生涯で最もお得な価格で購入できます。この期間限定のキャンペーンは、メールや提携サイトを通じてよく宣伝されており、販売者は強力な販売ツールへの生涯アクセス権を、継続的な料金なしで取得できます。 ThriveCart ブラックフライデー クーポンコード - 60%オフ ThriveCartのブラックフライデーセール2025期間中は、スタンダードプランとプロプランの両方で最大60%オフとなり、生涯有効な一括ペイメントで、強力なチェックアウトツール、高度なオートメーション、無制限の製品登録、そして販売、定期購入、アフィリエイトマネジメントのすべてに、月額料金なしでアクセスできます。 ThriveCartの30日間無料トライアルオファー ThriveCartは無料トライアルを提供していませんが、30日間の返金保証により、すべての機能をリスクなしで試すことができます。さらに現在、90%オフの割引クーポンを利用すれば、Proプランを最大450ドル節約でき、月額料金なしで生涯フルアクセスが可能になります。 ThriveCart生涯利用プラン – 2026年までのお得な割引(継続料金は一切かかりません) これは、 ThriveCartのクーポンコードの中でも最高の特典です。ThriveCartの永久アクセス権が手に入ります。一度支払えば、ThriveCart Standardを永久に利用できます。月額料金、年間更新料、決済手数料以外の取引ごとの手数料は一切かかりません。 価格設定: ThriveCart スタンダード生涯プラン: 495ドル(一括払い) ThriveCart Pro ライフタイムライセンス(Proアップグレード付き): 690ドル(一括払い) このサービスがお得な理由:同等の機能を備えたSaaS型ショッピングカートツール(SamCart、CartFlows Pro、WooCommerce+拡張機能など)は、年間588ドル~1,188ドルのサブスクリプション料金がかかります。ThriveCartの生涯価格は、3年間で同等のサブスクリプションと比較して1,200ドル~3,000ドル以上節約できます。 ThriveCart Proアップグレードクーポン – フルProバンドルがお得に ThriveCart Proへのアップグレードでは、Standard版に加えて、アフィリエイト管理、クライアント利用権限、売上税の自動計算、インテリジェントな事業予測、カスタムドメインサポートなど、強力な機能が追加されます。Proへのアップグレードは、Standard版の永久ライセンス価格に195ドルを追加することでご利用いただけます。 ThriveCart Proの合計価格:690ドル(一括払い)(スタンダード版495ドル+プロ版195ドル) サブスクリプション型サービスとの比較: ThriveCart Pro(月額690ドル)は、アフィリエイトシステムを備えた同等のサブスクリプション型カートツールと比較して、5年間で2,250ドル~5,250ドルの節約になります。 ThriveCart Learn+ クーポン – コースプラットフォームが無料 ThriveCartには、StandardおよびProの永久ライセンスすべてにThriveCart Learn (フル機能のLMS/コースプラットフォーム)が無料で付属しており、 ThriveCart ProにはThriveCart Learn+ (段階的なコンテンツ配信、コース修了証明書、高度な学生管理などの高度なコース機能)が無料で付属しています。 これにより、実質的にTeachableやKajabiの代替サービスを無料で利用でき、ThriveCartの1回限りの支払いに含まれています。 Learn+の価値:同等のコースプラットフォームは月額39ドル~199ドルです。ThriveCartの生涯契約にLearn+をバンドルすることで、年間500ドル~2,400ドル相当の価値が加わります。 アフィリエイトパートナー経由のThriveCart割引 – 検証済みのボーナス特典 ThriveCartは、従来の割引クーポンコードは提供していません。その代わりに、一部の提携パートナーが、標準の生涯利用料金に加えて、 ThriveCart限定の割引ボーナスを提供しています。これらのボーナスには通常、すぐに使えるファネルテンプレート、マスタークラスへのアクセス、または200ドルから1,000ドル相当の個別オンボーディングコールなどが含まれます。 【期限切れ】ThriveCart ブラックフライデー 2025 – ボーナスバンドルオファー ThriveCartの2025年ブラックフライデーキャンペーンでは、新規の生涯購入者向けに、追加テンプレート、トレーニング、延長サポートアクセスなどの限定ボーナスバンドルが提供されました。標準価格である495ドル/690ドルの生涯利用料は変更ありませんが、ボーナスパッケージは提供されなくなりました。2026年のプレビューについては、下記の季節限定セールセクションをご覧ください。 ThriveCartのクーポンコードを入手する方法は? ThriveCartの割引 を適用して 購入を完了するには、以下の5つの手順に従ってください。 ステップ1:上記で選択した特典の横にある「今すぐ申し込む」ボタンをクリックしてください。これにより、ThriveCartの公式チェックアウトページ、または提携パートナーのチェックアウトページが開きます。このページには、セッションに関連付けられた利用可能なボーナス特典が表示されます。 ステップ2:プランを選択してください。スタンダードプランかプロプランのどちらかです。ThriveCartのチェックアウトページで、スタンダードの永久ライセンス(495ドル)を選択するか、プロプランへのアップグレード(195ドル追加)を選択して、合計690ドルのプロプランバンドルをご利用ください。アフィリエイトマネジメントシステムを使用する場合や、売上税の自動計算が必要な場合は、プロプランへの追加投資に見合う価値があります。 ステップ3:ボーナス特典を確認してください。アフィリエイトパートナーのリンクから購入された場合、関連するボーナスパッケージは購入確認メールに記載されています。チェックアウト後にボーナスを受け取るための手順をご確認ください。 ステップ4:お支払い情報を入力してください。ThriveCartではクレジットカードとPayPalをご利用いただけます。定期的な請求はなく、お支払いは1回限りです。取引を完了する前に、合計金額(495ドルまたは690ドル)が正しいことをご確認ください。 ステップ5:ThriveCartアカウントにアクセスします。購入後数分以内に、ログイン手順が記載されたウェルカムメールが届きます。ThriveCartダッシュボードはすぐに利用可能になります。決済処理業者(Stripe、PayPal、またはApple Pay)を接続し、最初の製品を登録して販売を開始しましょう。 プロからのアドバイス: ThriveCartには無料トライアルはありません。プラットフォームには30日間の返金保証があり、これはリスクなしで評価できる期間として機能します。この期間を利用して、チェックアウトページを完全に設定し、支払いフローをテストし、保証期間が終了する前にThriveCartがビジネスに適していることを確認してください。 2026年におけるThriveCartの料金はいくらですか? 詳細価格比較:ThriveCartとサブスクリプション代替サービス プラットフォーム ThriveCart スタンダード ThriveCart Pro SamCart(スケール) CartFlows Pro カジャビ 価格設定モデル 1回限りの料金495ドル 1回限りの料金690ドル 年間588ドル 年間299ドル 年間1,188ドル 1年目の費用 495ドル 690ドル 588ドル 299ドル 1,188ドル 3年目の費用(合計) 495ドル 690ドル 1,764ドル 897ドル 3,564ドル 5年目の費用(合計) 495ドル 690ドル 2,940ドル 1,495ドル 5,940ドル 生涯節約額 vs SamCart — — 2,445ドル節約できました — — アフィリエイト管理 ✓(プロ) ✓ ✓(スケール) ✗ ✓ コースプラットフォーム ✓ 無料(学習) ✓ 無料(Learn+) ✗ ✗ ✓ 一括ペイメント ✓ ✓ ✗ ✗ ✗ 価格は2026年の料金を反映しています。サブスクリプションプラットフォームの料金は年間請求料金です。 ThriveCart StandardとPro - どちらを選ぶべきか? ThriveCart Standard(495ドルの一括払い)は、チームアフィリエイトプログラムなしでデジタル製品、物理製品、サービス、またはサブスクリプションを販売する個人クリエイターや小規模ビジネスオーナーに最適な選択肢です。無制限の製品、無制限のファネル、A/Bスプリットテスト、ワンクリックアップセル、オーダーバンプ、埋め込み可能なチェックアウト、StripeとPayPalの統合、そしてThriveCart Learn(組み込みのコースプラットフォーム)が含まれています。 ThriveCart Pro(一括払い690ドル - 495ドル + 195ドルのアップグレード)は、以下のような機能が必要な場合に最適な選択肢です。自社製品を宣伝するアフィリエイトを募集・管理するための組み込みアフィリエイトプログラム、自動売上税計算(Taxjarとの連携)、クライアント使用権限(クライアントのビジネスでThriveCartを実行)、インテリジェントなビジネス予測と収益予測、そして、段階的なスケジュール設定、修了証、高度な学生進捗状況追跡などの高度なコース機能を備えたThriveCart Learn+。 結論:ビジネスのどの段階であれアフィリエイトプログラムを構築する予定があるなら、最初からProプランを選ぶべきです。195ドルの追加料金は十分に正当化されます。TapfiliateやRewardfulのような単体のアフィリエイト管理プラットフォームは月額59ドルから199ドルかかるため、Proプランへのアップグレード費用は、別途ツールを用意する必要がなくなることで30日以内に元が取れます。 ThriveCartは学生割引や非営利団体割引を提供していますか? ThriveCartは、正式な学生割引プログラムや非営利団体向けの料金プランを提供していません。しかし、ThriveCartでの購入にかかる実質的なコストを削減する方法はいくつかあります。 生涯契約が実質的な割引: ThriveCartが提供する最大の割引は、495ドルの1回限りの価格設定そのものです。初めてデジタル製品ビジネスや副収入源を構築しようとしている学生にとって、月額料金がかからないということは、ThriveCartが最初の数件の販売が行われた瞬間から手頃な価格になることを意味します。これは、収益に関係なく月額49ドルから99ドルを請求するサブスクリプションプラットフォームとは異なります。 アフィリエイトパートナー特典:認証済みのアフィリエイトパートナー(このページにあるリンクなど)経由で購入すると、テンプレート、トレーニング、コンサルティングなど、200ドルから1,000ドル相当のボーナスパッケージが手に入ることがよくあります。これにより、定価を下げることなく追加価値が提供されるため、実質的なコストを削減できます。 事業経費/税控除:ほとんどの国では、ThriveCartは事業用ソフトウェア経費として認められ、全額税控除の対象となります。自営業のクリエイターや小規模事業主の場合、495ドルのThriveCartライセンスの税引き後費用は、所得税率に応じて300ドルから375ドルになることが多く、学生だけでなく誰にとっても大きな実質的な割引となります。 ThriveCart クーポンコード インド: ThriveCart は世界共通で USD で $495/$690 で販売されています。ThriveCart を購入するインドのユーザーは、このプラットフォームが国際クレジットカード/デビットカードと PayPal に対応していることに注意してください。どちらもインドの銀行で広く利用可能です。為替レートの変動により、USD での定期購読が高額になる可能性があるため、この一括払いモデルはインドの起業家にとって特に有利です。$495 の一括払いにより、将来の USD/INR の変動に関係なく、費用が永久に固定されます。 ThriveCartとは何ですか?2026年時点で、それは価値のあることだろうか? ThriveCartは、デジタル製品クリエイター、コース販売者、コーチ、コンサルタント、オンラインビジネスオーナー向けに特化して構築された、ホスティング型のショッピングカートおよび決済プラットフォームです。ジョシュ・バートレットによって設立され、2016年にサービスを開始したThriveCartは、5万社以上のオンライン販売業者をユーザーベースとして、年間数億ドル規模の売上を処理している。 ShopifyやWooCommerceといった一般的なeコマースプラットフォームは主に実店舗での商品リテール向けに構築されていますが、ThriveCartはコンバージョン率の高いデジタル商品のチェックアウトに特化して設計されています。ワンクリックアップセル、注文特典、定期購入マネジメント、アフィリエイトトラッキング、そしてあらゆるウェブサイト、ランディングページ、ファネルに直接埋め込めるチェックアウトフォームなど、多彩な機能を備えています。 ThriveCartの主な機能は以下のとおりです。 商品数と販売ファネル数は無制限で、決済処理業者の標準料金以外に販売ごとの取引手数料は一切かかりません。決済ページ、見出し、価格設定に関するA/Bテスト。ワンクリックでアップセルとダウンセルが可能。平均注文額を増加させる注文特典。購読およびペイメントプランのマネジメント(督促(自動的なペイメント不履行回収)を含む)。ActiveCampaign、ConvertKit、Drip、Mailchimp、Zapier、Teachable、Thinkific、WordPressなど、30以上のツールと直接連携できます。さらに、ThriveCart Learnコースプラットフォームが内蔵されており、追加費用なしでフル機能のLMS(学習管理システム)を利用できます。 ThriveCartは以下のような方に最適です。 ThriveCartは、コース、電子書籍、会員制サービス、テンプレート、ソフトウェア、コーチングプログラム、代行サービスなどを販売するデジタル製品クリエイターにとって最適なプラットフォームです。これは、毎月のSaaS料金の支払いにうんざりしていて、カートのインフラストラクチャを完全に所有したいと考えているクリエイターに特に適しています。ThriveCart Proのアフィリエイト管理システムは、製品ローンチとパートナー主導の販売のためのワンストップソリューションを提供します。 ThriveCartの欠点: ThriveCartは、大型の物理製品のeコマースには最適ではありません。在庫管理、配送連携、複数SKUの小売においては、Shopifyの方が優れたツールです。ThriveCartのダッシュボードデザインは機能的ではあるものの、SamCartのような新しい競合製品と比べると、視覚的な洗練度は劣る。また、無料トライアルがないため、新規ユーザーは30日間の返金期間を利用して自分に合うかどうかを判断しなければなりません。これは寛大な措置ではありますが、無料プランを提供しているプラットフォームと比べると、わずかながら不便さを感じる点です。 2026年になっても、それだけの価値はあるのだろうか? 12か月以上オンラインで販売を計画しているデジタル製品クリエイターにとって、495ドル~690ドルの買い切り価格のThriveCartは、SamCart(年間588ドル以上)、Kajabi(年間1,188ドル以上)、あるいはカート、アフィリエイトシステム、コースプラットフォームを個別に構築した場合の合計コストと比較すると、ほぼ間違いなく価値があります。計算は簡単です。同等の機能を備えたサブスクリプション型の代替サービスと比較すると、生涯契約は初年度で元が取れます。ThriveCartの生涯クーポンを現在の価格で入手すれば、将来の値上げから永久に保護されます。 結論:ThriveCartのお得なクーポンコードを入手しよう(2026年版) 現在入手可能なThriveCartの最もお得なクーポンコードは、生涯アクセス権のプランです。スタンダードプランは495ドル、プロプランは690ドルで、月額料金は一切かかりません。デジタル製品クリエイター、コース販売者、オンラインビジネスオーナーにとって、これは2026年に利用できる最も経済的に健全な決済プラットフォームへの投資と言えるでしょう。 ThriveCartと同等の機能を備えたサブスクリプションツールで、3~5年の期間で見てこれより低価格なものはありません。組み込みのアフィリエイトシステム(Pro)、無料コースプラットフォーム(Learn+)、そして取引手数料無料のモデルにより、あらゆる規模のビジネスにおいて魅力的な収益性を実現しています。 初めてのデジタル商品のためのフル機能搭載カートが必要な場合でも、既に確立されたビジネスのための強力なアフィリエイトプラットフォームが必要な場合でも、 ThriveCartの生涯利用プランは、毎月の購読料が一切発生しないため、毎月お得に利用できる割引です。価格が変更される前に、上の「生涯利用権を申し込む」ボタンをクリックして、2026年の価格を確定しましょう。 ThriveCartクーポンコードに関するよくある質問 ThriveCartの495ドルの価格から割引を受けられるクーポンコードはありますか? ThriveCartは、月額制SaaSプラットフォームのように割引率を示すクーポンコードを一般に公開していません。ThriveCart の割引は 、生涯利用料金(Standardプランは495ドル、Proプランは690ドル)そのものによって実現されており、これはサブスクリプション方式の代替サービスと比較して永続的な節約となります。一部のアフィリエイトパートナーは、標準価格に加えてボーナスパッケージ(テンプレート、トレーニング、コンサルティングなど)を提供しており、定価を下げることなく付加価値を高めています。これらのボーナス特典は、 従来の意味での ThriveCartクーポン に最も近いものと言えるでしょう。 ThriveCartは無料トライアルを提供していますか? いいえ。ThriveCartは無料トライアルを提供していません。その代わりに、すべての購入に対して30日間の返金保証が付いています。購入後30日以内に何らかの理由でご満足いただけない場合は、理由を問わず全額返金を請求できます。つまり、購入のリスクは30日間の無料トライアルと同等ですが、支払い情報を事前に入力する必要がある点が異なります。返金手続きを開始するには、購入後30日以内にThriveCartサポートにお問い合わせください。 ThriveCart StandardとThriveCart Proの違いは何ですか? ThriveCart Standard(495ドルの一括払い)には、デジタル製品、サブスクリプション、物理製品をオンラインで販売するために必要な機能がすべて含まれています。製品数無制限、ファネル、A/Bテスト、アップセル、オーダーバンプ、ThriveCart Learnなどが利用できます。ThriveCart Pro (690ドルの一括払い、Standardに195ドルのアップグレードを追加)には、組み込みのアフィリエイト管理システム、売上税の自動計算、クライアントの使用権限、インテリジェントな収益予測、高度なコース機能を備えたThriveCart Learn+が追加されます。アフィリエイトプログラムを運営したり、パートナー経由で販売したりする予定がある場合は、Proが最適な選択肢です。195ドルのアップグレードは、スタンドアロンのアフィリエイトプラットフォームと比較して、最初の1か月以内に元が取れます。 ThriveCartの永久ライセンスの価格は値上がりするのでしょうか? ThriveCartは、495ドルの生涯利用権は永続的なものではなく、いずれはサブスクリプション料金に移行すると複数回公言しています。この変更の時期は発表されておらず、2020年以降何度も延期されていますが、そのリスクは現実のものです。現在のThriveCartクーポンコードの価格は495ドルで、2018年から安定しています。早めに購入すれば、将来の価格変更に関わらず、現在の価格で生涯アクセスを確保できます。 インドでThriveCartは利用できますか? はい。ThriveCartはインドを含む世界中のユーザーが利用できます。このプラットフォームは、国際クレジットカードおよびデビットカード(Visa、Mastercard)とPayPalに対応しており、いずれもインドの主要銀行のほとんどを通じてインドの購入者が利用できます。ThriveCartは米ドルで請求を行い、495ドル/690ドルの1回限りの支払いは、単一の国際取引として処理されます。インドのデジタル起業家にとって、ThriveCartの1回限りの料金モデルは特に有利です。なぜなら、INR/USD為替レートによって変動する継続的なUSDの購読料が不要になるからです。 ThriveCartは、Razorpayのようなインドの決済ゲートウェイと連携できますか? ThriveCartは現在、決済処理業者としてStripe、PayPal、Apple Payをサポートしています。RazorpayはThriveCartに決済処理業者として標準で統合されていません。インドの販売者は、ThriveCartを通じてお客様からペイメントを受け取る際に、Stripe India(インドの企業が利用可能)またはPayPalを利用できます。お客様が主にUPIまたはネットバンキングで支払いを行うインドの販売者にとっては、30日間の返金期間中にこれを検討してみる価値があります。
查看全文
缺少 VISLANDS30_IV_SRCID_SYS_MEM_PROT_FAULT 处理程序函数 你好, ,请查找以下 AMDGPU 中断, #define VISLANDS30_IV_SRCID_SYS_PAGE_INV_FAULT 0x0000008c /* 140 */ #define VISLANDS30_IV_SRCID_SYS_MEM_PROT_FAULT 0x0000008d /* 141 */ #define VISLANDS30_IV_SRCID_SEM_PAGE_INV_FAULT 0x00000090 /* 144 */ #define VISLANDS30_IV_SRCID_SEM_MEM_PROT_FAULT 0x00000091 /* 145 */ #define VISLANDS30_IV_SRCID_GFX_PAGE_INV_FAULT 0x00000092 /* 146 */ #define VISLANDS30_IV_SRCID_GFX_MEM_PROT_FAULT 0x00000093 /* 147 */ 在 i.MX95 上加载 AMDGPU 驱动程序时,我收到了未注册的中断,即 140 和 141,但 AMDGPU 驱动程序不会处理这些中断,而 146 和 147 则会单独处理。 Re: VISLANDS30_IV_SRCID_SYS_MEM_PROT_FAULT Handler function missing 你好 这是因为头文件中的这些中断(140、141)属于系统/互连功能域,而不是 GPU 虚拟机,因为在处理虚拟机故障的驱动程序的 gmc_v8_ 0.c 模块中实现的 146 和 147。
查看全文
MPC5744P CPU crash under certain conditions, but unknown cause Hello We are implementing an automotive application with the MPC5744P (MAPBGA257 package, 1N15P cut), which is integrated along with a MC33908 SBC. Compiler is S32DS 2.1 , -O1 optimization. We have been able to reproduce this in 3 different product units, so we hope it is not a faulty silicon. This has been the workflow so far: The application development has been uneventful up to now. Adding a certain quantity of code causes, under certain conditions the core to hang completely. - First and foremost, the SBC reset conditions are checked while reproducing the issue: Reset line does not toggle to low, which means that the SBC does not induce a reset due to abnormal function. So, we focus on the MPC core. - The application has been instrumented with TRACE32 (Lauterbach Powerdebug Pro), and once the condition is reached, a DEBUG PORT FAIL condition arises. Using the reset detection capability, we are able to get to the trace information. The application crashes after a function returning a UINT8_T variable with value equal to 1. This translates to assigning 1 to R3, and then SE_BLR.  - IVORs from 0 to 32 are properly instrumented with branch-to-self instructions (except IVOR4 which jumps to the ISR prologue), so no IVOR trap is taking place. - After verifying that the problem can be reproduced in the same address, a breakpoint is set into that address to check system status before the crash. The system halts at the breakpoint. LR register is OK, stack is normal, everything OK.  - Then, single execution steps are taken to reproduce the crash, with no success. The program steps successfully through the normal flow. - But, if at any time, program flow is restored (no more stepping), the application crashes after some milliseconds (!!) - Checking the trace dump again, we see that it is the same function but with different return value. In a different session, it can even be another different function. - Adding a UINT8_T global spy variable to the function, changes the memory address the crash takes place. - Changing a significative amount of code in a totally unrelated place of the application can eliminate that behavior. As you see, it is very unreliable, and we have no clue of where to continue diagnosing this problem. Attaching code would be of little to no use, as the conditions to provoke this error are very particular, and the failure point, as you see, changes depending on unknown factors. PS: Our problem is similar to this: https://community.nxp.com/t5/MPC5xxx/Lauterbach-reports-MPC5602D-is-in-state-running-reset-what-does/td-p/589249 except that we are able to trace the execution up to the failing point. SWT is disabled on startup, by the way. How is it that the CPU does not arrive to an IVORx exception? Re: MPC5744P CPU crash under certain conditions, but unknown cause I recognize this thread is 4 years old...but I seem to be experiencing the same issue described in this thread, but with the MPC5777c device.  We are also using the MC33908 SBC.  With our CPU reset issue, we have been observing the external reset line not toggling low, getting "debug port fail" in TRACE32 when the fault condition occurs, observe a similar instruction set leading to the failure (return a value to function and then SE_BLR), see TRACE32 affecting the reset, etc etc.  The similarities are quite striking.  It looks like the CPU just stops processing. Was a solution to this issue ever discovered? Re: MPC5744P CPU crash under certain conditions, but unknown cause Hello, don't worry,I have opened a support ticked due to inactivity. I hope we can come up with a solution soon because the application is not reliable right now, unless 100% code coverage testing is done after any minor software change (as minor as adding a 1-byte global debug variable). You will understand that this is not a bearable development workflow. Re: MPC5744P CPU crash under certain conditions, but unknown cause I am apologizing for not hearing from me. I am currently out of office due to family reason. Yes, please create a ticket for this if there is no other response. Thanks for understanding. Re: MPC5744P CPU crash under certain conditions, but unknown cause Due to the lack of response, should I open a support ticket? Re: MPC5744P CPU crash under certain conditions, but unknown cause Further information. We have disabled manually DMA transfers and interrupts and provoked synthetically the issue (by manually setting the conditions for that).  The crash still happens, so we can discard DMA and interrupt influence. Also, if we put a hardware breakpoint in the conflicting line (where the crash happens), it breaks, and stepping is OK. But if we put a software breakpoint, the crash still happens (it does not break). Re: MPC5744P CPU crash under certain conditions, but unknown cause In further testing, I have found out that adding a SINGLE global variable to the system eliminates that crashing behavior. What we can't assure at the moment is that the issue doesn't arise in other conditions. I am really puzzled with this issue, and for the lack of answers I guess it's not a very common one. Mostly, the fact that even the Lauterbach Powerdebug Pro system is unable to shed any light on this issue, providing any single bit of information on CPU registers in order to pinpoint the causing event. Re: MPC5744P CPU crash under certain conditions, but unknown cause Hello Do you have any other advice for this issue?  Thank you Re: MPC5744P CPU crash under certain conditions, but unknown cause The problem persists. So far, Flash timing has been adjusted in PFCR1 as per datasheet values. MC_RGM DES and FES registers have been checked out, and no functional/destructive reset takes place. We have been able to create conditions for a 100% reproducible failure. When stepping through the instruction before the crash (using a breakpoint), there is no crash. But if you enter in free-running mode, the system crashes, and checking the trace report, the crash happens in that instruction in which we breaked before. Do you have any other idea we can try? Thank you Re: MPC5744P CPU crash under certain conditions, but unknown cause Thank you for your response. Have you measured RESET signal bu scope? Has MCU been reset? RESET signal has been measured during the reproducible incident that provokes this failure. The RESET signal is always high, so no external RESET takes place. According your description you says debugger affect the behavior in the meaning the fault does no happen. Also basically you said behavior is unpredictable but repeatable. Yes, basically if you break into the exact point that the system hangs, you can step through instructions with success. However, when leaving stepping mode and running continuously, the system hangs into that exact point. Also keep in mind that altering the software (adding variables, adding code) may, or may not, change the point where the system hang takes place. But once changed, this hang is 100% reproducible.  I would at first check you clocking configuration. In the datasheet section 3.16.3 you have defined prescribed number of flash wait states. Check 2.9.1 System clock frequency limitations Also there is several errata that woul be needed top check: ERR010639 ERR010640 ERR011073 https://www.nxp.com/docs/en/errata/MPC5744P_1N65H.pdf https://www.nxp.com/docs/en/errata/MPC5744P_1N15P.pdf The system has been working thousands of hours under different conditions and this condition has never showed up. Certain software revisions provoke this behavior. Which would be the relationship with the clocking configuration and the flash wait states? Just asking, to look into those hypothesis. Regarding the clocking, this issue happens in a known situation long time after power up. The erratas you mention seem to be related to power up, right?  The thing that puzzles me most, is that the system does NOT hang into any known exception handler. The debugger detects the core as halted/off/reset, and there is no visible symptom to this: right before the core hangs, the LR is OK, the Stack Pointer is well behind the stack size.  I also checked the software version against the E200 branch checker software, and it is ok regarding that. Checking out with my colleagues, we have found out that we previously have experienced this in the MPC5744P QFP144 version, years ago. So it is not just to this BGA257 1N15P part. I don't know how to proceed, seriously. I will look into your suggestions, but any additional hint is gratefully accepted!. PS: The clock mode entry code, executed at startup: /* Enable All Modes */ MC_ME.ME.R = 0x000005E2; /* Peripheral ON in every run mode */ MC_ME.RUN_PC[0].R = 0x000000FE; /******************** Configure XOSC for DRUN **********************/ /* Enable EXT OSC First */ XOSC.CTL.B.OSCM = 0x1; /* Change OSC mode to LCP (Loop Controlled Pierce Mode) */ XOSC.CTL.B.EOCV = 0x80; /* Set the End of Count Value for when to check stabilization. */ /* Enable XOSC in DRUN mode and select as SYS_CLK */ MC_ME.DRUN_MC.R = 0x00130031; /* RE enter the DRUM mode, to update the configuration */ MC_ME.MCTL.R = 0x30005AF0; /* Mode & Key */ MC_ME.MCTL.R = 0x3000A50F; /* Mode & Key inverted */ while(MC_ME.GS.B.S_MTRANS == 1); /* Wait for mode entry to complete */ while(MC_ME.GS.B.S_CURRENT_MODE != 0x3); /* Check DRUN mode has been entered */ while(!MC_ME.GS.B.S_XOSC); /* Wait for clock to stabilise */ /******************** PLL0, PLL1 **********************/ /* Route XOSC to PLL1 */ MC_CGM.AC4_SC.B.SELCTL = 1; /* Route XOSC PLL0 */ MC_CGM.AC3_SC.B.SELCTL = 1; /* Configure PLL0 Dividers for 160 MHz fPLL0_VCO = (fPLL0_ref x PLL0DV[MFD] x 2)/PLL0DV[PREDIV] = 40MHz x 8 x 2 / 1 = 640 MHz fPLL0_PHI = fPLL0_ref x PLL0DV[MFD] / (PLL0DV[PREDIV] x PLL0DV[RFDPHI] = 40MHz x 8 / (1 x 2) = 160 MHz fPLL0_PHI1 = fPLL0_ref x PLL0DV[MFD] / (PLL0DV[PREDIV] x PLL0DV[RFDPHI1]) = 40MHz x 8 / (1 x 😎 = 40 MHz */ PLLDIG.PLL0DV.B.RFDPHI1 = 8; PLLDIG.PLL0DV.B.RFDPHI = 2; PLLDIG.PLL0DV.B.PREDIV = 1; PLLDIG.PLL0DV.B.MFD = 8; /* Configure PLL1 Dividers for 200 MHz fPLL1_VCO = fPLL1_REF x (PLL1DV[MFD] + PLL1FD[FRCDIV]/2^12) = 40MHz x 20 + 0 = 800 MHz fPLL1_PHI = fPLL1_REF * ( (PLL1DV[MFD] + PLL1FD[FRCDIV]/2^12) / (2 x PLL1DV[RFDPHI]) ) = 40MHz x (20 + 0) / (2 x 2) = 200 MHz */ PLLDIG.PLL1DV.B.RFDPHI = 2; PLLDIG.PLL1DV.B.MFD = 20; /* Enable PLL0/PLL1 in DRUN mode and set PLL1 as SYS_CLK */ MC_ME.DRUN_MC.R = 0x001300F4; /******************** Configure Clock Dividers **********************/ SIUL2.MSCR[22].R = 0x22800001; /* Configure CLK_OUT (B6) */ //MC_CGM.AC6_SC.B.SELCTL = 0; /* source AC6 is internal RCOSC */ //MC_CGM.AC6_SC.B.SELCTL = 2; /* source AC6 is PLL0 PHI */ //MC_CGM.AC6_SC.B.SELCTL = 1; /* source AC6 is XOSC */ MC_CGM.AC6_SC.B.SELCTL = 4; /* source AC6 is PLL1 PHI */ MC_CGM.AC6_DC0.R = 0x80090000; /* Aux clock select 6 divider 0 --> div by 10 (CLK_OUT) */ MC_CGM.AC0_SC.B.SELCTL = 2; /* source AC0 is PLL0 PHI */ MC_CGM.AC0_DC0.R = 0x80000000; /* Aux clock select 0 divider 0 --> div by 1 (MOTC_CLK) */ MC_CGM.AC0_DC1.R = 0x80070000; /* Aux clock select 0 divider 1 --> div by 8 (SWG_CLK) */ MC_CGM.AC0_DC2.R = 0x80010000; /* Aux clock select 0 divider 2 --> div by 2 (ADC_CLK) */ MC_CGM.AC1_DC0.R = 0x80010000; /* Aux clock select 1 divider 0 --> div by 4 (FRAY_PLL_CLK) */ MC_CGM.AC1_DC1.R = 0x80030000; /* Aux clock select 1 divider 1 --> div by 4 (SENT_CLK) */ MC_CGM.AC2_DC0.R = 0x80030000; /* Aux clock select 2 divider 0 --> div by 4 (CAN_PLL_CLK) */ MC_CGM.SC_DC0.R = 0x80030000; //80070000 div by 8, 25mhz /* 80030000 Sys clock select divider 0 --> div by 4 (PBRIDGEx_CLK) -> DSPI clock = 50MHz, PIT clock = 50 MHz */ /******************** Start the core **********************/ /* Main and checker cores running in RUN3:0, DRUN, SAFE, TEST modes */ MC_ME.CCTL0.R = 0x00FE; /* Set PRAM controller WS to 1 since running SYS_CLK as PLL1 (200 MHz) */ PRAMC.PRCR1.B.FT_DIS = 1; /******************** Perform mode change **********************/ /* Mode change re-enter the DRUN mode, to start cores, clock tree & PLL1 */ MC_ME.MCTL.R = 0x30005AF0; /* Mode & Key */ MC_ME.MCTL.R = 0x3000A50F; /* Mode & Key inverted */ while(MC_ME.GS.B.S_MTRANS == 1); /* Wait for mode entry complete */ while(MC_ME.GS.B.S_CURRENT_MODE != 0x3); /* Check DRUN mode entered */ PS 2: Can the PFCR1 register values affect to this hang issue? Before the hang, the software is not performing any FLASH write. Re: MPC5744P CPU crash under certain conditions, but unknown cause Have you measured RESET signal bu scope? Has MCU been reset? According your description you says debugger affect the behavior in the meaning the fault does no happen. Also basically you said behavior is unpredictable but repeatable. I would at first check you clocking configuration. In the datasheet section 3.16.3 you have defined prescribed number of flash wait states. Check 2.9.1 System clock frequency limitations Also there is several errata that woul be needed top check: ERR010639 ERR010640 ERR011073 https://www.nxp.com/docs/en/errata/MPC5744P_1N65H.pdf https://www.nxp.com/docs/en/errata/MPC5744P_1N15P.pdf
查看全文
flexbuilder lsdk2108 支持 SERDES1 协议 0x3333 您好, 我们在自定义主板中使用 LS1046A,图像是使用 flexbuild lsdk2108 编译的,我们的设计与 ARDB 开发套件类似。SERDES1 支持两个 10G 端口和两个 1G 端口,不使用 SERDES2。 我们已经根据我们的自定义主板编译了图像,一切正常,10G 端口 (xgmii) 和 1G 端口 (sgmii) 都运行正常。在我们的一个应用中,我们希望将两个 10G 端口都用作 1G 端口。为此,我们更改了 rcw、uboot 和 linux dts 文件。随函附上这些文件以供参考。 编译和主板启动后,我们可以看到 Linux 日志仍在寻找 10G 端口,而 ubuntu 文件系统没有显示 fm1-mac1 和 fm1-mac2 端口。附上启动日志以供参考。 从启动日志中可以明显看出,我们缺少了一些需要更改的内容。在这方面,要求支持需要修改哪些文件才能满足我们的要求。 谢谢& Regards-- 纳古尔瓦利-赛亚德 Re: flexbuilder lsdk2108 support for SERDES1 protocol 0x3333 您好, 感谢您的回复。按照建议,在 rcw、u-boot 和 linux dts 文件中进行更改。从所附的上一个日志文件中可以看到,初始信息显示如下。 "ETH0:FM1-MAC1,ETH1:FM1-MAC2,ETH2:FM1-MAC3,ETH3:FM1-MAC4,ETH4:FM1-MAC5,ETH5:FM1-MAC6 " 更改 u-boot dts 文件后,出现 fm1-mac1 和 fm1-mac2。请建议我们需要对 eth.c 文件做哪些修改。 此外,是否还需要修改任何其他文件。 谢谢& Regards-- 纳古尔瓦利-赛亚德 Re: flexbuilder lsdk2108 support for SERDES1 protocol 0x3333 你好 是的--对于 LS1046A,将两个 10G SerDes1 端口改为 1G 并不仅仅是 Linux DTS 变动。你需要对齐所有三层:RCW、U-Boot 主板以太网修复和 Linux DTS。如果 Linux 仍在探测 10G 端口,而 fm1-mac1 / fm1-mac2 没有出现,那么最有可能的问题是 U-Boot 在 Linux 启动之前仍在 DT 中禁用这些 MAC 节点 要使两个 LS1046A 10G 端口用作 1G 端口,必须将 RCW 更改为 SGMII 协议,例如 0x3333 ,更新 U-Boot eth.c 以使其不会禁用这些 MAC 节点,并更新 Linux DTS,以便使用正确的 PHY 或固定链路配置将这些端口描述为 sgmii。 此致问候 Re: flexbuilder lsdk2108 support for SERDES1 protocol 0x3333 您好, 我们按照建议修改了 rcw、eth.c、uboot dts 和 linux dts。现在我们可以枚举 Linux 启动后的 fm1-mac1 和 fm1-mac2 端口(附上以供参考)。 但我们无法通过这些端口进行数据通信。 还附上了日志文件以供参考。 请审查这些修改意见,并就需要做哪些修改提出进一步建议。 谢谢 -- 纳古尔瓦利-赛亚德
查看全文
rptr 停留在 AMDGPU [GFX 环测试超时] 中 你好 ,当 Amdgpu 调用 amdgpu_ih_process() 函数时,它会检查 rptr 是否等于 wptr,如果不等于,它就会调用 amdgpu_irq_dispatch() 函数,在这里我得到了以下错误信息 [ 26.272978] [drm:amdgpu_ih_process [amdgpu]] amdgpu_ih_process: rptr 0, wptr 16 [ 26.281052] [drm:amdgpu_irq_dispatch [amdgpu]]未注册中断 src_id:140 of client_id:0 [ 26.454946] amdgpu 0000:01:00.0:[drm:amdgpu_ring_test_helper[amdgpu]]*ERROR* ring gfx 测试失败 (-110) [ 26.465393] [drm:amdgpu_device_init [amdgpu]]]*ERROR* hw_init of IP block failed -110 [ 26.474932] amdgpu 0000:01:00.0:amdgpu: amdgpu_device_ip_init 失败 [ 26.481415] amdgpu 0000:01:00.0:amdgpu: GPU 启动过程中出现致命错误 [ 26.487791] amdgpu 0000:01:00.0:amdgpu:amdgpu:整理设备。 [ 26.494006] [drm:gfx_v8_0_set_eop_interrupt_state [amdgpu]] invalid me 2 [ 26.501433] [drm:gfx_v8_0_set_eop_interrupt_state [amdgpu]] invalid me 2 [ 26.508860] [drm:gfx_v8_0_set_eop_interrupt_state [amdgpu]] invalid me 2 [ 26.516252] [drm:gfx_v8_0_set_eop_interrupt_state [amdgpu]] invalid me 2 Re: rptr is stuck in AMDGPU [GFX ring test timeout] 你好 请分享更多信息,您正在使用什么MPU、自定义或恩智浦EVK、BSP版本以及您正在运行的完整测试。
查看全文
S32G-VNP-RDB3 GMAC 你好,我正在用 GMAC 和 S32G-VNP-RDB3 主板进行帧抢占,但我成功实现了 1G bps。但我想把它改为 10M bps,但我做不到,那么限制必须是 1G bps 吗? Re: S32G-VNP-RDB3 GMAC 首先,感谢您的回答。我有两个 S32G-VNP-RDB3 主板,通过 1:1 的链路将 GMAC 相互连接,然后继续进行帧抢占。使用 M 型磁芯。我没有使用环回,而是继续进行。此时,我如图所示设置了时钟和设置,但我看到了一个现象,此时没有发生帧抢占的握手,就像 tx、rx 一样。我需要一个解决方案! Re: S32G-VNP-RDB3 GMAC 你好,@dongmin、 感谢您联系我们。关于您的问题,抢占配置并不只适用于 1G bps。 我迅速修改了Gmac_Ip_InternalLoopback,使用抢占和 10M bps,结果成功了。请提供以下信息,以便我为您提供更多帮助: 您说"不能" 配置为 10M bps 是什么意思? 请说明您是如何测试这两种配置的。 请说明您是在哪个内核上运行应用程序的。 请分享您的 RTD 和/或 BSP 版本。 谢谢。 Re: S32G-VNP-RDB3 GMAC 我现在就是这么用的! Re: S32G-VNP-RDB3 GMAC 你好@dongmin、 感谢您提供的详细信息。我会尝试在我这边重现这个问题,然后找到解决方案。 如果可能,请提供我在上次答复中要求的信息。 谢谢。 Re: S32G-VNP-RDB3 GMAC 你好,@dongmin、 对不起,我的回复晚了。我无法重现您的问题,能否与我分享您的项目?您可以使用本社区的私人信息功能或创建一个提及本主题的私人支持票据。 谢谢。
查看全文
2026 年最佳 IPTV 服务 Nigma TV 是2026年向美国、加拿大、英国和全球用户推荐的最佳IPTV服务之一——主要是因为它专为最重要的时候的稳定直播而打造。 Nigma TV拥有51,000多个直播频道和16万多部电影和电视剧在线点播,一次订阅即可为用户提供庞大的娱乐库。该服务支持高清、全高清、4K 和 UHD 流媒体,在智能电视、Firestick、Android、iOS、PC、Mac 和流行的 IPTV 播放器应用程序上表现出色。 Nigma TV 脱颖而出的原因在于它注重高峰时段和重大直播活动期间的稳定性。该平台采用防冻技术、快速服务器和流畅播放设计,以减少缓冲并保持流媒体的可靠运行。 对于在 2026 年寻找优质 IPTV 提供商的人来说,Nigma TV 是直播电视、体育、电影、连续剧和国际频道的有力选择。 官方网站:NIGMA.TV
查看全文
tea2376 phase shedding can't edit TEA2376 phase shedding beyond 0 30% or 40% load points in Ringo gui. is there a way to be able to fine tune MTP settings in Ringo? Re: tea2376 phase shedding Hello Lee,  I have forwarded your question to our application engineer supporting the TEA2376, please see his answer below.   There is no advanced tab or additional parameters available to further fine‑tune this setting at this time.   As a workaround, I suggest adjusting the PFC OPP threshold to help shift the phase‑shedding operating point, provided there is sufficient margin in your current OPP setting.   BRs, Tomas
查看全文
2026年版おすすめIPTVプロバイダー無料トライアル The 2026年に最高のIPTVプロバイダは、無料トライアルを提供することで、ユーザーがペイメントを支払う前にストリーミング品質、チャネルの利用可能性、およびデバイスとの互換性をテストできるようにします。これらのサービスは通常、スポーツ、映画、ライブTVなど数千ものグローバルチャネルに加え、柔軟な視聴が可能なVODコンテンツを提供している。ほとんどの無料トライアル期間は24時間から数日間で、バッファリング、速度、画質などのパフォーマンスを評価するのに十分な時間があります。主要なIPTVプロバイダーは、HD、フルHD、4Kストリーミングに対応しており、Firestick、スマートテレビ、Android、iOS、PCなどの人気デバイスと互換性があります。信頼性の高いサービスは、特にライブイベント時において、高い稼働率と最小限のバッファリングに重点を置いています。料金は一般的に手頃で、月額10ドルから20ドル程度であることが多く、IPTVは従来のケーブルテレビに代わる費用対効果の高い選択肢となっている。無料トライアルと迅速なカスタマーサポートの両方を提供するプロバイダーを選ぶことが、2026年にスムーズでリスクのないIPTV体験を確実にする最善の方法です。 公式サイト: https://tinyurl.com/4dwb66uy  
查看全文
s32ds Arm のアクティベーションに失敗しました S32DSを再インストールした後、アクティベーションコード60CA-0D4F-9A08-3EEBを使用した際に、「お使いのソフトウェアのアクティベーションコードは別の機能用です」というエラーメッセージが表示されました。 この問題について確認していただけますか?添付ファイルは私のインストールログです 回复: s32ds arm Activation failed キャンセルボタンをクリックした後、「ソフトウェアのアクティベーションコードは既にこのステーションで使用されています(3 アクティベート済み 2.2)」というエラーメッセージが表示されました。 回复: s32ds arm Activation failed はい、アクティベーションの問題は解決しました。 しかし、S32DSを開いてS32K144用の新しいプロジェクトを作成すると、プロジェクトフォルダを展開したときに「サポートされていないか、認識されない形式です」というエラーポップアップウィンドウが表示されます。ポップアップは通常の方法では閉じられません。 この問題にもかかわらず、プロジェクトは正常にコンパイルされているようだ。このエラーの原因を理解するのを手伝っていただけませんか? 回复: s32ds arm Activation failed こんにちは、 あなたのアカウントを確認したところ、木曜日にS32DSを有効化できたようですが、それでよろしいでしょうか? 回复: s32ds arm Activation failed こんにちは、 プロジェクトを共有していただけますか?このプロジェクトは、OSによる暗号化の影響を受けている可能性があります。
查看全文
LS1028A could not get PHY in U-Boot Hi, I'm developing my project with LS1028A. On my board the management interface (MDC/MDIO) of AR8031 connects to EMDIO. PHY address is 2. I read the PHY register using the following commands in U-Boot: =>mdio read 2 0 Reading from bus emdio-3 PHY at address 2: TT0 - 0x0 According U-Boot code, I know the character ‘T’ means MDIO busy. The EMDIO_CFG register definition gives us the description of all the bits. But how is BSY field set to 1? Does it set by hardware? and in what circumstances will it be set to 1? Besides, I have another test that disconnects the MDIO/MDC between LS1028 and AR8031.  BSY field is still 1. Re: LS1028A could not get PHY in U-Boot Hello, I've also run into the problem where the MDIO bus is unable to read the PHY chip. I was wondering if you could kindly share how you resolved it at the time. Thank you very much. Re: LS1028A could not get PHY in U-Boot Hi, @ainolike  I met the same problem on my project. The reference board has two phy chips(RGMII QSGMII interface) connected to the lsf0204 which work very well. And we add another phy (RGMII interaface) and cause the MDIO BUSY occasionally. Can you tell me how to fix it on your project in the end? Thank you  xinli Re: LS1028A could not get PHY in U-Boot I make a test that is removing lsf0204 from our board. And the MDIO is no longer busy.  Two PHY chips are connected to lsf0204. When disconnect one, theother can be read normally. Re: LS1028A could not get PHY in U-Boot There is a lsf0204 between LS1028A and PHY MDC/MDIO interface. PHY chip is disconnected from lsf0204, the BSY bit of register is still 1. Re: LS1028A could not get PHY in U-Boot I don't know much about hardware. Our hardware engineers say that it's a matter of electrical level. Re: LS1028A could not get PHY in U-Boot > our hardware has some changes. Which exactly changes? Re: LS1028A could not get PHY in U-Boot This problem is probably a hardware problem, because our hardware has some changes. The same U-Boot image can find PHY on the development board. I want to know what the MDIO busy implementation mechanism is, which is not described in detail in LS1028ARM.pdf. Re: LS1028A could not get PHY in U-Boot => md 0x1f8101c00 1f8101c00: 80839549 00008000 00000000 00000003 1f8101c10: 00030001 00000000 00000000 00000000 1f8101c20: 00000000 00000000 00000000 00000000 1f8101c30: 00000000 00000000 00000000 00000000 => md 0x1e00074 01e00074: 00000000 00000000 00000000 00000000 01e00084: 00000000 00000000 00000000 00000000 01e00094: 00000000 00000000 00000000 00000000 01e000a4: 870b0110 00000040 00000000 00000000 Re: LS1028A could not get PHY in U-Boot Please provide raw memory dump of the EMDIO registers and DEVDISR2.
查看全文