2359504_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2359504_en-US

2359504_en-US

tea2376 phase shedding

can't edit TEA2376 phase shedding beyond 0 30% or 40% load points in Ringo gui. is there a way to be able to fine tune MTP settings in Ringo?

Re: tea2376 phase shedding

Hello Lee, 

I have forwarded your question to our application engineer supporting the TEA2376, please see his answer below.
 
There is no advanced tab or additional parameters available to further fine‑tune this setting at this time.
 
As a workaround, I suggest adjusting the PFC OPP threshold to help shift the phase‑shedding operating point, provided there is sufficient margin in your current OPP setting.
 
BRs, Tomas
标记 (1)
无评分
版本历史
最后更新:
‎05-05-2026 03:31 AM
更新人: