Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Varification of EMC Compliance for MYD-Y6ULX-CHMI The MYD-Y6ULX-CHMI Display Panel is an ultra-low cost Human Machine Interface (HMI) solution based on 528MHz NXPi.MX6UL/6ULL ARM Cortext-A7 processor. It is a Linux-ready device with ported QT, can be used in various applications including POS, Intelligent access control and more others. The panel provides a well-designed hardware with various peripherals and rich software resources to help users accelerate their time to the market. The MYD-Y6ULX-CHMI consists of an MYD-Y6ULX-HMI Development Board and a 7-inch capacitive LCD mounting on its top. The LCD offers 800x480 pixels display resolution. The MYD-Y6ULX-HMI Development Board provides peripherals and interfaces including RS232, RS485, Ethernet, USB Host/Device, LCD, Camera, TF card slot and etc. Considering wireless communication and dial-up functions, MYIR offers an optional IO board MYB-Y6ULX-HMI-4GEXP for the MYD-Y6ULX-CHMI Display Panel. The IO Board features on board AP6212 module for WiFi/Bluetooth and a Mini-PCIe interface for USB based 4G LTE module. Moreover, the IO Board has extended one more Ethernet interface and Audio in/out ports to further enhance the functionality of the panel, thus making a complete solution for HMI applications. The MYD-Y6ULX-CHMI has passed the verification of EMC Compliance.           MYD-Y6ULX-CHMI Display Panel                            MYD-Y6ULX-CHMI Display Panel + MYB-Y6ULX-HMI-4GEXP The MYD-Y6ULX-CHMI Display Panel is an ultra-low cost Human Machine Interface (HMI) solution based on 528MHz NXPi.MX6UL/6ULL ARM Cortext-A7 processor. It is a Linux-ready device with ported QT, can be used in various applications including POS, Intelligent access control and more others. The panel provides a well-designed hardware with various peripherals and rich software resources to help users accelerate their time to the market. The MYD-Y6ULX-CHMI consists of an MYD-Y6ULX-HMI Development Board and a 7-inch capacitive LCD mounting on its top. The LCD offers 800x480 pixels display resolution. The MYD-Y6ULX-HMI Development Board provides peripherals and interfaces including RS232, RS485, Ethernet, USB Host/Device, LCD, Camera, TF card slot and etc. Considering wireless communication and dial-up functions, MYIR offers an optional IO board MYB-Y6ULX-HMI-4GEXP for the MYD-Y6ULX-CHMI Display Panel. The IO Board features on board AP6212 module for WiFi/Bluetooth and a Mini-PCIe interface for USB based 4G LTE module. Moreover, the IO Board has extended one more Ethernet interface and Audio in/out ports to further enhance the functionality of the panel, thus making a complete solution for HMI applications. The MYD-Y6ULX-CHMI has passed the verification of EMC Compliance.           MYD-Y6ULX-CHMI Display Panel                            MYD-Y6ULX-CHMI Display Panel + MYB-Y6ULX-HMI-4GEXP
View full article
INS-N2010 批量和带状等离子清洗配置及其在 IC 封装技术中的应用 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 等离子清洗在IC封装行业中得到了广泛的应用,用于清洗组装材料,以提高其后续工艺的清洁度,并提高整体封装或器件的可靠性。其中一个挑战是,当各种材料暴露于等离子体时,如何建立清洁过程的兼容性。随着近年来铜线在 IC 封装中的应用,污染的控制非常重要。已发现焊盘腐蚀对于器件和封装的可靠性至关重要,这是本文要解决的主要问题之一。我们将介绍评估结果,包括使用不同等离子清洗配置进行的表面分析和可靠性测试及其其他应用。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 等离子清洗在IC封装行业中得到了广泛的应用,用于清洗组装材料,以提高其后续工艺的清洁度,并提高整体封装或器件的可靠性。其中一个挑战是,当各种材料暴露于等离子体时,如何建立清洁过程的兼容性。随着近年来铜线在 IC 封装中的应用,污染的控制非常重要。已发现焊盘腐蚀对于器件和封装的可靠性至关重要,这是本文要解决的主要问题之一。我们将介绍评估结果,包括使用不同等离子清洗配置进行的表面分析和可靠性测试及其其他应用。 洞察与创新
View full article
FTF-ACC-F1259 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 同步多线程 (SMT) 是一种先进的处理器微架构功能,它允许独立执行线程更有效地利用超标量 CPU 管道组织。双向超标量流水线中的 SMT 实现以相对较小的增量动态功耗最大化双线程并发性。本次会议重点关注下一代 Power Architecture e200z9 处理器核心中包含的 SMT 功能,以及通过该微架构可实现的改进的性能/功率指标。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 同步多线程 (SMT) 是一种先进的处理器微架构功能,它允许独立执行线程更有效地利用超标量 CPU 管道组织。双向超标量流水线中的 SMT 实现以相对较小的增量动态功耗最大化双线程并发性。本次会议重点关注下一代 Power Architecture e200z9 处理器核心中包含的 SMT 功能,以及通过该微架构可实现的改进的性能/功率指标。 回复:FTF-ACC-F1259 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 新款e200z9什么时候上市?
View full article
PN7160 - RF 設定 GUI PN7160 RF 設定の基本的な GUI が利用可能です。添付ファイルをご覧ください。 この GUI は、PN7160 RF 設定のほとんどに対してNCIコマンドを生成できます。これは、ユーザーが適切な NCI コマンドを構築するのに役立つかもしれません。 現在、GUI は NXP ウェブページで利用可能です。 PN7160 RF 設定の基本的な GUI が利用可能です。 NFCフロントエンド・ソリューション
View full article
eIQ Toolkit for MCU - Getting Started Labs The tools previously bundled as part of eIQ Toolkit are now released as standalone packages and eIQ Toolkit will no longer be updated after the eIQ Toolkit v1.17 in Q3 2025. Going forward the tools previously included in eIQ Toolkit can now be found at: eIQ Neutron SDK now contains the latest versions of the Neutron Compiler tool (previously called the Neutron Converter tool before Aug 2026) eIQ Time Series Studio can now be found in a standalone package eIQ Model Creator provides an option for vision based model creation eIQ AI Toolkit will provide model optimization functionality (Coming Soon) Netron provides TFLite model viewing functionality This article will remain up for existing users. --------- eIQ Toolkit enables machine learning development with an intuitive GUI (named eIQ Portal) and development workflow tools, along with command line host tool options as part of the eIQ ML software development environment. Developers can create, optimize, debug and export ML models, as well as import datasets and models, rapidly train and deploy neural network models and ML workloads. The eIQ Portal provides output TensorFlow Lite models that seamlessly feed into eIQ inference engines like TensorFlow Lite and TensorFlow Lite for Microcontrollers. Using a tool called Model Runner, eIQ Toolkit can also generate runtime insights to help optimize neural network architectures on i.MX RT and i.MX devices. These labs go over how to use eIQ Portal. It is recommended to do them in the following order: Data Import Lab Model Runner Lab The labs are written for using a FRDM-MCXN947 and i.MX RT1170-EVK, but other eIQ supported devices can be used as well.  MCX N i.MX RT1050 i.MX RT1060 i.MX RT1064 i.MX RT1160 i.MX RT1170 i.MX RT1180 i.MX RT500 i.MX RT600 For details on the Time Series Studio tool please see the Time Series Studio lab guides. For  i.MX RT
View full article
FlexIo 模拟 UART 你好, 目前贵公司生产的S32K118芯片存在以下问题: (1)使用 FlexIO 模拟 SDK 版本(S32SDK_S32K1XX_RTM_4.0.1)的 UART 可以进行环回测试,官方演示也是环回测试的一个示例。然而,当使用 FlexIO 的 MCAL 版本 (SW32K1_S32M24x_RTD_R21-11_3.0.0) 模拟 UART 时,发现无法进行环回测试。是因为 MCAL 版本不支持吗? (2)考虑到 MCAL 版本不支持,如果使用 FlexIO 的 SDK 版本来模拟量产项目中的 UART,是否存在功能安全隐患? 最好的祝愿, NXP2。 Re: FlexIo Simulates UART 您好@NXP2 我不确定我是否正确理解了您的问题,但请注意,FlexIO 本身并不提供专用的内部环回功能。在 SDK 示例中,环回测试是通过使用导线将 FlexIO TX 和 RX 信号外部连接来实现的。 关于 S32SDK_S32K1XX_RTM_4.0.1,请注意,这是一个相对较旧的软件版本,目前已停止积极维护。我们通常建议使用 SW32K1_S32M24x_RTD_R21-11_3.0.0,因为它是 S32K1 系列的最新软件版本,并且会持续获得维护更新、错误修复和新功能。 另外,您能否提供更多关于该应用场景的信息?这将有助于我们更好地了解您的使用场景。 BR,VaneB Re: FlexIo Simulates UART 您好@NXP2 通常,环回用于测试和验证目的,以验证外围设备和通信路径的功能。一般不建议将其作为生产系统正常运行模式的一部分。 Re: FlexIo Simulates UART 你好, 你目前的理解是正确的。目前的测试方法是通过外部导线连接 FlexIOTX 和 RX 信号。 (1)目前,乘用车前照灯项目中是否有必要使用它?是否存在功能安全隐患?、 (2)与普通的LPUART有什么区别?它的性能是否稳定可靠? 此致, 恩智浦2
View full article
LPI2C 从机位错误问题 我使用的是S32K146,手册上说当从设备发送1但总线为0时会触发位错误。然而,在实际测试中,当从设备发送0但总线为1时也会触发位错误。我想知道这种现象是否正确? Re: An issue regarding slave bit errors in LPI2C 嗨@GXY , 是的,没错。当从机驱动 SDA 时,位错误标志会被触发,但采样结果却不同。 值比预期值大,不一定只在发送 1 而读取 0 时才如此。 我的猜测是,寄存器描述只是给出了一个位错误标志置位时的示例。 此致, 朱利安
View full article
i.MX8MP RAW 捕获最大几何尺寸 NXP社区的各位好, 我们正在尝试在 i.MX8MP 上使用特定的图像传感器。 我们正在尝试将 RAW12 捕获从 MIPI 推送到 RAM。看来唯一的方法是通过如下所述的 ISI 模块: 问题在于,关于几何限制的文档含糊不清,我们正在尝试确定 i.MX8MP 是否适合我们的应用。 图像的高度和宽度在 ISI 中使用 CHNL_IMG_CFG[WIDTH/HEIGHT] 寄存器定义。这些条目是 13 位的,理论上将我们限制在 8191 x 8191 的几何尺寸。 宽度似乎受到硬件的限制,因为行缓冲区实际上只能容纳 2K 像素,但文档概述了通过组合其他通道的行缓冲区来实现 4K 的方法。文档中没有说明是否可以达到 8191 像素的线宽寄存器限制。我们可以绕过 ISI 处理,我们的目标是直接将 RAW MIPI 捕获的数据推送到 RAM 中。 此外,与宽度限制不同,高度限制似乎并非由物理硬件引起。 是否有任何证据表明我们可以支持 CHNL_IMG_CFG[HEIGHT] 寄存器 13 位最大值所定义的 8191 行高度? 任何支持都将不胜感激。我已阅读过其他类似帖子,例如以下这些: https://community.nxp.com/t5/i-MX-Processors/Direct-MIPI-CSI2-to-memory-access-on-i-MX8MP/mp/2158946 https://community.nxp.com/t5/i-MX-Processors/I-MX8MP-ISI-maximum-supported-width/mp/1224069 但是,目前尚未确认是否支持 8191 宽度,我想知道这方面是否有任何更新。 此外,高度限制也没有明确规定。 谢谢 i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: i.MX8MP Maximum Geometry for RAW Capture i.MX8MP 的 ISI 驱动程序限制在 2K 分辨率,但如果使用链式缓冲区,ISI 可以支持高达 4K 的分辨率,但不支持 8191 像素宽。在 i.MX8MP 上,单个摄像头最高可支持 4K@30Hz 的分辨率。 Re: i.MX8MP Maximum Geometry for RAW Capture 感谢您的回复。 所以宽度限制与我最初的发现相符。 请问ISI模块的高度限制是多少?我们能否通过 ISI 实现 8191 车道高度? 谢谢 Re: i.MX8MP Maximum Geometry for RAW Capture 请参考驾驶员说明,最大高度为 8191。 #define MXC_ISI_MIN_WIDTH 1U #define MXC_ISI_MIN_HEIGHT 1U #define MXC_ISI_MAX_WIDTH_UNCHAINED 2048U #define MXC_ISI_MAX_WIDTH_CHAINED 4096U #define MXC_ISI_MAX_HEIGHT 8191U https://github.com/nxp-imx/linux-imx/blob/lf-6.12.y/drivers/media/platform/nxp/imx8-isi/imx8-isi-core.h
View full article
MPXV5004 Sensor Application question HI, I'm from a Commercial Glass & Dishwasher manufacture & we are looking at replacing our old diaphragm based pressure switches to the MPXV5004 pressure sensor with our control board, with reading the Datasheet it says: "Internal reliability and qualification test for dry air, and other media, are available from the factory. Contact the factory for information regarding media tolerance in your application". so my question is we can provide clean air to the sensor through an Air-Bell, but it wont be dry it will have around 60-70% humidity as we use hot water in the machines. will this affect the sensors reliability or longevity? If so, are there other sensors that could be used? or a recommended way that we could connect the tube from the Air-Bell to the pressure sensor?. Thanks Damien Pressure Sensors Re: MPXV5004 Sensor Application question Hello Damien, Thanks for using our community. You could protect the sensor using a high viscosity silicone. Please, take a look at the following thread: Re: 30% of MPXM2202GS failed within 2 months after installation -Josh
View full article
MMA9551 ファームウェアのアップグレードに失敗しました。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 私のボードには、mma9551 用のファームウェアがありません。これに基づいて、コマンドインタープリターを使用して、mma9551 に新しいバージョンをダウンロードします。フラッシュ保護解除モードに入った後、フラッシュを一括消去し、新しいバージョンでフラッシュを書き込みます。ただし、アップグレード プロセスは失敗します。書き込みフラッシュ応答エラー コードは 0xD0 です。リファレンスマニュアルを読んでみると、フラッシュにアクセスする権限がないことがわかりました。しかし、起動時にフラッシュ書き込みの失敗が発生しないのは非常に奇妙に思えます。いくつかのページの書き込みは成功しましたが、特定のページにアクセスする権限がないため、アップグレード プロセスが失敗しました。誰か何かアイデアを持っていますか? さらに奇妙なのは、ファームウェアを搭載した mma9551 を搭載したボードで新しいファームウェア バージョンをアップグレードする場合です。エラーもなく成功しました。 よろしくお願いします。 加速度センサ Re: MMA9551 upgrade firmware failed. <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、レスリー。 MMA9551L ボードに適切な FW がまだフラッシュされていないことに驚きました。詳細を教えていただけますか。このボードは公式デモキット KITMMA9551LEVM からのものですか、それともテープとリールからのデバイスが搭載されているものですか。デバイス パッケージ上の完全なマーキングとは何ですか? MMA955xL デバイスには、それぞれのデフォルトの FW と一部のキャリブレーション パラメータが当社の生産ラインでロードされており、さらに、対応するフラッシュ セグメントが保護されていることに注意してください。 したがって、お客様が NXP 独自の FW のロードを処理することは推奨されません。 デバイスが最初から機能していなかった場合、デバイスを交換して、デフォルトの FW が適切にロードされなかった理由を調査できます。 よろしく、ジャック。
View full article
gPTP 示例无法在 S32g399 上运行 你好, 我已经构建了 gptp_s32G_1.1.0配有: S32 RTD 版本 SW32G_RTD_4.4_5.0.0_QLP03_D2505S32G PFE MCAL 驱动程序 PFE_DRV_MCAL_S32G_RTM_1_6_0_D2505 S32G PFE 固件 PFE-FW_S32G_1.11.0 我运行了 make generate,然后运行 make,在 /output_AED-E_RDB3 中创建了 elf。我将此 elf 作为项目从 S32 DS 中的可执行文件加载,创建了 DEBUG_RAM 配置。 我注意到,在 DriversInitialization() 中,应用程序并没有超出 Mcu_GetPllStatus() 调用的范围。暂停执行后,我发现执行卡在 Clock_Ip_CompletePlldigRdivMfiMfnSdmenSsscgbypSpreadctlStepnoStepsize() 的 PLL 锁定上 ,除了修改 makefile 以选择正确的路径外,我自己没有做任何修改。它的构建没有错误,我只是用 S32 调试器刷新了它。 请告诉我如何解决这个问题,以及如何在 AED-E 模式下验证 gPTP 应用程序。谢谢、 Re: gPTP example not running on S32g399 @Joey_z 我使用的是 GLDBOX3:https://www.nxp.com/part/S32G-VNP-GLDBOX3 如果需要进行更改才能在本板上运行此应用程序,请描述我可以尝试的更改。或者,如果有一份应用笔记可以针对该板调整gPTP应用程序,那也应该起作用。 谢谢! Re: gPTP example not running on S32g399 你好 ,rizwan_at_disru ptdotcom 你使用的是 RDB3 板还是客户板? BR 乔伊 Re: gPTP example not running on S32g399 嗨,rizwan_at_disruptdotcom 您是否可以尝试使用 IVT 映像或 .cmm文件进行测试? BR 乔伊 Re: gPTP example not running on S32g399 你好@Joey_z 我们没有 lauterbach 调试器,只使用 S32 调试探器,该探测器可与我们在该板上的其他应用程序配合使用。我注意到 cmm 正在清除 sram 扇区,如果问题出在这里,能否请您告诉我如何使用 s32 调试探针进行同样的操作? 该示例并未创建 IVT,而是使用 DEBUG_RAM 配置直接尝试闪存的精灵。 里兹万 Re: gPTP example not running on S32g399 你好@Joey_z、 我没有对应用程序进行任何更改,只是更新了生成文件以启用在我的计算机上构建。 我已将 EBT 文件夹压缩包上传到驱动器。请访问此处: https://drive.google.com/file/d/1_3vj19gXmwHmqs20aAPOWAjENRCYusfg/view?usp=sharing Re: gPTP example not running on S32g399 hi,rizwan_at_disru ptdotcom 感谢您的回复。 你是如何生成代码和构建你的项目的?您对应用程序配置有任何修改意见吗? 请将您的 .elf文件给我的链接是https://support.nxp.com? 我会帮你检查的。 BR 乔伊 Re: gPTP example not running on S32g399 我还打开了一个支持案例:00959194
View full article
S32K344 ハングアップ問題 MCU: S32K344 OS: FreeRTOS S32 Design Studio: 3.4.3 問題: I2C 書き込みブロッキングによる MCU のハング (タイムアウトなし) こんにちは、チーム S32K344 MCU をベースにしたカスタム ボードを使用しています。特定の I2C エラー条件下では実行時に MCU がハングするという問題が発生しています。 I2C インターフェースを介して接続された IMU スレーブ デバイスがあります。時々、次のようなとき: IMUに電源が入っていない、または I2C書き込み操作が失敗する(例:ACKなし/バススタック) I2C 書き込み API はタイムアウト状態を返さないか、タイムアウト状態になりません。その結果、 I2C トランザクションを実行する FreeRTOS タスクが無期限に停止し、最終的にアプリケーションがハングすることになります。 観察: この問題は、スレーブが応答しないか、バスが低く保持されている場合に発生します。 I2C ドライバは転送の完了を待機してブロックしているように見えます。 RTOS またはドライバ レベルではタイムアウトまたは回復メカニズムはトリガーされません。 サポートのリクエスト: S32K344 上の I2C トランザクションにタイムアウトを追加または強制するにはどうすればよいですか? スタックした I2C バス (SDA/SCL が低く保持される) を回復するための推奨される方法はありますか? S32K3 デバイス上のFreeRTOS で I2C を安全に使用するベスト プラクティスは何ですか? このシナリオを堅牢に処理する NXP のドライバ構成または例はありますか? あらゆるガイダンスや参考資料をいただければ幸いです。 ありがとう、よろしく。 ヴィナイ Re: S32K344 Hanging issue こんにちは@vinaykl 、 非常に古い RTD をお持ちです。 何か理由があるのでしょうか? RTD 2.0.0 と現在の RTD 7.0.0 の間では多くのバグが修正されています。 I2C ドライバのブロッキング API を使用すると想定しています。 代わりに、GetStatus() とタイムアウトとともに非同期転送 API を使用してください。 スレーブデバイスが SDA を低く保持し続ける場合は回復できます。I2C ユーザーマニュアルを参照してください。 セクション3.1.16バスはクリア https://www.nxp.com/docs/en/ユーザーガイド/UM10204.pdf   RTD ドライバには回復用の API がありません。 例としてはAN4803があります I2C復元関数の定義 https://www.nxp.com/docs/en/application-note/AN4803.pdf よろしくお願いいたします。 ダニエル
View full article
[过滤器:垃圾邮件] evelynteddy 的帖子正文与 " *telegram* " 相符,板 " imx-processors "。 [过滤器:垃圾邮件] evelynteddy 的帖子正文与 " *telegram* " 相符,板 " imx-processors "。 帖子主题:回复:IMX7ULPEVK-等待根设备 /dev/mmcblk0p2... 职位机构: 如何从骗子手中找回丢失或被骗的加密货币,请访问 OPTIMISTIC HACKER GAIUS。 上周我的加密货币被骗后,我感到很无助,不知道该怎么办。我与乐观黑客盖乌斯取得了联系,他一直都很专业,有良好的沟通,并设定了合理的期望值。他细心地处理问题,经常提供最新信息,并描述了每一个步骤。通过坚持不懈的努力和专业技术,我被盗的加密货币被找到并追回。我吸取了重要的网络安全教训,并通过这次遭遇恢复了信心。我感谢你们在这段艰难时期给予我的帮助和指导。强烈建议 网站:optimistichackargaius.co m 电子邮件:support @ optimistichackargaius.com。 WhatsApp number:+44 737 674 0569 电报:t.me /OPTIMISTICHACKERGAIUSS 正文"电报" 匹配的过滤模式"*telegram*" 。 用户[id=259418,login=evelynteddy]的发帖因以下最终用户面临的错误而被拒绝: 信息正文中包含 Telegram,这在本社区是不允许的。请在发送您的帖子前删除这些内容。
View full article
Kinara ARA-SDK Licensing Hi NXP team (and anyone familiar with Ara-2 / Kinara tooling), I’m trying to understand the correct licensing/access path for compiling models for the Ara-2 (Kinara) compute module, especially now that Kinara has been acquired by NXP and NXP’s public materials describe SDK integration into NXP’s software ecosystem. My setup / goal Hardware: Geniatech Ara-2 compute module SDK: Geniatech-provided Kinara Ara-2 SDK r1.3 Use case: personal, non-commercial (research/study/testing) Model target: Qwen/Qwen2.5-7B-Instruct (GPTQ Int4) What works so far I can complete the Mode 1 flow to convert the model into ONNX. I end up with: model.onnx (small graph file) model.onnx.data (large external tensor data / weights) in the same directory. What fails Mode 2 (the compilation stage to generate a deployable .dvm) fails with license checkout/validation errors from the SDK’s build tools. From what I can tell, this blocks generating a .dvm even though ONNX export succeeds. Where I’m stuck I do not have a Kinara license key. Geniatech’s documentation indicates that obtaining the SDK license key must be done via Kinara. The Kinara customer support portal appears to reject registration using common personal email domains (e.g., gmail.com), so I can’t submit a request there. Why I’m asking here (NXP/Kinara integration confusion) NXP’s public material indicates Kinara’s SDK and model tools are being integrated into NXP’s ecosystem (including eIQ), and Ara-2 is now presented as an NXP product offering with related “Ara Software Development Kit” downloads. However, in practice, it’s not clear: where a developer is supposed to obtain a license key for compilation, and whether the “Ara SDK / eIQ integration” path is the supported route now. Questions Is a license key required to compile ONNX → .dvm using the Ara-2 SDK toolchain (r1.3 / ARA-SDK), even for personal/non-commercial use? If yes, what is the official process for an individual/hobbyist user to obtain evaluation/developer access (especially without a corporate email domain)? With an existing NXP account, where exactly should Ara-2 users obtain: the “official” Ara SDK binaries/toolchain (compiler), and/or the licensing mechanism needed for compilation? If compiling requires a license key that isn’t readily obtainable, are there any precompiled .dvm model packages (e.g., for Qwen 7B/Qwen2.5 7B) that NXP/Kinara/partners provide for Ara-2 users to run? If someone from NXP/Kinara can clarify the intended path (NXP portal vs legacy Kinara portal, and how licensing is handled now), that would help a lot. Re: Kinara ARA-SDK Licensing I have the same question! I got the device, driver. But no SDK and I guess no license either (if it is needed). The device is just sitting silently in my Lenovo ThinkCentre Ultra neo computer and not doing anything. Lenovo never finished its integration to Windows 11 as an NPU. I would like to use it at least to run some models on it or learning. It is now a completely unused piece of silicon in my PC. I guess it would help the adoption of the technology if more people would start using it. Re: Kinara ARA-SDK Licensing @kratafila mine was also basically unused silicon until I managed to get hold of a Linux SDK bundle via Geniatech. To be honest it is still unused silicon since I cannot get the models to compile and run. For what it’s worth, Geniatech (vendor of my Kinara Ara-2 M.2 module) shared these SDK/runtime downloads with me. They’re Linux-focused, and I’m not sure whether they’ll apply to the Ara-2 hardware inside your ThinkCentre (or help on Windows 11, there are included Windows binaries but I had more success with the Linux software), but they might still be useful if you can test under Linux / confirm your device works: 1) Drivers/runtime + sample .dvm models (Geniatech "customer ready" bundle): hxxps://mega[.]nz/file/nJcF0K5a#W-Ote-fp59hXoq4T0GGsaQmwGTRphWz0JATowyWjQpg 2) "Model compile" folder Geniatech initially sent me (note: this alone didn’t include the compiler binary): hxxps://mega[.]nz/file/KoclFQrJ#ifNOX7w2Y1qgLM6rnm7xPnUprwZZqhuRvelFG5p0MJQ 3) Full Ara-2 SDK tarball Geniatech later provided (this is the one that should include the actual toolchain/compiler, e.g. dvrun): hxxps://file[.]geniatech[.]com/down-eng/BSP/kinara_SDK_20251120[.]tar[.]bz2 If you do try any of the above and make progress (even just getting the SDK installed and seeing the device recognized), please post back here, not just for us, but because there seems to be broader confusion across multiple communities about the "official" working path and where the SDK/licensing is actually meant to come from as well as how to compile and run additional models.
View full article
PCA9698 のステータスをご存知ですか? こういうものが必要かもしれないと思いました。ステータスはどうですか?もっと新しい類似製品はありますか? ランディ Re: Do you know the status of PCA9698 ? こんにちは、ランディ。 PCA9698 は現在も生産中ですが、HVQFN56 バージョン (PCA9698BS) は製造が中止されます。TSSOP56 バージョン (PCA9698DGG) は引き続き完全にアクティブでサポートされており、新しいデザインに推奨される選択肢です。同じ 40 ビット GPIO 数と電流能力を単一チップで提供する新しい NXP デバイスは存在しないため、その機能が必要な場合、PCA9698DGG は依然として最適なソリューションです。 BRs、トーマス
View full article
S32R45 SptEcsIsrCb エラー! アラームの原因を検索すると、「PDMA での AXI 読み取りエラー」が表示されます。このアラームが発生する原因は何でしょうか? SPT エラー キューがオーバーフローしました。最初の 10 件のエラーのみが報告されます。最後に実行されたカーネルを確認してください! SPT完了 SptEcsIsrCb エラー!、ステータス: 0x11005、エラー情報: 0x10000 SptEcsIsrCb エラー!、ステータス: 0x11005、エラー情報: 0x10000 SptEcsIsrCb エラー!、ステータス: 0x11005、エラー情報: 0x10000 SptEcsIsrCb エラー!、ステータス: 0x11005、エラー情報: 0x10000 SptEcsIsrCb エラー!、ステータス: 0x11005、エラー情報: 0x10000 SptEcsIsrCb エラー!、ステータス: 0x11005、エラー情報: 0x10000 SptEcsIsrCb エラー!、ステータス: 0x11005、エラー情報: 0x10000 SptEcsIsrCb エラー!、ステータス: 0x11005、エラー情報: 0x10000 SptEcsIsrCb エラー!、ステータス: 0x11005、エラー情報: 0x10000 SptEcsIsrCb エラー!、ステータス: 0x11005、エラー情報: 0x10000 RsdkSptRun が完了しました。SPT プロセッシングが完了しました。次のカーネルの準備ができました。 Re: S32R45 SptEcsIsrCb error! こんにちはピーター、 ご返信ありがとうございます。   あなたが挙げた理由に従い、私は特に以下の点に重点を置いてコードを注意深くチェックしました。   WR_5、問題は見つかりませんでした。さらに、SPT カーネル コードは変更していません。   コード初期リスト:   AppMemAllocBuffer ( pHeapMem 、 & gSdadcSampleBufferBufH [インデックス]、 sizeof ( uint16_t ) * RSDK_SPT_RANGE512_4CH_IN_BUF_SIZE 、                           RSDK_SPT_DATA_ADDR_ALIGN_BYTES 、 RSDK_OALMEM_CHUNK_ID_CBRAM );   RelocSptCode ( gSptModuleCodeRelocBufH . virtAddr 、 RsdkSptRange512smp128crp4ch 、 RSDK_SPT_GET_KERNEL_SIZE ( RsdkSptRange512smp128crp4ch ));   np = 0 ; sptContext . kernelParList [ np ]. paramType= RSDK_SPT_PARAM_TYPE_ADDR ; sptContext 。 kernelParList [ np ++ ]。 paramValue = ( uintptr_t ) gSdadcSampleBufferBufH [ 0 ]。 phyAddr ;   sptContext . kernelParList [ np ]. paramType= RSDK_SPT_PARAM_TYPE_ADDR ; sptContext 。 kernelParList [ np ++ ]。 paramValue = ( uintptr_t ) gRadarCubeResultsBufH 。 phyAddr ;   sptContext . kernelParList [ np ]. paramType= RSDK_SPT_PARAM_TYPE_ADDR ; sptContext 。 kernelParList [ np ++ ]。 paramValue = ( uintptr_t ( gFft512TwiddleFactorsBufH . phyAddr );    sprintf (ファイル名、 " %s% s " 、 FILE_IN_PATH 、 "fft512_twiddle_factors.dat" ); /* RSDKデータは、PPCアーキテクチャとの互換性のため、ビッグエンディアン形式でファイルに保存されます。エンディアンの変換は、ファイルへのデータの読み書き時にのみ行われます。プロセッシングフロー内での変換は必要ありません。*/   DbgReadFileConvert ( fileName 、 0 、 ( char * ) gFft512TwiddleFactorsBufH . virtAddr 、 gFft512TwiddleFactorsBufH . numBytes 、 ENDIAN_CHANGE 、 DATA_BUFF_IS_CACHED );           sptContext . kernelParList [ np ]. paramType= RSDK_SPT_PARAM_TYPE_ADDR ; sptContext 。 kernelParList [ np ++ ]。 paramValue = ( uintptr_t ) gFft512BlackmanWindowBufH 。 phyAddr ;   sprintf (ファイル名、 " %s% s " 、 FILE_IN_PATH 、 "fft512_win_blackman.dat" ); DbgReadFileConvert ( fileName 、 0 、 ( char * ) gFft512BlackmanWindowBufH . virtAddr 、 gFft512BlackmanWindowBufH . numBytes 、 ENDIAN_CHANGE 、 DATA_BUFF_IS_CACHED );   sptContext . kernelParList [ np ]. paramType= RSDK_SPT_PARAM_TYPE_VALUE ; sptContext . kernelParList [ np ++ ]. paramValue = 3 ; /* 出力シフトなし */ sptContext . kernelParList [ np ]. paramType= RSDK_SPT_PARAM_TYPE_LAST ;   印刷リスト: gSptModuleCodeRelocBufH.phyAddr: 0x34000000 gSdadcSampleBufferBufH[0].phyAddr: 0x28000000 gSdadcSampleBufferBufH[1].phyAddr: 0x28003000 gSdadcSampleBufferBufH[2].phyAddr: 0x28006000 gSdadcSampleBufferBufH[3].phyAddr: 0x28009000 gRadarCubeResultsBufH.phyAddr: 0x34002000 gFft512TwiddleFactorsBufH.phyAddr: 0x340bd000 gFft512BlackmanWindowBufH.phyAddr: 0x340bf000 Re: S32R45 SptEcsIsrCb error! こんにちは、 考えられる原因は次のとおりです: 1. SPT入力とS32DS入力の不一致 SPT カーネル入力が予期された S32DS 構成と一致しませんでした。 PDMA は、SPT カーネルの構成によって決定されたアドレスでメモリを読み取ります。バッファ サイズ、キューブ ベース アドレス、またはチャネル カウントが揃っていない場合、PDMA は無効または予期しないメモリ位置を読み取ろうとする可能性があります → AXI 読み取りエラー。   2. 作業レジスタ(WR_x)の設定が正しくないか破損している PDMA が無効または誤って構成されたバッファを指す作業レジスタを使用する場合、AXI ファブリックは不正な読み取り要求を受信し、バス エラーをトリガーします。 https://community.nxp.com/t5/Other-NXP-Products/SPT3-1-1024-128-16range-don-t-work/mp/1621567   3. 同期PDMA実行モードと非同期PDMA実行モード .sync → .async .syncでモードでは、PDMA は誤った構成 (バッファ ポインタ、依存関係など) により満たされない可能性のある条件を待機します。 これにより、エラー フラグが蓄積され、PDMA エンジンが無効な読み取りを繰り返し試行すると AXI エラーが発生する可能性があります。   4. データ幅またはフォーマットが間違っている(例:WR_16とWR_11) PDMA が 16 ビットの複合データを期待しているが、ターゲット レジスタ/バッファが異なる幅/レイアウトに設定されている場合、AXI 読み取りバーストが不整合になる可能性があり、プロトコル エラー → AXI 読み取りエラーが発生します。   5. AXIプロトコルレベルのエラー(一般的な原因) S32R45 に固有のものではありませんが、AXI 読み取りエラー メカニズムは普遍的に適用されます。 バースト長またはサイズが無効です マップされていないアドレスまたは保護されたアドレスからの読み取りの試み スレーブタイムアウトまたは応答しないターゲット アップストリームの問題による読み取り応答エラー(SLVERR または DECERR) PDMA が不正な AXI トランザクションを生成すると、AXI インターコネクトは SLVERR を返します。これは PDMA 読み取りエラーとして表示されます。 あなたのケースで最も可能性の高い原因 両方のログに基づくと、主な容疑者は次のとおりです。 間違ったWR_xレジスタ(特にWR_5 / WR_16の選択) 非常に一般的には誤って構成され、無効な AXI 読み取りにつながります。 SPTカーネル入力とS32DS入力の不一致 以前のケースでは、見落とされ、根本原因として検証されることがよくあります。 PDMA同期モードが依存関係のデッドロックを引き起こす .syncを切り替えてみる→ .asyncデバッグ用。 よろしくお願いいたします。 ピーター     Re: S32R45 SptEcsIsrCb error! こんにちはピーター、 レーダー フロントエンドの波形サンプリング ポイントの数を 2 倍にすると、エラーは発生しなくなりましたが、チャープ バッファのサイズは変更されていません。問題をさらに分析するのにご協力ください。どうもありがとうございます。 Re: S32R45 SptEcsIsrCb error! こんにちは、 シナリオにおける最も可能性の高い根本原因: カーネルの予想されるチャープピッチと実際のバッファレイアウト間のストライド/アライメントの不一致 - サンプルを 2 倍にするとバーストサイズが揃い、バグがマスクされます。 WR_x 選択 / データ幅の不一致 (実数 vs 複素数、16 ビット vs その他)。サンプル数が変化すると偶然に修正されます。 kernelParList 内のパラメータ順序/タイプの混同 (ADDR と VALUE) が、特定のサイズの場合にのみ発生します。ミラー スレッドには同様のパラメータ シーケンスが示されており、インデックスをスリップするのは簡単です。 WR 24ビットオフセットエッジは、2倍にすると異なるパッキング/レイアウトで消えます。 よろしくお願いいたします。 ピーター
View full article
i.MX95 VPU H265 latency and performance(v4l2h265enc/v4l2h265dec) Hello, I am currently evaluating the H265 decode → encode pipeline on i.MX95 and I am observing significantly worse latency and stability compared to i.MX8MP, using similar workloads and configurations. Context On i.MX8MP, using: imxvpudec_h265 vpuenc_hevc I am able to achieve: Very low end-to-end latency (≈ 10 ms) Stable operation with multiple streams No visible freezes or artifacts On i.MX95, using: v4l2h265dec v4l2h265enc I observe: ~90 ms latency for a single decode → encode pipeline Freezes and visual artifacts when running 4 simultaneous camera streams Test pipeline To reproduce the issue, I used IP cameras (H265 over RTSP) with the following pipeline: test-launch "( rtspsrc location=rtsp://10.42.0.85 drop-on-latency=true latency=0 buffer-mode=4 ! rtph265depay ! h265parse config-interval=1 ! v4l2h265dec ! v4l2h265enc ! rtph265pay name=pay0 pt=96 )" This pipeline works correctly with a single camera, but when scaling to 4 cameras, freezes and artifacts start to appear. Questions Why is the H265 VPU pipeline on i.MX95 significantly more latent than on i.MX8MP? Is DMABUF zero-copy fully supported between v4l2h265dec and v4l2h265enc on i.MX95? If not, is there an implicit memory copy that could explain the additional latency and bandwidth pressure? Are there known limitations in the current i.MX95 VPU driver regarding: Low-latency operation Multi-stream decode + encode Internal buffering depth Are there recommended V4L2 controls or io-modes (capture/output-io-mode) to minimize latency on i.MX95? Is the i.MX95 VPU driver expected to reach performance parity with i.MX8MP in future BSP releases, or is the higher latency an inherent design tradeoff? Goal My objective is real-time, low-latency video processing (decode → process → encode), similar to what is achievable on i.MX8MP. Thank you for your support. Re: i.MX95 VPU H265 latency and performance(v4l2h265enc/v4l2h265dec) Hello, Which BSP version are you using on i.MX8MP and i.MX95 to recreate this issue? Are you using the same GST pipeline (other than the decoder/encoder elements) on both 8MP and 95? AFAIK, there is no known limitation that results in high latency on i.MX95. On i.MX95, encoder support mmap and dmabuf, which can make a pipeline to transfer dma-buf without copy b/w decoder and encoder. Does the IP camera encode without B frames? Then we can disable decode frame reorder, which will reduce the latency. Please check this. You can disable frame reorder using below v4l2 control " v4l2h264dec extra-controls="decode,display_delay_enable=1,display_delay=0" " You can list all v4l2 controls using below command: v4l2-ctl -l -d Regards Re: i.MX95 VPU H265 latency and performance(v4l2h265enc/v4l2h265dec) The kernel versions: imx95: 6.6.101-0 imx8mp: 6.6.84-0 Yes it is the same gstreamer pipeline. The IP camera encode without B frames. I tired your command and it doesn't solve the issue. There are still artifacts on the screen and the latency is high. However qualitatively speaking, it seems to remove the freezes. ``` v4l2-ctl -l -d /dev/v4l/by-path/platform-4c480000.vpu-video-index0 User Controls min_number_of_capture_buffers 0x00980927 (int) : min=1 max=32 step=1 default=1 value=1 flags=read-only thumbnail_mode 0x00981901 (bool) : default=0 value=0 flags=write-only Codec Controls h264_profile 0x00990a6b (menu) : min=0 max=4 default=0 value=0 (Baseline) hevc_profile 0x00990b67 (menu) : min=0 max=0 default=0 value=0 (Main) display_delay 0x00990b8d (int) : min=0 max=0 step=1 default=0 value=0 display_delay_enable 0x00990b8e (bool) : default=0 value=0 ``` ``` v4l2-ctl -l -d /dev/v4l/by-path/platform-4c480000.vpu-video-index1 User Controls horizontal_flip 0x00980914 (bool) : default=0 value=0 vertical_flip 0x00980915 (bool) : default=0 value=0 rotate 0x00980922 (int) : min=0 max=270 step=90 default=0 value=0 flags=modify-layout min_number_of_output_buffers 0x00980928 (int) : min=1 max=32 step=1 default=1 value=1 flags=read-only Codec Controls video_gop_size 0x009909cb (int) : min=0 max=2047 step=1 default=30 value=30 video_bitrate_mode 0x009909ce (menu) : min=0 max=1 default=1 value=1 (Constant Bitrate) flags=update video_bitrate 0x009909cf (int) : min=1 max=1500000000 step=1 default=2097152 value=2097152 frame_level_rate_control_enable 0x009909d7 (bool) : default=1 value=1 h264_mb_level_rate_control 0x009909da (bool) : default=1 value=1 number_of_mbs_in_a_slice 0x009909dc (int) : min=0 max=262143 step=1 default=1 value=1 slice_partitioning_method 0x009909dd (menu) : min=0 max=1 default=0 value=0 (Single) force_key_frame 0x009909e5 (button) : value=0 flags=write-only, execute-on-write intra_refresh_period 0x009909ec (int) : min=0 max=2160 step=1 default=0 value=0 intra_refresh_period_type 0x009909ed (menu) : min=0 max=1 default=1 value=1 (Cyclic) h264_i_frame_qp_value 0x00990a5e (int) : min=0 max=51 step=1 default=30 value=30 h264_p_frame_qp_value 0x00990a5f (int) : min=0 max=51 step=1 default=30 value=30 h264_b_frame_qp_value 0x00990a60 (int) : min=0 max=51 step=1 default=30 value=30 h264_minimum_qp_value 0x00990a61 (int) : min=0 max=51 step=1 default=8 value=8 h264_maximum_qp_value 0x00990a62 (int) : min=0 max=51 step=1 default=51 value=51 h264_8x8_transform_enable 0x00990a63 (bool) : default=1 value=1 h264_cpb_buffer_size 0x00990a64 (int) : min=0 max=18750000 step=1 default=0 value=0 h264_entropy_mode 0x00990a65 (menu) : min=0 max=1 default=1 value=1 (CABAC) h264_i_frame_period 0x00990a66 (int) : min=0 max=2047 step=1 default=0 value=0 h264_level 0x00990a67 (menu) : min=0 max=16 default=14 value=14 (5) h264_loop_filter_alpha_offset 0x00990a68 (int) : min=-6 max=6 step=1 default=0 value=0 h264_loop_filter_beta_offset 0x00990a69 (int) : min=-6 max=6 step=1 default=0 value=0 h264_loop_filter_mode 0x00990a6a (menu) : min=0 max=2 default=0 value=0 (Enabled) h264_profile 0x00990a6b (menu) : min=0 max=4 default=4 value=4 (High) vertical_size_of_sar 0x00990a6c (int) : min=0 max=65535 step=1 default=0 value=0 horizontal_size_of_sar 0x00990a6d (int) : min=0 max=65535 step=1 default=0 value=0 aspect_ratio_vui_enable 0x00990a6e (bool) : default=0 value=0 vui_aspect_ratio_idc 0x00990a6f (menu) : min=0 max=17 default=0 value=0 (Unspecified) h264_constrained_intra_pred 0x00990a7f (int) : min=0 max=1 step=1 default=0 value=0 h264_chroma_qp_index_offset 0x00990a80 (int) : min=-12 max=12 step=1 default=0 value=0 hevc_minimum_qp_value 0x00990b58 (int) : min=0 max=51 step=1 default=8 value=8 hevc_maximum_qp_value 0x00990b59 (int) : min=0 max=51 step=1 default=51 value=51 hevc_i_frame_qp_value 0x00990b5a (int) : min=0 max=51 step=1 default=30 value=30 hevc_p_frame_qp_value 0x00990b5b (int) : min=0 max=51 step=1 default=30 value=30 hevc_b_frame_qp_value 0x00990b5c (int) : min=0 max=51 step=1 default=30 value=30 hevc_profile 0x00990b67 (menu) : min=0 max=0 default=0 value=0 (Main) hevc_level 0x00990b68 (menu) : min=0 max=8 default=7 value=7 (5) hevc_loop_filter 0x00990b6c (menu) : min=0 max=2 default=1 value=1 (Enabled) hevc_loop_filter_beta_offset 0x00990b6d (int) : min=-6 max=6 step=1 default=0 value=0 hevc_loop_filter_tc_offset 0x00990b6e (int) : min=-6 max=6 step=1 default=0 value=0 hevc_refresh_type 0x00990b6f (menu) : min=0 max=2 default=2 value=2 (IDR) hevc_num_of_i_frame_b_w_2_idr 0x00990b70 (int) : min=0 max=2047 step=1 default=0 value=0 hevc_constant_intra_prediction 0x00990b72 (int) : min=0 max=1 step=1 default=0 value=0 hevc_strong_intra_smoothing 0x00990b76 (int) : min=0 max=1 step=1 default=1 value=1 hevc_tmv_prediction 0x00990b79 (int) : min=0 max=1 step=1 default=1 value=1 prepend_sps_and_pps_to_idr 0x00990b84 (int) : min=0 max=1 step=1 default=1 value=1 frame_skip_mode 0x00990b86 (menu) : min=0 max=2 default=0 value=0 (Disabled) average_qp_value 0x00990b91 (int) : min=0 max=51 step=1 default=0 value=0 flags=read-only ``` Re: i.MX95 VPU H265 latency and performance(v4l2h265enc/v4l2h265dec) The BSP versions are : imx8mp: lf-6.6.52-2.2.0 imx95: lf-6.6.52-2.2.1 Thank you Re: i.MX95 VPU H265 latency and performance(v4l2h265enc/v4l2h265dec) Yes the IP camera encode without B frames. I tried your command and it doesn't solve the issue. There are still artifacts on the screen and the latency is high. However qualitatively speaking, it seems to remove the freezes. Re: i.MX95 VPU H265 latency and performance(v4l2h265enc/v4l2h265dec) ok Also please confirm the B frame question I mentioned above. Regards Re: i.MX95 VPU H265 latency and performance(v4l2h265enc/v4l2h265dec) Hello, To confirm: the IP cameras encode without B frames (I-P only). I have applied display_delay_enable=1, display_delay=0 on the decoder. This helped remove freezes, but the latency remains at ~90 ms. To isolate the bottleneck, I used the GStreamer element-latency tracer on this pipeline: ``` rtspsrc location=rtsp://... drop-on-latency=true latency=0 buffer-mode=4 !  rtph265depay ! h265parse config-interval=1 !  v4l2h265dec extra-controls="decode,display_delay_enable=1,display_delay=0" capture-io-mode=4 output-io-mode=4 !  v4l2h265enc extra-controls="encode,video_bitrate_mode=1,video_bitrate=2097152,frame_level_rate_control_enable=0,video_gop_size=30" capture-io-mode=4 output-io-mode=4 !  h265parse config-interval=1 ! rtph265pay name=pay0 pt=96 ``` Per-element latency results (640x480 @ 30fps, single stream): v4l2h265enc: ~67 ms v4l2h265dec ~2 ms all other elements < 1 ms The encoder alone accounts for ~67 ms (~2 frame periods). This is consistent across runs. The decoder is fine at ~2 ms. I have tried: frame_level_rate_control_enable=0 capture-io-mode=4 and output-io-mode=4 (DMABUF) on both encoder and decoder Minimal queue buffering between elements (max-size-buffers=1) None of these significantly reduce the encoder latency. My questions, focused on the encoder: Is the Wave6 encoder expected to hold 2 frames internally before producing output? Is there a way to reduce this internal buffering (similar to display_delay=0 on the decoder side)? Does output-io-mode=5 (DMABUF_IMPORT) work on the encoder to achieve zero-copy from upstream? Would this help latency? Is there a V4L2 control or driver parameter to enable a low-latency / zero-delay encoding mode on the Wave6? On i.MX8MP, vpuenc_hevc achieves ~10 ms for the same workload. Is this latency gap with v4l2h265enc on i.MX95 expected to improve in future BSP releases? Thank you for your help.
View full article
调试工具在使用最新版 SDK_25_12_00 时显示为灰色,在使用旧版 SDK_25_03_00 时工作正常 运行 MCUXpresso IDE V25.6.136 版+ 带有 SDK_25_12_00 的 evkmimxrt685 板。调试开始时,所有调试工具(恢复...)都显示为灰色,无法运行项目。 使用旧版 SDK_25_03_00 可以正常工作,但使用 SDK_25_06_00 和 SDK_25_09_00 会出现同样的问题。 如何恢复调试工具 Re: Debug tools greyed out with latest SDK_25_12_00, work fine with older SDK_25_03_00 你好,卡洛斯,包括 hello world 在内的所有示例都出现了这种情况。它总是停在"void ResetISR(void) 函数的第一行,即 startup_mimxrt685s.c 中的 __asm volatile ("cpsid i") 行(第 381 行)。文件。我正在尝试运行 evkmimxrt685_dsp_mu_polling_cm33。该示例在 25.03 版本中运行正常。之后的所有版本(06、09、12)都有这个问题。对于 24.03 之后的 SDK 版本,我是否需要在集成开发环境中进行一些更改?我有截图,但如何发布呢?谢谢@bobvr Re: Debug tools greyed out with latest SDK_25_12_00, work fine with older SDK_25_03_00 你好,卡洛斯,我正在上传截图> 包括 hello world 在内的所有示例都出现了这种情况。它总是停在"void ResetISR(void) 函数的第一行,即启动目录下 startup_mimxrt685s.c 文件中的 __asm volatile ("cpsid i") 行(第 381 行)。它从未进入 main() 开始运行。 我试图运行 evkmimxrt685_dsp_mu_polling_ cm33。cm33。该示例在 25.03 版本中运行正常。之后的所有版本(06、09、12)都有这个问题。对于 24.03 之后的 SDK 版本,我是否需要在集成开发环境中做一些更改? 谢谢 bobvr Re: Debug tools greyed out with latest SDK_25_12_00, work fine with older SDK_25_03_00 你好@bobvr 能否请您介绍一下您的计算机使用的是哪个操作系统?Linux、Windows 10 还是 Windows 11? 能否请您检查一下 EVK 的 BOOT_SEL 是否选择正确? Re: Debug tools greyed out with latest SDK_25_12_00, work fine with older SDK_25_03_00 我正在戴尔 Alder Lake 台式机上运行 Windows 11。启动跳线 (JP1) 处于打开状态,根据手册(MIMXRT685-AUD-EVKUM 修订版 3-2023 年 7 月 21 日),这是默认设置。我想这就是您所说的"查看 EVK" 的 BOOT_SEL 的意思。谢谢 bobvr Re: Debug tools greyed out with latest SDK_25_12_00, work fine with older SDK_25_03_00 你好@bobvr 感谢您分享您的设置细节。 能否请您对闪存进行一次大规模擦除,然后重新进行调试? 为此,请在快速启动面板上更改链接服务器操作 然后使用 LinkServer 探测器将其返回到调试模式。 如果在此过程中出现任何错误信息,请分享截图。 Re: Debug tools greyed out with latest SDK_25_12_00, work fine with older SDK_25_03_00 卡洛斯,我试图用链接服务器进行大规模清除,但得到了错误信息--截图附后。 谢谢 Re: Debug tools greyed out with latest SDK_25_12_00, work fine with older SDK_25_03_00 卡洛斯,谢谢。在此之前,我想让您知道,我一直使用世纪佳缘 J-Link 探头,使用世纪佳缘 J-Link 探头" 菜单选项可进行"清除闪存操作。我应该用它清除还是用你上面提到的链接服务器探针清除? Re: Debug tools greyed out with latest SDK_25_12_00, work fine with older SDK_25_03_00 你好,卡洛斯,我使用 Segger J-Link 探头(不是链接服务器探头,因为该固件已被 Segger 固件覆盖)删除了闪存。 我知道我必须使用 Segger 探针来调试 ARM 内核和 HiFi4 DSP。我还将 Segger 固件更新到了最新的 8.98 版本。 我删除了调试启动文件,删除了工作区以在启动时生成一个新文件,还重新启动了板。还是同样的问题。 它说调试会话正在运行,但我无法调试。 正如我所说,03 之后的所有版本(06、09 和 12)都会出现这种情况。 它停在 startup_mimxrt685s.c 处文件。 在调试器控制台中,我确实看到了一条警告信息,但这可能是无害的。 "警告:无法将 "main "从主机编码 (CP1252) 转换为 UTF-32。 这种情况通常不会发生,请提交错误报告。 监测执行器 setrestartonClose=1 请告知下一步措施。谢谢 bobvr。 Re: Debug tools greyed out with latest SDK_25_12_00, work fine with older SDK_25_03_00 你好@bobvr 感谢您分享您正在使用的产品。 如果尝试使用链接服务器调试,问题是否仍然存在?如果您收到错误信息,请与我们分享。
View full article
RT1170 使用同步动态随机存取存储器(SDRAM) 处理堆和堆栈 我按照https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-debugging-when-application-is-built-for-SDRAM/m-p/1374145/highlight/true#M17210和 RT1170_BriefOverview_v210.pdf 中提到的步骤进行了操作。 我正在开发一个需要大量头部内存的应用程序。 按照提供的步骤,使用 RT1170_BriefOverview_v210.pdf 中提到的修改刷新 hello world,我可以在调试模式下使用同步动态随机存取存储器(SDRAM)。 但是在这种变化之后,同步动态随机存取存储器(SDRAM)也用于存储代码。 在我的应用程序中,我希望代码存储在闪存中,而 BOARD_SDRAM 仅用于堆和堆栈部分。 我将把我的应用程序闪存到闪存中,该应用程序的堆和栈部分将使用 BOARD_SDRAM。 请指导我进行所需的更改。 i.MX-RT1170 MIMXRT1170-EVK Re: RT1170 Use SDRAM for Heap and Stack 按照恩智浦支持中的步骤,我得以在 RT1170 EVKB 上加载多核项目(如何在 RT1176 & [RT1170] 中调试双核项目)。 当我能够从同步动态随机存取存储器(SDRAM)运行后,在 Master/Core M7 项目中,我进入了项目设置-> C/C++ 版本-> 设置-> 托管链接器脚本并禁用了 " 将应用程序链接到 RAM " 设置。 然后我得以刷新二进制文件,并确认应用程序在 RESET 时从闪存运行,并成功地将 M4 应用程序从闪存复制到同步动态随机存取存储器(SDRAM)。 Re: RT1170 Use SDRAM for Heap and Stack 你好@sibrain-himanshu、 感谢您对 NXP MIMXRT 系列的关注! 问题的根本原因在于您使用了这个步骤6: 这会将整个图像加载到 RAM 中执行,也是生成非 XIP 图像的选项。 对于您的应用场景,在启用和配置同步动态随机存取存储器(SDRAM)之后,您只需要在 MCUXpresso IDE 中正确配置 Head/Stack: 致以最诚挚的问候, Gavin Re: RT1170 Use SDRAM for Heap and Stack 你好@Gavin_Jia 在步骤 6 的基础上做了你建议的更改,并在预处理器中使用了 "XIP_BOOT_HEADER_DCD_ENABLE=1" 宏之后,我的固件使用了同步动态随机存取存储器(SDRAM)。 但我的应用程序是用 C++ 编写的,所以我最初对它进行了与 hello world C 应用程序相同的修改,但没有成功。 因此,还在 C++ 预处理器宏中添加了"USE_SDRAM" 和"XIP_BOOT_HEADER_DCD_ENABLE=1" 宏,结果成功了。 C++ 预处理器宏 C 预处理器宏 感谢您的帮助。
View full article
i.MX6ULL: Issue with 132MHz sdio clock out for BT+WiFi chip(Qualcomm QCA9377) Hello NXP community members, I have a custom board with an IMX6ULL and Qualcomm BT+Wifi combo chip on it. This project is based on Yocto kirkstone, linux-imx 5.15.71 kernel version. The communication method between mx6ull and qca9377 is sdio. I have a few questions about the occasional communication errors that occur during sdio communication between mx6ull and qca9377. 1. Set dts to use sdio clock speed of 132MHz imx6ul-14x14-evk.dtsi &usdhc1 { pinctrl-names = "default", "state_100mhz", "state_200mhz"; pinctrl-0 = <&pinctrl_usdhc1>; pinctrl-1 = <&pinctrl_usdhc1_100mhz>; pinctrl-2 = <&pinctrl_usdhc1_200mhz>; bus-width = <4>; vmmc-supply = <&reg_sd1_vmmc>; pm-ignore-notify; keep-power-in-suspend; non-removable; status = "okay"; }; &iomuxc { pinctrl_usdhc1: usdhc1grp { fsl,pins = < MX6UL_PAD_SD1_CMD__USDHC1_CMD 0x17059 MX6UL_PAD_SD1_CLK__USDHC1_CLK 0x10071 MX6UL_PAD_SD1_DATA0__USDHC1_DATA0 0x17059 MX6UL_PAD_SD1_DATA1__USDHC1_DATA1 0x17059 MX6UL_PAD_SD1_DATA2__USDHC1_DATA2 0x17059 MX6UL_PAD_SD1_DATA3__USDHC1_DATA3 0x17059 MX6UL_PAD_GPIO1_IO00__GPIO1_IO00 0x130b0 >; }; pinctrl_usdhc1_100mhz: usdhc1grp100mhz { fsl,pins = < MX6UL_PAD_SD1_CMD__USDHC1_CMD 0x170b9 MX6UL_PAD_SD1_CLK__USDHC1_CLK 0x100b9 MX6UL_PAD_SD1_DATA0__USDHC1_DATA0 0x170b9 MX6UL_PAD_SD1_DATA1__USDHC1_DATA1 0x170b9 MX6UL_PAD_SD1_DATA2__USDHC1_DATA2 0x170b9 MX6UL_PAD_SD1_DATA3__USDHC1_DATA3 0x170b9 >; }; pinctrl_usdhc1_200mhz: usdhc1grp200mhz { fsl,pins = < MX6UL_PAD_SD1_CMD__USDHC1_CMD 0x170f9 MX6UL_PAD_SD1_CLK__USDHC1_CLK 0x100f9 MX6UL_PAD_SD1_DATA0__USDHC1_DATA0 0x170f9 MX6UL_PAD_SD1_DATA1__USDHC1_DATA1 0x170f9 MX6UL_PAD_SD1_DATA2__USDHC1_DATA2 0x170f9 MX6UL_PAD_SD1_DATA3__USDHC1_DATA3 0x170f9 >; }; }; 2.  mmc0 info # cat /sys/kernel/debug/mmc0/ios clock: 132000000 Hz actual clock: 132000000 Hz vdd: 21 (3.3 ~ 3.4 V) bus mode: 2 (push-pull) chip select: 0 (don't care) power mode: 2 (on) bus width: 2 (4 bits) timing spec: 6 (sd uhs SDR104) signal voltage: 1 (1.80 V) driver type: 0 (driver type B) 3. Sometimes the sdio communication error log like below is printed AR6000: SDIO bus operation failed! MMC stack returned : -84 __HIFReadWrite, addr:0X001000, len:00000256, Read , Sync Debug Assert Caught, File /usr/src/debug/kernel-module-qca9377/3.1-r0/git/CORE/SERVICES/HIF/sdio/linux/native_sdio/src/hif.c, Line: 1459, Test:status == A_OK || status == A_ECANCELED "Change sdio clock speed (132MHz -> 50MHz)" 1. set dts to use sdio clock speed of 50MHz. imx6ul-14x14-evk.dtsi &usdhc1 { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_usdhc1>; bus-width = <4>; vmmc-supply = <&reg_sd1_vmmc>; pm-ignore-notify; keep-power-in-suspend; non-removable; status = "okay"; }; 2.  mmc0 info # cat /sys/kernel/debug/mmc0/ios clock: 50000000 Hz actual clock: 44000000 Hz vdd: 21 (3.3 ~ 3.4 V) bus mode: 2 (push-pull) chip select: 0 (don't care) power mode: 2 (on) bus width: 2 (4 bits) timing spec: 2 (sd high-speed) signal voltage: 0 (3.30 V) driver type: 0 (driver type B) 3. sdio communication error log is not displayed. 1. The sdio communication between mx6ull and qca9377 seems unstable when the sdio clock is set to 132MHz. Is there a way to improve it by modifying the dts value? 2. If not possible, what value do you recommend using for the sdio clock value? Thank you in advance. Best regards  i.MX6 All i.MX6UL Linux Yocto Project Re: i.MX6ULL: Issue with 132MHz sdio clock out for BT+WiFi chip(Qualcomm QCA9377) refer to the data sheet, Signaling level of SDR104/SDR50 mode is 1.8 V. Pls check your HW and double confirm this Re: i.MX6ULL: Issue with 132MHz sdio clock out for BT+WiFi chip(Qualcomm QCA9377) Dear  Joan Xie, Thank you for fast reply.   Let me explain ​a little more.   <HW> - Soc is NXP mx6ull processor (MCIMX6Y2DVM09AB) - mmc0 is connected to Qualcomm BT/WiFi Combo chip (sdio connection) -> 132MHz, 1.8V - mmc1 connected to 8G eMMC  -> 132MHz, 1.8V   <mmc0>     # cat /sys/kernel/debug/mmc0/ios     clock:     132000000 Hz     actual clock:  132000000 Hz     vdd:      21 (3.3 ~ 3.4 V)     bus mode:    2 (push-pull)     chip select:  0 (don't care)     power mode:   2 (on)     bus width:   2 (4 bits)     timing spec:  6 (sd uhs SDR104)     signal voltage: 1 (1.80 V)     driver type:  0 (driver type B)   <mmc1>     # cat /sys/kernel/debug/mmc1/ios     clock:     132000000 Hz     vdd:      21 (3.3 ~ 3.4 V)     bus mode:    2 (push-pull)     chip select:  0 (don't care)     power mode:   2 (on)     bus width:   3 (8 bits)     timing spec:  9 (mmc HS200)     signal voltage: 1 (1.80 V)     driver type:  0 (driver type B)   <Description> - Communication with the eMMC connected to mmc1 is running at 132MHz, 1.8V and there are no issues. - The sdio communication with the BT/WiFi chip connected to mmc0 is also driven at 132MHz, 1.8V, but intermittent sdio communication errors occur.   More questions is loke below: 1. For eMMC(mmc1), it seems to be guaranteed for HS200 (132MHz/1.8V), but for SDIO(mmc0) it seems to be guaranteed only up to 104MHz in SDR104 mode. Check please? 2. If so, is the maximum sdio clock speed guaranteed by the mx6ull chip up to 104MHz?    (I would like to confirm whether the MX6ULL chip can guarantee SDIO 132MHz clock speed.) Re: i.MX6ULL: Issue with 132MHz sdio clock out for BT+WiFi chip(Qualcomm QCA9377) Thank you for your fast reply. About question 1, I think I was a big mistaken. Sorry about that. And I checked that you  mentioned like below ""SD/SDIO UHS-I mode (up to 208 MHz in SDR mode, up to 50 MHz in DDR mode)" So, if we use sdr104 in mmc0, the maximum clock is 208MHz, so is it possible to guarantee a 132MHz clock? Re: i.MX6ULL: Issue with 132MHz sdio clock out for BT+WiFi chip(Qualcomm QCA9377) 1. For eMMC(mmc1), it seems to be guaranteed for HS200 (132MHz/1.8V), but for SDIO(mmc0) it seems to be guaranteed only up to 104MHz in SDR104 mode. Check please? >refer to the data sheet, can up to the UHS-I SDR104 mode 104MB/s max, not 104Mhz max, refer to the RM: SD/SDIO UHS-I mode (up to 208 MHz in SDR mode, up to 50 MHz in DDR mode) 2. If so, is the maximum sdio clock speed guaranteed by the mx6ull chip up to 104MHz? (I would like to confirm whether the MX6ULL chip can guarantee SDIO 132MHz clock speed.) >you can refer to the data sheet, for SDR104, the frequency can up to the 200Mhz, we have tested SDR104 on the mmc0 up to the 198Mhz, refer to your log, it seems your mmc1 works under  HS200?you can measure the clock by oscilloscope Re: i.MX6ULL: Issue with 132MHz sdio clock out for BT+WiFi chip(Qualcomm QCA9377) yes, you can refer to the dtsi file, which set the 132M as default, you also can dump the clock tree to check if the clock is 132Mhz or not Re: i.MX6ULL: Issue with 132MHz sdio clock out for BT+WiFi chip(Qualcomm QCA9377) Thank you joanxie, I'll check more to see if it's actually a clock speed issue and ask again. Thanks. Re: i.MX6ULL: Issue with 132MHz sdio clock out for BT+WiFi chip(Qualcomm QCA9377) I debugged the above content in SW. Please answer my questions after confirming the details. 1. Chip Errata for the i.MX 6ULL     "ERR010450 MMC: EMMC can only run under or equal to 150 MHz"     https://www.nxp.com/docs/en/errata/IMX6ULLCE.pdf        2. SW debug 1) error value define     include/uapi/asm-generic/errno.h:67:#define EILSEQ 84 /* Illegal byte sequence */ 2) EILSEQ setting location     - cmd         drivers/mmc/host/sdhci.c: sdhci_cmd_irq()             if (intmask & (SDHCI_INT_TIMEOUT | SDHCI_INT_CRC | SDHCI_INT_END_BIT | SDHCI_INT_INDEX)) {                 if (intmask & SDHCI_INT_TIMEOUT)                     host->cmd->error = -ETIMEDOUT;                 else                     host->cmd->error = -EILSEQ;                         - data         drivers/mmc/host/sdhci.c: sdhci_data_irq()             if (intmask & SDHCI_INT_DATA_TIMEOUT)                 host->data->error = -ETIMEDOUT;             else if (intmask & SDHCI_INT_DATA_END_BIT)                 host->data->error = -EILSEQ; 3) log     [418.109795] [sdhci_cmd_irq()] intmask = 0xa0001     [418.114178] [sdhci_data_irq()] intmask = 0x200002     [418.118999] AR6000: SDIO bus operation failed! MMC stack returned : -84     [418.125847] __HIFReadWrite, addr:0X000800, len:00000044, Read , Sync     [418.144284] Debug Assert Caught, File /usr/src/debug/kernel-module-qca9377/3.1-r0/git/CORE/SERVICES/HIF/sdio/linux/native_sdio/src/hif.c, Line: 1459, Test:status == A_OK || status == A_ECANCELED 3. SDHCI register 1) intmask value of sdhci_cmd_irq() is 0xa0001     Bit 0  (0x00001)😞 SDHCI_INT_RESPONSE  -> Command response OK     Bit 17 (0x20000)😞 SDHCI_INT_INDEX     -> Command index error     Bit 19 (0x80000)😞 SDHCI_INT_CRC       -> Command CRC error 2) intmask value of sdhci_data_irq() is 0x200002     Bit 1  (0x00002)😞 SDHCI_INT_DATA_END  -> Data OK     Bit 21 (0x200000)😞 SDHCI_INT_DATA_CRC -> Data CRC error 4. guess the casue     According to imx6ull Errata ERR010450,     "SDR104 at 1.8 V can only work below or equal to 150 MHz."     If it can operate at up to 150MHz, it seems likely that cmd/data CRC errors will occur at 132MHz due to timing margins caused by temperature/voltage fluctuations, etc. 5. Question     Currently, we are in a situation where we cannot adjust the value through HW tuning and must respond through SW.     It seems that lowering the sdio clock value can reduce or eliminate the CRC error rate. What is NXP's opinion? Thank you. Re: i.MX6ULL: Issue with 132MHz sdio clock out for BT+WiFi chip(Qualcomm QCA9377) Dear joanxie, Based on what you provided, I tested using the register below. sdhci-esdhc-imx.c #define ESDHC_MIX_CTRL_SMPCLK_SEL (1 << 23) #define ESDHC_MIX_CTRL_AUTO_TUNE_EN (1 << 24) #define ESDHC_MIX_CTRL_FBCLK_SEL (1 << 25)     SMPCLK_SEL        0     AUTO_TUNE_EN   1     FBCLK_SEL            1 1. test 1     1) set AUTO_TUNE_EN 1 -> 0     2) log         [ 39.150703] AR6000: Unregistering with the bus driver     3) wlan0 registration fail         $ ifconfig wlan0 up         ifconfig: SIOCGIFFLAGS: No such device 2. test 2     1) set FBCLK_SEL 1 -> 0     2) log         [ 39.160750] AR6000: Unregistering with the bus driver     3) also wlan0 registration fail         $ ifconfig wlan0 up         ifconfig: SIOCGIFFLAGS: No such device 3. test 3     1) set AUTO_TUNE_EN 1 -> 0 && FBCLK_SEL 1 -> 0     2) System freezes during boot as shown in the log below         [ 18.834619] wlan: loading driver v4.5.25.65         [ 18.894917] hifDeviceInserted: Dumping clocks (50000000,132000000) I tried modifying and testing it by referring to articles in the NXP community, but I was not satisfied with the results. Please note. Thanks for your help Re: i.MX6ULL: Issue with 132MHz sdio clock out for BT+WiFi chip(Qualcomm QCA9377) I consulted from wireless team, they have already verified WIFI with imx6ull via usdhc, and can set max clock is 150Mhz, so for imx6ull side, can support this, and I found some WIFI chip would affect autotunning, so I suggest that you can disable these registers to check, if these aren't your root cause, I suggest that you need check your HW and pcb design, if you couldn't confirm this, you can submit a ticket for SCHEMATIC review Re: i.MX6ULL: Issue with 132MHz sdio clock out for BT+WiFi chip(Qualcomm QCA9377) I consulted from wireless team, they have already verified WIFI with imx6ull via usdhc, and can set max clock is 150Mhz, so for imx6ull side, can support this, and I found some WIFI chip would affect autotunning, so I suggest that you can disable these registers to check, if these aren't your root cause, I suggest that you need check your HW and pcb design, if you couldn't confirm this, you can submit a ticket for SCHEMATIC review Re: i.MX6ULL: Issue with 132MHz sdio clock out for BT+WiFi chip(Qualcomm QCA9377) Dear joanxie, Thank you for fast reply. I'll let you know after check refer to your guide. Have a nice day and weekend! Re: i.MX6ULL: Issue with 132MHz sdio clock out for BT+WiFi chip(Qualcomm QCA9377) this is what I talked about before, the detailed information about auto-tuning affect the failure https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/uSDHC-auto-tuning-and-possible-SDIO-failures/ta-p/1352855 Re: i.MX6ULL: Issue with 132MHz sdio clock out for BT+WiFi chip(Qualcomm QCA9377) Dear joanxie, Thank you for your kind guide. I debugged this issue by referring to the link you provided. 1. patch 1    1) patch using refer to the link you provided       https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/uSDHC-auto-tuning-and-possible-SDIO-failures/ta-p/1352855 2. patch 2    1) add "fsl,sdio-async-interrupt-enabled" on dts file imx6ul-14x14-evk.dtsi: &usdhc1 { fsl,sdio-async-interrupt-enabled; //add this line     2)  below part is enabled sdhci-esdhc-imx.c: usdhc_auto_tuning_mode_sel() /* * If sdio device use async interrupt, it will use DAT[1] to signal * the device's interrupt asynchronous when use 4 data lines. * Then hardware auto tuning circuit MUST NOT check the DAT[1] line, * otherwise auto tuning will be impacted by this async interrupt, * and change the delay cell incorrectly, which then cause data/cmd * errors. * This is the hardware auto tuning circuit limitation. */ if (imx_data->boarddata.sdio_async_interrupt_enabled) auto_tune_buswidth = ESDHC_VEND_SPEC2_AUTO_TUNE_1BIT_EN; After patching the above, the problem was not reproduced through debugging. (sdio clock changing test(50MHz->100MHz->132MHz), ping test, iperf3 test etc..) Just one more question to confirm patch you guide. If I apply this patch, the problem will be fixed, but is there any possibility that it will have other effects on the sdio communication between mx6ull and the wifi chip?   Thank you for your support. Re: i.MX6ULL: Issue with 132MHz sdio clock out for BT+WiFi chip(Qualcomm QCA9377) it's glad to hear these patch work, but in fact the new bsp already merge the, as I known, I don't hear any other exist issue between imx6ull and wifi chip Re: i.MX6ULL: Issue with 132MHz sdio clock out for BT+WiFi chip(Qualcomm QCA9377) Thank you joanxie, I aslo check another yocto version (imx-6.6.52, fslc-6.1.72) I found  similar patch like below on yocto scarthgap imx-6.6.52 version /* * For USDHC, auto tuning circuit can not handle the async sdio * device interrupt correctly. When sdio device use 4 data lines, * async sdio interrupt will use the shared DAT[1], if enable auto * tuning circuit check these 4 data lines, include the DAT[1], * this circuit will detect this interrupt, take this as a data on * DAT[1], and adjust the delay cell wrongly. * This is the hardware design limitation, to avoid this, for sdio * device, config the auto tuning circuit only check DAT[0] and CMD * line. */ if (imx_data->init_card_type == MMC_TYPE_SDIO) auto_tune_buswidth = ESDHC_VEND_SPEC2_AUTO_TUNE_1BIT_EN; esdhc_clrset_le(host, ESDHC_VEND_SPEC2_AUTO_TUNE_MODE_MASK, auto_tune_buswidth | ESDHC_VEND_SPEC2_AUTO_TUNE_CMD_EN, ESDHC_VEND_SPEC2); but not patched on yocto scarthgap fslc-6.1.72 version. I will check other yocto version using your guidance.  Thank you for support.
View full article