Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement The i.MX Android O8.0.0_1.0.0 GA release is now available from IMX_SW page. Overview -> BSP Updates and Releases -> Android 8.0.0 Oreo (O8.0.0_1.0.0, 4.9 kernel) Files available: # Name Description 1 android_O8.0.0_1.0.0_docs.tar.gz i.MX Android O8.0.0_1.0.0 BSP Documentation 2 imx-o8.0.0_1.0.0_ga.tar.gz i.MX Android O8.0.0_1.0.0 proprietary surce code for i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo  i.MX 6Sololite, i.MX6SX and i.MX7D 3 android_O8.0.0_1.0.0_image_6dqpsabreauto.tar.gz Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE for Automotive Infotainment based on i.MX 6QuadPlus, i.MX 6Quad, and i.MX 6DualLite 4 android_O8.0.0_1.0.0_image_6dqpsabresd.tar.gz Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE Platform and SABRE Board based on i.MX 6QuadPlus, i.MX 6Quad and i.MX 6DualLite. 5 android_O8.0.0_1.0.0_image_6slevk.tar.gz Binary Demo Files of Android O8.0.0_1.0.0 BSP - i.MX 6Sololite evaluation kit. 6 android_O8.0.0_1.0.0_image_6sxsabresd.tar.gz Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE Board based on i.MX 6SoloX 7 android_O8.0.0_1.0.0_image_6sxsabreauto.tar.gz Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE for Automotive infotainment based on i.MX 6SoloX 8 android_O8.0.0_1.0.0_image_7dsabresd.tar.gz Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE Board based on i.MX 7Dual 9 fsl_aacp_dec_O8.0.0_1.0.0.tar.gz AAC Plus Codec for O8.0.0_1.0.0 10 android_O8.0.0_1.0.0_tools.tar.gz Manufacturing Toolkit and VivanteVTK for O8.0.0_1.0.0   Supported Hardware SoC/Boards: i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-SD board and platform i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-AI board and platform i.MX 6SoloLite EVK platform i.MX 6SoloX SABRE-SD board and platforms i.MX 6SoloX SABRE-AI board and platforms i.MX 7Dual SABRE-SD board and platform   Changes: Compared to the N7.1.2_2.0.0 release, this release has the following major changes: Upgraded the Android code base from android-7.1.2_r9 to android-8.0.0_r25. Removed the device partition and added the vendor partition. Enabled ION-based gralloc and EGL. Feature: For features please consult the release notes.   Known issues For known issues and more details please consult the Release Notes. Android i.MX6_All i.MX6DL i.MX6Dual i.MX6DualPlus6QuadPlus i.MX6Quad i.MX6S i.MX6SL i.MX6SoloX i.MX7Dual Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement codeaurora use mirrors below: git --config --global url." ".insteadOf " https://source.codeaurora.org" can be any one of below: https://beijing.source.codeaurora.org https://shanghai.source.codeaurora.org if manifest.xml use "git://source.codeaurora.org" you must be edit ~/.gitconfig add line below: [url "https://beijing.source.codeaurora.org"] insteadOf = git://codeaurora.org Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement 运行repo sync后完整输出信息是这样的:fatal: unable to access 'https://source.codeaurora.org/external/imx/aosp/platform/packages/apps/SoundRecorder/': GnuTLS recv error (-9): A TLS packet with unexpected length was received. error: Cannot fetch platform/packages/apps/SoundRecorder from https://source.codeaurora.org/external/imx/aosp/platform/packages/apps/SoundRecorder Fetching project platform/external/junit-params fatal: unable to access 'https://android.googlesource.com/platform/external/sonivox/': Failed to connect to android.googlesource.com port 443: Connection refused 请问如何解决,我已经使用Aosp | 镜像站使用帮助 | 清华大学开源软件镜像站 | Tsinghua Open Source Mirror 替代了repo里的glooel Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement I have same issue.    Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement you can use below features of git utility: git config --global url.https://aosp.tuna.tsinghua.edu.cn.insteadOf https://android.googlesource.com this will be replace url in git fetch request. Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement hi,  i git the source code base on the     source ~/imx-o8.0.0_1.0.0_ga/imx_android_setup.sh  , but it use the googlesouce.com. it had the error: fatal:uable to access "https://android.googlesource/com/platform/external/bart/": Failed to connet to android.googlesource.com port 443:Connection timed out. I am in China ,so Can you reply a way that  use  the  mirrors.tuna.tsinghua .edu.cn Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> It has been solved before, thank you! Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> You need to climb over the wall. Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> wilson chen hello, i.mx6 Have you managed to build the Android 8.0 system? I also encountered the same problem when building the environment, as follows: fatal: unable to access 'https://android.googlesource.com/platform/external/neven/': Failed to connect to android.googlesource.com port 443: Connection refused fatal: unable to access 'https://android.googlesource.com/platform/pdk/': Failed to connect to android.googlesource.com port 443: Connection refused fatal: unable to access 'https://android.googlesource.com/platform/developers/demos/': Failed to connect to android.googlesource.com port 443: Connection refused 烦请指教下,谢谢! Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Why when I use WIN10 system to open the mfg tool, when the imx6q board enters the download mode, there will be the prompt shown in the above picture. But if I use WIN7 system, this error will not appear. The mfgtool burning tool of android7.1.2 also has this problem. The board I use has no problem, and there is no problem burning android4.4.2\android5.1.1\anroid6.0.1\android7.1.1 systems under win10. . Please can the relevant personnel help to check it out!
查看全文
FRWY LS1046A TP NFC示例 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 展示 NFC 支持能力,为任何访问区域提供额外的安全保障。 (在 “我的视频” 中查看) 工业控制
查看全文
在i.MX上启用支持OSCCA算法工具箱的GmSSL(针对C-V2X更新) [中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343823  i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlus i.MX 8M | i.MX 8M Mini | i.MX 8M Nano i.MX6UL i.MX7Dual
查看全文
スマートホーム、スマートビルディング、照明向けのNXPコネクティビティソリューション <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このセッションでは、まず、NXPのワイヤレス・コネクティビティ・マイコン・ポートフォリオがIoT市場に対応するために含まれる製品、ソフトウェア、およびイネーブルメントの概要を説明します。次に、Thread™ネットワーキングテクノロジーと、NXPのThread StackおよびZigBee® Dotdotアプリケーションレイヤーを使用してアプリケーションを開発する方法について、より深く掘り下げてデモします。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このセッションでは、まず、NXPのワイヤレス・コネクティビティ・マイコン・ポートフォリオがIoT市場に対応するために含まれる製品、ソフトウェア、およびイネーブルメントの概要を説明します。次に、Thread™ネットワーキングテクノロジーと、NXPのThread StackおよびZigBee® Dotdotアプリケーションレイヤーを使用してアプリケーションを開発する方法について、より深く掘り下げてデモします。
查看全文
EdgeLock™ SE050:IoTエッジを保護するNXPの新世代プラグ&トラストソリューション <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> IoTセキュリティの課題に対処するための幅広く多様な組み込みソリューションを備えた企業は他にありません。セキュア・エレメントICから高度なマルチメディアおよびネットワーキング・マイクロプロセッサまで、NXPはエンドノードまたはエッジ・ノードのライフサイクル全体を保護するために必要な技術を提供します。さらに、Edgescale Cloudサービスソフトウェアを使用すると、デバイスの展開からデコミッショニングまでを維持できます。このクラスに参加して、NXPのセキュリティソリューションの概要をご覧ください。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> IoTセキュリティの課題に対処するための幅広く多様な組み込みソリューションを備えた企業は他にありません。セキュア・エレメントICから高度なマルチメディアおよびネットワーキング・マイクロプロセッサまで、NXPはエンドノードまたはエッジ・ノードのライフサイクル全体を保護するために必要な技術を提供します。さらに、Edgescale Cloudサービスソフトウェアを使用すると、デバイスの展開からデコミッショニングまでを維持できます。このクラスに参加して、NXPのセキュリティソリューションの概要をご覧ください。 ソフトウェアとツール
查看全文
如何许可软件 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 为您的软件生成许可证文件的指南。 #许可证问题 #codewarrior;软件;许可证问题
查看全文
示例 S32R274 Watchdog_example S32DS_1.1 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ******************************************************************************** * 详细说明: * 应用程序初始化 FCCU 和软件看门狗。SWT 超时后, * 微控制器已重置。 * * 宏 LONG_RESET 定义执行哪种重置。如果 LONG_RESET 为 1,则长 * 执行重置,否则执行短重置。 * * ---------------------------------------------------------------------------------------------- * 测试硬件:S32R274RRUEVB,MPC57xx主板 * 微控制器:S32R274KAMMM 1N58R *系统频率:PLL0 240MHz * Z4 核心 120MHz * 调试器:Lauterbach Trace32 * PeMicro USB-ML-PPCNEXUS * 目标:internal_FLASH(调试模式、debug_ram 和释放模式) * EVB连接:默认 * * ******************************************************************************** <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ******************************************************************************** * 详细说明: * 应用程序初始化 FCCU 和软件看门狗。SWT 超时后, * 微控制器已重置。 * * 宏 LONG_RESET 定义执行哪种重置。如果 LONG_RESET 为 1,则长 * 执行重置,否则执行短重置。 * * ---------------------------------------------------------------------------------------------- * 测试硬件:S32R274RRUEVB,MPC57xx主板 * 微控制器:S32R274KAMMM 1N58R *系统频率:PLL0 240MHz * Z4 核心 120MHz * 调试器:Lauterbach Trace32 * PeMicro USB-ML-PPCNEXUS * 目标:internal_FLASH(调试模式、debug_ram 和释放模式) * EVB连接:默认 * * ********************************************************************************
查看全文
车辆网络:时间敏感网络 (TSN),为自动驾驶提供可预测、可靠且强大的以太网网络 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 时间敏感网络是工业和汽车以太网领域的下一个热门领域。在本次会议中,我们将深入研究 TSN 标准,重点介绍与汽车领域最相关的关键特性。我们还将讨论使用 SJA1105TEL 汽车以太网交换机可以实现的潜在用例,并讨论支持在汽车中采用此类交换机的生态系统。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 时间敏感网络是工业和汽车以太网领域的下一个热门领域。在本次会议中,我们将深入研究 TSN 标准,重点介绍与汽车领域最相关的关键特性。我们还将讨论使用 SJA1105TEL 汽车以太网交换机可以实现的潜在用例,并讨论支持在汽车中采用此类交换机的生态系统。
查看全文
インフォテインメント、コネクティビティ、セキュリティ:カーラジオ、オーディオ、アンプ - 市場とテクノロジーの最新情報 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> インフォテインメント市場の動向とNXPの最新テクノロジーに関する最新情報。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> インフォテインメント市場の動向とNXPの最新テクノロジーに関する最新情報。 オーディオ処理と増幅
查看全文
Time Sensitive Networking(TSN)による産業用ネットワーキングの次の波 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> インダストリアルOEMは、デバイスでサポートする必要のある多数のネットワークプロトコルに悩まされてきました。新しいIEEEタイムセンシティブネットワーキング(TSN)規格は、複数の独自のプロトコルを共通のIEEEベースの規格に統合することを提供します。TSNで何ができるかを学びに来てください。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> インダストリアルOEMは、デバイスでサポートする必要のある多数のネットワークプロトコルに悩まされてきました。新しいIEEEタイムセンシティブネットワーキング(TSN)規格は、複数の独自のプロトコルを共通のIEEEベースの規格に統合することを提供します。TSNで何ができるかを学びに来てください。
查看全文
实践研讨会:在可扩展 i.MX 8 和 8X 平台上取得成功的技巧 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 加入此会议以了解 i.MX 8/8X 应用处理器,该处理器为工业和汽车市场提供了从成功的 i.MX 6 系列自然迁移的路径。本课程将重点介绍 CPU 性能、图形、多媒体、音频和连接方面的功能增强。并将涵盖安全、机器学习、Linux 和 Android 系统的构建和分发、存储设备管理、图形和演示设置方面的基础知识。您将在课程结束后了解 i.MX 8/8X 的功能以及如何在开发板上快速启动和运行。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 加入此会议以了解 i.MX 8/8X 应用处理器,该处理器为工业和汽车市场提供了从成功的 i.MX 6 系列自然迁移的路径。本课程将重点介绍 CPU 性能、图形、多媒体、音频和连接方面的功能增强。并将涵盖安全、机器学习、Linux 和 Android 系统的构建和分发、存储设备管理、图形和演示设置方面的基础知识。您将在课程结束后了解 i.MX 8/8X 的功能以及如何在开发板上快速启动和运行。 i.MX 应用处理器
查看全文
Kinetisデバイスのリセット・ピンに関する推奨事項 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> キネティス愛好家の皆さん、こんにちは!Kinetisマイクロコントローラのシステム・エンジニアリング・チームは、お客様が直面するあらゆる状況を目の当たりにしていますが、リセット・ピンの処理方法ほど特に問題となるものはありません。このドキュメントの目的は、Kinetisシステム・エンジニアリング部門で入手できるFAQ(よくある質問)のリストを提供することです。これは生きたリストとして意図されており、そのため、決して完全ではない可能性があります。ただし、以下の質問と回答がお役に立てば幸いです。 Q:Kinetisデバイスをデバッグするには、リセット信号を接続する必要がありますか? これはよく寄せられる質問です。厳密には、Kinetisデバイスのデバイス・リセット・ラインをデバッグ・コネクタに接続してデバッグを行う必要はありません。デバッグ・ポートのMDM-APレジスタにより、SWD_CLKラインとSWD_DIO・ラインのみを使用してシステム・リセット要求ビットを設定することにより、プロセッサをリセット状態に保持できます。 ただし、デバッグ コネクタからリセット行を省略する前に、特定のシナリオでデバイスをプログラムおよびデバッグする機能にどのように影響するかを慎重に検討する必要があります。 デバッガ/フラッシュプログラマまたは外部デバッグポッドにはリセットピンが必要ですか?使用している特定のツールが、リセットラインによるデバイスのリセットのみをサポートし、MDM-APを使用してデバイスをリセットする機能を提供していない可能性があります。 デバッグシグナルのデフォルト機能を変更しましたか?アプリケーションの他の機能にSWD_CLKやSWD_DIO信号を使用する必要がある場合があります。これは、ピン数の少ないパッケージに特に当てはまります。PORTx_PCRyレジスタを使用して機能を変更すると、これらの信号を介してMDM-APにアクセスできなくなります。リセット信号にアクセスできない場合、ピンの SWD 機能を無効にするコードがコアで実行されるのを防ぐ方法はありません。そのため、デバイスを再プログラムすることはできません。このような状況を防ぐには、次のいずれかを行う必要があります。 リセットが解放されてから数秒後に SWD ピンの機能を変更するようにコードを設定し、これが発生する前にデバッガーがコアを停止できるようにします。 これらのピンで SWD 関数を再プログラムしたり、SWD 関数を再度有効にしたりしない、ある種の "バックドア" メカニズムをコードに挿入します。たとえば、UARTまたはSPIインターフェースを介して送信される特定の文字シーケンスなどです。 一部のKinetisデバイスでは、リセット・ピンのリセット機能を無効にすることができます。この場合、SWD信号は、MDM-APを介してデバイスをリセットする手段としてのみ使用できます。リセット ピンを無効にするだけでなく、SWD ピン機能を変更する場合、デバイスを再プログラムできるようにするには、SWD 機能を再度有効にするバックドア手段を提供する必要があります。 Kinetisハードウェア・サポート Kinetis KシリーズMCU Kinetis Lシリーズ・マイクロコントローラ Kinetis Vシリーズ・マイクロコントローラ Kinetis Wシリーズ・マイクロコントローラ
查看全文
具备 SafeAssure ®认证功能的 i.MX 8 MCU — 摄像头、视频、音频、可信环境 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本课程将解释为 i.MX 8 提供的几种软件解决方案。SafeAssure 软件允许进行系统分区,充分利用 i.MX 8 的一些安全功能。Fast Path 软件允许在 2 个网络接口之间路由/桥接数据,以最大限度地提高数据路由性能,同时将主处理器的 CPU 负载要求降至最低。可信环境允许充分利用 Arm ® Trustzone 功能。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本课程将解释为 i.MX 8 提供的几种软件解决方案。SafeAssure 软件允许进行系统分区,充分利用 i.MX 8 的一些安全功能。Fast Path 软件允许在 2 个网络接口之间路由/桥接数据,以最大限度地提高数据路由性能,同时将主处理器的 CPU 负载要求降至最低。可信环境允许充分利用 Arm ® Trustzone 功能。
查看全文
WillyFog_Milestone_2 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このマイルストーンでは、新しく実装された機能は次のもので構成されます。 - ログイン/ログアウト機能の追加 - 管理者ユーザーが新しいユーザーを追加できるようにする - ユーザーごとにデバイスを分離し、デバイスごとにコマンドを分離する - ソニーのプロトコルを使用するデバイスへのIR学習機能の追加 - デバイスが学習モードのときにLEDを点灯させる (マイビデオで視聴) Linux Embedded Challenge 2017 (英語)
查看全文
快速物联网原型开发套件_Connects China <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 了解如何将物联网构想转化为概念验证,就像 1-2-3 一样简单,实现互联、安全、小型化的物联网终端节点。快速物联网套件集成了 30 多个有源组件(11 个 NXP 部件)以及驱动程序、中间件、示例应用程序,并具有基于 GUI 编程的创新 Web IDE,以及移动应用程序和物联网云服务。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 了解如何将物联网构想转化为概念验证,就像 1-2-3 一样简单,实现互联、安全、小型化的物联网终端节点。快速物联网套件集成了 30 多个有源组件(11 个 NXP 部件)以及驱动程序、中间件、示例应用程序,并具有基于 GUI 编程的创新 Web IDE,以及移动应用程序和物联网云服务。
查看全文
i.MX 8 series: eCockpit simulator (Virtual Reality) What’s it like to sit in a state-of-the art eCockpit? Put on a virtual reality headset and find out! Here, the virtual world meets the real world as live video content from 4 displays -- a HUD, cluster, infotainment and rear seat entertainment systems – is processed and streamed realtime from a single i.MX 8 applications processor.  i.MX 8 series will transform interactions in ways you’ve never imagined   NXP product recommended i.MX 8 ARMCortex-A53 Processor|NXP  Mobile
查看全文
HMB-N2042 スレッド コネクテッドホームを現実にする <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 家庭でのモノのインターネット(IoT)を実現するためには、企業はIPv6ベースのメッシュネットワークプロトコルからエンドユーザーエクスペリエンスまで、あらゆる側面に対応するオープンエコシステムアプローチが必要です。このクラスでは、Threadがスマートホームの状況にどのように適合するか、Threadが提供する主な利点、およびNXPが提供するビルディングブロックとThreadエコシステムの他のリソースを使用して、Thread製品コンセプトをアイデアから市場に製品化する方法について説明します。 ビデオプレゼンテーションを見る <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 家庭でのモノのインターネット(IoT)を実現するためには、企業はIPv6ベースのメッシュネットワークプロトコルからエンドユーザーエクスペリエンスまで、あらゆる側面に対応するオープンエコシステムアプローチが必要です。このクラスでは、Threadがスマートホームの状況にどのように適合するか、Threadが提供する主な利点、およびNXPが提供するビルディングブロックとThreadエコシステムの他のリソースを使用して、Thread製品コンセプトをアイデアから市場に製品化する方法について説明します。 ビデオプレゼンテーションを見る スマートホーム&ビル
查看全文
Flash Programmer Taskを使用したスタンドアロンプログラミング <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> スタンドアロン プログラミングは、CodeWarrior 10 でのプログラミングにデバッガが必要ない場合に広く使用されています。したがって、人々はプロジェクトファイルとソースファイルを使用せずに、elf / s19ファイルのみをプログラムターゲットに使用します。 Erich Stygerが書いた、ターゲットプログラミングのスタンドアロンプログラマとして「Flash File to Target」を使用することについて書かれた非常に有名な記事があります。 https://mcuoneclipse.com/2012/08/02/standalone-flash-programmer/   この方法に加えて、 Flash Programmer Task はスタンドアロンプログラミングにも適しています。私が知っているように、一部のお客様は、プログラミング中にチェックサム、ダンプフラッシュなども行うことができるため、この方法を使用することを好みます。以下では、 Flash Programmer Task のブレインストーミングの活用方法を順を追って紹介します。この記事はCodeWarrior 10.6.4およびFRDM-K64ボードに基づいていますが、方法はすべてのKinetis、HCS08、HCS12Zなどのデバイスで同じです   詳しくは添付の記事と動画をご覧ください。 全般
查看全文
Excel MPC5777C クロックコンフィギュレーター このコンフィグレーション・ツールにより、デバイスのPLL設定の計算とクロック・コンフィギュレーションMPC5777C簡素化されます。 バージョン1.3では、264MHz/300MHzのMCUバージョンを選択するオプションを追加した。                 次の手順に従います                 注意:マクロを有効にする必要があります!                 1. 使用済みのXOSCの周波数と、目的のPLL0およびPLL1出力を入力します。 - 「Clocks」シートのセルB14、Q13、Q20に値を入力します - 有効か無効かを確認します - 「PLLconfig」シートには、可能なPLL設定が表示されます   2. システムおよびAUXクロックセレクタとその分周器をコンフィギュレーションします。 - システム/ペリフェラルクロックの計算された周波数を確認します - 無効な場合は、 ソースクロックと分周器の値を変更して最大周波数を維持します                 3. 「Copy Code」ボタンを押して、生成されたコードをコピーする テスト
查看全文
AMF-AUT-T2349 - 恩智浦可信执行环境 (TEE) 堆栈 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 由于自动驾驶功能的发展与汽车安全能力密不可分,因此安全性正在成为任何 OEM 乃至整个行业的一个典型主题。任何车辆节点的安全架构中的许多组件都非常接近 SoC,利用硬件功能来实现预期的功能。为了满足客户需求,恩智浦提供了可信执行环境 (TEE) 堆栈,该堆栈提供了汽车所需的大量安全功能。了解 NXP TEE 堆栈的基础知识、功能以及如何将其集成到典型的安全节点架构中。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 由于自动驾驶功能的发展与汽车安全能力密不可分,因此安全性正在成为任何 OEM 乃至整个行业的一个典型主题。任何车辆节点的安全架构中的许多组件都非常接近 SoC,利用硬件功能来实现预期的功能。为了满足客户需求,恩智浦提供了可信执行环境 (TEE) 堆栈,该堆栈提供了汽车所需的大量安全功能。了解 NXP TEE 堆栈的基础知识、功能以及如何将其集成到典型的安全节点架构中。
查看全文