1119962_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1119962_en-US

1119962_en-US

Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement

The i.MX Android O8.0.0_1.0.0 GA release is now available from IMX_SW page. Overview -> BSP Updates and Releases -> Android 8.0.0 Oreo (O8.0.0_1.0.0, 4.9 kernel)


  • Files available:

#

Name

Description

1

android_O8.0.0_1.0.0_docs.tar.gz

i.MX Android O8.0.0_1.0.0 BSP Documentation

2

imx-o8.0.0_1.0.0_ga.tar.gz

i.MX Android O8.0.0_1.0.0 proprietary surce code for i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo  i.MX 6Sololite, i.MX6SX and i.MX7D

3


android_O8.0.0_1.0.0_image_6dqpsabreauto.tar.gz

Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE for Automotive Infotainment based on i.MX 6QuadPlus, i.MX 6Quad, and i.MX 6DualLite

4

android_O8.0.0_1.0.0_image_6dqpsabresd.tar.gz

Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE Platform and SABRE Board based on i.MX 6QuadPlus, i.MX 6Quad and i.MX 6DualLite.

5

android_O8.0.0_1.0.0_image_6slevk.tar.gz

Binary Demo Files of Android O8.0.0_1.0.0 BSP - i.MX 6Sololite evaluation kit.

6

android_O8.0.0_1.0.0_image_6sxsabresd.tar.gz

Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE Board based on i.MX 6SoloX

7


android_O8.0.0_1.0.0_image_6sxsabreauto.tar.gz

Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE for Automotive infotainment based on i.MX 6SoloX

8

android_O8.0.0_1.0.0_image_7dsabresd.tar.gz

Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE Board based on i.MX 7Dual

9

fsl_aacp_dec_O8.0.0_1.0.0.tar.gz

AAC Plus Codec for O8.0.0_1.0.0

10

android_O8.0.0_1.0.0_tools.tar.gz

Manufacturing Toolkit and VivanteVTK for O8.0.0_1.0.0

 

  • Supported Hardware SoC/Boards:
    • i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-SD board and platform
    • i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-AI board and platform
    • i.MX 6SoloLite EVK platform
    • i.MX 6SoloX SABRE-SD board and platforms
    • i.MX 6SoloX SABRE-AI board and platforms
    • i.MX 7Dual SABRE-SD board and platform

 

  • Changes:

Compared to the N7.1.2_2.0.0 release, this release has the following major changes:

  • Upgraded the Android code base from android-7.1.2_r9 to android-8.0.0_r25.
  • Removed the device partition and added the vendor partition.
  • Enabled ION-based gralloc and EGL.
  • Feature:

For features please consult the release notes.

 

  • Known issues

For known issues and more details please consult the Release Notes.

Androidi.MX6_Alli.MX6DLi.MX6Duali.MX6DualPlus6QuadPlusi.MX6Quadi.MX6Si.MX6SLi.MX6SoloXi.MX7DualRe: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement

codeaurora use mirrors below:

git --config --global url." ".insteadOf "https://source.codeaurora.org"

can be any one of below:

https://beijing.source.codeaurora.org

https://shanghai.source.codeaurora.org

if manifest.xml use "git://source.codeaurora.org" you must be edit

~/.gitconfig

add line below:

[url "https://beijing.source.codeaurora.org"]

insteadOf = git://codeaurora.org

Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement

运行repo sync后完整输出信息是这样的:fatal: unable to access 'https://source.codeaurora.org/external/imx/aosp/platform/packages/apps/SoundRecorder/': GnuTLS recv error (-9): A TLS packet with unexpected length was received.
error: Cannot fetch platform/packages/apps/SoundRecorder from https://source.codeaurora.org/external/imx/aosp/platform/packages/apps/SoundRecorder
Fetching project platform/external/junit-params
fatal: unable to access 'https://android.googlesource.com/platform/external/sonivox/': Failed to connect to android.googlesource.com port 443: Connection refused

请问如何解决,我已经使用Aosp | 镜像站使用帮助 | 清华大学开源软件镜像站 | Tsinghua Open Source Mirror 替代了repo里的glooel

Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement

I have same issue.   

Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement

you can use below features of git utility:

git config --global url.https://aosp.tuna.tsinghua.edu.cn.insteadOf https://android.googlesource.com

this will be replace url in git fetch request.

Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement

hi,

 i git the source code base on the     source ~/imx-o8.0.0_1.0.0_ga/imx_android_setup.sh  , but it use the googlesouce.com. it had the error: fatal:uable to access "https://android.googlesource/com/platform/external/bart/": Failed to connet to android.googlesource.com port 443:Connection timed out.

I am in China ,so Can you reply a way that  use  the  mirrors.tuna.tsinghua .edu.cn

Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement<meta http-equiv="Content-Type" content="text/html; charset=utf-8" />

It has been solved before, thank you!

Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement<meta http-equiv="Content-Type" content="text/html; charset=utf-8" />

You need to climb over the wall.

Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement<meta http-equiv="Content-Type" content="text/html; charset=utf-8" />

wilson chen hello, i.mx6 Have you managed to build the Android 8.0 system? I also encountered the same problem when building the environment, as follows:

fatal: unable to access 'https://android.googlesource.com/platform/external/neven/': Failed to connect to android.googlesource.com port 443: Connection refused
fatal: unable to access 'https://android.googlesource.com/platform/pdk/': Failed to connect to android.googlesource.com port 443: Connection refused
fatal: unable to access 'https://android.googlesource.com/platform/developers/demos/': Failed to connect to android.googlesource.com port 443: Connection refused
烦请指教下,谢谢!

Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement<meta http-equiv="Content-Type" content="text/html; charset=utf-8" />

pastedImage_1.png

Why when I use WIN10 system to open the mfg tool, when the imx6q board enters the download mode, there will be the prompt shown in the above picture. But if I use WIN7 system, this error will not appear. The mfgtool burning tool of android7.1.2 also has this problem. The board I use has no problem, and there is no problem burning android4.4.2\android5.1.1\anroid6.0.1\android7.1.1 systems under win10. .

Please can the relevant personnel help to check it out!

Tags (1)
No ratings
Version history
Last update:
‎01-06-2026 02:27 AM
Updated by: