Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
CodeWarrior 10 Command Line Interface – usage and examples Inside {CW10 install folder}\eclipse there is ecd.exe which is used to run build projects from command line. this article focuses on ecd.exe usage with examples. Especially How to use ecd.exe command to build, generateMakefiles,make and reference a project. General
記事全体を表示
Boundary Devices - Crank Storyboard demo on i.MX7 Nitrogen7 This video shows how the Crank Storyboard application framework is well suited to run on our i.MX7 Nitrogen7 board. Demo details This demonstration is based on the following: Nitrogen7 board​​ 800×480 LCD display​ Resistive touch Yocto Jethro release Linux kernel 3.14.52 Crank Software details Crank Software Inc. is an innovator in embedded graphical user interface (GUI) solutions. Their products and services enable R&D teams and UI Designers to quickly and collaboratively develop rich animated user interfaces for resource-constrained embedded. The demo above relies on the Crank Storyboard Engine which is: Multi-platform Supported on Linux, Android, QNX, WindowsCE among others Built for embedded Storyboard Embedded Engine scales from low-end to high-end processors 3D optimized For higher end products embedding a GPU For more information, please visit: https://boundarydevices.com/crank-software-demo-on-nitrogen7/ General
記事全体を表示
Automotive Ethernet AVB Demo: ADAS System and a complete Infotainment Solution Demo This demo shows an infotainment and ADAS system based on NXP Ethernet components and is divided in three main parts: Infotainment, Network and ADAS. In the infotainment part, a “Head Unit” ECU plays locally an MPEG movie and also streams it over Ethernet to the second “Rear Seat Unit” ECU. Both ECUs also execute in the backroad the NXP AVB SW stack. This enables the two ECUs to be perfectly synchronized with each other. Therefore the two ECUs can playback the very same video (and audio) frame at the same time on their local displays. In the network part the new Automotive Ethernet Switch (SJA1105EL) and PHYs (TJA1100HN) implement the Ethernet connectivity of the system. The switch executes the AVB “gPTP” synchronization SW that enables the infotainment application described above to operate. In the ADAS part a surround view camera captures a video stream and streams it to a “Cluster” ECU also connected via the automotive Ethernet network. The camera is based on the NXP “MPC5604E ” Salsa processor and on a competitor’s BroadR-Reach PHY. This also shows the interoperability of the TJA1100HN PHY with competitor’s products. Features: All displays are implemented with NXP i.MX6 processor, and a full implementation of the NXP Ethernet AVB Stack running on Linux. The camera is based on an NXP Salsa processor (MPC5304EKIT) . The Switch board that connects all displays and the camera uses the NXP SJA1105EL Automotive Ethernet switch and the TJA1100HN BroadR-Reach Ethernet PHY ______________________________________________________________________________________________________________ Featured NXP Products: Product Link IEEE 100BASE-T1 compliant Automotive Ethernet PHY Transceiver TJA1100HN | Automotive Ethernet PHY Transceiver | NXP  i.MX 6 Series i.MX 6 Series Applications Processors | Multicore Arm Cortex-A7/A9/M4 | NXP  Audio Video Bridging Software https://www.nxp.com/design/design-services/audio-video-bridging-software:AVB-SOFTWARE?&fsrch=1&sr=4&pageNum=1 Development Kit Enabling Video Over Ethernet with NXP® MPC5604E MCU NXP® MPC5604EKIT:Development Kit | NXP  ___________________________________________________________________________________________________________ Automotive
記事全体を表示
Novena - Open Source Laptop A new open-hardware computing platform, flexible and powerful, designed for use as a desktop, laptop, or standalone board. Novena is a 1.2GHz, Freescale quad-core ARM architecture computer closely coupled with a Xilinx FPGA. It's designed for users who care about open source, and/or want to modify and extend their hardware: all the documentation for the PCBs is open and free to download, the entire OS is buildable from source, and it comes with a variety of features that facilitate rapid prototyping. For more information check out Kousagi Studio and if you want to fund this project check out Crowd Supply General
記事全体を表示
Zephyr 模块、子系统和功能的资源 如果您对这些资源有任何疑问或问题,请 提出新问题,恩智浦支持团队将为您解答。 引导加载程序 Zephyr 将开源MCUboot引导加载程序作为一个模块包含在内,并使其易于用作 Zephyr 应用程序的引导加载程序。 NXP i.MX RT 系列上的 MCUboot 和 Zephyr 使用 MCUboot 和 Sysbuild 构建示例,以及 VS Code 中带有 MCUboot 的 Zephyr 应用 Zephyr MCUBoot + TF-M 处理器间通信 (IPC) 和多核 Zephyr 包含一个IPC子系统。Zephyr 还集成了开源OpenAMP框架,以便使用 RPMsg 协议实现核心之间的通信。 Zephyr OpenAMP 多核示例 RT1170构建双核图像 多核性能 电源管理(PM) Zephyr 包含一个电源管理子系统,受许多 NXP SOC 支持。 网络研讨会:利用 Zephyr OS 功能和模块加速开发 NXP SmartWatch 演示和网络研讨会:最大限度地降低 i.MX RT500 的功耗 PSA 和可信固件 (TF-M) FRDM-RW612 上的 TF-M PSA 加密示例 Zephyr MCUBoot + TF-M 启动代码及流程 为了便于移植,Zephyr 管理应用程序中未包含的启动代码。SOC、内存、设备驱动程序和一些子系统在 main() 之前初始化。 网络研讨会: Zephyr OS 和 NXP 让应用程序可移植性变得简单 添加自定义启动代码 返回Zephyr知识中心
記事全体を表示
ビデオ: S32R45 レーダー拡張パッケージのインストール (マイビデオで視聴)
記事全体を表示
PyeIQ v1.0 for BSP 5.4.3_2.0.0 Release Welcome to PyeIQ PyeIQ gathers everything needed by itself. It provides a simplified way to run ML applications, which avoids the user spending time on preparing the environment. PyeIQ Version Release Date Notes tag_v1.0 Apr 29, 2020 - tag_v2.0 - Planned for June i.MX Board BSP Release Building Status 8 QM 5.4.3_2.0.0 passing 8 MPlus 5.4.3_2.0.0 passing This video is currently being processed. Please try again in a few minutes. (view in My Videos) Getting Started with PyeIQ 1. Easy Installation If you prefer to build the package by yourself go to Appendix Section or follow the README file at the PyeIQ repo. 1.1 Copy the PyeIQ pre-built package attached to the board, and then install it by using pip3 tool: 1.2 Check the installation by starting an interactive shell:   1.3 Import PyeIQ and see the version: The output is the PyeIQ latest version installed in the system. (Optional) Install the following package to show downloading status: 2. Easy Running All demos and applications are automatically installed in /opt/eiq. 2.1 To run the demos: 2.2 To run the applications: 2.3 Use help if needed: 3. List of Available Demos and Applications Demo/App Name Demo/App Type i.MX Board BSP Release BSP Framework Inference Status Notes Label Image File Based QM, MPlus 5.4.3_2.0.0 TensorFlow Lite 2.1.0 GPU, NPU passing - Label Image Switch File Based QM, MPlus 5.4.3_2.0.0 TensorFlow Lite 2.1.0 GPU, NPU passing - Object Detection SSD/Camera QM, MPlus 5.4.3_2.0.0 TensorFlow Lite 2.1.0 GPU, NPU passing Need better model. Object Detection OpenCV SSD/Camera QM, MPlus 5.4.3_2.0.0 TensorFlow Lite 2.1.0 GPU, NPU passing Need better model. Object Detection N. GS. SSD/Camera QM, MPlus 5.4.3_2.0.0 TensorFlow Lite 2.1.0 GPU, NPU - Pending issues. Object Detection Yolov3 SSD/File QM, MPlus 5.4.3_2.0.0 TensorFlow Lite 2.1.0 GPU, NPU - Pending issues. Object Detection Yolov3 SSD/Camera QM, MPlus 5.4.3_2.0.0 TensorFlow Lite 2.1.0 GPU, NPU - Pending issues. Fire Detection File Based QM, MPlus 5.4.3_2.0.0 TensorFlow Lite 2.1.0 GPU, NPU passing - Fire Detection Camera QM, MPlus 5.4.3_2.0.0 TensorFlow Lite 2.1.0 GPU, NPU passing - Fire Detection Camera - 5.4.3_2.0.0 PyArmNN 19.08 - - Requires 19.11 Coral Posenet Camera - - - - - Ongoing NEO DLR Camera - - - - - Ongoing 4. Examples 4.1 Fire Detection Image 4.1.1 Non-fire Running Fire Detect Image:     Output: INFO: Created TensorFlow Lite delegate for NNAPI.                                                                        Applied NNAPI delegate.                                                                                                  Inference time: 0:00:00.264853                                                                                           Non-Fire   4.1.2 Fire Running Fire Detect Image: Output: INFO: Created TensorFlow Lite delegate for NNAPI.                                                                        Applied NNAPI delegate.                                                                                                  Inference time: 0:00:00.193055                                                                                           Fire    4.2 Fire Detection Camera Running Fire Detect Camera: Output: PyeIQ also supports training for Fire Detection demo, please refer to PyeIQ - Training and Conversion Support (Keras/TensorFlow Lite) . 4.3 Label Image Switch Running Switch Label Image: Output: Cores Comparison (CPU, GPU and NPU) Check the following graphical plot for Switch Label Image demo: Check the following graphical plot for the other demos: We are currently working to reduce the inference time on Fire Detection demos. Appendix Section The procedures described in this document target a GNU/Linux Distribution Ubuntu 18.04. 1. Software Requirements 1.1 Install the following packages in the GNU/Linux system: 1.2 Then, use pip3 tool to install the virtualenv tool: 2. Building the PyeIQ Package 2.1 Clone the repository: 2.2 Use virtualenv tool to create an isolated Python environment: 2.3 Generate the PyeIQ package: 2.4 Copy the package to the board: 2.5 To deactivate the virtual environment: Contact Feel free to contact us about any issue/bug you might have it. Your feedback is very welcome so we can improve the next version Alifer Moraes diegodorta marcofranchi Re: PyeIQ v1.0 for BSP 5.4.3_2.0.0 Release Hello  I cannot see the detailed command and description  for example, when I see your explanation in box, most things are empty Please check it again
記事全体を表示
英国大学挂科GPA低该怎么办 英国是大多数留学生向往的留学深造目的地之一,(【联系方式QQ-1252839746】当面临诸多例如:Probation、Withdrawal、Suspension、Dismissal、等学术警告问题的时候,很多学生选择了联系我们修改成绩单达到学分GPA要求或删除学术不良记录重新回到学校。)很多留学生在美国学习后都学到了很多知识,成长为更好的自己。但是,在学习过程中,难免遇到磕磕绊绊,比如:刚来到美国会遇到Culture shock(文化冲突);刚入学会听不懂老师的授课内容;生活上出现各种不可预期的困难;mid-term和final期间没日没夜地复习。历练中,很多学生成功克服困难,顺利完成学业,但也有一部分学生面对过 停学 ( Suspension )的尴尬。不过幸好美国愿意给犯错的学生二次入学的机会,并专门针对停学及开除学生提供一个申请流程,称为 Readmission (再次申请录取)。被停学的学生可以曲线救国,最终成功回到原来的校园。 学生被美国学校停学的理由有很多,例如作弊被抓丶GPA低丶违反校规丶代写代考被发现等等。在达到相应严重程度时,学校会给予学生短则一个季度或一个学期,长则一年甚至两年以上的停学处分。在被停学后,大多数学生都想在停学结束后重新回到原学校。那么学生就会面临 Readmission(重新申请录取/重新接纳)的情况。 T同学是美国某大学大二的学生,在被学校停学后,选择了回国待一年。但是当T同学在结束一年的停学后,提出 Readmission 想要重回学校时,学校却拒绝了T同学的请求,T同学一头雾水。 其实 Readmission 时,需要注意的细节有很多,但是大家往往忽略了这些重要内容。下面我们来详细讲解一下跟原学校申请再次录取的注意事项: 各大学对Readmission要求都不同 首先,学生被 停学 ( Suspension )后,学校对于Readmission有着不同程度的入学要求: 1丶停学期限一到,有的学校是无过多要求,直接颁发新的I-20让学生回到学校,这也是最轻松的Readmission。停学期间,学生需要进行一定的自我反省,并积极调整学习方法和学习知识。 2丶也有一部分的学校对再次申请入学是有要求的,涉及到学生需要在反省后,向学校提交Readmission申请表格及个人陈述,审核通过后,学生才能回到学校。 3丶最难的Readmission是学校要求学生重新入学前进行自我完善和提高,例如进行本学校暑期课程的学习或者在其他机构的学习,证明自己是有继续在原学校读书的能力同时可能会要求提供一些额外的支持材料。 申请时间有限制 学生需要仔细研究学校的开始申请日期和截止日期,并及时提交相关材料。如果错过了申请的时间,学生可能会错过重新入学的学期。T同学就是因为没有注意到截止时间,没有及时提交学校要求的材料,导致Readmission阶段仍需要进行二次申请。 停学期间不要贪图玩耍 建议学生停学期间不要回国。很多学生在国内把停学当作放假,各地游玩儿,在家打游戏,吃喝玩乐。这样极其不利于Readmission的申请,重新回到原学校的机率也会降低。 Readmission申请有风险 并不是所有申请Readmission的学生都会通过。学校对于每一位Readmission的学生都会严格的考量。包括学生停学期间的表现和回国态度,重新入学的提交材料审核等,如被认为不具有继续在原学校读书能力的学生有被拒风险。 当面临诸多例如:Probation、Withdrawal、Suspension、Dismissal、等学术警告问题的时候,很多学生选择了联系我们修改成绩单达到学分GPA要求或删除学术不良记录重新回到学校。【联系方式QQ-1252839746】
記事全体を表示
高性能 Layerscape 处理器 (LX2160A) 的应用 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> LX2160A 是恩智浦性能最高的多核设备,配备 16 个 Arm-v8 64 位 A72 内核,主频高达 2.2 GHz。它还具有 24 条运行速度为 25 GHz 的 SerDes 通道,支持双 100GE 接口和最多 24 条 PCIe Express 通道。它的安全加速可达 50 Gbps,数据压缩/解压缩可达 100 Gbps。本次会议将解释 LX2160A 对主要目标应用(5G、工业、ADAS、存储、NIC 和边缘路由)的适用性、基准测试结果(CoreMark、Dhrystone、DPDK、SpecInt 等)、软件和参考板支持、第三方板解决方案,以及它与 Xeon-D 系列设备相比的优势。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> LX2160A 是恩智浦性能最高的多核设备,配备 16 个 Arm-v8 64 位 A72 内核,主频高达 2.2 GHz。它还具有 24 条运行速度为 25 GHz 的 SerDes 通道,支持双 100GE 接口和最多 24 条 PCIe Express 通道。它的安全加速可达 50 Gbps,数据压缩/解压缩可达 100 Gbps。本次会议将解释 LX2160A 对主要目标应用(5G、工业、ADAS、存储、NIC 和边缘路由)的适用性、基准测试结果(CoreMark、Dhrystone、DPDK、SpecInt 等)、软件和参考板支持、第三方板解决方案,以及它与 Xeon-D 系列设备相比的优势。
記事全体を表示
Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement The i.MX Android O8.0.0_1.0.0 GA release is now available from IMX_SW page. Overview -> BSP Updates and Releases -> Android 8.0.0 Oreo (O8.0.0_1.0.0, 4.9 kernel) Files available: # Name Description 1 android_O8.0.0_1.0.0_docs.tar.gz i.MX Android O8.0.0_1.0.0 BSP Documentation 2 imx-o8.0.0_1.0.0_ga.tar.gz i.MX Android O8.0.0_1.0.0 proprietary surce code for i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo  i.MX 6Sololite, i.MX6SX and i.MX7D 3 android_O8.0.0_1.0.0_image_6dqpsabreauto.tar.gz Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE for Automotive Infotainment based on i.MX 6QuadPlus, i.MX 6Quad, and i.MX 6DualLite 4 android_O8.0.0_1.0.0_image_6dqpsabresd.tar.gz Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE Platform and SABRE Board based on i.MX 6QuadPlus, i.MX 6Quad and i.MX 6DualLite. 5 android_O8.0.0_1.0.0_image_6slevk.tar.gz Binary Demo Files of Android O8.0.0_1.0.0 BSP - i.MX 6Sololite evaluation kit. 6 android_O8.0.0_1.0.0_image_6sxsabresd.tar.gz Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE Board based on i.MX 6SoloX 7 android_O8.0.0_1.0.0_image_6sxsabreauto.tar.gz Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE for Automotive infotainment based on i.MX 6SoloX 8 android_O8.0.0_1.0.0_image_7dsabresd.tar.gz Binary Demo Files of Android O8.0.0_1.0.0 BSP - SABRE Board based on i.MX 7Dual 9 fsl_aacp_dec_O8.0.0_1.0.0.tar.gz AAC Plus Codec for O8.0.0_1.0.0 10 android_O8.0.0_1.0.0_tools.tar.gz Manufacturing Toolkit and VivanteVTK for O8.0.0_1.0.0   Supported Hardware SoC/Boards: i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-SD board and platform i.MX 6Quad, i.MX 6QuadPlus, and i.MX 6DualLite SABRE-AI board and platform i.MX 6SoloLite EVK platform i.MX 6SoloX SABRE-SD board and platforms i.MX 6SoloX SABRE-AI board and platforms i.MX 7Dual SABRE-SD board and platform   Changes: Compared to the N7.1.2_2.0.0 release, this release has the following major changes: Upgraded the Android code base from android-7.1.2_r9 to android-8.0.0_r25. Removed the device partition and added the vendor partition. Enabled ION-based gralloc and EGL. Feature: For features please consult the release notes.   Known issues For known issues and more details please consult the Release Notes. Android i.MX6_All i.MX6DL i.MX6Dual i.MX6DualPlus6QuadPlus i.MX6Quad i.MX6S i.MX6SL i.MX6SoloX i.MX7Dual Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement codeaurora use mirrors below: git --config --global url." ".insteadOf " https://source.codeaurora.org" can be any one of below: https://beijing.source.codeaurora.org https://shanghai.source.codeaurora.org if manifest.xml use "git://source.codeaurora.org" you must be edit ~/.gitconfig add line below: [url "https://beijing.source.codeaurora.org"] insteadOf = git://codeaurora.org Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement 运行repo sync后完整输出信息是这样的:fatal: unable to access 'https://source.codeaurora.org/external/imx/aosp/platform/packages/apps/SoundRecorder/': GnuTLS recv error (-9): A TLS packet with unexpected length was received. error: Cannot fetch platform/packages/apps/SoundRecorder from https://source.codeaurora.org/external/imx/aosp/platform/packages/apps/SoundRecorder Fetching project platform/external/junit-params fatal: unable to access 'https://android.googlesource.com/platform/external/sonivox/': Failed to connect to android.googlesource.com port 443: Connection refused 请问如何解决,我已经使用Aosp | 镜像站使用帮助 | 清华大学开源软件镜像站 | Tsinghua Open Source Mirror 替代了repo里的glooel Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement I have same issue.    Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement you can use below features of git utility: git config --global url.https://aosp.tuna.tsinghua.edu.cn.insteadOf https://android.googlesource.com this will be replace url in git fetch request. Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement hi,  i git the source code base on the     source ~/imx-o8.0.0_1.0.0_ga/imx_android_setup.sh  , but it use the googlesouce.com. it had the error: fatal:uable to access "https://android.googlesource/com/platform/external/bart/": Failed to connet to android.googlesource.com port 443:Connection timed out. I am in China ,so Can you reply a way that  use  the  mirrors.tuna.tsinghua .edu.cn Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> It has been solved before, thank you! Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> You need to climb over the wall. Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> wilson chen hello, i.mx6 Have you managed to build the Android 8.0 system? I also encountered the same problem when building the environment, as follows: fatal: unable to access 'https://android.googlesource.com/platform/external/neven/': Failed to connect to android.googlesource.com port 443: Connection refused fatal: unable to access 'https://android.googlesource.com/platform/pdk/': Failed to connect to android.googlesource.com port 443: Connection refused fatal: unable to access 'https://android.googlesource.com/platform/developers/demos/': Failed to connect to android.googlesource.com port 443: Connection refused 烦请指教下,谢谢! Re: Android O8.0.0_1.0.0 GA for Legacy imx6/7 Release Announcement <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Why when I use WIN10 system to open the mfg tool, when the imx6q board enters the download mode, there will be the prompt shown in the above picture. But if I use WIN7 system, this error will not appear. The mfgtool burning tool of android7.1.2 also has this problem. The board I use has no problem, and there is no problem burning android4.4.2\android5.1.1\anroid6.0.1\android7.1.1 systems under win10. . Please can the relevant personnel help to check it out!
記事全体を表示
FRWY LS1046A TP NFC示例 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 展示 NFC 支持能力,为任何访问区域提供额外的安全保障。 (在 “我的视频” 中查看) 工业控制
記事全体を表示
在i.MX上启用支持OSCCA算法工具箱的GmSSL(针对C-V2X更新) [中文翻译版] 见附件   原文链接: https://community.nxp.com/docs/DOC-343823  i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlus i.MX 8M | i.MX 8M Mini | i.MX 8M Nano i.MX6UL i.MX7Dual
記事全体を表示
スマートホーム、スマートビルディング、照明向けのNXPコネクティビティソリューション <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このセッションでは、まず、NXPのワイヤレス・コネクティビティ・マイコン・ポートフォリオがIoT市場に対応するために含まれる製品、ソフトウェア、およびイネーブルメントの概要を説明します。次に、Thread™ネットワーキングテクノロジーと、NXPのThread StackおよびZigBee® Dotdotアプリケーションレイヤーを使用してアプリケーションを開発する方法について、より深く掘り下げてデモします。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このセッションでは、まず、NXPのワイヤレス・コネクティビティ・マイコン・ポートフォリオがIoT市場に対応するために含まれる製品、ソフトウェア、およびイネーブルメントの概要を説明します。次に、Thread™ネットワーキングテクノロジーと、NXPのThread StackおよびZigBee® Dotdotアプリケーションレイヤーを使用してアプリケーションを開発する方法について、より深く掘り下げてデモします。
記事全体を表示
EdgeLock™ SE050:IoTエッジを保護するNXPの新世代プラグ&トラストソリューション <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> IoTセキュリティの課題に対処するための幅広く多様な組み込みソリューションを備えた企業は他にありません。セキュア・エレメントICから高度なマルチメディアおよびネットワーキング・マイクロプロセッサまで、NXPはエンドノードまたはエッジ・ノードのライフサイクル全体を保護するために必要な技術を提供します。さらに、Edgescale Cloudサービスソフトウェアを使用すると、デバイスの展開からデコミッショニングまでを維持できます。このクラスに参加して、NXPのセキュリティソリューションの概要をご覧ください。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> IoTセキュリティの課題に対処するための幅広く多様な組み込みソリューションを備えた企業は他にありません。セキュア・エレメントICから高度なマルチメディアおよびネットワーキング・マイクロプロセッサまで、NXPはエンドノードまたはエッジ・ノードのライフサイクル全体を保護するために必要な技術を提供します。さらに、Edgescale Cloudサービスソフトウェアを使用すると、デバイスの展開からデコミッショニングまでを維持できます。このクラスに参加して、NXPのセキュリティソリューションの概要をご覧ください。 ソフトウェアとツール
記事全体を表示
如何许可软件 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 为您的软件生成许可证文件的指南。 #许可证问题 #codewarrior;软件;许可证问题
記事全体を表示
示例 S32R274 Watchdog_example S32DS_1.1 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ******************************************************************************** * 详细说明: * 应用程序初始化 FCCU 和软件看门狗。SWT 超时后, * 微控制器已重置。 * * 宏 LONG_RESET 定义执行哪种重置。如果 LONG_RESET 为 1,则长 * 执行重置,否则执行短重置。 * * ---------------------------------------------------------------------------------------------- * 测试硬件:S32R274RRUEVB,MPC57xx主板 * 微控制器:S32R274KAMMM 1N58R *系统频率:PLL0 240MHz * Z4 核心 120MHz * 调试器:Lauterbach Trace32 * PeMicro USB-ML-PPCNEXUS * 目标:internal_FLASH(调试模式、debug_ram 和释放模式) * EVB连接:默认 * * ******************************************************************************** <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ******************************************************************************** * 详细说明: * 应用程序初始化 FCCU 和软件看门狗。SWT 超时后, * 微控制器已重置。 * * 宏 LONG_RESET 定义执行哪种重置。如果 LONG_RESET 为 1,则长 * 执行重置,否则执行短重置。 * * ---------------------------------------------------------------------------------------------- * 测试硬件:S32R274RRUEVB,MPC57xx主板 * 微控制器:S32R274KAMMM 1N58R *系统频率:PLL0 240MHz * Z4 核心 120MHz * 调试器:Lauterbach Trace32 * PeMicro USB-ML-PPCNEXUS * 目标:internal_FLASH(调试模式、debug_ram 和释放模式) * EVB连接:默认 * * ********************************************************************************
記事全体を表示
车辆网络:时间敏感网络 (TSN),为自动驾驶提供可预测、可靠且强大的以太网网络 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 时间敏感网络是工业和汽车以太网领域的下一个热门领域。在本次会议中,我们将深入研究 TSN 标准,重点介绍与汽车领域最相关的关键特性。我们还将讨论使用 SJA1105TEL 汽车以太网交换机可以实现的潜在用例,并讨论支持在汽车中采用此类交换机的生态系统。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 时间敏感网络是工业和汽车以太网领域的下一个热门领域。在本次会议中,我们将深入研究 TSN 标准,重点介绍与汽车领域最相关的关键特性。我们还将讨论使用 SJA1105TEL 汽车以太网交换机可以实现的潜在用例,并讨论支持在汽车中采用此类交换机的生态系统。
記事全体を表示
インフォテインメント、コネクティビティ、セキュリティ:カーラジオ、オーディオ、アンプ - 市場とテクノロジーの最新情報 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> インフォテインメント市場の動向とNXPの最新テクノロジーに関する最新情報。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> インフォテインメント市場の動向とNXPの最新テクノロジーに関する最新情報。 オーディオ処理と増幅
記事全体を表示
Time Sensitive Networking(TSN)による産業用ネットワーキングの次の波 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> インダストリアルOEMは、デバイスでサポートする必要のある多数のネットワークプロトコルに悩まされてきました。新しいIEEEタイムセンシティブネットワーキング(TSN)規格は、複数の独自のプロトコルを共通のIEEEベースの規格に統合することを提供します。TSNで何ができるかを学びに来てください。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> インダストリアルOEMは、デバイスでサポートする必要のある多数のネットワークプロトコルに悩まされてきました。新しいIEEEタイムセンシティブネットワーキング(TSN)規格は、複数の独自のプロトコルを共通のIEEEベースの規格に統合することを提供します。TSNで何ができるかを学びに来てください。
記事全体を表示
具备 SafeAssure ®认证功能的 i.MX 8 MCU — 摄像头、视频、音频、可信环境 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本课程将解释为 i.MX 8 提供的几种软件解决方案。SafeAssure 软件允许进行系统分区,充分利用 i.MX 8 的一些安全功能。Fast Path 软件允许在 2 个网络接口之间路由/桥接数据,以最大限度地提高数据路由性能,同时将主处理器的 CPU 负载要求降至最低。可信环境允许充分利用 Arm ® Trustzone 功能。 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 本课程将解释为 i.MX 8 提供的几种软件解决方案。SafeAssure 软件允许进行系统分区,充分利用 i.MX 8 的一些安全功能。Fast Path 软件允许在 2 个网络接口之间路由/桥接数据,以最大限度地提高数据路由性能,同时将主处理器的 CPU 负载要求降至最低。可信环境允许充分利用 Arm ® Trustzone 功能。
記事全体を表示