Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
SJA1110 port 2 PHY to MAC Hi, I have an SJA1110 connected to an external microcontroller via SPI and RMII. Managed to get the switch working vie SPI configuration upload. It seems, that the microcontroller is able to use the RMII interface, I can read out MII_PHYSID1  and MII_PHYSID2 as 0x001BB012. However, whatever I do, I cannot get the link status to "up". The PHY is connected via Ethernet cable to my computer. After writing the very large manuals, it is still unclear to me if I need to configure the port 2 PHY in any special way for use with the RMII interface. Is there some kind of power down which needs to be disabled? Does someone know, if the general procedure is comparable to the TJA1100? Thanks Re: SJA1110 port 2 PHY to MAC It works now. The RGMII Tx clock is generated by the external CPU, in the firmware was the wrong clock source selected. Setting it to a correctly configured clock source, made ethernet work for rx and tx. Re: SJA1110 port 2 PHY to MAC Hi Pavel, sorry, still open. Also, I think there was some misunderstanding how the switch port 2 MAC / PHY work together with the SMI and the RGMII. I hope I understand it right, that the switch port 2 with "phyless" use simply uses a SMI for configuration and RGMII for data transfer? When I read out via generic PHY functions the PHYID1/PHYID2 via SMI, I get 0x001B and 0xB012. Where does this come from? I checked "phyless", so is this info the PHY interface of the integrated CPU in the SJA1110? Meanwhile, I can receive UDP broadcast frames. Reading out the  // Read ACU port 2 status register ret = boardSJA1110_read_reg(0x1C4441, &cfg_stat); tells me, that Tx of the RGMII (connected to Rx of my CPU, correct? So Rx SJA1110 -> Tx external CPU and Tx SJA1110 -> Rx external CPU) is fine and clock present. However, it also tells that the Rx clock of the SJA1110 port 2 RGMII could not be detected, which may be the reason why I can not send and only receive frames. Unfortunately, the board I have received does give poor access to the Rx clock line of the RGMII, so I have a hard time to check what is happening there via oszi. As I understand, the external CPU should deliver a Tx clock signal to the Rx clock pin of the SJA1110 when RGMII is used. Grabbing the configuration code of the SJA1110 SDK for ACU_SJA1110_cfgPinMiix_t setting the clock source from the preconfigured "auto" to other options did not help, also playing around with ACU_SJA1110_cfgPinMiixId_t delay setting did not help. The configuration registers says always, that the RGMII of port 2 of the SJA1110 does not see a Rx clock. Should this clock be always there or just when something is sent? Best regards, Rainer Re: SJA1110 port 2 PHY to MAC Hi Rainer, I answered to your questions by email. Best regards, Pavel
View full article
Move S32DS3.4 license to New Computer Hello, My old computer was broken suddenly. And I'm trying to install S32SD3.4 in my new computer. But I encountered problem will the license. My license details:  License Applicable to Product(s):    Version    Description    3.4    S32 Design Studio for S32 Platform v.3.4   License Quantity:Fulfillment ID:Expiration Date:Product:Machine:Activation Code: 1 119777581 Aug 26, 2028 S32 Design Studio for S32 Platform v.3.4 3288C64F4AB78208C41AECE1A81C3C989BA229B2 E4DE-FECF-56E6-BEEC Re: Move S32DS3.4 license to New Computer Hello Robin, Total Number of Licenses of v3.4 still remains 1, but v3.5 had increased. It is very helpful when testing some software combination for customers. Would you please also help increase it for v3.4? Thank you very much. Re: Move S32DS3.4 license to New Computer Hi this issue could be caused by blocking the online communication with the licensing/activation server. I'd suggest you to try to activate the product using offline activation. see HOWTO: Activate S32 Design Studio - NXP Community Hope it helps Stan Re: Move S32DS3.4 license to New Computer Hi Go into "My NXP Account > Apps and Services > Activate my Software > View accounts > Select S32 Design Studio for S32 Platform v3.4". Once there, select "License Keys" and the License Information should be present. After clicking the link I sent you privately, does the Total Number of Licenses increase? Best Regards, Robin ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. -------------------------------------------------------------------------------
View full article
S32K324 HSEフラッシュと暗号テストの問題 NXPサポートチーム様 S32K324 マイクロに「HSE_FW_S32K344_12_2_69_1」をフラッシュしようとしています。 以下の投稿に添付されているスクリプトを使用してみました。 S32K324 および S32K312 HSE FW Lauterbach インターフェース スクリプトの要件。- NXPコミュニティ 最初の INSTALL スクリプトでは IVT イメージのみをインストールするように指示されていますが、ピンクのイメージしかないSO、それを使用できませんでした。 2 番目のスクリプト (HSE インターフェース スクリプト) はこれを使用してピンク色のイメージをインストールできますが、暗号化機能はいずれも動作しません。 そして、電子メールで提案されたとおり、確認を求められたアドレスの以下の値を取得しました。これらの値が予想通りであるかどうかをお知らせください。 また、キー プロビジョニングをデバッグしているときに、hse_ip_serv 関数に到達できることを確認できましたが、タイムアウトが発生したため、下の画像に示すように、HSE が応答を返すことができないようです。 サポートをお待ちしております。 よろしくお願いいたします。 ニティン・ヴィシュノイ Re: S32K324 HSE flashing and Crypto test issue 今後のコミュニケーションのため、このチケットをGMサポートフォーラムに移動しました。 S32K324 HSEフラッシュと暗号テストの問題 - NXPコミュニティ Re: S32K324 HSE flashing and Crypto test issue こんにちは@nitvishnoi はい、GSR レジスタのビット 0 が設定されているSO、致命的なエラーが原因で HSE がシャットダウンされました。データ キャッシュを無効にして、違いがあるかどうか確認してみます。 GM は、FAE とプライベート コミュニティ スペースを通じて直接サポートを受けることができます。さらなるサポートについては、むしろこれらのチャネルを使用することをお勧めします。 よろしくお願いいたします。 ルーカス Re: S32K324 HSE flashing and Crypto test issue こんにちは、ルーカス。 FSR レジスタと GSR レジスタの詳細は次のとおりです。何か見つかった場合はお知らせください。 今日午後 4 時 (東部標準時) に電話に参加したい場合はお知らせください。昨日、cinco に招待状を送りました。 よろしくお願いいたします。 ニティン・ヴィシュノイ Re: S32K324 HSE flashing and Crypto test issue こんにちは@nitvishnoi 0x4039_C028 の HSE GPR レジスタによると、HSE ファームウェアがインストールされています。 HSE サービスが完了せず、タイムアウトが発生した場合は、MU 内の FSR および GSR レジスタをチェックして何が起こったかを確認します。タイムアウトの一般的な問題は、何らかのサービスを呼び出すときに間違ったポインタが HSE に渡されることです。HSE がデータにアクセスできない場合 (権限不足、ダブル ビット ECC エラー、実装されていない領域にアクセスしているなど)、HSE はシャットダウンされます。 よろしくお願いいたします。 ルーカス
View full article
ntag424dna 写入耐久性 HI 我在问某些 NFC 标签上的写入操作 这里是谷歌: 1.直接更新标签上的计数器   许多 NFC 芯片,例如 NTAG 213、215 或 216,都有内置计数器,可以将其配置为每次扫描标签时递增。 当扫描具有此功能的标签时,芯片本身会更新存储在其存储器中的计数器值。该更新过程是一个写入操作。 该计数器可纳入 NDEF 信息,例如,将其添加到 URL 的末尾,这样每次扫描都会返回一个唯一的链接。 这种操作(计数)是否会计入每个芯片的"写入周期" 限制? 就 NTAG 424 DNA 的整体寿命而言,如果其他因素相同,没有启用读取计数器的芯片在技术上比有计数器的芯片寿命更长, 。 原因就在这里: 写耐久性: 每次读计数器递增,都被视为对芯片内存的一次写操作。 有限的写入周期: 包括 NTAG 424 DNA 在内的所有 NFC 芯片在可能发生故障之前所能承受的写入周期都是有限的。NTAG 424 DNA 的额定写入次数最少为 200,000 次。 减少写入次数,延长使用寿命: 如果芯片没有计数器,或计数器功能被禁用,则每次读取标签时都不会发生自动写入操作。这将从根本上保护芯片的写入耐久性,使其能够工作更长时间,理论上可达到最大写入周期限制,甚至更长,这取决于其他写入操作的频率。 这是真的吗?有相关文件吗? 我们正在开发Ntag的应用程序,以供大众TAP(营销),并需要知道何时需要为我们的解决方案更换芯片。 感谢您的指点。 Re: NTAG424DNA WRITE ENDURANCE 是的。 Re: NTAG424DNA WRITE ENDURANCE 因此,不同位置上的计数器更新不会影响标签的写入周期,从而无需在 200,000 计数时更换标签。是这样吗? Re: NTAG424DNA WRITE ENDURANCE NFC 计数器有一个机制,可存储& 从物理上不同的 EEPROM 存储位置读取的值。这样,可以达到 3 字节计数器的最大值,并且不会损坏 EEPROM 单元。
View full article
Zephyr を使用した MCXN947 上の MCUBoot と Edgelock セキュア・エンクレーブ FRDM-MCXN947 ボードを使用する IoT プロジェクトで Zephyr のオープン ソース MCUBoot モジュールを使用したいのですが、キーのセキュリティを強化するために Edgelock セキュア・エンクレーブも使用したいです。MCUBoot でセキュア・エンクレーブを使用するには、MCUBoot ソースを変更する必要があるため、これは難しいという認識でよろしいでしょうか? 私の考えが正しければ、FUTURE Zephyr / MCUBoot が Edgelock セキュア・エンクレーブを使用する可能性はありますか? この改善によりセキュリティが大幅に向上するというのは正しいでしょうか?それとも、標準の Zephyr MCUBoot のキー処理で満足すべきでしょうか? Re: MCUBoot and Edgelock Secure Enclave on an MCXN947 using Zephyr @Harry_Zhangこれがいつ実現されるかについて、何かフィードバックはありますか?すぐにでなければ、Zephyr で MCUBoot を使用して最高のキー セキュリティを維持する方法について何か提案はありますか? 幸運をお祈りしています。! クラーク Re: MCUBoot and Edgelock Secure Enclave on an MCXN947 using Zephyr こんにちは@ClarkS はい、MCUBoot で EdgeLock SE を使用するのは現時点では簡単ではなく、ソースの変更やカスタム統合レイヤーが必要になると思います。 お客様のご要望を弊社の担当チームに転送させていただきます。ご提案ありがとうございます。 BR ハリー
View full article
imx8mp hdmi 4k 显示 我现在使用imx8mp evk开发板,linux内核版本是linux-imx-5.10.9。使用HDMI接口,发现默认输出为1080p@60,请问怎么修改内核使HDMI输出为4K。 Re: imx8mp hdmi 4k 显示 您好,我这边也遇到了这个问题,方便了解一下你们最后是怎么解决这个问题的吗? Re: imx8mp hdmi 4k 显示 嗯,谢谢。 问题的关键在于我们是医疗设备公司,之前的用户界面是QT 开发的,平台是你们的imx6 imx7,现在高端产品线用你们的8了。之前所有的代码都是基于fb的,如果现在换到drm,代价很大............算了,我再研究下吧,看看能不能修改你们那部分源码,实现根据插拔的显示器数量创建不同个数的fbx Re: imx8mp hdmi 4k 显示 桌面系统不使用fb0,使用drm节点,即使fb0是可以用的,我们也不推荐,主流就是drm框架。 Re: imx8mp hdmi 4k 显示 我是没动你们内核中关于fb0生成的源码,现在是跟你们bsp里面一模一样的,你们的源码里面就是用drm框架最后生成了一个fb0,就这一个,不管插几个屏幕也是就这一个fb Re: imx8mp hdmi 4k 显示 也就是说lvds 和 hdmi都插着的情况下,虽然这两个分辨率不一样,但是内核申请的buffer是按照lvds的分辨率来的,hdmi和lvds显示的时候也都是用的这一个buffer,所以导致了现在hdmi显示异常喽? 那就难搞了.......... Re: imx8mp hdmi 4k 显示 我还以为hdmi会自适应切换分辨率 -->基于DRM API可以实现不同CRTC下的buffer分配,但是直接写fb0的话,就是会出现这种显示不匹配的问题。你在应用层分配的buffer肯定是针对某个屏幕,比如LVDS分辨率大小的buffer,那你写进去了,底层驱动只是直接把这块buffer丢进lcd控制器,驱动层很傻的不会自适应。你丢进去多大分辨率的buffer,他就原封不动显示这么大。 Re: imx8mp hdmi 4k 显示 我们是想实现双屏同显,qt向fb0写图像数据,希望fb0中的图像数据能够在1200*768的lvds和1920*1080的hdmi上同时显示。你认为这是做不到的吗? 现在qt那边用的是eglfs的形式,要想同显必须是eglfs-kms这种直接操作drm生成的cardx节点的才行吗? Re: imx8mp hdmi 4k 显示 我现在lvds屏幕是1200*768的,hdmi支持的分辨率最大是1920*1080的。所以你意思是如果要lvds和hdmi显示正常的话,hdmi的分辨率也要手动设置为1200*768这种或者相近的分辨率才行吗? 我还以为hdmi会自适应切换分辨率,我从hdmi显示器设置里看到现在的屏幕显示分辨率是1920*1080的,同时hdmi上显示的图像也是只有左上角有一块,且大小跟lvds大小相近 Re: imx8mp hdmi 4k 显示 测过了,可以自动识别4K。 lvds 和 hdmi共享同一个drm框架生成的fb0节点 --》这不是只能有一个分辨率吗?在你共享fb0的情况下,LVDS和HDMI屏幕分辨率是一样的吗? Re: imx8mp hdmi 4k 显示 有解决方案吗? 我现在还遇到一个问题,lvds 和 hdmi共享同一个drm框架生成的fb0节点,lvds和hdmi都被连接上后,hdmi显示的图像大小跟lvds是一样大的,没有铺满整个hdmi显示器,这是怎么回事? Re: imx8mp hdmi 4k 显示 我能看到一样的现象,稍后给你解决方法 Re: imx8mp hdmi 4k 显示 我烧写了L5.10.35_2.0.0的demo images,分别在2K和4K的屏幕上试过,还是只能显示1080p。 使用modetest检查HDMI最大为1920x1080@60,并没有4k的分辨率 Re: imx8mp hdmi 4k 显示 HMDI显示分辨率是自适应的,你试一下L5.10.35_2.0.0的demo images
View full article
LPC1768 シリーズに代わる推奨マイクロコントローラ シリーズは何ですか? こんにちは、 LPC17xx シリーズの正確なピン交換を提案していただける方はいらっしゃいますか。 既存のデザインがあり、ハードウェアの変更が問題ですが、LPC2148 ペリフェラル (UART、I2C、タイマーなど) を使用するコードが大量 (トン単位) あります。どの新しいファミリがペリフェラルソフトウェアと互換性がありますか? 新しいデザインに推奨されるシリーズのうち、ほぼ同等の機能 (メモリ サイズ、速度、ペリフェラルなど) を備えているのはどれですか。 Re: What is the recommended microcontroller series that replaces the LPC1768 series? 私も同じ疑問を抱いています。もう5年近く経っているのに、そう思っています。 新しいデザインに使用するマイクロコントローラのシリーズはどれを検討すればよいでしょうか? Re: What is the recommended microcontroller series that replaces the LPC1768 series? ハイ LPC1768 は LPC2368 の代替品です。LPC1769 は LPC1768 の代替品です。唯一の違いは最大クロック周波数(120Mhz)です。メモリが少ない代替品としては LPC1766 があります。LPC4078 は LPC176x の代替品として選択肢となります。( http://www.nxp.com/products/microcontrollers/core/cortex_m4_m4f/LPC4078FBD100.html ) なお、LPC4078 の発売時期は 2013 年で、寿命は 15 年です。 弊社の推奨は、220MHzのCortex M4コア(オプションでセカンダリCortex M0+コア搭載)をベースにしたLPC546xxまたはLPC540xx MCUシリーズ、同様のペリフェラル、最大512KBのフラッシュ、最大200KBのRAMです。詳細については、次のリンクをご覧ください: https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/lpc-cortex-m-mcus/lpc54000-series-cortex-m4-mcus :MC_1414576688124 LPC546xxとLPC540xxはLPC17xxのピン互換品ではありません 良い1日を、 ジャン・ジュン
View full article
リモートアクティベーションサーバーへのアクティベーション要求の送信中にエラーが発生しました NXPソフトウェアアクティベーション リモート アクティベーション サーバーにアクティベーション要求を送信し、結果の応答をプロセッシングするときにエラーが発生しました。ライセンス サーバーまたは Operations サーバーに接続できませんでした。(FNPエラー50041,41143,34) これはオンライン インストール中です、オフライン インストールも実行されていません、無効なオフライン応答、応答タイプが表示されています 回复: Error sending an activation request to a remote activation server S32 Design Studio for ARM バージョン 2.2 のインストール中に、「リモート アクティベーション サーバーにアクティベーション要求を送信し、結果の応答を処理中にエラーが発生しました。」というエラーが発生しました。ライセンス サーバーまたは Operations サーバーへの接続に失敗しました。(FNPエラー50041,41143,34)の問題を解決するにはどうすればよいですか?以下はログです。 Re: Error sending an activation request to a remote activation server ありがとうございます。解決しました。公式サイトを参考にしました。 https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32-Design-Studio-Offline-activation-issue-hot-fix/ta-p/1119120 Re: Error sending an activation request to a remote activation server これはインストール ログです。 Re: Error sending an activation request to a remote activation server これはログ内のエラー メッセージですが、管理者として実行しています。 Re: Error sending an activation request to a remote activation server これはオフラインの状況です Re: Error sending an activation request to a remote activation server こんにちは、 どのアプリケーションをアクティブ化しようとしているのかを教えていただけますか?また、エラーの画像を共有していただけますか? ぜひお知らせください。
View full article
KW45B41Z83 查询 您好,NXP团队, 我目前的项目正在使用 KW45 微控制器,我对它有一些疑问,需要您提供以下意见:- 1) KW45 MCU 是否支持 Autosar? 如果回答为 "是",请提供相关信息,以便实施。 2) KW45 是否支持引导加载器映像功能,我在 sdk 示例中没有找到相关示例,我需要执行固件升级,您能否提供一些相关信息。 请您就此提供一些意见。 感谢并致意 加内什-帕瓦尔 Re: KW45B41Z83 Query 你好,加内什 您是否已经有恩智浦的直接联系人或销售代表?如果您没有任何联系方式,请联系我们的代理商网络|NXP,以帮助您查看有关Autosar KW45支持的请求。 KW45 使用名为 " otac_att " 的示例支持引导加载程序;我建议使用 KW45 EVK 最新 SDK 版本 [25.03] 来查看此示例,本应用说明还描述了有关为 KW45 https://www.nxp.com/docs/en/application-note/AN13860.pdf 创建固件更新映像的示例和说明 顺祝商祺! 路易斯
View full article
看门狗定时器 MIMXRT1042XJM5B 的引脚配置 亲爱的团队 我们在即将到来的项目中使用 MIMXRT1042XJM5B,我们正在寻找 Watch Dog Timer 的引脚排列,在那里可以对其进行配置,请与我们联系 期待您的来信、 此致, Bhavesh Re: Pin configuration for Watch Dog timer MIMXRT1042XJM5B 你好@bhaveshtirex、 非常感谢您关注我们的产品并使用我们的社区。 关于"我们在即将开始的项目中使用 MIMXRT1042XJM5B,我们正在查找 Watch Dog Timer 的引脚输出,它可以在哪里配置" ,在 IMXRT1040RM 中,有一些关于 WDOG 外部信号的说明。 至于如何配置引脚,您可以使用 MCUXPresso IDE 中的引脚工具 希望它能帮到你。 如果您还有疑问,请告诉我。 祝你愉快 敬上 MayLiu
View full article
コピー: S32K314_324 RTD FLSおよびMemInFLS読み取りおよび書き込みパラメータの検証に関する質問 この投稿はここからのコピーです こんにちは、K3チーム 弊社のお客様 (SWS) は、以下の 4 種類のフラッシュ ドライバ パラメータの設定値が CPU 負荷とプロセッシング速度の最適なバランスを提供しているかどうかを NXP に確認および検証するよう依頼したいと考えています。 この評価は、現在の構成がパフォーマンスのボトルネックや不要な CPU オーバーヘッドにつながらないことを確認するために重要です。 Q1. 確認していただけますか? これはパフォーマンスを予測するのが難しいと思います... 1.FlsMaxRead高速モード – 256 バイト 2.FlsMaxReadNormalMode – 128バイト 3.FlsMaxWrite高速モード – 256 バイト (デフォルト) 4.FlsMaxWriteNormalMode – 128バイト RTD2.0.1 D2207を使用していますが、RTD 5.0.0にアップデートする予定です。もうすぐD2410。 - S32K3 リアルタイム・ドライバ バージョン 2.0.1_D2207 - S32K3_S32M27x リアルタイム・ドライバ ASR R21-11 バージョン 5.0.0_D2410 これらのパラメータは AUTOSAR 仕様であるにもかかわらず、RTD 2.0.1 および 5.0.0 を搭載した S32DS および EB-Tresos ではこれらのパラメータを見つけることができません... Q2. 通常モードと高速モードのパラメータを含むこれらのパラメータは、NXP RTD(図1)で使用できますか? Q3. このFlsTotalSizeパラメータはNXP RTD(図2)で使用できますか? 2025年9月10日の顧客レビュー会議中に以下の情報を得ました。 図1.ダヴィンチがそれを見せます。 図2.ダヴィンチがそれを見せます。 敬具、 ふみ 優先度: 高 RTD 出典: NXP社内 Re: Copy: S32K314_324 RTD FLS and MemInFLS Question about validation of Read and Write Parameters こんにちは@Nhi_Nguyen 、 SOありがとうございます! 心から、 ふみ Re: Copy: S32K314_324 RTD FLS and MemInFLS Question about validation of Read and Write Parameters こんにちは@Fumihiko_Satoさん 1. ドライバはFlsTotalSize を使用しません。 2. パッケージ4.0.0P24 は AUTOSAR 4.4 に準拠し、Fls が使用されるSO、これらのパラメーターが存在し、201 と同じです。 よろしくお願いいたします。 ニ Re: Copy: S32K314_324 RTD FLS and MemInFLS Question about validation of Read and Write Parameters こんにちは@Nhi_Nguyen 、 迅速なご対応誠にありがとうございます! FlsTotalSize は RTD 2.0.1 では「読み取り専用」になっていますが、RTD はこの値を使用するのでしょうか? お客様から値が間違っていると言われたためです。 内部的に確認してもらえますか? Q2.申し訳ありません、間違いがありました... お客様はS32M27xリアルタイム・ドライバAUTOSAR 4.4バージョン4.0.0にアップグレードします。P24. FLS DRV を調べた限りでは、5 種類のパラメータがあります。 これらのパラメータが RTD4.4 P24 に存在するかどうかをもう一度確認していただけますか? 敬具、 ふみ Re: Copy: S32K314_324 RTD FLS and MemInFLS Question about validation of Read and Write Parameters こんにちは@Fumihiko_Satoさん ユーザーが RTD2.0.1 を RTD 5.0.0 にスイッチした場合、これらのパラメータは RTD5.0.0 には存在しません。(図 1-1) 1. FlsMaxRead高速モード 2. FlsMaxReadNormalMode 3. FlsMaxWrite高速モード 4. FlsMaxWriteNormalMode 5. 合計サイズ => はい、RTD500 は Mem ドライバのみをサポートし、Fls はサポートしていないためです。これらのパラメータは、Fls の ASP 仕様で定義されています。SO、これらのパラメーターは RTD500 には存在せず、RTD500 の Mem ドライバには影響しません。 ユーザーがRTD 2.0.1のFlsTotalSizeの値を設定した場合、影響はありません。(図1-2) => 実際、このノードは読み取り専用SO、ユーザーはこれを構成できません。 よろしくお願いいたします。 ニ Re: Copy: S32K314_324 RTD FLS and MemInFLS Question about validation of Read and Write Parameters こんにちは@Nhi_Nguyen 、 サポートありがとうございます! ユーザーが RTD2.0.1 を RTD 5.0.0 にスイッチした場合、これらのパラメータは RTD5.0.0 には存在しません。(図 1-1) 1. FlsMaxRead高速モード 2. FlsMaxReadNormalMode 3. FlsMaxWrite高速モード 4. FlsMaxWriteNormalMode 5.フラッシュ合計サイズ ユーザーがRTD 2.0.1のFlsTotalSizeの値を設定した場合、影響はありません。(図1-2) それは正しいですか? 図1.ニ・アンス よろしくお願いします、 ふみ Re: Copy: S32K314_324 RTD FLS and MemInFLS Question about validation of Read and Write Parameters こんにちは@Luis_Garabo 、 4 つのパラメータFlsMaxRead Fast Mode、FlsMaxReadNormalMode、FlsMaxWrite Fast Mode、FlsMaxWriteNormalMode についての説明は次のとおりです。 高速/通常モードでのフラッシュ ドライバのジョブ プロセッシング機能の 1 サイクルで読み取り/書き込みできる最大バイト数。 SO、4 つのパラメータの値が大きい場合、同じ長さでの Main 関数のサイクル数は少なくなります。これもパフォーマンスの向上に役立ちます。 Fls_u32MaxRead/Write はフラッシュ ドライバの 1 サイクルで読み書きできる最大バイト数であり、これらの 4 つのパラメーターとデフォルト モードから計算されます。例えば: Fls のデフォルト モードが MEMIF_MODE_SLOW の場合、Fls_u32MaxRead/Write はFlsMaxReadNormalMode、FlsMaxWriteNormalMode から取得されます。 Fls のデフォルト モードが MEMIF_MODE_FAST の場合、Fls_u32MaxRead/Write は FlsMaxWrite高速モード、FlsMaxRead高速モードから取得されます。 S32K3リアルタイム・ドライバ バージョン2.0.1_D2207パッケージには、Fls ドライバがサポートされています。 パッケージS32K3_S32M27xリアルタイム・ドライバASR R21-11バージョン5.0.0_D2410では、メモリドライバがサポートされています。 それらは異なる ASR 仕様に従います。SO、これらのパラメータは RTD500 ではなく RTD201 にのみ存在します。 Q1.2.0.1 では、そうです。 Q2. はい、しかし設定できません よろしくお願いいたします。 ニ
View full article
IMX RT1064: 電源投入後の入力キーパーの状態 こんにちは、 私たちのシステムでは、電源投入後、非常に長い時間(数日間)にわたって POR_B を低レベル(リセット状態を維持するため)にCAN必要があります。電源投入直後、ピンの最後の状態は不明です。データシートの「リセット時のデフォルト設定」に「入力キーパー」値が記載されているピン(GPIO_EMC_00 など)の場合、リセット状態中のこれらのピンの状態は次のようになります。 ランダムな論理値 (Vss または Vdd) か浮動状態か? i.MXRT 106x Re: IMX RT1064: input keeper state after power up こんにちは@Olivier3 、 キーパー付きの GPIO ピンは、リセット前の状態に応じてハイまたはローの状態になりますが、フローティングにはなりません。 詳細については、次のリンクを確認してください。 i.MX RT1020 GPIO デフォルト設定 - NXPコミュニティ システムコントローラファームウェア101 - パッド構成サービス - NXPコミュニティ BR、 イサウルO。
View full article
GMAC0 クロックが s32g2 カーネルで動作しない - Linux BSP-43 こんにちは、皆さん。 私たちは、カスタム ボードで gmac0 が MII モードで PHY とインターフェースしている Linux BSP-43 の問題を解決しようとしています。 問題の詳細は下記のチケットに記載されています。このチケットを調査している NXP の担当者は休暇中です。誰か解決を手伝ってもらえませんか。私たちはすでにこれを優先して取り組むために多くの時間を費やしてきました。 https://community.nxp.com/t5/S32G/GMAC0-in-MII-mode-on-s32g2-not-getting-the-clk/mp/2170925#M14910 よろしくお願いいたします。 ミスバ Re: GMAC0 Clock not working on s32g2 kernel - Linux BSP-43 こんにちは@khan_misbahさん、 私の理解では、GMAC を MII モードで設定する必要があるということです。BSP は RDB2 ボード用であり、MII イーサネット PHY がないため、MII を構成するための簡単な手順はありません。このリクエストについては社内チームにお問い合わせする必要がありますが、祝日のためほとんどのメンバーが不在であることをご了承ください。彼らからのフィードバックを得るまでに時間がかかることをお詫び申し上げます。 できるだけ早くご連絡させていただきます。 ご理解のほどよろしくお願いいたします Re: GMAC0 Clock not working on s32g2 kernel - Linux BSP-43 こんにちは、 @khan_misbahさん、 緊急性は理解しておりますが、ご参照の投稿を確認し、問題と現在の状況を把握するために少し時間をください。 よろしくお願いします。
View full article
H265 解码占用 iMX8M Plus 更多的 CPU 负载 大家好, ,我正在尝试获取 vpu 的 clk_summary。我的 vpu_g1 设置为 "Y",但 vpu_g2 设置为 "N"。是不是因为这个原因,当我解码 H265 时,CPU 负载增加到 85% ,而解码 H264 时 CPU 负载仅为 7% 。 H265 解码命令: ./g2dec -tbs encoded.hevc -Oout.yuv H264 解码命令: /hx170dec-arm- otest_hxdec.yuv DOP_Animation_W_.H264 c at /sys/kernel/debug/clk/clk_summary | grep vpu vpu _g1 0 0 0 800000000 0 0 0 0 800000000 0 0 0 800000000 N 38300000.vpu_g1clk_hantro vpu_pll_ref_sel 0 0 0 24000000 0 0 50000 Y deviceless no_connection_id vpu_pll 0 0 700000000 0 0 50000 Y deviceless no_connection_id vpu_pll_bypass 0 0 700000000 0 0 50000 Y deviceless no_connection_id vpu_pll_out 0 0 700000000 0 0 50000 N deviceless no_connection_id vpu_g2 0 0 700000000 0 0 50000 N deviceless no_connection_idno_connection_id vpu_pll_out 0 0 0 700000000 0 0 50000 N deviceless no_connection_id vpu_g2 0 0 700000000 0 0 50000Ndeviceless no_connection_id vpu_g2_root_clk 0 0 700000000 0 0 50000 N 38310000.vpu_g2clk_hantro 谢谢、 i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: H265 Decoding consumed more cpu load on iMX8M Plus 你好,在用上市 gst-launch 之前 我没有使用任何其他命令。 致敬, Zhiming Re: H265 Decoding consumed more cpu load on iMX8M Plus 你好,你是 怎么在执行 gst-launch 命令时运行最高命令的。 谢谢, Hariharan Re: H265 Decoding consumed more cpu load on iMX8M Plus 您好, 使用 gstreamer 的 i.MX8MP EVK 不存在 CPU 负载问题。 root@imx8mpevk:~# gst-launch-1.0 filesrc location=test_MediaCoder_HEVC_demo_video.mp4 typefind=true ! video/quicktime ! aiurdemux ! h265parse ! queue max-size-time=0 ! v4l2h265dec ! autovideosink Setting pipeline to PAUSED ... ====== V4L2DEC: 1.26.0 build on May 7 2025 08:46:20. ====== Pipeline is PREROLLING ... ====== AIUR: 4.10.0 build on May 10 2025 01:33:22. ====== Core: MPEG4PARSER_06.22.14 build on Apr 28 2025 08:50:53 file: /usr/lib/imx-mm/parser/lib_mp4_parser_arm_elinux.so.3.2 ------------------------ Track 00 [video_0] Enabled Duration: 0:00:59.958333000 Language: und Mime: video/x-h265, parsed=(boolean)true, alignment=(string)au, stream-format=(string)hev1, width=(int)1920, height=(int)800, framerate=(fraction)24/1, codec_data=(buffer)01016000000080000000000078f000fcfdf8f800000f03a00001001840010c01ffff0160000003008000000300000300789dc090a100010021420101016000000300800000030000030078a003c080321659de491b6bc0400800a2000100064401c173d189 ------------------------ ------------------------ Track 01 [audio_0] Enabled Duration: 0:01:01.347120000 Language: und Mime: audio/mpeg, mpegversion=(int)4, channels=(int)1, rate=(int)22050, bitrate=(int)28992, stream-format=(string)raw, codec_data=(buffer)138856e5a54880 ------------------------ Redistribute latency... Redistribute latency... Pipeline is PREROLLED ... Setting pipeline to PLAYING ... Redistribute latency... New clock: GstSystemClock ^Chandling interrupt. (37.5 %) Interrupt: Stopping pipeline ... Execution ended after 0:00:23.068026502 Setting pipeline to NULL ... Total showed frames (556), playing for (0:00:23.067971879), fps (24.103). Freeing pipeline ... root@imx8mpevk:~# cat /sys/kernel/debug/clk/clk_summary | grep vpu vpu_vc8000e 0 0 0 500000000 0 0 50000 Y deviceless no_connection_id vpu_vc8ke_root_clk 0 0 0 500000000 0 0 50000 N 38320000.vpu_vc8000e clk_hantro_vc8000e vpu_bus 0 0 0 800000000 0 0 50000 Y deviceless no_connection_id vpu_root_clk 0 0 0 800000000 0 0 50000 N 38320000.vpu_vc8000e clk_hantro_vc8000e_bus 38310000.vpu_g2 clk_hantro_bus 38300000.vpu_g1 clk_hantro_bus vpu_g1 0 0 0 800000000 0 0 50000 Y deviceless no_connection_id vpu_g1_root_clk 0 0 0 800000000 0 0 50000 N 38300000.vpu_g1 clk_hantro vpu_pll_ref_sel 0 0 0 24000000 0 0 50000 Y deviceless no_connection_id vpu_pll 0 0 0 700000000 0 0 50000 Y deviceless no_connection_id vpu_pll_bypass 0 0 0 700000000 0 0 50000 Y deviceless no_connection_id vpu_pll_out 0 0 0 700000000 0 0 50000 N deviceless no_connection_id vpu_g2 0 0 0 700000000 0 0 50000 N deviceless no_connection_id vpu_g2_root_clk 0 0 0 700000000 0 0 50000 N 38310000.vpu_g2 clk_hantro 问题应该来自您的g2dec 应用程序。 致敬, Zhiming
View full article
K82マイクロコントローラのQSPIエイリアス領域の使い方 皆様、 現在、FRDM-K82F 評価ボード上の led_demo_qspi_alias デモ プロジェクトに取り組んでおり、デバッグ目的で K82 マイクロコントローラ上の QSPI エイリアス領域を活用する方法をより深く理解したいと考えています。 MBOOTQSPIUG ドキュメントに記載されている手順を慎重に実行しましたが、残念ながら期待どおりの結果は得られませんでした。参考までに、NXPコミュニティフォーラムの「frdmk82のled_demo_qspi_aliasサンプルプロジェクト使用時のトラブルシューティング」というトピックで私の問題も説明しました。 ここで、J-Link デバッガーと MCUXpresso を使用してプロジェクトをロードしてみることにしました。次のような動作が観察されました。 起動時に、プログラム カウンターがブートローダー領域で停止しているように見えます。 しかし、プログラムカウンタをmain()のアドレス(.mapから取得)に手動で設定すると、ファイル) の場合、デバッグ セッションが正常に開始されます。 この動作の原因は何なのか明確にしていただけますか?特に、MBOOTQSPIUG ドキュメントの手順が私のCASEでは機能しないと思われることを考慮すると、この起動の問題を回避するための推奨される方法はありますか? サポートをよろしくお願いいたします。 敬具、 ウラジミール・ジトリ Re: How use QSPI Alias region in K82 microcontroller こんにちは@Vladimir_Zitoli お問い合わせいただきありがとうございます。 - MBOOTQSPIUG ドキュメントの「第 8 章 QuadSPI エイリアス領域で実行されるアプリケーション」を参照しましたか?この章では、エイリアス メモリ領域からアプリケーションをダウンロードして実行する方法について説明します。手順の説明は IAR IDEs に基づいていることに注意してください。MCUXpresso IDE を使用している場合は、リンカー ファイルを設定するときに特に注意してください。 以下はその例です。 - MCUXpresso IDEで「led_demo_qspi_alias_a000」デモをデバッグするだけであれば、以下に示すように、リセット処理設定をSOFTに変更してください。 搭載デバッグ プローブを CMSIS-DAP に変更します。 BR アリス
View full article
TL431 稳压器电阻器 大家好 我对 TEA1733T ic 有一些疑问,希望得到澄清。 tea1733t ic 数据表: https://www.nxp.com/docs/en/data-sheet/TEA1733T.pdf 应用说明: https://www.nxp.com/docs/en/application-note/AN10868.pdf 图 1-这是 TEA1733T 集成电路的参考示意图。 1- 我的第一个问题是,如果我想要 24 伏 3 安培的输出电压,那么电阻 R23 和 R24 的值是多少(如何选择这些电阻)? 2- 我的第二个问题是,在栅极电压为 10-12V 和开关频率为 66khz 的情况下,馈入变压器原边的 MOSFET 的开关电压是多少? 谢谢! 隔离栅极驱动器 Re: tl431 regulator resistor 您好@TomasVaverka我有一些疑问,能否请您解释一下? 1-(MBR20100) 这个 D9 和 D10 二极管的目的是什么? 2- OPTIMER 和 ISENSE 引脚内部如何工作? 应用说明: https://www.nxp.com/docs/en/application-note/AN10868.pdf Re: tl431 regulator resistor 感谢@TomasVaverka的回答。 Re: tl431 regulator resistor 你好,贾斯汀、 对于 24V/3A 输出,反馈分频器(R23 和 R24)将 TL431 参考设置为 2.5V。比例是 因此,如果 R24 = 5.1 kΩ,R23 ≈ 43 kΩ。 R25 和 C17 构成环路稳定性补偿网络的一部分。典型值为 R25 = 1 kΩ-10 kΩ,C17 = 100 nF-470 nF,根据 AN10868 进行调整。 MOSFET 切换整流后的直流总线电压,115 VAC 输入约为 160 V,230 VAC 输入约为 325 V。门驱动器电压为 10—12 V,开关频率约为 66 kHz。 BRs, Tomas
View full article
[i.MX RT1064] SD 卡初始化卡住且未触发信号命令超时 您好! 我目前正在尝试提高配备 MIMXRT1064 CVL5B 处理器的定制板上 SD 卡接口的可靠性。通过使用 SDK 中的 sdmmc 示例,我可以基本运行一切。我可以与卡通信并读写数据。但在极少数情况下,我的应用程序会在初始化 SD 卡时卡住。我将问题归咎于 SD 卡插槽的机械故障导致的杂散卡检测信号。即使插槽中没有卡,固件也会尝试初始化 SD 卡,并一直等待命令完成。这当然是硬件问题,但不应该永久性地阻止我们程序的执行。 我试图在 MIMXRT1064-EVK 评估板上重现这个问题,但它的 SD 卡插槽似乎更坚固一些,不会被空白的微型 SD 卡所欺骗。但是通过使用 25.09 SDK 中的 sdcard_polling 示例并修改 sdmmc_config.c 中的 board_sdcardgetDetectStatus 函数,我得以触发评估板上的问题行为即使没有插入 SD 卡,也会返回 true: bool BOARD_SDCardGetDetectStatus(void) { return true; } 如果没有 SD 卡,初始化过程就会陷入 USDHC_WaitCommandDone 函数的 while 循环: static status_t USDHC_WaitCommandDone(USDHC_Type *base, usdhc_command_t *command, bool pollingCmdDone) { assert(NULL != command); status_t error = kStatus_Success; uint32_t interruptStatus = 0U; /* check if need polling command done or not */ if (pollingCmdDone) { /* Wait command complete or USDHC encounters error. */ while (!(IS_USDHC_FLAG_SET(interruptStatus, kUSDHC_CommandFlag))) { // SD card initialization gets stuck running this loop interruptStatus = USDHC_GetInterruptStatusFlags(base); } if ((interruptStatus & (uint32_t)kUSDHC_CommandErrorFlag) != 0UL) { error = kStatus_Fail; } /* Receive response when command completes successfully. */ if (error == kStatus_Success) { error = USDHC_ReceiveCommandResponse(base, command); } USDHC_ClearInterruptStatusFlags(base, kUSDHC_CommandFlag); } return error; } 下面是完整的堆栈跟踪: USDHC_WaitCommandDone() at fsl_usdhc.c:729 0x7000741a USDHC_TransferBlocking() at fsl_usdhc.c:1.641 0x70007f3e SDMMCHOST_TransferFunction() at fsl_sdmmc_host.c:190 0x7000a960 SD_SendInterfaceCondition() at fsl_sd.c:1.206 0x70004430 SD_ProbeBusVoltage() at fsl_sd.c:1.950 0x70005388 sdcard_init() at fsl_sd.c:2.020 0x7000549a SD_CardInit() at fsl_sd.c:2.107 0x700055ea main() at sdcard_polling.c:174 0x70002bb6 通常情况下,SD 卡会响应命令,导致 USDHC1.INT_STATUS.CC 标志被设置,从而允许程序退出 while 循环。当没有卡时,我希望 USDHC1.INT_STATUS 错误标志(如 CTOE 命令超时错误)被设置,并最终导致 init 函数返回错误。但这种情况从未发生过。我还检查了 USDHC1.INT_STATUS_EN.CTOESEN 是否启用,以及 SD 时钟是否正常工作。 我假设在这种情况下应该触发命令超时是否正确,还是这种行为正确? 有没有其他方法可以确保初始化失败,并且在没有插入 SD 卡时不会卡住?我想避免修改整个 SD 驱动程序,但限制 while 循环中的重试次数是我目前能想到的唯一解决方案。 问候 Jan i.MX RT106x
View full article
i.MX8MMのYoctoのu-boot-imxからDFUを削除する 私たちは Yocto (kirkstone 4.0.4) を使って U-Boot for imx8mm_evk をビルドしています。U-Boot から DFU を完全に削除したいと考えています。 構成フラグメントを使用してU-Bootを構成する方法はわかっていますが、他のオプションではすでに成功しています。しかし、何らかの理由で、この単純な設定フラグメントは機能しません。 CONFIG_DFU=n CONFIG_CMD_DFU=n do_configureログから、フラグメントが使用されていることを確認しました。 CONFIG_DFUの値は、フラグメントremove_dfu.cfgによって再定義されます。 前の値: CONFIG_DFU=y 新しい値: CONFIG_DFU=n CONFIG_CMD_DFUの値は、フラグメント remove_dfu.cfg によって再定義されます。 前の値: # CONFIG_CMD_DFU が設定されていません 新しい値: CONFIG_CMD_DFU=n また、他のフラグメントがこれらの変更を上書きしないことも確認しました。ただし、do_configureが完了すると、最終的な .configureファイルのCONFIG_DFU=y(CONFIG_CMD_DFUはまだオフ)です。何らかの理由で、レシピが「make oldconfig」を実行すると、値が元に戻ります。 なぜ設定は一見DFUを強制的にオンにしたいのですか?私はdo_configure:appendで変更を強制することでそれを削除することができますが、それは非常に厄介なハックであり、私は別の解決策を好むでしょう。 Re:i.MX8MMのYoctoのu-boot-imxからDFUを削除する 私は自分自身の質問に答えます:すべてのKconfigファイルを調べて、CONFIG_EFI_CAPSULE_FIRMWARE_FITとCONFIG_EFI_CAPSULE_FIRMWARE_RAWがDFUを強制的に有効にしていることがわかりました。EFIローダーを無効にしたとき、通常の方法でDFUも無効にすることができました。 Re:i.MX8MMのYoctoのu-boot-imxからDFUを削除する それはうまくいきません。元の投稿で説明したように、何らかの理由で「oe_runmake oldconfig」を実行すると、設定ファイルで無効になっている場合でも「CONFIG_DFU=y」が設定されます。私はその理由を理解しようとしています。
View full article
使用 LS1046A 的定制板上的 U-Boot 无法启动 我目前正在使用 LS1046A 检查定制板上的启动过程。创建PBL和U-Boot并写入QSPI后,输出如下日志,之后便无任何显示: 信息:BL31:准备从 EL3 退出到正常世界 信息:入口点地址 = 0x82000000 信息:SPSR = 0x3c9 由于我手头有 LS1046ARDB,我怀疑挂起是由于硬件配置的差异造成的。在定制板上,USB、SATA、PCIe都没有用到,所以没有连接。 存储库中是否有任何区域位于 https://github.com/nxp-qoriq/atf/tree/lf_v2.6 这可能会影响操作吗?(DDR 运行没有任何问题。) 回复:U-Boot 无法在使用 LS1046A 的定制板上启动 请在 u-boot 源代码中的 arch/arm/cpu/armv8/fsl-layerscape/soc.c 中注释“erratum_a009007()”。 如果没有帮助,请使用 CodeWarrior for ARMv8 调试 BL31 和 u-boot。 可能“检查(附加到运行目标)”会对客户有所帮助。请参阅附件 inspect.png 中标记为红色的检查图标。点击该图标后,CodeWarrior将会附加到目标板上,不会影响目标板上正在运行的软件。 然后目标板正在执行的反汇编代码将被捕获并显示在CodeWarrior IDE中,请参考附件disassemble.png。 然后参考下面的文档来调试BL31和u-boot。 https://community.nxp.com/t5/Layerscape-Knowledge-Base/Debugging-ATF-and-u-boot-with-CodeWarrior-for-ARMv8/ta-p/1684233
View full article
SDK 中的示例应用程序 ethosu_apps 未按预期运行 我正在尝试按照说明(来自第 6.2.7 节)从下载的 SDK 构建 Cortex-M33 固件。 使用 GNU arm 工具链 13.x,我可以编译演示应用程序 ethosu_apps 但是当我运行 uboot 时,我看到 Cortex M33 的 COM/串行端口中有错误日志 ================== 初始化 Arm Ethos-U E:推理期间发生 NPU 错误。(ethosu_driver.c:542) E: NPU 状态=0x00000804,qread=0,cmd_end_reached=0(ethosu_device_u55_u65.c:182) 节点 ethos-u(编号 0)调用失败,状态为 1 E:调用推理失败:job=job(inference_process.cpp:281) 推理状态:失败 ================== 我希望它能按原样工作,有人能帮助我吗? NPU|ML 回复:来自 SDK 的示例应用程序,即 ethosu_apps,未按预期运行 谢谢@Chavira 。 使用提供的补丁,我可以看到 label_image 按预期工作。 回复:来自 SDK 的示例应用程序,即 ethosu_apps,未按预期运行 谢谢@Chavira , 通过建议的更改,我可以看到 ethosu_apps.bin 在从 uboot 启动时似乎按预期工作。 您有机会研究一下我在帖子中提到的问题吗? 回复:来自 SDK 的示例应用程序,即 ethosu_apps,未按预期运行 很高兴看到快速的回应。 恐怕在您的步骤 #3 中,您需要将external_delegate参数传递给label_image 推理在 ETHOSU 上运行,否则推理在 A55 上运行,这就是推理结果在 A55 行中的原因。 (请原谅我将 label_image_release 与 label_image 混淆了,它实际上是 label_image ) 如果您为 label_image 提供外部委托参数,则会在 M33 控制台上看到日志,请参阅第 2.7.2 节 (如果命令不起作用,您可能需要提供 vela 模型——对我来说,它仅适用于 vela 模型) > cd /usr/bin/tensorflow-lite-2.16.2/examples > vela mobilenet_v1_1.0_224_quant.tflite > ./label_image -m output/mobilenet_v1_1.0_224_quant_vela.tflite -i grace_hopper.bmp -l labels.txt --external_delegate_path=/usr/lib/libethosu_delegate.so 对于我来说,使用默认/原始的 ethosu_firmware 上述步骤运行正常(如下), /usr/bin/tensorflow-lite-2.16.2/examples# ./label_image -m output/mobilenet_v1_1.0_224_quant_vela.tflite -i grace_hopper.bmp -l labels.txt -external_delegate_path=/usr/lib/libethosu_delegate.so INFO: Loaded model output/mobilenet_v1_1.0_224_quant_vela.tflite INFO: resolved reporter INFO: before CreateAllDelegates INFO: Ethosu delegate: device_name set to /dev/ethosu0. INFO: Ethosu delegate: cache_file_path set to . INFO: Ethosu delegate: timeout set to 60000000000. INFO: Ethosu delegate: enable_cycle_counter set to 0. INFO: Ethosu delegate: enable_profiling set to 0. INFO: Ethosu delegate: profiling_buffer_size set to 2048. INFO: Ethosu delegate: pmu_event0 set to 0. INFO: Ethosu delegate: pmu_event1 set to 0. INFO: Ethosu delegate: pmu_event2 set to 0. INFO: Ethosu delegate: pmu_event3 set to 0. INFO: EXTERNAL delegate created. INFO: EthosuDelegate: 1 nodes delegated out of 1 nodes with 1 partitions. INFO: Applied EXTERNAL delegate. INFO: settings->number_of_warmup_runs 2 INFO: invoked INFO: average time: 3.762 ms INFO: Predicted label = 907 但是如果我用编译好的版本替换默认的版本,我会看到错误(如下)并且可以在 M33 控制台中看到日志,我的期望是使用编译好的 ethosu_firmware 推断应该会成功 /lib/firmware/# reboot /lib/firmware/# cp ethosu_apps_rpmsg.elf ethosu_firmware /usr/bin/tensorflow-lite-2.16.2/examples# ./label_image -m output/mobilenet_v1_1.0_224_quant_vela.tflite -i grace_hopper.bmp -l labels.txt -external_delegate_path=/usr/lib/libethosu_delegate.so INFO: Loaded model output/mobilenet_v1_1.0_224_quant_vela.tflite INFO: resolved reporter INFO: before CreateAllDelegates INFO: Ethosu delegate: device_name set to /dev/ethosu0. INFO: Ethosu delegate: cache_file_path set to . INFO: Ethosu delegate: timeout set to 60000000000. INFO: Ethosu delegate: enable_cycle_counter set to 0. INFO: Ethosu delegate: enable_profiling set to 0. INFO: Ethosu delegate: profiling_buffer_size set to 2048. INFO: Ethosu delegate: pmu_event0 set to 0. INFO: Ethosu delegate: pmu_event1 set to 0. INFO: Ethosu delegate: pmu_event2 set to 0. INFO: Ethosu delegate: pmu_event3 set to 0. INFO: EXTERNAL delegate created. INFO: EthosuDelegate: 1 nodes delegated out of 1 nodes with 1 partitions. INFO: Applied EXTERNAL delegate. INFO: settings->number_of_warmup_runs 2 ERROR: Ethos_u inference failed ERROR: Node number 1 (EthosuDelegate) failed to invoke. ERROR: Failed to invoke tflite *** 在这两种情况下,我都能在 M33 COM 端口上看到预期的日志 2. 我对使用“remoteproc0”从 Linux 即运行 M33 可执行文件的观察与您的完全相同。 3. 推理运行器是在 ethosu 上运行推理的不同示例。此示例似乎适用于步骤 1 中的两个固件 #cd /usr/bin/ethosu/examples #./inference_runner -d /dev/ethosu0 -n output/mobilenet_v1_1.0_224_quant_vela.tflite -i grace_hopper.bmp -l labels.txt -o output_data_detection -t 1080000000 回复:来自 SDK 的示例应用程序,即 ethosu_apps,未按预期运行 Chavira,感谢您的确认。在ethosu_apps上 ethosu_apps_rpmsg 需要做一点说明,您这边可以确认一下吗? 我做了什么? 1. 使用 2.16 sdk 构建 ethosu_apps_rpmsg 应用程序 2. 启动 Linux,将 ethosu_firmware 替换为 #1 的 elf 3. 在 Linux 上对 ethosu 运行默认推理测试 ./label_image_release -m 输出/mobilenet_v1_1.0_224_quant_vela.tflite -i grace_hopper.bmp -l lab 信息:已加载模型输出/mobilenet_v1_1.0_224_quant_vela.tflite 信息:已解决的报告者 信息:在 CreateAllDelegates 之前 信息:Ethosu 委托:设备名称设置为 /dev/ethosu0。 信息:Ethosu 代表:cache_file_path 设置为 。 信息:Ethosu 代表:超时设置为 60000000000。 信息:Ethosu 代表:enable_cycle_counter 设置为 0。 信息:Ethosu 代表:enable_profiling 设置为 0。 信息:Ethosu 代表:profiling_buffer_size 设置为 2048。 信息:Ethosu 代表:pmu_event0 设置为 0。 信息:Ethosu 代表:pmu_event1 设置为 0。 信息:Ethosu 代表:pmu_event2 设置为 0。 信息:Ethosu 代表:pmu_event3 设置为 0。 信息:已创建外部代表。 信息:EthosuDelegate:1 个节点中有 1 个分区,已委托 1 个节点。 信息:已应用外部代表。 信息:设置->预热运行次数 2 错误:Ethos_u 推理失败 错误:节点 1(EthosuDelegate)调用失败。 错误:无法调用 tflite! 4. 观察 M33 com-port 中的日志 与默认的 ethosu_firmware 可执行文件相比,我可以看到日志是相同的 附言: 而 inference_runner 命令与我的 ethosu_firmware 配合良好 ./inference_runner-d /dev/ethosu0 -n 输出/mobilenet_v1_1.0_224_quant_vela.tflite -i grace_hopper.bmp -l 标签.txt -o 输出数据检测 -t 1080000000 回复:来自 SDK 的示例应用程序,即 ethosu_apps,未按预期运行 谢谢您的回复。 我正在使用 imx93_evk 的 sdk(不是 imx93_qsb),我不确定它是否有任何区别。 >tftp 0x80000000 ethosu_apps.bin >cp.b 0x80000000 0x201e0000 0x20000 >bootaux 0x1ffe0000 0 我是否在 uboot 中设置了任何环境变量?如果我遗漏了任何步骤,请告诉我。 附言: SDK 中的 ethosu_apps_rpmsg 应用程序行为异常,类似于 ethosu_firmware
View full article