Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
在 imx8MP 上安全启动 我已经生成了密钥并在 iMX8M plus 板上进行了熔丝,但我现在无法使用签名图像刷新板。超级根密钥熔丝表正在闪入板。 Re: Secure boot on iMX8MP 是的,我已经遵循了恩智浦半导体提供的安卓网络安全用户指南,而且我已经在板上融合了超级根密钥熔丝表。我正在开发 Android14 电路板支持包。 1.在 uuu_defconfig 中设置 CONFIG_IMX_HAB=y。 2.生成密钥(超级根密钥和证书颁发机构密钥) 3.从超级根密钥表中生成了熔丝。 4。在板上闪过桌子。 Re: Secure boot on iMX8MP 你好, 你关注了 i.MX 安卓网络安全用户指南吗? 你能分享一下你所遵循的步骤吗? 另外,你正在使用哪个安卓版本? 最诚挚的问候/致敬,Ald o。 Re: Secure boot on iMX8MP 您好, ,您所遵循的步骤看起来是正确的,但我现在无法完全理解这里的问题,您在哪里能够闪存并测试是否有任何 hab 事件? 设备处于关闭状态吗? 此外,在尝试闪存时,您是否在 UUU 或 uboot 日志中看到任何内容? 最崇高的敬意/Saludos, Aldo。 Re: Secure boot on iMX8MP 我在两个文件 imx8mp_iwg40m_4gb_android_uuu_defconfig 和 imx8mp_iwg40m_4gb_android_defconfig 中设置了 CONFIG_IMX_HAB=y。启用 HAB 功能的文件是否正确?我正在为 4GB 的 imx8M Plus 板构建。 Re: Secure boot on iMX8MP 您好, ,确实有问题,因为您有许多 HAB 事件,特别是HAB_INV_SIGNATURE,这意味着您的引导加载程序中的签名不正确,因此请确保您使用的是正确的签名。 ,致以最崇高的敬意/Saludos, Aldo。 Re: Secure boot on iMX8MP 你好 刷新 i.mx8M Plus 的板后,hab_status 显示如下: iWave-G40>hab_status 安全启动已禁用 HAB配置:0xf0,HAB状态:0x66 --------- HAB 事件 1 ----------------- 事件数据: 0xdb 0x00 0x1c 0x45 0x33 0x18 0xc0 0x00 0xca 0x00 0x14 0x00 0x02 0xc5 0x1d 0x00 0x00 0x00 0x0d 0x3c 0x40 0x1f 0xad 0xc0 0x00 0x00 0x30 0x20 STS = HAB_FAILURE (0x33) RSN = HAB_INV_SIGNATURE (0x18) CTX = HAB_CTX_COMMAND (0xC0) ENG = HAB_ENG_ANY (0x00) --------- HAB 事件 2 ----------------- 事件数据: 0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00 0x00 0x00 0x00 0x40 0x1f 0xdd 0xc0 0x00 0x00 0x00 0x20 STS = HAB_FAILURE (0x33) RSN = HAB_INV_ASSERTION (0x0C) CTX = HAB_CTX_ASSERT (0xA0) ENG = HAB_ENG_ANY (0x00) --------- HAB 事件 3 ----------------- 事件数据: 0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00 0x00 0x00 0x00 0x40 0x1f 0xbd 0xc0 0x00 0x00 0x00 0x00 0x20 STS = HAB_FAILURE (0x33) RSN = HAB_INV_ASSERTION (0x0C) CTX = HAB_CTX_ASSERT (0xA0) ENG = HAB_ENG_ANY (0x00) --------- HAB 事件 4 ----------------- 事件数据: 0xdb 0x00 0x1c 0x45 0x33 0x18 0xc0 0x00 0xca 0x00 0x14 0x00 0x02 0xc5 0x1d 0x00 0x00 0x00 0x0d 0x3c 0x40 0x1f 0xad 0xc0 0x00 0x00 0x30 0x20 STS = HAB_FAILURE (0x33) RSN = HAB_INV_SIGNATURE (0x18) CTX = HAB_CTX_COMMAND (0xC0) ENG = HAB_ENG_ANY (0x00) --------- HAB 事件 5 ----------------- 事件数据: 0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00 0x00 0x00 0x00 0x40 0x1f 0xad 0xc0 0x00 0x00 0x00 0x04 STS = HAB_FAILURE (0x33) RSN = HAB_INV_ASSERTION (0x0C) CTX = HAB_CTX_ASSERT (0xA0) ENG = HAB_ENG_ANY (0x00) --------- HAB 事件 6 ----------------- 事件数据: 0xdb 0x00 0x34 0x45 0x33 0x18 0xc0 0x00 0xca 0x00 0x2c 0x00 0x02 0xc5 0x1d 0x00 0x00 0x00 0x0d 0x54 0x40 0x1f 0xad 0xc0 0x00 0x000x10 0x20 0x40 0x20 0x00 0x00 0x00 0x13 0xe0 0x10 0x40 0x33 0xe0 0x10 0x00 0x01 0x01 0x30 0x00 0x97 0x00 0x00 0x00 0x00 0xaa 0x70 STS = HAB_FAILURE (0x33) RSN = HAB_INV_SIGNATURE (0x18) CTX = HAB_CTX_COMMAND (0xC0) ENG = HAB_ENG_ANY (0x00) --------- HAB 事件 7 ----------------- 事件数据: 0xdb 0x00 0x34 0x45 0x33 0x18 0xc0 0x00 0xca 0x00 0x2c 0x00 0x02 0xc5 0x1d 0x00 0x00 0x00 0x0d 0x54 0x40 0x1f 0xad 0xc0 0x00 0x000x10 0x20 0x40 0x20 0x00 0x00 0x00 0x13 0xe0 0x10 0x40 0x33 0xe0 0x10 0x00 0x01 0x01 0x30 0x00 0x97 0x00 0x00 0x00 0x00 0xaa 0x70 STS = HAB_FAILURE (0x33) RSN = HAB_INV_SIGNATURE (0x18) CTX = HAB_CTX_COMMAND (0xC0) ENG = HAB_ENG_ANY (0x00) --------- HAB 事件 8 ----------------- 事件数据: 0xdb 0x00 0x14 0x45 0x33 0x0c 0xa0 0x00 0x00 0x00 0x00 0x40 0x1f 0xad 0xc0 0x00 0x00 0x00 0x04 STS = HAB_FAILURE (0x33) RSN = HAB_INV_ASSERTION (0x0C) CTX = HAB_CTX_ASSERT (0xA0) ENG = HAB_ENG_ANY (0x00) 我已正确执行所有步骤,能否请您检查一下? 此致, 苏亚希米 Re: Secure boot on iMX8MP 您好, 是的,配置标志是正确的(CONFIG_IMX_HAB),遗憾的是,我不能对您使用的 defconfig 做太多评论,因为这不是恩智浦的 EVK。 最诚挚的问候/Saludos, Aldo.
View full article
TDA8035 运行模式下的 IDD (INTF) 电流消耗 大家好,团队, 当 TDA8035 处于运行模式时,VDD (INTF) = 3.3 V 时 VDD (INTF) 的近似功耗是多少? 顺祝商祺! 西尔万 Re: TDA8035 IDD(INTF) current consumption in active mode 你好@sylvainbouriot TDA8035 的大电流通路(板卡电源、VCC 限流、DC/DC)均位于 VDDP 中,与 VDD (INTF) 无关。 VDD (INTF) 主要负责数字控制逻辑、I/O 参考和时钟分频控制。其功耗非常低。 运行模式下的 IDD (INTF) 通常在 1 到 3 mA(典型值)的范围内。
View full article
Field oriented control : ADC sample delay Hello, I work on the example design MBDT AN13902. This motor algorithm works at 10kHz, so ADC and PWM are synchronous. The AN13767 is the same SW without MBDT. And in this application note, we can see the ADC samples are processed directly during the ""FOC calculation". So, during the same 100µs time.   I added a comparator on the same ADC input to trig a GPIO when the signal is above its middle value. And see a delay of 224µs between the theoretical trigger (the physical signal) and the output GPIO signal, so more than 2 loop times. (We know a GPIO can rise and fall multiple times in the same 100µs, so its rise time is almost negligible) This time is the minimal time achievable, because the input ADC signal is not synchronous to the ADC, the real delay varies from 224µs to 324µs. But keep in mind 224µs is the real delay. Do you know a reason which could explain this ? Best regards Jérémy Re: Field oriented control : ADC sample delay Hi, from the description I am not fully sure how your measurement is done, which signals are used. According AN13767 and its project setting, The BCTU list contains 4 items, 2 parallel conversions are done on ADC0/ADC1. This is triggered by eMIOS0 ch4 flag, at falling edge of ch4 output signal. The Bctu_FIFO1_WatermarkNotification is called after those 4 conversions are done and result stored onto FIFO1. So you can add some GPIO setting/toggling into this notification and measure this with respect of eMIOS0 ch4 output. This should be within 100us period and notification delay much less. BR, Petr
View full article
MCUXpresso IDE v11.2.0 [Build 4120] [2020-07-09] Hi, I am using "MCUXpresso IDE v11.2.0 [Build 4120] [2020-07-09]" on FRDM-K66. I found some warning errors today when I compile my project. But, it works fine before, and never got these kind of warnings. Actually, there are no warning error after compiling finished. See attached document... Can anyone tell me how to remove these kind warnings? Thanks, Christie Re: MCUXpresso IDE v11.2.0 [Build 4120] [2020-07-09] Hi Celeste, I tried to clear and re-build and didn't work. Then, I tried to delete these definitions and compiled, and it worked. I added these definitions back and re-complied, and it worked as well... I do not know why it works in this way? Thanks, Christie Re: MCUXpresso IDE v11.2.0 [Build 4120] [2020-07-09] Hello @a8Chcx , Thanks for reaching out. The warnings you are seeing are typically caused by an IDE indexer or cache issue rather than a real build problem, especially if the project still compiles with zero warnings. We recommend cleaning the workspace and rebuilding the index (Project → Clean, then right‑click project → Index → Rebuild). If the issue persists, please share the exact warning text so we can investigate further. Best regards, Celeste Re: MCUXpresso IDE v11.2.0 [Build 4120] [2020-07-09] Hi Christie, Have these definitions actually been used in your project? Could you please share a screenshot of the exact warning messages you are seeing? Additionally, you may try creating a new workspace and re-importing your project into it. Sometimes this helps resolve issues caused by corrupted IDE caches. BR Celeste
View full article
使用 S32 Design Studio 和 EB Tresos Studio 对 S32Z/E 进行编译和调试 本指南介绍在 S32Z/E 平台上运行示例项目的基本步骤。它侧重于帮助开发人员使用 S32设计工作室和 EB Tres os Studio 设置环境、安装所需工具以及使用示例应用程序。该文档为创建项目、生成代码、编译和调试提供了清晰的说明,使其成为工程师探索在 S32Z/E 设备上进行实时软件开发的绝佳起点。
View full article
Enable 3.3 V and 5 V Regulators for Expansion Header on i.MX9 boards This patch series enables the external 3.3 V and 5 V power rails used by the Raspberry Pi expansion connector on the i.MX93-QSB, i.MX93-FRDM, and i.MX91-FRDM boards. These regulators were already defined in the device tree but left disabled by default. By activating them, the RPI-compatible expansion header can properly power external modules, HATs, and add‑on boards. Changes by board: i.MX93-QSB Enables the 3.3 V and 5 V external supply lines used by the RPI connector. i.MX93-FRDM Enables the 3.3 V and 5 V external supply lines used by the RPI connector. i.MX91-FRDM Enables the 3.3 V and 5 V external supply lines used by the RPI connector. Purpose: Provide proper power to the Raspberry Pi compatible expansion port. Improve hardware compatibility for users attaching external HATs or modules. Align all i.MX9 reference boards to use a consistent power‑tree configuration for the RPI connector.
View full article
如何在 CanIf User RxIndication 回调中获取 CAN ID? 你好,我使用的是带有 SW32K1_S32M24x_RTD_R21-11_3.0.0 的 S32K144,并已将 CanIf 配置为使用自定义回调函数。 我的配置: CanIfRxPduUserRxIndicationName 设置为"Service_CanIf_RxIndication" 当收到 CAN 消息时,CanIf_RxIndication() 将调用该回调。 问题 我注意到在 CanIf_RxIndication() 中,CAN ID 可通过 Mailbox->CanId 参数获得。但是,在我的 Service_CanIf_RxIndication() 回调中,我只能接收到 PduId,而无法检索到实际的 CAN ID。此外,我还注意到 CanIf.h 标题状态:" 短截线版本-此文件仅包含示例代码。" 我的问题 1.我能修改或替换 CanIf.c 吗?短截线代码? 自 CanIf.h 起 明确表示它是 " 短截线 版本 " 和 " 示例代码 ",修改 Canif.c 以将 CAN ID 传递给用户回调是否可以接受? 2。修改短截线代码会违反 AUTOSAR 架构吗? 如果我自定义 CanIF 短截线实现,这是否会破坏 AUTOSAR 合规性或导致任何兼容性问题? 3.是否有其他解决方案? 有没有推荐的方法可以在不修改CanIF源代码的情况下将CAN ID传递给上层回调? 环境 MCU: S32K144 RTD 版本:SW32K1_S32M24x_RTD_R21-11_3.0.0 集成开发环境S32 Design Studio 3.6 感谢您的帮助! Re: How to get CAN ID in CanIf User RxIndication callback? 你好,@Soratari、 Q1。是的,短截线模块是用来编辑/替换的。由于 Canif 模块是一个短截线,它只提供了 CAN 驱动程序所需的头文件,例如 CANIF_CBK.H。 Q2. 不,只要您遵守指南,不更改标准化函数名、变量等,就不会违反 ASR 架构。 Q3。通常,短截线模块用于测试目的。您应该使用第三方供应商(如 Elektrobit (EB)、Vector 等)提供的 CanIf、EthIf& LinIf。不过,出于调试目的,可以自行修改。 致以最诚挚的问候, Julián
View full article
S32K312 FlexCANメールボックスとCANチャンネルの対応 こんにちは。S32K312 が 3 つの CAN チャネルで構成され、CAN0 が Legacy RxFiFO で有効になっており、メールボックスの数が 32 に設定され、フィルター テーブルの数が 8 に設定されています。CAN1 は受信に標準のメールボックスを使用し、メールボックスの数は 32 に設定されています。 1. CAN1 はメールボックス 18 を使用して正常にメールを受信できますか? 現在、メールボックス 18 を使用してメールを受信できますが、各 CAN が具体的にどのようにメールボックスを占有するのかがよく分かりません。 2. CAN1 を受信用に RxFiFO に切り替えた場合、CAN1 の FIFO メールアドレスは 32 から始まる 8 つのメールアドレスのいずれかになりますか? ありがたい。 S32K3 S32K31XEVB-Q100 S32K312EVB-Q172 Re: S32K312关于FlexCAN的邮箱和CAN通道的对应 こんにちは@Florence100733さん、 両方の質問を完全に理解できたかどうかわかりませんので、誤解があればご指摘ください。 1.can1の受信メールボックスを18で正常に受信できるかどうか、現状18で受信はできるのですが、各canがどのようにメールボックスを占有しているかがよく分かりません。 はい、正常に受信できます。CAN0 の RxFIFO の使用は CAN1 からのメールボックスを消費しません。各 CAN インスタンス (FlexCAN0、FlexCAN1、…) には、独立した MB スペースと RAM があります。メッセージバッファは、アドレスオフセット0080hから始まるFlexCAN組み込みRAMにマッピングされます。73.6.5章「FlexCANメッセージバッファのメモリマップ」を参照してください。 2. can1 が受信のために RxFiFO にスイッチする場合、can1 の fifo メールボックスは 32 から始まる 8 つのメールボックスですか? レガシー RxFiFO について言及していると思います。いいえ、受信は常にMB0から開始されます。73.6.6 章「レガシー RX FIFO 構造」を参照してください。「MCR[RFEN] = 1 の場合、メモリ領域 80h~DCh (通常は MB 0~5 によって占有されます) は受信レガシー FIFO エンジンによって使用されます。」 レガシー FIFO は 6 つのメッセージまで格納できることに留意してください。 よろしくお願いします、 ジュリアン
View full article
「S32ZE_R52_NXP_RTOS_4_7_181_RTM_1_1_0_D2412_DesignStudio_updatesite.zip」のインストール方法 こんにちは、 GreenVIPから「S32ZE_R52_NXP_RTOS_4_7_181_RTM_1_1_0_D2412_DesignStudio_updatesite」をインストールしましたが、次のスクリーンショットでは見つかりませんでした。 再度インストールしたらエラーヒントが出ました。 私を助けてください。 ご回答をお待ちしています。 Re: How to install "S32ZE_R52_NXP_RTOS_4_7_181_RTM_1_1_0_D2412_DesignStudio_updatesite.zip" こんにちは、 Lvyang508さん ご返信よろしくお願いします。 SW32ZE_RTD_R21-11_2.0.1_D2505_をインストールしましたか? S32DS IDE に DesignStudio_updatesite.zip がありますか? BR ジョーイ Re: How to install "S32ZE_R52_NXP_RTOS_4_7_181_RTM_1_1_0_D2412_DesignStudio_updatesite.zip" S32DS IDE: プラットフォーム 3.6.5 用 S32DS UG_S32ZE_GreenVIP.pdfに従って対応するパッケージをダウンロードし、インストールしました。 Re: How to install "S32ZE_R52_NXP_RTOS_4_7_181_RTM_1_1_0_D2412_DesignStudio_updatesite.zip" こんにちは、 Lvyang508さん RTD のバージョンを確認してください。RTD と RTOS パッケージの間に競合があるようです。 また、使用している S32DS IDE のバージョンは何ですか? BR ジョーイ Re: How to install "S32ZE_R52_NXP_RTOS_4_7_181_RTM_1_1_0_D2412_DesignStudio_updatesite.zip&&&& こんにちは、ジョーイ。 SW32ZE_RTD_R21-11_2.0.1_D2505_をインストールしました S32DS IDE の DesignStudio_updatesite.zip。 よろしくお願いします! Re: How to install "S32ZE_R52_NXP_RTOS_4_7_181_RTM_1_1_0_D2412_DesignStudio_updatesite.zip&&&& こんにちは、 Lvyang508 ご返信よろしくお願いします。 この問題はバージョンの競合によって発生している可能性があります。UG_S32ZE_GreenVIP.pdf を参照して、S32DS IDE 3.6.1 を使用してください。 BR ジョーイ Re: How to install "S32ZE_R52_NXP_RTOS_4_7_181_RTM_1_1_0_D2412_DesignStudio_updatesite.zip&&&& こんにちは、ジョーイ。    ご返信ありがとうございます。 S32IDE 3.6.1をインストールしました。しかし、問題はまだ残っています。 BR、
View full article
iMX93 FRDM 上的 DMS 嗨,团队、 是否有人在 i.MX93 FRDM 平台上实施或评估过驾驶员监控系统 (DMS) 演示? 我正在寻找与以下功能相关的详细信息或引用: 人脸侦测 人脸地标检测 虹膜/眼睛地标检测 驾驶员行为检测,如吸烟和使用手机 如果有任何演示、参考设计、SDK 示例或合作伙伴解决方案,请分享详细信息或相关文档。 提前感谢您的支持。 致以最诚挚的问候, Ajnas FRDM 培训 Re: DMS on iMX93 FRDM 你好@ajnas-c、 感谢您联系恩智浦支持中心! 您可以通过下面的链接查看该演示的详细信息和源代码: https://github.com/nxp-imx-support/nxp-demo-experience-demos-list/tree/lf-6.12.3_1.0.0/scripts/machine_learning/dms 此致 查维拉
View full article
S32K324のBISTデバッグに関する質問 こんにちはチーム BIST デバッグガイダンスについてお聞きしてもよろしいでしょうか? お客様は RTD (MCAL) 付きの S32K324 を使用しています。 BIST_RUN API の実行後、MCU はリセットされたように見えます。(もちろん、UM に続く BIST では PLL による正しいクロックが使用されます。) ただし、MC_RGM には「STCU_URF」と表示されています。 STCUに確認しましたが、重大な理由はわかりませんでした。 これらは「まだ進行中で、MBIST 実行に失敗しました」のように表示されますが、これらもデフォルト値です。 このCASEに関して、より詳しい情報を入手できるのはどちらでしょうか? よろしくお願いします。 優先度: 重要 SAFETY_SW 出典: 直接お客様 Re: Question about BIST debugging of S32K324 こんにちは@Luke_Chun 、 MBSPLLEN / LBSWPLLEN が「0」であれば正しく、これは検証済みの構成 STCU2 セットアップの一部です。 設定の場合、関数のパラメータが何であるかを意味します。例: Bist_Run ( BIST_SAFETYBOOT_CFG ); 構成から、お客様が LBIST および MBIST 回復不能障害対応を設定したことがわかります。これが、表示されるリセットの原因です。 これらのタブに何も設定されていないことを確認してください。 この設定後、BIST は終了し、リセット後に結果を調べることができます。 おそらく、MBIST または LBIST で何らかの障害が発生し、これが前提条件が間違っている (おそらく一部のクロックが実行されていない) という手がかりになります。 よろしくお願いいたします ラドスラフ   Re: Question about BIST debugging of S32K324 こんにちは@RadoslavB ご返信ありがとうございます。 BIST に関するフィードバックは次のとおりです。 以下の行ではブレークポイントが使用されました。 以下はSTCUレジスタです。 1つの質問は、RUNSW: MBSPLLEN/LBSWPLLENが「0」であることです。 「PLLなし」を意味します。正しい構成ですか? また、以下の STCU に異常な構成はありましたか? よろしくお願いします。 Re: Question about BIST debugging of S32K324 こんにちは@Luke_Chun 、 破壊的リセット STCU2 レジスタがデフォルトに設定されると、レジスタから根本原因に関する詳細情報を見つけることはできません。 どの BIST 構成を実行しているかを把握し、BIST を開始する関数Bist_SelfTestTrigger()の命令の直前に STCU2 レジスタを確認すると便利です。 SAFETYBASE_REG_WRITE32 ( BIST_STCU_RUNSW_REG 、 BIST_STCU_RUNSW_RUN_BIT ); LBUFM と MBUFM が設定されていない場合、それにもかかわらず STCU_URF が設定される可能性があるのはなぜなのか、HW チームに質問することになります。 理想的には、クロックの初期化直後に BIST を実行し (クロックを起動して実行するだけ、他には何も行わない)、他のペリフェラルは初期化せず、Core_1 をリセット状態に保ち、FCCU を有効にせず、MPU と XRDC を無効のままにし、すべてのウォッチドッグを無効のままにして、PMIC をデバッグ モードのままにして、LBIST_CLK が 40 MHz であることを確認します。 比較のために、K344 の SAF デモ例で、MCU モジュール (クロックと McuModeSettingConf) がどのように構成されているかを確認できます。 敬具、 ラドスラフ Re: Question about BIST debugging of S32K324 こんにちは@RadoslavB ご対応ありがとうございます。 あなたの言及によって私はもう一歩前進することができます。 以下を使用すると、STCU_URF は発生しません。 しかし、別の結果が表示されています。 RMG が更新されませんでした (以下によりリセットが発生していないと思います)。 また、ERR_STAT には WDTOSW が表示されており、RFSF が発生しています。 両方のエラーが発生する可能性についてお尋ねしてもよろしいでしょうか? (WDTOSW はクロック構成に関連しているのではないかと推測しています...もう一度確認してみます...) しかし、RFSF についての情報はありませんでした...) ありがとう。 Re: Question about BIST debugging of S32K324 こんにちは@Luke_Chun SAF リリースバージョンとは何ですか? BIST 実行前にブレークポイントが表示され、同じポイントで STCU2 レジスタのスクリーンショットが取得されていますか?BIST 実行前であっても ERR_STAT が設定される理由がわかりません。 RFSR - eMcem 構成でこの FCCU 障害が無効になっていることを確認してください BIST は eMcem_Init の前に実行する必要があるため、理想的には、すべての NCF チャネルに対して FCCU を完全に無効にする必要があります。SAF デモの例をご覧ください。 WDTOSW - はい、BIST がタイムアウト内に実行されなかったようです。そのため、いくつかの低速クロックが設定されている、またはいくつかの必須クロックが無効になっています - SAF デモからの MCU クロック セットを参照してください。 敬具、 ラドスラフ Re: Question about BIST debugging of S32K324 こんにちは@Luke_Chun 、 1) クロック (このCASEは分周器) を有効にすることは最低限必要ですが、BIST では最大可能周波数 (最大周波数のクロック ソース PLL) で構成する必要があります。デフォルトの FIRC ではなく、すべての MUX 除数または乗数は、最大出力クロック周波数を提供するように設定されます。など) => これにより、BIST タイムアウトが超過しないようにすることができます。 正確に確認するには、RTD MCU プラグインを使用することをお勧めします。レジスタを探索するのではなく、周波数を出力します。 2) FCCU が無効になっていることがわかります (リセット後のデフォルト状態)。NCF5 に NCF_S0 が設定されているのは、NXP が FCCU をこのように設計しているためです。チャネルを有効にする必要はありませんが、FCCU チャネルを有効にしているにもかかわらず、ステータス フラグは常に設定されます。 NCF5 には DCMROD レジスタによって記述される他の多くの障害があり、これによって NCF5 の正確な障害原因がわかりますが、この場合は STCU2 RF (これは DCMROD5 に報告されます) であると仮定します。 NCF5 が表示されるということは、BIST エラーがまだあることを意味します。 - お客様が eMcem を使用しない場合、FCCU をどのように構成しますか?無効になっているようですが、BIST を実行する意味は何でしょうか? BIST は、ほとんどの場合 FCCU に報告される HW セーフティメカニズムの潜在的な障害をチェックするだけです。したがって、FCCU を無効にして BIST を実行すると、お客様アプリケーションは QM レベルに降格され、セーフティ ASIL アプリケーションを実行できなくなります。 BIST 後には ST_DONE 機能リセットが必要です。BIST リセット後、お客様はBist_GetFailLists() を呼び出して BIST 結果を評価する必要がありますが、結果はどうなりますか? BIST ドライバーの使用方法については、SAF デモの例を参照してください。 Bist_Run() は NCF5 ステータス フラグをクリアできません。実際、これがフラグが設定されている理由です。 敬具、 ラドスラフ Re: Question about BIST debugging of S32K324 こんにちは@RadoslavB ご対応ありがとうございます。 皆様のサポートにより、BIST は機能しています。 しかし、いくつか質問があります。 1. 最後の理由はクロックの設定に関連しています。 MUX7、8、9、10 はクロックの有効化を行いませんでした。 有効にした後は正常に動作します。 これは近づいていますか? 2. FCCU については、おっしゃるとおり FCCU に確認いたしました。 ご覧のとおり、NCF_s0_5 が設定されています... ただし、お客様は eMECM を使用していません (emecm_init を呼び出していません)。 上記はMCUリセット後の状態です。 ただし、BIST_RUN API 中はクリアされます... これは機能していますか? ありがとう。 Re: Question about BIST debugging of S32K324 こんにちは@RadoslavB フィードバックはこちらです。 1. お客様はSPD1.0.5を使用します。SAF が使用されます。 FCCU は実装されますが、この段階では BIST が最初の項目です。 2. はい、Clock は以下のように使用されます。 3. BIST後、STCUおよびFCCUに障害情報は発生しませんでした。 4. 異常の 1 つは、リセット理由がなく、BIST_BUSY であることです。 BIST_BUSY の場合の確認方法を教えてください。 ありがとう。 Re: Question about BIST debugging of S32K324 こんにちは@Luke_Chun 、 Bist_GetExecStatus が BIST_BUSY を返す場合、このビットが設定されている(BIST 操作がまだ完了していない)ことを意味します。 しかし、スクリーンショットを見るとこのビットは 0 なので、なぜ BIST_BUSY が返されるのか分かりません。 Bist_Specific_GetExecStatus() をデバッグしてみると、次のようになります: uint32 ReadRunSw = SAFETYBASE_REG_READ32 ( BIST_STCU_RUNSW_REG ); MBIST11 も実行されていることがわかります。これは、顧客アプリケーションでは使用すべきではない BIST_DIAGNOSTIC_CFG を実行していることを意味します。BIST_SAFETYBOOT_CFG を実行させてください。 クロック設定の一部しかカバーしていないスニペットから**bleep**設定を検証できません。お客様はクロックのMCUプラグイン設定を比較する必要がありますが、私の能力ではここではサポートできません。繰り返しますが、すべてのクロックを最大周波数で有効にするだけで済みます。 敬具、 ラドスラフ
View full article
オンラインカスタマーサービスWeChat: xins4698 Marlboro社のゲームアカウントのパスワードを忘れましたか? オンラインカスタマーサービスWeChat: xins4698 Marlboro社のゲームアカウントのパスワードを忘れましたか? LPCマーケティング LPC51Uxx LPC546xx LPC54xxx LPC55xx LPC800
View full article
FlexCAN3FD fSYS (CHI) vs. fCANCLK (PE) clarification Hello everyone, I'm seeking some clarification regarding the peripheral and the oscillator clock frequencies fed to the canFD module. Is my understanding correct that the peripheral clock is the CAN_CLK_ROOT in CMM that can be muxed and divided to have different frequencies, while the oscillator clock is the static 24MHz clock from the crystal oscillator? If so, does that mean that the duration of 1 time quanta is fixed to 41.67 ns which is what goes into the bit timing calculations? This doesn't seem right to me so I'd appreciate it if anyone can correct my confusion. I see that some of the equations in the RM involve both of these clocks. Thank you, Lam  i.MXRT 106x Re: FlexCAN3FD fSYS (CHI) vs. fCANCLK (PE) clarification Hi again @mayliu1 , so if fSYS is the system clock frequency, would it be AHB_CLK_ROOT, which is 420Mhz in my case? if so, is it involved in the calculation of the time quanta? I don't suppose so but the language, particularly the use of the words oscillator and peripheral, is a little bit confusing to me. I initially did think that the time quanta was directly derived from just the flexCAN clock. Best Regards, Lam Re: FlexCAN3FD fSYS (CHI) vs. fCANCLK (PE) clarification Hi @LamK , Thank you so much for your interest in our products and for using our community. In IMXRT1060RM, it describe as below shown. fCANCLK is the Protocol Engine (PE) Clock , it can be configured via CAN_CLK_ROOT. fSYS is the frequency of operation of the system clock. Also, the duration TQ is not  fixed to 41.67 ns, it  involve both the CAN engine clock and the  PRESDIV parameter.    For more detail information about Clock, I suggest you can check Clocks in  Config Tools . Best Regards MayLiu Re: FlexCAN3FD fSYS (CHI) vs. fCANCLK (PE) clarification Hi @LamK , Thanks for your updated information. Regarding your question: so if fSYS is the system clock frequency, would it be AHB_CLK_ROOT, which is 420Mhz in my case? I do not think so. Please check the IMXRT1060RM. Best Regards MayLiu Re: FlexCAN3FD fSYS (CHI) vs. fCANCLK (PE) clarification Ok thank you @mayliu1, I could have found that information about the clocks in the Clock Consumers tab, looks pretty useful. Ultimately I was concerned that the fSYS could be involved in the calculation of time quanta when I saw the equation NumClkBit which made me equate peripheral clocks with time quanta, which wasn't the case and was where my confusion come from. Thank you for your help again. Best Regards, Lam Re: FlexCAN3FD fSYS (CHI) vs. fCANCLK (PE) clarification You are welcome.
View full article
HSE 数据仅在多次软复位后才会反映在内存中 遵循的步骤: 1.向 Cyclone 图像创建者 2 提供 HSE ELF 文件(包含在 HSE 存储位置编程的 HSE 数据字节)。创建 Cyclone .sap文件以启用 HSE 并对其进行编程。 3.闪存 .sap使用 Cyclone 调试器通过 JTAG 在 S32K312 板上进行文件。 4。重启电源。 5。加载工作空间并验证内存中的 HSE 数据。 6。通过调试器执行多次软复位。 观察到的行为: - 初始电源循环后,HSE 数据不会立即反映在内存中。 • 只有在多次软复位后,HSE 数据才会在内存中可见。(问题) • 还尝试过延迟地允许,行为还是相同 的问题: • 为什么 HSE 数据需要多次软复位才能在内存中反映出来? • 是否有推荐的解决方法(例如,RESET序列或配置更改)? Re: HSE data reflected in memory only after multiple soft resets 你好@abdul_rahiman_csg 首先,你能否解释一下 " 提供 HSE ELF 文件(包含在 HSE 存储位置编程的 HSE 数据字节)" 是什么意思? 安装 HSE 固件后,只有 HSE 才有权访问 HSE 安全存储器(HSE 固件、HSE 数据)。安全内存从内存映射中删除,用户根本无法访问。 此致, Lukas Re: HSE data reflected in memory only after multiple soft resets 该 ELF 包含在 0x004D2000-0x004D2060 和 0x1B000000-0x1B000360 地址范围内编程的 HSE 数据。 Re: HSE data reflected in memory only after multiple soft resets 你好@abdul_rahiman_csg 从微控制器的角度来看,这是没有意义的。这似乎与工具有关。您能否尝试直接与 Pemicro 讨论此事? https://www.pemicro.com/support/index.cfm 此致, Lukas
View full article
RW612 - WiFi 信道状态信息(CSI) 我目前正试图从 FRDM-RW612 中提取 CSI 数据。我假设我缺少导致 CSI 回调无法运行的关键元器件,因为错误配置参数确实会导致固件宣布错误,例如频道配置不正确等。不幸的是,我仍然无法获得 CSI 的任何回调。 如有任何帮助,我们将不胜感激! Re: RW612 - WiFi Channel State Information (CSI) 亲爱的@rb_ots、 我们为客户提供了《渠道状态信息 (CSI) 应用笔记》。(AN14281) 该应用程序可指导您逐步在 FRDM-RW612 上进行 CSI 测试。 您可以通过链接访问 AN,这是一份在线文件。 https://docs.nxp.com/bundle/AN14281/page/topics/about_this_document.html 请试试看 此致, 卫东 Re: RW612 - WiFi Channel State Information (CSI) 是的!这正是我要找的东西,帮了我大忙。
View full article
[RTD500 IP] S32K388 Lpuart_UART割り込みエコー(LPUART4) こちらのリンクをご参照ください: [RTD600 IP] S32K312-EVB LPuart 割り込みエコー S32K388プラットフォームでの検証と学習中に、割り込みがエコーされないことが判明しましたが、原因は不明です。修正した例を添付します。 詳細情報: ボード: S32K388 S32DS3.5+RTD500 Re: [RTD500 IP] S32K388 Lpuart_UART interrupt echo(LPUART4) こんにちは、 割り込み/コールバックが受信のためにヒットされない、またはコードがエコーバックを送信しないことを意味しますか? BR、ペトル Re: [RTD500 IP] S32K388 Lpuart_UART interrupt echo(LPUART4) デバッグ中に割り込みコールバックが発生し、UART4 RXで受信したデータを確認しました。論理的には、RXで受信したデータはTXを介して直接送信され、コンソールにエコーされるはずですが、コンソールには何も表示されません。エラーの原因が不明なため、ご支援いただければ幸いです。 Re: [RTD500 IP] S32K388 Lpuart_UART interrupt echo(LPUART4) こんにちは、 受信ブールフラグ bRxFlag が最適化されて削除されているか、同様のようです。これはコールバックで設定されていますが、main の if ステートメントは実行されないため、文字列は返されません。 フラグを揮発性として設定してみる /* 受信フラグ */ 揮発性ブール bRxFlag = false; BR、ペトル
View full article
S32 Design Studio 3.1(Windows/Linux)发布! <meta http-equiv="Content-Type" content="text/html; charset=utf-8" />         产品发布公告 汽车微控制器和处理器 S32 设计工作室v3.1         Austin, Texas, USA 2019年4月4日   NXP 半导体汽车微控制器和处理器嵌入式工具团队很高兴地宣布发布 S32 Design Studio v3.1。以下是它的一些主要特点: 适用于 ARM32 和 aarch64 裸板和 Linux 目标的 NXP GCC 工具链(GCC 版本 6.3.1 20170509,构建 1574 修订版 g924fb68) S32 调试探针支持 S32 调试器和 S32 跟踪工具,适用于 S32V234 集成S32 Trace工具,提供软件分析功能(分析、代码覆盖率等) P&E调试器支持S32V23x 劳特巴赫 Trace32 ® 支持 提供 S32 Flash 工具,支持 S32V234 的 Flash/SD/MMC 内存编程 已集成适用于 S32V23x 0.9.0 Beta 版的 S32 SDK。发行说明请点击此处。 S32DS扩展和更新 S32 配置工具框架 (EAR7),包含引脚、时钟、外设、DCD、IVT 和 DDR 配置工具 S32 Design Studio版本 版本约定已改变。下图红框中标识的版本: 完整的 S32 Design Studio v3.1 发行说明可在此处获取。   安装 要下载安装程序,请访问 S32 Design Studio 产品页面下载部分或单击此处的直接内容。     安装程序要求输入激活 ID。安装包开始下载后,您应该会收到一封包含激活 ID 的通知电子邮件。 安装程序仅安装基本工具/包。为了开始开发,必须安装至少一个开发包。目前唯一可用的应用程序包是Vision S32V2xx (其他包即将推出) 。应用程序包由S32DS 扩展和更新管理。 技术支持 S32 Design Studio 问题通过 S32DS 公共 NXP 社区空间进行跟踪。 https://community.nxp.com/community/s32/s32ds  
View full article
i.MX6:Android 连接到 ADB <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 在适用于 i.MX5x 的旧版 Android 版本 R10.3.x 中,我按照用户指南的说明安装了 USB 驱动程序,并且能够成功设置 ADB 连接。不幸的是,对于同一台 PC,ADB 无法检测到使用 R13.5 的 i.MX6SL EVK。更新 Android SDK 工具没有帮助。 原因是新的 Android 设备使用与旧版本不同的 USB VID。因此,为了解决这个问题,我们需要更新 ADB 配置以扫描新的供应商 ID。以下是更新 Windows PC 的 ADB 配置的步骤。这些步骤(以及适用于 Linux PC 的步骤)也可以在 R10,3.x 中找到用户指南。 1. 运行SDK的工具生成ADB配置文件: C:\Program Files\Android\android-sdk\tools> android.bat 更新 adb 2.修改adb usb配置文件,添加新的供应商id 0x18d1。 File: X:\Profile\ \.android\adb_usb.ini # ANDROID 第三方 USB 供应商 ID 列表——请勿编辑。 # 使用“android update adb”来生成。 每行 # 1 个 USB 供应商 ID。 0x15a2 0x18d1 3. 在您的 Android BSP 发布包中解压 Freescale Android USB win 驱动程序“android_usb_fsl.zip”。如果您在当前包中找不到此文件,请获取 i.MX5x 的 R10.3.x 版本并将其解压。 4. 如果“android_usb_fsl.zip”是从旧版本中提取的,则解压后的“android_usb_fsl”中的文件“tetherxp.inf”可能不是更新的文件。因此,请覆盖解压后的“android_usb_fsl.zip”中的文件“tetherxp.inf”通过新的“tetherxp.inf”在您当前的 Android BSP 版本中。 5. 在i.MX6设备上启用“USB调试”选项 系统设置 -> 开发者选项 -> USB调试 6. 将 Android 设备连接到 PC,在设备管理器中卸载名为“Android Phone”的旧驱动程序,然后通过扫描和定位 .inf 文件重新安装驱动程序您手动解压 android_usb_fsl.zip 的目录下的文件。 7.重启ADB服务器 C:\Program Files\Android\android-sdk\platform-tools> adb kill-server C:\Program Files\Android\android-sdk\platform-tools> adb 启动服务器 8.最后,测试你的ADB连接 C:\Program Files\Android\android-sdk\platform-tools> adb 设备 已连接设备列表 0123456789ABCDEF 设备 恭喜!您的 ADB 现已开始工作。如果您有关于此主题的更多信息,请随时发表评论。 本文档由以下讨论生成: i.MX6:Android 连接到 ADB Android i.MX6_全部 回复:i.MX6:Android 连接到 ADB <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 如何在 ubuntu 16.04 环境中运行这个 回复:i.MX6:Android 连接到 ADB <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我不知道在哪里可以找到用于下载 i.MX5x 的 R10.3.x 版本。之后我也不知道该把这些文件放在哪里。 回复:i.MX6:Android 连接到 ADB <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 您好,我可以通过 USB 连接到 imx6 开发板,但无法通过其本地网络 IP 地址访问,我可以 ping 该设备,但 adb 说无法连接,该开发板正在 imx6 演示 android 图像上运行。
View full article
Freedom開発プラットフォーム <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> フリースケールのFreedom開発プラットフォームは、フリースケールの最新のARM® Cortex-M0™+ベースのKinetis KL25Zマイクロコントローラを搭載した低コストの評価および開発プラットフォームです 新機能!クイックスタートガイド 顔立ち: KL25Z128VLK4--Cortex-M0+ MCU搭載: - 128KBフラッシュ、16KBのSRAM - 最大48MHz動作 - USBフルスピードコントローラー OpenSDA--高度なUSBデバッグ・インターフェース トリコロールLED 静電容量式タッチ・スライダ フリースケールMMA8451Q加速度センサ 柔軟な電源オプション - いずれかのオンボードUSBコネクタから電源を供給 - コイン型電池ホルダー(オプションのポピュレーションオプション) - オプションのIOヘッダーからの5V-9V Vin - オプションのIOヘッダーに5Vを提供 - 3.3VとオプションのIOヘッダー間 リセットボタン 拡張IOフォームファクタは、Arduino™互換ハードウェア用に設計された周辺機器を受け入れます Freedom開発プラットフォーム Kinetis Lシリーズ・マイクロコントローラ Re: フリースケール・フリーダム開発プラットフォーム <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 再起動を押してボードを接続し、Debug-App_Pemircro_v106をドラッグしました。SDAをBOOTLOADERに接続し、ボードを電源に抜いて再接続しましたが、それでもうまくいきませんでした。なぜかわかりませんが、何かを更新する必要があるかもしれませんか? Re: フリースケール・フリーダム開発プラットフォーム <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ああ、それはあなたがまだMSDブートローダーモードであることを意味します(デバイスはFRDM-KL25Zディスクドライブとして列挙されますか? Debug-THE App_* を読み込む必要があります。SDA、参照 Freedom KL25Zボード上のOpenSDA これがお役に立てば幸いです。 Re: フリースケール・フリーダム開発プラットフォーム <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> [ポート] の下に強調表示されているものが表示されますが、Jungo の下には WinDriver しか表示されません。 Re: フリースケール・フリーダム開発プラットフォーム <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> USB CDCドライバーが正しくインストールされていることを確認できますか? 「Device Manager」の3番目の画像(「OpenSDA Debug Driver and Virtual COM Port」)を参照してください。 USBドライバーの修正 Re: フリースケール・フリーダム開発プラットフォーム <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> クイックスタートガイドの指示に従いましたが、2番(OpenSDA-CDCシリアルポートはデバイス管理にあります)に到達したとき、FRDM-KL25Zドライブを参照してOpenSDAポートにインストールし、[次へ]をクリックすると、「デバイスに最適なドライバーソフトウェアがインストールされています」と表示されます。そのため、デモコードをデバッグしても、接続が見つかりません。何かが足りないのでしょうか? Re: フリースケール・フリーダム開発プラットフォーム <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> おかげで、それは理にかなっています。 製品のフィールドアップデートでは、USBブートローダーを直接KL25に使用します (アプリケーションノート:USBファームウェアアップグレードAN4370) まあ、これを試してみるのが楽しみです! はい、信じられないほど低コストです。KL25は信じられないほどのスペックを持っています。すごいですね。 Re: フリースケール・フリーダム開発プラットフォーム <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> このMCUがあなたにとって役立つかどうかを確認し、生産ボードのプロトタイプを作成するのは良いことです。その目的は、非常に低コストのテストドライブを提供することであり、それは素晴らしい仕事をしています。 あなたがそう選択した場合、プログラマーを自由に購入し、開発サイクル全体を通じて使用することができます。10ピンヘッダーを入力するだけで、すぐに使用できます。12.00のデモボード(プログラマだけでなく、完全なシンボリックデバッガも含まれる)の場合、何を期待していたのかわかりません。 また、USBDMファイルをダウンロードすれば、カスタムボードで使用することができますが、そのままでは、USBDMインターフェースを使用しない限り、ボードに付属していた正確なチップでのみ使用できます。 プロダクションプログラマーの概念は、数千枚のボードのうち10枚を製造する場合に適用され、プログラマーにコードを保持するため、ダウンロードし続ける必要はありません。あなたがほんの数個を作っているだけなら、どんなプログラマーでも大丈夫です。 >これは「これから作るデザインにOpenSDAを使うべきではない」ということなのでしょうか? はい、OpenSDAを他のチップと同じように使用することはできません。USDBMアプローチを使用するか、BDMを購入する必要があります。 Re: フリースケール・フリーダム開発プラットフォーム <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> OpenSDAは製品に使用しないでくださいか? Open SDAユーザーガイドには次のように書かれていることに気づきました。 MSD フラッシュ プログラマは、特定のターゲット設定をプログラムするように設計されています。検証や構成はサポートしておらず 、実動プログラマとしては推奨されません。P&EマイクロコンピュータシステムズのCyclone製品は、生産プログラミングに推奨されます。 Open SDA がプロダクション プログラミングで推奨されない場合。では、それは本当に何に良いのでしょうか? プロダクションプログラマーが必要な場合は、開発中にこのプログラマーを使用するのもよいでしょう。 OpenSDAを使用して製品を設計するプロセスについて混乱しています。これにより、開発中にオープンSDAが使用され、生産中に放棄されます。つまり、製品は生産で使用するためにオープンSDAなしで再設計されますか? それとも、OpenSDAコンポーネントは開発ボードでのみ使用され、数百または数千を作成して本番環境でプログラムするときに単に無視されますか? 理解できるように助けてください。 つまり、PICでは、プログラマーを購入し、デバッグ、開発、および生産に使用します。 openSDAが「プロダクションプログラマーとして推奨されない」としたら、その目的が理解できません これは、「これから生産されるデザインにOpenSDAを使用すべきではない」ということでしょうか? ? ありがとうございます Re: フリースケール・フリーダム開発プラットフォーム <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> はい、デバッグとブートロードの 2 つの異なるモードがあります。 OpenSDAの詳細とスクリーンショットはこちらでご覧いただけます。 http://mcuoneclipse.wordpress.com/2012/09/20/opensda-on-the-freedom-kl25z-board/ お役に立てば幸いです。 Erich Re: フリースケール・フリーダム開発プラットフォーム <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> そうです、ジム。 基本的に、OpenSDAを使用してボードをプログラムおよびデバッグする場合は、次のようにします。 - ブートローダーモードにして、デバッグsdaファイルをドラッグアンドドロップします。 また、任意の.srecをドラッグアンドドロップしたい場合は、外出先でプログラムするためのファイル: - ブートローダーモードにして、MSD sdaファイルをドラッグアンドドロップします。 Re: フリースケール・フリーダム開発プラットフォーム <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ここに別の注意点があります。SDAを使用してデバッグする場合は、DEBUG SDAファイルを使用して再プログラムする必要があります。 Re: フリースケール・フリーダム開発プラットフォーム <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 問題が見つかりましたが、マウントされたディレクトリは実際にはファイルシステムではありません。P&Eからドライバをロードし、実際にボードをプログラムするディレクトリにファイルをコピーする必要があります。(そして、LASTSTAT.TXTにはプログラミングではなく完了と表示されます...)。これは、コピー操作に比較的長い時間がかかる場合(つまり、進行状況バーが表示されます)。それを行うと、宣伝どおりに機能します。 Re: フリースケール・フリーダム開発プラットフォーム <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ボードを受け取り、クイックスタートガイドの指示に従って、ボードを受け取ったとき、すぐにFRDM-KL25ZドライブとしてPCにマウントされました。次に、 OpenSDAの概要 の指示に従い、BOOTLOADERドライブで再起動しました。その後、指示に従って、 ファイルMSD-FRDM-KL25Z_Pemicro_v105にコピーしました。QuickStart データからの SDA 。ドライブを取り出し、USBを抜いてから、USBを再接続しました。この時点から、BOOTLOADERフォルダのみが表示され、表示されるまでに約5分かかります。ボード上のSDA_INFO.HTMファイルを見ると、まだブートローダーのバージョンが1.01と表示されています。次に何をすべきかについての提案はありますか?
View full article
i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ** 如果您无法访问www.youtube.com ,您可以在这里观看 Wi-Fi Display Sink 演示:** ******** http://v.youku.com/v_show/id_XNzczMzQ2MTc2.html******** 我们现在已经拥有强大的 i.MX 6 来支持 Android kitkat。因此我们还在其中开发了WiFi Display Sink。 借助 Wi-FI 显示技术,我们可以通过 Wi-Fi P2p 将屏幕和音频投射到另一个屏幕上。它也被命名为 Miracast。 飞思卡尔通过提供 Wi-Fi 显示接收器功能扩展了 Android 系统。此功能使用的 Wi-Fi 硬件模块包括 Realtek RTL8821AS、RTL8723AS 和 AR6233 SDIO 卡。但该功能的设计允许移植到任何 Wi-Fi 硬件模块。使用飞思卡尔Wi-Fi 显示接收器 API 和演示应用程序,用户可以轻松开发自己的接收器应用程序。此功能已在多款最流行的 Android 手机和平板电脑上得到验证。 我们的Wi-Fi显示器具有以下突出特点: 低延迟 支持UIBC(当源设备使用Freescale Android maddev_kk4.4.3-2.0.0时) 网络拥塞快速恢复 兼容不同供应商的 Wi-Fi 芯片和 Wi-Fi 显示设备 从演示视频中我们可以投射秒表并通过它测量延迟。以下是高质量的视频镜头,我们可以计算出实际延迟小于 200 毫秒! 对于 WiFi 显示规格,下图中的橙色部分是在我们的 WiFi 显示中实现的。 参考页面: Miracast - 维基百科 Wi-Fi 认证 Miracast | Wi-Fi 联盟   有关 i.MX6 中的 Wi-Fi 显示接收器的更多信息和详细信息,请发送询问至[email protected] 。 Re: Wi-Fi Display Sink in i.MX6 Android release android6.0  的uibc 似乎用不了,请问,有没有库的源码部分? 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 大家好, 如何使设备成为 Miracast 接收器? 此致, 阿拉文斯 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,Haoran,Realtek 8821AS 是一款组合式 wifi-BT,你知道 KK4.4 中的这款芯片组模块是否支持蓝牙吗? 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 对于 HDCP 支持,我们在 L5.0 GA 版本中提供支持。请查看发布文档,了解如何在 WIFI Display Sink 包中获取 HDCP 支持。 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Hi, 我有一些问题。 我得到了 WFD Sink 的包并在 i.mx6dq sabresd 板上成功测试了它。 但我无法在 WFD Sink 应用程序中测试 UIBC。 我使用三星 Galaxy S4 到 WFD 源设备。 UIBC 是否仅支持飞思卡尔源设备和接收设备之间? 我怎样才能获得 WFD 源包? 谢谢。 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Hi Haoran, 我也想了解 HDCP 发展的时间表。我们很快就会看到吗? 此致, Yufeng 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 此网站上可供下载的 Android 软件包是否具有 Miracast 功能,还是我必须专门向销售人员询问? 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Hi  HDCP 现在能工作吗? i.mx6 仅在 HDMI 中具有 HDCP 模块,是否可以将 HDCP 实现到 i.mx6? 谢谢。 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 您写道“基于 i.MX6 DualLite 和 i.MX6 Quad 处理器的飞思卡尔 Wifi 显示器。它可在我们的 Android 和 Linux BSP 上使用。” 我一直在寻找基于 i.MX6 AI 平台的 yocto linux 上的 Miracast Sink 解决方案。 您能否告诉我如何获取 Linux 的扩展 Wifi Display 接收器功能包? 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Hi Bryan, 感谢您对我们的 Wifi Display 感兴趣。 对于购买这些物品,我认为我们的营销和销售部门很快就会在我的岗位上与您签约。 我是研发工程师,能够为您提供技术支持。 基于 i.MX6 DualLite 和 i.MX6 Quad 处理器的飞思卡尔 Wifi 显示器。它在我们的 Android 和 Linux BSP 上可用。 我们支持 Source 和 Sink 功能并遵循 Wifi Display 规范。 i.MX6 DualLite/Quad 同时支持 HDMI 和 LVDS 输出。所以我认为我们的解决方案可以满足您的要求。 对于如何启动它,请获取一两个我们的“Sabresd”平台和 SDIO wifi 模块,并从我们的销售处获取 Wifi Display Sink 包,然后您就可以对其进行评估。 谢谢! BRs, 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 问候, 我是飞思卡尔社区的新人。我一直在寻找 Android 平台上的 Miracast Sink 解决方案。这种可能性非常有趣。 是否有关于如何购买正确的硬件并运行 Miracast Sink 解决方案的分步指南? 我正在考虑将其作为会议室解决方案。我很乐意使用这种硬件和软件组合来构建解决方案。 如果我在这里说得有些不妥,请原谅我。请给我适当的指示。 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,Saurabh, 谢谢您的回复。我如何判断这是 HDCP 验证还是其他问题?有什么方法可以启用日志吗? 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 某些设备需要 HDCP 验证,Imx6 硬件无法通过 HDCP 验证。所以这是有可能的。 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> Hi, 我让该包在魔杖板上运行,但无法将其连接到接收器或源设备。 当我将其用作接收设备时,我使用以下命令进行了测试: # wfd -l 192.168.2.123:1234 其中192.168.2.123 是 wandboard 的 IP 用于测试的源设备是 Sony Xperia Z3 和 Moto X,两者都未能找到作为 miracast 接收器的 wandboard。请注意,这两个设备都可以作为接收器连接到小米盒子。 对于 miracast 源测试,我尝试使用以下命令: # wfd -c 到小米盒子和另一个运行 Android 4.3 的 imx6 板(作为接收器的命令是 wfd -l : ) 我是否正确使用了该包或者遗漏了什么? 谢谢! 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 事实上,它们每一个对于我们的 Wifi 显示器来说都足够了。从我们在开发环境中的性能测试来看,RTL8821AS 会更好,因为它是新设计的并且支持 80211ac。 要订购它们,您可以请求 Realtek 或 Silex 的官方帮助。 谢谢! 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 非常感谢您的有益回复。 关于Wi-Fi SDIO卡,您提到的三个模块(Realtek RTL8821AS,RTL8723AS和AR6233)中,您推荐哪一个性能最佳?您是否知道我们可以在哪里方便地订购一些? 感谢并致意 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 感谢您的关注。 我们正在为我们的 wifi 显示接收器开发 HDCP。稍后将会发布。 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 伟大的!!! HDCP 有用吗? 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我们在 Android_kk4.4.2_1.0.0 版本中有一个单独扩展的 Wi-Fi 显示接收器功能包。请参阅下面的社区主题和附加的发行说明: https://community.freescale.com/docs/DOC-102180 有关 Android 4.4 Extended 软件包产品的更多详细信息,请联系[email protected] 。 •      飞思卡尔正在提供额外的软件包来扩展 Android KK4.4 核心功能。这些软件包将提供给已获批准的客户(需向[email protected]提出申请),Freescale.com 网站上不会公开提供。 •      有两个可用软件包: 1.      扩展多媒体功能包 2.      Wi-Fi 显示接收器功能包 •      源代码包将“按原样”提供,不提供支持,并将通过外联网网站提供给批准的客户。 •      客户可以选择从飞思卡尔购买支持或定制服务。 谢谢! BRs, 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 做得好!看起来很棒。 我想知道什么时候可以推出支持 Wi-Fi 显示接收器的 BSP? 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 极好的! 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 干得好,团队! 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 酷极了! 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 伟大的! 回复:i.MX6 Android 版本中的 Wi-Fi 显示接收器 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 太棒了!
View full article