Unable to install SECRDR S32K1 in S32DS 3.6.6 I installed S32DS 3.6.6, and noticed there were no project examples for S32K1 devices. So I went to install new software, and I used the jar file DesignStudio_updatesite.zip: Then I selected the applicable items: When I proceed, there is a message at the bottom about "Cannot perform operation": Followed by a "Remediation Page": In the end, one of the packages is installed, but I do not find the project examples for S32K1xx in New | S32DS Project from Example. Is something wrong with 3.6.6, or with the Designupdate archive? Re: Unable to install SECRDR S32K1 in S32DS 3.6.6 Thank you Peter. 3.6.0 was released November 2024. Is it really true that RTD is unsupported in 3.6.1 through 3.6.6??? I'm not sure how users are supposed to know based on what you underlined that RTD is not supported by later versions of S32DS, as that is not explicit. From a user perspective, 3.6.1 - 3.6.6 are therefore useless if you need RTD. That is hard because there are really a lot of needed updates through 3.6.6. Thanks, Matt Re: Unable to install SECRDR S32K1 in S32DS 3.6.6 Hello,
I installed S32DS 3.6.6, and noticed there were no project examples for S32K1 devices.
The examples are part of RTDs or SDKs and will become available once you install the driver package.
Before you install the RTD, check the requirements for particular driver package.
Use extension and updates for install of updatesite zip packages:
Here is the guide:
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32DS-Extensions-amp-Updates-Explanation-and-How-To-Use/ta-p/1128543
I do not have S32DS installed so I cant confirm if QLP3 is not working on S32DS 3.6.6.
But always refer to the release notes on each package you are going to install to prevent issues.
Best regards,
Peter Re: Unable to install SECRDR S32K1 in S32DS 3.6.6 In desperation I tried the older 3.0.0 QLP02 RTD drivers, and they worked! 3.0.0 QLP03 is BROKEN. Re: Unable to install SECRDR S32K1 in S32DS 3.6.6 Here is a more detailed error: Re: Unable to install SECRDR S32K1 in S32DS 3.6.6 Not sure if this is related - Re: Unable to install SECRDR S32K1 in S32DS 3.6.6 Hello,
I really cannot speak for SW team, but from my experience the compatibility is always the main issue between RTD and S32DS.
3.6.0 was released November 2024. Is it really true that RTD is unsupported in 3.6.1 through 3.6.6???
I never tied it so I cannot confirm this.
But it should be possible to run it also on 3.6.6.
@jiri_kral can you comment here?
Also project examples are usually part of basic major version of RTD,.
Best regards,
Peter Re: Unable to install SECRDR S32K1 in S32DS 3.6.6 We are really stuck. We are unable to install a working combination of S32DS, GCC, and RTD. If there is a magic combination of versions that is known good, please advise. Re: Unable to install SECRDR S32K1 in S32DS 3.6.6 Hello,
I was speaking with S32DS team.
“It is necessary to use the base version without any patches. You currently has Patch 03 installed, but this patch is intended to be applied only on top of the official release. Furthermore, these patch versions have not been formally tested.”
Best regards,
Peter
View full article