Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
Issues with Ethernet Enablement and Network Connectivity on NXP S32G-VNP-RDB2 I have powered on the NXP S32G RDB2 Board and was able to communicate serially with PuTTY.  However when I want to connect ethernet cable to it. Even though I tried assigning static IPs, it wouldn't ping. I want to enable the ethernet driver or solve the issue so that I can test my usecases. Re: Issues with Ethernet Enablement and Network Connectivity on NXP S32G-VNP-RDB2 Hello @chenyin_h , I am glad to share that finally it is pinging and tested out by connecting to router and creating a private network with other boards, for now I am exploring ethernet communications at other ports too. For any other problems, I shall open another ticket or post. Thank you! Re: Issues with Ethernet Enablement and Network Connectivity on NXP S32G-VNP-RDB2 Hello, @vigneshrk0482  Thanks for your reply. I have just tested it on my local RDB2 with default BSP35.0 images(without any other settings), the eth0 could be used correctly. The testing log is attached for your reference. BR Chenyin Re: Issues with Ethernet Enablement and Network Connectivity on NXP S32G-VNP-RDB2 Hello @chenyin_h , The BSP version is Auto Linux 35 (U-boot from SD Card) and using the GMAC port. However I think that the ethernet is not enabled. When I checked eth0 in ip route it says NO-CARRIER but in ifconfig it says UP. Also I want to use this to communicate with Raspberry Pi to NXP board. Please guide me what steps to do as I have tried all the attempts. Re: Issues with Ethernet Enablement and Network Connectivity on NXP S32G-VNP-RDB2 Hello, @vigneshrk0482  Thanks for the post. May I know which version BSP(or other software package) is used for your test? which network port was used? BR Chenyin 
View full article
无法在地址 0x80000000 写入数据 我正在确认使用 LS1046A 的定制开发板能否启动。我在 https://github.com/nxp-qoriq/atf.git 上创建了 PBL, 以启用 QSPI 模式启动。但是,执行时控制台消息停留在“NOTICE: BL2: Built: [日期和时间]”处。 根据建议,我使用 QCVS DDR 工具访问 DDR,但读写均失败。此外,当我在[目标连接]选项卡中运行[诊断连接]时,在[测试DDR内存访问]部分输出了一个错误:“无法在地址0x80000000处写入数据”。 需要修改https://github.com/nxp-qoriq/atf.git上的哪些区域才能初始化我的自定义板的DDR?目前,我正在基于LS1046ARDB创建一个PBL。 谢谢。 回复:无法在地址 0x80000000 写入数据 是的,请使用DDRv工具提供的参数。 回复:无法在地址 0x80000000 写入数据 感谢您,DDR初始化成功。不过第三步也是必须的,所以我会记下来。 3.在ATF代码中,勘误表A09803设置“ddr_out:address=0x1080114,value=0x401160”,但在DDRv工具生成的DDR初始化文件中,它被描述为CCSR_BE_M(0x01080114,0x00401150 | 0x00000020)。因此,通过修改 ddr_init.c将 0x401170 写入 0x114,成功。 这是一个错误吗? 回复:无法在地址 0x80000000 写入数据 1.首先,对于在定制板上引入的新DDR,我们建议客户使用QCVS DDRv工具进行验证和优化,以获得优化的参数,以便在atf源代码中使用它们。 有关 QCVS DDRv 工具的使用,您可以参考以下文档。 https://www.nxp.com.cn/docs/en/user-guide/QCVS_DDR_User_Guide.pdf https://community.nxp.com/t5/Qonverge-Knowledge-Base/DDR-Controller-Configuration-on-LS2085-LS2080-Bringing-up/ta-p/1128310 您可以使用“从 SPD 读取”方法创建 QCVS DDR 项目,然后连接到您的自定义板进行验证以获取优化参数并构建以生成代码 ddr_init.c并在 ATF 源代码中使用它。 2.根据您的定制板修改atf源代码。 返回文件夹flexbuild_lsdk2108_github,运行以下命令获取atf源代码。 $ flex-builder-c atf-m ls1046ardb-b qspi 转到 atf 源代码文件夹 components/firmware/atf/,请根据您的定制板修改 ddr 控制器初始化文件 plat/nxp/soc-ls1046a/ls1046ardb/ddr_init.c。 使用以下命令重建 atf。 $ flex-builder-c atf-m ls1046ardb-b qspi 您将在文件夹 flexbuild_lsdk2108_github/build/firmware/atf/ls1046ardb/ 中获得 atf 图像 bl2_qspi.pbl 和 fip_uboot.bin。 请在 QSPI 闪存的 0 处部署 bl2_qspi.pbl 并在 0x100000 处部署 fip_uboot.bin。
View full article
I.MX8 MINI的PCIE问题 您好,我们使用i.MX 8M Mini Quad作为产品的主控制器,考虑到它不支持USB3.0的功能,我们就计划使用它的PCIE接口配合UPD720202K8-711-BAA-A芯片来实现USB3.0的功能。但是我在“i.MX 8M Mini Hardware Developer’s Guide”中看到“使用适当的外部 PCIe 参考时钟发生器”。我想了解一下为何要建议使用外部的PCIe时钟发生器呢?在我的这个方案中如果不作用外部时钟发生器可以吗?会有什么影响? (我目前的设计是没有使用外部时钟发生器,UPD720202K8和I.MX8的PCIE_TX,PCIE_RX通过0.1uF电容相连,PCIE_CLK是直连的。) i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlus i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: I.MX8 MINI的PCIE问题 现在我也是想要使用内部参考时钟,在设备树中将ext_osc属性改为了0,但是还是没有时钟输出可能是什么原因呢,使用的是Linux4.14.78版本的内核 Re: I.MX8 MINI的PCIE问题 Hi @mytemp  我们不建议客户使用内部时钟。根据我们的测试,内部时钟的抖动比标准高出约 30%。 不过内部PLL可以通过PCIe Gen 2 一致性测试,也有其他客户用内部时钟。还是建议你在测试阶段保留外部时钟,如果内部时钟无法达到你们的稳定性要求,可以切换到外部时钟。
View full article
Changes to the p_flash of the S32K312 may cause the program to run erratically. Hi,nxp 1.By modifying the linker_flash_s32k312.ld file, the starting address of p_flash was changed from 0x00400000 to 0x00440200, resulting in the program malfunctioning, as shown in the attached image. The code is included in the attachment. 2.The expected outcome is that the program does not feed the watchdog and should restart from the beginning, rather than malfunctioning. That's all, thank you. Re: Changes to the p_flash of the S32K312 may cause the program to run erratically. Hi, Erase the entire chip and reload the program. Thanks Re: Changes to the p_flash of the S32K312 may cause the program to run erratically. I modified the original project by changing the starting address of int_pflash to 0x00500000 in the linker_flash_s32k312.ld file, but the program still runs incorrectly. Am I misunderstanding something, or is there another area that I haven't changed? 1)linker_flash_s32k312.ld->MEMORY 2)Schematic of program malfunction Re: Changes to the p_flash of the S32K312 may cause the program to run erratically. You can place it at 0x50_0000, which is a valid IVT address and it is in the next block, so it can be programmed by the bootloader in the 0x40_0000 block. Regarding the HSE_FW, please create a new thread. Thank you, BR, Daniel Re: Changes to the p_flash of the S32K312 may cause the program to run erratically. Hi,danielmartnek 1.I understand that this project should be flashed by a bootloader, right? Reply:Yes,There are other matters to pay attention to. 2.But if you flash the project directly (DM181S_S32K312_BOOT.elf), the SBAF then searches for the first valid IVT starting from the lowest address at 0x00400000. Reply:According to your intention, when debugging the app project online without the bootloader, the starting address of int_pflash still needs to be set to 0x00400000. 3.Additionally, if we enable the HSE firmware later on, how should we debug the app project that does not include the bootloader, and how do we allocate memory? Re: Changes to the p_flash of the S32K312 may cause the program to run erratically. Hi @victory, I understand that this project should be flashed by a bootloader, right? But if you flash the project directly (DM181S_S32K312_BOOT.elf), the SBAF then searches for the first valid IVT starting from the lowest address at 0x00400000. Regards, Daniel
View full article
RTC callback function cannot be triggered I am using the S32K344 chip and plan to use RTC to generate logs with timestamps and store them in the SD card, but I am unable to access callback functions. Re: RTC callback function cannot be triggered Yes, I did all of these。 Re: RTC callback function cannot be triggered Hi @SCoder41, Have you set a date and time configuration for the RTC? You also need to set the interrupt driver for the RTC IRQ: After setting a date and time, and the RTC IRQ, the RTC alarm callback should be stepped into when the alarm date&time = current date&time. Keep in mind you do need to install the handler and enable the IRQ in the source code, as well as setting the time&date, configuring the alarm, enabling interrupt and starting the counter to enable the basic functionality of the RTC alarm. Best regards, Julián
View full article
S32_Design_Studio_for_S32_Platform_3.6.0 のインストール中にエラーが発生しました S32 Design Studio for S32 Platform 3.6.0 をインストールできませんWindows 10 Proで。 インストールログにエラーエントリがあります。 S32 Design Studio for S32 Platform 3.6.0(インストールすべてのアンインストーラコンポーネント) ステータス: ERROR 追記事項: ERROR - Error writing LaunchAnywhere components (Access Denied) 私のアクティベーションコードにはいくつかのプロレムがあります。 オンライン登録とオフライン登録のどちらを使用するかは関係なく、結果は常に同じです:ライセンスを確認すると、インストールプロセスが停止および終了します。 これに対する解決策はありますか? ありがとうございます リチャード 日時:S32_Design_Studio_for_S32_Platform_3.6.0のインストール中にエラーが発生しました   結局、問題はWindowsまたは使用されたインストールソフトウェアであるInstallAnywhereのいずれかにあることが判明しました。WindowsのメインディスクCには約11GBの空き容量しかなかったため、十分な容量があるディスクDにソフトウェアをインストールすることを計画しました。ただし、S32 Design Studioは、インストール中に一時ファイル用に約12.5GBのスペースを必要とします。インストーラー S32DS_3.6.0_win32.x86_64.exeを起動してみたところ、エラーメッセージが表示されました(チェコ語のスクリーンショットが添付されています)。 「完全な設置には十分なスペースがありません。インストーラーを配置する一時フォルダを選択してください。 そこで、ディスクD上のフォルダを選択しましたが、インストールは常に上記のエラーで終了しました。結局、ディスクCのスペースを空けたおかげで、ディスクCのスペースを合計13GB空けた後、インストールは予想通りに進みました。 問題は解決しました。 感謝 リチャード 日時:S32_Design_Studio_for_S32_Platform_3.6.0のインストール中にエラーが発生しました こんにちは、@rick1964。 同様の状況は、以前にコミュニティで議論されました。以下のコミュニティスレッドを見て、そこで提供された解決策が役に立ったかどうか教えてください。 Windows 11 で S32DS V3.6 のインストールが失敗します。 - RomanVR。 日時:S32_Design_Studio_for_S32_Platform_3.6.0のインストール中にエラーが発生しました ありがとう、でも 私はこれを何度か試しました。licfixを使用してライセンスを削除してから、インストールを実行し、転記エラーを避けるために電子メールから直接アクティベーションコードをコピーします。結果は常に同じです (添付資料を参照)。奇妙なことに、同じコードを使用して、別の古いコンピューター(Windows 7を実行)にStudioを問題なく正常にインストールしました。インストールに失敗したコンピュータには、すでにS32 Design Studio for Armと他のソフトウェア(MUXpresso、FreeMaster)がインストールされています。 よろしくお願いいたします。 リチャード 日時:S32_Design_Studio_for_S32_Platform_3.6.0のインストール中にエラーが発生しました こんにちは@rick1964  管理者権限でS32DSインストーラーを実行し、アクティベーションコードにタイプミスがないことを確認してください。このエラーは、通常、ユーザー権限の制限が原因です。 これがお役に立てるかどうか教えてください。 - RomanVR。
View full article
BSP Version Required for dm-eiq-genai-flow-demonstrator on i.MX95 Hi Team, I’m exploring the dm-eiq-genai-flow-demonstrator (GenAI Flow) on the i.MX95 platform working within a Yocto environment. Could you please clarify:      1. Which BSP version (e.g., L6.12.20_2.0.0) is minimum required to run the demo end-to-end?     2. Does this BSP include all necessary elements—such as updated Neutron delegate, TFLite  runtime, and tooling—to support LLM inference (RAG)?     3. Are there any additional Yocto meta-layers or image recipes (for example meta-eiq-        genai) recommended for this demo? Thanks in advance for your insights! Best regards, Varshil Gandhi Re: BSP Version Required for dm-eiq-genai-flow-demonstrator on i.MX95 Hi Varshil, Thanks for your questions. Let me try to answer them: 1. The package was initially made for Q1 BSP L6.12.3-1.0.0 for i.MX95 rev Ax. 2. This Q1 BSP does not directly include what's necessary to leverage Neutron on LLM inferences. That's why the package provides a meta-layer. 3. This meta-eiq-genai-flow meta-layer provides the possibility to add a Onnxruntime Neutron Execution Provider to accelerate the LLM operations on Neutron and free up some CPU resources, with associated patches/files for Kernel and Neutron Fw. Please note that we are using onnxruntime and not TF lite for this project. That being said, Q2 BSP (e.g., L6.12.20_2.0.0) is being released this days. It supports the B0 revision of i.MX95 but without LLM acceleration on Neutron, only CPU mode is functional. Thanks and best regards, Pierre  
View full article
S32k344 uart 模块无法同时发送和接收信号 你好 , 当我使用 EB tresos 配置 uart 计划时,我不知道如何同时使用发送和接收功能,因为当其中一个接口发送或接收数据时,另一个接口会相互阻塞。例如我使用 UART_AsyncReceive 准备接收数据,如果没有数据输入,uart 的状态就是 UART_STATUS_OPERATION_ONGOING,在这种情况下,Uart_AsyncSend 无法正常工作, ,谁能帮帮我?非常感谢 Re: S32k344 uart moudule can not send and receive at the same time 很奇怪,已经一年了,没有人回应你。我们的 RTD3 也遇到了同样的问题。我们还没有找到解决方案,尤其是因为我们使用的是发送和接收数据的定期任务。我想知道你们是否找到了解决这些基本 UART 问题的方法。令人吃惊的是,恩智浦竟然没有设法解决这些根本性问题。
View full article
LPC1769 是否已过期? 您好, 目前 LPC1769 的供应情况非常糟糕。到目前为止,Mouser和Digikey已经停产了我购买的零件(LPC1769FBD100,551),法内尔甚至表示该设备已停产: 贸泽公司称有替代品,但交货期为 52 周: 恩智浦该设备的当前生产状态是什么? 谢谢。 Re: LPC1769 EOL? 您说得没错,LPC1769 的长寿计划将持续到 2024 年底。 你好@Omar_Anguiano、 快进四年,现在是 2025 年,根据产品寿命页面显示,LPC1769 已退出寿命计划。 在产品页面上,该部件仍然是"active" 。 恩智浦会将LPC1769FBD100供货多久? 谢谢。 丹尼尔 Re: LPC1769 EOL? 分销商也无法获得这些部件。 情况非常糟糕。 Re: LPC1769 EOL? 谢谢@Omar_Anguiano的回复。 你写道 不过,我们不会在论坛上对此进行更详细的讨论,敬请谅解。 很抱歉不能回答您最后的问题。 如果不是在论坛上,我在哪里可以得到问题的答案? 作为恩智浦产品的客户(尽管数量相对较少),我认为这些都是值得回答的问题。尤其是,恩智浦最近推出的其他控制器(如 LPC552*)的可用性也很低。今后,我学会了在选择控制器时不要只看技术特性,还要看是否可用。此外,选择代码包可能会对可用性产生很大的影响(例如,从HLQFP迁移到VFBGA以获得更好的可用性)。我认为,要做出正确的决定,需要与恩智浦的专家进行讨论。 干杯, Dan . Re: LPC1769 EOL? 考虑到半导体供应的整体工业形势,你关于可用性的问题是可以理解的。许多专业出版物中都发表了许多关于这个问题的分析文章,它们为我们行业在去年发生的最初触发信号和动态提供了良好的背景信息。 不过,我们不会在论坛上对此进行更详细的讨论,敬请谅解。 很抱歉不能回答您最后的问题。 致以最崇高的敬意, Omar Re: LPC1769 EOL? 亲爱的@Omar_Anguiano、 我很高兴我在 1 月底订购了我的 LPC1769 设备。现在,大约一个月后,该设备不再可用。我不敢想象,如果我当时没有下订单,会发生什么。这完全是运气。 正如你所确认的那样,该设备尚未停产,但是,52 周的交货时间对我来说还是出乎意料的。 预计恩智浦设备会缺货一整年,这通常吗? 我能指望恩智浦在大约一年后再次推出这款设备吗? 谢谢。 丹 Re: LPC1769 EOL? Hello 您说得没错,LPC1769 的长寿计划将持续到 2024 年底。 LPC1769FBD100,551 和 LPC1769FBD100K 的区别在于包装。 请告诉我这是否回答了您的问题,如果您有更多问题,请随时咨询我。 致以最崇高的敬意, Omar Re: LPC1769 EOL? @Omar_AnguianoOmar,谢谢,您能否确认我们的计算结果正确,LPC1769 的长寿计划将持续到 2024 年底? LPC1769FBD100,551 和 LPC1769FBD100K 有什么区别?产品数据手册中没有提及 " K " 零件号。 Re: LPC1769 EOL? Hello LPC1769 并非 EOL,该部件属于长寿命计划,因此在该计划结束之前,该部件不会成为 EOL。 如果您有更多问题,请随时与我联系。 致以最崇高的敬意, Omar Re: LPC1769 EOL? 你可能需要直接联系恩智浦或官方代理商,以获得澄清。 通常情况下,硅料供应商会向客户发送信息,告知即将发生的 EOL 事件和可能的最后购买选择。我(即我的公司)正在为 90 年代中期的一个 MCU 进行一项研究。每种类型的数量都在 4 位数范围内,因此数量并不多。 Re: LPC1769 EOL? 我也没想到它要到2024年才会停产,但是,我认为一款一年才能上市的设备已经接近停产了。至少这种供应短缺是非常出人意料的,促使我尽早更换现有设计中的这款处理器。 Re: LPC1769 EOL? 据此 https://www.nxp.com/products/product-information/product-longevity:PRDCT_LONGEVITY_HM lpc1769fbd100 自 2009 年 12 月用上市以来的使用寿命为 15 年...
View full article
IMX93QSB 的 Flexspi_nor_polling_transfer SDK 示例中的供应商 ID 问题 大家好 我使用适用于 VSCode 的 MCUXpresso 来测试类似 imx93-qsb 的定制板的外围设备。从 SDK 项目 " flexspi_nor_polling_transfer " 开始,我想测试或非闪存 MT25QU01GBBB8E12 的功能,它与示例中使用的芯片非常相似:MT25QU512ABB。 当谈到函数 flexspi_nor_get_vendor_id 时,它给出 0xFF 而不是 0x20,然后它会成功完成最后一次操作。         我使用的是与示例相同的 SPI 外设(SD3 焊盘上的 flexSPI1),我不明白为什么我没有正确读取 ID 供应商。谁能帮帮我? Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB 值得一提的是,在扩展 SPI 模式下使用 IS25WX256 时,读 ID 命令 0x9E 也有问题。命令格式为 "FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x9e, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 4),"。每次使用时,我都会读到 `0x888cadce`。 Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB 你好@AldoG、 我试着在 flexspi_nor_get_vendor_id 功能中加入一些 PRINTF 命令,以了解 vendorID 值是怎么回事。 输出结果是这样的 我还尝试将 flashXfer.seqIndex 改为 4 *NOR_CMD_LUT_SEQ_IDX_READID,结果输出发生了变化: 我不知道在功能内部反复推敲是否会有帮助。也许问题出在 seqIndex 值本身。请告诉我您的想法。 此致, 鲍勃 Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB 您好, ,我发现您使用的正是原样,而不是我建议添加的内容。 我不认为是内存工作不正常,而是获取 ID 的 LUT 命令工作不正常,所以我才提到是否有可能检查发送是否正确。 致以最崇高的敬意/问候, Aldo。 Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB 你好 我很确定闪存运行良好,因为我已经能够使用这个 UUU 命令放置针对 或非-flash 的引导加载程序: uuu.exe-b qspi imx-启动-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot 在 FlexSPI Serial NOR 中设置启动配置,我可以看到引导加载程序运行正常。但我还是不明白,为什么在 MCUXpresso 的 VScode 中使用该项目会出现问题。 如果您能帮助我,请告诉我,我也需要使用 iMX93 的 M33 内核。 谢谢! 鲍勃 Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB 您好, 感谢您的分享,我会仔细检查的。 同时,您有办法检查硬件上的信号吗? 致以最崇高的敬意/问候, Aldo。 Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB 你好,阿尔多、 谢谢你帮我。遗憾的是,对 LUT 的更改并不能解决问题,我仍然在 Vendor ID 上读取到 0xff 的值。我与大家分享整个 C 代码: /* * 版权所有 (c) 2016,飞思卡尔半导体有限公司 * 2016-2018 恩智浦版权所有 * 保留所有权利。 * * * SPDX 许可证标识符:BSD-3 条款 */ #include "pin_mux.h" #include "clock_config.h" #include " board.h " #include "fsl_debug_console.h" #include "fsl_rgpio.h" #include "fsl_lpi2c.h" #include "fsl_iomuxc.h" #include "fsl_lpi2c.c" #include "fsl_flexspi.h" #include "app.h" #include "fsl_debug_console.h" #include "fsl_cache.h" #include "pin_mux.h" #include "clock_config.h" #include " board.h " #include "fsl_common.h" /******************************************************************************* * 定义 ******************************************************************************/ /******************************************************************************* * 原型 ******************************************************************************/ /******************************************************************************* * 变量 ******************************************************************************/ /* 程序数据缓冲区应以 4 字节对齐,这样可以避免总线故障,因为此内存区域配置为 MPU 的设备内存。*/ SDK_ALIGN(静态 uint8_t s_nor_program_buffer[256], 4); 静态 uint8_t s_nor_read_buffer[256]; 外部 status_t flexspi_nor_flash_erase_sector(FLEXSPI_Type *基, uint32_t 地址); 外部 status_t flexspi_nor_flash_page_program(FLEXSPI_Type *基, uint32_t dstAddr, 常数 uint32_t *src); 外部 status_t flexspi_nor_get_vendor_id(FLEXSPI_Type *基础, uint8_t *vendorId); 外部 status_t flexspi_nor_enable_quad_mode(FLEXSPI_Type *基); 外部 status_t flexspi_nor_erase_chip(FLEXSPI_Type *基); 外部 void flexspi_nor_flash_init(FLEXSPI_Type *基); /******************************************************************************* * 代码 ******************************************************************************/ flexspi_device_config_t deviceconfig ={ .flexspiRootClk = 12000000, //12 MHz, ok per noi .闪存大小 = 闪存大小, .CSIntervalUnit = kFLEXSPI_CsIntervalUnit1SckCycle, .CSInterval = 2, .CSHoldTime = 3, .CSSetupTime = 3, .数据验证时间 = 0, .列空间 = 0, .启用 WordAddress = 0, .AWRSeqIndex = 0, .AWRSeqNumber = 0, .ARDSeqIndex = nor_cmd_lut_seq_idx_read, .ARDSeqNumber = 1, .AHBWriteWaitUnit = kFLEXSPI_AhbWriteWaitUnit2AhbCycle, .AHBWriteWaitInterval = 0, }; const uint32_t customLUT[自定义长度] ={ /* 快速读取四通道模式 -SDR */ [4 * nor_cmd_lut_seq_idx_read + 0] = flexspi_lut_seq(kFLEXSPI_Command_SDR, kFLEXSPI_4PAD, 0xEB, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_4PAD, 0x18), [4 * nor_cmd_lut_seq_idx_read + 1] = flexspi_lut_seq( kFLEXSPI_Command_DUMMY_SDR, kFLEXSPI_4PAD, 0x0A, kFLEXSPI_Command_READ_SDR, kFLEXSPI_4PAD, 0x04), /* 读取状态寄存器 */ [4 * nor_cmd_lut_seq_idx_readstatusreg] = flexspi_lut_seq(kFLEXSPI_Command_SDR, kFLEXSPI_4PAD, 0xB5, kFLEXSPI_Command_DUMMY_SDR, kFLEXSPI_4PAD, 0x0), [4 * nor_cmd_lut_seq_idx_readstatusreg + 1] = flexspi_lut_seq(kFLEXSPI_Command_READ_SDR, kFLEXSPI_4PAD, 0x04, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0x0), /* 读取 ID */ [4 * nor_cmd_lut_seq_idx_readid] = flexspi_lut_seq(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x9E, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04),// modifica mia da 0x9F A 0X9E /* 写入启用 4 焊盘 */ [4 * nor_cmd_lut_seq_idx_writeenable_opi] = flexspi_lut_seq(kFLEXSPI_Command_SDR, kFLEXSPI_4PAD, 0x06, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0x00), /* 启用写入功能 */ [4 * nor_cmd_lut_seq_idx_writeenable] = flexspi_lut_seq(kFLEXSPI_Command_SDR, kFLEXSPI_4PAD, 0x06, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0), /* 擦除扇区 */ [4 * nor_cmd_lut_seq_idx_erasesector] = flexspi_lut_seq(kFLEXSPI_Command_SDR, kFLEXSPI_4PAD, 0x20, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_4PAD, 0x18), /* 程序 */ [4 * nor_cmd_lut_seq_idx_pageprogram_quad] = flexspi_lut_seq(kFLEXSPI_Command_SDR, kFLEXSPI_4PAD, 0x32, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_4PAD, 0x18), [4 * nor_cmd_lut_seq_idx_pageprogram_quad + 1] = flexspi_lut_seq(kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_4PAD, 0x01, kFLEXSPI_Command_STOP, kFLEXSPI_4PAD, 0), /* 进入四重模式 */ [4 * nor_cmd_lut_seq_idx_enablequad] = flexspi_lut_seq(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x35, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0x00), /* 虚拟写入,当 AHB 写入命令触发时,不执行任何操作。*/ [4 * nor_cmd_lut_seq_idx_write] = flexspi_lut_seq(kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0x0, kFLEXSPI_Command_STOP, kFLEXSPI_1PAD, 0x0), /* 使用 Qual SDR 读取功能读取状态寄存器 */ [4 * nor_cmd_lut_seq_idx_readstatus_opi] = flexspi_lut_seq(kFLEXSPI_Command_SDR, kFLEXSPI_4PAD, 0x05, kFLEXSPI_Command_READ_SDR, kFLEXSPI_4PAD, 0x02), }; int main(void) { uint32_t i = 0; status_t 状态; uint8_t 供应商 ID = 0; pcal6524_handle_t 句柄; /* 关闭 clang-format */ const clock_root_config_t lpi2cClkCfg ={ .时钟关闭 = false, .mux = 0,// 24MHz 振荡源 .分隔 = 1 }; /* clang-format on */ BOARD_ConfigMPU(); BOARD_InitBootPins(); BOARD_BootClockRUN(); BOARD_InitDebugConsole(); CLOCK_SetRootClock(BOARD_PCAL6524_I2C_CLOCK_ROOT, &lpi2cClkCfg); CLOCK_EnableClock(BOARD_PCAL6524_I2C_CLOCK_GATE); /* 为 M.2 或非闪存卡设置 3.3V */ BOARD_InitPCAL6524(&句柄); PCAL6524_SetDirection(&处理, (1 << BOARD_PCAL6524_EXT1_PWREN), kPCAL6524_Output); PCAL6524_SetPins(&处理, (1 << BOARD_PCAL6524_EXT1_PWREN)); flexspi_nor_flash_init(example_flexspi); PRINTF("\r\nFLEXSPI 示例启动!\r\n"); /* 获取供应商 ID。*/ 状态 = flexspi_nor_get_vendor_id(示例, &vendorID); 如果(status != kStatus_Success)     { 返回 状态;    } PRINTF("供应商 ID: 0x%x\("......")", vendorID); #if !(定义(xip_external_flash)) /* 擦除整个芯片 .*/ PRINTF("通过 FlexSPI 擦除整个芯片...\r\n"); 状态 = flexspi_nor_erase_chip(example_flexspi); 如果状态 !=kStatus_Success)     { 返回状态    } PRINTF("擦除完毕\r\n"); #endif /* 进入四重模式。*/ 状态 = flexspi_nor_enable_quad_mode(example_flexspi); 如果(status != kStatus_Success)     { 返回 状态;    } /* 擦除扇区。*/ PRINTF (" 通过 FlexSpi 擦除序列号 或非...\ r\n "); 状态 = flexspi_nor_flash_erase_sector(示例, 示例 * SECTOR_SIZE); 如果(status != kStatus_Success)     { PRINTF("擦除扇区失败 !\)"); 返回 -1;    } memset(s_nor_program_buffer, 0xFFU, ((s_nor_program_buffer)); DCACHE_InvalidateByRange(example_flexspi_amba_base + 示例 * ()()()()()(, flash_page_size); memcpy(s_nor_read_buffer, (void *)(example_flexspi_amba_base + 示例 * SECTOR_SIZE), ((s_nor_read_buffer)); 如果(memcmp(s_nor_program_buffer, s_nor_read_buffer, ((s_nor_program_buffer)))     { PRINTF("Erase data - read out data value incorrect !\r\n "); 返回 -1;    } 不然     { PRINTF("Erase data - successfully. \r\n");    } 为(i = 0; i < 0xFFU; i++)     { s_nor_program_buffer[i] = i;    } 状态 = flexspi_nor_flash_page_program(示例, 示例 * SECTOR_SIZE, (空格 *)s_nor_program_buffer); 如果(status != kStatus_Success)     { PRINTF("页面程序失败 !\r\n"); 返回 -1;    } DCACHE_InvalidateByRange(example_flexspi_amba_base + 示例 * ()()()()()(, flash_page_size); memcpy(s_nor_read_buffer, (void *)(example_flexspi_amba_base + 示例 * SECTOR_SIZE), ((s_nor_read_buffer)); 如果(memcmp(s_nor_read_buffer, s_nor_program_buffer, ((s_nor_program_buffer)) != 0)     { PRINTF("程序数据 - 读出数据值不正确 !\r\n "); 返回 -1;    } 不然     { PRINTF("程序数据 - 成功。 \r\n");    } 状态 = flexspi_nor_get_vendor_id(示例, &vendorID); 如果(status != kStatus_Success)     { 返回 状态;    } PRINTF("供应商 ID: 0x%x\("......")", vendorID); PRINTF("状态: %d\,......。", status); 虽然(1)     {    } } Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB 您好, 感谢您的测试,那么很可能是在执行 READ ID 时 LUT 序列不正确,请尝试对 LUT 进行以下更改: /* 读 ID */ [4 * NOR_CMD_LUT_SEQ_IDX_READID] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD,0x9E, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 0x04), 请尝试并告知我结果。 致以最崇高的敬意/问候, Aldo。 Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB 是的,我按照您的建议添加了这段代码: 遗憾的是,正如你所看到的,一切都没有改变: @AldoG你有其他想法吗? 谢谢! 鲍勃 Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB 您好, hw 上的一切看起来都很好,您能否尝试在数据编程后添加读取供应商 ID 的功能? 致以最崇高的敬意/问候, Aldo。 Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB 你好,阿尔多、 感谢您的回复。这些是连接 Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB 你好, 这可能是由于没有正确处理SPI内存上的RESET信号造成的,你能分享一下你是如何连接内存的吗? 如果您能提供一个小的原理图,那将会非常有帮助。 致以最崇高的敬意/问候, Aldo。
View full article
IMX93QSB の Flexspi_nor_polling_transfer SDKs の例におけるベンダー ID の問題 こんにちは、みんな、 imx93-qsb に似たカスタム ボードのペリフェラルをテストするために、VSCode 用の MCUXpresso を使用しています。SDK プロジェクト「flexspi_nor_polling_transfer」から始めて、例で使用されているチップMT25QU512ABB と非常によく似た NOR フラッシュ MT25QU01GBBB8E12 の機能をテストしたいと思います。 関数flexspi_nor_get_vendor_idでは0x20 ではなく 0xFF が返され、最後の操作は正常に完了します。         例と同じ SPI ペリフェラル (SD3 パッドの flexSPI1) を使用していますが、ID ベンダーを正しく読み取れない理由がわかりません。誰か助けてくれませんか? Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB ちなみに、拡張 SPI モードで IS25WX256 を使用する場合、Read ID コマンド 0x9E でも問題が発生します。コマンドは `FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x9e, kFLEXSPI_Command_READ_SDR, kFLEXSPI_1PAD, 4),` です。使用するたびに `0x888cadce` を読み取ります。 Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB こんにちは@AldoG 、 vendorID 値で何が起こっているかを理解するために、flexspi_nor_get_vendor_id 関数内に PRINTF コマンドをいくつか配置してみました。 出力は次のようになります。 また、flashXfer.seqIndex を 4 * NOR_CMD_LUT_SEQ_IDX_READID に変更してみましたが、出力は次のように変わりました。 関数内を何度も確認することが役に立つかどうかはわかりません。おそらく問題は seqIndex 値自体にあります。あなたの考えを聞かせてください。 よろしくお願いいたします。 ボブ Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB こんにちは、 私が推奨した追加事項からわかるように、あなたはまさにその例をそのまま使用しています。 メモリが正しく機能していないというよりは、ID を取得するための LUT コマンドが正しく機能していないのではないかと思います。そのため、正しく送信されているかどうかを確認できるかどうかを言及しました。 よろしくお願いいたします。 アルド。 Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB こんにちは、 次の UUU コマンドを使用して nor-flash をターゲットとするブートローダーを配置できたため、フラッシュ メモリが正常に動作していることはほぼ確実です。 uuu.exe -b qspi imx-boot-imx93-11x11-lpddr4x-evk-sd.bin-flash_singleboot FlexSPI Serial NOR でブート構成を設定すると、ブートローダが正しく実行されていることがわかります。しかし、なぜこのプロジェクトを MCUXpresso for VScode で使用すると問題が発生するのか、まだわかりません。 ご協力いただける場合はお知らせください。iMX93 の M33 コアでも作業する必要があります。 ありがとうございます ボブ Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB こんにちは、 共有していただきありがとうございます。注意深く確認させていただきます。 ところで、ハードウェア上の信号を確認する方法はありますか? よろしくお願いいたします。 アルド。 Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB こんにちは、アルドさん。 助けてくれてありがとう。残念ながら、この LUT の変更は解決策ではなく、ベンダー ID では依然として 0xff が読み取られます。C コード全体を皆さんと共有します。 /* * 著作権 (c) 2016、Freescale Semiconductor, Inc. * 著作権 2016-2018 NXP * 無断転載を禁じます。 * * * SPDXライセンス識別子: BSD-3条項 */  #include "pin_mux.h"  #include "clock_config.h"  #include "board.h"  #include "fsl_debug_console.h"  #include "fsl_rgpio.h"  #include "fsl_lpi2c.h"  #include "fsl_iomuxc.h"  #include "fsl_lpi2c.c" #include "fsl_flexspi.h" #include "app.h" #include "fsl_debug_console.h" #include "fsl_cache.h" #include "pin_mux.h" #include "clock_config.h" #include "board.h" #include "fsl_common.h" /**************************************************************************************** * 定義 **********************************************************************************/ /**************************************************************************************** * プロトタイプ **********************************************************************************/ /**************************************************************************************** * 変数 **********************************************************************************/ /* プログラムデータバッファは4バイトのアラインメントにする必要があります。これにより、このメモリ領域が次のように構成されているため、バスフォールトをCAN。 MPU によるデバイス メモリ。*/ SDK_ALIGN (静的uint8_t s_nor_program_buffer [ 256 ], 4 ); 静的uint8_t s_nor_read_buffer [ 256 ]; extern status_t flexspi_nor_flash_erase_sector ( FLEXSPI_Type *ベース、 uint32_tアドレス); extern status_t flexspi_nor_flash_page_program ( FLEXSPI_Type * base 、 uint32_t dstAddr 、 const uint32_t * src ); 外部status_t flexspi_nor_get_vendor_id ( FLEXSPI_Type *ベース、 uint8_t *ベンダーID ); 外部status_t flexspi_nor_enable_quad_mode ( FLEXSPI_Type *ベース); 外部status_t flexspi_nor_erase_chip ( FLEXSPI_Type *ベース); 外部void flexspi_nor_flash_init ( FLEXSPI_Type *ベース); /**************************************************************************************** * コード **********************************************************************************/ flexspi_device_config_tデバイス構成= { . flexspiRootClk       = 12000000 , //12 MHz、ノイズあたりOK .フラッシュサイズ            = FLASH_SIZE 、 . CS間隔単位       = kFLEXSPI_CsIntervalUnit1SckCycle 、 . CS間隔           = 2 、 .CSホールド時間           = 3 、 . CSセットアップ時間          = 3 、 .データ有効時間        = 0 、 .列スペース          = 0 、 . enableWordAddress    = 0 、 . AWRSeqIndex          = 0 、 . AWRシーケンス番号         = 0 、 . ARDSeqインデックス          = NOR_CMD_LUT_SEQ_IDX_READ 、 . ARDシーケンス番号         = 1 、 . AHBWriteWaitUnit     = kFLEXSPI_AhbWriteWaitUnit2AhbCycle 、 . AHBWriteWaitInterval = 0 , }; const uint32_t customLUT [ CUSTOM_LUT_LENGTH ] = { /* 高速読み取りクアッドモード -SDR */ [ 4 * NOR_CMD_LUT_SEQ_IDX_READ + 0 ] =         FLEXSPI_LUT_SEQ ( kFLEXSPI_Command_SDR 、 kFLEXSPI_4PAD 、 0xEB 、 kFLEXSPI_Command_RADDR_SDR 、 kFLEXSPI_4PAD 、 0x18 )、 [ 4 * NOR_CMD_LUT_SEQ_IDX_READ + 1 ] = FLEXSPI_LUT_SEQ (         kFLEXSPI_Command_DUMMY_SDR 、 kFLEXSPI_4PAD 、 0x0A 、 kFLEXSPI_Command_READ_SDR 、 kFLEXSPI_4PAD 、 0x04 )、 /* ステータスレジスタの読み取り */ [ 4 * NOR_CMD_LUT_SEQ_IDX_READSTATUSREG ] =         FLEXSPI_LUT_SEQ ( kFLEXSPI_Command_SDR 、 kFLEXSPI_4PAD 、 0xB5 、 kFLEXSPI_Command_DUMMY_SDR 、 kFLEXSPI_4PAD 、 0x0 )、 [ 4 * NOR_CMD_LUT_SEQ_IDX_READSTATUSREG + 1 ] =         FLEXSPI_LUT_SEQ ( kFLEXSPI_Command_READ_SDR 、 kFLEXSPI_4PAD 、 0x04 、 kFLEXSPI_Command_STOP 、 kFLEXSPI_1PAD 、 0x0 )、 /* ID を読み取る */ [ 4 * NOR_CMD_LUT_SEQ_IDX_READID ] =         FLEXSPI_LUT_SEQ ( kFLEXSPI_Command_SDR , kFLEXSPI_1PAD , 0x9E , kFLEXSPI_Command_READ_SDR , kFLEXSPI_1PAD , 0x04 ), // 0x9F から 0X9E に変更 /* 書き込み可能4パッド */ [ 4 * NOR_CMD_LUT_SEQ_IDX_WRITEENABLE_OPI ] =         FLEXSPI_LUT_SEQ ( kFLEXSPI_Command_SDR 、 kFLEXSPI_4PAD 、 0x06 、 kFLEXSPI_Command_STOP 、 kFLEXSPI_1PAD 、 0x00 )、 /* 書き込み許可 */ [ 4 * NOR_CMD_LUT_SEQ_IDX_WRITEENABLE ] =         FLEXSPI_LUT_SEQ ( kFLEXSPI_Command_SDR 、 kFLEXSPI_4PAD 、 0x06 、 kFLEXSPI_Command_STOP 、 kFLEXSPI_1PAD 、 0 )、 /* セクタ消去 */ [ 4 * NOR_CMD_LUT_SEQ_IDX_ERASESECTOR ] =         FLEXSPI_LUT_SEQ ( kFLEXSPI_Command_SDR 、 kFLEXSPI_4PAD 、 0x20 、 kFLEXSPI_Command_RADDR_SDR 、 kFLEXSPI_4PAD 、 0x18 )、 /* プログラム */ [ 4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_QUAD ] =         FLEXSPI_LUT_SEQ ( kFLEXSPI_Command_SDR 、 kFLEXSPI_4PAD 、 0x32 、 kFLEXSPI_Command_RADDR_SDR 、 kFLEXSPI_4PAD 、 0x18 )、 [ 4 * NOR_CMD_LUT_SEQ_IDX_PAGEPROGRAM_QUAD + 1 ] =         FLEXSPI_LUT_SEQ ( kFLEXSPI_Command_WRITE_SDR 、 kFLEXSPI_4PAD 、 0x01 、 kFLEXSPI_Command_STOP 、 kFLEXSPI_4PAD 、 0 )、 /* クアッドモードに入る */ [ 4 * NOR_CMD_LUT_SEQ_IDX_ENABLEQUAD ] =         FLEXSPI_LUT_SEQ ( kFLEXSPI_Command_SDR 、 kFLEXSPI_1PAD 、 0x35 、 kFLEXSPI_Command_STOP 、 kFLEXSPI_1PAD 、 0x00 )、 /* ダミー書き込み。AHB 書き込みコマンドがトリガーされたときには何もしません。*/ [ 4 * NOR_CMD_LUT_SEQ_IDX_WRITE ] =         FLEXSPI_LUT_SEQ ( kFLEXSPI_Command_STOP 、 kFLEXSPI_1PAD 、 0x0 、 kFLEXSPI_Command_STOP 、 kFLEXSPI_1PAD 、 0x0 )、 /* Qual SDR読み取りを使用してステータスレジスタを読み取る */ [ 4 * NOR_CMD_LUT_SEQ_IDX_READSTATUS_OPI ] =         FLEXSPI_LUT_SEQ ( kFLEXSPI_Command_SDR 、 kFLEXSPI_4PAD 、 0x05 、 kFLEXSPI_Command_READ_SDR 、 kFLEXSPI_4PAD 、 0x02 )、 }; int main ( void ) {     uint32_t i = 0 ;     status_tステータス;     uint8_tベンダーID = 0 ;     pcal6524_handle_tハンドル; /* clang-format オフ */     const clock_root_config_t lpi2cClkCfg = { .clockOff = false 、​ . mux = 0 , // 24MHz発振器ソース . div = 1 }; /* clang-format オン */     BOARD_ConfigMPU ();     BOARD_InitBootPins ();     BOARD_BootClockRUN ();     BOARD_InitDebugConsole ();     CLOCK_SetRootClock ( BOARD_PCAL6524_I2C_CLOCK_ROOT 、 & lpi2cClkCfg );     CLOCK_EnableClock ( BOARD_PCAL6524_I2C_CLOCK_GATE ); /* M.2 nor フラッシュカードに 3.3V を設定します */     BOARD_InitPCAL6524 ( &ハンドル);     PCAL6524_SetDirection ( &ハンドル, ( 1 << BOARD_PCAL6524_EXT1_PWREN ), kPCAL6524_Output );     PCAL6524_SetPins ( &ハンドル, ( 1 << BOARD_PCAL6524_EXT1_PWREN ));     flexspi_nor_flash_init ( EXAMPLE_FLEXSPI );     PRINTF ( " \r\n FLEXSPI の例を開始しました! \r\n " ); /* ベンダーIDを取得します。 */     ステータス= flexspi_nor_get_vendor_id ( EXAMPLE_FLEXSPI 、 & vendorID );     if (ステータス!= kStatus_Success )     {         ステータスを返します。    }     PRINTF ( "ベンダーID: 0x %x \r\n " , vendorID ); #if ! (定義済み( XIP_EXTERNAL_FLASH )) /* チップ全体を消去します。*/     PRINTF ( "FlexSPI 経由でチップ全体を消去しています... \r\n " ); ステータス= flexspi_nor_erase_chip (EXAMPLE_FLEXSPI);     if (ステータス!= kStatus_Success)     {         ステータスを返します。    }     PRINTF ( "消去が完了しました! \r\n " ); #endif /* クアッドモードに入ります。*/     ステータス= flexspi_nor_enable_quad_mode ( EXAMPLE_FLEXSPI );     if (ステータス!= kStatus_Success )     {         ステータスを返します。    } /* セクタを消去します。*/     PRINTF ( "FlexSPI 経由のシリアル NOR を消去しています... \r\n " );     ステータス= flexspi_nor_flash_erase_sector ( EXAMPLE_FLEXSPI 、 EXAMPLE_SECTOR * SECTOR_SIZE );     if (ステータス!= kStatus_Success )     {         PRINTF ( "セクター消去失敗! \r\n " );         - 1を返します。    }     memset ( s_nor_program_buffer 、 0xFFU 、 sizeof ( s_nor_program_buffer ));     DCACHE_InvalidateByRange ( EXAMPLE_FLEXSPI_AMBA_BASE + EXAMPLE_SECTOR * SECTOR_SIZE 、 FLASH_PAGE_SIZE );     memcpy ( s_nor_read_buffer , ( void * )( EXAMPLE_FLEXSPI_AMBA_BASE + EXAMPLE_SECTOR * SECTOR_SIZE ),            sizeof ( s_nor_read_buffer ));     memcmp ()の場合、 s_nor_program_buffer 、 s_nor_read_buffer 、 sizeof ( )の場合、 s_nor_program_bufferは、次のようになります。     {         PRINTF ( "データを消去 - 読み取ったデータ値が正しくありません! \r\n " );         - 1を返します。    }     それ以外     {         PRINTF ( "データの消去 - 正常に完了しました。 \r\n " );    }     ( i = 0 ; i < 0xFFU ; i ++ )の場合     {         s_nor_program_buffer [ i ] = i ;    }     ステータス=         flexspi_nor_flash_page_program ( EXAMPLE_FLEXSPI 、 EXAMPLE_SECTOR * SECTOR_SIZE 、 ( void * ) s_nor_program_buffer );     if (ステータス!= kStatus_Success )     {         PRINTF ( "ページ プログラム エラー! \r\n " );         - 1を返します。    }     DCACHE_InvalidateByRange ( EXAMPLE_FLEXSPI_AMBA_BASE + EXAMPLE_SECTOR * SECTOR_SIZE 、 FLASH_PAGE_SIZE );     memcpy ( s_nor_read_buffer , ( void * )( EXAMPLE_FLEXSPI_AMBA_BASE + EXAMPLE_SECTOR * SECTOR_SIZE ),            sizeof ( s_nor_read_buffer ));     memcmp ( s_nor_read_buffer 、 s_nor_program_buffer 、 sizeof ( s_nor_program_buffer ) ) != 0の場合     {         PRINTF ( "プログラムデータ - 読み取ったデータ値が正しくありません! \r\n " );         - 1を返します。    }     それ以外     {         PRINTF ( "プログラムデータ - 正常に実行されました。 \r\n " );    }     ステータス= flexspi_nor_get_vendor_id ( EXAMPLE_FLEXSPI 、 & vendorID );     if (ステータス!= kStatus_Success )     {         ステータスを返します。    }     PRINTF ( "ベンダーID: 0x %x \r\n " , vendorID );     PRINTF ( "ステータス: %d \r\n " , status );     一方( 1 )     {    } } Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB こんにちは、 テストしていただきありがとうございます。READ ID の実行時に LUT シーケンスが正しくない可能性が最も高いため、LUT で次の変更を試してください。 /* ID を読み取る */ [4 * NOR_CMD_LUT_SEQ_IDX_READID] = FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR、kFLEXSPI_1PAD、 0x9E 、kFLEXSPI_Command_READ_SDR、kFLEXSPI_1PAD、0x04)、 ぜひお試しいただき、結果を教えてください。 よろしくお願いいたします。 アルド。 Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB はい、ご提案どおりに次のコードを追加しました: 残念ながら、CANのとおり何も変わっていません。 @AldoG他にアイデアはありますか? ありがとうございます ボブ Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB こんにちは、 ハードウェアはすべて正常に見えますが、データがプログラムされた後にベンダー ID を読み取る機能を追加していただけますか? よろしくお願いいたします。 アルド。 Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB こんにちは、アルドさん。 ご返信ありがとうございます。これらは接続です Re: Vendor ID issue in Flexspi_nor_polling_transfer SDK example for IMX93QSB こんにちは、 これは、SPI メモリ上でリセット信号が正しく処理されていないことが原因で発生する可能性があります。メモリをどのように接続しているか教えていただけますか? 小さな回路図を共有していただければ、本当に助かります。 よろしくお願いいたします。 アルド。
View full article
[RW612] デュアルアンテナスループット こんにちは、 現在、RW612 を使用して開発しており、Wi-Fi と BLE が同時に動作する機能に取り組んでいます。 このシステムは、Wi-Fi と BLE に別々のアンテナを備えたデュアルアンテナ構成を使用します。 以下は、MCUXpresso IDE で現在使用されている SDK の詳細です。 * SDK名: SDK_2.x_FRDM-RW612 * SDKバージョン: 24.12.00 * マニフェストバージョン: 3.15.0 テスト中に、2.4GHz 帯域の Wi-Fi に接続し、同時に BLE 操作を実行すると、Wi-Fi のスループットが大幅に低下することがわかりました。 一方、5GHz帯は目立った劣化もなく安定して動作します。 ただし、私たちのユースCASEでは 2.4GHz 動作も必要なので、この問題に対処する必要があります。 調査中に、「AN14121: RW61x の共存の概要」という文書を見つけました。質問させてください。私たちのようなデュアルアンテナ設定では、特別に PTA (Priority Traffic Arbiter) 設定を別々に構成する必要があるのでしょうか? さらに、FRDM-RW612 SDK で提供される Wi-Fi および BLE ファームウェア (rw61x_sb_wifi_a2.bin および rw61x_sb_ble_a2.bin) は、シングルアンテナ構成用に設計されているようです。デュアルアンテナ設定用に別のファームウェアバージョンはありますか?もしSOなら、それを入手することは可能でしょうか? ありがとう。 Re: [RW612] Dual Antenna Throughput こんにちは@hclee 共存はデフォルトで有効になっているため、構成する必要はありません。BT と 2.4G Wi-Fi が同時に動作すると、2.4G Wi-Fi と BT の中断を回避するためにスループットが低下します。 ただし、coex に関するデモを提供しており、SDKs で参照できます: \middleware\wireless\coex\build_coex.sh このシェルをビルドし、J-Link を使用してボードにフラッシュします。 よろしくお願いいたします。 ショーン 機密文書を入手するには NDA が必要です。 Re: [RW612] Dual Antenna Throughput こんにちは、 @shaun_wu 現在、デュアルアンテナで構成されたカスタムボードを使用しています。 私たちのアプリケーションでは、Wi-Fi 経由でサーバーからデータをストリーミングしながら、同時に BLE 経由でデータを送信します。 テスト中に、ダウンロードに 2.4GHz Wi-Fi 帯域を使用し、送信に BLE を使用すると、Wi-Fi スループットが著しく低下することが確認されました。 当社のボードではデュアルアンテナ設定を使用しているため、このシナリオで共存メカニズムを適切に有効にするために必要な特定の構成手順があるかどうかをお尋ねしたいと思います。 提供されたリンクにアクセスしようとしましたが、次のメッセージが表示されました: 「あなたのユーザーIDにはダウンロードを続行するための十分な権限がありません。」 コンテンツを表示またはダウンロードするために必要な権限がないようです。 よろしくお願いします ヘクリー Re: [RW612] Dual Antenna Throughput こんにちは@hclee FRDM ボードは 1 つのアンテナ構成のみをサポートしています。カスタム ボードを使用していますか? 調査中に、「AN14121: RW61x の共存の概要」という文書を見つけました。質問させてください。私たちのようなデュアルアンテナ設定では、特別に PTA (Priority Traffic Arbiter) 設定を別々に構成する必要があるのでしょうか? --> Wi-Fi 2.4G と BT の中断を回避するために共存メカニズムは使用できません。 さらに、FRDM-RW612 SDK で提供される Wi-Fi および BLE ファームウェア (rw61x_sb_wifi_a2.bin および rw61x_sb_ble_a2.bin) は、シングルアンテナ構成用に設計されているようです。デュアルアンテナ設定用に別のファームウェアバージョンはありますか?もしSOなら、それを入手することは可能でしょうか? --> frdm ボードのハードウェアはデュアル アンテナをサポートしていません。evk 設計を参照できます。当社はデュアル アンテナの設計と構成を提供します。https://www.nxp.com/webapp/Download?colCode=RD-RW61X-BGA-IPA-2A-V4&appType=license よろしくお願いいたします。 ショーン よろしくお願いいたします。 ショーン
View full article
[S32K144 EVB] 多个信号集中在一个引脚上 参考您的文档: [J2-19] 和 [J2-17] 的引脚同时为信号 [PTE10]&[ PTA3] 和 [PTE11]&[PTA2] 定义。 现在,我必须同时使用 [PTA2]、[PTA3]、[PTE10] 和 [PTE11] 端口。 我如何知道 [J2-19] 引脚的信号是 [PTE10] 还是 [PTA3]? J2-17] 引脚的信号是 [PTE11] 还是 [PTA2]? Re: [S32K144 EVB] Multiple signals concentrated on one pin Hi@CY9 您需要查看原理图来了解一切。 "DNP"->不填充
View full article
访问 DCP 寄存器导致 i.MX6 处理器崩溃,怀疑存在硬件设计缺陷?寻求帮助 我在使用 i.MX6 处理器时遇到了一个关键问题,希望得到社区的帮助。在我们生产的一批电路板中,大约20%的样本在访问DCP寄存器后导致处理器崩溃。以下是详细的背景和信息:     # 问题描述 生产了一批电路板,发现20%的样品表现出相同的缺陷。 当代码尝试访问 DCP 寄存器(地址 0x02284000)时,处理器完全崩溃,甚至 JTAG 调试器也无法再访问内核。JTAG 报告错误: "错误:数据在 0x02284000 终止,dfsr = 0x00000008"。 一旦发生此错误,处理器将无法继续执行(即使输入"c" 继续执行)。 3 号和 6 号板有缺陷。暂时观察到,与其他板相比,这些板上的 VDD_SNVS_IN 电压略高。   Error data abort错误数据中止 can access可以访问 # 硬件环境 我不确定电路电压点设计是否存在差异,所以我测量了故障电路板与其他板之间的电压差。 -处理器:i.MX6ULL (MCIMX6Y2) - 故障板编号:3 号和 5 号(故障率约 20%) - 普通板数量:剩余的 80% 的板     # 代码复制 以下代码用于重现该问题。如果未注释 DCP 访问部分,则 LED 停止闪烁(处理器崩溃): 通过 JTAG 手动访问 DCP 也会触发信号错误:   >>> set $R = 0x2284000 >>> p/x *$R     #include "MCIMX6Y2.h" #include "fsl_iomuxc.h" #include "pad_config.h" #define LED_PAD_CONFIG_DATA 0x13008 int main() { CCM_CCGR1_CG13(0x3); CCM_CCGR3_CG6(0x3); IOMUXC_SetPinMux(RGB_RED_LED_IOMUXC,0); IOMUXC_SetPinConfig(RGB_RED_LED_IOMUXC, LED_PAD_CONFIG_DATA); GPIO1->GDIR |= (1<<4); GPIO1->DR |= (1<<4); while(1) { GPIO1->DR &= ~(1<<4); // led on delay(0xFFFFF); GPIO1->DR |= (1<<4); // led off delay(0xFFFFF); #if 0 // Turn on the code, MCU will be crash int *ptr = 0x2284000; // This is DCP address UART1_PrintHex32(*(ptr)); #endif } return 0; }   # 其他调查结果 - 访问 0x2284000 时,普通板返回 0x10000281(如预期)。 -根据手册 IMX6ULLRM.pdf,我们测试了所有其他外设寄存器,没有一个触发信号数据中止。该问题仅限于 DCP 区域。   well (ADC1_HC0) set $R = 0x2198000 p/x *$R well (AIPSTZ1_MPR) set $R = 0x207C000 p/x *$R ...... well (TEMPMON_TEMPSENSE0) set $R = 0x20C8180 p/x *$R well (TSC_BASIC_SETTING) set $R = 0x2040000 p/x *$R 请求帮助 -DCP 与时钟树之间的关系:DCP 模块依赖哪些时钟?是否需要任何特殊的时钟配置? -硬件设计缺陷:VDD_SNVS_IN 电压稍高可能是原因吗?是否还有其他电压或信号需要检查? -软件配置:是否有任何特殊的 DCP 初始化步骤或保护机制? -JTAG 调试:是否有办法在 DCP 访问失败后恢复 JTAG 连接?     Re: Accessing DCP Register Causes i.MX6 Processor Crash, Suspected Hardware Design Defect? Seeking H 您是否遵循了我们指南中的需求: Re: Accessing DCP Register Causes i.MX6 Processor Crash, Suspected Hardware Design Defect? Seeking H 1. 时序上满足的,2MS。 2. 采用纽扣电池供电,依旧在访问DCP寄存器后Crash Re: Accessing DCP Register Causes i.MX6 Processor Crash, Suspected Hardware Design Defect? Seeking H 1.IMX6ULLIEC.pdf 表 10 工作范围描述 VDD_SNVS_IN,工作范围在 2.8~3.6V。 典型 3.0V。 2.但是手册并未说明,提前多长时间? 原理图设计上,vdd_snvs_in 的确比vdd_high_in 和vdd_soc_in 先上电。 示波器观察的确如此,大约提前 1ms,是否足够? 是否因上电时序引起状态不一致,下面的实验很好验证。     电源树 3.的确总共做了 10 套板子,2 块存在相同故障。 4.板子跑uboot+linux卡死。 uboot/arch/arm/mach-imx/mx6/soc.c 试图从 DCP 模块获取随机数作为序列号时,SOC Crash。 于是尝试编写裸机LED程序,在代码里读写DCP寄存器,同样崩溃 int arch_misc_init(void) { if (IS_ENABLED(CONFIG_FSL_DCP_RNG)) { struct udevice *dev; int ret; ret = uclass_get_device_by_driver(UCLASS_RNG, DM_DRIVER_GET(dcp_rng), &dev); if (ret) printf("Failed to initialize dcp rng: %d\n", ret); } setup_serial_number(); return 0; } 接下来的尝试: 1.将所有板子时序一同测试时序是否一致,测试vdd_snvs_in 究竟有多少抖动。 2.板子接入纽扣电池 3.0v,保证 vdd_snvs_in一定处于最先上电,避免时序影响。 完成上述之后再回帖 Re: Accessing DCP Register Causes i.MX6 Processor Crash, Suspected Hardware Design Defect? Seeking H VDD_SNVS_IN这个电源一般要求为3.0V,设计电路板时,这个电源需要第一个输出出来,给到CPU 的 P12 引脚(VDD_SNVS_IN 脚)。你这里也是符合要求的这里。 还有在手册里你也可以看到 If VDD_SNVS_IN is directly supplied by a coin cell, a schottky diode is required between VDD_HIGH_IN and VDD_SNVS_IN 你这里的设计都符合要求吗?还有,你这里总共做了10块板子, 有两块是不好使的? 你板子上跑的是什么软件?
View full article
I2C 快速模式上升/下降时间下限 I2C 标准 (UM10204) 规定了快速模式下上升/下降时间的下限。 这是否是为了管理欠调和防止 EMS? 如果不是这些问题,是否就没有必要遵守下限? 这是另一家处理 I2C 的制造商的意见。 Re: I2C Fast Mode Rise/Fall Time Lower Limit 你好,托马斯、 感谢您的快速回复。 这很有帮助。 然而,既然如此,为什么快速模式增强版的上升时间更快,却没有最短限制呢? Re: I2C Fast Mode Rise/Fall Time Lower Limit Hi Keitaro、 定义下限不仅是为了管理电磁敏感度和下冲,也是为了确保符合I²C的设备之间强大的信号完整性和互操作性。 以下是制定这一规范的主要原因: - 信号完整性:过快的转换会导致反射、振铃和时序违规,尤其是在具有较长迹线或较高电容的系统中。下限有助于保持通信稳定。 - EMS 和欠冲:快速边缘会增加高频辐射,并可能因电感效应导致欠冲。时间限制有助于降低这些风险。 -设备兼容性:I²C 总线专为多设备、多供应商环境而设计。遵守定时规格可确保在所有兼容设备上可靠运行。 虽然在不担心 EMS 和欠冲的受控环境中,在下限之外运行在技术上是可行的,但这样做意味着偏离 I²C 标准。这可能会影响兼容性和长期可靠性。 总之,即使 EMS 和欠调不是直接问题,我也建议遵守规定的时序限制,以保持合规性并确保性能的一致性。 BRs, Tomas
View full article
一部のUdiskがMCIMX6ULL-EVK評価ボードで列挙に失敗する 128GB と 64GB の 2 つの Udisk があります。これら 2 つは両方とも MX8MP-EVK 評価ボードで列挙できます。MCIMX6ULL-EVK 評価ボードでは 64GB を列挙できますが、64GB は列挙できません。 MCIMX6ULL-EVK 評価ボードの NXP デモ ファームウェア L4.1.15_2.0.0 と L5.4.24-2.1.0_images_MX6UL7D の両方でこの問題を再現できます。 以下は、MCIMX6ULL-EVK 評価ボードのテスト ログです。 NXP i.MX リリース ディストリビューション 5.4-zeus imx6ul7d ttymxc0 imx6ul7d ログイン: root 最終ログイン: 2020年5月28日(木) 16:05:12 UTC、tty7 ルート@imx6ul7d:~# ルート@imx6ul7d:~# root@imx6ul7d:~# 64GBのudiskを試すが、いつも失敗する -sh: 変更: コマンドが見つかりません ルート@imx6ul7d:~# ルート@imx6ul7d:~# root@imx6ul7d:~# [ 33.127440] VSD_3V3: 無効化 [ 33.130571] CAN-3v3: 無効化 [ 33.977402] usb 1-1: ci_hdrc を使用した新しい高速 USB デバイス番号 2 [ 34.030526] usb 1-1: 新しいUSBデバイスが見つかりました、idVendor=346d、idProduct=5678、bcdDevice= 3.20 [ 34.038928] usb 1-1: 新しいUSBデバイス文字列: Mfr=1、製品=2、SerialNumber=3 [ 34.046215] usb 1-1: 製品: ディスク 20 [ 34.056993] usb 1-1: メーカー: USB [ 34.064009] usb 1-1: シリアル番号: FC31114725D35 [ 34.081397] usb-storage 1-1:1.0: USBマスストレージデバイスが検出されました [ 34.105046] SCSIホスト0: USBストレージ1-1:1.0 [ 35.129674] scsi 0:0:0:0: ダイレクトアクセス ベンダー C 製品コード 3.20 PQ: 0 ANSI: 4 [ 35.154632] sd 0:0:0:0: [sda] 122880000 512バイトの論理ブロック: (62.9 GB/58.6 GiB) [ 35.170574] sd 0:0:0:0: [sda] 書き込み保護はオフです [ 35.190603] sd 0:0:0:0: [sda] キャッシュモードページが見つかりません [ 35.195948] sd 0:0:0:0: [sda] ドライブキャッシュを想定: ライトスルー [ 35.236559] sda: sda1 [ 35.252883] sd 0:0:0:0: [sda] SCSIリムーバブルディスクが接続されました [ 35.273942] usb 1-1: USB切断、デバイス番号2 [ 35.284399] sd 0:0:0:0: [sda] タグ#0 失敗 結果: ホストバイト=DID_ERROR ドライバーバイト=DRIVER_OK [ 35.292811] sd 0:0:0:0: [sda] タグ#0 CDB: 読み取り(10) 28 00 07 52 ff 80 00 00 08 00 [ 35.300184] blk_update_request: I/Oエラー、デバイスSDA、セクター122879872 op 0x0:(READ) フラグ0x80700 phys_seg 1 prioクラス0 [ 35.320469] scsi 0:0:0:0: [sda] tag#0 失敗 結果: ホストバイト=DID_ERROR ドライバーバイト=DRIVER_OK [ 35.329034] scsi 0:0:0:0: [sda] タグ#0 CDB: 読み取り(10) 28 00 07 52 ff 80 00 00 08 00 [ 35.336534] blk_update_request: I/Oエラー、デバイスSDA、セクター122879872 op 0x0:(READ) フラグ0x0 phys_seg 1 prioクラス0 [ 35.347154] デバイスSDAのバッファI/Oエラー、論理ブロック15359984、非同期ページ読み取り [ 35.727532] usb 1-1: ci_hdrc を使用した新しい高速 USB デバイス番号 3 [ 46.307351] USB 1-1: デバイスがアドレス3を受け入れません、エラー -110 [ 46.457428] usb 1-1: ci_hdrc を使用した新しい高速 USB デバイス番号 4 [ 51.967329] USB 1-1: デバイスがアドレス4を受け入れません、エラー -71 [ 51.973421] usb usb1-port1: 電源を入れ直す [ 52.467402] usb 1-1: ci_hdrc を使用した新しい高速 USB デバイス番号 5 [ 52.637376] USB 1-1: デバイス応答なし、デバイスディスクリプタ読み取り/64、エラー -71 [ 57.927378] USB 1-1: デバイス応答なし、デバイスディスクリプタ読み取り/64、エラー -71 [ 58.197409] usb 1-1: ci_hdrc を使用した新しい高速 USB デバイス番号 6 [ 58.367365] USB 1-1: デバイス応答なし、デバイスディスクリプタ読み取り/64、エラー -71 [ 63.687362] USB 1-1: デバイス応答なし、デバイスディスクリプタ読み取り/64、エラー -71 [ 63.807378] usb usb1-port1: USBデバイスを列挙できません ルート@imx6ul7d:~# ルート@imx6ul7d:~# ルート@imx6ul7d:~# ルート@imx6ul7d:~# root@imx6ul7d:~# [ 76.317394] usb 1-1: ci_hdrc を使用して新しい高速USBデバイス番号7を作成しました [ 76.370177] usb 1-1: 新しいUSBデバイスが見つかりました、idVendor=346d、idProduct=5678、bcdDevice= 3.20 [ 76.378577] usb 1-1: 新しいUSBデバイス文字列: Mfr=1、製品=2、SerialNumber=3 [ 76.385854] usb 1-1: 製品: ディスク 20 [ 76.397014] usb 1-1: メーカー: USB [ 76.403918] usb 1-1: シリアル番号: FC31114725D35 [ 76.422972] usb-storage 1-1:1.0: USBマスストレージデバイスが検出されました [ 76.445697] SCSIホスト0: USBストレージ1-1:1.0 [ 77.529821] scsi 0:0:0:0: ダイレクトアクセス ベンダー C 製品コード 3.20 PQ: 0 ANSI: 4 [ 77.554400] sd 0:0:0:0: [sda] 122880000 512バイトの論理ブロック: (62.9 GB/58.6 GiB) [ 77.570541] sd 0:0:0:0: [sda] 書き込み保護はオフです [ 77.587488] sd 0:0:0:0: [sda] キャッシュモードページが見つかりません [ 77.592898] sd 0:0:0:0: [sda] ドライブキャッシュを想定: ライトスルー [ 77.648590] sda: sda1 [ 77.662782] sd 0:0:0:0: [sda] SCSIリムーバブルディスクが接続されました [ 77.683719] usb 1-1: USB切断、デバイス番号7 [ 77.694214] sd 0:0:0:0: [sda] タグ#0 失敗 結果: ホストバイト=DID_ERROR ドライバーバイト=DRIVER_OK [ 77.702615] sd 0:0:0:0: [sda] タグ#0 CDB: 読み取り(10) 28 00 07 52 ff 80 00 00 08 00 [ 77.709992] blk_update_request: I/Oエラー、デバイスSDA、セクター122879872 op 0x0:(READ) フラグ0x80700 phys_seg 1 prioクラス0 [ 77.730370] scsi 0:0:0:0: [sda] tag#0 失敗 結果: ホストバイト=DID_ERROR ドライバーバイト=DRIVER_OK [ 77.738932] scsi 0:0:0:0: [sda] タグ#0 CDB: 読み取り(10) 28 00 07 52 ff 80 00 00 08 00 [ 77.746434] blk_update_request: I/Oエラー、デバイスSDA、セクター122879872 op 0x0:(READ) フラグ0x0 phys_seg 1 prioクラス0 [ 77.757035] デバイスSDAのバッファI/Oエラー、論理ブロック15359984、非同期ページ読み取り [ 78.147306] usb 1-1: ci_hdrc を使用した新しい高速 USB デバイス番号 8 [ 86.837348] USB 1-1: デバイスがアドレス8を受け入れません、エラー -71 [ 87.947309] usb 1-1: ci_hdrc を使用した新しい高速 USB デバイス番号 9 [ 88.397411] USB 1-1: デバイスがアドレス9を受け入れません、エラー -71 [ 88.403501] usb usb1-port1: 電源を入れ直す ルート@imx6ul7d:~# ルート@imx6ul7d:~# ルート@imx6ul7d:~# ルート@imx6ul7d:~# ルート@imx6ul7d:~# ルート@imx6ul7d:~# ルート@imx6ul7d:~# root@imx6ul7d:~# 128GB udisk を変更すると、常に成功します -sh: 変更: コマンドが見つかりません ルート@imx6ul7d:~# ルート@imx6ul7d:~# ルート@imx6ul7d:~# root@imx6ul7d:~# [ 134.957400] usb 1-1: ci_hdrc を使用して新しい高速USBデバイス番号11を作成しました [ 135.010205] usb 1-1: 新しいUSBデバイスが見つかりました、idVendor=346d、idProduct=5678、bcdDevice= 3.20 [ 135.018605] usb 1-1: 新しいUSBデバイス文字列: Mfr=1、製品=2、SerialNumber=3 [ 135.025887] usb 1-1: 製品: ディスク 20 [ 135.037000] usb 1-1: メーカー: USB [ 135.043977] usb 1-1: シリアル番号: FC2900B1485C4 [ 135.062849] usb-storage 1-1:1.0: USBマスストレージデバイスが検出されました [ 135.085469] SCSIホスト0: USBストレージ1-1:1.0 [ 136.169604] scsi 0:0:0:0: ダイレクト アクセス ベンダー C 製品コード 3.20 PQ: 0 ANSI: 4 [ 136.194433] sd 0:0:0:0: [sda] 245760000 512バイトの論理ブロック: (126 GB/117 GiB) [ 136.210578] sd 0:0:0:0: [sda] 書き込み保護はオフです [ 136.227848] sd 0:0:0:0: [sda] キャッシュモードページが見つかりません [ 136.233272] sd 0:0:0:0: [sda] ドライブキャッシュを想定: ライトスルー [ 136.289093] sda: sda1 [ 136.310555] sd 0:0:0:0: [sda] SCSIリムーバブルディスクが接続されました [ 138.115645] EXT4-fs (sda1): 順序付きデータモードでマウントされたファイルシステム。オプション: (null) ルート@imx6ul7d:~# ルート@imx6ul7d:~# ルート@imx6ul7d:~# ルート@imx6ul7d:~# df ファイルシステム 1Kブロック 使用済み 使用可能 使用率 マウント先 /dev/root 1215192 746488 387904 66% / devtmpfs 168088 4 168084 1% /dev tmpfs 250520 0 250520 0% /dev/shm tmpfs 250520 8972 241548 4% /run tmpfs 250520 0 250520 0% /sys/fs/cgroup tmpfs 250520 4 250516 1% /tmp tmpfs 250520 148 250372 1% /var/volatile /dev/mmcblk1p1 27130 10722 16408 40% /run/media/mmcblk1p1 tmpfs 50104 4 50100 1% /run/media/ユーザー/0 /dev/sda1 120819424 61452 114597592 1% /run/media/sda1 root@imx6ul7d:~# [ 161.140099] usb 1-1: USB切断、デバイス番号11 [ 164.677402] usb 1-1: ci_hdrc を使用して新しい高速USBデバイス番号12を作成しました [ 164.730130] usb 1-1: 新しいUSBデバイスが見つかりました、idVendor=346d、idProduct=5678、bcdDevice= 3.20 [ 164.738530] usb 1-1: 新しいUSBデバイス文字列: Mfr=1、製品=2、SerialNumber=3 [ 164.745816] usb 1-1: 製品: ディスク 20 [ 164.756858] usb 1-1: メーカー: USB [ 164.763932] usb 1-1: シリアル番号: FC2900B1485C4 [ 164.790406] usb-storage 1-1:1.0: USBマスストレージデバイスが検出されました [ 164.822090] SCSIホスト0: USBストレージ1-1:1.0 [ 165.849535] scsi 0:0:0:0: ダイレクト アクセス ベンダー C 製品コード 3.20 PQ: 0 ANSI: 4 [ 165.874608] sd 0:0:0:0: [sda] 245760000 512バイトの論理ブロック: (126 GB/117 GiB) [ 165.887981] sd 0:0:0:0: [sda] 書き込み保護はオフです [ 165.907494] sd 0:0:0:0: [sda] キャッシュモードページが見つかりません [ 165.912845] sd 0:0:0:0: [sda] ドライブキャッシュを想定: ライトスルー [ 165.958829] sda: sda1 [ 165.979338] sd 0:0:0:0: [sda] SCSIリムーバブルディスクが接続されました [ 167.820051] EXT4-fs (sda1): 順序付きデータモードでマウントされたファイルシステム。オプション: (null) ルート@imx6ul7d:~# ルート@imx6ul7d:~# root@imx6ul7d:~# [ 178.797249] usb 1-1: USB切断、デバイス番号12 ルート@imx6ul7d:~# ルート@imx6ul7d:~# ルート@imx6ul7d:~# ルート@imx6ul7d:~# root@imx6ul7d:~# 64GB udisk を再試行するが、常に失敗する -sh: 変更: コマンドが見つかりません ルート@imx6ul7d:~# ルート@imx6ul7d:~# root@imx6ul7d:~# [ 206.277395] usb 1-1: ci_hdrc を使用して新しい高速USBデバイス番号13を作成しました [ 206.330256] usb 1-1: 新しいUSBデバイスが見つかりました、idVendor=346d、idProduct=5678、bcdDevice= 3.20 [ 206.338667] usb 1-1: 新しいUSBデバイス文字列: Mfr=1、製品=2、SerialNumber=3 [ 206.345948] usb 1-1: 製品: ディスク 20 [ 206.356882] usb 1-1: メーカー: USB [ 206.363925] usb 1-1: シリアル番号: FC31114725D35 [ 206.381244] usb-storage 1-1:1.0: USBマスストレージデバイスが検出されました [ 206.403761] scsi ホスト0: usb-storage 1-1:1.0 [ 207.449663] scsi 0:0:0:0: ダイレクトアクセス ベンダー C 製品コード 3.20 PQ: 0 ANSI: 4 [ 207.474740] sd 0:0:0:0: [sda] 122880000 512バイトの論理ブロック: (62.9 GB/58.6 GiB) [ 207.487973] sd 0:0:0:0: [sda] 書き込み保護はオフです [ 207.510688] sd 0:0:0:0: [sda] キャッシュモードページが見つかりません [ 207.516111] sd 0:0:0:0: [sda] ドライブキャッシュを想定: ライトスルー [ 207.558710] sda: sda1 [ 207.579364] sd 0:0:0:0: [sda] SCSIリムーバブルディスクが接続されました [ 207.596929] usb 1-1: USB切断、デバイス番号13 [ 207.602671] sd 0:0:0:0: [sda] タグ#0 失敗 結果: ホストバイト=DID_ERROR ドライバーバイト=DRIVER_OK [ 207.611076] sd 0:0:0:0: [sda] タグ#0 CDB: 読み取り(10) 28 00 07 52 ff 80 00 00 08 00 [ 207.618463] blk_update_request: I/Oエラー、デバイスSDA、セクター122879872 op 0x0:(READ) フラグ0x80700 phys_seg 1 prioクラス0 [ 207.643260] scsi 0:0:0:0: [sda] tag#0 失敗 結果: ホストバイト=DID_ERROR ドライバーバイト=DRIVER_OK [ 207.651824] scsi 0:0:0:0: [sda] タグ#0 CDB: 読み取り(10) 28 00 07 52 ff 80 00 00 08 00 [ 207.659379] blk_update_request: I/Oエラー、デバイスSDA、セクター122879872 op 0x0:(READ) フラグ0x0 phys_seg 1 prioクラス0 [ 207.669949] デバイスSDAのバッファI/Oエラー、論理ブロック15359984、非同期ページ読み取り [ 208.067342] usb 1-1: ci_hdrc を使用した新しい高速 USB デバイス番号 14 ルート@imx6ul7d:~# ルート@imx6ul7d:~# ルート@imx6ul7d:~# root@imx6ul7d:~# [ 218.627329] usb 1-1: デバイスがアドレス14を受け入れません、エラー -110 [ 218.777517] usb 1-1: ci_hdrc を使用した新しい高速 USB デバイス番号 15 [ 224.287335] USB 1-1: デバイスがアドレス15を受け入れません、エラー -71 [ 224.293525] usb usb1-port1: 電源を入れ直してみる [ 224.787394] usb 1-1: ci_hdrc を使用した新しい高速 USB デバイス番号 16 [ 224.957376] USB 1-1: デバイス応答なし、デバイスディスクリプタ読み取り/64、エラー -71 [ 230.247424] USB 1-1: デバイス応答なし、デバイスディスクリプタ読み取り/64、エラー -71 [ 230.517415] usb 1-1: ci_hdrc を使用した新しい高速 USB デバイス番号 17 [ 230.687412] USB 1-1: デバイス応答なし、デバイスディスクリプタ読み取り/64、エラー -71 [ 236.007405] USB 1-1: デバイス応答なし、デバイスディスクリプタ読み取り/64、エラー -71 [ 236.127474] usb usb1-port1: USBデバイスを列挙できません ルート@imx6ul7d:~# ルート@imx6ul7d:~# ルート@imx6ul7d:~# root@imx6ul7d:~# [ 1177.397394] usb 1-1: ci_hdrc を使用して新しい高速USBデバイス番号18を作成しました [ 1177.450285] usb 1-1: 新しいUSBデバイスが見つかりました、idVendor=346d、idProduct=5678、bcdDevice= 3.20 [ 1177.458688] usb 1-1: 新しいUSBデバイス文字列: Mfr=1、製品=2、SerialNumber=3 [ 1177.465961] usb 1-1: 製品: ディスク 20 [ 1177.476789] usb 1-1: メーカー: USB [ 1177.483826] usb 1-1: シリアル番号: FC31114725D35 [ 1177.503847] usb-storage 1-1:1.0: USBマスストレージデバイスが検出されました [ 1177.525431] SCSIホスト0: USBストレージ1-1:1.0 [ 1178.569560] scsi 0:0:0:0: ダイレクトアクセス ベンダー C 製品コード 3.20 PQ: 0 ANSI: 4 [ 1178.595649] sd 0:0:0:0: [sda] 122880000 512バイトの論理ブロック: (62.9 GB/58.6 GiB) [ 1178.612255] sd 0:0:0:0: [sda] 書き込み保護はオフです [ 1178.634376] sd 0:0:0:0: [sda] キャッシュモードページが見つかりません [ 1178.639860] sd 0:0:0:0: [sda] ドライブキャッシュを想定: ライトスルー [ 1178.667061] sda: sda1 [ 1178.683380] sd 0:0:0:0: [sda] SCSIリムーバブルディスクが接続されました [ 1178.704463] usb 1-1: USB切断、デバイス番号18 [ 1178.713191] sd 0:0:0:0: [sda] タグ#0 失敗 結果: ホストバイト=DID_ERROR ドライバーバイト=DRIVER_OK [ 1178.721585] sd 0:0:0:0: [sda] タグ#0 CDB: 読み取り(10) 28 00 07 52 ff 80 00 00 08 00 [ 1178.728953] blk_update_request: I/Oエラー、デバイスSDA、セクター122879872 op 0x0:(READ) フラグ0x80700 phys_seg 1 prioクラス0 [ 1178.753859] scsi 0:0:0:0: [sda] tag#0 失敗 結果: ホストバイト=DID_ERROR ドライバーバイト=DRIVER_OK [ 1178.762423] scsi 0:0:0:0: [sda] タグ#0 CDB: 読み取り(10) 28 00 07 52 ff 80 00 00 08 00 [ 1178.769993] blk_update_request: I/Oエラー、デバイスSDA、セクター122879872 op 0x0:(READ) フラグ0x0 phys_seg 1 prioクラス0 [ 1178.780566] デバイスSDAのバッファI/Oエラー、論理ブロック15359984、非同期ページ読み取り [ 1179.167312] usb 1-1: ci_hdrc を使用して新しい高速USBデバイス番号19を作成しました [ 1179.747351] USB 1-1: デバイスがアドレス19を受け入れません、エラー -71 [ 1231.457317] usb 1-1: ci_hdrc を使用した新しい高速 USB デバイス番号 21 [ 1231.509890] usb 1-1: 新しいUSBデバイスが見つかりました、idVendor=346d、idProduct=5678、bcdDevice= 3.20 [ 1231.518295] usb 1-1: 新しいUSBデバイス文字列: Mfr=1、Product=2、SerialNumber=3 [ 1231.525582] usb 1-1: 製品: ディスク 20 [ 1231.536329] usb 1-1: メーカー: USB [ 1231.543336] usb 1-1: シリアル番号: FC31114725D35 [ 1231.561890] usb-storage 1-1:1.0: USBマスストレージデバイスが検出されました [ 1231.584731] SCSIホスト0: USBストレージ1-1:1.0 [ 1232.649677] scsi 0:0:0:0: ダイレクトアクセス ベンダー C 製品コード 3.20 PQ: 0 ANSI: 4 [ 1232.674366] sd 0:0:0:0: [sda] 122880000 512バイトの論理ブロック: (62.9 GB/58.6 GiB) [ 1232.687983] sd 0:0:0:0: [sda] 書き込み保護はオフです [ 1232.710654] sd 0:0:0:0: [sda] キャッシュモードページが見つかりません [ 1232.716076] sd 0:0:0:0: [sda] ドライブキャッシュを想定: ライトスルー [ 1232.768537] sda: sda1 [ 1232.790606] sd 0:0:0:0: [sda] SCSIリムーバブルディスクが接続されました [ 1232.809177] usb 1-1: USB切断、デバイス番号21 [ 1232.820341] sd 0:0:0:0: [sda] タグ#0 失敗 結果: ホストバイト=DID_ERROR ドライバーバイト=DRIVER_OK [ 1232.828769] sd 0:0:0:0: [sda] タグ#0 CDB: 読み取り(10) 28 00 07 52 ff 80 00 00 08 00 [ 1232.836102] blk_update_request: I/Oエラー、デバイスSDA、セクター122879872 op 0x0:(READ) フラグ0x80700 phys_seg 1 prioクラス0 [ 1232.858688] scsi 0:0:0:0: [sda] tag#0 失敗 結果: ホストバイト=DID_ERROR ドライバーバイト=DRIVER_OK [ 1232.867266] scsi 0:0:0:0: [sda] タグ#0 CDB: 読み取り(10) 28 00 07 52 ff 80 00 00 08 00 [ 1232.874768] blk_update_request: I/Oエラー、デバイスSDA、セクター122879872 op 0x0:(READ) フラグ0x0 phys_seg 1 prioクラス0 [ 1232.885360] デバイスSDAのバッファI/Oエラー、論理ブロック15359984、非同期ページ読み取り [ 1233.277349] usb 1-1: ci_hdrc を使用した新しい高速 USB デバイス番号 22 ルート@imx6ul7d:~# ルート@imx6ul7d:~# ルート@imx6ul7d:~# df ファイルシステム 1Kブロック 使用済み 使用可能 使用率 マウント先 /dev/root 1215192 746488 387904 66% / devtmpfs 168088 4 168084 1% /dev tmpfs 250520 0 250520 0% /dev/shm tmpfs 250520 8952 241568 4% /実行 tmpfs 250520 0 250520 0% /sys/fs/cgroup tmpfs 250520 4 250516 1% /tmp tmpfs 250520 184 250336 1% /var/volatile /dev/mmcblk1p1 27130 10722 16408 40% /run/media/mmcblk1p1 tmpfs 50104 4 50100 1% /run/user/0 root@imx6ul7d:~# [ 1243.827330] usb 1-1: デバイスがアドレス22を受け入れません、エラー -110 [ 1243.977433] usb 1-1: ci_hdrc を使用した新しい高速 USB デバイス番号 23 root@imx6ul7d:~# [ 1249.487330] usb 1-1: デバイスがアドレス23を受け入れません、エラー -71 [ 1249.493511] usb usb1-port1: 電源を入れ直す [ 1249.987411] usb 1-1: ci_hdrc を使用した新しい高速 USB デバイス番号 24 [ 1250.157372] USB 1-1: デバイス応答なし、デバイスディスクリプタ読み取り/64、エラー -71 [ 1255.447396] USB 1-1: デバイス応答なし、デバイスディスクリプタ読み取り/64、エラー -71 [ 1255.717429] usb 1-1: ci_hdrc を使用した新しい高速 USB デバイス番号 25 [ 1255.887415] USB 1-1: デバイス応答なし、デバイスディスクリプタ読み取り/64、エラー -71 [ 1261.207667] USB 1-1: デバイス応答なし、デバイスディスクリプタ読み取り/64、エラー -71 [ 1261.327356] usb usb1-port1: USBデバイスを列挙できません Udisk を除き、ハードウェアとソフトウェアは両方とも NXP 製です。この問題の根本的な原因は何でしょうか? i.MX6UL Re: Some Udisks fail to be enumerated in the MCIMX6ULL-EVK evaluation board この問題の根本的な原因は、この 64GB Udisk が USB 2.0 と適切に下位互換性がないことです。 Re: Some Udisks fail to be enumerated in the MCIMX6ULL-EVK evaluation board タイプミスの訂正: 128GB Udisk はMCIMX6ULL-EVK 評価ボードで列挙できますが、64GB Udisk は列挙できません。   追加情報:前述の Thinkplus Udisk はどちらもLenovo ブランドの製品です。下の図に示すように:
View full article
NDA 申請を提出してから署名を得るまでに通常はどのくらいの時間がかかりますか? https://support.nxp.com/s に NDA リクエストを送信しました (サービスリクエスト:00624736に申請したところ、法務部に提出済みとの返信をいただきましたが、1週間経っても何の連絡もありません。却下されたのか、法務部がまだ確認していないのか、はっきりしません。 このNDAに署名するには通常どのくらい時間がかかりますか?
View full article
Serial Downloader実行時のFlexSPI構成は? i.MX RT1021 で eFuse を serialNOR フラッシュ (BOOT_CFG1[7:4] = 0) から起動するように設定し、Serial Downloader モードで実行していて、JTAG デバッガでブレークインした場合、接続されている Serial NOR Flash デバイスの内容を flexSPI で表示できますか。 つまりbootROM シリアル ダウンロード アプリケーションは、フラッシュにアクセスするために flexSPI を正しく設定していますか? FlexSPI/MCR0レジスタ(@0x402a8000)を読み取ると、次のように表示されます0xffff80c2 これにより、MCR0[MDIS]ビット= 1になり、flexSPIインターフェース全体が無効になります。私は(JTAGデバッガを介して)[MDIS]ビットをまったくクリアできません。 メモリは0x60000000(フラッシュの開始)に読み取って意味不明な読み取りをします。ただし、MCUExpresso GUI フラッシュ ツールは、そこに FCFB ブロックが書き込まれ、検証されます。 i.MXRT 102倍 Re:シリアルダウンローダー実行中のFlexSPI構成? Deigoさん、ありがとうございました。また、Kinetisブートローダイメージとそれを使用するホストPCのblhostアプリケーションも見つけることができました。sdphostを使用すると、ブートローダーイメージをMCU RAMにアップロードし、MCUがシリアルダウンロードモードにあるときにそれを使用して周囲を見回すことができました。
View full article
S32k312 在S32DS 工具中配置CANFD功能 请问: 1.S32K312 在S32DS 工具中配置CANFD功能 ,发现有Drivers 和MCAL两项,如果只在RTOS中使用是不是只需要在Drivers添加CAN Driver即可? 2.是否有CANFD功能只在RTOS使用的Demo code,或是CANFD配置及收发流程? Re: S32k312 在S32DS 工具中配置CANFD功能 Hi@Bert2023 1.RTD驱动提供了两种开发方式来满住客户的需求,其包涵了LLD和HLD两个独立的部分,分别对应Drivers和MCAL,对于有Autosar需求的人,可以选择MCAL来配置亦或者使用EB(推荐),如果没有Autosar要求,那么Drivers更合适,其配置更直观简洁。 所以你直接使用Drivers的FlexCAN组件即可。 2.我可以给你一些配置CAN的用例,但是如果你想要一个FreeRTOS的FlexCAN收发例程,我想我们是没有的,FreeRTOS是一个第三方提供的,我们不去支持FreeRTOS的问题(这应该不难做,参考我们提供的例程应该很容易实现)。 你可以看看下面的例程,S32K3的FlexCAN模块用法都是几乎一样的 https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K358-FlexCAN-TXRX-ISR-S32DS35-RTD400/ta-p/1981987
View full article
关于随机数生成器函数的问题 大家好,各位队员。 希望一切顺利 我看到一位 NXP 工程师在这个论坛上对 TRNG 相关问题的回答是“TRNG 在内部运行以生成构建 PRNG 的种子”。 那么,这是否意味着不需要输入单独的种子值来生成随机数? Ps:我知道使用DRBG算法时需要输入一个具有一定熵的种子。DRBG算法和PRNG是不同的概念吗? 回复:关于随机数生成器函数的问题 没错,我问的是 S32K 上的 CSEc。谢谢您的帮助!我的问题已经全部解决了 回复:关于随机数生成器函数的问题 你好@Derek_Yoon 我们讨论的是 S32K1 上的 CSEc 吗?这是由 SHE 规范给出的。初始种子由 CMD_INIT_RNG 命令生成。然后,您可以生成随机数,而不需要重新播种。您在运行时唯一可以做的额外事情是运行 CMD_EXTEND_SEED 命令来提供 128 位熵。无论何时需要额外的熵,您都可以调用此命令。 问候, 卢卡斯
View full article