2063006_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2063006_en-US

2063006_en-US

Issues with Ethernet Enablement and Network Connectivity on NXP S32G-VNP-RDB2

I have powered on the NXP S32G RDB2 Board and was able to communicate serially with PuTTY.  However when I want to connect ethernet cable to it. Even though I tried assigning static IPs, it wouldn't ping. I want to enable the ethernet driver or solve the issue so that I can test my usecases.

Re: Issues with Ethernet Enablement and Network Connectivity on NXP S32G-VNP-RDB2

Hello @chenyin_h , I am glad to share that finally it is pinging and tested out by connecting to router and creating a private network with other boards, for now I am exploring ethernet communications at other ports too. For any other problems, I shall open another ticket or post.

Thank you!

Re: Issues with Ethernet Enablement and Network Connectivity on NXP S32G-VNP-RDB2

Hello, @vigneshrk0482 

Thanks for your reply.

I have just tested it on my local RDB2 with default BSP35.0 images(without any other settings), the eth0 could be used correctly.

The testing log is attached for your reference.


BR

Chenyin

Re: Issues with Ethernet Enablement and Network Connectivity on NXP S32G-VNP-RDB2

Hello @chenyin_h ,

The BSP version is Auto Linux 35 (U-boot from SD Card) and using the GMAC port. However I think that the ethernet is not enabled. When I checked eth0 in ip route it says NO-CARRIER but in ifconfig it says UP. Also I want to use this to communicate with Raspberry Pi to NXP board. Please guide me what steps to do as I have tried all the attempts.

Re: Issues with Ethernet Enablement and Network Connectivity on NXP S32G-VNP-RDB2

Hello, @vigneshrk0482 

Thanks for the post.

May I know which version BSP(or other software package) is used for your test? which network port was used?


BR

Chenyin 

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 09:53 PM
更新者: