2122841_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2122841_en-US

2122841_en-US

BSP Version Required for dm-eiq-genai-flow-demonstrator on i.MX95

Hi Team,

I’m exploring the dm-eiq-genai-flow-demonstrator (GenAI Flow) on the i.MX95 platform working within a Yocto environment. Could you please clarify:

     1. Which BSP version (e.g., L6.12.20_2.0.0) is minimum required to run the demo end-to-end?

    2. Does this BSP include all necessary elements—such as updated Neutron delegate, TFLite  runtime, and tooling—to support LLM inference (RAG)?

    3. Are there any additional Yocto meta-layers or image recipes (for example meta-eiq-        genai) recommended for this demo?

Thanks in advance for your insights!

Best regards,
Varshil Gandhi

Re: BSP Version Required for dm-eiq-genai-flow-demonstrator on i.MX95

Hi Varshil,
Thanks for your questions.
Let me try to answer them:
1. The package was initially made for Q1 BSP L6.12.3-1.0.0 for i.MX95 rev Ax.
2. This Q1 BSP does not directly include what's necessary to leverage Neutron on LLM inferences. That's why the package provides a meta-layer.
3. This meta-eiq-genai-flow meta-layer provides the possibility to add a Onnxruntime Neutron Execution Provider to accelerate the LLM operations on Neutron and free up some CPU resources, with associated patches/files for Kernel and Neutron Fw. Please note that we are using onnxruntime and not TF lite for this project.

That being said, 
Q2 BSP (e.g., L6.12.20_2.0.0) is being released this days. It supports the B0 revision of i.MX95 but without LLM acceleration on Neutron, only CPU mode is functional.


Thanks and best regards,

Pierre
 

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 06:54 PM
更新者: