LX2160ARDB: DDR validation Hi, We have loaded the RCW file(rcw_2200_750_2900_19_5_2.bin) from the LSDK into SD card and in DDR configuration panel, when Read SPD is done we are getting as "Unsupported raw card revision. Set the CLK to DQS skew values manually." How to perform DDR validation of LX2160ARDB in QCVS tool Priyaa_0-1788337942087.pngPriyaa_0-1788337942087.pngPriyaa_0-1788337942087.pngPriyaa_0-1788337942087.pngPriyaa_0-1788337942087.pngPriyaa_0-1788337942087.pngPriyaa_0-1788337942087.pngPriyaa_0-1788337942087.pngPriyaa_0-1788337942087.png Re: LX2160ARDB: DDR validation Hi June Lu, Thanks for the support for USB the result of the command is (bin) 51 % findcc cwtaps 0 (bin) 51 % and for ethernet connection (bin) 51 % findcc cwtaps FSL07E3D5 (10.1.66.150): CodeWarrior TAP v2 Cortex-10 Probe Tip Boot Loader v1.0.1 Operating System v1.0.5 1 for now can we proceed further using ethernet connection for ddr validation? Re: LX2160ARDB: DDR validation (bin) 52 % show cc
0: USB open failure
There are no command converters configured
it indicates that the CWTAP cannot be detected through the USB connection.
Please check the USB cable connection and ensure the CWTAP is properly recognized by the host PC.
Also, please run the command below and share the result:
(bin) 6 % findcc cwtaps
Thanks. Re: LX2160ARDB: DDR validation Hi June Lu, CodeWarrior Version- Priyaa_0-1788417354430.pngPriyaa_0-1788417354430.pngPriyaa_0-1788417354430.pngPriyaa_0-1788417354430.pngPriyaa_0-1788417354430.pngPriyaa_0-1788417354430.pngPriyaa_0-1788417354430.pngPriyaa_0-1788417354430.pngPriyaa_0-1788417354430.png (bin) 49 % log v CCS Linux Release Build 503.0.0.220812-p0 verbose logging (bin) 50 % delete all (bin) 51 % config cc cwtap (bin) 52 % show cc 0: USB open failure There are no command converters configured (bin) 53 % (bin) 53 % source IDcode.tcl Scanning for available TAPs connected via USB..... No TAPs found connected via USB ++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++ + + Available Remote Connections + + 1 - CodeWarriorTAP - + 2 - GigabitTAP - + + x - Exit Script without Changes + ++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++ Specify connection: can't read "CONNECTION()": no such element in array (bin) 54 % (bin) 54 % Able to connect through ethernet and ping the target. Even after updating CodeWarrior to v11.5.12, reading SPD gives same as "Unsupported raw card revision. Set the CLK to DQS skew values manually." Thank you Re: LX2160ARDB: DDR validation Please confirm the CodeWarrior version from Help → About CodeWarrior Development Studio for QorIQ LS Series (ARM v8 ISA).
Please follow the instructions in "CCS Windows Release Build 503.0.0.220812-p0.txt" to verify the connection status.
We recommend testing the USB connection first, followed by the Ethernet connection.
It seems that the IP address has changed. Could you please confirm whether you can successfully ping the target? Re: LX2160ARDB: DDR validation Hi June Lu, We are using CodeWarrior 11.5.0 and the DIMM is original module given with the LX2160ARDB Updated CodeWarrior with archive com.freescale.armv8.11.5.12.GA.Lin.updatesite.221209.zip for v11.5.12 Now unable to detect the JTAG Priyaa_0-1788412965825.pngPriyaa_0-1788412965825.pngPriyaa_0-1788412965825.pngPriyaa_0-1788412965825.pngPriyaa_0-1788412965825.pngPriyaa_0-1788412965825.pngPriyaa_0-1788412965825.pngPriyaa_0-1788412965825.pngPriyaa_0-1788412965825.png Thankyou Re: LX2160ARDB: DDR validation I followed your sequence and was able to read the SPD successfully.
Could you please confirm which version of CodeWarrior you are using? Is it CodeWarrior 11.5.12?
Also, is the DIMM an original module?
Thanks. Re: LX2160ARDB: DDR validation Hi June Lu, After booting through FlexSPI, loaded the RCW file through tftpboot at u-boot and mmc write commands as below => tftpboot 0x90000000 rcw_2200_750_2900_19_5_2.bin => mmc dev 0; mmc write 0x90000000 8 1 => qixis_reset sd (during this command the D19 got turned on and off) And for DDR configuration, when reading from SPD getting as "Unsupported raw card revision. Set the CLK to DQS skew values manually." Re: LX2160ARDB: DDR validation How do you load the RCW file(rcw_2200_750_2900_19_5_2.bin) from the LSDK into SD card?
Has the D19 turned on and off?
DDR validation of LX2160ARDB in QCVS tool, you could refer to:
QCVS_DDR_User_Guide
Thanks Re: LX2160ARDB: DDR validation Diagnose Connection successfully done Priyaa_0-1788431456696.pngPriyaa_0-1788431456696.pngPriyaa_0-1788431456696.pngPriyaa_0-1788431456696.pngPriyaa_0-1788431456696.pngPriyaa_0-1788431456696.pngPriyaa_0-1788431456696.pngPriyaa_0-1788431456696.png And DDR configuration after reading SPD is as below Priyaa_1-1788432417841.pngPriyaa_1-1788432417841.pngPriyaa_1-1788432417841.pngPriyaa_1-1788432417841.pngPriyaa_1-1788432417841.pngPriyaa_1-1788432417841.pngPriyaa_1-1788432417841.pngPriyaa_1-1788432417841.png Could you please confirm whether DDR validation is started successully? Cause I'm facing an issue that the Start Validation button is enabled but the validation getting cancelled just after the start.. Re: LX2160ARDB: DDR validation Hi June Lu, Connected through ethernet and able to find LX2160A as provided in the text file Priyaa_0-1788427814124.pngPriyaa_0-1788427814124.pngPriyaa_0-1788427814124.pngPriyaa_0-1788427814124.pngPriyaa_0-1788427814124.pngPriyaa_0-1788427814124.pngPriyaa_0-1788427814124.png But reading SPD gives as "Unsupported raw card revision. Set the CLK to DQS skew values manually." in DDR configuration window And how to verify the SPD values are read successfully? Re: LX2160ARDB: DDR validation This is the successful screenshot.
June_Lu_0-1788429917395.pngJune_Lu_0-1788429917395.pngJune_Lu_0-1788429917395.pngJune_Lu_0-1788429917395.pngJune_Lu_0-1788429917395.pngJune_Lu_0-1788429917395.png
I used the USB to connect to the CWTAP. You need to set the Probe with correct IP address.
Could you run the "Diagnose Connection" successfully?
June_Lu_1-1788430165643.pngJune_Lu_1-1788430165643.pngJune_Lu_1-1788430165643.pngJune_Lu_1-1788430165643.pngJune_Lu_1-1788430165643.pngJune_Lu_1-1788430165643.png
Re: LX2160ARDB: DDR validation (bin) 50 % delete all
(bin) 51 % config cc cwtap:10.1.66.150
(bin) 52 % show cc
(bin) 53 % source IDcode.tcl
If you could find LX2160A same as the "CCS Windows Release Build 503.0.0.220812-p0.txt".
You could proceed using ethernet connection with IP address: 10.1.66.150 for ddr validation.
Thanks Re: LX2160ARDB: DDR validation Hi June Lu, Following the user guide, created a project again for DDR configuration and reading of SPD has done as below Priyaa_0-1788498272408.pngPriyaa_0-1788498272408.pngPriyaa_0-1788498272408.pngPriyaa_0-1788498272408.png And the DIMM modules are inserted in the J14, J17 connectors of RDB Re: LX2160ARDB: DDR validation Hi June Lu, After changing the switch(SW1) to SD card mode where the RCW source is present, we were able to do the validation. Thanks for the support.. Re: LX2160ARDB: DDR validation It seem your screen shot is not same as me, missing button "Back" and "Cancel".
Have you follow the QCVS_DDR_User_Guide, 1.1.1 Using DDR configuration tool?
Thanks Re: LX2160ARDB: DDR validation It looks like you were able to read the SPD successfully, although the screenshot is slightly different from what I see on my side.
Please set SW1[1:4] to 1001 to boot from eMMC, where the RCW source has been configured for DDR validation.
Also, please confirm that "Target Connects" shows as connected see the screen shot.
Once confirmed, you can proceed with the DDR validation.
June_Lu_0-1788504721222.png
Re: LX2160ARDB: DDR validation Hi June Lu, To boot the LX2160ARDB from SD card is DDR register values has to be modified in the u-boot source or it reads from SPD of DIMMs? Kindly clarify...thank you Re: LX2160ARDB: DDR validation For the standard LX2160ARDB with DIMM slots, DDR registers are configured automatically by reading SPD from the installed DIMMs — handled by the TF-A BL2 stage (ddr_init.c), not U-Boot. You only need to modify the ATF source if using custom DIMMs on the LX2160ARDB.
If there are any new questions, please create a new thread so we can track them properly, as this case has been inactive for quite some time.
Thanks.
查看全文