ECSPI_SCLK signal integrity Hi, I'm using the i.MX8M mini. I measured the waveform of SCLK and MISO at the i.MX end. The SCLK is output by i.MX as the master, but there are distortions such as glitches on the rising edge. When capturing data form MISO, does the i.MX8 use this SCLK waveform? Is my unerstanding correct that the internal circuit driving the data acquisition uses a clean singal that is isolated by buffers, and is not affected by external reflections? CH1 (Yellow) : SCLK CH2 (Blue): MISO Thanks, Re: ECSPI_SCLK signal integrity Dear janxie, Thank you for your reply. I understand that we currently don't have the internal design diagram, so we cannot resolve my question at this time. Best Regards, Re: ECSPI_SCLK signal integrity refer to the RM, I only find this diagram, though I don't have internal design diagram, but the ecspi design can provide the clean signal to the SCLK, if all of your boards get the jitter, should check the HW design or measurement tools, if only one or two boards have this issue, maybe you can do the AB test to confirm if this issue is related to the chip
Re: ECSPI_SCLK signal integrity Dear janxie, Thank you for your reply. I understand that ECSPI uses SCLK signal for Shift register. And SCLK wavefore is important for Slave device. I'd like to know the i.MX inside diagram. Figure 1. is my understanding. Do you mean that Figure 2 is correct? Thanks, Re: ECSPI_SCLK signal integrity 1)When capturing data form MISO, does the i.MX8 use this SCLK waveform?
>yes, refer to the reference manual, The ECSPI master uses the Chip Select (SS) signal to enable an external SPI device, and uses the SCLK signal to transfer data in and out of the Shift register. 2)Is my unerstanding correct that the internal circuit driving the data acquisition uses a clean singal that is isolated by buffers, and is not affected by external reflections?
> the signal integrity issues present at the pin would be affected by external, so you need to double check your HW design
查看全文