Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
How to setup sai1 tdm mode for imx8mq-evk? The end goal is to configure sai1, txd0 for 8 frame, 32-bit, TDM mode (if it's not already) under Yocto Linux.  In "fsl-imx8mq-evk.dts", I see "fsl,sai-multi-lane" and "fsl,dataline,dsd = ...", but there's no mention (that I can find) in the devicetree documentation fsl-sai.txt file to describe either of these two options.    I don't know if I'm even looking in the right place given my goal.  Where should the sai be configured under Linux?   For what it's worth, I think I see how the ak4458 gets configured in alsa.state and alsa.conf, but I'm guessing that this will tell the ak4458 driver how to configure the ak4458, and what I really need is the other end, the sai configuration.   John i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Linux Multimedia Yocto Project Re: How to setup sai1 tdm mode for imx8mq-evk? Hello everyone, I'm trying to setup a TDM8 on IMXRT1170-EVKB using SAI1 starting from the example "sai_edma_tdm_playback_cm7",provided by MCUXpresso. I'm not using AUD-EXP-42448 necessary for the example so i'm just connected to J76 pins and my goal is to send someting to SAI_RX0 and resend it on SAI_TX0. Can someone explain me how to correctly configure a TDM communication using SAI1?   Re: How to setup sai1 tdm mode for imx8mq-evk? Thank you John, your suggestions will help me a lot and I will try to implement the tdm mode in SAI driver. thank you once again, Sreedhar Re: How to setup sai1 tdm mode for imx8mq-evk? Sorry it's taken a while to respond, but that was quite a while ago and I'm still trying to remember what I did.   It doesn't readily take the form of a "patch" and in the end, there's very little, if anything, different in fsl_sai.c, and a whole lot of changes in other places.   The sai driver is, I think, set up to handle tdm mode, the trick is to create a codec driver that configures the sai driver with the proper parameters.  In the end, I created a new imx- "codec" file based on an existing codec, added my own parameters for my codec in the devicetree so that I could set the format and the tdm width from the devicetree, and then added the codec to the kernel config so it could be selected and built in the kernel configuration and build.    You might be able to shorten some of those steps by creating your own imx-codec file, but simply hardcode the slots, width and fmt into the imx_(yourcodecname)_hw_params() function.  Take a look at imx-ak4485.c and the calls to snd_soc_dai_set_fmt() and snd_soc_dai_set_tdm_slot().   Hope this helps.  If you still want to see my version of the "not a codec" codec driver, I can provide it, but it may take me a while to clean up the code to be presentable.   John Re: How to setup sai1 tdm mode for imx8mq-evk? Hi John, Good day!! I understand from your post https://community.nxp.com/thread/499282 , you made tdm operation succesful in sai1 as master. Could you please let us know the changes you have made to the fsl_sai.c diver for supporting tdm operation. Could you please post the patch of it. Thank you, Sreedhar Re: How to setup sai1 tdm mode for imx8mq-evk? See https://community.nxp.com/thread/499282  Re: How to setup sai1 tdm mode for imx8mq-evk?  Update, and a follow-up question involving the same setup.  I've had some luck hacking at the fsl_sai.c driver to support 8-frame tdm on sai1 and successfully drove an AKM4458 eval board with the imx8mq eval board as frame sync and bit clock master.  The next step is to configure the imx8mq eval board as frame sync and bit clock slave instead of master.   I thought this would be as simple as: NOT setting the BCD bit in TCR2 NOT setting the FSD bit in TCR4 But having done this, and confirming the register settings (and supplying the external frame sync and bit clock), I no longer see data on the transmit line, and the 'play' operation eventually errors out with an I/O error.  To add to the mystery, MCLK is no longer being generated by the imx8mq EVK.  I thought that would have been independent of the two bits in the TCR2 and TCR4 registers. Is there something else that must be done in software or the kernel configuration to change a working SAI1 clock master to a clock slave ? John Re: How to setup sai1 tdm mode for imx8mq-evk?  Hi John unfortunately currently there are no tdm configurations which could be set through dts file, so one will have to change sai driver according to tdm configuration for used codec (that should be described in codec datasheet). > I'd like to know what "sai-multi-lane" and "dataline,dsd = ..." do.   one can check driver sources: driver linux/sound/soc/fsl/fsl_sai.c fsl_sai.c\fsl\soc\sound - linux-imx - i.MX Linux kernel Note NXP has special service for helping porting drivers for customer needs NXP Professional Services | NXP  Best regards igor Re: How to setup sai1 tdm mode for imx8mq-evk? Hi, Igor, Thank you for replying, but I'm not sure you completely understood.  I know about the documentation you linked to in your reply, I specifically mentioned them in my original.  But there are two options included in the devicetree for the evk (and apparently supported in the sai driver, from what I can tell) that are not included in the documentation.   I'd like to know what "sai-multi-lane" and "dataline,dsd = ..." do.   As for your suggestion to set the slot widths, please forgive my ignorance, but how would that best be accomplished?  In a user-space app ?  Wouldn't it be better to modify the fsl_sai.c driver to support TDM options in the devicetree?  Or is that more complicated than it seems?   John Re: How to setup sai1 tdm mode for imx8mq-evk? Hi John tdm is supported in sai driver linux/sound/soc/fsl/fsl_sai.c fsl_sai.c\fsl\soc\sound - linux-imx - i.MX Linux kernel  fsl-sai.txt\sound\bindings\devicetree\Documentation - linux-imx - i.MX Linux kernel  unfortunately there are no tdm configurations which could be set in dts file. fsl-sai.txt\sound\bindings\devicetree\Documentation - linux-imx - i.MX Linux kernel  one can check driver for tdm settings, in fsl_sai_set_dai_tdm_slot(), sai->slot_width = slot_width; and set them to necessary values. Best regards igor ----------------------------------------------------------------------------------------------------------------------- Note: If this post answers your question, please click the Correct Answer button. Thank you! -----------------------------------------------------------------------------------------------------------------------
記事全体を表示
如何为 imx8mq-evk 设置 sai1 tdm 模式? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 最终目标是在 Yocto Linux 下将 sai1、txd0 配置为 8 帧、32 位、TDM 模式(如果尚未配置)。 在"fsl-imx8mq-evk.dts" 中,我看到"fsl,sai-multi-lane" 和"fsl,dataline,dsd = ..." ,但在 devicetree 文档 fsl-sai.txt 文件中没有提到(我能找到)这两个选项中的任何一个。 我不知道我的目标是否正确。 在 Linux 下应在何处配置 sai? 不管怎样,我想我知道alsa.state 和 alsa.conf 是如何配置 ak4458 的了、但我猜这将告诉 ak4458 驱动程序如何配置 ak4458,而我真正需要的是另一端,即 sai 配置。 约翰 i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Linux 多媒体 Yocto Project Re: How to setup sai1 tdm mode for imx8mq-evk? 大家好,我正在尝试在 IMXRT1170-EVKB 上使用 SAI1 设置 TDM8,从 MCUXpresso 提供的示例"sai_edma_tdm_playback_cm7" 开始。我没有使用示例中所需的 AUD-EXP-42448,所以我只是连接到 J76 引脚,我的目标是向 SAI_RX0 发送信息,然后在 SAI_TX0 上重新发送。 谁能告诉我如何使用 SAI1 正确配置 TDM 通信?   Re: How to setup sai1 tdm mode for imx8mq-evk? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 谢谢你,约翰、 您的建议对我帮助很大,我会尝试在 SAI 驱动程序中实现 tdm 模式。 再次感谢您、 斯里达尔 Re: How to setup sai1 tdm mode for imx8mq-evk? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 很抱歉过了很久才回复,但那是很久以前的事了,我还在努力回想我都做了些什么。 "补丁" 的形式,最终,fsl_sai.c 几乎没有什么不同、以及其他地方的许多变化。 我认为 sai 驱动程序安装为处理 tdm 模式,诀窍是创建一个编解码器驱动程序,使用正确的参数配置 sai 驱动程序。最后,我基于现有编解码器创建了一个新的 imx-" 编解码器 " 文件,在 devicetree 中为我的编解码器添加了自己的参数,这样我就可以从 devicetree 中设置格式和 tdm 宽度,然后将编解码器添加到内核配置中,这样就可以在内核配置和版本中进行选择和版本。 您也许可以通过创建自己的 imx-codec 文件来缩短其中的一些步骤,但只需将槽位、宽度和 fmt 硬编码到 imx_(yourcodecname)_hw_params() 函数中即可。 请查看 imx-ak4485.c 以及对 snd_soc_dai_set_fmt() 和 snd_soc_dai_set_tdm_slot() 的调用。 希望对您有所帮助。 如果你还想看我的"not a codec" 编解码器驱动程序版本,我可以提供,但我可能要花一些时间来整理代码,使其更易于使用。 约翰 Re: How to setup sai1 tdm mode for imx8mq-evk? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,约翰、 日安 我从您的帖子中了解到https://community.nxp.com/thread/499282作为主人,您在 Sai1 成功地进行了 tdm 操作。 你能否与我们联系你对 fsl_sai.c 所做的更改支持 TDM 运行的潜水员。 能否请您发布一下补丁。 谢谢你,斯里达尔 Re: How to setup sai1 tdm mode for imx8mq-evk? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 参见https://community.nxp.com/thread/499282 Re: How to setup sai1 tdm mode for imx8mq-evk?  <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 更新,以及涉及相同设置的后续问题。 我在黑客攻击 fsl_sai.c 时取得了一些进展。该驱动程序支持 sai1 上的 8 帧 tdm,并成功驱动了使用 imx8mq 评估板作为帧同步和位时钟主器的 AKM4458 评估板。下一步是将 imx8mq 评估板配置为帧同步和位时钟从机而不是主机。 我以为这很简单: 不要在 TCR2 中设置 BCD 位 不设置 TCR4 中的 FSD 位 但是,在完成上述操作并确认寄存器设置(以及提供外部帧同步和位时钟)后,我就再也看不到传输线上的数据了,而且 "播放 "操作最终也因 I/O 错误而出错。 更令人费解的是,MCLK 不再由 imx8mq EVK 产生。 我以为这与 TCR2 和 TCR4 寄存器中的两个位无关。 要将工作中的 SAI1 时钟主控程序变为时钟从属程序,是否还需要在软件或内核配置中做其他操作? 约翰 Re: How to setup sai1 tdm mode for imx8mq-evk?  <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,约翰 遗憾的是,目前还没有可以通过 dts 文件设置的 tdm 配置、 因此,必须根据所用编解码器的 tdm 配置更改 sai 驱动程序(即 应在编解码器数据表中说明)。 > 我想知道" sai-multi-lane" 和"dataline,dsd = ..." 的作用。 可以查看驱动程序源代码:driver linux/sound/soc/fsl/fsl_sai.c fsl_sai.c\fsl\soc\sound - linux-imx - i.MX Linux 内核 注意:恩智浦提供特殊服务,帮助移植驱动程序以满足客户需求 恩智浦专业服务 | 恩智浦 问候 igor Re: How to setup sai1 tdm mode for imx8mq-evk? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,伊戈尔 谢谢您的回复,但我不确定您是否完全理解。 我知道你在回复中链接到的文档,我在原文中特别提到了它们。 但 evk 的 devicetree 中包含了两个选项(据我所知,sai 驱动程序显然也支持这两个选项),而这两个选项并未包含在文档中。 我想知道" sai-multi-lane" 和"dataline,dsd = ..." 的作用。 至于您提出的设置插槽宽度的建议,请原谅我的无知,但怎样才能最好地实现呢? 在用户空间应用程序中? 修改 fsl_sai.c 是否更好?驱动程序是否支持 Devicetree 中的 TDM 选项? 还是说,这比想象的要复杂得多? 约翰 Re: How to setup sai1 tdm mode for imx8mq-evk? <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 嗨,约翰 sai 驱动程序 linux/sound/soc/fsl/fsl_sai.c 支持 tdm fsl_sai.c\fsl\soc\sound - linux-imx - i.MX Linux 内核 fsl-sai.txt\sound\bindings\devicetree\Documentation - linux-imx - i.MX Linux 内核 遗憾的是,没有可以在 dts 文件中设置的 tdm 配置。 fsl-sai.txt\sound\bindings\devicetree\Documentation - linux-imx - i.MX Linux 内核 可以检查驱动程序的 tdm 设置,在 fsl_sai_set_dai_tdm_slot() 中,sai->slot_width = slot_width; 并将其设置为必要的值。 问候 igor ----------------------------------------------------------------------------------------------------------------------- 注:如果本帖回答了您的问题,请点击 "正确答案 "按钮。Thank you! -----------------------------------------------------------------------------------------------------------------------
記事全体を表示
S32k312 的 PLL 计算 大家好 我在设计中使用的是 S32K312 微芯片。请帮我计算 PLL 的输出频率。我们使用的是 40 MHz 的外部晶振。你能提供一个计算示例吗?如果我们使用 40 MHz 晶振可以吗? 请提供 S32K312 的时钟计算器。 Re: PLL calculation for S32k312 你好@mogilipuri_harish,你能解决这个问题吗?我也遇到了同样的问题。我的配置完全相同,使用的是 MCAL 6.0.0 版 S32K312。 面对"PLL ODIV2 = 2" 超出范围的误差 Re: PLL calculation for S32k312 Hi@mogilipuri_hari sh 除数据表外,没有更多关于时钟配置的指导文件 如图所示,RTD 2.0.1 及以上版本有用于 S32K312 的例程。 Re: PLL calculation for S32k312 嗨 我正在尝试进行 PLL 时钟计算。您能提供一些如何进行计算的说明吗?比如参考文档。我没有在工具中找到 S32k312 示例,能否请您分享一下,这将对我有所帮助。 Re: PLL calculation for S32k312 您好, 供你参考,例如: PLL 输出频率范围必须在 640MHz~1,28GHz 之间。 Re: PLL calculation for S32k312 您好, 没有完全理解你的问题,你的意思是哪些分频器值可以改变? 图中的这些参数可以更改,您可以在 S32 DS 中查看这些时钟树配置。 Re: PLL calculation for S32k312 在这里,我们可以更改哪些变量值? Re: PLL calculation for S32k312 谢谢提醒 在 S32K312 中,CORE_CLK=160Mhz 仍可运行,但不建议客户使用这种方式,会有未知风险 Re: PLL calculation for S32k312 你好,森伦特、 实际上,S32k312 的核心时钟频率为 120Mhz。 Re: PLL calculation for S32k312 Hi@mogilipuri_harish FXOSC 的频率可以从 8MHz 到 40MHz,所以 40MHz 的晶振应该没问题。 您可以使用"S32 Design Studio for S32 Platform" 设置时钟树。 例如: PS: 我们提供的 S32K312EVB 使用 16MHz 外部晶振
記事全体を表示
SFPモジュールがLinuxで動作しない 現在、カスタム LS1046A ベースのボードの立ち上げ作業の真っ最中で、Linux を正常に起動できるまでになりました (lsdk2108_yocto_tiny_LS_arm64.itb を使用)。 現在直面している問題は、SFP モジュールがスイッチとのリンクを確立しないということですが、Linux の u-boot でのみ正常に動作します。 出力は次のとおりです。 [ 2.105567] sfp sfp-xfi0: Host maximum power 3.0W [ 2.110647] sfp sfp-xfi1: Host maximum power 3.0W [ 2.133460] fsl_dpaa_mac 1ae2000.ethernet eth0: Probed interface eth0 [ 2.158141] fsl_dpaa_mac 1ae8000.ethernet eth1: Probed interface eth1 [ 2.182874] fsl_dpaa_mac 1aea000.ethernet eth2: Probed interface eth2 [ 2.207768] fsl_dpaa_mac 1af0000.ethernet eth3: Probed interface eth3 [ 2.232690] fsl_dpaa_mac 1af2000.ethernet eth4: Probed interface eth4 [ 2.239517] clk: Disabling unused clocks [ 2.244553] Freeing unused kernel memory: 3008K [ 2.249175] Run /init as init process INIT: version 2.99 booting Starting udev [ 2.358215] udevd[125]: starting version 3.2.10 [ 2.434319] sfp sfp-xfi0: module FLEXOPTIX P.8596.02 rev A sn F7B2H4B dc 240827 [ 2.488055] sfp sfp-xfi1: module FLEXOPTIX P.C30.1 rev 1.0 sn F7B0V11-B dc 240722 [ 2.495775] hwmon hwmon6: temp1_input not attached to any thermal zone [ 3.394590] random: crng init done [ 3.401138] udevd[126]: starting eudev-3.2.10 [ 3.442182] fsl_dpaa_mac 1ae2000.ethernet fm1-mac2: renamed from eth0 [ 3.483254] fsl_dpaa_mac 1ae8000.ethernet fm1-mac5: renamed from eth1 [ 3.514694] fsl_dpaa_mac 1aea000.ethernet fm1-mac6: renamed from eth2 [ 3.538708] fsl_dpaa_mac 1af0000.ethernet fm1-mac9: renamed from eth3 [ 3.566712] fsl_dpaa_mac 1af2000.ethernet fm1-mac10: renamed from eth4 ご覧のとおり、挿入された両方のモジュールが正しく検出され、いずれのインターフェースでも問題は報告されておらず、起動すると正常に動作します。 root@TinyLinux:~# ip link set fm1-mac9 up [ 14.332682] fsl_dpaa_mac 1af0000.ethernet fm1-mac9: configuring for inband/10gbase-kr link mode root@TinyLinux:~# ip link set fm1-mac10 up [ 19.500673] fsl_dpaa_mac 1af2000.ethernet fm1-mac10: configuring for inband/10gbase-kr link mode root@TinyLinux:~# ip a 1: lo: mtu 65536 qdisc noqueue qlen 1000 link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00 inet 127.0.0.1/8 scope host lo valid_lft forever preferred_lft forever 2: fm1-mac2: mtu 1500 qdisc noop qlen 1000 link/ether 00:04:9f:08:06:4a brd ff:ff:ff:ff:ff:ff 3: fm1-mac5: mtu 1500 qdisc noop qlen 1000 link/ether 00:04:9f:08:06:4b brd ff:ff:ff:ff:ff:ff 4: fm1-mac6: mtu 1500 qdisc noop qlen 1000 link/ether 00:04:9f:08:06:4c brd ff:ff:ff:ff:ff:ff 5: fm1-mac9: mtu 1500 qdisc mq qlen 1000 link/ether 00:04:9f:08:06:4d brd ff:ff:ff:ff:ff:ff 6: fm1-mac10: mtu 1500 qdisc mq qlen 1000 link/ether 00:04:9f:08:06:4e brd ff:ff:ff:ff:ff:ff デバイス ツリーでどのモードを試しても、キャリアなしになる理由がわかりません。xfi、xsgmii、10gbase-r を試しましたが、何も機能しません。 お知らせ下さい。 QorIQ LS1デバイス Re: SFP module not working in Linux Serdes クロックをどのように設定しますか?私も興味があります Re: SFP module not working in Linux こんにちは 、 私たちも同じ問題に直面しています。私たちは、serdes1 レーン 1 上の LX2160ardb ベースのカスタム開発ボードに 10G の物理インターフェースを導入しています。ケージは検出できますが、リンクを確立できません。また、SerDes リファレンス クロックを 156.25Mhz に設定しました。 ありがとう Re: SFP module not working in Linux 後世のために: 問題を修正しました。クロック MUX を低く駆動していたピンの RCW を構成するのを忘れていたため、必要な156.25 MHzではなく、 100 MHz のクロックが Serdes リファレンス クロック入力に供給されていたことが判明しました。RCW を修正した後、すべてが正常に動作するようになりました。
記事全体を表示
关于 ADC 通道分配 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好,社区 在数据表 99 中分配给 ADC1_IN0 至 ADC1_IN3。 另一方面,在《参考手册》的 ADC 存储器映射中,ADC1 有 CH_A 到 CH_D。 是否可以将通道 0 指定为 CHA_SEL,通道 1 指定为 CHB_SEL,通道 2 指定为 CHC_SEL,通道 3 指定为 CHD_SEL,以支持以下操作? IN0-CH_A IN1-CH_B IN2-CH_C IN3-CH_D 顺祝商祺! 请访问 i.MX7 双核 About ADC channel assignment 你好,伊戈尔帕季科夫。 这是一个解决方案,但我不明白,所以我有一个问题。 根据数据手册中的引脚分配,ADC1_IN0 至 ADC2_IN3 共有八个物理输入端。 在参考手册中,adcx_ch_A_CFG1 的 CHA_SEL 的范围从 0 到 15。 ADC1_INx 和 Channelx 对应的是什么? 还是它们互不相关? 应如何设置 ADC2_IN0? 顺祝商祺! Re: About ADC channel assignment <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 后藤 是的,这是可能的。如第 14.1.1 节所述概述 i.MX 7Dual 应用处理器参考手册 "ADC 最多支持五个逻辑组(ChA / ChB / ChC / ChD / SW)的转换。每组可从 0 - 15 个物理通道中选择一个通道 。" 问候 igor ----------------------------------------------------------------------------------------------------------------------- 注:如果本帖回答了您的问题,请点击 "正确答案 "按钮。Thank you! -----------------------------------------------------------------------------------------------------------------------
記事全体を表示
如何使用 s32k144 aips? HI 我需要动态保护和解除保护闪存。 因此,我研究了 MPU、闪存保护寄存器和 AIPS。 无法解决 MPU 和闪存保护寄存器问题。 而 AIPS(外设访问保护)的解释不足以在 RM 中使用。 我认为 OPACR 中的 wp bits 与此有关。 但我不知道每个 wp 位都指向哪里。 请详细说明如何使用 AIPS? 谢谢! 顺祝商祺! 菲利普 Re: How to use s32k144 aips? 你好,@minsky、 您能创建一个新的主题吗? Re: How to use s32k144 aips? 你好,请问外设的访问控制如何确定在哪个寄存器的哪个插槽中? Re: How to use s32k144 aips? 你好,菲利普、 X "表示 S32K1 衍生型号上有外设访问控制。 FTFC 的外设访问控制位于 OPACRA 的 0 号插槽。 这取决于您的要求,如果您想保护 FTFC 寄存器不被写入,则设置 OPACRA[WP0] = 1。 此致, 丹尼尔 Re: How to use s32k144 aips? 你好,丹尼尔 X'是什么意思? 您想对哪些外设寄存器进行写保护? :我想对 FTFC 进行写保护。 因此,应该是 OPACR Slot1。 但我该如何保护呢? 谢谢! 顺祝商祺! 菲利普 Re: How to use s32k144 aips? 你好,菲利普、 您想对哪些外设寄存器进行写保护? 请参阅 RM 随附的S32K1xx_Mamory_Map.xlsx。 此致, 丹尼尔
記事全体を表示
リモートアクティベーションサーバーへのアクティベーション要求の送信中にエラーが発生しました NXPソフトウェアアクティベーション リモート アクティベーション サーバーにアクティベーション要求を送信し、結果の応答をプロセッシングするときにエラーが発生しました。ライセンス サーバーまたは Operations サーバーに接続できませんでした。(FNPエラー50041,41143,34) これはオンライン インストール中です、オフライン インストールも実行されていません、無効なオフライン応答、応答タイプが表示されています 回复: Error sending an activation request to a remote activation server S32 Design Studio for ARM バージョン 2.2 のインストール中に、「リモート アクティベーション サーバーにアクティベーション要求を送信し、結果の応答を処理中にエラーが発生しました。」というエラーが発生しました。ライセンス サーバーまたは Operations サーバーへの接続に失敗しました。(FNPエラー50041,41143,34)の問題を解決するにはどうすればよいですか?以下はログです。 Re: Error sending an activation request to a remote activation server ありがとうございます。解決しました。公式サイトを参考にしました。 https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32-Design-Studio-Offline-activation-issue-hot-fix/ta-p/1119120 Re: Error sending an activation request to a remote activation server これはインストール ログです。 Re: Error sending an activation request to a remote activation server これはログ内のエラー メッセージですが、管理者として実行しています。 Re: Error sending an activation request to a remote activation server これはオフラインの状況です Re: Error sending an activation request to a remote activation server こんにちは、 どのアプリケーションをアクティブ化しようとしているのかを教えていただけますか?また、エラーの画像を共有していただけますか? ぜひお知らせください。
記事全体を表示
ksz8863およびlwipとのインターフェースとなるLPC1768 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ハイ LPC1768 をリファレンス デザインとして使用すると、lwip tcp の例で問題なく動作します。 UDP の例では、Windows アプリからデータを送受信 CAN。 Microchip の 3 ポート スイッチ ksz8863 を LPC1768 にコネクテッドしましたが、udp が動作しません。 ステータスは次のとおりです: 1.スイッチへのリンクがあり、PHYレジスタを読み取るのと同じコードで読み取ることができます(mdioとmdcはfunc1です) 2. ビットバン、SMI、MIIを使用してチップにアクセスできます(mdioとmdcをgpio - func0に変更します) 3. スイッチで PHY モードではなく MAC モードを使用しようとしましたが、どちらも機能しませんでした。 マイクロコントローラにイーサネット・スイッチをコネクテッドして lwip を操作した人はいますか? コードに変更を加える必要はありますか? スイッチを phymore モードまたは mac モードで動作するように設定する必要がありますか (念のため) 質問はLPC1768 + ksz8863 + lwip + udpに直接CAN ただし、任意のマイクロ コントローラ -> ポート スイッチ -> lwip + udp にも適用されます。 どのような情報でも歓迎します。 よろしくお願いします。 LPC17xx LPCOpen Re: LPC1768 to interface with ksz8863 and lwip 可能であれば、ksz8863とlpc1768のインターフェース図を共有してください。 Re: LPC1768 to interface with ksz8863 and lwip こんにちは、 KSZ8863 と LPC4088 をインターフェースすることも計画しています。同じシリーズの NXP の LPC1768 を使用したことがあるので、LPC4088 用のドライバを実装する際に役立つコードを共有していただけませんか? ご返信をお待ちしております。 よろしくお願いします。 ディーパク Re: LPC1768 to interface with ksz8863 and lwip <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 問題を発見しました emac_config.h内 PHYアドレスがある /* MII/RMIIにコネクテッドされたPHYアドレス */ #LPC_PHYDEF_PHYADDR 3 を定義する 物理アドレスは3であるべきである スイッチには3つのポートがあり、MIIは現在ポート3にコネクテッドされているため リファレンス・デザインではポート1にコネクテッドされていた これが唯一行うべき変更点です。
記事全体を表示
AH1902 アプリケーションのヒント UJA1169Aのデータシート(2020年5月12日改訂版)の12.2節では、AH1902アプリケーションヒント - ミニ高速CANシステムの基礎に関する文書について説明しています。 チップ UJA116xA。このドキュメントを NXP の Web サイトで見つけることができません。入手可能でしょうか? デイブ 回复: AH1902 Application hints 私も同じです。この文書は見つかりましたか?
記事全体を表示
AH1902 Application hints In the data sheet (Rev 1,12 May 2020) for the UJA1169A, section 12.2 describes a document, AH1902 Application Hints - Mini high speed CAN system basis chips UJA116xA. I am unable to find this document on the NXP website. Is it available? Dave 回复: AH1902 Application hints The same to me. Do you find this document now?
記事全体を表示
ADCチャネル割り当てについて <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、コミュニティの皆様 データシートの表99のADC1_IN0~ADC1_IN3に割り当てられます。 一方、リファレンスマニュアルのADCメモリマップでは、ADC1にはCH_AからCH_Dがあります。 以下をサポートするために、チャネル 0 を CHA_SEL、チャネル 1 を CHB_SEL、チャネル 2 を CHC_SEL、チャネル 3 を CHD_SEL に割り当てることは可能ですか? IN0-CH_A IN1-CH_B IN2-CH_C IN3-CH_D よろしくお願いいたします www.freescale.comのサイトに入って下さい i.MX7Dual About ADC channel assignment こんにちは、igorpadykovさん。 解決策なのですが、理解できないSO質問があります。 データシートのピン割り当てによると、ADC1_IN0 から ADC2_IN3 までの 8 つの物理入力があります。 リファレンスマニュアルでは、ADCx_CH_A_CFG1 の CHA_SEL の範囲は 0 ~ 15 です。 ADC1_INx と Channelx は何に対応していますか? それとも無関係でしょうか? ADC2_IN0はどのように設定すればよいでしょうか? よろしくお願いいたします。 Re: About ADC channel assignment <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは後藤 はい、可能です。14.1.1節で説明したように概要 i.MX 7デュアルアプリケーションプロセッサリファレンスマニュアル 「ADCは最大5つのロジックグループ(ChA / ChB / ChC / ChD / SW)をサポートします。各グループは1つのチャンネルを選択できます 0 〜 15 の物理チャネル。 よろしくお願いします イゴール ----------------------------------------------------------------------------------------------------------------------- 注: この投稿で質問が解決した場合は、「正解」ボタンをクリックしてください。ありがとう! -----------------------------------------------------------------------------------------------------------------------
記事全体を表示
PLL calculation for S32k312 hello team, i am using the S32K312 microchip in our design. can please help me to calculate the PLL output frequency. We are using 40 MHz external crystal oscillator. can you provide one example calculation? is it okay if you we are using 40 MHz crystal oscillator?  please provide the clock calculator for S32K312. Re: PLL calculation for S32k312 Hi @mogilipuri_harish , were you able to resolve this issue. i am also dealing with same issue. i do have exactly same configuration , using MCAL 6.0.0 for S32K312. facing error with "PLL ODIV2 = 2 " out of range Re: PLL calculation for S32k312 Hi@mogilipuri_hari sh Apart from the data sheet, there is no more guidance document for clock configuration As shown in the figure,the version RTD 2.0.1 and above have routines for S32K312 Re: PLL calculation for S32k312 hi  i am trying do this PLL clock calculation. can you given some notes how to do this calculation? like reference document. and i didn't find S32k312 example in tools, can you please share that it will be helpful to me. Re: PLL calculation for S32k312 Hi, for your reference,for example: PLL output frequency must be in range:640MHz~1,28GHz. Re: PLL calculation for S32k312 Hi, Didn't fully understand your question, do you mean which divider values can be changed? these parameters in the picture can be changed, you can view these clock tree configuration in S32 DS. Re: PLL calculation for S32k312 here what are the variable values we can change?? Re: PLL calculation for S32k312 thanks for reminding In S32K312, CORE_CLK=160Mhz can still run, but it is not recommended for customers to use this way, there will be unknown risks Re: PLL calculation for S32k312 hello senlent, actually core clock frequency for S32k312 is 120Mhz. Re: PLL calculation for S32k312 Hi@mogilipuri_harish The FXOSC can be from 8MHz to40MHz,so the 40MHz crystal oscillator should be ok. you can use "S32 Design Studio for S32 Platform" to set the clock tree. for example: PS:The S32K312EVB we provide uses a 16MHz external crystal oscillator
記事全体を表示
AH1902 应用提示 在 UJA1169A 的数据表(2020 年 5 月 12 日修订版 1)中,第 12.2 节介绍了一份文件,即 AH1902 应用提示 - Mini 高速 CAN 系统基础 芯片 UJA116xA。我无法在恩智浦网站上找到这份文件。有吗? 戴夫 回复: AH1902 Application hints 我也一样。你现在找到这份文件了吗?
記事全体を表示
How to use s32k144 aips? Hi I need to protect and unprotect the flash memory dynamicaly. So I studied MPU and Flash protection register and AIPS. MPU and Flash protection register cannot be solution. And the AIPS(peripheral access protection) explanation is not enough to use in RM. I think wp bits in OPACR is something related. But I can't figure out that each wp bits indicate to where. Can you please explain how to use AIPS in detail? Thanks Best Regards Phillip Re: How to use s32k144 aips? Hi @minsky, Can you create a new thread? Re: How to use s32k144 aips? Hi, how is the access control for a peripheral determined in which register in which slot? Re: How to use s32k144 aips? Hi Phillip, the 'X' means that the Peripheral Access Control is present on the S32K1 derivative. The Peripheral Access Control for FTFC is in OPACRA, Slot 0. It depends on your requirements, if you want to write-protect the FTFC registers agains any write, set OPACRA[WP0] = 1. Regards, Daniel Re: How to use s32k144 aips? Hi Daniel What does the 'x's mean? Which peripheral registers do you want to write-protect? : I want to write-protect the FTFC. So OPACR Slot1 would be the one. But how can I protect? Thanks Best Regards Phillip Re: How to use s32k144 aips? Hello Phillip, Which peripheral registers do you want to write-protect? Please refer to the S32K1xx_Mamory_Map.xlsx that is attached to the RM. Regards, Daniel
記事全体を表示
Error sending an activation request to a remote activation server NXP Software Activation Error sending an activation request to a remote activation server and processing theresulting response.Failed to connect to the license server or Operations server. (FNP error50041,41143,34) 这是在线安装,离线安装也不行,显示invalid offline response,response type 回复: Error sending an activation request to a remote activation server I encountered while installing S32 Design Studio for ARM Version 2.2, Error sending an activation request to a remote activation server and processing theresulting response . Failed to connect to the license server or Operations server. (FNP error 50041,41143,34) problem, how to solve it, here is the log Re: Error sending an activation request to a remote activation server thanks I have solved it, the official website referenced https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32-Design-Studio-Offline-activation-issue-hot-fix /ta-p/1119120 Re: Error sending an activation request to a remote activation server This is the installation log Re: Error sending an activation request to a remote activation server This is the log error message, but I'm running it as administrator Re: Error sending an activation request to a remote activation server This is offline situation Re: Error sending an activation request to a remote activation server Hi, Can you let us know which application you are trying to activate? Also, can you share an image of your error? Please, let us know.
記事全体を表示
About ADC channel assignment Hello,Community Assigned to ADC1_IN0 to ADC1_IN3 in Table 99 of the data sheet. On the other hand, in the ADC memory map of Reference Manual, ADC1 has CH_A to CH_D. Is it possible to assign Channel 0 to CHA_SEL, Channel 1 to CHB_SEL, Channel 2 to CHC_SEL, and Channel 3 to CHD_SEL to support the following? IN0-CH_A IN1-CH_B IN2-CH_C IN3-CH_D best regards Goto i.MX7Dual About ADC channel assignment Hello igorpadykov. This is a solution, but I don't understand it, so I have a question. According to the pin assignment in the datasheet, there are eight physical inputs, ADC1_IN0 to ADC2_IN3. In the reference manual, CHA_SEL of ADCx_CH_A_CFG1 ranges from 0 to 15. What do ADC1_INx and Channelx correspond to? Or are they unrelated? How should I set ADC2_IN0? Best regards. Re: About ADC channel assignment Hi Goto yes this is possible. As described in sect.14.1.1 Overview i.MX 7Dual Applications Processor Reference Manual "ADC supports conversion up to five logic groups (ChA / ChB / ChC / ChD / SW). Each group can select one channel from 0 - 15 physical channels." Best regards igor ----------------------------------------------------------------------------------------------------------------------- Note: If this post answers your question, please click the Correct Answer button. Thank you! -----------------------------------------------------------------------------------------------------------------------
記事全体を表示
s32k144 aips の使い方は? ハイ フラッシュメモリを動的に保護したり保護解除したりする必要があります。 SO、MPU とフラッシュ保護レジスタ、AIPS について勉強しました。 MPU およびフラッシュ保護レジスタは解決できません。 また、AIPS(ペリフェラルアクセス保護)の説明は、RM で使用するには不十分です。 OPACR の wp ビットは関連していると思います。 しかし、各 wp ビットがどこを示しているのかわかりません。 AIPSの使い方を詳しく教えていただけますか? よろしくお願いします。 よろしくお願いいたします。 フィリップ Re: How to use s32k144 aips? こんにちは@minsky 、 新しいThreadを作成していただけますか? Re: How to use s32k144 aips? こんにちは。周辺機器のアクセス制御では、どのレジスタとどのスロットにあるかをどのように決定するのでしょうか? Re: How to use s32k144 aips? こんにちは、フィリップ。 「X」は、S32K1 派生製品にペリフェラル アクセス制御が存在することを意味します。 FTFC の周辺アクセス制御は、OPACRA のスロット 0 にあります。 要件によって異なりますが、FTFCレジスタを書き込みから保護する場合は、OPACRA[WP0] = 1を設定します。 よろしくお願いいたします。 ダニエル Re: How to use s32k144 aips? こんにちは、ダニエル 「x」は何を意味していますか? どのペリフェラルレジスタを書き込み保護しますか? : FTFC を書き込み禁止にしたいです。 SO OPACR Slot1 が該当します。 でもどうやってCAN? よろしくお願いします。 よろしくお願いいたします。 フィリップ Re: How to use s32k144 aips? こんにちは、フィリップ。 どのペリフェラルレジスタを書き込み保護しますか? RM に添付されているS32K1xx_Mamory_Map.xlsxを参照してください。 よろしくお願いいたします。 ダニエル
記事全体を表示
S32k312のPLL計算 こんにちは、チーム 私たちのデザインでは S32K312 マイクロチップを使用しています。PLL 出力周波数の計算を手伝っていただけますか。40 MHz の外部水晶発振器を使用しています。CAN計算例を一つ教えていただけますか?40MHzの水晶発振器を使用しても大丈夫でしょうか? S32K312 用のクロック計算機を提供してください。 Re: PLL calculation for S32k312 こんにちは@mogilipuri_harish 、この問題は解決できましたか。私も同じ問題を抱えています。私もまったく同じ構成で、S32K312 に MCAL 6.0.0 を使用しています。 「PLL ODIV2 = 2」が範囲外のためエラーが発生しました Re: PLL calculation for S32k312 こんにちは @mogilipuri_hari sh データシート以外に、クロック設定に関するガイダンス文書は存在しません。 図に示すように、RTD 2.0.1以降のバージョンにはS32K312用のルーチンがあります。 Re: PLL calculation for S32k312 こんにちは この PLL クロックの計算を試みています。この計算のやり方について、いくつかメモをCANいただけますか?参考資料のようなもの。ツール内に S32k312 の例が見つからなかったのですが、役立つと思うので共有していただけますか。 Re: PLL calculation for S32k312 こんにちは、 参考までに、例えば: PLL 出力周波数は 640MHz ~ 1.28GHz の範囲内である必要があります。 Re: PLL calculation for S32k312 こんにちは、 質問を完全に理解できませんでした。どの仕切り値を変更CANかということでしょうか? 画像内のこれらのパラメータはCAN変更可能で、S32 DS でこれらのクロック ツリー構成を表示できます。 Re: PLL calculation for S32k312 ここで変更できる変数値は何ですか? Re: PLL calculation for S32k312 思い出させてくれてありがとう S32K312ではCORE_CLK=160Mhzでも動作可能ですが、お客様がこの方法を使用することは推奨されません。未知のリスクがあります。 Re: PLL calculation for S32k312 こんにちは、センレントさん 実際、S32k312 のコアクロック周波数は 120Mhz です。 Re: PLL calculation for S32k312 こんにちは@mogilipuri_harish FXOSC は 8MHz から 40MHz までCAN、SO、40MHz の水晶発振器でも問題ないはずです。 「S32 Design Studio for S32 プラットフォーム」を使用してクロックツリーを設定できます。 以下にその例をご紹介します。 PS:当社が提供するS32K312EVBは16MHzの外部水晶発振器を使用しています
記事全体を表示
SFP module not working in Linux We're in the middle of bringing up a custom LS1046A-based board and we've gotten far enough to boot into Linux successfully (using lsdk2108_yocto_tiny_LS_arm64.itb). The problem we're facing currently is that SFP modules will not establish a link with the switch, but only in Linux, in u-boot, it works fine. Here's the output: [ 2.105567] sfp sfp-xfi0: Host maximum power 3.0W [ 2.110647] sfp sfp-xfi1: Host maximum power 3.0W [ 2.133460] fsl_dpaa_mac 1ae2000.ethernet eth0: Probed interface eth0 [ 2.158141] fsl_dpaa_mac 1ae8000.ethernet eth1: Probed interface eth1 [ 2.182874] fsl_dpaa_mac 1aea000.ethernet eth2: Probed interface eth2 [ 2.207768] fsl_dpaa_mac 1af0000.ethernet eth3: Probed interface eth3 [ 2.232690] fsl_dpaa_mac 1af2000.ethernet eth4: Probed interface eth4 [ 2.239517] clk: Disabling unused clocks [ 2.244553] Freeing unused kernel memory: 3008K [ 2.249175] Run /init as init process INIT: version 2.99 booting Starting udev [ 2.358215] udevd[125]: starting version 3.2.10 [ 2.434319] sfp sfp-xfi0: module FLEXOPTIX P.8596.02 rev A sn F7B2H4B dc 240827 [ 2.488055] sfp sfp-xfi1: module FLEXOPTIX P.C30.1 rev 1.0 sn F7B0V11-B dc 240722 [ 2.495775] hwmon hwmon6: temp1_input not attached to any thermal zone [ 3.394590] random: crng init done [ 3.401138] udevd[126]: starting eudev-3.2.10 [ 3.442182] fsl_dpaa_mac 1ae2000.ethernet fm1-mac2: renamed from eth0 [ 3.483254] fsl_dpaa_mac 1ae8000.ethernet fm1-mac5: renamed from eth1 [ 3.514694] fsl_dpaa_mac 1aea000.ethernet fm1-mac6: renamed from eth2 [ 3.538708] fsl_dpaa_mac 1af0000.ethernet fm1-mac9: renamed from eth3 [ 3.566712] fsl_dpaa_mac 1af2000.ethernet fm1-mac10: renamed from eth4 As you can see, both modules that are inserted are correctly detected, no issues reported on any of the interfaces either, if I bring them up, they work fine: root@TinyLinux:~# ip link set fm1-mac9 up [ 14.332682] fsl_dpaa_mac 1af0000.ethernet fm1-mac9: configuring for inband/10gbase-kr link mode root@TinyLinux:~# ip link set fm1-mac10 up [ 19.500673] fsl_dpaa_mac 1af2000.ethernet fm1-mac10: configuring for inband/10gbase-kr link mode root@TinyLinux:~# ip a 1: lo: mtu 65536 qdisc noqueue qlen 1000 link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00 inet 127.0.0.1/8 scope host lo valid_lft forever preferred_lft forever 2: fm1-mac2: mtu 1500 qdisc noop qlen 1000 link/ether 00:04:9f:08:06:4a brd ff:ff:ff:ff:ff:ff 3: fm1-mac5: mtu 1500 qdisc noop qlen 1000 link/ether 00:04:9f:08:06:4b brd ff:ff:ff:ff:ff:ff 4: fm1-mac6: mtu 1500 qdisc noop qlen 1000 link/ether 00:04:9f:08:06:4c brd ff:ff:ff:ff:ff:ff 5: fm1-mac9: mtu 1500 qdisc mq qlen 1000 link/ether 00:04:9f:08:06:4d brd ff:ff:ff:ff:ff:ff 6: fm1-mac10: mtu 1500 qdisc mq qlen 1000 link/ether 00:04:9f:08:06:4e brd ff:ff:ff:ff:ff:ff I don't understand why no-carrier, regardless which mode I try in the device tree, I've tried xfi, xsgmii, 10gbase-r, nothing works. Please advise. QorIQ LS1 Devices Re: SFP module not working in Linux How do you configure the serdes clock? I am also interested Re: SFP module not working in Linux Hello , We too are facing the same issue. We are bringing up 10G phyless interface on LX2160ardb based custom developed board on serdes1 lane1. We are able to detect the cage but unable to bring link up. We have also configured serdes reference clock for 156.25Mhz. Thank you Re: SFP module not working in Linux For posterity; We fixed the issue, turns out that we forgot to configure RCW for the pin that was driving our clock mux low, which fed 100 Mhz clock into the Serdes reference clock input, rather than 156.25 MHz that it needs. After we fixed RCW, everything started to work properly.
記事全体を表示
Coexistence of RW612 #RW612 Based on the documentation regarding coexistence for RW61x, here is the link: Coexistence Overview for RW61x  ,it is evident that Bluetooth LE and 802.15.4 cannot coexist. The coexistence details primarily focus on two modes: one involving Wi-Fi and Bluetooth LE, and the other involving Wi-Fi and 802.15.4. Therefore, my inquiry pertains to the feasibility of utilizing Wi-Fi, Bluetooth, and 802.15.4 concurrently in my project based on RW612. In the event that simultaneous operation is not feasible, is there a potential scenario where the application initiates with a work mode featuring Wi-Fi and 802.15.4, transitioning to a Wi-Fi and Bluetooth LE mode upon the need for Bluetooth configuration (e.g., triggered by a user pushing a configuration button), and subsequently reverting back to the initial Wi-Fi and 802.15.4 mode once the configuration is completed? Evaluation Board Re: Coexistence of RW612 OK Thanks! Re: Coexistence of RW612 Dear @yongqiangtang123 , FRDMRW612 is OK for you. so download it's SDK, please! About evaluation board of RW612, yes, it is not showed in hardware list. Thanks! Regards, weidong Re: Coexistence of RW612 Dear Weidong, It seems that only the information about FRDMEW612 can be found on the official website, and there is no relevant introduction about RW612 - EVK. Do you have this information on your side? Thank you! Best regards, YongQiang Re: Coexistence of RW612 Dear @yongqiangtang123 , FRDMRW612 & RW612-EVK board are both OK for you. You can select one of them. --FRDMRW612 is for customer's solution expansion, which is main streaming product. --RW612-EVK board is demonstrate all kinds of RW612 feature for customers. Anyway, as long as there exists what you are concern in SDK, it is enough for you. Thanks! Regards, weidong Re: Coexistence of RW612 Dear Weidong, Thank you very much for your response! You've provided a wealth of the details I need. There's just one more thing I'd like to confirm. Which discovery board should I select? Perhaps the FRDMRW612?I noticed that this board has a PCB antenna and a u.FL connector. I'm wondering if one is for Wi - Fi and the other is for BLE/802.15.4. If so, we can test each of the three radios individually and also test their coexistence. Thank you! Best regards, YongQiang Re: Coexistence of RW612 Dear @yongqiangtang123 , Please use 2.16_100 version of SDK, don't use 24.12, See the screenshot!   Then find middleware/wireless/coex/examples/coex_app ### 3. Build coex examples: Modify these macros to generate different coexistence images, | coexistence images | COEX_ENABLE_WIFI | COEX_ENABLE_BLE | COEX_ENABLE_OT | Simulation Case | | ------------------ | ---------------- | --------------- | -------------- | ------------------------ | | WiFi + BLE | ON | ON | OFF | Matter over WiFi | | WiFi + OT | ON | OFF | ON | / | | BLE + OT | OFF | ON | ON | Matter over Thread | | WiFi + BLE + OT | ON | ON | ON | Matter over WiFi + OT BR | > NOTE: If building BLE+OT, the ot libs should set `DOT_NXP_ENABLE_WPA_SUPP_MBEDTLS` to `OFF`. Modify these options according to your needs, | Options | Value | | ------------------ | ------------------------------------------------------------------------------------------------------- | | COEX_NXP_BASE | `edgefast` (default) - base on edgefast-shell | | COEX_EXAMPLE_BOARD | `rdrw612bga` (default) - RW612-BGA, `frdmrw612` - FRDMRW612 | | CMAKE_BUILD_TYPE | `flash_debug`(default), `flash_release` (**Use this option if you need to test throughput.**) | ...... these information should be helpful for your applications, check it carefully, please! About zigbee examples:   middleware/wireless/zigbee Thanks! Regards, weidong Re: Coexistence of RW612 Hello Weidong, Thank you for your helpful response! Additionally, after downloading the SDK_24.12.00_FRDM-RW612 from https://mcuxpresso.nxp.com/en/dashboard, I noticed that I could only find examples related to the coexistence of Wi-Fi and BLE. Could you please provide examples related to Zigbee 3.0 and the coexistence of Wi-Fi, BLE, and 802.15.4? Thank you! Best Regards, YongQiang Re: Coexistence of RW612 Dear @yongqiangtang123 , I checked your questions with internal team. Maybe you see the description in the Application Note.  >>In this document and for RW612 only, Bluetooth LE/802.15.4 represents Bluetooth LE or 802.15.4 as both radios cannot coexist. It means that BLE & 802.15.4 share the same RF Radio internally, BLE and 802.15.4 use the same RF Radio in time-division. So for RW612, WiFi, BLE, and 802.15.4 can be designed to work simultaneously. [Note] In SDK document, there are 2 commands to configure coexistence. -- wlan-single-ant-duty-cycle --wlan-dual-ant-duty-cycle Thanks! Regards, weidong Re: Coexistence of RW612 Hi , In spite of the age of this post, I was hoping you could provide non-secure access to this repo. git clone ssh://[email protected]/connint/ot-nxp.git -b ot-nxp-devel  Results in: ssh: connect to host bitbucket.sw.nxp.com port 22: Connection refused fatal: Could not read from remote repository. Please make sure you have the correct access rights and the repository exists. Also Cloning into 'ot-nxp'... fatal: unable to access 'http://bitbucket.sw.nxp.com/connint/ot-nxp.git/': gnutls_handshake() failed: Handshake failed I need to work with WIFI and BLE at the same time on an RW612 using SDK v2.16and was hoping for as many examples as possible. Thank you.
記事全体を表示