Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
HSE INSTALL S32K311 下面的所有内容都是从附件中复制 S32DS版本:S32DS.3.5_b220726_win32.x86_64 (1).exe RTD版本:SW32K3_RTD_R21-11_3.0.0_P07_D2306_DS_updatesite.zip S32K311支持包版本:SW32K3_S32DS_3.5.6_D2309.zip SBAF版本:SBAF_S32K311_0_0_15_0, Bin文件:s32k311_Secure_Baf_0.12.0_0.15.0.6_pb230804.bin.pink HSE版本:HSE_FW_S32K311_0_2_40_0, bin文件为s32k311_hse_fw_0.12.0_2.40.0_pb230730.bin.pink 使用FULL_MEM 没有安全启动 当前遇到的一个问题 程序运行会一直卡在这里while ( FALSE == HSE_CheckStatus(HSE_STATUS_INIT_OK) ); 图片3.png   图片4.png 图片1.png 图片5.png   图片6.png   图片2.png      Re: HSE INSTALL S32K311 这个是补充的printf信息 DCMROF21: 0x00040000 HSE GPR3: 0x000000C0 Current_SBAF_Version-0x4039c020: 0x00000C00 LC 配置字-0x4039C02C: 0x00000000 生命周期相关信息-0x402AC200: 0x00000000 HSE Status: 0x00000000 我从网上查阅资料,是不是芯片出场自带的SBAF不识别我现在使用的HSE固件? Re: HSE INSTALL S32K311 我怀疑是SBAF没有将flash中的hse固件复制到hse_nvm中,如果是这个问题,我应该怎么解决 Re: HSE INSTALL S32K311 这个是我打印的数据 DCMROF21: 0x00040000 HSE GPR3: 0x000000C0 HSE Status: 0x00000000 HSE 固件未启动(NVM 空或固件损坏) 111.png Re: HSE INSTALL S32K311 嗨@iiiddd 请问能否提供 HSE_CONFIG_GPR3 (0x4039C028) 的值?位 0 表示 HSE 固件是否存在。 BR,VaneB Re: HSE INSTALL S32K311 我在编写 UTEST 时调用了 RTD 库。 gHsePort_FlsIf.writeApi(UTEST_BASE_ADDR,(uint8_t*)hseFwFeatureFlag,FW_FEATURE_FLAG_LEN); 将使用 FLS_MAX_VIRTUAL_SECTOR 定义。我的 RTD 库默认值为 135,但访问地址 0x1B000000UL 需要 136。我使用的RTD库与HSE不兼容吗? Re: HSE INSTALL S32K311 嗨@iiiddd HSE_CONFIG_GPR3[0] 位未设置,这表明设备上不存在 HSE 硬件。 作为参考,下图显示了为在 S32K311 设备上安装 HSE FW FULL_MEM 而配置的链接器文件示例: VaneB_0-1784568701705.png Re: HSE INSTALL S32K311 我在调试时发现 pflash 中有与 hse 固件对应的数据。你的意思是说,sbaf 未能将 pflash 中的固件复制到 hsenvm 中吗?如果这是问题所在,那么可能是什么原因造成的呢?
View full article
mc9s08qg8 代码战士(经典 IDE)v6.3 Windows 11 我下载了文件,但是无法安装,安装程序提示我的操作系统不兼容。我使用的是Windows 11系统。 Re: mc9s08qg8 code warrior (Classic IDE) v6.3 windows 11 你好, 要在Windows 11系统中使用CodeWarrior,请更新至v11.1版本。我正在寻找 MC9S08QG8 设备,并且有此版本可供选择。 您可以从此链接下载: CodeWarrior ® for MCUs (Eclipse IDE) 11.1 此致敬礼,路易斯
View full article
i.MX RT1050 Download Algorithm My current development environment is MCUXPRESSO IDE, using the i.MX RT1050. I understand that because the i.MX RT1050 doesn't have internal flash, an algorithm needs to be downloaded when using external flash. However, this downloaded algorithm is dependent on the chosen flash memory. Does the official documentation explain how to obtain the desired downloaded algorithm for quick and easy use? Re: i.MX RT1050 下载算法 Hi SDFDSFSF, We suggest you do it in the following order: 1. Select an external Flash download algorithm in the project properties. NXP provides some mainstream Flash download algorithms. You can right-click the project -> Properties -> MCU settings -> Memory details and select the NXP-supported flash driver: ShellyZhang_0-1783670863188.png The flash driver for MCUXpresso is usually located under nxp\LinkServer_xx.x.xx\binaries\Flash, with the .cfx extension. 2. If the selected Flash memory supports SFDP, try the SFDP driver first. In MCUXpresso, you can choose a driver like MIMXRT1050_SFDP_QSPI.cfx. The significance of this type of SFDP driver is that it reduces the dependence on specific part number-specific algorithms through flash self-describing parameters. 3. Create your own using a template. Please refer to the application manual : https://www.nxp.com/docs/en/application-note/AN13386.pdfGenerate a custom CFX file. When modifying it, key parameters should be derived from test results of the external flash datasheet and the flexspi_nor_polling demo in the SDK. In addition to the download algorithm, XIP/Boot Header configuration is also required. Please refer to Solved: Flash interface initialization - NXP Community. The above are the basic methods. You can provide more specific details, such as what model of Flash you are using, what specific difficulties you are encountering at this stage, and this will help you better. Best Regards, Shelly Zhang i.MX RT1050 下载算法 I'm using J-Link, and in MCUXpresso I selected MIMXRT1050_SFDP_QSPI.cfx. Download failed. Re: i.MX RT1050 下载算法 How can I create my own J-Link algorithm for the IMXRT1052 in the MCUXpresso IDE? My Flash file is WINBOD 25Q256JVEQ. My current MCUXpresso IDE version is MCUXpresso IDE v25.6. SDK_EVBK is version 26.06.00. I don't know which example program can be modified to generate the download algorithm I want. Re: i.MX RT1050 下载算法 Dear @SDFDSFSF , The reference example is located in the nxp/LinkServer directory, with the project name iMXRT1050_QSPI: ShellyZhang_0-1784857501325.png If your pinouts differ from the evaluation board, you will need to modify the pinout configuration. The Flash configuration also needs to be modified according to the datasheet. Please confirm the following: 1. Check if the Flash hardware pins are configured correctly. The FlexSPI pins must be configured according to the RT1050 hardware development manual : ShellyZhang_1-1784857962728.png Only group A or group B can be selected, and FlexSPI_DQS needs to be left floating. 2. Import the evkbimxrt1050_flexspi_nor_polling_transfer example into the SDK, and modify the flash configuration according to the flash datasheet. (This step can be omitted; it's only to verify that the flash configuration is correct.) 3. Modify the correct flash configuration in the iMXRT1050_QSPI project. Please refer to the following for this step. https://www.nxp.com/docs/en/application-note/AN13386.pdf Best Regards, Shelly Zhang Re: i.MX RT1050 下载算法 It's possible that your hardware pin configuration differs from the evaluation board. We suggest you modify the iMXRT1050_QSPI project to generate the cfx file yourself. Re: i.MX RT1050 下载算法 Is it okay if I use J-Link in the MCUXpresso IDE? I've seen some people say that the MCUXpresso IDE algorithm can only be used in CMSIS-DAP type emulators?
View full article
S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff I developed the program in S32DS. When trying to transmit CAN frames, only a short low-level pulse  is output on the TX pin, and the subsequent ID and data bits are truncated, so complete frames cannot be sent. No data is received by the USB-CAN analyzer, and the FlexCAN controller directly enters the bus-off state. I have checked clock configuration and register values, and tested different CAN channels, but the problem remains unsolved. I want to figure out which configuration parameter is set incorrectly. Thanks for your help. Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff Hi Julián, Thank you for your reply. I'd like to correct and add some important details to my earlier message, which was written in a hurry. Board: This is a third-party board (not an NXP EVB), model S32K148_REV2_Q144. Worth noting: I found errors in the seller's schematic (labeled transceiver position didn't match the actual PCB silkscreen), so the reference design documentation for this board may not be fully reliable. Official CAN example: I did try building Can_example_S32K148, but hit environment issues unrelated to CAN itself (missing toolchain/include paths, and finally a version mismatch error between Port_Ci_Port_Ip.h and Port_Ci_Port_Ip_Cfg.h — "different vendor ids"/"AutoSar Version Numbers are different"). This looks like an RTD package version mismatch with my own project, not an IDE version issue. I'll try to resolve it, but I don't think it's central to the hardware problem. New evidence (from my own project you already reviewed): I've done deeper verification with a logic analyzer since my last message: MB8 content is 100% correct — read directly from registers right after CDD_CanTransmit(): CS=0x0C080000 (CODE=0xC pending, DLC=8), ID=0x00400304 (>>18 = 0x10, matches config), DATA=0x01020304/0x05060708 (matches my 8-byte payload exactly). TX signal at the pin is correct too — probing PTE5 and the transceiver's TXD input simultaneously (200MHz logic analyzer), the two waveforms are identical, confirming the PCB trace is fine. But transmission aborts after only ~8-9 bit transitions (roughly SOF + a few arbitration bits), and the controller enters Bus-Off shortly after (ESR1 confirms FLTCONF=11, TXERRCNT increments each attempt). CANH/CANL show zero activity, even with the USB-CAN analyzer properly connected and 120Ω termination enabled (bus not floating). As a control test, I ran the same setup (floating vs. terminated) on a different, known-working STM32 board — CANH showed proper transitions once terminated. On my S32K148 board under identical terminated conditions, CANH/CANL remain completely flat. Same result on CAN1 (different pins/transceiver). Since MCU-side TXD is confirmed correct up to the transceiver input, but CANH/CANL never respond even with proper termination, I suspect the transceiver output stage (or something shared between both channels, e.g. supply transient behavior — I haven't been able to check this with a scope, only a logic analyzer). Questions: Does "TXD correct at transceiver input, but CANH/CANL completely flat under proper termination" more strongly suggest a transceiver hardware fault, or are there other common board-level issues (enable/standby circuit, supply decoupling) that could cause this exact symptom? Is it expected for FlexCAN to abort after only the first few arbitration bits (rather than completing the full frame and failing at the ACK slot) when there's no real bus activity? Want to confirm my understanding of the bit-monitoring mechanism. For the RTD version mismatch in the example project — is there a way to check which RTD version matches a given S32 Configuration Tool release, so I can get a matching example package? Thanks again for your help. Best regards, April Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff Hi Julián, I’m really surprised and thankful for your reply to my question.   I am using a self-designed hardware board; only the power supply circuit differs from the official EVB schematic, while the rest of the circuits are consistent with the reference design. I have tested the official CAN example project. I only configured CAN0 pins without enabling and configuring the PORT module inside the MCAL layer, and the project keeps failing to compile repeatedly.   The specific compile error is: " f../board/Port_Ci_Port_Ip_Cfg.h:47:10: fatal error: Port_Ci_Port_Ip_Types.h: No such file or directory".   I have this header file available in my self-configured project files, yet after importing this official example project, this header file is not generated automatically during code generation. Could this missing header file error be caused by mismatched IDE software versions? At present I’m developing on S32DS for S32 Platform, and I am downloading S32DS for ARM 2.2.2 to switch the development environment. Looking forward to your guidance.   Best regards,   April Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff Hello @April, From your project, configuration and routine seem to be correct. Could you please share if you are using an S32K148EVB from NXP, or if this is a custom design? Have you tried testing the Can_example_S32K148 project included within the RTD? You can simply add the CAN0 pins and disable loop back mode to enable Tx/Rx and test the routine.  Lastly, have you confirmed that both nodes (S32K148 and CAN analyzer) are set to the same bit timing and protocol configuration (CAN vs CAN FD)? You can use the following tool to calculate the values: MPC5xxx/S32Kxx/LPCxxxx: CAN / CAN FD bit timing calculation. If you are using a custom design, you can refer to the S32K148 EVB's schematic and Hardware Design Guidelines for S32K1xx for the CAN interface design and recommendations. Best regards, Julián Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff Hello @April, 1. Yes, this points to a transceiver fault, rather than module configuration. Can you check which transceiver is being used in your custom design? I'd recommend checking STB, EN, S, RS, WAKE, INH, or similar pins against the actual mounted transceiver. S32K148 EVB uses a UJA1132HW, however, if you are using something like a TJA1043, you must configure it to Normal mode (STB_N = high EN = high). 2.  Yes, early abort after a few arbitration bits is plausible if the transceiver is not actually driving the bus. 3. Usually, the "different vendor ids"/ "AutoSar Version Numbers are different" errors show up when importing a project, and trying to update the configuration with a different RTD / S32 Config Tool version, however, if you simply imported the example from "File -> New -> S32DS Project From Example", there should not be any compatibility issues: Julin_AragnM_0-1784738938507.png From the project you've shared, I can see you are using S32K1 RTD 3.0.0 QLP04, however, when I imported the project, I can see from properties that GCC 11.4 is configured: Julin_AragnM_1-1784739211073.png From RTD release notes, 3.0.0 QLP04 only supports NXP GCC 10.2: Julin_AragnM_3-1784739259075.png I'm not sure how you imported and compiled the project, but please make sure you have at least S32DS 3.6.4, and only one RTD package installed. S32DS does not support multiple RTD versions installed simultaneously. Best regards, Julián Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff Hello @April, Thank you for the additional information. 1. Regarding TJA1051, it is true this transceiver only has the S pin in order to configure normal mode, however, please check if you are using TJA1051T/E derivative, as this has an additional EN pin you must drive HIGH: Julin_AragnM_0-1784829788604.png 2. The 'File not found' error is most likely caused by a wrong Port configuration, and consequently, wrong code generation by the tool. The error you've shared in the Port container is caused because the 'Pins' functional group name should be named after 'Port container name' + 'Peripheral functional group name', in your case 'PortContainer_0_VS_0' Julin_AragnM_2-1784829995267.png Julin_AragnM_1-1784829932110.png Before requesting RMA, can you please test the project I've attached? It is a simple test code in MCAL, which enables Rx in interrupt, and Tx in polling mode. After 10 successful echoed frames, the green led is toggled.  I've tested the routine through the J11 CAN header, with a PCAN-USB analyzer, with the following settings: Julin_AragnM_3-1784830112924.png I can see the frames successfully being echoed, and the green led toggled every 10 frames: Julin_AragnM_4-1784830143208.png Since I've used S32K148-EVB, there is no need for transceiver enablement, however, in your setup, check that the TJA1051 is correctly enabled (and if it also needs EN pin to be enabled). Best regards, Julián Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff Hi Julián, Thanks again for your patience with this — a few updates since my last message. Transceiver check: I looked more closely and confirmed it's a TJA1051, not a UJA1132-series SBC. This one only has a single enable pin (S pin), which is hardwired to ground on my board (= Normal mode), so the multi-pin STB_N/EN logic you mentioned doesn't really apply here — that part of the control circuit already looks correct. Cross-check with a second, independent project: I built and ran a completely different CAN demo for this board (from the reseller, using the older Processor Expert/S32 SDK stack — can_pal — instead of RTD/AUTOSAR). Pressing the button correctly calls CAN_Send(), but I noticed the return value is consistently STATUS_BUSY (0x002), meaning the previous transmission never actually completes. And just like with my RTD project, the USB-CAN analyzer receives nothing at all, on all three channels. So now I have two completely independent driver stacks giving me the same result, which makes me fairly confident this isn't a software/config issue on my end. Regarding the official example project: I switched the GCC version back to 10.2 as you suggested, but I'm still hitting the same "file not found" errors during the build. I dug into it a bit more and I now suspect it might be related to the Port module (MCAL layer) not being fully configured — there seems to be a validation error tied to how the Port module and the Pins tool's functional group are linked, but I haven't been able to get it configured correctly no matter what I try.  April_4-1784786142962.png they are form example: April_0-1784785801363.png April_1-1784785825602.png This is from the project I built myself earlier: April_2-1784786013234.png April_3-1784786034737.png Given everything so far — control pin wiring looks correct, TXD is confirmed correct at the pin, and two independent software stacks show consistent "no bus activity" / stuck transmission behavior across all three channels — do you think this is solid enough to treat as a hardware fault and proceed with an RMA, or is there anything else worth checking first? Thanks again for all your help with this. Best regards, April Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff Hello @April, I'm really glad everything works as expected now!  May I know the reason for the previous error? Was it simple HW connections?  Have a nice day as well! Best regards, Julián Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff Hello @Julián_AragónM, Haha,It wasn’t wiring issues. The original TJA1051 transceiver module was defective and caused the BusOff issue. Again, thank you so much for all your help ! ^_^ Best regards, April Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff Hello Julián, I can’t wait to tell you that everything works perfectly now! I’m absolutely thrilled to share the good news. I’ve ordered brand new MCU boards and CAN transceivers for retesting, and the communication runs flawlessly this time. It turns out the constant BusOff error I ran into before was purely a hardware fault. I also loaded up the test project you attached, and it works great too. Your sample code can send and receive CAN frames smoothly just as you described. I really appreciate all the patient guidance you gave me these days. I was totally stuck and helpless troubleshooting this issue alone, and your detailed replies pulled me out of the mess. Wish you good health, smooth work, and happiness every day! Best regards, April
View full article
S32K148EVB-Q176 received with UJA1131 instead of UJA1132 Hi, I recently bought an S32K148EVB-Q176 board. According to the documentation and schematics, I expected it to come with a UJA1132, but the board I received has a UJA1131. Because of this, I only have one LIN interface, while I was expecting the features of the UJA1132. I just wanted to ask if this is normal. Are there different versions of the S32K148EVB-Q176 with different SBCs, or did I receive the wrong board? Thank you! Re: S32K148EVB-Q176 received with UJA1131 instead of UJA1132 Hello @sousou54, Thank you for the report. This issue is currently under investigation. Could you please provide a photo of the large white label located on the product box? The information on this label can help us identify the manufacturing details of the board. Since the label may contain product-specific information, you can share the photo through a private message or by opening a support case (Support) rather than posting it publicly. Best regards, Julián Re: S32K148EVB-Q176 received with UJA1131 instead of UJA1132 Hello @sousou54, Just to inform you, I've received your pictures, and I have forwarded to the appropriate team. I am waiting for a response. Thank you for your understanding and cooperation. Best regards, Julián Re: S32K148EVB-Q176 received with UJA1131 instead of UJA1132 Hi @sousou54, For further information on this matter, please contact your NXP representative, or distributor from which you bought this kit. They should be able to provide assistance. Best regards, Julián 
View full article
mc9s08qg8 コードウォリアー(クラシックIDE)v6.3 Windows 11 ファイルをダウンロードしましたが、インストールできません。インストーラーによると、私のOSが間違っているとのことです。私はWindows 11を使用していますか? Re: mc9s08qg8 code warrior (Classic IDE) v6.3 windows 11 こんにちは、 CodeWarriorをWindows 11で使用するには、バージョン11.1にアップデートしてください。MC9S08QG8というデバイスを探していたのですが、このバージョンが見つかりました。 こちらのリンクからダウンロードできます: CodeWarrior® for MCUS (Eclipse IDE) 11.1 敬具、ルイス
View full article
Training material(PPT and Video) list for S32K3 (until Jan. 2026) Hi,     After you login www.nxp.com and       请切换到ENGLISH模式      Snipaste_2026-02-02_16-10-05.png     点击下面链接 https://www.nxp.com/design/design-center/training:TRAINING-EVENTS?collection=trainings&start=0&max=12&sorting=sort_date.desc&parameters=TrainingType.Topics.deviceTax.applicationTax.country.region.application.TrainingLanguage.TrainingFormat.skillLevel.durationTime.provider&language=en&query=TrainingFormat%3E%3EOnline::training_date%3E%3E2026-02-02..*&keyword=s32k&siblings=false    You can get the following training topics with input the topic as searching keyword.  S32K3  Part 1 MKT Overview (DFAE Only) Training Presentation S32K3  Part 3 Hardware and Software Tools Overview (DFAE Only) Training Presentation S32K3  Part 5 RTD Overview and Demo (DFAE Only) Training Presentation S32K3 and MCSPTE1AK344 Motor Control Kit Training Presentation S32K3 Booting and Startup Process Memory (Chinese) Training Video S32K3 Debug Based on MCAL and FreeMASTER S32K3 Debug Based-On MCAL EB Freemaster (Chinese) Training Video S32K3 Debugging Skills Training Presentation S32K3 Deep Dive and Design Tips Part 1 Training Presentation S32K3 Deep Dive and Design Tips Part 2 Training Presentation S32K3 Deep Dive and Design Tips Part 3 Training Presentation S32K3 Deep Dive and Design Tips Part 4 Training Presentation S32K3 DFAE Day 1 Training Presentation S32K3 DFAE Day 2 Training Presentation S32K3 DFAE Training  HSE Security Aspects Day 2 S32K3 DFAE Training  Memory Link Boot Day 2 S32K3 DFAE Training Day 1 S32K3 Documents Location On Security Safety (Chinese) Training Video S32K3 Getting Started Training Presentation S32K3 How to Request Access to Safety Documentation S32K3 HSE Security Library Enablement Training Presentation S32K3 HSE-B with Demo (Chinese) Training Video S32K3 Memory Link Boot (Chinese) Training Video S32K3 Part 2 Architecture and Technical Overview DFAE Only Training Presentation S32K3 Part 4 K1 to K3 Hardware and Software Migration Guide DFAE Only Training Presentation S32K3 Safey Design Consideration Training Presentation S32K3 Software Enablement DFAE Training Part 1 S32K3 Software Enablement DFAE Training Part 1 - Auto MCU RTD Demo Porting Techniques S32K3 Software Enablement DFAE Training Part 1 - Getting Start with S32K RTD Features S32K3 Software Enablement DFAE Training Part 1 - HAL and EL demos Show S32K3 Software Enablement DFAE Training Part 1 - How to Import RTD MCAL to IAR project S32K3 Software Enablement DFAE Training Part 1 - How to Import RTD MCAL to S32DS project S32K3 Software Enablement DFAE Training Part 1 - How to Use GHS Complier Build S32K3 RTD MCAL S32K3 Software Enablement DFAE Training Part 1 - SW Commercial Offering HAL and EL Bundle S32K3 Software Enablement DFAE Training Part 2 S32K3 Software Enablement DFAE Training Part 2 - AUTOSAR and MCAL Architecture S32K3 Software Enablement DFAE Training Part 2 - MCAL Training AE S32K3 Software Enablement DFAE Training Part 2 - MCAL Training CAN S32K3 Software Enablement DFAE Training Part 2 - MCAL Training CRC S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Crypto S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Dio S32K3 Software Enablement DFAE Training Part 2 - MCAL Training DPGA S32K3 Software Enablement DFAE Training Part 2 - MCAL Training ETH S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Fee S32K3 Software Enablement DFAE Training Part 2 - MCAL Training GDU S32K3 Software Enablement DFAE Training Part 2 - MCAL Training I2C S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Icu S32K3 Software Enablement DFAE Training Part 2 - MCAL Training MCL S32K3 Software Enablement DFAE Training Part 2 - MCAL Training MCU S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Mem S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Mem Acc S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Mem Eep S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Mem EXFIs S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Mem INFIs S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Multicore S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Ocu S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Port S32K3 Software Enablement DFAE Training Part 2 - MCAL Training SPI S32K3 Software Enablement DFAE Training Part 2 - MCAL Training UART S32K3 Software Enablement DFAE Training Part 3 S32K3 Software Enablement DFAE Training Part 3 - Function Safety General S32K3 Software Enablement DFAE Training Part 3 - Hands-On Creating Projects with Multiple MCAL Modules S32K3 Software Enablement DFAE Training Part 3 - Hands-On Creating Projects with Multiple MCAL Modules S32K3 Software Enablement DFAE Training Part 3 - HSE Hands-On Workshop-S32K3 HSE Security Library Enablement S32K3 Software Enablement DFAE Training Part 3 - HSE Hands-On Workshop-S32K3 HSE Security Library Enablement S32K3 Software Enablement DFAE Training Part 3 - HSE NXP Security on S32K3 S32K3 Software Enablement DFAE Training Part 3 - HSE NXP Security on S32K3 S32K3 Software Enablement DFAE Training Part 3 - Integrating Safety with S32 Safety Software Framework S32K3 Software Enablement DFAE Training Part 3 - Introduction of S32K3 HSE and Debugging Techniques S32K3 T-BOX Business Training Presentation S32K3 Zonal Aggregators, Telematics Box and Communications Protocols Training Presentation GC DFAE Training S32K SW Day 5 Training Presentation Introduction to S32K Hardware Security Engine HSE Library and Debugging Techniques Training Presentation K3 booting and startup process           Re: Training material(PPT and Video) list for S32K3 (until Jan. 2026) 享受这些培训! 干杯 奥利弗 Re: Training material(PPT and Video) list for S32K3 (until Jan. 2026) 我现在在哪里可以找到这些材料? 回复: Training material(PPT and Video) list for S32K3 (until Jan. 2026) 现在看不见了。我需要crypto的配置视频
View full article
S32K148 FlexCAN 出力SOFパルスのみバスオフに入ります 私はこのプログラムをS32DSで開発しました。CANフレームを送信しようとする際、TXピンには短い低レベルパルスのみが出力され、その後のIDやデータビットが切り詰められるため、完全なフレームを送信できません。USB-CANアナライザーにはデータが受信されず、FlexCANコントローラは直接バスオフ状態に入ります。 クロック設定やレジスタ値を確認し、さまざまなCANチャネルも試しましたが、問題は解決していません。どの設定パラメータが誤って設定されているのかを突き止めたい。ご協力いただきありがとうございます。 Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff こんにちは、ジュリアンさん。 お返事ありがとうございます。先ほどのメッセージは急いで書いたため、いくつか重要な点を訂正し、追加したいと思います。 取締役会: これはサードパーティ製のボード(NXP EVBではありません)、モデルS32K148_REV2_Q144です。注意点として、販売者の回路図に誤り(ラベル付けされたトランシーバ位置が実際のPCBシルクスクリーンと一致しない)を見つけたため、この基板の**リファレンス・デザイン** **ドキュメント**は完全に信頼できるとは限りません。 公式CANの例: ビルドCan_example_S32K148試みましたが、CAN自体とは無関係な環境問題(ツールチェーンやインクルーパスの欠如、Port_Ci_Port_Ip.hとPort_Ci_Port_Ip_Cfg.hのバージョンミスマッチ—「異なるベンダーID」や「AutoSarバージョン番号が異なる」など)に遭遇しました。これは自分のプロジェクトとRTDパッケージのバージョンが不一致しているのであって、IDEの問題ではありません。解決しようと思いますが、ハードウェアの問題の中心ではないと思います。 新たな証拠(既にレビューいただいた私のプロジェクトから):前回のメッセージ以降、ロジックアナライザを使ってより詳細な検証を行いました。 MB8 の内容は 100% 正しいです。CDD_CanTransmit() の直後にレジスタから直接読み取った結果は次のとおりです。CS=0x0C080000 (CODE=0xC 保留中、DLC=8)、ID=0x00400304 (>>18 = 0x10、設定と一致)、DATA=0x01020304/0x05060708 (私の 8 バイトのペイロードと完全に一致)。 ピンのTX信号も正確で 、PTE5とトランシーバのTXD入力を同時に探査(200MHzロジックアナライザ)すると、2つの波形は同一であり、PCBトレースは問題ないことが確認できます。 しかし、送信はわずか8〜9ビットの遷移( おおよそSOF + 数ビットの仲裁ビット)で中止され、コントローラーは間もなくバスオフに入ります(ESR1がFLTCONF=11を確認し、TXERRCNTは各試みごとに増分します)。 CANH/CANLは、USB-CANアナライザーを正しく接続し、120Ω終端を有効にしていても(バスがフローティングしていない状態)でも、活動はゼロです。対照実験として、同じ設定(フローティング状態と終端状態)を別の正常に動作することが確認されているSTM32ボードで実行したところ、終端状態になるとCANHは適切な遷移を示しました。私のS32K148ボードでは、同一の終端条件下において、CANH/CANLは完全に平坦なままです。 CAN1でも同じ結果でした(ピンやトランシーバが違う)。 MCU側のTXDはトランシーバ入力まで正確であることが確認されていますが、CANH/CANLは適切な終端をしても応答しません。したがって、トランシーバの出力段階(または両チャネルで共有されている何か、例えば電源の過渡的な挙動については、オシロスコープでは確認できず、ロジックアナライザでしか確認できていません。 質問: 「TXDはトランシーバー入力で修正されるが、適切な終端でCANH/CANLは完全にフラット」というのは、トランシーバーのハードウェア故障を強く示唆するのでしょうか?それとも、他に一般的な基板レベルの問題(有効化/スタンバイ回路、電源デカップリング)がこの症状を引き起こす可能性があるのでしょうか? 実際のバスアクティビティがない場合、FlexCANは最初の数ビットのアービトレーション処理が完了した時点で(フレーム全体を完了してACKスロットで失敗するのではなく)処理を中止するのが想定される動作でしょうか?ビット監視メカニズムに関する私の理解を確認したいです。 サンプルプロジェクトのRTDバージョンの不一致についてですが、どのRTDバージョンが特定のS32構成ツールのリリースと一致しているか確認する方法はありますか?そうすれば、一致するサンプルパッケージを入手できます。 ご協力ありがとうございました。 よろしくお願いいたします、エイプリル Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff こんにちは、ジュリアンさん。 私の質問にご回答いただき、本当に驚き、そして感謝しています。   私は自作のハードウェアボードを使っています。公式のEVB回路と異なるのは電源回路のみであり、それ以外の回路はリファレンス・デザインと整合しています。 公式のCAN例プロジェクトもテストしました。MCALレイヤー内のPORTモジュールを有効化および設定せずにCAN0ピンのみを設定したところ、プロジェクトのコンパイルが繰り返し失敗します。   具体的なコンパイルエラーは次のとおりです。 「 f ../board/Port_Ci_Port_Ip_Cfg.h:47:10: fatal error: Port_Ci_Port_Ip_Types.h: そのようなファイルまたはディレクトリはありません"。   自分で設定したプロジェクトファイルにはこのヘッダーファイルが存在するのですが、公式のサンプルプロジェクトをインポートした後、コード生成時にこのヘッダーファイルが自動的に生成されません。 このヘッダーファイルの欠如エラーは、IDEソフトウェアのバージョンが不一致であることが原因かもしれませんか?現在は S32プラットフォーム用のS32DSで開発しており、開発環境を切り替えるために ARM 2.2.2用のS32DS をダウンロードしています。 ご指導をお待ちしております。   よろしくお願いいたします。   4月 Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff こんにちは、 @April さん。 プロジェクトを見る限り、設定と手順は正しいようです。NXPのS32K148EVBを使っているのか、それともカスタムデザインなのか教えていただけますか? RTDに含まれているCan_example_S32K148プロジェクトをテストしてみましたか?CAN0ピンを追加し、ループバックモードを無効にしてTx/Rxを有効にしてルーチンをテストするだけで済みます。 最後に、両方のノード(S32K148とCANアナライザー)が同じビットタイミングとプロトコル構成(CAN対CAN FD)に設定されているか確認しましたか?以下のツールを使って値を計算できます:MPC5xxx/S32Kxx/LPCxxxx: CAN / CAN FD ビットタイミング計算。 カスタム設計を使用する場合は、S32K148 EVBの回路図およびS32K1xxのハードウェア設計ガイドラインを参照して、CANインターフェース設計や推奨事項を確認できます。 よろしくお願いします、 ジュリアン Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff こんにちは、 @April さん。 1. はい、これはモジュール構成ではなくトランシーバの故障を示しています。カスタム設計で使われているトランシーバは確認できますか? I'd recommend checking STB, EN, S, RS, WAKE, INH, or similar pins against the actual mounted トランシーバ. S32K148 EVBはUJA1132HWを使用しますが、 TJA1043のようなものを使用する場合は、ノーマルモード( STB_N = high、 EN = high)に設定する必要があります。 2. はい、トランシーバが実際にバスを駆動していない場合、数ビットの仲裁後の早期中止は可能です。 3. 通常、「異なるベンダーID」や「AutoSarバージョン番号が異なる」というエラーは、プロジェクトをインポートし、異なるRTDやS32設定ツールのバージョンで設定を更新しようとした際に発生しますが、単に「File -> New -> S32DS Project From Example」から例をインポートした場合は、互換性の問題は起きないはずです。 Julin_AragnM_0-1784738938507.png 共有してくれたプロジェクトから、S32K1 RTD 3.0.0を使っているようですねしかし、プロジェクトをインポートしたところ、プロパティからGCC 11.4が設定されていることがわかります: Julin_AragnM_1-1784739211073.png RTDリリースノートより、3.0.0QLP04はNXP GCC 10.2のみをサポートしています: Julin_AragnM_3-1784739259075.png プロジェクトをどのようにインポートしてコンパイルしたのかはわかりませんが、少なくともS32DS 3.6.4がインストールされていることを確認してください。RTDパッケージは1つだけインストールされていました。S32DSは複数のRTDバージョンを同時にサポートしていません。 よろしくお願いします、 ジュリアン Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff こんにちは、ジュリアンさん。 この件に関して、引き続きご辛抱いただきありがとうございます。前回のメッセージ以降、いくつか更新情報があります。 トランシーバーチェック: よく見てみたら、UJA1132シリーズSBCではなく TJA1051であることが確認されました。このモデルはイネーブピン(Sピン)が1つだけで、ボードのアースにハードワイヤードされている(=ノーマルモード)ので、あなたが言及したマルチピンSTB_N/ENのロジックはここではあまり当てはまりません。制御回路のその部分はすでに正しく見えます。 別の独立したプロジェクトと照合してください: このボード用に全く異なるCANデモを作って実行しました(リセラーから、RTD/AUTOSARの代わりに古いプロセッサ Expert/S32 SDKスタック(can_pal)を使って)。ボタンを正しく押すとCAN_Send()が呼び出されますが、戻り値が常にSTATUS_BUSY(0x002)であることに気づきました。これは、前回の送信が実際には完了していないことを意味します。そして私のRTDプロジェクトと同様に、USB-CANアナライザーは3つのチャネルすべてで何も受信しません。つまり、完全に独立した2つのドライバースタックが同じ結果になっているので、これはソフトウェアや設定の問題ではないとかなり自信を持っています。 公式の例プロジェクトについて: ご提案通りGCCバージョンを10.2に戻しましたが、ビルド中に同じ「ファイルが見つかりません」エラーが出ます。さらに調べてみたところ、ポートモジュール(MCALレイヤー)が完全に設定されていないことに関係しているのではないかと疑っています。ポートモジュールとピンツールの機能グループの連携に関連した検証エラーがあるようですが、どんなに試しても正しく設定できていません。 April_4-1784786142962.png これらは例です。 April_0-1784785801363.png April_1-1784785825602.png これは私が以前自分で作ったプロジェクトからのものです。 April_2-1784786013234.png April_3-1784786034737.png これまでの状況を踏まえると、コントロールピンの配線は正確で、ピンのTXDも正確であることが確認され、2つの独立したソフトウェアスタックでも3つのチャネルすべてで一貫して「バス活動なし」/送信動作が止まっていることを示しています。これをハードウェアの故障として扱いRMAを進めるに値すると思いますか?それとも他に最初に確認すべき点はありますか? この件に関してご協力いただき、改めて感謝申し上げます。 よろしくお願いいたします、エイプリル Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff こんにちは、 @April さん。 追加情報ありがとうございます。 1. TJA1051に関して、このトランシーバはノーマルモードを設定するためにSピンのみを持っていますが、TJA1051T/E微分を使っている場合は、 HIGHを駆動しなければならない追加のENピンがあるので確認してください。 Julin_AragnM_0-1784829788604.png 2. 「ファイルが見つかりません」エラーは、ポート設定の誤り、ひいてはツールによるコード生成の誤りが原因である可能性が最も高いです。あなたが共有したポートコンテナのエラーは、「ピン」機能グループ名が 「ポートコンテナ名」+「ペリフェラル機能グループ」の後に名前付けされるべきであり、あなたの場合は「PortContainer_0_VS_0」と呼ばれています。 Julin_AragnM_2-1784829995267.png Julin_AragnM_1-1784829932110.png RMAを依頼する前に、添付したプロジェクトをテストしてもらえますか?これはMCALのシンプルなテストコードで、Rxを割り込みモードで、Txをポーリングモードで有効にします。10回のフレームのエコーが正常に完了すると、緑色のLEDが点滅します。 J11 CANヘッダーとPCAN-USBアナライザーでルーチンを以下の設定でテストしました: Julin_AragnM_3-1784830112924.png フレームが正常にエコーされているのが見え、緑色のLEDは10フレームごとに切り替えられていました: Julin_AragnM_4-1784830143208.png 私はS32K148-EVBを使っているのでトランシーバーのイネーブルメントは不要ですが、あなたの環境ではTJA1051が正しく有効になっているか(そしてENピンも有効化が必要かどうか)を確認してください。 よろしくお願いします、 ジュリアン Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff こんにちは、 @April さん。 すべてが期待通りに動作するようになって本当に嬉しいです! 先ほどのエラーの原因を教えていただけますか?単純なハードウェア接続だったのでしょうか? あなたも良い一日をお過ごしください! よろしくお願いします、 ジュリアン Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff こんにちは、ジュリアンさん。 すべてが完璧に動作していることをお伝えするのが待ちきれません!この朗報をお伝えできて、本当に嬉しいです。再テスト用に新しいMCUボードとCANトランシーバーを注文しましたが、今回は通信が完璧に動作しています。以前発生していた頻繁なBusOffエラーは、完全にハードウェアの故障だったことが判明しました。 添付していただいたテストプロジェクトも読み込んでみましたが、こちらも問題なく動作しました。サンプルコードは、あなたが説明した通り、CANフレームをスムーズに送受信できます。 この数日間、あなたが私に与えてくれた忍耐強い指導に本当に感謝しています。この問題の解決に一人では全く手詰まりで途方に暮れていましたが、あなたの詳細な回答のおかげで窮地から抜け出すことができました。 皆様のご健康と、仕事の順調な進行、そして毎日の幸せをお祈り申し上げます! よろしくお願いします、 4月 Re: S32K148 FlexCAN Only Output SOF Pulse then Enter BusOff こんにちは、 @Julián_AragónM さん、 ハハ、配線の問題じゃなかったよ。元のTJA1051トランシーバーモジュールは欠陥があり、BusOffの問題を引き起こしました。 改めて、たくさんの助けを本当にありがとうございます!^_^ よろしくお願いします、 4月
View full article
CSI demo question Hi, This is Bryan form Quectel FAE team. We are planning to prepare some CSI-related demos for the NXP trade show in September. Could you provide some assistance with demo examples? For instance, I noticed you have examples similar to motion detection — I would like to know how to analyze and work with the CSI data captured on our board.  We have rw610 && rw612 my email : [email protected] Re: CSI demo question Hi, @BryanNiu  By the way, to download our default SDK, you can just directly go to below link: Select Board | MCUXpresso SDK Builder Input and choose FRDM-RW612, then download the latest: SDK 26.06.00. Best regards, Christine. Re: CSI demo question Hi, @BryanNiu  For RW610 and RW612, both of them supports CSI. We already have demo in the default SDK release: wifi_cli example. The wifi_cli application is used to configure CSI generation and collection. The application is included in the SDK release. To generate CSI data, flash wi-fi_cli application onto the Wi-Fi device and run the following commands: wlan-set-csi-param-header wlan-set-csi-filter wlan-csi-cfg wlan-auto-null-tx For the details, you can refer to: AN14281: Channel State Information (CSI) on FreeRTOS | NXP Semiconductors Please let me know whether still have any other concerns on this case, if no, please do not hesitate to mark my answer as a solution for this thread. Best regards, Christine. Re: CSI demo question Hi @Christine_Li  Thank you for the information. We have successfully run the basic wifi_cli example from the SDK. We would like to go further and analyze CSI data to develop a demo. I came across the following repository for CSI motion detection on the RW61x — would this demo be compatible with our module? https://github.com/nxp-appcodehub/dm-motion-detection-using-wifi-csi-on-rw61x  Or is there a similar demo you could recommend? Thanks  Bryan Re: CSI demo question Hi, @BryanNiu  The demo you mentioned in the shared link is also designed for FRDM-RW612.  So, yes, it should work on FRDM-RW612. If you are using a RW612 module, I think it should also work. But from the SDK version, it is using SDK 25.09.00, a little older. Currently our latest SDK version is SDK 26.06.00. You can have a try with our latest SDK 26.06.00, and according the the AN I provided to you to learn more info about CSI on RW612. Please let me know whether still have any other concerns on this case. Best regards, Christine.
View full article
i.MX RT1050 ダウンロードアルゴリズム 現在使用している開発環境は、i.MX RT1050 を使用した MCUXPRESSO IDE です。i.MX RT1050 には内蔵フラッシュメモリがないため、外部フラッシュメモリを使用する際にはアルゴリズムをダウンロードする必要があることは理解しています。しかし、ダウンロードするアルゴリズムは使用するフラッシュメモリによって異なります。公式ドキュメントには、目的のアルゴリズムを迅速かつ容易に入手する方法が記載されていますか? Re: i.MX RT1050 下载算法 こんにちは、SDFDSFSFさん、 以下の順序で行うことをお勧めします。 1. プロジェクトのプロパティで、外部のFlashダウンロードアルゴリズムを選択します。NXPは、いくつかの主要なFlashダウンロードアルゴリズムを提供しています。 プロジェクトを右クリックして「プロパティ」→「MCU設定」→「メモリの詳細」を選択し、NXPがサポートするフラッシュドライバを選択してください。 ShellyZhang_0-1783670863188.png MCUXpresso 用のフラッシュドライバは通常、nxp\LinkServer_xx.x.xx\binaries\Flash ディレクトリにあり、拡張子は .cfx です。 2. 選択したフラッシュメモリがSFDPをサポートしている場合は、まずSFDPドライバを試してください。 MCUXpressoでは、MIMXRT1050_SFDP_QSPI.cfxのようなドライバを選択できます。このタイプのSFDPドライバの重要な点は、フラッシュメモリに自己記述パラメータを組み込むことで、特定の部品番号固有のアルゴリズムへの依存度を低減できることです。 3. テンプレートを使って自分で作成する。 アプリケーションマニュアルを参照してください:https://www.nxp.com/docs/en/application-note/AN13386.pdfカスタムCFXファイルを生成します。変更する際は、主要なパラメータは、外部フラッシュデータシートのテスト結果とSDKに含まれるflexspi_nor_pollingデモから取得する必要があります。 ダウンロードアルゴリズムに加えて、XIP/ブートヘッダーの設定も必要です。詳細については、「解決済み:フラッシュインターフェースの初期化 - NXPコミュニティ」を参照してください。 上記は基本的な方法です。使用しているFlashの機種や、現時点でどのような問題に直面しているかなど、より詳細な情報を提供していただければ、より的確なサポートを提供できます。 よろしくお願いします、 シェリー・チャン i.MX RT1050 下载算法 J-Linkを使用しており、 MCUXpressoでMIMXRT1050_SFDP_QSPI.cfxを選択しました。ダウンロードに失敗しました。 Re: i.MX RT1050 下载算法 MCUXpresso IDEでIMXRT1052用の独自のJ-Linkアルゴリズムを作成するにはどうすればよいですか? 私のFlashファイルはWINBOD 25Q256JVEQです。 現在使用しているMCUXpresso IDEのバージョンはMCUXpresso IDE v25.6です。SDK_EVBKのバージョンは26.06.00です。どのサンプルプログラムを修正すれば、目的のダウンロードアルゴリズムを生成できるのか分かりません。 Re: i.MX RT1050 下载算法 お使いのハードウェアのピン構成が評価ボードと異なる可能性があります。iMXRT1050_QSPIプロジェクトを修正して、cfxファイルを独自に生成することをお勧めします。 Re: i.MX RT1050 下载算法 MCUXpresso IDEでJ-Linkを使用しても問題ないでしょうか? MCUXpresso IDEのアルゴリズムはCMSIS-DAPタイプのエミュレータでしか使用できないという意見も見かけたのですが。 Re: i.MX RT1050 下载算法 @SDFDSFSF様、 参考例は、nxp/LinkServer ディレクトリにあり、プロジェクト名は iMXRT1050_QSPI です。 ShellyZhang_0-1784857501325.png ピン配置が評価ボードと異なる場合は、ピン配置構成を変更する必要があります。フラッシュメモリ構成もデータシートに従って変更する必要があります。 以下の点をご確認ください。 1. フラッシュハードウェアのピンが正しく設定されているか確認してください。FlexSPIピンはRT1050ハードウェア開発マニュアルに従って設定する必要があります。 ShellyZhang_1-1784857962728.png グループAまたはグループBのいずれか一方のみを選択でき、FlexSPI_DQSは選択解除せずにそのままにしておく必要があります。 2. evkbimxrt1050_flexspi_nor_polling_transfer サンプルを SDK にインポートし、フラッシュデータシートに従ってフラッシュ構成を変更します。(この手順は省略可能です。フラッシュ構成が正しいことを確認するためだけのものです。) 3. iMXRT1050_QSPIプロジェクトで、正しいフラッシュ構成に変更します。この手順については、以下を参照してください。 https://www.nxp.com/docs/en/application-note/AN13386.pdf よろしくお願いします、 シェリー・チャン
View full article
S32K344 QSPI Initializations SCLK does not produce the expected value. I'm using the S32K344 LQFP176 to build a product that accesses QSPI peripherals. We want to make QSPI similar to LSPI in application, not to access FLASH, but to use ordinary devices. I've configured the clock tree QSPI_SFCK to 20MHz, disabled the relevant FLASH registers, and used a LUT table. During debugging, I observed the LUT executing, but QSPI's SCLK isn't being generated, although ultra-high-speed waveforms are appearing on SD0-SD3. Could you please help me figure out how to use this QSPI to access non-FLASH devices? Re: S32K344 QSPI Initializes SCLK不按我们希望出来 The S32K344 QuadSPI module is primarily intended as a serial flash memory interface, not as a generic LSPI-like interface for arbitrary QSPI peripherals. The QSPI_SFCK clock configuration only provides the clock source for the QuadSPI module; it does not automatically generate an external SCLK. The external SCKFA signal is generated only as part of a valid QuadSPI command sequence executed by the flash-oriented LUT/IP command engine. Therefore, if the connected device does not follow a flash-like command/address/data protocol, or if the LUT sequence/pin configuration does not match such a transaction, the behavior may not be suitable for this application. For a generic external device, LSPI should be used if the required protocol can be implemented there. If QuadSPI must be used, the external device protocol would need to be compatible with the QuadSPI flash-style transaction model, and the LUT sequence, pin muxing, chip select, command/address/data phases, and IP command trigger need to be checked accordingly.
View full article
CSIデモ問題 こんにちは、 こちらはQuectelのFAEチームのブライアンです。 9月に開催されるNXPの展示会に向けて、CSI関連のデモをいくつか準備する予定です。デモの例について少し助けていただけますか? 例えば、モーション検知に似た例がいくつかありましたが、ボード上で取得したCSIデータをどのように分析し、活用すればよいのか教えていただきたいです。 rw610とrw612があります 私のメールアドレス:[email protected] Re: CSI demo question こんにちは、 @BryanNiu RW610とRW612はどちらもCSIをサポートしています。 すでにデフォルトのSDKリリースにデモが入っています:wifi_cli例です。 wifi_cliアプリケーションはCSIの生成および収集の設定に使用されます。このアプリケーションはSDKリリースに含まれています。CSIデータを生成するには、Wi-FiデバイスにWi-fi_cliアプリケーションをフラッシュし、以下のコマンドを実行します。 wlan-set-csi-param-header wlan-set-csi-filter wlan-csi-cfg wlan-auto-null-tx 詳細については以下をご覧ください: AN14281: FreeRTOSのチャネルステートインフォメーション(CSI) | NXPセミコンダクターズ この件に関して他に懸念があれば教えてください。もしなければ、このスレッドの解決策として私の回答をマークしてください。 よろしくお願いいたします。 Christine。 Re: CSI demo question こんにちは、 @Christine_Li さん。 情報ありがとうございます。SDKの基本的なwifi_cli例を成功裏に実行しました。 さらに一歩進んで、CSIデータを分析してデモを開発したいと考えています。RW61x上でCSIモーション検知を行うための以下のリポジトリを見つけました。このデモは弊社のモジュールと互換性がありますか? https://github.com/nxp-appcodehub/dm-motion-detection-using-wifi-csi-on-rw61x あるいは、似たようなデモをおすすめできますか? よろしくお願いします。 ブライアン Re: CSI demo question こんにちは、 @BryanNiu 共有リンクで言及されているデモも、FRDM-RW612向けに設計されています。 ですので、はい、FRDM-RW612では動作するはずです。 RW612モジュールを使用している場合でも、同様に動作するはずです。 しかしSDKバージョンでは、少し古いSDK 25.09.00を使っています。現在、最新のSDKバージョンはSDK 26.06.00です。 最新のSDK 26.06.00と、私が提供したANに従って、CSIのRW612についての詳細を知りたい方はぜひ試してみてください。 この件に関して他に懸念があれば教えてください。 よろしくお願いいたします。 Christine。
View full article
Training material (PPT and Video) list for S32K3 (until Jan. 2026) Hi. After you login www.nxp.com and Please switch to ENGLISH mode      Snipaste_2026-02-02_16-10-05.png Click on the link below https://www.nxp.com/design/design-center/training:TRAINING-EVENTS?collection=trainings &start=0 &max=12 &sorting=sort_date. desc &parameters=TrainingType.Topics.deviceTax.applicationTax.country.region.application.TrainingLanguage.TrainingFormat.skillLevel. durationTime.provider &language=en &query=TrainingFormat %3E%3EOnline::training_date %3E%3E2026-02-02... * &keyword=s32k &siblings=false You can get the following training topics with input the topic as You can get the following training topics with input the topic as searching keyword. S32K3 Part 1 MKT Overview (DFAE Only) Training Presentation S32K3 Part 3 Hardware and Software Tools Overview (DFAE Only) Training Presentation S32K3 Part 5 RTD Overview and Demo (DFAE Only) Training Presentation S32K3 and MCSPTE1AK344 Motor Control Kit Training Presentation S32K3 Booting and Startup Process Memory (Chinese) Training Video S32K3 Debug Based on MCAL and FreeMASTER S32K3 Debug Based-On MCAL EB Freemaster (Chinese) Training Video S32K3 Debugging Skills Training Presentation S32K3 Deep Dive and Design Tips Part 1 Training Presentation S32K3 Deep Dive and Design Tips Part 2 Training Presentation S32K3 Deep Dive and Design Tips Part 3 Training Presentation S32K3 Deep Dive and Design Tips Part 4 Training Presentation S32K3 DFAE Day 1 Training Presentation S32K3 DFAE Day 2 Training Presentation S32K3 DFAE Training HSE Security Aspects Day 2 S32K3 DFAE Training Memory Link Boot Day 2 S32K3 DFAE Training Day 1 S32K3 Documents Location On Security Safety (Chinese) Training Video S32K3 Getting Started Training Presentation S32K3 How to Request Access to Safety Documentation S32K3 HSE Security Library Enablement Training Presentation S32K3 HSE-B with Demo (Chinese) Training Video S32K3 Memory Link Boot (Chinese) Training Video S32K3 Part 2 Architecture and Technical Overview DFAE Only Training Presentation S32K3 Part 4 K1 to K3 Hardware and Software Migration Guide DFAE Only Training Presentation S32K3 Safey Design Consideration Training Presentation S32K3 Software Enablement DFAE Training Part 1 S32K3 Software Enablement DFAE Training Part 1 - Auto MCU RTD Demo Porting Techniques S32K3 Software Enablement DFAE Training Part 1 - Getting Started with S32K RTD Features S32K3 Software Enablement DFAE Training Part 1 - HAL and EL demos Show S32K3 Software Enablement DFAE Training Part 1 - How to Import RTD MCAL to IAR project S32K3 Software Enablement DFAE Training Part 1 - How to Import RTD MCAL to S32DS project S32K3 Software Enablement DFAE Training Part 1 - How to Use GHS Complier Build S32K3 RTD MCAL S32K3 Software Enablement DFAE Training Part 1 - SW Commercial Offering HAL and EL Bundle S32K3 Software Enablement DFAE Training Part 2 S32K3 Software Enablement DFAE Training Part 2 - AUTOSAR and MCAL Architecture S32K3 Software Enablement DFAE Training Part 2 - MCAL Training AE S32K3 Software Enablement DFAE Training Part 2 - MCAL Training CAN S32K3 Software Enablement DFAE Training Part 2 - MCAL Training CRC S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Crypto S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Dio S32K3 Software Enablement DFAE Training Part 2 - MCAL Training DPGA S32K3 Software Enablement DFAE Training Part 2 - MCAL Training ETH S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Fee S32K3 Software Enablement DFAE Training Part 2 - MCAL Training GDUs S32K3 Software Enablement DFAE Training Part 2 - MCAL Training I2C S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Icu S32K3 Software Enablement DFAE Training Part 2 - MCAL Training MCL S32K3 Software Enablement DFAE Training Part 2 - MCAL Training MCUs S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Mem S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Mem Acc S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Mem Eep S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Mem EXFIs S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Mem INFIs S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Multicore S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Ocu S32K3 Software Enablement DFAE Training Part 2 - MCAL Training Port S32K3 Software Enablement DFAE Training Part 2 - MCAL Training SPI S32K3 Software Enablement DFAE Training Part 2 - MCAL Training UART S32K3 Software Enablement DFAE Training Part 3 S32K3 Software Enablement DFAE Training Part 3 - Function Safety General S32K3 Software Enablement DFAE Training Part 3 - Hands-On Creating Projects with Multiple MCAL Modules S32K3 Software Enablement DFAE Training Part 3 - Hands-On Creating Projects with Multiple MCAL Modules S32K3 Software Enablement DFAE Training Part 3 - HSE Hands-On Workshop-S32K3 HSE Security Library Enablement S32K3 Software Enablement DFAE Training Part 3 - HSE Hands-On Workshop-S32K3 HSE Security Library Enablement S32K3 Software Enablement DFAE Training Part 3 - HSE NXP Security on S32K3 S32K3 Software Enablement DFAE Training Part 3 - HSE NXP Security on S32K3 S32K3 Software Enablement DFAE Training Part 3 - Integrating Safety with S32 Safety Software Framework S32K3 Software Enablement DFAE Training Part 3 - Introduction of S32K3 HSE and Debugging Techniques S32K3 T-BOX Business Training Presentation S32K3 Zonal Aggregators, Telematics Box and Communications Protocols Training Presentation GC DFAE Training S32K SW Day 5 Training Presentation Introduction to S32K Hardware Security Engine HSE Library and Debugging Techniques Training Presentation K3 booting and startup process           Re: Training material(PPT and Video) list for S32K3 (until Jan. 2026) Enjoy these training! Cheers! Oliver Re: Training material(PPT and Video) list for S32K3 (until Jan. 2026) Where do I find this material now? 回复: Training material(PPT and Video) list for S32K3 (until Jan. 2026) It's not visible now. I need a configuration video for Crypto.
View full article
S32K3の研修資料(PPTとビデオ)リスト(2026年1月まで) こんにちは、 www.nxp.com に ログイン し、 英語モードに切り替えてください。      Snipaste_2026-02-02_16-10-05.png 下のリンクをクリックしてください https://www.nxp.com/design/design-center/training:TRAINING-EVENTS?collection=trainings&start=0&max=12&sorting=sort_date.desc&parameters=TrainingType.Top ics.deviceTax.applicationTax.country.region.application.TrainingLanguage.TrainingFormat.skillLevel.durationTime.provider&language=en&query=TrainingFormat %3E% 3EOnline::training_date %3E% 3E2026-02-02..*&keyword=s32k&siblings=false 検索キーワードとしてトピックを入力すると、次のトレーニング トピックを取得できます。 S32K3 パート 1 MKT の概要 (DFAE のみ) トレーニング プレゼンテーション S32K3 パート3 ハードウェアおよびソフトウェアツールの概要(DFAEのみ)トレーニングプレゼンテーション S32K3 パート5 RTDの概要とデモ(DFAEのみ)トレーニングプレゼンテーション S32K3およびMCSPTE1AK344モーター制御キットトレーニングプレゼンテーション S32K3 のブートと起動プロセスメモリ(中国語)トレーニングビデオ MCALとFreeMASTERに基づくS32K3デバッグ S32K3 デバッグベースの MCAL EB Freemaster (中国語) トレーニングビデオ S32K3 デバッグスキルトレーニングプレゼンテーション S32K3 の詳細と設計のヒント パート 1 トレーニング プレゼンテーション S32K3 の詳細と設計のヒント パート 2 トレーニング プレゼンテーション S32K3 ディープダイブと設計のヒント パート3 トレーニングプレゼンテーション S32K3 ディープダイブと設計のヒント パート4 トレーニングプレゼンテーション S32K3 DFAE 1日目トレーニングプレゼンテーション S32K3 DFAE 2日目トレーニングプレゼンテーション S32K3 DFAE トレーニング HSE セキュリティ側面 2 日目 S32K3 DFAE トレーニング メモリリンク ブート 2 日目 S32K3 DFAE トレーニング 1 日目 S32K3 ドキュメントの場所とセキュリティ安全性(中国語)トレーニングビデオ S32K3 入門トレーニング プレゼンテーション S32K3 安全文書へのアクセス要求方法 S32K3 HSEセキュリティライブラリ有効化トレーニングプレゼンテーション S32K3 HSE-B デモ付き(中国語)トレーニングビデオ S32K3 メモリリンクブート(中国語)トレーニングビデオ S32K3 パート2 アーキテクチャと技術概要 DFAE 限定トレーニング プレゼンテーション S32K3 パート4 K1からK3へのハードウェアおよびソフトウェア移行ガイド DFAEのみのトレーニングプレゼンテーション S32K3 安全設計考慮トレーニングプレゼンテーション S32K3 ソフトウェア有効化 DFAE トレーニング パート 1 S32K3 ソフトウェア有効化 DFAE トレーニング パート 1 - 車載 MCU RTD デモ移植テクニック S32K3 ソフトウェア有効化 DFAE トレーニング パート 1 - S32K RTD 機能の使用開始 S32K3ソフトウェア有効化DFAEトレーニングパート1 - HALおよびELデモ表示 S32K3 ソフトウェア有効化 DFAE トレーニング パート 1 - RTD MCAL を IAR プロジェクトにインポートする方法 S32K3 ソフトウェア有効化 DFAE トレーニング パート 1 - RTD MCAL を S32DS プロジェクトにインポートする方法 S32K3 ソフトウェア有効化 DFAE トレーニング パート 1 - GHS コンパイラの使用方法と S32K3 RTD MCAL のビルド S32K3 ソフトウェア有効化 DFAE トレーニング パート 1 - SW 商用提供 HAL および EL バンドル S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - AUTOSAR および MCAL アーキテクチャ S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング AE S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング CAN S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング CRC S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング 暗号 S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング Dio S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング DPGA S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング ETH S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング料金 S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング GDU S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング I2C S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング Icu S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング MCL S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング MCU S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング メモ S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング メモリ アカウント S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング メモ S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング Mem EXFIs S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング Mem INFIs S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング マルチコア S32K3ソフトウェア有効化DFAEトレーニングパート2 - MCALトレーニングOcu S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング ポート S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング SPI S32K3 ソフトウェア有効化 DFAE トレーニング パート 2 - MCAL トレーニング UART S32K3 ソフトウェア有効化 DFAE トレーニング パート 3 S32K3 ソフトウェア有効化 DFAE トレーニング パート 3 - 機能安全全般 S32K3 ソフトウェア有効化 DFAE トレーニング パート 3 - 複数の MCAL モジュールを使用したプロジェクトの作成の実践 S32K3 ソフトウェア有効化 DFAE トレーニング パート 3 - 複数の MCAL モジュールを使用したプロジェクトの作成の実践 S32K3 ソフトウェア有効化 DFAE トレーニング パート 3 - HSE ハンズオン ワークショップ - S32K3 HSE セキュリティ ライブラリ有効化 S32K3 ソフトウェア有効化 DFAE トレーニング パート 3 - HSE ハンズオン ワークショップ - S32K3 HSE セキュリティ ライブラリ有効化 S32K3 ソフトウェア有効化 DFAE トレーニング パート 3 - S32K3 における HSE NXP セキュリティ S32K3 ソフトウェア有効化 DFAE トレーニング パート 3 - S32K3 における HSE NXP セキュリティ S32K3 ソフトウェア有効化 DFAE トレーニング パート 3 - S32 安全ソフトウェア フレームワークによる安全性の統合 S32K3 ソフトウェア有効化 DFAE トレーニング パート 3 - S32K3 HSE とデバッグ手法の紹介 S32K3 T-BOXビジネストレーニングプレゼンテーション S32K3 ゾーンアグリゲータ、テレマティクスボックス、通信プロトコルのトレーニングプレゼンテーション GC DFAE トレーニング S32K SW 5日目トレーニングプレゼンテーション S32K ハードウェア セキュリティ エンジン HSE ライブラリとデバッグ手法の紹介トレーニング プレゼンテーション K3のブートと起動プロセス           Re: Training material(PPT and Video) list for S32K3 (until Jan. 2026) トレーニングを楽しんでください! 乾杯! オリバー Re: Training material(PPT and Video) list for S32K3 (until Jan. 2026) この資料は今どこで入手できますか? 回复: Training material(PPT and Video) list for S32K3 (until Jan. 2026) 今は表示されていません。Cryptoの設定方法に関するビデオが必要です。
View full article
NXPS32K358:引导加载程序跳转到应用程序后,FreeRTOS 任务未运行 我们创建了一个示例应用程序项目,并将其用作引导加载程序。实际的应用程序项目与之完全相同,唯一的区别在于闪存起始地址。 引导加载程序成功跳转到应用程序,应用程序开始执行。但是,应用程序中的 xTaskCreate() 函数并未执行。 从引导加载程序跳转到基于 FreeRTOS 的应用程序时,是否需要任何额外的配置?例如,在应用程序能够创建和执行 FreeRTOS 任务之前,是否必须执行任何与启动、中断、向量表、堆栈指针或调度程序相关的配置? 我提到了 统一引导加载程序演示 社区提交的工单。我没有找到解决方案。问题只出现在引入 FreeRTOS 时,不引入 RTOS 时应用程序运行正常。  它适用于 S32K344,但不适用于 NXPS32K358。 如有需要,请告知是否需要提供其他信息。 Re: NXPS32K358: FreeRTOS Tasks Not Running After Bootloader Jumps to Application 我们项目中使用的引导加载程序到应用程序的跳转代码: 无效 Boot_JumpToApp(uint32 i_AppAddr) { uint32_t appStack; uint32_t func; uint8 i;   DisableAllInterrupts();   S32_SysTick->CSRr = 0; S32_SysTick->RVR = 0; S32_SysTick->CVR = 0;   for(i = 0; i < 10; i++)     { S32_NVIC->ICER[i] = 0xFFFFFFFFU; S32_NVIC->ICPR[i] = 0xFFFFFFFFU;    } appStack = *(volatile uint32_t *)0x00442000; __set_MSP(appStack); S32_SCB->VTOR = 0x00442000; func = *(uint32_t volatile *)(((uint32_t)0x00442004)); (* (void (*) (void)) func)(); } Re: NXPS32K358: FreeRTOS Tasks Not Running After Bootloader Jumps to Application 你好@Indhumathi , 为了缩小问题根源范围,请您验证一下以下中断处理程序是否正在执行? SVC 处理程序 (vPortSVCHandler) — 负责启动第一个 FreeRTOS 任务 PendSV 处理程序 (vPortPendSVHandler) — 负责任务之间的上下文切换 SysTick 处理程序(vPortSysTickHandler / xPortSysTickHandler)——负责 FreeRTOS 滴答 最简单的检查方法是在应用程序中每个处理程序的入口处设置断点或 GPIO 开关。 谢谢! 此致, 丹尼尔
View full article
CSI演示问题 您好, 这是来自 Quectel FAE 团队的 Bryan。 我们计划为9月份的NXP贸易展准备一些与CSI相关的演示。您能否提供一些示例演示? 例如,我注意到你们有类似运动检测的例子——我想知道如何分析和处理我们板上捕获的 CSI 数据。 我们有 rw610 和 rw612 我的邮箱:[email protected] Re: CSI demo question 你好, @BryanNiu RW610 和 RW612 都支持 CSI。 我们在默认 SDK 版本中已经有了演示:wifi_cli 示例。 wifi_cli 应用程序用于配置 CSI 的生成和收集。该应用程序已包含在 SDK 版本中。要生成 CSI 数据,请将 wi-fi_cli 应用程序刷写到 Wi-Fi 设备上,然后运行以下命令: wlan-set-csi-param-header wlan-set-csi-filter wlan-csi-cfg wlan-auto-null-tx 详情请参阅: AN14281:FreeRTOS 上的通道状态信息 (CSI) | 恩智浦半导体 如果您对此案还有其他疑问,请告知;如果没有,请随时将我的回答标记为本帖的解决方案。 顺祝商祺! Christine。 Re: CSI demo question 嗨@Christine_Li 谢谢你提供的信息。我们已成功运行 SDK 中的基本 wifi_cli 示例。 我们希望更进一步,分析CSI数据,以开发一个演示程序。我在 RW61x 上找到了以下 CSI 运动检测的存储库——这个演示与我们的模块兼容吗? https://github.com/nxp-appcodehub/dm-motion-detection-using-wifi-csi-on-rw61x 或者您能否推荐一些类似的演示? 谢谢  布莱恩 Re: CSI demo question 你好, @BryanNiu 您在分享的链接中提到的演示也是为 FRDM-RW612 设计的。 所以,是的,它应该可以在 FRDM-RW612 上运行。 如果你使用的是 RW612 模块,我认为应该也可以。 但从 SDK 版本来看,它使用的是 SDK 25.09.00,版本稍旧一些。目前我们最新的 SDK 版本是 SDK 26.06.00。 您可以尝试使用我们最新的 SDK 26.06.00,并根据我提供给您的 AN 了解更多关于 RW612 上 CSI 的信息。 如果您对此案还有其他疑问,请告知。 顺祝商祺! Christine。
View full article
S32K344 QSPI初期化において、SCLKが期待される値を生成しません。 私はS32K344 LQFP176を使用して、QSPI周辺機器にアクセスする製品を開発しています。FLASHへのアクセスではなく、通常のデバイスを使用するために、アプリケーション上でQSPIをLSPIのように動作させたいと考えています。 クロックツリーQSPI_SFCKを20MHzに設定し、関連するFLASHレジスタを無効にして、LUTテーブルを使用しました。デバッグ中にLUTが実行されていることは確認できましたが、SD0~SD3には超高速波形が表示されているにもかかわらず、QSPIのSCLKが生成されていません。このQSPIを使用して非FLASHデバイスにアクセスする方法を教えていただけないでしょうか? Re: S32K344 QSPI Initializes SCLK不按我们希望出来 S32K344 QuadSPIモジュールは主にシリアルフラッシュメモリインターフェースとして意図されており、任意のQSPIペリフェラル向けの汎用LSPIのようなインターフェースとしては意図されていません。QSPI_SFCKクロック構成はQuadSPIモジュールのクロックソースを提供するだけであり、外部SCLKを自動的に生成するものではありません。外部SCKFA信号は、フラッシュ指向LUT/IPコマンドエンジンによって実行される有効なQuadSPIコマンドシーケンスの一部としてのみ生成されます。したがって、コネクテッドデバイスがフラッシュのようなコマンド/アドレス/データプロトコルを守っていなかったり、LUTシーケンスやピンの設定がそのようなトランザクションと一致しない場合、この動作はこのアプリケーションには適さない可能性があります。汎用外部デバイスでは、必要なプロトコルが実装できるならLSPIを使うべきです。QuadSPIを使用する場合、外部デバイスプロトコルはQuadSPIフラッシュスタイルのトランザクションモデルと互換性があり、LUTシーケンス、ピンマルチパキシング、チップセレクト、コマンド/アドレス/データフェーズ、IPコマンドトリガーを適切にチェックする必要があります。
View full article
S32K148EVB-Q176はUJA1132ではなくUJA1131と共に受領されました。 こんにちは、 最近、S32K148EVB-Q176という基板を購入しました。ドキュメントや設計図によると、UJA1132が付いていると思っていましたが、届いたボードにはUJA1131が付いていました。 そのため、UJA1132の機能を期待していたのに、LINインターフェースは1つしかありません。 これは普通のことなのかどうか、お聞きしたかっただけです。S32K148EVB-Q176には、異なるSBCを搭載した複数のバージョンが存在するのでしょうか?それとも、私が受け取ったボードが間違っていたのでしょうか? ご回答をお待ちしています。 Re: S32K148EVB-Q176 received with UJA1131 instead of UJA1132 こんにちは、@sousou54 さん。 ご報告ありがとうございます。この件は現在調査中です。 商品箱に貼られている大きな白いラベルの写真を教えていただけますか?このラベルの情報は、基板の製造詳細を特定するのに役立ちます。 ラベルに製品固有の情報が含まれている場合があるため、公開するのではなく、プライベートメッセージやサポートケース(サポート)を開くことで共有できます。 よろしくお願いします、 ジュリアン Re: S32K148EVB-Q176 received with UJA1131 instead of UJA1132 こんにちは、@sousou54 さん。 念のためお知らせしますが、お送りいただいた写真を受け取りましたので、担当チームに転送いたしました。 返信をお待ちしています。ご理解とご協力ありがとうございます。 よろしくお願いします、 ジュリアン Re: S32K148EVB-Q176 received with UJA1131 instead of UJA1132 こんにちは、 @sousou54 さん。 この件についての詳細は、NXPの担当者またはこのキットを購入した代理店までお問い合わせください。彼らは支援を提供できるはずだ。 よろしくお願いします、 ジュリアン
View full article
SAF85xx HSE 更新 SMR 你好,恩智浦、 当只有签名字节因代码内容变化而变化,但代码大小、起始地址、密钥、签名指针... 没有更改时,我们是否需要更新 SMR? Re: SAF85xx HSE Update SMR 你好 SMR(安全内存区域)条目包含 HSE 用来验证应用程序映像的元数据。即使 大小保持不变 起始地址保持不变 密钥句柄保持不变 签名指针保持不变 ......对代码内容的任何修改都会产生不同的签名,HSE 必须验证新签名。 因此,必须使用更新的签名字节重写保存签名的 SMR 条目。 SMR 条目是经过身份验证的启动链的一部分;除非其相应的 SMR 条目反映了新的签名,否则 HSE 无法验证更新的二进制文件。 参考:Aptiv 有直接的恩智浦 FAE,请随时与他联系了解详情。 顺祝商祺! Peter Re: SAF85xx HSE Update SMR 感谢您的回复 Re: SAF85xx HSE Update SMR 你好, 如果我刷入新的应用程序和新的签名(映射新的应用程序)呢?如果“代码大小、起始地址、密钥、指向签名的指针”没有改变,是否需要重新安装SMR?
View full article
i.MX95でCPU/GPU/VPUを無効にして消費電力を減らす方法 こんにちは、NXPさん。 当社は、i.MX95ベースのシステム全体の消費電力を削減する方法を模索しています。 以下の質問について、教えていただけますか? 不要なときに個々のCPUコアを完全にシャットダウンすることは可能ですか? アプリケーションがGPUやVPUを使わない場合、完全に電源を切ることは可能でしょうか? CPU/GPU/VPUが不要なら、起動後にデフォルトで無効にしてさらに消費電力を減らすことは可能でしょうか?(デバイスツリーによる?) 最低限の電力消費を実現するための推奨ソフトウェア構成や参考資料はありますか? 私たちのBSPはYocto 5.2 / Linux 6.12.xをベースにしています。 ありがとうございます。 よろしくお願いいたします。 ショーン Linux Re: Reducing Power Consumption by Disabling CPU/GPU/VPU on i.MX95 ご質問は下記までお問い合わせください。 不要なときに個々のCPUコアを完全にシャットダウンすることは可能ですか? A: はい、可能です。 アプリケーションがGPUやVPUを使わない場合、完全に電源を切ることは可能でしょうか? A:はい、使わないなら使ってください。 CPU/GPU/VPUが不要なら、起動後にデフォルトで無効にしてさらに消費電力を減らすことは可能でしょうか?(デバイスツリーによる?) A: はい、GPU/VPUスタイルのプラットフォームデバイスの場合、通常は該当デバイスツリーのnode status = "disabled"を設定するのが一般的な方法です。そのためLinuxはそのデバイスをレジスタやプローブにしません。 最低限の電力消費を実現するための推奨ソフトウェア構成や参考資料はありますか? A: AN14449 — i.MX 95 電力消費測定:測定された低消費電力ユースケース、BCU手順、DSM、Linuxサスペンド、BBSMの主要な参考資料です。 ご質問があれば、お気軽にお問い合わせください 素敵な一日をお過ごしください
View full article