Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
MC9S08QG8 CODE WARRIOR WELL, I WILL HAVE TO SAY GOOD BYE, IF THE DERIVATIVE MC9S08QG8 CAN NOT BE SEEN IN CW V6.3 OR CW 11.1. I HAVE WORKED AT GETTING THIS CODE TO WORK FOR 40 DAYS NOW. U SAID IT WAS OK, BUT I CAN NOT FIND ANY CW V6.3 WINDOWS 11 THAT WILL RUN AND DEBUG IN CW 11.1 OR CD 6.3. IF I AM WRONG , PLEASE LET ME KNOW.  Re: MC9S08QG8 CODE WARRIOR Hello, The MC9S08QG8 device is available in CodeWarrior v11.1 under the section S08>HCS08Q Family>MC9S08QG8 I tested with the following setup: OS: Windows 11 CodeWarrior: 11.1 Device: MC9S08QG8 in board DEMO9S08QG8 Debug Connection: Via the connection in board DEMO9S08QG8 (USB-to-BDM interface) Best Regards,
View full article
Cloud lab Guide Visit Cloud Lab official websites: NXP Cloud Lab | NXP Semiconductors Find answers to common questions along with troubleshooting techniques related to using Cloud lab. 1. Registration How to register a cloud lab account? No additional account is required, you can just use your NXP account to sign in Cloud lab. Learn more about NXP account My NXP Account FAQs | NXP Semiconductors. 2. Sign in How to  log in Cloud lab.com Log in with your NXP Email address and password. Once logged-in, you should be able to access the cloud lab home page 3. Book your favorite EVKs How to book your favorite EVKs? You can book the HARDWARE Take “hardware” for example, all hot hardware will be shown by clicking “HARDWARE”, You can also click on the filter button-“view all boards”, to see all the EVKs in the Cloud Lab. Select one EVK and click “BOOK NOW”. Here, you can use it now by clicking on “USE NOW” or book the time to make an appointment. USE NOW: means you can immediately use this EVK, just need to select an end time and click “CONFIRM BOOK” Reserve an EVK: select the date and time  and click “CONFIRM BOOK” After booked,  pop-up windows will take you to “my book” page. Please note that user can only book one EVKs  in the same period. How can I check my reservation? You can manage your booking in “MY BOOK” page.  Let’s click the “debug” button and experience the cloud lab. 4. Debugging Is there any manual or guide for new cloud lab users? Scroll down to click the  “Download cloud lab manual” button to find more instructions about the cloud lab.  How can I watch the video  during debugging? You can watch the video of EVK board and see the light status. But please note that , the video will be closed in 30s. Pls click “ ” to play the video again. How can I debug my EVK board?  The command line will automatically connect the board serial port, when the camera is turned on. All EVK boards are Linux system, pls login with root.  Can I reset my EVK board when I facing some errors? Sure. Please click “Power Reset EVK” to hard reboot the board and wait several second, the board will be rebooted. Can I reinstall my EVK when I facing some errors? Sure. You can click the “Reinstall the system” button to recover the default setting. (It will take several minutes to reinstall the system , this action will also delete the files you created or modified. Pls save your copy before you reinstall the system.) How  can I upload/download files  during debugging? Click the “upload files to EVK” to upload the file you need. Please note that If you would like to upload files to board's Network File System(NFS),  you will find your files in board's /home/root path. If you would like to upload your own Image or dtb file,  use "TFTP" tab. 5. Support How  can I get supports from NXP engineers? Please go to Cloud lab Forum to raise a ticket for supports. https://community.nxp.com/t5/Cloud-Lab-Forums/ct-p/Cloud-Lab 6. Connect us If you any concern or any suggestion about our cloud lab, please don’t be hesitate to email us [email protected] Cloud Lab-Hardware Cloud Lab-Software Cloud Lab-Solution
View full article
クラウドラボのログインと使用ガイド NXP Cloud Labsのウェブサイトをご覧ください: NXP Cloud Labs|組み込み設計を容易に行えるワンストップのクラウド開発プラットフォーム。 クラウドラボの利用に関する質問への回答や、クラウドラボ利用中に発生する問題のトラブルシューティングに関するヒントやコツをご覧ください。 1. 登録 クラウドラボのアカウントを登録するにはどうすればよいですか? NXP Cloud Labsにログインするために、追加のアカウント登録は必要ありません。NXPアカウントをお持ちであれば、ログインしてCloud Labsをご利用いただけます。 NXPアカウント登録について| NXPアカウントに関するよくある質問 | NXPセミコンダクターズ 2. ログイン クラウドラボにログインするにはどうすればよいですか? NXP.COMに登録したメールアドレスとパスワードを入力してください。 ログインに成功すると、次のページが表示されます。「ログイン」をクリックすると、Cloud Experimentのホームページに移動します。 3. 予約 興味のある開発ボードを予約するにはどうすればよいですか? 興味のあるハードウェア/ソフトウェア/システムソリューション/アプリケーションの例をクリックしてください。「ハードウェア」を例にとると、現在人気のハードウェアが表示されます。また、クラウド実験で現在オンラインになっているすべての開発ボードを表示することもできます。 興味のある開発ボードを1つ選択し、「今すぐ予約注文」をクリックしてください。すぐに使用するか、試用期間を設定するかを選択できます。 今すぐ利用:現在時刻からサービスをご利用いただけます。終了時刻を選択後、「予約確定」をクリックしてください。 利用予約をするには、希望の日付、開始時間、終了時間を選択し、「予約を確定」をクリックしてください。   予約が完了すると、予約ページに移動します(ただし、お客様お一人につき、デバッグ用の開発ボードは同時に1枚のみ予約可能ですのでご注意ください)。 注文した開発ボードを確認するにはどうすればよいですか? 「マイオーダー」ページでは、ご注文いただいたすべての開発ボードが表示され、注文内容を管理できます。下の「デバッグ」をクリックして、早速お試しください! 4. デバッグ デバッグ画面に入ったら、何をすればいいですか? コマンドボックスの一番下までマウスをドラッグすると、「クラウドラボマニュアルをダウンロード」という項目が表示されます。それをクリックすると、クラウドラボの操作ガイドがダウンロードされます。 デバッグ画面に入った後、どのようにビデオを視聴すればよいですか? 開発ボードのライブ映像を見ると、ボードの状態とインジケーターランプが表示されます。なお、映像は30秒後に自動的に終了します。再生するには、映像右上隅の再生ボタンをクリックしてください。 デバッグ方法は? カメラの電源を入れると、画面下部のコマンドラインが自動的に開発ボードのシリアルポートに接続されます。現在、すべての開発ボードはLinux 6.1.36を使用しており、ネットワークブートに対応しています。 デバッグ中は、Linuxファイルシステムに「root」ユーザーとしてログインしてください。  デバッグ中にいくつか問題が発生しました。予約注文した開発ボードを再起動することはできますか? はい、コマンドラインの右上隅にある「PowerReset EVK」ボタンをクリックすると、開発ボードの電源をオフにして再起動できます。 デバッグ中に、プリインストールされている開発ボードでポートが使用中と表示された場合、どうすればよいですか? 再接続するには、右上隅にある「再接続」ボタンをクリックしてください。 デバッグ中に問題が発生しました。予約注文した開発ボードにシステムを再インストールしたり、 Image/dtb/ファイルシステムを元のバージョンに復元したりすることは可能でしょうか? はい。「システムを再インストール」ボタンをクリックしてください。(この操作には時間がかかりますので、ご注意ください。この操作を行うと、使用中に作成または変更したファイルはすべて削除されます。このボタンをクリックする前に、必要なファイルはすべて保存してください。) デバッグプロセス中に 必要なファイルを アップロード / ダウンロードするにはどうすればよいですか? デバッグプロセス中に必要なすべてのファイルをアップロードするには、「EVKにファイルをアップロード」をクリックしてください。  ご注意ください:テストファイルを開発ボードのネットワークファイルシステム(NFS)にアップロードする場合、アップロードが成功すると、アップロードされたファイルは開発ボードの/home/rootパスに保存されます。独自のコンパイル済みイメージまたはdtbファイルを使用する場合は、TFTPボタンを選択してください。 5. テクニカルサポート NXPのエンジニアから技術サポートを受けるにはどうすればよいですか? ユーザーは、NXPコミュニティのクラウドラボセクション( https://community.nxp.com/t5/Cloud-Lab/bd-p/Cloud-Lab )にログインするか、デバッグウィンドウをクリックすることで、質問をしたり、サポートを受けたりすることができます。「コミュニティQ&A」セクションをクリックすると、NXPコミュニティクラウドラボのエリアに移動し、そこで質問を投稿できます。 6. お問い合わせ クラウドラボのご利用中に問題が発生した場合、またはご提案がございましたら、メールにてご連絡ください。( [email protected] ) クラウドラボ用ハードウェア クラウドラボソフトウェア クラウドラボソリューション
View full article
云实验室登录使用指南 访问云实验室网站:恩智浦云实验室 | 一站式云上开发平台,助力轻松开展嵌入式设计 查找云实验室使用等相关问题的解答以及在云实验室使用过程中相关的疑难解答技巧。 1. 注册 如何注册云实验室账号? 恩智浦云实验室登录并不需要额外注册账号,拥有恩智浦账号即可登录体验云实验室 了解恩智浦账号的注册 恩智浦账号常见问题解答 | NXP 半导体 2. 登录 如何登录云实验室? 输入您在NXP.COM 注册的电子邮箱地址及密码 登录成功后会有如下的页面提示,点击“登录”后您将进入到云实验的首页。 3. 预定 如何预定您感兴趣的开发板? 点击您感兴趣的硬件/软件/系统方案/应用范例 以“硬件”举例,您将看到当前热门的硬件, 同时您可以点击查看当前云实验所有上线的开发板 选择其中一款您感兴趣的开发板,点击“立即预定”,在这里您可以选择立即使用和预约使用 立即使用:即从当前时间开始使用,选择好结束时间后,点击“确认预定” 预约使用:选择需要使用的日期,开始时间及结束时间,点击“确认预定”   预定成功后,将根据提示前往我的预定界面(请注意,同一时间段,同一客户只能预定一块开发板进行调试。) 如何查看我所预定的开发板? 在“我的预定”页面中,您将看到所有的您预定过的开发板并且管理您的预定,下面点击“调试”开始体验吧 4. 调试 进入调试界面后,我应该如何操作? 将鼠标拖到命令框最下方,可以看到Download cloud lab manual, 点击可下载云实验操作指南 进入调试界面后,如何观看视频? 观看当前开发板的实时视频,可以看到开发板的状态以及指示灯亮灭。需要注意的是,视频30s会自动取消,如果需要重新播放,需要点击视频右上角的播放按键, 如何进行调试? 摄像头打开后下方的命令行会自动进入开发板串口,目前所有开发板系统均为Linux6.1.36,支持网络启动。 调试时请使用“root” 登录Linux 文件系统  在调试过程中,我遇到了一些问题,我可以重启我预定的开发板么? 可以,点击命令行右上角“PowerReset EVK”按钮可以实现开发板的掉电及重启 在调试过程中,如果我预定的开发板能显示端口被占用,我应该如何操作? 点击右上角“Reconnection”按键即可重新连接。 在调试过程中,我遇到了问题,我可以将我预定的开发板进行重装系统或者将将Image/dtb/文件系统恢复为原始版本么? 可以。点击“Reinstall system”按钮。(此操作需要花费较长时间,请谨慎操作。 此操作会删除您在使用过程中新建/ 修改的文件,请在点击此按键前保存您所需要的文件信息)   在调试过程中,我如何上传/下载我所需要的文件? 点击“upload files to EVK”,可以上传您在调试过程中所有需要的文件,  需要注意的是:如果您想上传测试文件到开发板的网络文件系统(NFS),上传成功后,您会在开发板的/home/root路径下找到您上传的文件;如果您想使用自己编译的Image或dtb文件,选择TFTP 按键。 5. 技术支持 如何获得恩智浦工程师的技术支持? 用户可以通过登录恩智浦社区云实验室专区(https://community.nxp.com/t5/Cloud-Lab/bd-p/Cloud-Lab)提问获取帮助,或者点击调试窗口的 “Community Q&A” 跳转到恩智浦社区云实验室专区进行提问。       6. 联系我们 如果您在使用过程中有任何的问题或者您对我们的云实验室有任何的建议,你可以通过邮件的方式联系我们。([email protected]) Cloud Lab-Hardware Cloud Lab-Software Cloud Lab-Solution
View full article
Cloud Lab Overview Welcome to use the Cloud lab.com. The Cloud lab is NXP’s first global platform where allows users to explore the latest NXP hardware, software or solutions online. Here users can remotely connect an evaluation board and do code debugging or technical evaluation online. All these EVKs are set in our onsite lab, each one is equipped with a high-definition camera, which monitors its status in real time. Users simply book the resource they are interested in, then they can use it within the predetermined period of time. After each usage period ending, the platform will automatically reinstall the system and clear the history to protect the privacy of each user. Our vision is to provide users with open resources, convenient and secure services and a cost-saving and resource-saving R&D experience. The Cloud Lab is willing to be a new fertile ground for every developer to test their ideas on new hardware platforms in time, experience the changes brought about by the latest NXP technologies, and receive real-time and professional technical support from NXP engineers. Let’s go! Explore the Cloud Lab and unlock your potential!  Click to visit :NXP Cloud Lab | NXP Semiconductors 欢迎使用云实验室官网。云实验室是恩智浦在全球范围内第一个可供用户线上使用恩智浦最新硬件、软件或解决方案的平台。 在这里,用户可以远程访问开发板进行线上调试和开发。这些开发板都安装在线下的实验室中,每块板子上方配有一个高清摄像头,可实时监控板子的状态。 用户只需在网站简单的预定其感兴趣的资源,就可在预定时间内尽情使用。每当一段预定时间结束,平台会自动重装系统、清理历史记录来保护每位用户的隐私。 我们的愿景是为用户提供开放的资源、便捷又安全的服务以及节约成本和资源的研发体验。 云实验室愿作每一位开发者的新沃土,让大家可以及时在新的硬件平台上测试他们的想法,体验最新恩智浦技术带来的变化,并获得恩智浦工程师实时和专业的技术支持。 来吧,让我们开启云实验室的大门,解锁无限之可能! 点击访问:恩智浦云实验室 | 一站式云上开发平台,助力轻松开展嵌入式设计 Cloud Lab-Hardware Cloud Lab-Software Cloud Lab-Solution
View full article
Cloud Lab Login and Usage Guide Visit the NXP Cloud Labs website: NXP Cloud Labs | A one-stop cloud development platform to help you easily conduct embedded design. Find answers to questions related to using the cloud lab, as well as tips and tricks for troubleshooting related problems during the use of the cloud lab. 1. Registration How do I register a cloud lab account? No additional account registration is required to log in to NXP Cloud Labs; you can log in and experience the Cloud Labs with an NXP account. Understanding NXP Account Registration | NXP Account FAQs | NXP Semiconductors 2. Log in How do I log in to the cloud lab? Enter the email address and password you registered with NXP.COM After successfully logging in, you will see the following page prompt. Click "Log in" and you will be taken to the homepage of Cloud Experiment. 3. Reservation How can I reserve the development board that interests me? Click on the hardware/software/system solution/application example that interests you. Taking "hardware" as an example, you will see currently popular hardware. You can also click to view all the development boards currently online in the cloud experiment. Select one of the development boards that interests you and click "Pre-order Now". Here you can choose to use it immediately or schedule a trial period. Use Now: Start using the service from the current time. After selecting the end time, click "Confirm Reservation". To reserve a use: Select the desired date, start time, and end time, then click "Confirm Reservation".   After successful reservation, you will be directed to your reservation page (please note that each customer can only reserve one development board for debugging at the same time). How can I check the development board I ordered? On the "My Orders" page, you will see all the development boards you have ordered and be able to manage your orders. Click "Debug" below to start experiencing it! 4. Debugging Once I enter the debugging interface, what should I do? Drag your mouse to the bottom of the command box, and you'll see "Download cloud lab manual." Click it to download the cloud lab operation guide. How do I watch the video after entering the debugging interface? Watching the live video of the development board will show its status and the indicator lights. Note that the video will automatically cancel after 30 seconds. To replay it, click the play button in the upper right corner of the video. How to debug? Once the camera is turned on, the command line at the bottom will automatically enter the development board's serial port. Currently, all development boards use Linux 6.1.36 and support network boot. Please log in to the Linux file system as "root" during debugging.  During the debugging process, I encountered some problems. Can I restart my pre-ordered development board? Yes, clicking the "PowerReset EVK" button in the upper right corner of the command line can power off and restart the development board. During debugging, if my pre-installed development board shows that the port is occupied, what should I do? Click the "Reconnection" button in the upper right corner to reconnect. During the debugging process, I encountered a problem. Can I reinstall the system on my pre-ordered development board or restore the Image/dtb/ file system to its original version? Yes. Click the "Reinstall system" button. (This operation will take a long time, please proceed with caution. This operation will delete any files you create/modify during use, please save any necessary files before clicking this button.) How do I upload / download the files I need during the debugging process ? Click "upload files to EVK" to upload all the files you need during the debugging process.  Please note: If you want to upload test files to the development board's Network File System (NFS), you will find the uploaded files in the /home/root path of the development board after a successful upload; if you want to use your own compiled Image or dtb files, select the TFTP button. 5. Technical Support How can I get technical support from NXP engineers? Users can ask questions and get help by logging into the NXP Community Cloud Lab section ( https://community.nxp.com/t5/Cloud-Lab/bd-p/Cloud-Lab ), or by clicking the debug window. The "Community Q&A" section will redirect you to the NXP Community Cloud Labs area to ask your questions. 6. Contact Us If you encounter any problems during use or have any suggestions for our cloud lab, please contact us via email: ( [email protected] ) Cloud Lab-Hardware Cloud Lab-Software Cloud Lab-Solution
View full article
Compilation Error on imx-95-FRDM unknown base path for fd 4, path include couldn't allocate absolute path for 'include'. tar: ./usr/include: Cannot mkdir: Bad address tar: ./usr/include/xen/gntdev.h: Cannot open: No such file or directory got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path include couldn't allocate absolute path for 'include'. got *at() syscall for unknown directory, fd 4 unknown base path for fd 4, path include couldn't allocate absolute path for 'include'. tar: ./usr/include: Cannot mkdir: Bad address tar: ./usr/include/xen/evtchn.h: Cannot open: No such file or directory Re: Compilation Error on imx-95-FRDM Hi @Asadeds  What is your BSP version? I checked it on my Imx95 FRDM and there are no problems. B.R
View full article
What kind of port does the T Embed have? I have the standard model T Embed, but i have no Idea what kind of port it has (the other port, not usb c), because the official site says its a grove port, the lilygo Wiki site says its a qwiic port. Can anyone help me please?
View full article
I.MX93 boot waiting for known usb device Bought IMX93 from Mouser  for NXPLinux summer school program, I used there the automated script to boot the board,  ./scripts/ loss.py boot command . After executing the command I keep getting waiting  for known usb device. Will appreciate all the help to enable me progress Ias am stuck . FRDM-i.MX93  Re: I.MX93 boot waiting for known usb device @Fidelbanks thanks a lot for your interest in i.MX FRDM board. I think your problem is similar with  https://community.nxp.com/t5/i-MX-Processors/I-MX93-UUU-emmc-sdcard-LIBUSB-ERROR-TIMEOUT-Error/td-p/2402801 @pengyong_zhang Linux kernel summer school is a project that wants to help people getting started with learning linux kernel by using the i.MX93 frdm board.  https://nxp-research.github.io/lkss-main/2026/about.html#getting-started We provided a script that helps users boot the board using the serial download mode Re: I.MX93 boot waiting for known usb device Hi @Fidelbanks  What project are you referring to? If you want to get started with the development board, you can directly use the demo image from the NPX website. I'm not familiar with how your summer school program is implemented. B.R
View full article
PPF0900AMBA1ES Hi NXP team, I'm working on a custom board based on the i.MX95 (MIMX9596, 19x19 package, LPDDR5), using the PPF0900AMBA1ES PMIC. Could you please confirm: 1.Does this part number ship with OTP already programmed, or is it a non-programmed engineering sample? 2.If it is non-programmed, what is the recommended procedure to program (or emulate) the OTP configuration for bring-up and evaluation purposes? 3.Is a reference OTP configuration file (.CFG) available for an i.MX95 + LPDDR5 (19x19) implementation that we could use as a starting point? For context, our schematic closely follows the i.MX95 EVK reference design (PF09 + PF5301 + PF5302), and we're currently doing initial power-on bring-up. Thank you. PMIC Re: PPF0900AMBA1ES  PPF0900AMBA1ES is OTP part which mean had already done OTP. https://www.nxp.com/docs/en/supporting-information/MPF0900AMBA1ES.zip OTP file please download from above link.
View full article
S32G2 Enabling Multicore Application Hi, nxp fellows: We are preparing to use multi-core to run programs in the S32G274A chip, using A53 to run Linux and M7 to run LLCE_CAN. We referred to "Enabling Multicore Application on S32G2 using S32G2 Platform Software Integration", according to 5.2. Configure the bootloader, installed the recommended software packages, and configured them following the steps. zhipeng_7-1786181958976.pngzhipeng_7-1786181958976.pngzhipeng_7-1786181958976.pngzhipeng_7-1786181958976.png There is an error in 5.3. Build The Bootloader during compilation. The launch.bat file was edited. zhipeng_0-1786182860528.pngzhipeng_0-1786182860528.pngzhipeng_0-1786182860528.pngzhipeng_0-1786182860528.png An error occurred after running launch.bat.  zhipeng_0-1786180508617.pngzhipeng_0-1786180508617.pngzhipeng_0-1786180508617.pngzhipeng_0-1786180508617.png After commenting out the relevant code. zhipeng_5-1786181360466.pngzhipeng_5-1786181360466.pngzhipeng_5-1786181360466.pngzhipeng_5-1786181360466.png zhipeng_2-1786180921774.pngzhipeng_2-1786180921774.pngzhipeng_2-1786180921774.pngzhipeng_2-1786180921774.png I found the CryptoDal.h file in the installation directory. zhipeng_4-1786181305215.pngzhipeng_4-1786181305215.pngzhipeng_4-1786181305215.pngzhipeng_4-1786181305215.png zhipeng_6-1786181450684.pngzhipeng_6-1786181450684.pngzhipeng_6-1786181450684.pngzhipeng_6-1786181450684.png Where could there be any mistakes? Thanks. Re: S32G2 Enabling Multicore Application Hi,zhipeng Is Secure Boot enabled in the configuration? Try to enable the Secure boot, check if the issue will disappear. Joey_z_2-1786353784256.pngJoey_z_2-1786353784256.pngJoey_z_2-1786353784256.pngJoey_z_2-1786353784256.png BR Joey Re: S32G2 Enabling Multicore Application Hi, @Joey_z  Yes, after adding, it will show "undeclared" on the third image. Commenting out will show "No such file or directory", on the fifth image. zhipeng_1-1786347067301.pngzhipeng_1-1786347067301.pngzhipeng_1-1786347067301.pngzhipeng_1-1786347067301.png "CryptoDal.h" is located in D:\NXP\Integration_Reference_Examples_S32G2_2022_06\code\framework\realtime\bsw\dal\cryptodal\generic\include "Hse_Ip.h" is located in D:\NXP\SW32G_RTD_4.4_3.0.2_HF01\eclipse\plugins\Crypto_TS_T40D11M30I2R0\include I have found both files in their respective folders, and the file paths are also written in launch.bat. The current problem feels like the plugin path was not included during the compilation process. BR Re: S32G2 Enabling Multicore Application Hi,zhipeng For your issue, will there be an error if the following contents are added? Is it commenting out won't cause an error? Joey_z_0-1786328574726.pngJoey_z_0-1786328574726.pngJoey_z_0-1786328574726.pngJoey_z_0-1786328574726.png BR Joey 回复: S32G2 Enabling Multicore Application Hi,ZhiPeng Thank you for your information. Could you share more information with me? 1.Do you only boot ATF and uboot on A core? Have any output on the UART of A core? 2.What is the M core function? is it about the UART/CAN function? BR Joey 回复: S32G2 Enabling Multicore Application Hi, @Joey_z  The previous bootloader compilation was successful. Now, I have written the image into the NOR flash and after booting, there is no output on the UART. I referred to AN13750. Here are my operation steps: I followed the "S32G2_LinuxBSP_42.0_User_Manual.pdf", and installed u-boot bsp42.0-2022.04 and ATF bsp42.0-2.10 in Ubuntu 20. I modified s32_mmc.c and s32_common.mk according to 0001-fip-align-and-mmc-init.patch. zhipeng_0-1787646642108.pngzhipeng_0-1787646642108.pngzhipeng_0-1787646642108.png zhipeng_1-1787646670172.pngzhipeng_1-1787646670172.pngzhipeng_1-1787646670172.png zhipeng_2-1787646683855.pngzhipeng_2-1787646683855.pngzhipeng_2-1787646683855.png I compiled u-boot and ATF. make CROSS_COMPILE=/opt/S32G/arm-gnu-toolchain-11.3.rel1-x86_64-aarch64-none-linux-gnu/bin/aarch64-none-linux-gnu- ARCH=aarch64 PLAT=s32g274ardb2 BL33=../u-boot/u-boot-nodtb.bin Image Layout DCD: Offset: 0x200 Size: 0x1c IVT: Offset: 0x1000 Size: 0x100 AppBootCode Header: Offset: 0x1200 Size: 0x40 Application: Offset: 0x1240 Size: 0x33e00 Boot Core: A53_0 IVT Location: SD/eMMC Load address: 0x342f8f00 Entry point: 0x34302000 I wrote the fip.s32 onto the SD card. After replacing the fip, the SD card was still able to boot, and the date of the u-boot changed. U-Boot 2022.04-00213-g5a6f62071f (Aug 24 2026 - 10:35:21 +0800) Configure the bootloader. zhipeng_3-1787647428751.pngzhipeng_3-1787647428751.pngzhipeng_3-1787647428751.png zhipeng_4-1787647490093.pngzhipeng_4-1787647490093.pngzhipeng_4-1787647490093.png zhipeng_5-1787647533346.pngzhipeng_5-1787647533346.pngzhipeng_5-1787647533346.png zhipeng_6-1787647547310.pngzhipeng_6-1787647547310.pngzhipeng_6-1787647547310.png Generate S32G Boot Image zhipeng_7-1787647657415.pngzhipeng_7-1787647657415.pngzhipeng_7-1787647657415.png select the bt_m7_blob.bin to write it to the address 0x0. select the fip.bin to write it to the address 0x100000. select theS32G274A_M7.bin to write it to the address 0x200000. zhipeng_8-1787647865193.pngzhipeng_8-1787647865193.pngzhipeng_8-1787647865193.png Now neither the UART nor the CAN is responding. Please help me analyze the situation. Thanks. 回复: S32G2 Enabling Multicore Application Hi, @Joey_z  Thanks for your reply. 1. Yes, only ATF and u-boot were booted on the A core. The UART did not have any output. 2. The M core ran the LLCE_CAN and Lpspi programs, integrating the "Can_Llce_DS_Loopback_S32G274A_M7" and "Lpspi_Ip_Transfer_S32G274A_M7" routines. It first used SPI communication and then ran LLCE_CAN. I would like to add some more information: 1. The entire process was carried out according to AN13750, with only a few differences: I used BSP42 and S32DS3.5 versions; I replaced the IPCF routines with LLCE_CAN and only configured M7_0. 2. I compiled BSP42 using Yocto and generated the.sdcard. After importing the SD card, Linux could be started. 3. I compiled the u-boot and ATF of BSP42 according to the "AN13750, 4. Prepare images for Cortex-A53 cores" section. After re-importing the.sdcard and fip.s32 into the SD card, Linux could still be started in SD mode. However, when importing the bootloader and fip.bin into the norflash, no output was obtained. 4. I burned a UART routine for the M7 core separately in the norflash, and Linux could be started and outputted. This proved that the burning tool and norflash were normal. 5. I burned the LLCE_CAN program separately in the norflash. The program did not run, and there was no CAN output. 6. I attempted to configure the EB bootloader to start A53 separately, but re-burning the norflash still did not result in any output. Thanks. 回复: S32G2 Enabling Multicore Application Hi,zhipeng 1. I understand that your LLCE_CAN is running on the M core. Please test the bootloader's startup of this program M core independently. During the startup process, do not load the A core Image. 2. In your testing, the bootloader can start the UART program of M7, but can it cannot start the LLCE_CAN? 3. Have you tried using the bootloader to only boot the A53?  I have created a new case for this issue in the system in Chinese, the case number is the: 01000969. This will facilitate communication. BR Joey 回复: S32G2 Enabling Multicore Application Hi,zhipeng Thank you for contacting us. I will support you in the internal case. BR Joey 回复: S32G2 Enabling Multicore Application Hello, @Joey_z  The delay was quite long and the previous case was closed. We recently purchased the Lauterbach debugger. I ran Bootloader.elf using Trace32. As shown in the picture, in the Hse_Ip_GetHseStatus function, the return value u32Status of the Mu_Ip_GetFlagStatusRegister function is 0, and the return value of the function is 0. The program gets stuck in the while loop. I tried adding the Hse_Ip_Init function, but it didn't work. I captured the Hse_Ip_apMuBase data. It seems to be a problem with the HSE. Can you help me analyze it? Are there any other places that need to be tested? Best regards.
View full article
Skid-steer robot state space modelling???? Hey everyone! I'm a beginner and just started working at a decently big lab with a bunch of people and I needed to figure a few things out. We're working on a skid-steer robot. I understand the dynamic and kinematic equations mathematically, but I don't know HOW exactly to convert them into state space. (which was the requirement) My team has the CAD model and they need to extract the Inertial Mass Parameters. They're a very chaotic group and I tried asking them, but they themselves don't have it together.😭 There's no well put resource for this kinda stuff either, and I'm genuinely at a loss of how to proceed with anything meaningful. Any pointers, help, and resources are appreciated! Cheers. Re: Skid-steer robot state space modelling???? Hello @prash, Could you please, provide me the following information? -Which NXP product are you currently using? Are you working with one of our EVKs, a custom board based on NXP MCU/MPU product, or another hardware solution? -Which IDE you are using? BR Habib
View full article
Compatibility of Camera module with OX05B1S Sensor and in-built ISP with i.MX95 FRDM Hi All, Want to know if camera module with ox05b1s sensor and in-built ISP (similar to 5MP RGB-IR Global Shutter GMSL2 Camera for NVIDIA Jetson AGX Orin would be compatible with i.MX95 FRDM board). I do understand that i.MX95 only have MIPI_CSI2 port hence I need to find GMSL2 to MIPI_CSI2 converter, however my question is specifically related to compatibility of existing driver that is part of NXP Linux BSP. Will driver Camera driver of NXP Linux release directly work with this camera module? Do I need to make modification in dtb file? Any other modifications would or additional work that I need to plan for? Re: Compatibility of Camera module with OX05B1S Sensor and in-built ISP with i.MX95 FRDM Hello, The camera will not work directly with the i.MX95 BSP driver. The OX05B1S sensor driver may be reusable, but the GMSL2 setup adds another layer that needs integration. You will likely need DTB changes for the SerDes configuration (GMSL2 bridge, I2C routing, GPIOs, CSI-2 link) and possibly driver modifications for the GMSL2 serializer/deserializer. It’s not a plug-and-play Maxim Time Clock setup, so plan for some BSP customization and validation work. Re: Compatibility of Camera module with OX05B1S Sensor and in-built ISP with i.MX95 FRDM Hi @sarve043swaray  Thank you for the response. Could you please provide some guidance on how to modify dtb file also any idea on where to (file/folder) integrate serializer/de-serializer i2c command? Regards Re: Compatibility of Camera module with OX05B1S Sensor and in-built ISP with i.MX95 FRDM is this your similar topic? you can refer to this,  https://community.nxp.com/t5/i-MX-Processors/OX05B1S-GMSL2-camera-with-MAX96717-MAX96724-on-i-MX95/td-p/2403429 this is about imx95 camera porting guide, you also can refer to this to get to know the basic porting steps on the imx95 https://docs.nxp.com/bundle/UG10215/page/topics/imx95_applications_processor_camera_software_archi.html you also can refer to the 7.3.10.3 Camera modules of user guide, currently imx95 supports  X-MX95MBDESER01 (MAX96724 deserializer) + 4 modules X-MX95MBCAM10001 (Omnivision OX03C10 camera + MAX96717 serializer, if your requirement is similar, you can develop based on this dts, you can find all of device tree files as below, find the chapter 7.3.10.3  https://www.nxp.com/docs/en/user-guide/UG10163.pdf
View full article
Whether USB serial download mode can work or not Hi Sir, In our current project, our product has only “one” “USB-C” port, running USB 2.0 High Speed. Our target application is to use this USB port as USB host role to connect USB stick or solid state drives for local recording. However, our next revision PCB circuitry is to pull up 56K Ohm to VCC_5V0 on both CC pins of USB-C, as shown below. That is, we hardwire fixed the USB port to USB host based on CC configuration definition. There is no separate Jumper / Switch / Type-C Controller(DRP(Dual Role Port) logic IC) circuitry that can switch the CC pin between host and device. We would like to know, based on this circuitry, can i.MX8M+ USB Serial Download Mode still work? We understand when i.MX8M+ Boot ROM activates USB Serial Download mode, the port is automatically configured as a USB device(for USB Serial Download mode to work), but that should mean the chip's ROM code only controls the internal USB PHY to be device mode, it cannot override the hardware's external CC resistor states(Type-C Port role). As a result, the PC is entirely unable to enumerate the i.MX 8M Plus via USB(both cannot finish handshaking(Type-C Attach) from USB physical layer point of view), which causes the UUU programming to fail. If the above statement is correct, the USB Serial Download Mode will become inoperable before boot(i.e. will not work at all), resulting in the loss of factory production flashing and system unbricking capabilities. Is our understanding correct? Best regards Re: Whether USB serial download mode can work or not Hi @Esther_Liu  You are right, If you force CC to be a pull-up, it will remain in HOST mode, and UUU will likely malfunction. B.R
View full article
S32K324 write DFlash by FEE Hello, There is a question about S32K324 write DFlash by FEE: I plan to write approximately 50 bytes of data into the DFalsh of S32K324 using the FEE method. Since the hardware power supply on the circuit board has a backup time of around 0.743ms, I need to save the critical data within this time frame. Is it feasible to write to the DFlash using the FEE method? If it is not feasible, are there any other options? Thanks. Re: S32K324 write DFlash by FEE Hi@mmyjh_123 For a power-off backup window of 0.743 milliseconds, FEE is not safe. Even "close to 1 millisecond," the write execution time for a single Fls_MainFunction block already exceeds your available hold time. You could try using C40_Ip. Using Quad-page (1024 bits) program time, a 50-byte write would theoretically take 450 microseconds. However, within 0.743 milliseconds, any erase operation during an emergency hold is impossible; erasing an 8 KB sector could take up to 30 milliseconds. Therefore, when implementing this functionality using C40_Ip, always erase the DFLASH address to be programmed during idle periods. Furthermore, if the board can detect input voltage drops before the MCU power failure, commit operations should begin at the earliest possible threshold. Otherwise, add a large capacity capacitor/backup power to ensure the guaranteed window covers the worst-case software path and flash programming margin. The above is only a theoretical analysis; multiple real-world tests are recommended, ensuring sufficient design margins. Re: S32K324 write DFlash by FEE Ok, thanks a lot.
View full article
I.MX93 - UUU emmc/sdcard LIBUSB_ERROR_TIMEOUT Error Hi NXP Team, We are trying to flash an i.MX93 board using a .wic image file provided by our team. We have two i.MX93 boards with the same hardware revision (SCH-96411 REV_B2). On one board, we are able to successfully flash the .wic image. However, when attempting to flash the same image on the second board, we encounter an error. We have tested both: emmc_all (for eMMC flashing) sd_all (using an SD card) In both cases, the same issue occurs on the second board. We would appreciate your support in troubleshooting and resolving this issue. Please let us know if you need any additional logs, error messages, or board information. Providing both uuu command and debugProviding both uuu command and debugProviding both uuu command and debugProviding both uuu command and debug uuu supported listuuu supported listuuu supported listuuu supported list i.mx93 usb identifiedi.mx93 usb identifiedi.mx93 usb identifiedi.mx93 usb identified Re: I.MX93 - UUU emmc/sdcard LIBUSB_ERROR_TIMEOUT Error Hi, Thank you for your interest in NXP Semiconductor products, It's good to have schematic identification, I would recommend confirming i.MX 93 top marking though. Confirm that they share TOP marking. Please download latest prebuilt image release from Linux. Finally, you are trying to flash both of them in serial download and do they have any fuses blown? Regards Re: I.MX93 - UUU emmc/sdcard LIBUSB_ERROR_TIMEOUT Error Hi Please find the attached images. We noticed some changes in the IC part numbers. We also tried flashing the SD card externally and then inserting it into the i.MX93 board, but we are still encountering the same issue. Additionally, we would like to bring to your attention that an image is already present in the eMMC, and the board is able to boot successfully from it. However, when we attempt to flash a new image, we encounter errors. Please find the attached debug logs below. One observation is that the preloaded image that came with the board is showing U-Boot SPL 2025.04, whereas the image we are attempting to use shows U-Boot SPL 2024.04. We downloaded the latest Linux 6.18.20_2.0.0 (i.MX93 EVK, FRDM) release. However, we could only find the 14x14 EVK WIC image and were unable to locate an 11x11 FRDM WIC image package. Could you please confirm whether the 14x14 image is the correct one to use for our board, or if there is a separate 11x11 FRDM image available? SD Card Boot: U-Boot SPL 2024.04+gde16f4f1722+p0 (Sep 02 2024 - 10:44:35 +0000) SOC: 0xa1009300 LC: 0x2040010 PMIC: PCA9451A PMIC: Over Drive Voltage Mode DDR: 3733MTS DDR: 3733MTS M33 prepare ok eMMC Boot: U-Boot SPL 2025.04-g99518e6b6f20 (Feb 02 2026 - 05:52:54 +0000) PMIC: PCA9451A PMIC: Over Drive Voltage Mode DDR: 3733MTS found DRAM 2CS_2GB DRAM matched M33 prepare ok Normal Boot Trying to boot from BOOTROM Boot Stage: Primary boot image offset 0x8000, pagesize 0x200, ivt offset 0x0 Load image from 0x57800 by ROM_API NOTICE: TRDC init done NOTICE: BL31: v2.12.0(release):lf-6.18.2-1.0.0 NOTICE: BL31: Built : 07:53:18, Feb 10 2026 /****************************************************/ Regarding the fuse being blown, could you please let us know how we can verify whether the fuses have been programmed or blown on the board? Thank you. Issue board - imx93Issue board - imx93Issue board - imx93 Working board - imx93Working board - imx93Working board - imx93 Re: I.MX93 - UUU emmc/sdcard LIBUSB_ERROR_TIMEOUT Error I've got similar issues and per my understanding, the Chinese manufacturer who is behind FRDM series changed DDR RAM IC. This requires re-training DDR and update to u-boot, which was done for the board software, committed to nxp's u-boot repo, but the BSPs, Yocto layers and binary images on web site wasn't updated. Basically newer boards work with built-in u-boot only, everything your developers build with BSPs (and u-boot from 2024) will not even start due to invalid ddr configuration. You could confirm this issue by booting from board's u-boot, stop it using keyboard and then manually load your custom linux kernel and DT from the SD card.
View full article
To simulate full load condition on the imx95lpddr5 evk How to simulate the full-load operating condition on the i.MX95 LPDDR5 EVK board. Is there any image available or pre-compiled application for this? I am using linux multimedia image. Re: To simulate full load condition on the imx95lpddr5 evk Hello, You can use this application note as reference: https://www.nxp.com/docs/en/application-note/AN14449.pdf There are different use case scenarios to reach high CPU load testing. I suggest you take a look in: CA55 CoreMark eIQ Benchmark (GPU) eIQ Benchmark (NPU) Best regards. 
View full article
Support for mobile SDRAM (1V8) on RT1171CVM8B We are investigating the use of RT1171CVM8B on a new product. Does this i.MX RT family member support mobile (low power, 1.8V) SDRAM? It is not immediately clear from the datasheet, reference manual and available application notes and schematics that it does; it is inferred by the port drivers being specified for both 1V8 and 3V3 (NVCC_EMC1,2). It is also inferred from similar questions and answers in the affirmative for the i.MX RT1060 and RT1050. I would like to avoid a gotcha where some obscure part of the EMC or SDRAM interface fails with 1V8 parts;  Otherwise, why is it not clearly listed in the datasheet!? Kind regards, George Tzanatos. Re: Support for mobile SDRAM (1V8) on RT1171CVM8B Dear @georgetzanatos , The RT1171 does support Mobile SDRAM (low-power 1.8 V SDRAM). We agree that the current documentation does not state this explicitly. In the datasheet and reference manual, the memory protocol support and I/O voltage modes are described separately rather than being combined into a single "Mobile SDRAM support" statement. I understand your concern. Please feel free to use Mobile SDRAM on the RT1171. The key requirement is to configure the relevant NVCC_EMC1/2 power domains for 1.8V operation to match the SDRAM I/O voltage level.   Best Regards, Shelly
View full article
MC9S08QG8 COMPILER, how do i get the c compiler for this chip well, i have a product developed with a MC9S08QG8 chip. i need to make some c code changes. i am using windows11. What software product do i use to generate the debugger for the chip. I am using a Wiztronics interface board from the pc usb port to the chip in my product. i have tried 8 different software packages, and none of them have the final debugger working. What softwage package do u suggest to use for debugging.  I am lost in ur devlopment center . Re: MC9S08QG8 COMPILER, how do i get the c compiler for this chip Hello The CodeWarrior tool version 11.1, is supported in windows 11, this tool supports different connections [P&E USB Multilink Universal / USB Multilink, P&E Cyclone, Open Source BDM, P&E Full chip simulation] You can download the tool from this link: CodeWarrior® for MCUs (Eclipse IDE) v11.1 I look for the MC9S08QG8 device and is available in this version. Best Regards, Luis
View full article
FRDM-MCX N947 and OV5640 Camera I am currently porting a camera streaming pipeline (previously working on ESP32-S3) to the FRDM-MCXN947. The target resolution is 1080p capturing from an OV5640 camera module, processing via MCXN947 hardware accelerators, and streaming over SPI to an ESP32-C5 for Wi-Fi transmission. Hardware Pipeline: OV5640 Camera (DVP 8-bit) -> MCXN947 (FlexIO / SmartDMA) -> External PSRAM -> SPI -> ESP32-C5 -> Wi-Fi Current Progress & Setup SCCB / I2C Control: Fully functional. Camera register read/write operations succeed, and initialization passes. SmartDMA Baseline: Tested the stock NXP SDK SmartDMA examples for the OV7670 (using internal SRAM), which works as expected. Goal: Expand this to 1080p resolution using the OV5640 with external PSRAM buffering and FlexIO capture. Issue 1: FlexIO Pin Remapping & Invalid Data on D4/D5 When attempting 8-bit parallel capture via FlexIO, data lines D4 and D5 fail to read valid pixel data, while lines D0-D3, D6, and D7 behave correctly. Initial Pin Mapping: D0-D3: P1_4, P1_5, P1_6, P1_7 D4-D5: P3_4, P3_5 (Problematic: No valid pixel data) D6-D7: P1_10, P1_11 Control: VSYNC -> P1_18, HREF -> P1_19, XCLK -> P2_2 SCCB: SCL -> P3_2, SDA -> P3_3 Troubleshooting Attempted: I attempted remapping D4 and D5 to alternative pins and updated the corresponding FlexIO and Pin Mux configurations: Remapped D4: P2_8 Remapped D5: P2_9 Even with this remapping, D4 and D5 still do not capture valid data. Issue 2: SmartDMA Routing to External PSRAM for 1080p Because 1080p frame buffers exceed internal SRAM capacity, frames must be buffered into external PSRAM in real time. I am seeking best practices and configuration steps to configure SmartDMA to route incoming FlexIO camera data directly to external PSRAM without CPU intervention or frame tearing. Any insights, pin mapping suggestions, or reference code would be greatly appreciated! Board Design Communication & Control(I3C | I2C | SPI | FlexCAN | Ethernet | FlexIO) MCXN Re: FRDM-MCX N947 and OV5640 Camera Hi @DocMonster7  We have verified the official SDK example frdmmcxn947_smartdma_camera_flexio_mculcd_cm33_core0 on the FRDM-MCXN947 board with an OV7670 camera connected through the J9 camera interface. In this reference design, CAMERA_D4 and CAMERA_D5 are mapped to P3_4 and P3_5 respectively, and image capture works correctly. Based on this validation, P3_4 and P3_5 appear to be functioning correctly as camera data inputs. Therefore, the issue is unlikely to be caused by a limitation of these MCU pins themselves. We would recommend further checking the OV5640 hardware connections, signal integrity, pin mux configuration, and any modifications made to the original SmartDMA camera capture implementation. Harry_Zhang_0-1786329719002.pngHarry_Zhang_0-1786329719002.png BR Harry Re: FRDM-MCX N947 and OV5640 Camera Hi Harry, Thank you for verifying the SmartDMA OV7670 SDK example on J9. That clarifies the distinction. The reason for the discrepancy is the capture peripheral being used SmartDMA (EZH Engine): Directly samples GPIOs/EZH ports (where P3_4 and P3_5 on J9 function properly as EZH_LCD_D4/D5). FlexIO Parallel Engine (fsl_flexio_camera): Requires 8 contiguous FlexIO shifter data pins (FLEXIO0_D12 through FLEXIO0_D19). On the FRDM-MCXN947, P3_4 and P3_5 on J9 do not have FlexIO pin muxing. To get contiguous FlexIO D16/D17 lines, they must be routed to P3_8 (TP16) and P3_9 (TP15). When routing D4 to P3_8 (TP16) for FlexIO capture, we encountered active hardware contention on P3_8 (an active-drive GPIO test clamped at ~0.15V - 1.3V) because P3_8 is shared with the onboard QSPI Flash (U8 Winbond W25Q64, FlexSPI0_A_DATA0). Re: FRDM-MCX N947 and OV5640 Camera Hi @DocMonster7  Thanks for your sharing. If you do not have further question, please accept it as solution. BR Harry
View full article