Hello, There is a question about S32K324 write DFlash by FEE:
I plan to write approximately 50 bytes of data into the DFalsh of S32K324 using the FEE method. Since the hardware power supply on the circuit board has a backup time of around 0.743ms, I need to save the critical data within this time frame. Is it feasible to write to the DFlash using the FEE method? If it is not feasible, are there any other options?
Thanks.