2403116_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2403116_en-US

2403116_en-US

MC9S08QG8 CODE WARRIOR

WELL, I WILL HAVE TO SAY GOOD BYE, IF THE DERIVATIVE MC9S08QG8 CAN NOT BE SEEN IN CW V6.3 OR CW 11.1. I HAVE WORKED AT GETTING THIS CODE TO WORK FOR 40 DAYS NOW. U SAID IT WAS OK, BUT I CAN NOT FIND ANY CW V6.3 WINDOWS 11 THAT WILL RUN AND DEBUG IN CW 11.1 OR CD 6.3. IF I AM WRONG , PLEASE LET ME KNOW. 

Re: MC9S08QG8 CODE WARRIOR

Hello,

The MC9S08QG8 device is available in CodeWarrior v11.1 under the section S08>HCS08Q Family>MC9S08QG8

I tested with the following setup:

OS: Windows 11

CodeWarrior: 11.1

Device: MC9S08QG8 in board DEMO9S08QG8

Debug Connection: Via the connection in board DEMO9S08QG8 (USB-to-BDM interface)

luis_maravilla_1-1786488162478.pngluis_maravilla_1-1786488162478.png

Best Regards,

Tags (1)
No ratings
Version history
Last update:
2 weeks ago
Updated by: