2402992_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2402992_en-US

2402992_en-US

MC9S08QG8 COMPILER, how do i get the c compiler for this chip

well, i have a product developed with a MC9S08QG8 chip. i need to make some c code changes. i am using windows11. What software product do i use to generate the debugger for the chip. I am using a Wiztronics interface board from the pc usb port to the chip in my product. i have tried 8 different software packages, and none of them have the final debugger working. What softwage package do u suggest to use for debugging.  I am lost in ur devlopment center .

Re: MC9S08QG8 COMPILER, how do i get the c compiler for this chip

Hello

The CodeWarrior tool version 11.1, is supported in windows 11, this tool supports different connections [P&E USB Multilink Universal / USB Multilink, P&E Cyclone, Open Source BDM, P&E Full chip simulation]

You can download the tool from this link: CodeWarrior® for MCUs (Eclipse IDE) v11.1

I look for the MC9S08QG8 device and is available in this version.

Best Regards, Luis

Tags (1)
No ratings
Version history
Last update:
yesterday
Updated by: