Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
PN7221+Android16 EDLA certification issues PN7221, Android 16   The EDLA-certified build only supports partial NFC functions. Card detection works in our tests, but EMVCo, firmware upgrade and other features are unavailable. Root cause identified via comparison is as follows:   The EDLA build uses Google's prebuilt NFC service, while the AOSP build is compiled with NXP patches integrated.   Below is the EDLA-related build configuration snippet:   apex_set {   name: "com.google.android.nfcservices_compressed",   apex_name: "com.android.nfcservices",   overrides: ["com.android.nfcservices"],   owner: "google",   set: "com.google.android.nfcservices_compressed.apks",   filename: "com.google.android.nfcservices_compressed.apex",   exported_bootclasspath_fragments: ["com.android.nfcservices-bootclasspath-fragment"],   } Could you advise how to import NXP patches under this scenario? Are there alternative solutions? For other customers using NXP NFC chips, what approaches are adopted to pass EDLA certification while retaining full NFC functionality? Re: PN7221+Android16 EDLA certification issues Hello @zhangkai  Based on our analysis, the issue is likely caused by the EDLA build using Google's prebuilt NFC APEX (com.android.nfcservices) instead of the NFC module integrated with NXP Android middleware. The NXP Android 16 solution extends multiple layers of the Android NFC stack, including the NFC framework, NFC service, EMVCo framework, HAL, and associated libraries. If the Google prebuilt NFC service is used, only standard NFC features may remain available, while NXP-specific features such as EMVCo functionality, firmware update support, and other middleware extensions may not be active. At present, NXP's Android 16 porting documentation does not describe a method to directly patch or modify Google's prebuilt EDLA NFC APEX. The typical NXP integration approach is based on AOSP source integration and rebuilding the NFC stack with NXP middleware. For customers requiring full PN7221 functionality, we recommend evaluating whether the NFC APEX can be rebuilt with the NXP NFC middleware included, or consulting Google/OEM support regarding customization of the EDLA NFC module while maintaining EDLA compliance.
查看全文
PCA2131: AF (Alarm Flag) in Control Register 2 will not be able to clear Hi everyone, I am currently integrating the PCA2131 Automotive RTC into a Battery Management System (BMS). I am encountering a persistent issue where the Alarm Flag (AF, bit 4 of Control_2 register 01h) is stuck high. Basic SPI communication is functioning perfectly-I can successfully set and read the time registers without issue. However, I cannot clear the AF flag during initialization. Important Context: I have already ensured that all Alarm Enable (AE_X) bits in the alarm registers (0Ah through 0Eh) are set to 1 (disabled) prior to attempting to clear the AF flag. The sequence I am executing: Read Control_2 (Register 01h). The AF bit reads as 1. Clear the flag by setting AF = 0 and AIE = 0 in my local struct. Write the modified byte back to Control_2. Read Control_2 again. The AF bit is still 1. I have attached screenshots from my debug session showing the register states before clearing, during the clear operation, and after reading it back. My Questions: Given that all AE_X bits are disabled, what other internal conditions could force the AF flag to immediately re-assert (or prevent it from clearing)? Any insights or recommendations would be greatly appreciated! Re: PCA2131: AF (Alarm Flag) in Control Register 2 will not be able to clear Hi Jozef, Thank you for your support and for pointing me in the right direction. I checked the SPI messages using the picoscope and verified that the hardware values were correct. Following your suggestion, I debugged my code further and confirmed that the root cause was indeed a bitfield ordering mismatch. I have fixed the mismatch, and the issue is now fully resolved. Thanks again for your help! Best regards, Vikas Re: PCA2131: AF (Alarm Flag) in Control Register 2 will not be able to clear Hi Vikas, thank you for confirmation. Given the PCA2131 behavior described in the datasheet, and assuming AE_S/AE_M/AE_H/AE_D/AE_W are all 1. it does not look the RTC is legitimately re-triggering AF. Most likely cause is bitfield ordering mismatch. Could you please catch and share the scopes of the three reading, writing SPI messages? To confirm the timing and registers/bits written and read.  JozefKozon_2-1783678052638.png With Best Regards, Jozef Re: PCA2131: AF (Alarm Flag) in Control Register 2 will not be able to clear Oops, sorry for the typo! The correct address is 0Eh to 12h. I just double-checked, and I did have it correct in my code, so it was just a mistake in my message. Re: PCA2131: AF (Alarm Flag) in Control Register 2 will not be able to clear Hi Vikas, please double check the Alarm registers. These registers have address 0Eh to 12h.  JozefKozon_0-1783672873300.png JozefKozon_1-1783672931555.png Please try to set all the AE_x bits to 1 again.  With Best Regards, Jozef
查看全文
Utility software issues How do I download the NXP MCUXpresso IDE development software used for the LPC1765FBD100? Thank you. Analog (ADC|CMP|DAC|OpAmps) Core and Memory Development Board Re: 工具软件问题 Hello, you can find the MCUXPresso download link here: Free Professional ARM Development Tools | NXP Semiconductors Celeste_Liu_0-1783663550952.png BR Celeste
查看全文
S32G399A 串行启动 I/O 确认 你好 我正在阅读S32G3参考手册。 串行启动部分提到,CAN 和 UART 接口使用: UART:RX = PAD[42],TX = PAD[41] CAN:RX = PAD[43],TX = PAD[44] 但是,我在 SoC 焊盘列表或引脚描述中找不到 PAD[41]、PAD[42]、PAD[43] 或 PAD[44]。 请问 PAD[41]、PAD[42]、PAD[43] 和 PAD[44] 分别对应哪些 SoC 物理引脚或信号? 另外,这些焊盘是否与 BootROM 串行启动模式使用的特定 LINFlexD 实例和 FlexCAN 实例相关联? MichaelTao_0-1783673199172.png MichaelTao_1-1783673210769.png Re: S32G399A serial boot IO confirm 你好, MichaelTao 感谢您与我们联系。 我已经收到您的问题,我会帮您核实。 BR 乔伊 Re: S32G399A serial boot IO confirm 您好, MichaelTao 请参考 S32G3 参考手册中的附件 S32G_IOMUX.xlsx,以获取有关您所描述的引脚对应关系的更多信息。 Joey_z_0-1783907635236.png Joey_z_1-1783907648304.png 希望这些信息对您有所帮助。 BR 乔伊
查看全文
FLEXCAN EDMA - CANメッセージのバースト受信時にACKエラーが発生する i.MXRT1176では、EDMAとFLEXCANを使用しています。(SDK 26.03) DMA転送完了時にコールバック関数が定義されています。 これが私たちの流れです。 1.転送を開始するには、`FLEXCAN_TransferReceiveFifoEDMA()` を呼び出してください。 2. DMA転送完了時にユーザー定義コールバックが呼び出されます。 3. データはDMAバッファからコピーされ、メッセージの受信を継続するために`FLEXCAN_TransferReceiveFifoEDMA()`が呼び出されます。 4. 手順2~4を繰り返す 別のノードから最小限のフレーム間隔でバースト的にメッセージを送信すると、ACKエラーの数が増加することがわかりました。つまり、iMXがメッセージをACKできないということです。 処理の流れを追っていくと、DMA転送完了コールバックが発生するたびに、FLEXCAN上でDMAが無効化されているようです。「FLEXCAN_TransferReceiveFifoEDMA()」が呼び出されると再び有効化されます。 これは「FLEXCAN_EnableRxFifoDMA()」を呼び出すことで行います。有効化/無効化DMAはFLEXCANのMCRレジスタ内のDMAビットを更新し、フリーズモードでのみ可能です。メッセージを一気に受信しているため、FLEXCANがフリーズモードに設定されている間に送信が進行中である可能性があります。そして、着信メッセージをACKで確認できません。   `FLEXCAN_EnableRxFifoDMA()` の呼び出しを削除することで、すべての ACK エラーが解消されることを確認しましたが、今度は一部のメッセージがドロップされるようになりました。また、メッセージの間隔を空けて送信してみたところ、ACKエラーも解消されました。これが実装上の問題なのか、それとも別の方法で再設計すべきか確認していただけますか? Re: FLEXCAN EDMA - ACK errors while receiving a burst of CAN messages こんにちは、@r-uv さん。 詳細な分析をありがとうございました。あなたの観察はSDKの実装と一致しています。 FLEXCAN_TransferReceiveFifoEDMA() は、有限長のトランザクション API です。DMA完了の後、ドライバーはRx FIFO DMA要求を無効化し、次の呼び出しで再び有効化します。MCR[DMA]を変更するにはフリーズモードが必要となるため、最小IFSトラフィックの次のフレームがFlexCANが通常モードに戻る前に到着する可能性があり、その結果ACKが欠落する可能性があります。 これは、繰り返し行われるDMAの有効化/無効化操作を削除するとACKエラーは解消されるものの、フレームのドロップが依然として発生する理由も説明しています。フリーズに関連するACKギャップは解消されますが、eDMA転送は継続的に再有効化されないためです。 連続的なバーストトラフィックについては、Rx FIFO DMA要求を有効にし、ハードウェアチェーンのピンポン/散乱集いTCDを使用して次のバッファが自動的に有効化されるようにすることを推奨します。これは、FLEXCAN_TransferReceiveFifoEDMA() を繰り返し再起動するのではなく、連続した DMA 受信パスを必要とします。 よろしくお願いします、 ギャビン Re: FLEXCAN EDMA - ACK errors while receiving a burst of CAN messages ご回答ありがとうございます。SDKにこのサポートを追加する計画はありますか?現在のトランザクションAPI実装だけでなく、継続的なDMAベースの実装はどうでしょうか?
查看全文
私のS32 Design Studio for ARMバージョン2.2のライセンスが期限切れになりました。延長手続きをお願いできますでしょうか?よろしくお願いいたします。 私のS32 Design Studio for ARMバージョン2.2のライセンスが期限切れになりました。延長手続きをお願いできますでしょうか?よろしくお願いいたします。 Re: S32 Design Studio for ARM Version 2.2 许可证到期,麻烦帮忙延期,谢谢! こんにちは、 お客様のS32DSライセンスが延長されました。
查看全文
MPC5746C hangs (no boot, no UART) at 115°C ambient Part: MPC5746C (Power Architecture Z4, SDK: NXP MPC57xx platform SDK) During thermal chamber testing at 115°C ambient, our MPC5746C-based board becomes completely unresponsive on boot — no UART console output at all, and this happens on every boot attempt at that temperature. The part appears to fully recover after cooling: reflashing/rebooting at room temperature restores normal operation with no persistent damage. Interestingly, we can still successfully reprogram flash via PEMicro JTAG debug probe while the board is at 115°C — we've confirmed this by flashing a build with an incremented version string at temperature and reading back the new version after cooling down. So the debug-probe flash path works at 115°C; only the application boot path hangs/bad state. From manual it states MCU can with hold upto 125°C.  Could you please help us to root cause the issue and how fix this issue. Re: MPC5746C hangs (no boot, no UART) at 115°C ambient Hello, From manual it states MCU can with hold upto 125°C. Yes, that is not an issue. Could you please help us to root cause the issue and how fix this issue. Since this is your custom board and issue disappear after cooling I suspect: 1. Clock startup issue (highest probability) At 115°C: External crystal (FXOSC) startup time increases. Oscillator gain margin decreases. Load capacitors shift value with temperature. PCB leakage increases. The debugger can still access the part because debug logic uses its own infrastructure and does not depend on the application reaching main(). FXOSC status bits CMU clock-monitor faults FIRC-only boot experiment Run entirely from FIRC and disable external crystal temporarily The fact that JTAG programming continues to work at 115°C is the strongest clue that the core infrastructure remains alive and the failure is occurring very early in the application boot path rather than in the flash array itself best regards, Peter Re: MPC5746C hangs (no boot, no UART) at 115°C ambient Thank you for the insight @petervlna. Following up on this, my colleague @mnargund and me investigated further, we were able to get the MPC5746C booting successfully at 115°C. Here is a summary of what we found. Root Cause: During pre-initialization, we configured the system to bring up FIRC, FXOSC, and PLL, and then switched the system clock from FIRC to PLL. Following this, we triggered a mode transition to DRUN mode (even though the system was already in DRUN mode by default, a transition to the same mode is required for the new configuration to take effect, as mentioned in the manual), and polled MC_ME_GS.MTRANS to wait for the transition to complete. However, even after MC_ME_GS.MTRANS cleared, the code faulted with an IVOR1 exception, maybe indicating the transition had not fully stabilized by the time execution continued. At elevated temperatures (115°C), the transition appears to take longer than at room temperature, causing the system to be in an inconsistent state when the next instructions were executed. Workaround applied: We inserted an explicit software delay after the MC_ME_GS.MTRANS poll and before proceeding with the rest of initialization. With a 500 ms delay, the boot is consistently successful at 115°C. We also tested a 100 ms delay, which also works reliably in our setup.  Is there a maximum recommended software delay that can safely be inserted at this point in initialization? Is there a recommended practice to ensure reliable clock stabilization before proceeding, across the full operating temperature range up to 125°C?
查看全文
PN7221+Android16 EDLA認証に関する問題 PN7221、Android 16   EDLA認証を受けたビルドは、部分的なNFC機能のみをサポートしています。当社のテストではカード検出機能は正常に動作しましたが、EMVCo、ファームウェアのアップグレード、その他の機能は利用できません。比較によって特定された根本原因は以下のとおりです。   EDLAビルドはGoogleの既製NFCサービスを使用する一方、AOSPビルドはNXPのパッチを統合してコンパイルされている。   以下は、EDLA関連のビルド構成の抜粋です。   apex_set {   名前:「com.google.android.nfcservices_compressed」   apex_name:「com.android.nfcservices」   オーバーライド: ["com.android.nfcservices"],   所有者: "google"、   セット:「com.google.android.nfcservices_compressed.apks」   ファイル名:「com.google.android.nfcservices_compressed.apex」、   exported_bootclasspath_fragments: ["com.android.nfcservices-bootclasspath-fragment"],   } このシナリオでNXPパッチをインポートする方法を教えてもらえますか?代替案はありますか?NXP NFCチップを使用している他のお客様に対して、完全なNFC機能を維持しつつEDLA認証に合格するためにどのようなアプローチが取られていますか? Re: PN7221+Android16 EDLA certification issues こんにちは、 @zhangkai さん。 私たちの分析によると、この問題はGoogleのプリビルドNFC APEX(com.android.nfcservices)を用いたEDLAビルドが原因である可能性が高いですNXPのAndroidミドルウェアと統合されたNFCモジュールの代わりに、 NXP Android 16ソリューションは、NFCフレームワーク、NFCサービス、EMVCoフレームワーク、HALおよび関連ライブラリを含むAndroid NFCスタックの複数層を拡張しています。GoogleのプリビルトNFCサービスを使用する場合、標準的なNFC機能のみが利用可能になり、EMVCo機能、ファームウェアアップデートサポート、その他のミドルウェア拡張などのNXP固有の機能はアクティブでない場合があります。 現時点でNXPのAndroid 16移植ドキュメントには、Googleの既製品EDLA NFC APEXを直接パッチまたは修正する方法について説明されていません。NXPの一般的な統合アプローチは、AOSPソースコードの統合と、NXPミドルウェアを用いたNFCスタックの再構築に基づいています。 PN7221のフル機能を必要とするお客様には、NXP NFCミドルウェアを含んでNFC APEXを再構築できるか、EDLA準拠を維持しつつEDLA NFCモジュールのカスタマイズについてGoogleやOEMのサポートに相談することをお勧めします。
查看全文
ユーティリティソフトウェアの問題 LPC1765FBD100で使用するNXP MCUXpresso IDE開発ソフトウェアはどのようにダウンロードできますか? よろしくお願いします。 アナログ(ADC|CMP|DAC|オペアンプ) コアとメモリ 開発委員会 Re: 工具软件问题 こんにちは。MCUXPressoのダウンロードリンクはこちらです:無料のプロフェッショナルARM開発ツール|NXPセミコンダクターズ Celeste_Liu_0-1783663550952.png BR セレステ
查看全文
スワップ要求: HSE_SRV_ID_ACTIVATE_PASSIVE_BLOCK (Hse_Ip_ServiceRequest 経由) が 0xAA55A11E を返します こんにちは、現在S32K314HMSマイクロコントローラでA/Bスワップを試みています。交換リクエストは以下の方法で行われます。   /* ジョブステータス変数をリセットします */       SwapJobStatus = SWAP_JOB_PENDING ; /* HSEリクエストのサービス記述子を設定します */ swapHseSrvDescriptor.srvId = HSE_SRV_ID_ACTIVATE_PASSIVE_BLOCK; /* HSE IPレイヤーに送信するリクエストパラメータを設定します */       swapHseIpRequest.eReqType = HSE_IP_REQTYPE_ASYNC_POLL ;​​       swapHseIpRequest.u32Timeout = SWAP_TIMEOUT ;​​ swapHseIpRequest.pfCallback = SwapProcessMuChannelResponse; /* サービスリクエストをHSE IPレイヤーに送信します */ if (HSE_SRV_RSP_OK != Hse_Ip_ServiceRequest(SWAP_MU_INSTANCE, SWAP_MU_ADMIN_CHANNEL, &swapHseIpRequest, &swapHseSrvDescriptor))     {          結果= E_NOT_OK ;      } 次に、swapHseIpRequest.pfCallback ( SwapProcessMuChannelResponse)が呼び出され、返される HseResponse は次のようになります。 static void SwapProcessMuChannelResponse ( uint8 u8MuInstance , uint8 u8MuChannel ,                                              hseSrvResponse_t HseResponse 、 void * pCallbackParam ) {    if ( HseResponse == HSE_SRV_RSP_OK )     {       vFotaH_Appl_SwapJobStatus = SWAP_JOB_OK ;    }    それ以外     {       vFotaH_Appl_SwapJobStatus = SWAP_JOB_FAILED ;       VStdLib_ConvertUint32ToUint8ArrayBigEndian (( uint32 ) HseResponse , DebugData );    } } #define HSE_SRV_RSP_NOT_SUPPORTED (( hseSrvResponse_t ) 0xAA55A11EUL ) /**< @brief サポートされていない操作または機能です。 */ これは散発的に発生し、時にはスワップが期待どおりに機能することもあります。その理由は何でしょうか?HSEがこの返還コードを返答する理由やシナリオはどこで見つけられますか? このスワップは、リセットや電源オンの数分後にアップデートシーケンスの終了時にトリガーされます(つまりHSEは100%初期化されています)。 Re: Swap request: HSE_SRV_ID_ACTIVATE_PASSIVE_BLOCK via Hse_Ip_ServiceRequest returns 0xAA55A11E こんにちは、@AlexI さん。 これはパラメータのない非常にシンプルなサービスです。私が考えられる唯一の説明は、データキャッシュメモリが原因であるということです。記述子がキャッシュ不可能なメモリ領域に配置されていることを確認してください。 一般的に、HSEとの通信に使用されるすべてのデータオブジェクトは、キャッシュを認識できないため、キャッシュ対応できないメモリに強制的に移行する必要があります。 今回の理由はおそらく違うかもしれませんが、DTCMメモリを使う場合、バックドアアドレスを使う必要があるということです。通常のアドレスは、そのメモリを所有するコアからのみ参照可能です。他のバス・マスタ(他のコア、DMA、HSEなど)はバックドアアドレスを通じてのみこのメモリを認識できます。 lukaszadrapa_0-1783694396770.png よろしくお願いいたします。 ルーカス Re: Swap request: HSE_SRV_ID_ACTIVATE_PASSIVE_BLOCK via Hse_Ip_ServiceRequest returns 0xAA55A11E @lukaszadrapa さん、ご回答ありがとうございます。 実装を変更して、swapHseSrvDescriptorとswapHseIpRequestが初期値を持ち、起動時にリンカーによって初期化されるようにしました。実行時ではなく、今は動作しています。
查看全文
MPC5746C 在 115°C 环境温度下死机(无法启动,UART 无输出) 部件号: MPC5746C(电源架构 Z4,SDK:NXP MPC57xx 平台 SDK) 在 115°C 环境温度下进行热室测试时,我们基于 MPC5746C 的板在启动时完全无响应——没有任何 UART 控制台输出,并且在该温度下每次启动尝试都会发生这种情况。冷却后该部件似乎完全恢复:在室温下重新刷写/重启即可恢复正常运行,且不会造成永久性损坏。 有趣的是,即使电路板温度高达 115°C,我们仍然可以通过 PEMicro JTAG 调试探针成功地对闪存进行重新编程——我们通过在高温下刷入版本字符串递增的构建版本,并在冷却后读取新版本,证实了这一点。因此,调试探测闪存路径在 115°C 下工作;只有应用程序启动路径挂起/处于错误状态。 手册上说MCU可以承受高达125°C的温度。 请问您能否帮我们找出问题的根本原因以及如何解决这个问题? Re: MPC5746C hangs (no boot, no UART) at 115°C ambient 你好, 手册上说MCU可以承受高达125°C的温度。 是的,这不是问题。 请问您能否帮我们找出问题的根本原因以及如何解决这个问题? 由于这是你的定制板,而且问题在冷却后消失,我怀疑: 1. 时钟启动问题(可能性最高) 在 115°C 时: 外部晶体(FXOSC)启动时间增加。 振荡器增益裕度降低。 负载电容的电容值会随温度变化。 PCB漏电加剧。 调试器仍然可以访问该部分,因为调试逻辑使用自己的基础架构,并不依赖于应用程序是否执行到 main() 函数。 FXOSC 状态位 CMU时钟监测故障 仅 FIRC 启动实验 完全通过 FIRC 运行,并暂时禁用外部晶振。 JTAG编程在115°C下仍能正常工作,这有力地表明核心基础设施仍然运行正常,故障发生在应用程序启动路径的早期阶段,而不是闪存阵列本身。 顺祝商祺! Peter Re: MPC5746C hangs (no boot, no UART) at 115°C ambient 感谢@petervlna的真知灼见。 随后,我和我的同事@mnargund进行了进一步调查,我们成功地让 MPC5746C 在 115°C 下启动。以下是我们发现的结果总结。 根本原因:在预初始化期间,我们配置系统启动 FIRC、FXOSC 和 PLL,然后将系统时钟从 FIRC 切换到 PLL。随后,我们触发了向 DRUN 模式的模式转换(尽管系统默认已处于 DRUN 模式,但如手册中所述,需要转换到相同模式才能使新配置生效),并轮询 MC_ME_GS.MTRANS 以等待转换完成。 然而,即使在 MC_ME_GS.MTRANS 清除之后,代码仍然出现 IVOR1 异常,这可能表明在执行继续进行时,转换尚未完全稳定。在高温(115°C)下,转变似乎比在室温下需要更长时间,导致系统在执行下一条指令时处于不一致的状态。 已采取的变通方法:我们在 MC_ME_GS.MTRANS 轮询之后、在继续执行其余初始化操作之前插入了一个显式的软件延迟。延迟 500 毫秒,在 115°C 下启动始终成功。我们还测试了 100 毫秒的延迟,在我们的设置中也能可靠地工作。 在初始化过程中,是否存在一个可以安全插入的最大推荐软件延迟? 在高达 125°C 的整个工作温度范围内,是否有推荐的做法来确保时钟稳定可靠?
查看全文
PCA2131: コントロールレジスタ2のAF(アラームフラグ)はクリアできません こんにちは、皆さん 現在、 PCA2131 オートモーティブ RTCをバッテリー・マネジメント・システム(BMS)に統合しています。 アラームフラグ(AF、Control_2レジスタ01hのビット4)がハイのままになるという問題が継続的に発生しています。基本的なSPI通信は完璧に動作しており、タイムレジスタの設定や読み込みは問題なくできます。しかし、初期化時にAFフラグをクリアできません。 重要な背景情報: AFフラグをクリアする前に、アラームレジスタ(0Ah~0Eh)内のすべてのアラーム有効化(AE_X)ビットが1(無効)に設定されていることを既に確認済みです。 私が実行しているシーケンス: Control_2(レジスタ01h)を読み取ります。AFビットは1と読み取られます。 ローカル構造体でAF = 0とAIE = 0に設定してフラグをクリアします。 変更したバイトをControl_2に書き戻す。 Control_2をもう一度読み込んでください。AFビットはまだ1です。 デバッグセッションのスクリーンショットを添付しました。クリア前、クリア操作中、および読み出し後のレジスタの状態を示しています。 私の質問: すべてのAE_Xビットが無効化されている場合、他にAFフラグを即座に再アサートさせる(またはクリアを妨げる)内部条件は何でしょうか? ご意見やご提案をいただければ大変ありがたいです! Re: PCA2131: AF (Alarm Flag) in Control Register 2 will not be able to clear こんにちは、ヨゼフさん。 あなたのサポートと正しい方向への教えてくださり、ありがとうございます。 私はピコスコープを使ってSPIメッセージを確認し、ハードウェアの値が正しいことを検証しました。ご提案に従い、さらにコードをデバッグし、根本原因がビットフィールドの順序の不一致であることを確認しました。 不一致を修正しましたので、問題は完全に解決しました。ご協力ありがとうございました! よろしくお願いします、 ヴィカス Re: PCA2131: AF (Alarm Flag) in Control Register 2 will not be able to clear こんにちは、ヴィカスさん。 ご確認いただきありがとうございます。データシートに記載されている PCA2131 の動作を考慮すると、AE_S/AE_M/AE_H/AE_D/AE_W がすべて 1 であると仮定すると、RTC が AF を正しく再トリガーしているようには見えません。最も可能性の高い原因はビットフィールドの順序ミスマッチです。3つの読み書きSPIメッセージの範囲をぜひ教えていただけますか?タイミングと、書き込みおよび読み出しされたレジスタ/ビットを確認するため。 JozefKozon_2-1783678052638.png 敬具、 ヨゼフ Re: PCA2131: AF (Alarm Flag) in Control Register 2 will not be able to clear おっと、タイプミスでごめんなさい!正しいアドレスは0Ehから12hです。再確認したところ、コードに正しく記載されていたので、メッセージの誤りでした。 Re: PCA2131: AF (Alarm Flag) in Control Register 2 will not be able to clear こんにちは、ヴィカスさん。 警報記録を再度確認してください。これらのレジスタのアドレスは0Ehから12hです。 JozefKozon_0-1783672873300.png JozefKozon_1-1783672931555.png AE_xビットをすべて1に再度設定してみてください。 敬具、 ヨゼフ
查看全文
Zone Node Overview 1 Table of Contents • Introduction • Overview • Context • References • Conclusion 2 Introduction This article series explains the role and behavior of a zonal controller communication component in a modern automotive electrical/electronic (E/E) architecture. This first article provides a short, high-level introduction to the zonal node and establishes a common understanding of its main responsibilities. The series gradually explains how this component enables message exchange between in-vehicle communication networks, with a particular focus on routed and broadcast communication over CAN and LIN. Later articles move from these concepts into more detailed design and implementation topics. As the entry point to the Zonal Communication and Control series, this article focuses on the zonal node from an architectural perspective. It does not cover system-level use cases or application-specific configurations, which are addressed in later articles. 3 Overview This article introduces an S32K3-based zonal node and explains how it connects to several in-vehicle networks. In practice, the zonal node sits between central vehicle controllers and local devices such as sensors, actuators, or small control modules, helping messages move between them. The zonal node receives messages from the central controller and forwards them to local nodes, while also sending status information and responses back to the central side. Depending on the system design, it can distribute the same message to multiple nodes or route specific messages only to the intended recipients. In addition to message forwarding, the zonal node may perform limited local processing, such as message filtering, signal aggregation, data validation, or basic decision-making related to communication handling. However, higher-level functional decisions are typically managed by central controllers, with the zonal node focusing primarily on efficient and reliable data exchange. This role becomes clearer in the context of evolving automotive E/E architectures. Traditional designs relied on many purpose-specific electronic control units (ECUs) connected through dedicated wiring. As system complexity increased, that approach added wiring weight, raised cost, and limited scalability. dragostoma_0-1782905205237.png Figure 1. Zonal controller highlighted within the EV architecture Zonal architectures address these limitations by grouping nearby functions within the same physical area of the vehicle and moving more processing into central computing units. In this model, the zonal controller manages local communication and forwards relevant information to the central system. In this context, the S32K3 MCU family supports the required functionality by providing automotive communication interfaces such as CAN FD and LIN. On devices that include the necessary interfaces, the zonal node can connect different network types and handle message traffic between them. Within the scope of this project, the S32K3 platform is suitable for implementing the zonal node due to its available communication peripherals, processing capability, and automotive safety features, which are sufficient for the number of connected nodes and the complexity of the communication tasks considered. This article is intended for: System architects evaluating zonal or domain-based vehicle designs Embedded software engineers implementing communication routing logic Engineers evaluating MCU platforms for multi-network automotive applications By reading this series, you will understand why zonal communication components matter, how they fit into modern vehicle architectures, and how the S32K3 platform can support this role. 4 Context In a complete vehicle system, the zonal node sits between the central control system and local hardware. Its main job is to pass, route, or translate messages, not to make application-level decisions. Keeping these roles separate helps the system remain predictable, reliable, and easier to scale. The zonal node may receive messages from central controllers that manage vehicle-wide functions or from local devices such as sensors, actuators, and smaller control modules. It then exchanges this information across different networks in a controlled and time-aware way. Note: CAN and LIN remain important because they are widely used in automotive systems and are well suited to many control tasks. The S32K3 family supports these needs with integrated CAN FD and LIN interfaces and Arm® Cortex®-M7 CPU cores for routing and control tasks. It also includes automotive safety features aligned with ISO 26262 and low-power modes that are useful in some system designs. Together, these features allow the zonal node to handle several communication channels at the same time while keeping the network interfaces clearly separated. High-Level Architecture Diagram dragostoma_1-1782905238932.png Figure 2. Diagram concept for S32K3 Zonal Node Figure 2 shows where the zonal node sits in the system: between the central control side and the local edge nodes, acting as the bridge between networks. Later articles will expand this context in a structured way. The series will first present the overall system, then describe the software and hardware environment that supports the zonal node. It will also cover internal control logic and key communication topics such as CAN-to-CAN routing, LIN-to-CAN routing, and Ethernet-to-CAN communication. Finally, it will discuss common challenges in multi-network routing and zonal integration. 5 References NXP Body Domain and Zonal Controller S32K3 for Zonal Aggregator 6 Conclusion This article provided a high-level introduction to the S32K3-based zonal node as a communication component in modern automotive architectures. It explained what the node does and where it fits in the system, creating a basis for the more detailed topics covered later in the series. Instead of focusing on implementation details, this introductory article explained why zonal nodes are needed and which problems they help address. The next articles in the series will build on this foundation by exploring system structure, configuration, communication routing strategies, and design challenges in greater detail.
查看全文
版本 2 问题:C 代码生成、预览 你好! 我开始测试 GUI Guider 版本 2,发现了一些问题(从空白模板和 Windows 模拟器开始)。 我开始定义顶层的内容,添加了一个图像按钮,并创建了一个事件处理程序,以便在长按按钮时切换状态。 生成的代码存在一些错误,例如: gg_event_layer_top.c: static void lv_layer_top()_event_handler(lv_event_t * e) { ... } void gg_event_init_layer_top ( gg_ui_t * ui😞 lv_obj_add_event_cb(ui->layer_top.lv_layer_top(), lv_layer_top()_event_handler, LV_EVENT_ALL, ui); (括号会导致解析错误) 手动删除括号后,会出现以下错误: .../generated/events/gg_event_layer_top.c:59:38: 错误:'gg_layer_top_t' 没有名为 'lv_layer_top' 的成员 (gg_layer_top_t 定义中不包含该成员) 我是否遗漏了某些定义,导致无法正确生成这些函数? Re: Version 2 issues: C code generation, preview 嗨@poldo 请问如何重现这个问题? Harry_Zhang_0-1783917409079.png BR 哈里 Re: Version 2 issues: C code generation, preview 您好@Harry_Zhang ,感谢您的回复。 我这样做了: - 在 layer_top 上(添加了可点击标志,这是必要的吗?)我创建了一个用于放置按钮的容器(没有添加可点击标志)。 - 我在容器内创建了一个图像按钮(添加了可点击的标志) 我已将“长按”事件附加到按钮上。 poldo_0-1784023768341.png 生成的代码包含上述语法错误。 // In gg_event_layer_top.c static void lv_layer_top()_event_handler(lv_event_t * e) { gg_ui_t * ui = lv_event_get_user_data(e); lv_event_code_t code = lv_event_get_code(e); switch(code) { default: break; } } void gg_event_init_layer_top(gg_ui_t * ui) { lv_obj_add_event_cb(ui->layer_top.lv_layer_top(), lv_layer_top()_event_handler, LV_EVENT_ALL, ui); lv_obj_add_event_cb(ui->layer_top.Keypad_btnEnable, Keypad_btnEnable_event_handler, LV_EVENT_ALL, ui); } 去掉括号后,语法错误是关于成员 lv_layer_top 不存在的: // In custom.h typedef struct { lv_obj_t * Keypad; lv_obj_t * Keypad_btnEnable; } gg_layer_top_t; BR 波尔多 Re: Version 2 issues: C code generation, preview 嗨@poldo 我尝试重现这个问题。 Harry_Zhang_0-1784102463813.png 生成的代码是正确的。 Harry_Zhang_1-1784102495298.png 请问我错过了什么? BR 哈里 Re: Version 2 issues: C code generation, preview 嗨@Harry_Zhang 。 问题出在顶层创建对象时。我附上文件供您审阅和测试。 Re: Version 2 issues: C code generation, preview 这是一个漏洞,修复起来很简单。找到你的 guiguider 文件,并以文本模式打开它。找到 event_list,删除任何多余的内容,然后使用指南重新加载项目。生成的代码将恢复正常。 Re: Version 2 issues: C code generation, preview 嗨@poldo 感谢您提供的项目,我们已经重现了这个问题。 这是个漏洞。 我们将在下一个版本中修复这个问题。 感谢您的理解。 BR 哈里 Re: Version 2 issues: C code generation, preview 谢谢你, @Harry_Zhang 。 在等待更新期间,有没有什么变通方法可以使用? BR
查看全文
Utilize pipe for logging Hi community, I am trying to integrate freemaster pipes for logging (and maybe use more of its functionality later on). As I am running linux I tried to go the freemaster light + python path. I can properly connect but when trying to open the pipeline and print my piped log messages I am not receiving any data via the rpc server. To verify the target implementation I also checked via the Windows GUI which could read the pipe properly, so the issue seems to be on the PC side. See attached example python script. Any hints welcome. best regards Re: Utilize pipe for logging Never mind, seems I have to explicitly call PipeFlush on the receiver side. Did not expect that. Attached the working example as reference. Re: Utilize pipe for logging Hello,  it is great you got it finally working. I confirm the PipeFlush needs to be called as it causes the pipe data to be exchanged in both directions. This is actually the only pipe call which causes a physical data transfer. All other operations at both PC and target sides are just buffering the data to pipe buffers. When using FreeMASTER protocol, the PC is the only initiator of communication. The target board cannot start it by itself. The PipeFlush is the place where PC gives the target a chance to report (and then send) any new pipe data. Regards, Michal
查看全文
Request to Extend License for S32 Design Studio for ARM 2018.R1 We are currently using S32 Design Studio for ARM 2018.R1 (Windows) for one of our products. The license has recently expired, and we are unable to activate the software. When we attempt to generate an activation key using our activation code, the generated key is also reported as expired, preventing us from using the IDE. Our activation code is: Activation Code: FF6A-EDA4-CDF0-7186 Could you please extend or renew the license associated with this activation code, or advise us on the appropriate steps to regain access to the software? Your assistance would be greatly appreciated, as this project depends on this development environment. Thank you. Re: Request to Extend License for S32 Design Studio for ARM 2018.R1 Hi,  your S32DS license has been extended.  Re: Request to Extend License for S32 Design Studio for ARM 2018.R1 Thanks. But I am still unable to activate the software. I tried both online and offline activations and it failed. This is what i get as the error: kasundinesh_0-1784003465339.png
查看全文
S32K144EVB-Q100 Rev D Schematic Hi. I'm looking for the schematic for S32K144EVB-Q100 Rev D. I cannot seem to make the board send any CAN messages. Is there sample code available to send message on CAN 0 on that board? I was able to use SPI and confirm the CAN transceiver is in forced normal mode so CAN should be working. Re: S32K144EVB-Q100 Rev D Schematic You may check the sample code at S32DS for S32K144EVB... Please share if any since i can not found it... Re: S32K144EVB-Q100 Rev D Schematic Hello @rosejp03, I've sent you a private message on the community regarding the design files. Regarding the CAN functionality, Rev. C (the current board I am using) & Rev. D have the same exact CAN design and transceiver (UJA1169): S32K144EVB-Q100 Rev. DS32K144EVB-Q100 Rev. DS32K144EVB-Q100 Rev. D S32K144EVB Rev. C1S32K144EVB Rev. C1S32K144EVB Rev. C1 Are you using any existing example? Either the AN5413: S32K1xx Series Cookbook or the ones included through the RTD package?  Are you using the 12V jack connector? Change J107 position to 1-2 and power the board with 12V. How are you testing CAN communication? Are you using another EVB, a CAN analyzer, or anything else? Can you try scoping the bus?  Best regards, Julián Re: S32K144EVB-Q100 Rev D Schematic Hi @db16122, If you also need the design files for S32K144EVB Rev. D, please let me know. Best regards, Julián
查看全文
ログ記録にパイプを利用する こんにちは、コミュニティの皆さん、 ログ記録のためにfreemasterパイプを統合しようとしています(そして、将来的にはその他の機能も利用したいと思っています)。 Linuxを使っているので、FreeMaster Light + Pythonの道を試しました。 正常に接続はできますが、パイプラインを開いてパイプログメッセージを印刷しようとすると、rpcサーバー経由でデータが一切届きません。 ターゲット実装を確認するために、Windows GUIでパイプを正しく読み取れるか確認したので、問題はPC側にあるようです。 添付のPythonスクリプトの例を参照してください。どんなヒントでも歓迎です。 よろしくお願いいたします Re: Utilize pipe for logging まあいいや、レシーバでPipeFlushを明示的に呼ぶ必要があるようだ。それは予想外だった。参考として、動作例を添付しました。 Re: Utilize pipe for logging こんにちは、 ようやく動作するようになってよかったですね。PipeFlushを呼び出す必要があることを確認しました。なぜなら、この関数はパイプデータの双方向交換を引き起こすからです。これは、物理的なデータ転送を引き起こす唯一のパイプ呼び出しです。PC側とターゲット側の両方におけるその他の操作はすべて、データをパイプバッファにバッファリングするだけです。 FreeMASTERプロトコルを使用する場合、通信の開始者はPCのみとなります。ターゲットボードは自動で起動できません。PipeFlushは、PCがターゲットに対して新しいパイプデータを報告(そして送信)する機会を与える場所です。 よろしくお願いいたします。 ミハル
查看全文
LPC18xxのウォッチドッグリセットを検出できません ウォッチドッグリセットが発生したことを検出する際に問題が発生しています。現在、ユーザーガイドに記載されている手順に従っています。 ウォッチドッグのタイムアウトフラグ(WDTOF)を調べることで、ウォッチドッグがリセット状態を引き起こしているかどうかを判断できます。WDTOFフラグはソフトウェアによってクリアされなければなりません。 デバイスのリセットは正しく行われるものの、その後フラグが設定されていないようです。 LPC4357で似たような問題に関する古い投稿(解決済み:LPC4357:ウォッチドッグリセットを検出できない - NXPコミュニティ)を見かけましたが、LPC18xxのエラッタには何も記載されていませんでした。 LPC18xxも上記と同じ問題を抱えているかどうか確認していただけますか? lpc18xx Re: Cannot detect watchdog reset for LPC18xx こんにちは@ejg 投稿ありがとうございます! どのLPC18xxを使っているのか、具体的に教えていただけますか? また、国旗をレビューしたのはいつですか? lpc18xx_wwdt.hからWWDT_Init関数を呼び出すと割り込みフラグが消去されるため、WDTOFを読み込む必要があります。 Re: Cannot detect watchdog reset for LPC18xx こんにちは、 @carlos_o さん、ご返信ありがとうございます。 私はLPC1837を使用しています。 このフラグは、他のWWDTレジスタとやり取りする前に、起動時にチェックされます。CMSIS SystemInitが完了したら、systickを設定し、このフラグを確認します。 Re: Cannot detect watchdog reset for LPC18xx こんにちは@ejg はい、LPC18xxはLPC43xxと同じ問題を抱えています。 コアリセットの原因を特定するには、LPC18xxユーザーマニュアルのセクション14.5.1「コアリセットの原因を特定する」を参照してください。 Alice_Yang_0-1784105602643.png BR アリック
查看全文
S32K144EVB-Q100 Rev D 原理图 你好。我正在寻找S32K144EVB-Q100 Rev D的原理图。我似乎无法让该板发送任何CAN消息。是否有可用于在该板上通过 CAN 0 发送消息的示例代码?我使用 SPI 确认了 CAN 收发器处于强制正常模式,因此 CAN 应该可以正常工作。 Re: S32K144EVB-Q100 Rev D Schematic 您可以查看 S32DS 中针对S32K144EVB 的示例代码……如果您有相关代码,请分享一下,因为我找不到…… Re: S32K144EVB-Q100 Rev D Schematic 你好@db16122 , 如果您还需要 S32K144EVB Rev. D 的设计文件,请告诉我。 此致, 朱利安 Re: S32K144EVB-Q100 Rev D Schematic 你好@rosejp03 , 关于设计文件,我已经通过社区私信联系你了。 关于 CAN 功能,Rev. C(我目前使用的电路板)和 Rev. D 具有完全相同的 CAN 设计和收发器 (UJA1169): S32K144EVB-Q100 Rev. DS32K144EVB-Q100 修订版 D S32K144EVB Rev. C1S32K144EVB 修订版 C1 你使用的是现有示例吗?是AN5413: S32K1xx 系列食谱,还是 RTD 软件包中包含的食谱? 你使用的是12V电源插孔吗?将J107 位置改为 1-2,并用 12V 电源为电路板供电。 你们是如何测试CAN通信的?您使用的是其他 EVB、CAN 分析仪还是其他设备?你能尝试用示波器探测一下总线吗? 此致, 朱利安
查看全文