Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
IW612 WLAN 5GHz transmission Hi,  We are planning to use IW612 SoC for WLAN in one of our IoT product, target market is US and Canada. IW612 supports dual band 2.4Ghz and 5GHz. Is there a way or configuration to turn 5GHz WIFI Operation OFF, as ISED Canada doesn't allow UNII-1 (5150-5250Mhz) WIFI transmission in outdoor environment without a license and limits operation to Indoor ONLY. Our product operates in Outdoor and we would like a way to Disable 5GHz entirely and operate on 2.4Ghz only. RSS-247 — Digital Transmission Systems, Frequency Hopping Systems and Licence-Exempt Local Area Network Devices in 902-928 MHz, 2400-2483.5 MHz, 5150-5350 MHz, and 5470-5895 MHz bands Can you confirm and share settings for same? Regards, Arun RF Re: IW612 WLAN 5GHz transmission Hello @pantarun_92  iw612 support loading power table, you could custom power table or use sample table for Canada region. It will disable not allowed channels and support DFS channel. Best Regards Shaun
View full article
imx95 和 vfio_pci 直通 您好, 我们希望在 IMX95 SoC 上使用具有 PCI 直通功能的虚拟机。这似乎完全不可能,因为 SMMU 不是缓存一致的,而 vfio_pci 驱动程序需要缓存一致性。参见: https://community.nxp.com/t5/i-MX-Processors/i-MX95-19x19-EVK-SMMU-coherent-table-walks-IDR0-COHACC-and-vfio/mp/2410515 和 https://github.com/NXP/dpdk/blob/25.11-qoriq/nxp/README_imx95_enetc_vf_vfio#L32 禁用 IOMMU 不是一个可行的方案。另外,我怀疑这样做是否会有帮助,因为内核参数是这样写的: MODULE_PARM_DESC(enable_unsafe_noiommu_mode, "启用不安全、无 IOMMU 模式。此模式不提供设备隔离、DMA 转换、主机内核保护,不能用于将设备分配给虚拟机,需要 RAWIO 权限,并且会污染内核。如果你不知道这是做什么用的,请远离。(默认值:false)"); 能否确认一下,是否真的无法将 IMX95 SoC 与(安全的)PCI 直通一起使用?如果不是,那我到底漏掉了什么? 此致, -迈克尔 Re: imx95 and vfio_pci passthrough 您好, 感谢您的快速回复。但我不太确定我是否完全理解了。为了确保万无一失,我们不想使用 DPDK,而是使用通用的 qemu/kvm 虚拟机,并在其中传递 PCI 设备。这与 uio-pci-generic 框架有何关系? 谢谢, -迈克尔 Re: imx95 and vfio_pci passthrough 您好, 感谢您对恩智浦半导体产品的关注, 在这种情况下,你需要采纳我同事的回复,也就是 DPDK 团队的回复。唯一的替代方案就是回复中提到的那个: “如果客户希望将 SMMU 用于其他用例,但可以接受绕过 DPDK(不想在 bootargs 中使用 iommu.passthrough=1 或在 dts 中禁用 SMMU 节点)。 然后可以尝试绑定 uio-pci-generic 框架并禁用 VSI-PSI 消息传递(export ENETC4_VSI_MSG_DISABLE=1)。但是禁用 VSI-PSI 消息意味着用户将无法使用某些 ENETC 功能,例如混杂模式、VLAN MAC 过滤和链路信息。 此致
View full article
How to get the full datasheet for BMA8420 ? not Product Brief   Subject: Inquiry regarding BMA8420 for Hydrogen Fuel Cell Stack EIS Measurement   Dear Technical Support Team, I am currently developing an Electrochemical Impedance Spectroscopy (EIS) measurement system for hydrogen fuel cells.   To utilize the BMA8420, I would like to review its technical specifications, but I have been unable to locate the datasheet online.   I would highly appreciate your guidance on the following questions: Can the BMA8420 be used to measure the EIS of a hydrogen fuel cell stack? How can I obtain the BMA8420 full datasheet(not Product Brief ) ? Contact point in Korea ? Thank you for your support, and I look forward to hearing from you.   Best regards, Young, Kim       BMA8420   <-- link image.png #BMA8420
View full article
求助关于RT1052显示旋转问题 因为购买的屏幕是竖屏,而我需要横屏显示。我使用的是guiguider生成RT1052的基础显示代码 并且添加软件旋转 disp_drv.sw_rotate = 1; disp_drv.rotated = 1;   设置成单缓冲 SDK_ALIGN( __attribute__((section("lvglDisplayBuffer"))) static uint8_t s_frameBuffer[1][DEMO_FB_SIZE], DEMO_FB_ALIGN); SDK_ALIGN( __attribute__((section("lvglDisplayBuffer"))) static uint8_t s_lvglBuffer[DEMO_DB_SIZE], DEMO_FB_ALIGN); 屏幕能够正常显示,但是刷新速度太慢,不符合我的需求。   设置成双缓冲 SDK_ALIGN( __attribute__((section("lvglDisplayBuffer"))) static uint8_t s_frameBuffer[2][DEMO_FB_SIZE], DEMO_FB_ALIGN); 只有背光亮,屏幕黑屏。 这是为什么?   #if FB_USE_SRAM static void DEMO_WaitVsync(lv_disp_drv_t *disp_drv) { s_framePending = true; #if defined(SDK_OS_FREE_RTOS) if (xSemaphoreTake(s_frameSema, portMAX_DELAY) != pdTRUE) { PRINTF("Display flush failed\r\n"); assert(0); } #else while (s_framePending) { } #endif } static void copy_area(const lv_area_t *area, lv_color_t *color_p, uint8_t *fb, uint32_t fbStrideBytes) { uint32_t y; uint32_t areaWidth = lv_area_get_width(area); fb += (area->y1 * fbStrideBytes + area->x1 * sizeof(lv_color_t)); for (y = area->y1; y <= area->y2; y++) { lv_memcpy(fb, color_p, areaWidth * sizeof(lv_color_t)); fb += fbStrideBytes; color_p += areaWidth; } } static void DEMO_FlushDisplay(lv_disp_drv_t *disp_drv, const lv_area_t *area, lv_color_t *color_p) { /* Wait VSYNC for each small update. */ DEMO_WaitVsync(disp_drv); /* Copy data from draw buffer to frame buffer. */ copy_area(area, color_p, (uint8_t*) s_frameBuffer, LCD_WIDTH * LCD_FB_BYTE_PER_PIXEL); SCB_CleanInvalidateDCache(); lv_disp_flush_ready(disp_drv); } #else static void DEMO_FlushDisplay(lv_disp_drv_t *disp_drv, const lv_area_t *area, lv_color_t *color_p) { // DCACHE_CleanByRange((uint32_t)color_p, DEMO_FB_SIZE); DCACHE_CleanInvalidateByRange((uint32_t)color_p, DEMO_FB_SIZE); ELCDIF_SetNextBufferAddr(LCDIF, (uint32_t)color_p); s_framePending = true; #if defined(SDK_OS_FREE_RTOS) if (xSemaphoreTake(s_frameSema, portMAX_DELAY) == pdTRUE) { /* IMPORTANT!!! * Inform the graphics library that you are ready with the flushing*/ lv_disp_flush_ready(disp_drv); } else { PRINTF("Display flush failed\r\n"); assert(0); } #else while (s_framePending) { } /* IMPORTANT!!! * Inform the graphics library that you are ready with the flushing*/ lv_disp_flush_ready(disp_drv); #endif } #endif i.MXRT 105x Re: 求助关于RT1052显示旋转问题 Hi @dsd , 感谢您的问题! 首先,请检查以下LVGL的限制,启用了full_refresh=1时,不支持屏幕旋转。请参考: 1. https://github.com/lvgl/lvgl/issues/4060 2. https://forum.lvgl.io/t/why-cannot-rotate-a-full-refreshed-display/10490/3   另外,RT1050有硬件pxp支持旋转,这是更推荐的方案,请参考:https://docs.nxp.com/bundle/GUIGUIDERUG-1.6.1/page/topics/rotate_screen_and_widgets.html 以及SDK中的PXP旋转相关demo。   Best regards, Gavin Re: 求助关于RT1052显示旋转问题 Helllo, 在使用 NXP i.MX RT1052 结合 Guiguider (LVGL) 进行屏幕旋转开发时,你遇到的“单缓冲刷新慢、双缓冲黑屏”问题,核心原因在于软件旋转(Software Rotate)与硬件 ELCDIF 控制器、双缓冲切换机制以及内存地址索引没有适配好。 Best Regards Re: 求助关于RT1052显示旋转问题 非常感谢,pxp旋转确实可行,完美解决问题
View full article
S32K3 Floating point cfg Hello Team, In my project, i am trying to do arithmetic operation using float data, but calculation is not happening as expected. #define macro -31.374 when i try to print in macro value using UTILS PRINTF, i am getting -32.374, similarly for other values, value get incremented by 1. Because of this, my calculations not happening as expected. Is there any cfg i need to do for this?  My current target setting nirmal_masilamani_0-1790009448678.pngnirmal_masilamani_0-1790009448678.png Re: S32K3 Floating point cfg Hi @nirmal_masilamani  Could you please clarify what you mean by "UTILS PRINTF"? How are you performing the calculations? Are the results stored in a float variable? If yes, does the variable already contain the wrong value when viewed in the debugger, or is the issue only observed when printing it? BR, VaneB Re: S32K3 Floating point cfg Hello @VaneB , Thank you for your support, yes issue was in PRINTF function, while debugging i was able to read the proper data.
View full article
Help Required Replacing Default Winbond Flash with Everspin Memory Custom Flash Driver Hello NXP Community, I am working on an i.MX RT1170 EVKB / MIMXRT1176 board and need some guidance regarding replacing the default Winbond external memory with an Everspin EM032LXQADG13IS2T memory device. Current Hardware The board originally uses a Winbond W25Q512 device. I have replaced it with: Everspin EM032LXQADG13IS2T The main issue is that the Everspin memory does not support SFDP, whereas the default Winbond memory supports SFDP. Current Status I have already been able to communicate with the Everspin memory using the i.MX RT1170 FlexSPI interface. The memory is functionally working when the application is running from RAM. In particular: FlexSPI communication with the Everspin memory is working. Memory read/write operations can be performed. The application image (XIP image) can be loaded/programmed into the Everspin memory using a memory write code. The image stored in the Everspin memory can then be accessed/executed successfully. However, I currently cannot flash/program the application directly to the Everspin memory using the normal i.MX RT1170 flash programming. Since the Everspin memory does not support SFDP, I suspect that the default FlexSPI flash driver/configuration used for the Winbond memory cannot automatically identify/configure the Everspin device. I would like to understand the recommended NXP approach for supporting a non-SFDP memory device. I would appreciate guidance on 1. How can I create a custom flash driver for the Everspin EM032LXQADG13IS2T on i.MX RT1170? 2. Is there an existing example of supporting a non-SFDP SPI/QSPI memory with the i.MX RT1170 FlexSPI controller? Boot ROM|Booting | Flash Development Board Re: Help Required Replacing Default Winbond Flash with Everspin Memory Custom Flash Driver Dear @jyothzz , Thank you for your questions. Yes, the MIMXRT1170_SFDP_QSPI.cfx flash driver is the default flash driver used by the RT1170 EVK and the MCUXpresso SDK: ShellyZhang_0-1790052100477.png Currently, there is no existing example of supporting a non-SFDP SPI/QSPI memory with the i.MX RT1170 FlexSPI controller. The flash drivers that are directly supported without customer modification are listed below: ShellyZhang_1-1790052161488.png You may refer to the information below to create a custom flash driver:  1. https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/How-to-create-a-new-Flash-driver-of-the-MCUXPresso-IDE/ta-p/1274718 2. https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/RT1170-flexSPI1-secondary-QSPI-flash-debug-flashdriver/tac-p/1938828 If you have any questions while developing the custom flash driver, please feel free to reach out. Best Regards, Shelly Re: Help Required Replacing Default Winbond Flash with Everspin Memory Custom Flash Driver Hi @ShellyZhang  Thank you For response it was of great help. We have resolved the flash driver issue with the new memory which does not support SFDP. We used the same i.MXRT117x_SFDP_QSPI Driver. We modifying the SFDP part referring to the non-SFDP Driver of i.MXRT1050_QSPI. Then generated a new driver file (.cfx) which worked fine . Once again thanking you for your guidance. Regards, JYOTHISH
View full article
Request for MTTF-FIT Reliability Data Dear Sir/Madam, I am currently calculating the MTBF value for our product, in which we have used the components manufactured by your company. Therefore, I kindly request you to provide the MTTF and/or FIT value for the below-mentioned component(s), if available. This information will help us to calculate the MTBF of our product accurately. Part Number: NTS0104BQ,115 Description: Voltage Level Translator Bidirectional 1 Circuit 4 Channel 50Mbps 14-DHVQFN (2.5x3) If any additional information regarding the operating conditions or application is required to provide the reliability data, please let us know. Thank you for your support. Cloud Lab online debug online laboratory Virtual test
View full article
imx95とvfio_pciパススルー こんにちは、 IMX95 SoC上でPCIパススルー機能を備えた仮想マシンを使用したいと考えています。しかし、SMMUはキャッシュコヒーレントではなく、vfio_pciドライバーがそれを必要としているため、これは全く不可能のようです。関連項目: https://community.nxp.com/t5/i-MX-Processors/i-MX95-19x19-EVK-SMMU-coherent-table-walks-IDR0-COHACC-and-vfio/mp/2410515 そして https://github.com/NXP/dpdk/blob/25.11-qoriq/nxp/README_imx95_enetc_vf_vfio#L32 IOMMUを無効にすることはできません。また、カーネルパラメータが次のように書かれているので、役に立つとは思えません。 MODULE_PARM_DESC(enable_unsafe_noiommu_mode, "安全でない、IOMMUなしモードを有効にします。このモードはデバイス隔離を提供せず、DMA変換もホストカーネル保護も提供せず、 仮想マシンへのデバイス割り当てには使用できず、RAWIO権限が必要で、カーネルを汚染します。これが何のためにあるのか分からない場合は、離れてください。(デフォルト:false)""); IMX95 SoCを(安全な)PCIパススルーで使うのは本当に不可能なのでしょうか?そうでないなら、私が何か見落としているのでしょうか? よろしくお願いします、 マイケル Re: imx95 and vfio_pci passthrough こんにちは、 迅速なご回答ありがとうございます。でも、完全に理解できているかどうか自信がありません。念のため確認ですが、DPDKは使用せず、PCIデバイスをパススルーする汎用的なqemu/kvm仮想マシンを使用したいと考えています。これはuio-pci-genericフレームワークとどのように関連しているのでしょうか? ありがとう、 マイケル Re: imx95 and vfio_pci passthrough こんにちは、 NXP Semiconductors製品にご関心いただきありがとうございます。 この場合、DPDKチームの同僚の回答に従う必要があります。唯一の選択肢は、回答で述べられているものです。 「顧客が他の用途でSMMUを使いたいが、DPDKではバイパスしても許容される場合(bootargsでiommu.passthrough=1を使いたくない、DTSでSMMUノードを無効にしたくない場合)。 その後、uio-pci-genericフレームワークのバインドを試み、VSI-PSIメッセージングを無効にすることができます(エクスポートENETC4_VSI_MSG_DISABLE=1)。しかしVSI-PSIメッセージを無効にすると、ユーザーはpromisc、VLAN MACフィルタリング、リンク情報などのENETC機能の一部を使えなくなります。」 よろしくお願いします。
View full article
MIMXRT1176 ADP – SEGGER J-Link debugging issue Hi everyone, I am currently working with the MIMXRT1176 / i.MX RT1170 platform. I initially used the MIMXRT1170-EVKB for development, but have now shifted to the MIMXRT1176-ADP for interfacing a parallel RGB panel. I am facing an issue with SEGGER J-Link debugging on the ADP board. Environment: Board: MIMXRT1176-ADP Board revision: 700-51950 REV A1 Schematic revision: SCH-51950 REV B1 MCUXpresso IDE: v25.6.136 MCUXpresso SDK: v25.09.00 SEGGER J-Link: latest version On the EVKB, both J-Link and LinkServer worked without any issues. However, on the ADP: Firmware flashes successfully. Debugger reaches the first line of main(). If I Step Over once, it stops at: Break at address "0xdeadbeee" with no debug information available, or outside of program code. Breakpoints at other locations work and are hit correctly. However, Resume/Continue from a breakpoint again results in 0xDEADBEEE. Could someone please confirm whether J-Link is fully supported with MCUXpresso IDE on the MIMXRT1176-ADP, and whether there is any specific J-Link script, reset/debug configuration, or ADP-specific initialization required? Could this be related to the memory configuration, external flash/SDRAM, or startup code on the ADP? Any guidance or working J-Link configuration for the ADP would be greatly appreciated. Thanks! Re: MIMXRT1176 ADP – SEGGER J-Link debugging issue Hi @HasanIqbalKhan , Thanks for your questions! As far as I know, when using JLink with the RT1170-ADP in MCUXpresso IDE, only "attach" is supported while direct debugging is not supported. This is likely a support issue with the JLink flashloader. In IAR, this issue has been resolved. We apologize for any inconvenience this may cause. Best regards, Gavin Re: MIMXRT1176 ADP – SEGGER J-Link debugging issue One more thing I tried, I connected an external MCU-Link and then tried debugging via the LinkServer in MCUXpresso IDE. The Execution reached main, I am able to step through from there, but when I try to resume execution it gives "Break at address "0x0" with no debug information available, or outside of program code.", and sometimes when I try to restart execution, it gives "Break at address "0x2230c8" with no debug information available, or outside of program code." For reference I am trying to run the "MIMXRT1176_dashboard_bt_ble_multiprofile" project, SW1 on the board is set to 01 and SW5 on the board is set to 000000000000. I tried to test with MCU-Link because the EVKB board uses the same and works fine. Also I do not think we can use Jlink, as it is clearly mentioned on their website that there is no support for octal flash, which the ADP board uses. Thanks. Re: MIMXRT1176 ADP – SEGGER J-Link debugging issue Is it possible to use debug via USB (J33) ? Re: MIMXRT1176 ADP – SEGGER J-Link debugging issue Hi @HasanIqbalKhan , 1. J33 is USB-OTG1 and cannot be used for debugging.  2. It’s not that JLink doesn’t support Octal Flash; it’s just that by default, it only recognizes the flash found on the EVK/EVKB. As for IAR, this is because a corresponding download algorithm is provided. If you’re interested in this topic, you can refer to the RT-UFL project. 3. For information on current debugger/IDE support, please refer to: AN14387: https://docs.nxp.com/bundle/AN14378/page/topics/download_images_to_ADP_board.html Best regards, Gavin
View full article
需要帮助:将默认的 Winbond 闪存替换为 Everspin Memory 自定义闪存驱动程序 NXP社区的各位朋友,大家好! 我正在使用i.MX RT1170 EVKB / MIMXRT1176开发板,需要一些关于将默认的 Winbond 外部存储器替换为Everspin EM032LXQADG13IS2T存储器的指导。 当前硬件 主板原先使用的是Winbond W25Q512设备。我已经将其更换为: Everspin EM032LXQADG13IS2T 主要问题是 Everspin 内存不支持 SFDP ,而默认的 Winbond 内存支持 SFDP。 当前状态 我已经能够使用 i.MX RT1170 FlexSPI 接口与 Everspin 内存进行通信。 当应用程序从 RAM 运行时,内存功能正常。尤其: FlexSPI 与 Everspin 存储器的通信正常。 可以执行内存读/写操作。 可以使用内存写入代码将应用程序映像(XIP 映像)加载/编程到 Everspin 内存中。 然后就可以成功访问/执行存储在 Everspin 内存中的图像。 但是,我目前无法使用正常的 i.MX RT1170 闪存编程将应用程序直接烧录/编程到 Everspin 存储器中。 由于 Everspin 存储器不支持 SFDP,我怀疑 Winbond 存储器使用的默认 FlexSPI 闪存驱动程序/配置无法自动识别/配置 Everspin 设备。 我想了解恩智浦 (NXP) 推荐的对非 SFDP 存储设备的支持方法。 我希望得到一些指导。 1. 如何为 i.MX RT1170 上的 Everspin EM032LXQADG13IS2T 创建自定义闪存驱动程序? 2. 是否有使用 i.MX RT1170 FlexSPI 控制器支持非 SFDP SPI/QSPI 存储器的现有示例? 启动 ROM | 启动配置 | 闪存 开发板 Re: Help Required Replacing Default Winbond Flash with Everspin Memory Custom Flash Driver 亲爱的@jyothzz , 谢谢你的提问。 是的,MIMXRT1170_SFDP_QSPI.cfx 闪存驱动程序是 RT1170 EVK 和 MCUXpresso SDK 使用的默认闪存驱动程序: ShellyZhang_0-1790052100477.png 目前还没有使用 i.MX RT1170 FlexSPI 控制器支持非 SFDP SPI/QSPI 存储器的例子。以下列出了无需用户修改即可直接支持的闪存驱动程序: ShellyZhang_1-1790052161488.png 您可以参考以下信息来创建自定义闪存驱动器: 1. https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/How-to-create-a-new-Flash-driver-of-the-MCUXPresso-IDE/ta-p/1274718 2. https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/RT1170-flexSPI1-secondary-QSPI-flash-debug-flashdriver/tac-p/1938828 如果您在开发自定义闪存驱动程序时有任何疑问,请随时联系我们。 顺祝商祺! 雪莉 Re: Help Required Replacing Default Winbond Flash with Everspin Memory Custom Flash Driver 你好@ShellyZhang 非常感谢您的回复,这对我帮助很大。 我们已经解决了新内存不支持SFDP的闪存驱动程序问题。 我们使用了相同的 i.MXRT117x_SFDP_QSPI 驱动程序。我们正在修改 SFDP 部分,使其与 i.MXRT1050_QSPI 的非 SFDP 驱动程序相关。 然后生成了一个新的驱动程序文件(.cfx),运行正常。 再次感谢您的指导。 问候, 占星术
View full article
S32K3 浮動小数点設定ファイル こんにちは、チームの皆さん、 私のプロジェクトでは、浮動小数点数データを使用して算術演算を行おうとしていますが、計算が期待どおりに行われません。 #define macro -31.374 UTILS PRINTF を使用してマクロ値を表示しようとすると、 -32.374 になります。同様に他の値についても、値は1ずつ増加します。 そのため、計算結果が期待通りにならなかった。 これに関して何か設定ファイル(cfg)を作成する必要はありますか? 現在の目標設定 nirmal_masilamani_0-1790009448678.pngnirmal_masilamani_0-1790009448678.png Re: S32K3 Floating point cfg こんにちは、 @nirmal_masilamani さん。 「UTILS PRINTF」とは具体的に何を指しているのか教えていただけますか? どのように計算を行っていますか?結果は浮動小数点変数に格納されますか?はいの場合、デバッガーで確認した時点で既に変数に誤った値が含まれているのでしょうか、それとも問題はそれを印刷した時のみ発生するのでしょうか? BR、VaneB Re: S32K3 Floating point cfg こんにちは、 @VaneB さん。 サポートありがとうございます。はい、問題はPRINTF関数にありました。デバッグ中に正しいデータを読み取ることができました。
View full article
MIMXRT1176 ADP – SEGGER J-Link 调试问题 大家好, 我目前正在使用MIMXRT1176 / i.MX RT1170 平台。最初我使用MIMXRT1170-EVKB进行开发,但现在已改用MIMXRT1176-ADP来连接并行 RGB 面板。 我 在使用 ADP 板上的 SEGGER J-Link 进行调试时 遇到了问题 。 环境: 电路板:MIMXRT1176-ADP 电路板修订: 700-51950 REV A1 原理图修订: SCH-51950 REV B1 MCUXpresso IDE: v25.6.136 MCUXpresso SDK: v25.09.00 SEGGER J-Link:最新版本 在EVKB上, J-Link 和 LinkServer 都能正常工作。但是,在 ADP 上: 固件刷写成功。 调试器到达main() 函数的第一行。 如果我跨过一次,它会停在: 在地址“0xdeadbeee”处断点,没有可用的调试信息,或者在程序代码之外。 其他位置的断点都能正常工作并被正确触发。 但是, 从断点 恢复/继续操作 再次会导致 0xDEADBEEE 错误 。 请问有人可以确认一下MIMXRT1176-ADP 上的 MCUXpresso IDE 是否完全支持 J-Link吗?是否需要任何特定的J-Link 脚本、复位/调试配置或 ADP 特定的初始化? 这是否与 ADP 上的 内存配置、外部闪存/同步动态随机存取存储器(SDRAM) 或启动代码 有关? 非常感谢您能提供任何关于ADP的J-Link配置指导或有效方案。 谢谢您! Re: MIMXRT1176 ADP – SEGGER J-Link debugging issue 你好@HasanIqbalKhan , 谢谢你的提问! 据我所知,在 MCUXpresso IDE 中使用 JLink 和 RT1170-ADP 时,仅支持“attach”功能,不支持直接调试。这很可能是 JLink 闪存加载器的支持问题。在 IAR 中,这个问题已经解决。由此造成的不便,我们深表歉意。 此致, 加文 Re: MIMXRT1176 ADP – SEGGER J-Link debugging issue 我还尝试了另一种方法,连接了一个外部 MCU-Link,然后尝试通过 MCUXpresso IDE 中的 LinkServer 进行调试。 程序执行到 main 函数后,我可以从那里单步执行,但是当我尝试恢复执行时,它会显示“在地址 0x0 处中断,没有可用的调试信息,或者中断在程序代码之外。”,有时当我尝试重新启动执行时,它会显示“在地址 0x2230c8 处中断,没有可用的调试信息,或者中断在程序代码之外。” 作为参考,我正在尝试运行“MIMXRT1176_dashboard_bt_ble_multiprofile”项目,板上的SW1设置为01,板上的SW5设置为000000000000。 我尝试使用 MCU-Link 进行测试,因为 EVKB 板也使用相同的 MCU-Link,而且测试结果良好。 另外,我认为我们不能使用 Jlink,因为他们的网站上明确提到不支持八进制闪存,而 ADP 板使用的是八进制闪存。 谢谢。 Re: MIMXRT1176 ADP – SEGGER J-Link debugging issue 是否可以通过 USB (J33) 进行调试? Re: MIMXRT1176 ADP – SEGGER J-Link debugging issue 你好@HasanIqbalKhan , 1. J33 是 USB-OTG1 接口,不能用于调试。 2. 并不是 JLink 不支持八进制闪存;只是默认情况下,它只能识别 EVK/EVKB 上的闪存。至于 IAR,这是因为提供了相应的下载算法。如果您对这个话题感兴趣,可以参考 RT-UFL 项目。 3. 有关当前调试器/IDE 支持的信息,请参阅:AN14387: https://docs.nxp.com/bundle/AN14378/page/topics/download_images_to_ADP_board.html 此致, 加文
View full article
ROMブートローダーのWriteMemoryコマンドのCRC16計算 現在、別のマイコンとKL17内蔵のUART ROMブートローダーを使ってKL17のマイクロコントローラをプログラムしようとしています。少なくとも紙の上では、pingと消去は完了しましたが、KL17へのデータ書き込みに苦戦しています。データシートの例(43ページ)には、これらのバイト(CRC16バイトとメモリ書き込みコマンドパケットを除くフレーミングパケット)について、次のように記載されています。 0x5A, 0xA4, 0x0C, 0x00, 0x04, 0x00 , 0x00, 0x02, 0x00, 0x04, 0x00, 0x20, 0x64, 0x00, 0x00, 0x00 CRC16バイトは0x06 0x5Aになります。しかし、27ページに記載されているCRC16アルゴリズムでは、私の環境では0x2b 0x56が出力されます。また、CRC16の計算方法のさまざまなバリエーションを含む様々なCRC16カリキュレータをオンラインで試しましたが、どれも出0x06 0x5Aはありませんでした。 Noay_0-1790003799652.png 私の推測では、計算に含めるべきバイトが欠けているのかもしれません(どのバイトかは分かりません。なぜなら、その後のデータパケットはすべてそれぞれCRC16バイトが割り当てられているからです)。あるいは誰かがデータシートを誤ったのかもしれません(これもまたKL17サブファミリ参照マニュアルにまさに同じ例なので可能性は低いです)。 Re: Rom Bootloader WriteMemory Command CRC16 calculation こんにちは、 @Noay さん。 投稿ありがとうございます。リファレンス・マニュアルの「0x06 0x5A」値は誤りで、おそらくドキュメントの問題だと思います。ご提供いただいた情報に基づくと、CRC計算結果の「0x2B 0x56」は正しいようです。 blhostツールを使ってブートローダーコマンドのデバッグは可能です。パラメータ「-d」を指定すると、ホストとターゲット間のすべての通信プロセスが提供されます。 KL27ボードでこの機能を試してみました。下のスクリーンショットをご覧ください。 KL17のEVBボードは入手できません。同じ方法をKL17デバイスで試してみて、どんな結果が得られるか試してみませんか? ドキュメントの誤りをお詫びします。この件を社内チームと共有し、それに応じて文書を更新するよう提案します。 BR セレステ
View full article
ティッククロックの設定および基準クロックの選択に関して こんにちは: ベアメタルティッククロック(S32K358デバイス)を設定したいと考えています。BaseNXPの設定を図1に示します。この設定でティッククロックに接続できますか?2. デバイスツリー内のどのクロックに「48MHz」が設定されていますか? sunshine88_0-1789971547489.png sunshine88_1-1789971658567.png 設定後、OsIf_Init(NULL_PTR); OsIfDelay(x); を使用して呼び出すことはできますか? どうもありがとうございます! Re: 关于滴答时钟建立及基时钟的选择 こんにちは、@sunshine88 さん。 OsIfSystemTimerClockFreqはCORE_CLKに対応し、私の場合は160MHzです: PavelL_0-1789999751219.png PavelL_1-1789999832315.png よろしくお願いいたします。 パベル
View full article
FreeMASTER Communication Driver 3.0 for i.MX、LPC、Kinetis、DSC 親愛なるみんな ダウンロードページで https://www.nxp.com/design/design-center/software/development-software/freemaster-run-time-debugging-tool:FREEMASTER パッケージが pberna67_1-1790030347425.png しかし、ダウンロードボタンをクリックしても、ダウンロード統計は表示されません。LPC1766をサポートする必要がありますが、バージョン3ではサポートされていないようです(ドライバが示されているのに不思議です)。それでもバージョンV2にはドライバが見当たりませんLPC1766 ありがとうございます パオロ Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC 親愛なるパオロ、 FreeMASTERドライバーを入手するために使ったリンクは正しいです。残念ながら、このドライバーはNXP MCUXpresso SDKでサポートされる新しいデバイスのみに対応しています。このLPC1766はSDKでサポートされていません。 LPC1766を使用する際には、以下の2つの選択肢があります。 - JTAG (Segger J-Link または LPCLink2/CMSIS-DAP) を介して FreeMASTER を使用する - これにより、変数を検査および制御できるようになります。通信ドライバは不要で、FreeMASTERはMCUが稼働中もメモリにアクセスします。 - ドライバーを別の部品に取り寄せて、LPC1766に移植する。詳細は下記をご覧ください。 SDK依存の理由は、FreeMASTERドライバーが通信ドライバーをSDKの低レベルドライバーの上に重ねているからです。サポートするMCUのいずれかを選択すると、SDKビルダーリンクからFreeMASTERのフル「ミドルウェア」ドライバーを入手できます。例えば(例:MCXN947)。ダウンロード後、FreeMASTERのコードはmiddleware/freemasterディレクトリにあります。 FreeMASTERパッケージ(src/drivers)には他にも、あなたにとって役立つ可能性のある他のドライバーも含まれます。mcuxsdkディレクトリにはSDKの低レベルに基づくプライマリドライバーが入っていますが、FreeMASTERのドライバーコードの構造を理解するためにも確認できます。「dreg」ディレクトリにはSDKに依存しないドライバーが含まれています。「デレッグ」ドライバは代わりにダイレクトレジスタアクセスを使っています。これは基本的に必要なものですが、残念ながらレガシーLPCはリストに含まれていません。NXP DSC、Kinetis、Power Architecture、S12Z、S32プラットフォーム向けのこのようなドライバーがあります。この概念をLPCに移植するのは非常に簡単な作業となるだろう。 よろしくお願いいたします。 ミハル Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC マイケル様 迅速なご返信ありがとうございます! 私はすでにJlink/MCU LinkとMCU Link2をドライバーなしで使って変数の読み書きに使っていますが、アプリケーションコマンドマネジメント(それ以上のものではありません)も追加したいと思っています。USB/UART/CAN などのサポートは必要ありません...インターフェースのサポートです。 「dreg」ディレクトリにはSDKに依存しないドライバーが含まれています。「デレッグ」ドライバは代わりにダイレクトレジスタアクセスを使っています。これは基本的に必要なものですが、残念ながらレガシーLPCはリストに含まれていません。」 これらの追加制限を踏まえて、dregディレクトリの内容だけで十分だと思いますか? V2バージョンのドライバーもLPC1766対応していると読みました。それは本当ですか?このドライバーを送ってもらえますか? ありがとう、パオロ。 Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC こんにちは、パオロさん。 いいえ、V2ドライバーはLPCをサポートしていません。HCS08、HCS12、ColdFire、PowerPCなどの一部のレガシーなプラットフォームをサポートしていますが、LPCはサポートしていません。 もし単にアプリケーションコマンドを有効にしたいだけなら、アプリケーションの制御方法を変える方がずっと簡単で一般的により良い解決策だと思います。アプリケーションコマンドは、FreeMASTERが制御リクエストパラメータを書き込む変数をいくつか選び、別の変数を「処理リクエスト」として使うことで簡単に置き換えられます。ターゲットアプリケーションがこのリクエスト変数セットを検出すると、制御コマンドを処理し、リクエスト変数をゼロに戻して確認できます。この動作は機能的にアプリケーションコマンドと同等であり、通信ドライバなしでJTAG上で動作することを可能にします。 もう一つの質問に答えると、「ドレッグ」ドライバは直接使えるものではありません。前述の通り、LPCはサポートされていませんが、自分で簡単にポートを作成できます。freemaster_kxx_uart.cのようなUARTファイルを見ると、原子的なUART操作を行うドライバ関数が見つかります。例えば、割り込みを有効にする場合: この単純な関数はUART周辺レジスタ上で直接動作していることがわかります。これをLPCに移植するには、LPC UARTモジュール(Kinetis Oneとは異なる)上で動作する類似の関数を作成する必要があります。 よろしくお願いいたします。 ミハル Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC 親愛なるマイケルへ、 あなたのために、Application Commandのサポートなしで直接JLink SWD接続を使うよう説得されました(つまり、ドライバーをLPC1766に移植する必要はありません)。しかし、最近気づいたのはTSAテーブルもサポートしなければならないということです。実は、自分の製品用にコンフィギュレーター(パラメータ読み書き)を作りたいのですが、その中のファームウェアがバージョンを変えてしまうことがあります。バージョン番号を知るためのディスプレイがないため、事前にどのファームウェアイメージバージョンが読み込まれているかを知ることはできず、正しいFreeMasterのAXFファイルを事前に読み込むことはできません。ホストプロセッサから変数のアドレスを読み取る必要があるので、残念ながらターゲットドライバーを:(に移植する必要があります。他にこの問題を回避する方法がない限り。 唯一の疑問は、あなたがこう書いていることです: 「この単純な関数がUARTペリフェラルレジスタに直接動作していることがわかります。これをLPCに移植するには、LPC UARTモジュール(Kinetisとは異なる)上で動作する類似の機能を作る必要があります。」 ペリフェラル通信ドライバ(UART、CAN、USB)を移植する必要はないはずです。なぜならSWDをサポートすれば十分だからです。それは正しいですか?このオプションだけの「パストレース」について、もう少し詳しく教えてもらえますか? パオロ Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC 親愛なるマイケルへ 私は Keil MCB1700 ボードを使って、lpcxpresso54114 SDK のfreemaster_examples/fmstr_example_pdbdmをLPC1768プラットフォームに移植しました。すべて順調に動作しています。NXPは非常に良い仕事をした。移植作業中にコードの変更は一切なく、非常に簡単な作業だった。 残念ながら、このフォーラムに.zipファイルとして添付することはできません。ファイル よろしくお願いいたします パオロ ありがとうございます。
View full article
S32DS v3.4が起動時にクラッシュし、アクティベーションIDを取得できず、オフラインライセンスファイルが必要です NXPサポートの皆様、 私のS32 Design Studio for S32 プラットフォーム v3.4ライセンスが期限切れまたは行方不明になっています。ソフトウェアを起動すると、「Product Licenses - NXP Licenses」ウィンドウが表示され、「Status: License Missing」と表示されます。どのボタン(Activate、Details、Close)でも即座にクラッシュし、ソフトウェア全体が閉じられます。 私が持っている情報は以下のとおりです。 登録メールアドレス: [[email protected]] ソフトウェアアクティベーションコード: DC1D-EDC9-8B34-496C(元のダウンロードメールより、アカウント名:pang yun) S32DS バージョン: v3.4 バックエンドでライセンスを延長してもらえますか? ご協力いただき、誠にありがとうございました。 Re: S32DS v3.4 crashes upon opening, cannot retrieve Activation ID, need offline license file こんにちは、 お客様のS32DSライセンスが延長されました。コードを使ってS32DSを再度有効化してください。
View full article
MR-VMU-RT1176 外部内存 在定制板上使用 MR-FMUM-RT1176 时,是否可以添加额外的外部存储器?由于并非所有 SEMC 引脚都可通过连接器使用,而且两个 FLEXSPI 都已被使用。 Re: MR-VMU-RT1176 External RAM 嗨@Zaregg , 感谢您对 NXP MIMXRT 系列产品的关注! 如果仅使用 MR-FMUM-RT1176 模块而自行设计载板,则无法添加外部存储器。如果您确实需要 同步动态随机存取存储器(SDRAM) 或 HyperRAM 等内存映射扩展,唯一的途径是自行设计芯片级扩展,以充分发挥 SEMC 或 FlexSPI 总线的性能。如果可以使用外置闪存/EEPROM,那么可行的方案如下: (1)重新分区模块上的八进制闪存 (2)通过 lpspi/lpi2c 在载板上添加串行设备。   此致, 加文
View full article
远程访问 FreeMASTER 各位 我希望通过连接到同一局域网中的另一台 PC,经由 Jlink 连接到目标设备 (LPC1766) 的 PC 来访问运行在 PC 上的 FreeMaster。即使通过浏览器(任意浏览器)连接到本地电脑,使用附件中的简单示例都能正常工作,但如果将所有文件(附件)移动到另一台电脑上,最后在远程浏览器中打开 Test.htm 文件,变量读取功能就无法正常工作。 请尊重 NXP 的原始示例,其中指示的是本地主机,现在地址已更改,它始终指向运行 FreeMASTER 的 PC。 pberna67_0-1790032198582.pngpberna67_0-1790032198582.png 有人知道这是什么原因造成的吗? 是否可以在远程PC上创建一个Windows应用程序窗体,使其能够(作为DCOM客户端?我不太清楚)连接到运行FreeMASTER(DCOM服务器?)的“本地”PC上的FreeMASTER,并且该FreeMASTER通过Jlink模拟器连接到目标? 1)本地PC的FreeMASTER配置是什么? 2) 如何通过 Visual Basic .NET 窗体应用程序从远程 PC(运行 FreeMASTER 的计算机)访问本地 PC? 之所以会问这些问题,是因为我的开发电脑上安装了微软 Visual Studio。.NET 运行所在的机器与 FreeMASTER 和目标板 (LPC1766) 所在的机器不在同一台机器上。 Re: Remote access to FreeMASTER 问题已解决 🙂 对不起 这是因为这两台电脑分别有两个不同的配置文件,一个是公共配置文件,一个是私有配置文件,所以 FreeMASTER 防火墙设置阻止了公共配置文件的所有端口。如果两台电脑上的个人资料都设置为私密,则通信会发生
View full article
imx95 ジェイルハウス iommu 設定 こんにちは、 Jailhouse上でi.MX95のIOMMUを設定することは可能ですか? 私はhttps://github.com/nxp-imx/imx-jailhouse/blob/lf-6.18.20_2.0.0/configs/arm64/imx8qm.cとhttps://github.com/nxp-imx/imx-jailhouse/blob/lf-6.18.20_2.0.0/configs/arm64/imx95.cを比較していますが、後者には.iommu_unitsがありません。定義済み。これは見落としでしょうか、それともi.MX95では不可能な機能なのでしょうか?私の理解では、i.MX95は新しいSMMUv3をサポートしており、ルートセルファイルには次のようなものがあると思います。 .iommu_units= { ヤージュ .type = JAILHOUSE_IOMMU_SMMUV3, .base = 0x36600000、 .size = 0x100000、 }、 } ありがとうございます。 Re: imx95 jailhouse iommu configuration AEチームと話し合った。 IOMMU は i.MX95 ではデフォルトで有効になっています。 Re: imx95 jailhouse iommu configuration IOMMU設定はシステムマネージャーの設定ファイルとカーネルDTSでデフォルトで有効化されています
View full article
FreeMASTERへのリモートアクセス 皆さん 同じローカルネットワークに接続された別のPCを経て、Jlink経由でターゲット(LPC1766)に接続したPC上でFreeMasterにアクセスしたいと思っています。添付の簡単な例を使用して、eブラウザ(任意のブラウザ)経由でローカルPCに接続した場合、接続自体は正しく機能するのですが、添付のすべてのファイルを別のPCに移動してから、リモートブラウザでTest.htmを開くと、変数の読み取りが機能しなくなります。 NXPの元の例ではlocal-hostが指定されていましたが、現在はアドレスが変更され、常にFreeMASTERが実行されるPCを指すようになっています。 pberna67_0-1790032198582.pngpberna67_0-1790032198582.png この問題の原因について何か心当たりはありますか? リモートPCでWindowsアプリフォームを作成し、(DCOMクライアントとして??,不明ですが)FreeMASTER(DCOM Server?)が動作する「ローカル」PCのFreeMASTERに接続し、Jlinkエミュレーターでターゲットに接続することは可能でしょうか?   1) ローカルPCのFreeMASTERの設定は? 2) Visual Basic .NET Form APPを使って(FreeMASTERが動いている)リモートPCからローカルPCにアクセスするにはどうすればいいですか? これらの質問の理由は、私の開発用PCにMicrosoft Visual Studioがインストールされているためです。.NET が実行されるマシンは、FreeMASTER とターゲットボード (LPC1766) が動作しているマシンとは異なります。 Re: Remote access to FreeMASTER 問題解決 🙂 すみません これは、2台のPCがパブリックとプライベートの2つの異なるプロファイルを持っているため、FreeMASTERファイアウォールの設定がパブリックプロファイルのすべてのポートをブロックしていることに関連しています。両方の PC のプロファイルがプライベートに設定されている場合、通信は
View full article