Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
S32 Design Studio for ARM v2.2のライセンスは期限切れです こんにちは、私のARM v2.2用のS32 Design Studio ライセンスが期限切れになりました。延長してもらえますか? 有効期限:2026年6月29日 製品:ARM v2.2用S32 Design Studio ライセンス:27ED-C7E9-C2B4-9D3E Re: license of S32 Design Studio for ARM v2.2 has expired こんにちは、 お客様のS32DSライセンスが延長されました。
View full article
HSE INSTALL S32K311 All the content below is copied from the attachment. S32DS version: S32DS.3.5_b220726_win32.x86_64 (1).exe RTD version: SW32K3_RTD_R21-11_3.0.0_P07_D2306_DS_updatesite.zip S32K311 Support Package Version: SW32K3_S32DS_3.5.6_D2309.zip SBAF version: SBAF_S32K311_0_0_15_0 Bin file: s32k311_Secure_Baf_0.12.0_0.15.0.6_pb230804.bin.pink HSE version: HSE_FW_S32K311_0_2_40_0 The bin file is s32k311_hse_fw_0.12.0_2.40.0_pb230730.bin.pink Use FULL_MEM No safe boot A problem currently encountered The program will get stuck here: `while ( FALSE == HSE_CheckStatus(HSE_STATUS_INIT_OK) );` 图片3.png   图片4.png 图片1.png 图片5.png   图片6.png   图片2.png     Re: HSE INSTALL S32K311 This is supplementary printf information. DCMROF21: 0x00040000 HSE GPR3: 0x000000C0 Current_SBAF_Version-0x4039c020: 0x00000C00 LC configuration word -0x4039C02C: 0x00000000 Lifecycle-related information - 0x402AC200: 0x00000000 HSE Status: 0x00000000 I've looked up information online, and it seems the SBAF that comes with the chip doesn't recognize the HSE firmware I'm currently using. Re: HSE INSTALL S32K311 I suspect that SBAF failed to copy the HSE firmware from the flash memory to the HSE_NVM. If this is the problem, how should I resolve it? Re: HSE INSTALL S32K311 This is the data I printed. DCMROF21: 0x00040000 HSE GPR3: 0x000000C0 HSE Status: 0x00000000 HSE firmware not started (NVM empty or firmware corrupted) 111.png Re: HSE INSTALL S32K311 Hi @iiiddd  Could you please share the value of HSE_CONFIG_GPR3 (0x4039C028)? Bit 0 indicates whether the HSE Firmware is present. BR, VaneB Re: HSE INSTALL S32K311 The RTD library I'm using is called when writing UTEST. gHsePort_FlsIf.writeApi(UTEST_BASE_ADDR,(uint8_t*)hseFwFeatureFlag,FW_FEATURE_FLAG_LEN); The FLS_MAX_VIRTUAL_SECTOR definition will be used. My RTD library defaults to 135, but accessing the address 0x1B000000UL requires 136. Is the RTD library I'm using incompatible with HSE? Re: HSE INSTALL S32K311 Hi @iiiddd  The HSE_CONFIG_GPR3[0] bit is not set, which indicates that the HSE hardware is not present on the device. For reference, the following image shows an example of a linker file configured for the installation of the HSE FW FULL_MEM on an S32K311 device: VaneB_0-1784568701705.png Re: HSE INSTALL S32K311 When I was debugging, I found that there were data in the pflash corresponding to the hse firmware. Do you mean that sbaf failed to copy the firmware in the pflash to the hsenvm? If this is the problem, what might have caused it?
View full article
关于 MIMX9121CVVXCAA 的 RTC_XTALI 信号处理 您好,我正在考虑使用 i.MX91 SoC MIMX9121CVVXCAA。 问题: RTC 的时钟使用 SoC 内部振荡器电路的时钟,无需外部振荡器。 我计划将 RTC_XTALI 和 RTC_XTALO 引脚断开。我是否应该将板上的 RTC_XTALI 引脚拉低?期待您的回复。 Re: MIMX9121CVVXCAAのRTC_XTALI信号処理について 推荐 如果需要 RTC 功能,请按照UG10147中的建议,使用外部 32.768 kHz 晶体(带适当的负载电容),或者为RTC_XTALI提供频率低于 50 kHz 且幅度不超过NVCC_BBSM_1P8 的外部时钟。 如果 RTC 未使用,只需将RTC_XTALI和RTC_XTALO断开连接 (NC) 即可。不要添加下拉电阻。此外,确保这些走线到电源和地线的绝缘电阻大于100 MΩ ,以避免因焊剂残留、湿气或与相邻走线耦合而引起的泄漏。 i.MX 91 没有独立运行的内部 32.768 kHz 振荡器。因此,如果不需要 RTC 功能,则RTC_XTALI和RTC_XTALO应保持NC 状态,并且不应添加下拉电阻。这是因为数据手册规定,这些引脚到电源或地的漏电路径应大于100 MΩ 。 推奨事项 RTC机能が必要な场合は、 UG10147の推奨に従い、32.768kHz水晶発振子(负担负担を含む)を接続するか、 RTC_XTALIに周波数50 kHz未満、振幅がNVCC_BBSM_1P8を超えない外部クロックを入力してください。 RTC机能を使用しない场合は、 RTC_XTALIとRTC_XTALOの両方をNC (未接続)のままとしてください。プルダウン抵抗は追加しないでください。また、furakkusu残渣、湿気、または邻接配线によるリーク电流を防ぐため、これらの配线と电源/GND间の绝縁抗が100 MΩ以上となるようにしてください。 i.MX 91 には、単独で动作する内蔵32.768 kHz発振器はありません。したがって、RTC机能を使用しない场合は、 RTC_XTALIおよびRTC_XTALOをNC (未接続)のままとし、プルダウン抵抗を追加しないでください。データshitoでは、これらのピンから电源またはGNDへのリーク経路は100 MΩ以上であることが要求されています。
View full article
Local Access Windows (LAWs), memory overlap About LAW understanding : about the B4860 , just e.g B4860QDS; Local Access Windows (LAWs): in the B4860_QDS_Init.tcl file have set the Local Access Window Registers (as below have defined the phy address 0x000000, size 2Gbytes target to DDR) and in the  dpaa_demo.c of CW_SC_3900FP_v10.8.3\SC\StarCore_Support\SmartDSP\demos add the LAW setting the phy address 0x20000000 target  to  QMAN my query or confusing is  the LAW 10 setting (0x0000000~0x7fffffff target to DDR)   memory overlapped with  QMAN software port  LAW setting the phy address 0x20000000 target  to  QMAN. memory overlapped  between LAW , is it ok? and can explain detail why it can work ? there is not descript memory overlapped situation of LAW  in the reference manual of B4860.  ## LAW10 to DDRC2  # LAWBARH  mem [CCSR_ADDR 0x000CA0] = 0x00000000  # LAWBARL  mem [CCSR_ADDR 0x000CA4] = 0x00000000  # LAWAR  mem [CCSR_ADDR 0x000CA8] = 0x8110001E Re: Local Access Windows (LAWs), memory overlap It’s interesting how local administrative systems handle data integration, especially when managing complex files like local access windows and memory overlap. Navigating these technicalities can sometimes feel as complicated as dealing with a newsportnewscourt.org schedule. Having a reliable, centralized resource to clear up the confusion makes a huge difference. Hopefully, more updates will roll out soon to make these processes much smoother for everyone involved. Re: Local Access Windows (LAWs), memory overlap Thanks for sharing the [RTD200P04 MCAL] S32M244 PWM PDB ADC MCAL demo—really helpful for developers working with embedded systems. For those handling compliance or security logging alongside hardware interfaces, reviewing Missouri offense records could offer useful insights for managing real-world data inputs. Always good to bridge technical applications with broader contextual awareness. Re: Local Access Windows (LAWs), memory overlap Please refer to the B4860 QorIQ Qonverge Multicore Baseband Processor Reference Manual, 2.3.1 Precedence of Local Access Windows.
View full article
S32 Design Studio for ARM v2.2 的许可证已过期。 您好,我的 S32 Design Studio for ARM v2.2 许可证已过期。你能帮我延长一下吗? 有效期至:2026年6月29日 产品:S32 Design Studio for ARM v2.2 许可证:27ED-C7E9-C2B4-9D3E Re: license of S32 Design Studio for ARM v2.2 has expired 你好, 您的S32DS许可证已延期。
View full article
ローカルアクセスウィンドウ(LAW)、メモリの重複 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> LAWの理解について:B4860について、例えばB4860QDSなど。 ローカルアクセスウィンドウ(LAW): B4860_QDS_Init.tclファイル内でローカルアクセスウィンドウレジスタを設定しています(以下のように、phyアドレス0x000000、サイズ2GbytesのターゲットをDDRに定義しています) CW_SC_3900FP_v10.8.3\SC\StarCore_Support\SmartDSP\demos の dpaa_demo.c 内 LAW設定をQMANに物理アドレス0x20000000ターゲットとして追加します。 私の疑問や混乱は、LAW 10の設定(0x0000000~0x7fffffff ターゲットをDDRに)メモリがQMANソフトウェアのポートLAWと重なっていて、ターゲット0x20000000のPHYアドレスをQMANに設定したことです。 記憶がLAWで重なっているのですが、大丈夫ですか?そして、なぜそれが機能するのか詳細を説明できますか?B4860の**リファレンス・マニュアル**には、LAWのメモリ重複状況の記述はありません。 ## LAW10からDDRC2へ # ローバー mem [CCSR_ADDR 0x000CA0] = 0x00000000 # LAWBARL mem [CCSR_ADDR 0x000CA4] = 0x00000000 # 戦争 mem [CCSR_ADDR 0x000CA8] = 0x8110001E Re: Local Access Windows (LAWs), memory overlap ローカル管理システムがデータ統合をどのように扱うかは興味深いです。特にローカルアクセスウィンドウやメモリの重複のような複雑なファイルを管理する際には。こうした細かい問題を乗り越えることは、時に、newsportnewscourt.org を扱うのと同じくらい複雑に感じることがありますスケジュール。混乱を解消するための信頼できる一元化された情報源があることは、非常に大きな違いを生む。関係者全員にとってこれらのプロセスがよりスムーズになるよう、近いうちにさらなるアップデートが実施されることを期待します。 Re: Local Access Windows (LAWs), memory overlap [RTD200P04 MCAL] S32M244 PWM PDB ADC MCALのデモを共有していただきありがとうございます。組み込みシステムを開発している開発者にとって非常に役立ちます。コンプライアンスやセキュリティログをハードウェアインターフェースと併用する方にとって、 ミズーリ州のオフェンス記録 を確認することは、実際のデータ入力を管理するための有用な洞察を提供するかもしれません。技術的なアプリケーションとより広い文脈認識をつなぐのはいつも良いことです。 Re: Local Access Windows (LAWs), memory overlap <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> B4860 QorIQ Qonverge マルチコアベースバンドプロセッサリファレンスマニュアル2.3.1「ローカルアクセスウィンドウの優先順位」をご参照ください。
View full article
NXPはMC33XS2410のプロトタイピング用にシンプルなTSSOP28ブレークアウト/アダプタボードを提供していますか? こんにちは、皆さん 現在、12Vの自動車プロジェクトのためのプロトタイピングとテストベンチを設置中です。NXP社の推奨に従い、保護回路にはMC33XS2410(eFuse)を選定しました。 しかし、私たちは組み立て工房で、現時点ではカスタムPCBの**デザイン**や製造ができないため、0.65mmのピッチとサーマルパッドを持つHTSSOP28**パッケージ**の扱いは手配線にとって物理的に難しいです。 フル機能のFRDM-XS2410EVB評価ボードは認識していますが、この特定のテストベンチでの即時のニーズには複雑すぎ、規模も高すぎます。ピンにアクセスするための最小限の方法だけで十分です。 Aries ElectronicsのLCQT-TSSOP28ブレイクアウトボードのような汎用サードパーティアダプターを購入する前に、NXPコミュニティにお聞きしたいと思います。 NXPは、MC33XS2410のHTSSOP28パッケージを標準の2.54mm DIPピンに変換するための、低コストで最小限のブレイクアウトボードやプロトタイピングアダプターを提供していますか? そうでない場合、NXPは、このチップとの互換性が実証されている特定のサードパーティ製アダプタまたはソケットのブランドを公式に推奨していますか(露出した中央パッドの接地および放熱要件を考慮して)? お時間とご協力、本当にありがとうございました! 評価ボード StarCore DSP Re: Does NXP offer a simple TSSOP28 breakout/adapter board for MC33XS2410 prototyping トーマスさん、説明と注意点を教えていただきありがとうございます。私のカードに関しては、それが解決策だと思います。 Re: Does NXP offer a simple TSSOP28 breakout/adapter board for MC33XS2410 prototyping こんにちは、モハメドさん。 現在、MC33XS2410 HTSSOP28パッケージを標準の2.54 mm DIPスタイルのフットプリントに直接変換する専用の低コストブレイクアウトボードやアダプターボードは提供していません。ご指摘の通り、私たちはFRDM-XS2410EVBを提供しており、これは単純なパッケージ適応ではなく、完全な機能評価を目的としています。 重要な考慮点の一つは、MC33XS2410パッケージの露出したサーマルパッドであり、熱性能と電気性能の両方を考慮してGNDにはんだ付けされるべきです。また、露出パッドをグラウンドプレーンに接続し、生産設計では熱放散を改善するために熱ビアを使用することも推奨しています。 また、汎用ブレークアウトボードは、一般的に機能プロトタイプの作成や低消費電力のベンチテストに適している点にご注意ください。しかし、適切に設計されたPCBで得られる熱性能を通常は提供できず、テスト可能な最大連続電流を制限する可能性があります。 もし用途がデバイスの電流制限付近で動作する必要がある場合は、熱性能を慎重に評価するか、公式の評価ボードを使うことをお勧めします。 BRs、トーマス
View full article
S32K312 EVB - SD Card SPI Initialization using LPSPI Hardware PCS0 Hi, I am implementing an SD Card driver over SPI on the S32K312 EVB using RTD 6.0.0 (Non-AUTOSAR Lpspi_ Ip driver). According to the SD Physical Layer Simplified Specification, the SPI initialization sequence is: Keep CS HIGH after power-up. Generate at least 74 clock pulses (I am sending 80 clocks by transmitting 10 bytes of 0xFF). Pull CS LOW. Send CMD0 (0x40 00 00 00 00 95). Keep CS LOW while polling with 0xFF until the card responds with **R1 = 0x01`. My issue is with hardware-controlled PCS0. When using the Lpspi_Ip driver with hardware PCS0, the PCS signal is automatically asserted/deasserted by the LPSPI peripheral during SPI transfers. Because of this, I cannot generate the initial 80 clock pulses while keeping CS HIGH and then CMD0 with CS LOW, as required by the SD specification. I have the following questions: Does the S32K312 LPSPI peripheral support keeping PCS inactive (HIGH) while generating SPI clocks? Is there any Lpspi_Ip API, register configuration, or recommended method to manually control PCS or temporarily disable hardware PCS during the SD card initialization sequence? If not, is the recommended approach to configure the SD card CS pin as a GPIO and manually control it while using LPSPI only for SCK, MOSI, and MISO? Additionally, if NXP has any reference implementation, application note, example project, or SDK/RTD example demonstrating SD card communication over SPI on the S32K3 series, could you please share the reference? Thank you. Re: S32K312 EVB - SD Card SPI Initialization using LPSPI Hardware PCS0 Hi @parvathitp  The PCS (Peripheral Chip Select) signal is designed to be controlled by the LPSPI module. When a hardware PCS is selected, it is automatically asserted and deasserted by the LPSPI peripheral during SPI frame transfers. There is no dedicated API available to manually control a hardware PCS signal while it is assigned to the LPSPI module. Therefore, as you mentioned, the best approach for this case is to configure the CS pin as a GPIO. In this configuration, the CS signal is controlled through the SIUL2/GPIO APIs, and you are responsible for controlling it.  Currently, there is no S32K3-specific application note, example project, or reference document that demonstrates this exact implementation. BR, VaneB
View full article
NXP是否提供用于MC33XS2410原型设计的简易TSSOP28分线/适配器板? 大家好, 我们目前正在为一个 12V 汽车项目搭建原型和测试平台。根据 NXP 的建议,我们为保护电路选择了 MC33XS2410(电子熔断器)。 然而,由于我们身处组装车间,目前无法设计或制造定制PCB,因此对于手工布线而言,处理HTSSOP28封装(间距为0.65mm,带有散热焊盘)在物理上具有挑战性。 虽然我们知道功能齐全的 FRDM-XS2410EVB 评估板,但它对于我们目前在这个特定测试台上的需求来说太复杂、太大、太贵了。我们只需要一种最简便的方法来访问引脚。 在购买通用第三方适配器(例如 Aries Electronics 的 LCQT-TSSOP28 分线板)之前,我们想先咨询一下 NXP 社区: NXP 是否提供低成本、极简的转接板或原型适配器,专门用于将 MC33XS2410 的 HTSSOP28 封装转换为标准的 2.54mm DIP 引脚? 如果没有,NXP 是否正式推荐任何经过验证可与该芯片良好配合使用的第三方适配器或插座品牌(考虑到裸露中心焊盘的接地和散热要求)? 非常感谢您抽出时间提供帮助! 评估板 StarCore DSP Re: Does NXP offer a simple TSSOP28 breakout/adapter board for MC33XS2410 prototyping 感谢托马斯的解释和注意事项,我想这就是我该如何处理我的卡片的方法。 Re: Does NXP offer a simple TSSOP28 breakout/adapter board for MC33XS2410 prototyping 你好,穆罕默德, 目前我们没有提供专用的低成本转接板或适配器板,可以将 MC33XS2410 HTSSOP28 封装直接转换为标准的 2.54 毫米 DIP 封装。您说得对,我们提供的 FRDM-XS2410EVB 是用于全面功能评估,而不是简单的代码包,软件包适配。 一个重要的考虑因素是 MC33XS2410 封装的裸露散热焊盘,为了保证散热和电气性能,应该将其焊接至 GND。我们还建议将裸露的焊盘连接到接地平面,并且在生产设计中,使用导热过孔来改善散热。 另请注意,通用分线板通常适用于功能原型设计和低功耗台式测试。然而,它们通常无法提供设计合理的 PCB 所能达到的热性能,这可能会限制可以测试的最大连续电流。 如果您的应用需要接近设备的限流运行,我建议您仔细评估其散热性能,或者使用官方评估板。 BRs,托马斯
View full article
license of S32 Design Studio for ARM v2.2 has expired Hi, my license of S32 Design Studio for ARM v2.2 has expired. Could you please extend it for me? Expiration Date: Jun 29, 2026 Product: S32 Design Studio for ARM v2.2 license:27ED-C7E9-C2B4-9D3E Re: license of S32 Design Studio for ARM v2.2 has expired Hi,  your S32DS license has been extended. 
View full article
本地访问窗口(LAW),内存重叠 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 关于 LAW 理解:关于 B4860,例如 B4860QDS; 本地访问窗口(LAW): 在 B4860_QDS_Init.tcl 文件中设置了本地访问窗口寄存器(如下所示,定义了物理地址 0x000000,大小 2Gbytes,目标为 DDR)。 在 CW_SC_3900FP_v10.8.3\SC\StarCore_Support\SmartDSP\demos 目录下的 dpaa_demo.c 文件中 将 LAW 设置 phy 地址 0x20000000 添加到 QMAN 我的疑问或困惑是,LAW 10 设置(目标地址为 0x0000000~0x7fffffff 的 DDR 内存)与 QMAN 软件端口 LAW 设置(目标地址为 0x20000000 的 QMAN 内存)重叠。 LAW 内存重叠,这样可以吗?能否详细解释一下为什么可以运行?B4860 参考手册中没有描述 LAW 内存重叠的情况。 ## LAW10 至 DDRC2 # LAWBARH mem [CCSR_ADDR 0x000CA0] = 0x00000000 # 律师协会 内存 [CCSR_ADDR 0x000CA4] = 0x00000000 # LAWAR 内存 [CCSR_ADDR 0x000CA8] = 0x8110001E Re: Local Access Windows (LAWs), memory overlap 本地管理系统如何处理数据集成是一件很有趣的事情,尤其是在管理本地访问窗口和内存重叠等复杂文件时。处理这些技术细节有时会感觉像处理newsportnewscourt.org一样复杂。日程。拥有一个可靠的、集中的资源来消除困惑,会产生巨大的影响。希望后续会有更多更新推出,使这些流程对所有相关人员来说都更加顺畅。 Re: Local Access Windows (LAWs), memory overlap 感谢分享 [RTD200P04 MCAL] S32M244 PWM PDB ADC MCAL 演示——这对从事嵌入式系统开发的开发人员来说真的很有帮助。对于那些负责处理合规性或网络安全日志记录以及硬件接口的人员来说,审查密苏里州的犯罪记录可以为管理现实世界的数据输入提供有用的见解。将技术应用与更广泛的背景知识联系起来总是有益的。 Re: Local Access Windows (LAWs), memory overlap <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 请参阅 B4860 QorIQ Qonverge 多核基带处理器参考手册,2.3.1 本地访问窗口的优先级。
View full article
MIMX9121CVVXCAAのRTC_XTALI信号処理について こんにちは、i.MX91 SOC MIMX9121CVVXCAA使用を検討しています。 質問内容: RTC用のクロックはSOC内部の発振回路のクロックを使用することで、外部発振子を未実装にして RTC_XTALIとRTC_XTALOピンは何も接続しないように考えています。RTC_XTALIのピンは基板側でプルダウンしたほうがいいのでしょうか。回答をお待ちしております。 Re: MIMX9121CVVXCAAのRTC_XTALI信号処理について 推奨事項 RTC機能が必要な場合は、 UG10147の推奨事項に従って、外部32.768kHz水晶発振器(適切な負荷コンデンサ付き)を使用するか、または、周波数が50kHz未満で振幅がNVCC_BBSM_1P8を超えない外部クロックをRTC_XTALIに供給してください。 RTCが使われていない場合は、単にそのまま RTC_XTALI と接続されていない(NC) RTC_XTALO してください。プルダウン抵抗器は追加しないでください。さらに、フラックス残留物、湿気、または隣接する配線との結合による漏洩を防ぐため、これらの配線から電源および接地までの絶縁抵抗が100 MΩ以上であることを確認してください。 i.MX 91には、独立して動作する内部32.768kHz発振器は搭載されていません。したがって、RTC機能が不要であれば、 RTC_XTALI と RTC_XTALO は NCのままにし、プルダウン抵抗を追加すべきではありません。これは、データシートに、これらのピンから電源またはグランドへのリーク経路が100 MΩ以上である必要があると規定されているためです。 推奨事項 RTC機能が必要な場合は、 UG10147の推奨、32.768 kHzの水晶発振子(負荷容量を含む)を接続するか、 RTC_XTALIに周波数50 kHz未満、振幅がNVCC_BBSM_1P8を超えない外部クロックを入力してください。 RTC機能を使用しない場合は、RTC_XTALI と RTC_XTALO の両方を NC(未接続) のままとしてください。プルダウン抵抗は追加しないでください。また、 フラックス残渣、湿気、または隣接配線によるリーク電流を防ぐため、これらの配線と電源/GND間の絶縁抵抗が 100 MΩ以上 となるようにしてください。 i.MX 91 には、単独で動作する内蔵32.768 kHz発振器はありません。したがって、 RTC機能を使用しない場合は、RTC_XTALI および RTC_XTALO を NC(未接続) のままとし、プルダウン抵抗を追加しないでください。データシートでは、これらのピンから電源またはGNDへのリーク経路は 100 MΩ以上 であることが要求されています。
View full article
AAOS 15 User Switch Crash on i.MX8QM Multi-Display Setup Hello Team, We are running Android Automotive OS 15 (AAOS 15) on the i.MX8QuadMax board with a multi-display setup (Main Display + Passenger Display). We are observing an issue with the default Car Launcher during user switching: System boots normally and the launcher is displayed on both main and passenger displays. When switching from the current user to a new user or guest user, both the main display and passenger display crash and become unusable. The issue is consistently reproducible after user switching. We would like to know: Is there any known issue related to user switching in AAOS 15 on i.MX8QM multi-display systems? Are there any additional configurations required for passenger display handling during user switch? What logs or debug information should we collect to further analyze this issue? Any suggestions or guidance would be appreciated. Thanks. Re: AAOS 15 User Switch Crash on i.MX8QM Multi-Display Setup Hi @AldoG, Thanks for the clarification.   We are using the NXP i.MX8QM MEK board with NXP BSP. Since this issue is related to Android Automotive, could you please let us know the correct support channel or forum where we should raise our AAOS-related questions? Thank you. Re: AAOS 15 User Switch Crash on i.MX8QM Multi-Display Setup Hello, Are you using NXP MEK board? If yes, you are using NXP BSP? Please note that we do not support Android Automotive we can provide asistance if issues are found on our BSP release. Best regards/Saludos, Aldo. Re: AAOS 15 User Switch Crash on i.MX8QM Multi-Display Setup Hi @AldoG, Thank you for the response. I have attached the full logcat,the reproduction steps.and changes we made to bring multi displays. Reproduction Steps: Boot AAOS 15 on i.MX8QM with center and passenger displays enabled. Open User Settings on the passenger display. Create or switch to a new user/guest user on the passenger display. During the user switch, com.android.car.carlauncher crashes with:   android.view.WindowManager$InvalidDisplayException: Unable to add window -- the specified display can not be found From the log, it appears that CarLauncher is trying to resume on a display that is no longer available or has an invalid display mapping after the user switch. Could you please advise: Whether this is a known issue in AAOS 15 multi-user/multi-display scenarios on i.MX8QM? Which component is responsible for assigning the display during user switching (OccupantZone, CarUserService, TaskDisplayArea, or WindowManager)? Are there any known requirements or patches related to MUMD (Multi-User Multi-Display) support for launcher launching on secondary displays? Is there any recommended debug information we should collect to identify why the display becomes invalid after the user switch?
View full article
AAOS 15 用户切换在 i.MX8QM 多显示器设置中崩溃 各位团队成员,大家好! 我们在 i.MX8QuadMax 板 上 运行 Android Automotive OS 15(AAOS 15), 采用多显示器设置( 主 显示器 + 乘客 显示器) 。 我们发现 用户 切换过程 中 默认 的 汽车 启动 器 存在 问题 : 系统 正常 启动 , 主 显示屏 和 乘客 显示屏 上 均 显示 启动 器 。 当 从 当前 用户 切换 到 新 用户 或 访客 用户 时 , 主 显示屏 和 乘客 显示屏 都会 崩溃 并 变得 无法 使用 。 用户 切换 后, 该 问题 始终 可以 重现 。 我们 想 知道 : 在 i.MX8QM 多 显示器 系统 中 , AAOS 15 是否 存在 与 用户切换 相关 的 已知 问题 ? 用户 切换 期间, 乘客 显示屏 的 处理 是否 需要 任何 额外 的 配置 ? 我们 应该 收集 哪些 日志 或 调试 信息 来 进一步 分析 此 问题? 任何建议或指导都将不胜感激。 谢谢。 Re: AAOS 15 User Switch Crash on i.MX8QM Multi-Display Setup 嗨@AldoG , 谢谢你的解释。   我们 正在 使用 NXP i.MX8QM MEK 板 和 NXP 电路板支持包 。由于 此 问题 与 Android Automotive 相关 , 请问 我们 应该 通过 哪个 支持 渠道 或 论坛 提出 与 AAOS 相关 的 问题 ? 谢谢。 Re: AAOS 15 User Switch Crash on i.MX8QM Multi-Display Setup 你好, 你使用的是NXP MEK开发板吗? 如果是,您使用的是NXP 电路板支持包。吗? 请注意,我们不提供 Android Automotive 的支持,但如果我们的 电路板支持包。 版本出现问题,我们可以提供帮助。 此致敬礼/Saludos, 阿尔多。 Re: AAOS 15 User Switch Crash on i.MX8QM Multi-Display Setup 嗨@AldoG , 谢谢你的回复。我 已 附上 完整的 logcat 日志 、 重现 步骤 以及 我们为实现多显示器功能所做的更改。 重现步骤: 在 i.MX8QM 上 启动 AAOS 15 ,并 启用 中央 和 乘客 显示屏 。 打开 乘客 显示屏 上的 用户 设置 。 在 乘客 显示屏 上 创建 或 切换 到 新 用户 /访客 用户 。 用户 切换 期间 , com.android.car.carlauncher 崩溃 并显示以下错误信息:   android.view.WindowManager$InvalidDisplayException: 无法添加窗口——找不到指定的显示器。 从日志 来看 ,用户 切换 后, CarLauncher 似乎正在尝试在 不再 可用 的 显示器 或 显示 映射 无效 的 显示器上恢复运行 。 请问 您 能否 提供以下建议: 在 i.MX8QM 上, AAOS 15 多 用户/多 显示器 场景 中 是否 存在 已知 问题 ? 在用户切换期间,哪个 元器件 负责 分配 显示 内容 (OccupantZone、 CarUserService、 TaskDisplayArea 或 WindowManager)? 对于 在 辅助 显示器 上 启动 启动器 , 是否 存在 与 MUMD (多用户 多显示器) 支持 相关的 已知 要求 或 补丁 ? 是否 有 任何 建议 的 调试 信息 需要 收集 , 以 确定 用户 切换 后 显示 失效 的 原因 ?
View full article
S32K312 EVB - 使用 LPSPI 硬件 PCS0 进行 SD 卡 SPI 初始化 您好, 我正在使用 RTD 6.0.0(非 AUTOSAR Lpspi_ Ip 驱动程序)在 S32K312 EVB 上通过 SPI 实现 SD 卡驱动程序。 根据SD物理层简化规范,SPI初始化序列为: 启动后保持 CS 值高。 生成至少 74 个时钟脉冲(我通过发送 10 字节的 0xFF 来发送 80 个时钟)。 拉低 CS。 发送 CMD0 (0x40 00 00 00 00 95)。 在轮询 0xFF 时保持 CS 低,直到卡响应 **R1 = 0x01`。 我的问题出在硬件控制的PCS0上。 当使用 Lpspi_Ip 驱动程序和硬件 PCS0 时,在 SPI 传输期间,LPSPI 外设会自动钳位/置低 PCS 信号。因此,我无法按照 SD 规范的要求,在保持 CS 高电平的同时生成初始 80 个时钟脉冲,然后在保持 CS 低电平的同时生成 CMD0。 我有以下几个问题: S32K312 LPSPI 外设是否支持在生成 SPI 时钟时保持 PCS 非活动(高电平)? 在 SD 卡初始化序列期间,是否有任何 Lpspi_Ip API、寄存器配置或推荐的方法来手动控制 PCS 或暂时禁用硬件 PCS? 如果不是,推荐的方法是否是将 SD 卡 CS 引脚配置为 GPIO 并手动控制它,而仅使用 LPSPI 控制 SCK、MOSI 和 MISO? 此外,如果 NXP 有任何参考实现、应用笔记、示例项目或 SDK/RTD 示例演示 S32K3 系列通过 SPI 进行 SD 卡通信,能否请您分享一下参考资料? 谢谢! Re: S32K312 EVB - SD Card SPI Initialization using LPSPI Hardware PCS0 嗨@parvathitp PCS(外设片选)信号设计为由 LPSPI 模块控制。当选择硬件 PCS 时,LPSPI 外设会在 SPI 帧传输期间自动对其进行钳位和取消置位。 当硬件 PCS 信号分配给 LPSPI 模块时,没有专用的 API 可用于手动控制该信号。因此,正如您所提到的,这种情况的最佳方法是将 CS 引脚配置为 GPIO。 在此配置中,CS 信号通过 SIUL2/GPIO API 进行控制,您负责控制它。 目前还没有专门针对 S32K3 的应用说明、示例项目或参考文档来演示这种确切的实现方式。 BR,VaneB
View full article
S32K 比较器公差/偏移 我们正在对S32K116比较器进行一些测试: 我们向 INN(或 INP)施加输入电压(238mV),以带隙为参考,然后我们将 VOSEL 从 0 增加到 255,并监测比较器输出何时发生变化。 不知何故,当输入电压和带隙的连接互换时,我们在 MCU2 上观察到了不同的容差/偏移。(详情请参见测试1和测试2) 1)这是像VAIO那样已知的某种功能,还是其他什么功能? 2)对于这种公差/偏差,它是否稳定,我们可以通过校准消除它吗? (例如,记录目标电压下的触发信号) 测试1:输入电压接V-,带隙接V+ ,低速模式 Sid_Zhou_5-1784193940847.png 测试2:输入电压接V+,带隙接V- ,低速模式 Sid_Zhou_6-1784193974436.png Re: S32K comparator tolerance/offset 1)输入引脚 CMP0_IN 始终设置为通道 0。(PIN26,PTA0) 是的,输入电压仍然通过相同的 CMP0_IN 引脚 26、PTA0 输入。 2)带隙 我想弄清楚的特性并不是两个MCU之间的区别。当 INN 和 INP 互换时,同一个 MCU 的容差/偏移量就会不同。我认为在这种交换过程中带隙不应该发生变化。(此处MCU1的数据仅供参考) 3) VDD/VDDA: 这两个MCU使用相同的+3.3V网络(LDO容差在1.25%以内)。 我完全理解MCU的带隙会有所不同,但是,我再次强调,我检查的是交换后的带隙差异。 4)测试方法 上述测试数据并非增加输入电压,而是使用固定输入电压,并增加 VOSEL 值。(关于降低 VOSEL 值,我尚未测试,稍后会进行检查。) 对于固定 VOSEL 的增加/减少输入电压的情况,有类似的 -9mV。 IncreaseInput_FixedVOSEL.PNG 5)滞后现象 我确实有低速模式下磁滞现象的测试数据: 此处的测试数据是固定输入电压并增加 VOSEL: Hysteresis_LowSpeedMode.PNG 6)MCU照片 您可以参考附件照片“MCU1.PNG”和“MCU2.PNG”。 阻焊层是 FS32K11-6LFMMF-ON96V-S12YM16 Re: S32K comparator tolerance/offset 你好 Sid_Zhou, 您将输入电压连接到了哪个 CMP0_IN 引脚? 当交换 INN 和 INP 时,输入电压是否仍然通过同一个 CMP0_IN 引脚输入? 此外,带隙电压范围在 0.97-1.03V 之间。您是否考虑过暂时排除两个 MCU 的带隙电压不同所导致的问题?例如,能否使用不同的 CMP0_IN 引脚来输入更精确的外部电压基准? 你检查过两个 S32K1 的 VDD/VDDA 电压是否相同吗? 调试过程中是否确认 OFFSET=1 和 HYSTCTR=0? 我注意到您提高了输入电压并记录了 VOSEL。你试过降低输入电压并记录VOSEL值吗?另外,检查一下模拟比较器的迟滞是否受到影响,虽然我看到你已将 HYSTCTR 配置为 0。 拍摄两张 S32K116 照片,并告诉我 MCU 掩模。 此致敬礼, Robin Re: S32K comparator tolerance/offset 感谢您的详细解释。我现在明白您关心的是 S32K1 数据手册中的VAIO (模拟输入偏移电压)参数。 我在内部看到了AE团队的解释: AIO偏移量是比较器本身的偏移量,即INP和INN之间的偏移量。 由于 INL 误差是对 DNL 的积分,因此 INL 误差包含了 DNL 误差。 错误为 |V_AIO| + |INL| 根据我的理解,直接使用来自外部信号源的两个模拟电压分别输入INP和INN来测试VAIO应该比使用带隙分压器更直观。 关于您的问题:对于同一个 MCU,VAIO 不是一个随机值,不会随意地随时间变化,而是会随着工作条件(尤其是温度)而漂移。数据表中的 VAIO 值应理解为整个温度范围内的保证/最坏情况极限。 在设计阈值时,不要将 VAIO 视为可忽略不计或固定的校准值。保持裕量基于全温最坏情况 |VAIO|,加上 DAC/INL 误差。 我还查看了您之前关于此问题的讨论: S32K116 比较器容差。 看来CMP的精度无法满足您的需求。您是否考虑过 S32K1XXRM Rev14.2 的“ 44.5.5 自动比较功能”部分中描述的功能? S32K1 数据手册 Rev15 中的“ 表 41. 12 位 ADC 特性 (2.7 V 至 3 V) ”显示最大 TUE 为 ±8 LSB。这似乎比CMP更准确。 Re: S32K comparator tolerance/offset 感谢您的详细解释。 我注意到,在我们的应用中,ADC 可能具有更高的精度。 但是,从高层架构来看,我们有使用 CMP 作为功能安全监视器的要求,我不确定是否可以将其更改为 ADC。
View full article
S32K comparator tolerance/offset we are having some test on the comparator of S32K116: we apply an input voltage(238mV) to INN (or INP), use bandgap as reference, then we increase VOSEL from 0 to 255 and monitor when the comparator output changed. Somehow, we see different tolerance/offset on MCU2 when the connection of input voltage and bandgap is swapped.  (Details shown in Test1 and Test2) 1) Is this some kind of known feature like VAIO or something else? 2) For this tolerance/offset, is it stable and can we eliminate this by calibration? (like record the trigger VOSEL at the target voltage) Test1: Input Voltage on V-, Bandgap on V+, Low Speed Mode Sid_Zhou_5-1784193940847.png Test2: Input Voltage on V+, Bandgap on V-, Low Speed Mode Sid_Zhou_6-1784193974436.png Re: S32K comparator tolerance/offset 1) Input Pin CMP0_IN is always set to channel 0. (PIN26, PTA0) Yes, input voltage still being input through the same CMP0_IN Pin26, PTA0. 2) Bandgap The feature I want to figure out is not the difference between two MCU.  It is this different tolerance/offset from the same MCU when INN and INP is swapped. I think the bandgap should not change during this swapped.  (The data of MCU1 here is just use as reference) 3) VDD/VDDA: The two MCU are using same +3.3V network (LDO within 1.25% tolerance).  I am fully understanding there will be difference between MCUs bandgap, but, again, it is the difference during swapped I am checking. 4) test method The test data above is not increasing input voltage, it is using fixed input voltage, and increasing VOSEL. (For decreasing VOSEL, i have not test yet, will check this later.) As for increasing/decreasing input voltage with fixed VOSEL, there is similar -9mV.  IncreaseInput_FixedVOSEL.PNG  5) Hysteresis I do have test data for hysteresis in low-speed mode: Test data here is fixing input voltage and increase VOSEL:  Hysteresis_LowSpeedMode.PNG  6) MCU photos you can refer to attached photo "MCU1.PNG" and "MCU2.PNG" Solder mask is  FS32K11-6LFMFM-ON96V-S12YM16 Re: S32K comparator tolerance/offset Hi Sid_Zhou, Which CMP0_IN pin are you connecting the input voltage to? When swapping INN and INP, is the input voltage still being input through the same CMP0_IN pin? Also, the BandGap voltage range is between 0.97-1.03V. Have you considered temporarily ruling out issues caused by different BandGap voltages on the two MCUs? For example, could you use a different CMP0_IN pin to input a more accurate external voltage reference? Have you checked whether the VDD/VDDA voltages of the two S32K1s are the same? Were OFFSET=1 and HYSTCTR=0 confirmed during debugging? I noticed you increased the input voltage and recorded VOSEL. Have you tested decreasing the input voltage and recording VOSEL? Also, check if the Analog comparator hysteresis is affected, although I see you configured HYSTCTR=0. Take two S32K116 photos and tell me the MCU mask. Best Regards, Robin Re: S32K comparator tolerance/offset Thank you for your detailed explanation. I now understand that you are concerned about the VAIO (Analog Input Offset Voltage) parameter in the S32K1 Datasheet. Internally, I saw the AE team's explanation: The AIO offset is the offset of the comparator itself. the offset between INP and INN. The INL error includes the DNL error since it is an integral over the DNL. The error is then |V_AIO| + |INL| Based on my understanding, directly using two analog voltages from an external signal source to input INP and INN respectively to test VAIO should be more intuitive than using bandgap voltage divider.  Regarding your question:  for the same MCU, VAIO is not a random value that changes arbitrarily from moment to moment , but it can drift with operating conditions, especially temperature. The VAIO value in the datasheet should be understood as a guaranteed/worst-case limit over the full temperature range. When designing the threshold, do not treat VAIO as negligible or as a fixed calibrated-out value . Keep margin based on the full-temperature worst-case |VAIO| , plus the DAC/INL error. I also checked your previous discussion on this: S32K116 comparator tolerance. It seems that CMP's accuracy doesn't meet your needs. Have you considered the feature described in section "44.5.5 Automatic compare function" of S32K1XXRM Rev14.2? "Table 41. 12-bit ADC characteristics (2.7 V to 3 V)" in S32K1 DataSheet Rev15 shows a maximum TUE of ±8 LSB. This appears to be more accurate than CMP. Re: S32K comparator tolerance/offset Thanks for your detailed explanation. I noted that the ADC may have better accuracy in our application. But somehow, we have requirements for using CMP as safety monitor from high level architecture and i am not sure if this can be changed to ADC.
View full article
S32K312 EVB - LPSPIハードウェアPCS0を使用したSDカードSPI初期化 こんにちは、 私はRTD 6.0.0(Non-AUTOSAR Lpspi_ Ipドライバー)を使って、S32K312 EVB上でSPI経由でSDカードドライバーを実装しています。 SD物理層簡略仕様書によると、SPI初期化シーケンスは次のとおりです。 電源投入後はCSレベルをHIGHに維持してください。 少なくとも74個のクロックパルスを生成します(私は0xFFを10バイト送信することで80個のクロックを送信しています)。 CS LOW を引いてください。 CMD0 (0x40 00 00 00 00 95) を送信します。 カードが「R1 = 0x01」と応答するまで、0xFFでポーリングしながらCSをLOWに保ってください。 私の問題は、ハードウェア制御のPCS0に関するものです。 ハードウェアPCS0でLpspi_Ipドライバを使用する場合、SPI転送中にLPSPIペリフェラルによってPCS信号が自動的にアサッサーされます。そのため、SD仕様で求められるCSをHIGHに保ち、その後CMD0とCS LOWを保持しながら最初の80クロックパルスを生成できません。 私には以下の質問があります。 S32K312 LPSPIペリフェラルは、SPIクロックを生成しながらPCSを非アクティブ(HIGH)に保つことに対応していますか? SDカードの初期化シーケンス中にPCSを手動で制御したり、一時的にハードウェアPCSを無効化したりするための、Lpspi_Ip APIやレジスタ設定、または推奨される方法はありますか? そうでない場合、推奨されるアプローチは、SDカードのCSピンをGPIOとして構成し、SCK、MOSI、およびMISOのみにLPSPIを使用しながら手動で制御することでしょうか? また、NXPがS32K3シリーズでSPIを介したSDカード通信を示すリファレンス実装、アプリケーションノート、サンプルプロジェクト、SDK/RTDの例があれば、ぜひ教えていただけますか? よろしくお願いします。 Re: S32K312 EVB - SD Card SPI Initialization using LPSPI Hardware PCS0 こんにちは、 @parvathitp PCS(周辺チップセレクト)信号はLPSPIモジュールによって制御されるよう設計されています。ハードウェアPCSを選択すると、SPIフレーム転送中にLPSPIペリフェラルによって自動的にアサッティングおよびデアッサートされます。 LPSPIモジュールに割り当てられているハードウェアPCS信号を手動で制御するための専用APIは提供されていません。したがって、あなたが言及したように、この場合の最良の方法はCSピンをGPIOとして設定することです。 この構成では、CS信号はSIUL2/GPIO APIを介して制御され、その制御はユーザーの責任となります。 現在、この正確な実装を示すS32K3専用のアプリケーションノート、例プロジェクト、参考文書は存在しません。 BR、VaneB
View full article
HSE INSTALL S32K311 下面的所有内容都是从附件中复制 S32DS版本:S32DS.3.5_b220726_win32.x86_64 (1).exe RTD版本:SW32K3_RTD_R21-11_3.0.0_P07_D2306_DS_updatesite.zip S32K311支持包版本:SW32K3_S32DS_3.5.6_D2309.zip SBAF版本:SBAF_S32K311_0_0_15_0, Bin文件:s32k311_Secure_Baf_0.12.0_0.15.0.6_pb230804.bin.pink HSE版本:HSE_FW_S32K311_0_2_40_0, bin文件为s32k311_hse_fw_0.12.0_2.40.0_pb230730.bin.pink 使用FULL_MEM 没有安全启动 当前遇到的一个问题 程序运行会一直卡在这里while ( FALSE == HSE_CheckStatus(HSE_STATUS_INIT_OK) ); 图片3.png   图片4.png 图片1.png 图片5.png   图片6.png   图片2.png      Re: HSE INSTALL S32K311 这个是补充的printf信息 DCMROF21: 0x00040000 HSE GPR3: 0x000000C0 Current_SBAF_Version-0x4039c020: 0x00000C00 LC 配置字-0x4039C02C: 0x00000000 生命周期相关信息-0x402AC200: 0x00000000 HSE Status: 0x00000000 我从网上查阅资料,是不是芯片出场自带的SBAF不识别我现在使用的HSE固件? Re: HSE INSTALL S32K311 我怀疑是SBAF没有将flash中的hse固件复制到hse_nvm中,如果是这个问题,我应该怎么解决 Re: HSE INSTALL S32K311 这个是我打印的数据 DCMROF21: 0x00040000 HSE GPR3: 0x000000C0 HSE Status: 0x00000000 HSE 固件未启动(NVM 空或固件损坏) 111.png Re: HSE INSTALL S32K311 嗨@iiiddd 请问能否提供 HSE_CONFIG_GPR3 (0x4039C028) 的值?位 0 表示 HSE 固件是否存在。 BR,VaneB Re: HSE INSTALL S32K311 我在编写 UTEST 时调用了 RTD 库。 gHsePort_FlsIf.writeApi(UTEST_BASE_ADDR,(uint8_t*)hseFwFeatureFlag,FW_FEATURE_FLAG_LEN); 将使用 FLS_MAX_VIRTUAL_SECTOR 定义。我的 RTD 库默认值为 135,但访问地址 0x1B000000UL 需要 136。我使用的RTD库与HSE不兼容吗? Re: HSE INSTALL S32K311 嗨@iiiddd HSE_CONFIG_GPR3[0] 位未设置,这表明设备上不存在 HSE 硬件。 作为参考,下图显示了为在 S32K311 设备上安装 HSE FW FULL_MEM 而配置的链接器文件示例: VaneB_0-1784568701705.png Re: HSE INSTALL S32K311 我在调试时发现 pflash 中有与 hse 固件对应的数据。你的意思是说,sbaf 未能将 pflash 中的固件复制到 hsenvm 中吗?如果这是问题所在,那么可能是什么原因造成的呢?
View full article
MRF13750H原理图 如何将 MRF13750H-915MHz 板转换为原理图?MRF13750H 数据手册包含 915 MHz 的参考板布局,但不包含原理图。 Luis_V_1-1784224999094.png
View full article