988777_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

988777_en-US

988777_en-US

Local Access Windows (LAWs), memory overlap

About LAW understanding : about the B4860 , just e.g B4860QDS;

Local Access Windows (LAWs):

in the B4860_QDS_Init.tcl file have set the Local Access Window Registers (as below have defined the phy address 0x000000, size 2Gbytes target to DDR)

and in the  dpaa_demo.c of CW_SC_3900FP_v10.8.3\SC\StarCore_Support\SmartDSP\demos

add the LAW setting the phy address 0x20000000 target  to  QMAN

my query or confusing is  the LAW 10 setting (0x0000000~0x7fffffff target to DDR)   memory overlapped with  QMAN software port  LAW setting the phy address 0x20000000 target  to  QMAN.

memory overlapped  between LAW , is it ok? and can explain detail why it can work ? there is not descript memory overlapped situation of LAW  in the reference manual of B4860.


 ## LAW10 to DDRC2
 # LAWBARH
 mem [CCSR_ADDR 0x000CA0] = 0x00000000
 # LAWBARL
 mem [CCSR_ADDR 0x000CA4] = 0x00000000
 # LAWAR
 mem [CCSR_ADDR 0x000CA8] = 0x8110001E

Re: Local Access Windows (LAWs), memory overlap

It’s interesting how local administrative systems handle data integration, especially when managing complex files like local access windows and memory overlap. Navigating these technicalities can sometimes feel as complicated as dealing with a newsportnewscourt.org schedule. Having a reliable, centralized resource to clear up the confusion makes a huge difference. Hopefully, more updates will roll out soon to make these processes much smoother for everyone involved.

Re: Local Access Windows (LAWs), memory overlap

Thanks for sharing the [RTD200P04 MCAL] S32M244 PWM PDB ADC MCAL demo—really helpful for developers working with embedded systems. For those handling compliance or security logging alongside hardware interfaces, reviewing Missouri offense records could offer useful insights for managing real-world data inputs. Always good to bridge technical applications with broader contextual awareness.

Re: Local Access Windows (LAWs), memory overlap

Please refer to the B4860 QorIQ Qonverge Multicore Baseband Processor Reference Manual, 2.3.1 Precedence of Local Access Windows.

标记 (1)
无评分
版本历史
最后更新:
‎07-17-2026 03:30 AM
更新人: