Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
MCXN947:添加 PWM SDK 元器件时出错 亲爱的恩智浦团队 我正在查看这个例子: https://github.com/nxp-appcodehub/dm-fashion-mnist-recognition-on-mcxn947/tree/df78550534b2a30410f56311cad05eb18956ed16 该示例在我的 FRDM-MCXN947 上运行良好。当我尝试通过 " Manage SDK 元器件 " 工具添加一个 PWM SDK 元器件时,编译中断时出现了许多错误。 有什么办法可以解决这种情况吗? 顺便说一下,我使用的是 MCUXpressio IDE 24.9 和 SDK 2.16.1 版。 谢谢。 MCX N Re: MCXN947: Erros Adding PWM SDK Components 你好@wklee 您能否尝试手动将 pwm 驱动程序添加到该项目中? BR 哈利 Re: MCXN947: Erros Adding PWM SDK Components 我从 GitHub 下载了示例,并将其导入到 mcuxpresso。 然后,我尝试通过 SDK 管理器添加 PWM 驱动程序。 它要求更新源代码,我同意了。之后,又有许多编译中断。 谢谢。 Re: MCXN947: Erros Adding PWM SDK Components 你好@wklee 请问您是否创建了新项目? 如何重现这个问题? BR 哈利
View full article
Anomaly motor control at certain speed on S32K MC Devkit software Hello, I'm running a BLDC motor in no-load condition using the firmware from the S32K BLDC/PMSM Development Kit, specifically the PMSM FOC 2Sh firmware. While operating the motor, I noticed that the graphs for certain RPMs (e.g., 2000, 3000, 4000) differ from those at other RPMs (such as 2500 and 3500), which generally follow a more consistent pattern. When measuring with a tachometer, the actual RPM usually matches the target RPM, but for those specific RPMs, the motor fails to maintain the required speed accurately - although the error is not very large. (like ±10 RPM) Could you explain why this problem occurs? Set RPM to 2000Set RPM to 2000 Set RPM to 2500Set RPM to 2500 Set RPM to 3000Set RPM to 3000 Set RPM to 3500Set RPM to 3500 Set RPM to 4000Set RPM to 4000 Re: Anomaly motor control at certain speed on S32K MC Devkit software Thank you for your interest in our products and for contributing to our community. Seems a motor parameter tuning issue… Depending of the S32K BLDC/PMSM Development Kit, it use by default the Sunrise motor 42BLY3A78-24110 or the Linix 45ZWN24-40 motor, and use the following parameter file, for example: In case you change the motor, the appropriate electrical parameters must be entered and tune the parameters of the different control schemes. I recommend you to take as reference the following training to learn how to use our MCAT Tool: Motor Control Application Tuning (MCAT) Tool – PMSM Servo Tuning I hope this information is helpful.
View full article
[HSE] [S32K31X] Crypto_KeyElementSet RSA Key support Customer attempted to store the public key used for SignatureVerify in the HSE NvM Catalog, but it appears that the current NXP Crypto does not support Crypto_KeyElementSet for RSA keys like the below.   The customer would like to ask whether there are any plans to support Crypto_KeyElementSet for RSA keys. The customer is using RTD 4.0.0. Additionally, is there currently any other method to store the key used for SignatureVerify in the HSE NvM Catalog? HSE_FW SECURITY_CRYPTO Re: [HSE] [S32K31X] Crypto_KeyElementSet RSA Key support Hello Alex, Since there have been no follow-up questions and 7 business days have passed since the last update, I am closing this case. In case of any further queries, please re-open the case or create a new one for support. Thanks, Sindhu Re: [HSE] [S32K31X] Crypto_KeyElementSet RSA Key support Hello Alex, RSA Key import in Autosar defined formats (CRYPTO_43_HSE_KE_FORMAT_BIN_RSA_PUBLICKEY, CRYPTO_43_HSE_KE_FORMAT_BIN_RSA_PRIVATEKEY) is not supported by Driver. But in crypto driver there is provision of importing key using custom format (CRYPTO_43_HSE_KE_FORMAT_BIN_CUSTOM_IMPORT_EXPORT). Type defines to be used for custom format is Crypto_43_HSE_KeyImportExportType. Thanks, Sindhu
View full article
[HSE] [S32K31X] Crypto_KeyElementSet RSA 密钥支持 客户试图在 HSE NvM 目录中存储用于 SignatureVerify 的公钥,但目前的 NXP Crypto 似乎不支持用于 RSA 密钥的 Crypto_KeyElementSet,如下所示。   客户想知道是否有计划支持 RSA 密钥的 Crypto_KeyElementSet。客户使用的是 RTD 4.0.0。 此外,目前是否有其他方法在 HSE NvM 目录中存储用于 SignatureVerify 的密钥? HSE_FW 安全加密 Re: [HSE] [S32K31X] Crypto_KeyElementSet RSA Key support 您好,亚历克斯, 由于没有后续问题,且距离上次更新已过去 7 个工作日,我将结案。如果还有其他疑问,请重新打开案例或创建新案例寻求支持。 谢谢, Sindhu Re: [HSE] [S32K31X] Crypto_KeyElementSet RSA Key support 你好,亚历克斯、 驱动程序不支持以 Autosar 定义格式(CRYPTO_43_HSE_KE_FORMAT_BIN_RSA_PUBLICKEY、 CRYPTO_43_HSE_KE_FORMAT_BIN_RSA_PRIVATEKEY)导入 RSA 密钥。 但是在加密驱动程序中配置了使用自定义格式(CRYP TO_43_HSE_KE_FORMAT_BIN_CUSTOM_IMPORT_EXPORT_BIN_CUSTOM_IMPORT_EXPORT_ 用于自定义格式的类型定义为 Crypt_43_HSE_KeyImportExportType。 谢谢! 辛杜
View full article
MCXN947: Erros Adding PWM SDK Components Dear NXP team, I am checking out this example: https://github.com/nxp-appcodehub/dm-fashion-mnist-recognition-on-mcxn947/tree/df78550534b2a30410f56311cad05eb18956ed16 The example works well on my FRDM-MCXN947. When I try to add one a PWM SDK component through the "Manage SDK Components" tool, the compilation breaks with many errors.  Is there anyway to get about this situation?  By the way, I am using MCUXpressio IDE 24.9 with SDK version 2.16.1. Thanks. MCXN Re: MCXN947: Erros Adding PWM SDK Components Hi @wklee  Can you try manually adding  pwm driver into this project? BR Harry Re: MCXN947: Erros Adding PWM SDK Components I download the example from GitHub and imported it to mcuxpresso. Then i try to add PWM driver through SDK manager. It asked for updating the source code, which I agreed. After that, many compilation breaks. Thanks. Re: MCXN947: Erros Adding PWM SDK Components Hi @wklee  May i ask if you create the new project? How can i reproduce this issue? BR Harry
View full article
LLCE LIN割り込み S32G3 には 4 つの LLCE lin チャネルがあり、Lin1 チャネルをスレーブとして、Lin0、2、3 をマスターとして設定しました。 スレーブの受信応答機能を検証する必要があります。 EB で LIN1 の割り込みを設定し、有効にしました。コールバック関数は Lin_CmdFromLlceIsr です。LIN1 に LIN メッセージを送信すると、LIN1 は割り込み応答を入力しません。代わりに LIN2 割り込みを有効にした場合にのみ、割り込みを入力でき、この時点で LIN1 は応答を返します。なぜこのようなことが起こるのでしょうか。 Re: LLCE LIN interrupt こんにちは、 @pmboat ご返信ありがとうございます。 デフォルトでは、LIN LLCE ファームウェアは内部 CORE 2 で実行されているため、LLCE LIN のCASEは LLCE_INT2 が使用されます。 BR チェイン Re: LLCE LIN interrupt はい、返信ありがとうございます。 私が使用するパッケージは次のとおりです。 1. SW32G_RTD_4.4_5.0.0_QLP03 2. S32G_LLCE_1_0_10 チップはs32g399aです。 Re: LLCE LIN interrupt こんにちは、 @pmboat ご投稿ありがとうございます。 1. LLCE LIN と提携しているようですが、本当ですか? 2. 使用している RTD/LLCE FW のバージョンはどれですか? BR チェイン
View full article
RTDを使用したセーフティ設定に関する質問 こんにちはチーム S32K314 の RTD(MCAL/SPD) 構成について教えていただけますか? Q1.割り込み付き PLL LOL に関する RTD の「構成」が見つかりませんでした。 どの構成(MCAL RTD と SPD から)で LOL のリセットまたは割り込みを構成できますか? Q2.割り込み付き LVD と HVD については、どれが LVD と HVD に関連しているのかわかりませんでした。 LVD および HVD からの割り込み反応は、「MCU_ERROR_ISR_NOTIFICATION」と「MCU_PMC_NOTIFICATION」のどちらでしょうか? Q3.ERM0 構成の場合、以下のコードのように ERM(RTD/SPD を使用) を構成するにはどうすればよいでしょうか? よろしくお願いします。 RTD S32_CONFIG_TOOL S32DS Re: Question about Safety configuration using RTD はい、そうです ユーザーは EB Tresos のこのノードでユーザー通知を設定できます。MCU_ERROR_ISR_NOTIFICATIONは PMC_VoltageError_IRQHandler > ...> Mcu_Ipw_ReportPowerErrorsCallback で呼び出され、その後この通知が呼び出されます。 Re: Question about Safety configuration using RTD こんにちは@cuongnguyenphu ご返信ありがとうございます。 念のため確認ですが、LVD/HVD は MCU_ERROR_ISR_NOTIFICATION と関係があるのでしょうか? よろしくお願いします。 (このチケットを閉じます...) Re: Question about Safety configuration using RTD こんにちは@Luke_Chun 1.PLL LOL の割り込みを設定するには、プラットフォーム モジュールで指定した IRQ が正しい必要があります。SoC_PLL_IRQn (NVIC 212) を有効にする必要があります。リファレンスマニュアルとヘッダーファイルには次のように記載されています。 ただし、RTD パッケージを確認すると、この割り込み用の ISR は提供されていません。SPD パッケージでも見つかりません。SO ユーザーはこの割り込みハンドラー用に独自の ISR を実装する必要があります。 2. NVIC 52のリファレンスマニュアルに記載されている割り込み付きLVDおよびHVD: RTD の MCU 統合マニュアルでは、これを処理するための ISR 名 PMC_VoltageError_IRQHandler を提供しています。 RTD のプラットフォームで IRQ「PMC_IRQn」を使用して設定し、有効にすることができます。 PMC_VoltageError_IRQHandler() では、 「MCU_ERROR_ISR_NOTIFICATION」マクロを介して MCU 構成のユーザー定義のコールバック通知 McuErrorIsrNotification も呼び出します。 3. ERM の設定方法: - RTD パッケージの場合: EB Tresos / S32CT には、ユーザーが ERM レジスタの値を設定できるようにするための設定がありません。しかし、RTD は、ユーザーがこのレジスタに値を設定できるように、BaseNXP/header/S32K314_ERM.h にマクロを提供しています。 ユーザーはこれらのマクロをベアメタル コードとして使用し、レジスタに値を設定できます。 - SPDパッケージでは、eMcemプラグイン、ファイルeMcem_Erm.cを参照します。関数eMcem_Erm_Init()では、以下のマクロを使用してERM[CR]レジスタに値を設定します:ERM_CR_ADDR32()、SAFETYBASE_REG_WRITE32()  
View full article
[HSE] [S32K31X] Crypto_KeyElementSet RSAキーのサポート お客様は、SignatureVerify に使用される公開キーを HSE NvM カタログに保存しようとしましたが、現在の NXP Crypto では、以下のような RSA キーの Crypto_KeyElementSet をサポートしていないようです。   お客様は、RSA キーに対して Crypto_KeyElementSet をサポートする予定があるかどうかを尋ねたいと考えています。お客様は RTD 4.0.0 を使用しています。 さらに、現在、SignatureVerify に使用されるキーを HSE NvM カタログに保存する他の方法はありますか? HSE_FW SECURITY_CRYPTO Re: [HSE] [S32K31X] Crypto_KeyElementSet RSA Key support こんにちは、アレックス。 フォローアップの質問がなく、最後の更新から 7 営業日が経過したため、このCASEを終了します。さらに質問がある場合は、CASEを再度開くか、サポート用に新しいCASEを作成してください。 ありがとう、 シンドゥ Re: [HSE] [S32K31X] Crypto_KeyElementSet RSA Key support こんにちは、アレックス。 AUTOSAR定義フォーマットでのRSAキーインポート( CRYPTO_43_HSE_KE_FORMAT_BIN_RSA_PUBLICKEY 、 CRYPTO_43_HSE_KE_FORMAT_BIN_RSA_PRIVATEKEY ) はドライバではサポートされていません。 ただし、暗号ドライバには、カスタム形式 ( CRYPTO_43_HSE_KE_FORMAT_BIN_CUSTOM_IMPORT_EXPORT ) を使用してキーをインポートする機能があります。 カスタムフォーマットに使用する型定義は Crypto_43_HSE_KeyImportExportType 。 ありがとうございます シンドゥ
View full article
FS32K116LAT0MLFT/FS32K116LAT0MLFRのトップマーキングとパッケージ仕様 こんにちは、 トップマーキングの意味を検証するのを手伝ってもらえますか? 行 1-2: FS32K116LAM-> 最後の M はどういう意味ですか? 3行目: ON96V 4行目: CTVREB また、トレイまたはテープ パッケージの象限位置についても教えてください。 Re: FS32K116LAT0MLFT/FS32K116LAT0MLFR top marking and package specification こんにちは、 @cynthia_pinto さん、 文字「M」は温度範囲(-40 °C ~ 125 °C)を示します。S32K データシートの 3.2 章 (ご注文情報) を参照してください。 標準注文可能部品のリストについては、データシートに添付されているスプレッドシート (S32K1xx_Orderable_Part_Number_List.xlsx) を参照することもCAN。 3 行目と 4 行目のマークは内部コーディングを示します。 最後に、「購入オプション」ページにパッケージ情報が表示されます: FS32K116LAT0MLFT 製品情報 | NXP Semiconductors 。 よろしくお願いします、 ジュリアン
View full article
i.mx93 EVK SDIO Wifi DTS RESET 引脚 我在 imx93 EVK 上调用外部 uSD 模块(TI cc33xx)时遇到了问题。 我已经从 linux-imx github 仓库中编译并版本了内核和 DTS 文件,然后在 EVK 上从 eMMC 启动并运行了它们。 在 DTS 中,我禁用了 M.2 SDIO 接口 usdhc3,并修改了 usdhc2 以支持 microSD 插槽。 wifi 卡开机并尝试初始化,但无法加载固件,因为它缺少与模块 RESET 引脚的连接。 我试过很多不同的设置,都无法正常工作。我正在尝试将模块中的 RESET 引脚连接到 imx 93 EVK (11x11) 上的 40 针 GPIO 接头。我最能从代码和 EVK 参考手册中看出,imx93 40 引脚接头的地址为 gpio2,而且我的 DTS 设置中有这些相关部分: reg_usdhc2_vmmc: regulator-usdhc2 { compatible = "regulator-fixed"; regulator-name = "WLAN_EN"; regulator-min-microvolt = <3300000>; regulator-max-microvolt = <3300000>; gpio = <&gpio2 7 GPIO_ACTIVE_HIGH>; /* * IW612 wifi chip needs more delay than other wifi chips to complete * the host interface initialization after power up, otherwise the * internal state of IW612 may be unstable, resulting in the failure of * the SDIO3.0 switch voltage. */ startup-delay-us = <20000>; enable-active-high; regulator-always-on; }; usdhc2_pwrseq: usdhc2_pwrseq { compatible = "mmc-pwrseq-simple"; // reset-gpios = <&pcal6524 20 GPIO_ACTIVE_LOW>; reset-gpios = <&gpio2 7 GPIO_ACTIVE_LOW>; post-power-on-delay-ms = <10>; power-off-delay-us = <80>; }; &usdhc2 { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_usdhc2>, <&pinctrl_usdhc2_wlan>; mmc-pwrseq = <&usdhc2_pwrseq>; vmmc-supply = <&reg_usdhc2_vmmc>; bus-width = <4>; keep-power-in-suspend; cap-power-off-card; non-removable; max-frequency = <10000000>; status = "okay"; #address-cells = <1>; #size-cells = <0>; wlcore: wlcore@2 { compatible = "ti,cc33xx"; reg = <2>; //interrupt-parent = <&pcal6524>; //interrupts = <5 IRQ_TYPE_EDGE_FALLING>; }; btti: btti@1 { compatible = "ti,cc33xxbt"; reg = <1>; }; }; pinctrl_reg_usdhc2_vmmc: regusdhc2vmmcgrp { fsl,pins = < MX93_PAD_SD2_RESET_B__USDHC2_RESET_B 0x31e >; }; 我将模块的 RESET 引脚连接到 40 引脚接头上的引脚 26。我做错了什么? 我应该在 EVK 上使用不同的密码进行 RESET 吗? Re: i.MX93 EVK SDIO Wifi DTS Reset Pin 您好! 看起来不错。唯一的建议是使用两个不同的 PAD 进行启用和 RESET。在这种情况下,您需要使用 SAM GPIO2_IO07 来实现这些功能。 顺祝商祺! 萨拉斯 Re: i.MX93 EVK SDIO Wifi DTS Reset Pin @Manuel_Salas感谢您的回复。 这些 usdhc2 部件看起来更好吗? reg_usdhc2_vmmc: regulator-usdhc2 { compatible = "regulator-fixed"; regulator-name = "WLAN_EN"; regulator-min-microvolt = <3300000>; regulator-max-microvolt = <3300000>; gpio = <&gpio2 7 GPIO_ACTIVE_HIGH>; /* * IW612 wifi chip needs more delay than other wifi chips to complete * the host interface initialization after power up, otherwise the * internal state of IW612 may be unstable, resulting in the failure of * the SDIO3.0 switch voltage. */ startup-delay-us = <20000>; enable-active-high; regulator-always-on; }; usdhc2_pwrseq: usdhc2_pwrseq { compatible = "mmc-pwrseq-simple"; // reset-gpios = <&pcal6524 20 GPIO_ACTIVE_LOW>; reset-gpios = <&gpio2 7 GPIO_ACTIVE_HIGH>; post-power-on-delay-ms = <10>; power-off-delay-us = <80>; }; &usdhc2 { pinctrl-names = "default"; pinctrl-0 = <&pinctrl_usdhc2>, <&pinctrl_usdhc2_wlan>, <&pinctrl_reg_usdhc2_vmmc>; mmc-pwrseq = <&usdhc2_pwrseq>; vmmc-supply = <&reg_usdhc2_vmmc>; bus-width = <4>; keep-power-in-suspend; no-1-8-v; cap-power-off-card; //non-removable; max-frequency = <10000000>; status = "okay"; #address-cells = <1>; #size-cells = <0>; wlcore: wlcore@2 { compatible = "ti,cc33xx"; reg = <2>; //interrupt-parent = <&pcal6524>; //interrupts = <5 IRQ_TYPE_EDGE_FALLING>; }; btti: btti@1 { compatible = "ti,cc33xxbt"; reg = <1>; }; }; pinctrl_reg_usdhc2_vmmc: regusdhc2vmmcgrp { fsl,pins = < MX93_PAD_GPIO_IO07__GPIO2_IO07 0x31e >; }; pinctrl_usdhc2_wlan: usdhc2wlangrp { fsl,pins = < MX93_PAD_CCM_CLKO1__GPIO3_IO26 0x31e >; }; 或者,我是否应该在&usdhc2 中以不同于 pinctrl-0 的方式处理? Re: i.MX93 EVK SDIO Wifi DTS Reset Pin 你好@rtwheato 我希望你过得很好。 PAD 存在混淆。 40 针接头中的 PAD 26 是 & gpio2 7 (EXP_GPIO_IO07),你在设备树 SD2_RESET_B 中使用的是不同的 PAD。 如果要使用 26 号 PIN(EXP_GPIO_IO07),则应改为 MX93_PAD_GPIO_IO07__GPIO2_IO07 顺祝商祺! 萨拉斯
View full article
S32K MC Devkit ソフトウェアの特定の速度での異常なモーター制御 こんにちは。S32K BLDC/PMSM 開発キットのファームウェア、具体的には PMSM FOC 2Sh ファームウェアを使用して、BLDC モーターを無負荷状態で実行しています。モーターを操作しているときに、特定の RPM (例: 2000、3000、4000) のグラフが、一般的にはより一貫したパターンに従う他の RPM (2500 や 3500 など) のグラフと異なることに気付きました。タコメーターで測定する場合、実際の RPM は通常、目標 RPM と一致しますが、特定の RPM では、モーターは必要な速度を正確に維持できません (ただし、誤差はそれほど大きくありません)。(±10 RPM など) この問題が発生する理由を説明していただけますか? Set RPM to 2000RPMを2000に設定する Set RPM to 2500RPMを2500に設定する Set RPM to 3000RPMを3000に設定する Set RPM to 3500RPMを3500に設定する Set RPM to 4000RPMを4000に設定する Re: Anomaly motor control at certain speed on S32K MC Devkit software 当社製品にご興味をお持ちいただき、また当社コミュニティに貢献していただき、ありがとうございます。 モーターパラメータの調整の問題のようです… S32K BLDC/PMSM 開発キットに応じて、デフォルトでSunrise モーター 42BLY3A78-24110またはLinix 45ZWN24-40 モーターが使用され、次のパラメータ ファイルが使用されます。例: モーターを変更するCASEは、適切な電気パラメータを入力し、さまざまな制御スキームのパラメータを調整する必要があります。 MCAT ツールの使用方法を学習するには、次のトレーニングを参考にすることをお勧めします。 モータ制御アプリケーションチューニング(MCAT)ツール - PMSMサーボチューニング この情報が役に立つことを願います。
View full article
Yocto BSP imx-5.4.70-2.3.0imx-image-full のビルディング中にフェッチ失敗 (spirv-tools / glslang) が発生しました こんにちは、 Yocto BSP imx-5.4.70-2.3.0 (ブランチ: imx-linux-zeus、マニフェスト: imx-5.4.70-2.3.0.xml) をビルドしようとしていますが、imx-image-full のビルド中にフェッチ エラーが発生しました。 エラーは次のとおりです: エラー: spirv-tools-git-r0 do_fetch: URL のフェッチャー失敗: 'git://github.com/KhronosGroup/SPIRV-Tools.git;name=spirv-tools;branch=main;protocol=https'。どのソースからも URL を取得できません。 エラー: glslang-git-r0 do_fetch: URL のフェッチャー失敗: 'git://github.com/KhronosGroup/glslang'。どのソースからも URL を取得できません。 興味深いことに、bitbake の外部で手動でフェッチしようとすると、正常に動作します。 git クローンhttps://github.com/KhronosGroup/glslang.git git チェックアウト 703bd9caab50b139428cea1aaff9974ebee5742e git クローンhttps://github.com/KhronosGroup/SPIRV-Tools.git git チェックアウト 9b3cc3e05337358d0bd9fec1b7a51e3cbf55312b したがって、ネットワーク接続は正常であり、リポジトリにアクセスできます。 Yocto のフェッチャーがここで失敗する理由を誰か教えてくれませんか? プロトコルの不一致 (git:// と https://) はありますか? レシピを更新したり、zeus ブランチのパッチを適用したりする必要がありますか? または、これらの依存関係を正常に取得するための推奨される回避策はありますか? よろしくお願いいたします。 評価ボード Re: Yocto BSP imx-5.4.70-2.3.0 Fetch failure (spirv-tools / glslang) while building imx-image-full こんにちは@binil ! ドキュメントを確認しているときに、GitHub が git:// プロトコルをサポートしなくなったことに気付きました。リポジトリでの作業を続行するには、HTTPS または SSH にスイッチする必要があります。 それに応じてリポジトリの URL を更新してください。 よろしくお願いします、 チャビラ Re: Yocto BSP imx-5.4.70-2.3.0 Fetch failure (spirv-tools / glslang) while building imx-image-full 添付画像をご確認ください Re: Yocto BSP imx-5.4.70-2.3.0 Fetch failure (spirv-tools / glslang) while building imx-image-full こんにちは@binil 、 NXP サポートにお問い合わせいただきありがとうございます。 フェッチエラーを示すログファイルを共有していただけますか?問題をより深く理解するために、自分の側で分析したいと思います。 並行して、私の側でエラーを再現してみます。 よろしくお願いします、 チャビラ
View full article
DS 3.6.3完全なMSYS2は含まれませんか? Design Studio 3.6.1 から 3.6.3 にアップデートしました(新規インストール)、Windows の場合。今、私のビルド システムは mingw gcc を見つけられなくなりました: S32DS.3.6.3/S32DS/build_tools/msys32/mingw32/bin/i686-w64-mingw32-gcc.exe 確かにそこには存在しません。 DS 3.6.1 および DS 3.6.3 のリリースノートどちらも、Design Studio には「MSYS2 2022.06-1」が含まれていると主張しています。SO 同じバージョンなので、DS 3.6.3でも変更はないと思います。しかし、両方の DS バージョンの msys32 フォルダーを比較すると、gcc が欠落しているだけでなく、多くの違いが明らかになります。 これは意図的なものですか? DS 3.6.4はリリースされるのかこれを「修復」するものですか? 回避策として、DS3.6.1 インストールから DS3.6.3 インストールに msys32 フォルダーをコピーするだけで CAN ますか? Re: DS 3.6.3 does not including full MSYS2? こんにちは、 遅れて申し訳ありません。S32DS v3.6.3 以降では MSYS2 が完全に削除され、ビルド ツールに必要な部分のみが残ります。完全な msys2 が必要な場合は、自分でインストール CAN。
View full article
Figure out the memory map of RT595 and start address/offset while loading FW into internal PSRAM thr Dear Sir, In order to figure out the start address/offset while loading FW into internal PSRAM through BLHost based on RT595. Would you kindly advise us what's the start address/offset and how to determine start address/offset based on the FW while loading FW into internal PSRAM through BLHost, please advise us if there is any document to address it. Thank you. @RossZWChen Re: Figure out the memory map of RT595 and start address/offset while loading FW into internal PSRAM Hi @Mike_Sun  Are you using our EVK?  Here is an snapshot of theFigure 2. MIMXRT595-EVK block diagram ( from UM12285 MIMXRT595-EVK Board User Manual)  I highligthed the PSRAM connections to FlexSPI0 or FlexSPI0.  Are you connecting the PSRAM to FlexSPI0/1?  Thank you!  Diego
View full article
复制: 获取分区 ID 无法正常工作 本帖复制自 此处 您好,恩智浦技术支持、 我在尝试使用 OsIf 模块中的获取分区 ID 时遇到了问题。我认为我有 3 个主要问题。 1.我不太清楚您试图使用的索引。在 OsIf_apxMultiPartitionPredefinedConfig 中,我本希望看到由实际操作系统定义的宏,而不是实际数字。我认为我的部分问题在于,你是根据 EcuC 中分区的索引来定义这个数组的,但我使用的操作系统(ETAS)是按字母顺序生成分区的,因此数字并不一致。生成硬编码列表是否是我需要考虑的长期策略? 2.不同模块的分区索引似乎不同。在 Adc 中,生成的表将我的分区 "ASILDCoreA "放在索引 2 中,但 Spi 将该分区放在零索引中。我不知道如何才能做到这一点......因为它们是通过 OsIf 中完全相同的函数访问的。我希望所有这些表中的 "ASILDCoreA "都在同一个索引中。您能确认这是生成代码中的缺陷吗?我附上了生成代码的截图,并附上了我的项目。 3.您正试图在您的 RTD 模块中使用 OsIf 中的 GetApplication(),以确定它们是从 EcuM_Driver_Init 中的哪个分区执行的。在 EcuM Init 结束之前,ETAS 不支持调用任何操作系统函数。那么......你认为 Mcal 模块应该在操作系统启动后排序,就像在 Rte_Init 任务中一样,还是说 ETAS 应该在操作系统启动前支持 GetApplication()?我不知道谁需要改变他们的设计假设......但现在,没有人想用 MCU1 来为通用汽车工作。 谢谢、 斯宾塞 优先级:中等 RTD 来源:恩智浦内部来源:恩智浦内部 Re: Copy: Get Partition ID not working correctly 你好@Luis_Garabo、 1.2,我尝试为 RTM600 版本配置多核,但我看不出 Adc、Spi 有任何问题。他们使用的是什么软件包? 3.从 Mcal 的观点来看,GetApplicationID() 的返回值用于识别正在运行的任务的应用程序标识符,因此,从我的观点来看,你只需确保正确获取应用程序标识符,并将其传递给 OsIf_apxMultiPartitionPredefinedConfig[应用程序标识符],就像这样: 顺祝商祺! Nhi
View full article
Yocto BSP imx-5.4.70-2.3.0 Fetch failure (spirv-tools / glslang) while building imx-image-full Hello, I am trying to build the Yocto BSP imx-5.4.70-2.3.0 (branch: imx-linux-zeus, manifest: imx-5.4.70-2.3.0.xml) and I am hitting fetch failures during the build of imx-image-full. The errors are: ERROR: spirv-tools-git-r0 do_fetch: Fetcher failure for URL: 'git://github.com/KhronosGroup/SPIRV-Tools.git;name=spirv-tools;branch=main;protocol=https'. Unable to fetch URL from any source. ERROR: glslang-git-r0 do_fetch: Fetcher failure for URL: 'git://github.com/KhronosGroup/glslang'. Unable to fetch URL from any source. Interestingly, when I try to fetch manually outside of bitbake, it works fine: git clone https://github.com/KhronosGroup/glslang.git git checkout 703bd9caab50b139428cea1aaff9974ebee5742e git clone https://github.com/KhronosGroup/SPIRV-Tools.git git checkout 9b3cc3e05337358d0bd9fec1b7a51e3cbf55312b So, network connectivity is fine and the repositories are accessible. Can anyone help me understand why Yocto’s fetcher is failing here? Is there a protocol mismatch (git:// vs https://)? Do I need to update the recipe or apply a patch for zeus branch? Or is there any recommended workaround to fetch these dependencies successfully? Thanks in advance. Evaluation Board Re: Yocto BSP imx-5.4.70-2.3.0 Fetch failure (spirv-tools / glslang) while building imx-image-full HI @binil! While reviewing the documentation, I noticed that GitHub no longer supports the git:// protocol. To continue working with repositories, you'll need to switch to either HTTPS or SSH. Please update your repository URLs accordingly. Best regards, Chavira Re: Yocto BSP imx-5.4.70-2.3.0 Fetch failure (spirv-tools / glslang) while building imx-image-full Please check the attached image Re: Yocto BSP imx-5.4.70-2.3.0 Fetch failure (spirv-tools / glslang) while building imx-image-full Hi @binil, Thank you for contacting NXP Support! Could you please share the log file showing the fetch errors? I’d like to analyze it on my end to better understand the issue. In parallel, I’ll attempt to replicate the error on my side. Best regards, Chavira
View full article
视窗工具建议 您好,NXP团队: 我们正在使用 kw45 向 Windows 应用程序发送数据,nxp 能否推荐任何嗅探器工具来检查 Windows 中的数据。 请建议是否有任何工具可以将数据从 KW45 发送到我们可以看到数据的任何 Windows 应用程序。 开发板 Re: Windows tool suggestions 你好 希望你一切顺利。 恩智浦目前没有为Windows提供专用的嗅探器工具。欢迎使用任何符合要求的嗅探器工具。 谨致问候, Ana Sofia。
View full article
RT595のメモリマップと、FWを内部PSRAMにロードする際の開始アドレス/オフセットを把握する 拝啓、 RT595 に基づいて BLHost を介して FW を内部 PSRAM にロードするときに、開始アドレス/オフセットを把握します。開始アドレス/オフセットとは何か、また、BLHost を介して内部 PSRAM に FW をロードする際に FW に基づいて開始アドレス/オフセットを決定する方法について教えてください。これに対処するドキュメントがあればお知らせください。ありがとう。 @RossZWChen Re: Figure out the memory map of RT595 and start address/offset while loading FW into internal PSRAM こんにちは@Mike_Sun 弊社のEVKをご利用いただいていますか? これは図2のMIMXRT595-EVKブロック図のスナップショットです( UM12285より) MIMXRT595-EVK ボード ユーザー マニュアル) FlexSPI0 または FlexSPI0 への PSRAM 接続を強調表示しました。 PSRAMをFlexSPI0/1に接続していますか? よろしくお願いいたします。 ディエゴ
View full article
关于使用 RTD 进行功能安全配置的问题 你好,团队 请问 S32K314 的热电阻(MCAL/SPD)配置如何? Q1.我没有在 RTD 上找到关于带中断的 PLL LOL 的 "配置"。 哪种配置(来自带有 SPD 的 MCAL RTD)可以配置 LOL 的 RESET 或中断? Q2.对于带中断功能的低压检测 和 HVD,我没看清哪个与低压检测 和 HVD 有关。 请问哪一个是低压检测和 HVD 的中断反应,“MCU_ERROR_ISR_NOTIFICATION” 还是 “MCU_PMC_NOTIFICATION”? Q3.对于 ERM0 配置,如何配置 ERM(使用 RTD/SPD),例如下面的代码? 谢谢! RTD S32_CONFIG_TOOL S32DS Re: Question about Safety configuration using RTD 是的 用户可在 EB Tresos 的此节点中配置其用户通知,MCU_ERROR_ISR_NOTIFICATION 将在 PMC_VoltageError_IRQHandler> 中调用 ...> 然后,Mcu_Ipw_ReportPowerErrorsCallback 将调用此通知 Re: Question about Safety configuration using RTD 你好@congnguyenphu 感谢您的回复。 为了再次确认,低压检测/HVD 与 MCU_ERROR_ISR_NOTIFICATION 有关,不是吗? 谢谢! (我将关闭此票......) Re: Question about Safety configuration using RTD 你好@Luke_Chun 1.要配置 PLL LOL 的中断,Platform 模块中指向的 IRQ 必须正确。应启用 SoC_PLL_IRQn(NVIC 212)。它在参考手册和我们的头文件中提到: 但是,我检查了 RTD 代码包,我们不为这个中断提供 ISR。我在 SPD 包中也找不到。因此,用户需要为该中断处理程序实现自己的 ISR。 2。NVIC 52 参考手册中提及的带中断的低压检测 和 HVD: 在 RTD 的 MCU 集成手册中,我们提供了名为 PMC_VoltageError_IRQHandler 的 ISR 来处理该问题: 您可以在 RTD 平台中通过 IRQ"PMC_IRQn" 配置并启用它。 在 PMC_VoltageError_IRQHandler() 中,它还通过"MCU_ERROR_ISR_NOTIFICATION "宏调用MCU 配置中用户自定义的回调通知 McuErrorIsrNotification。 3.如何配置 ERM: -在 RTD 代码包中:我们在 EB Tresos/S32CT 上没有配置来帮助用户配置 ERM 寄存器的值。但 RTD 在 BaseNXP/header/S32K314_ERM.h 中提供了宏,帮助用户设置该寄存器的值: 用户可以使用这些宏作为裸机代码来设置寄存器的值。 -在 SPD 代码包中:我指的是 emcem 插件,文件 emceM_ERM.C在函数 eMcem_Erm_Init()中,以下宏用于设置 ERM[CR] 寄存器的值:erm_cr_addr32()、safetybase_reg_write32()  
View full article
程序卡在 FreeRTOS 的 prvPortStartFirstTask 函数中 你好 最近,我在调试 S32K322 的 freertos 程序时遇到了一个问题:程序在运行时会卡在 prvPortStartFirstTask 函数中。 (开发平台:S32DS.3.6.2 芯片型号S32K322 RTD:SW32K3_S32M27x_RTD_R21-11_6.0.0_D2506_DesignStudio_updatesite FreeRTOS:SW32K3_FreeRTOS_10.6.0_CD_4.0.0_DS_updatesite_D2312 调试工具:SEGGER J-Link) Freertos 配置如下 我也研究过类似问题的解决方案,主要有两种方法:更新 FreeRTOS 版本;② 用 PE 烧录器替换调试工具。 由于我没有 PE 刻录机,我尝试了第一种方案,情况如下: 首先,我卸载了 SW32K3_SreeRTOS_10.6.0_CD_4.0_Supdatesite_S2312,然后安装 SW32K3_SreeRTOS_11.1.0_6.0.0_CD1_S2506-DesightStudio_uupdatesite(因为此版本的 freertos 与我的 RTD6.0 和 S32DS 3.6.2 兼容)。版本),并且在帮助 ->S32DS 扩展和更新 ->Installed 中显示安装确实成功。 但出现了两个问题: ① 没有操作系统层,更不用说 freertos 选项了 ② Freertos 没有例行程序 看来第一种方法失败了,所以我想问问是否有其他方法可以解决我的问题。谢谢
View full article