Hello, I'm running a BLDC motor in no-load condition using the firmware from the S32K BLDC/PMSM Development Kit, specifically the PMSM FOC 2Sh firmware. While operating the motor, I noticed that the graphs for certain RPMs (e.g., 2000, 3000, 4000) differ from those at other RPMs (such as 2500 and 3500), which generally follow a more consistent pattern. When measuring with a tachometer, the actual RPM usually matches the target RPM, but for those specific RPMs, the motor fails to maintain the required speed accurately - although the error is not very large. (like ±10 RPM) Could you explain why this problem occurs?
Set RPM to 2000Set RPM to 2000
Set RPM to 2500Set RPM to 2500
Set RPM to 3000Set RPM to 3000
Set RPM to 3500Set RPM to 3500
Set RPM to 4000Set RPM to 4000
Thank you for your interest in our products and for contributing to our community.
Seems a motor parameter tuning issue…
Depending of the S32K BLDC/PMSM Development Kit, it use by default the Sunrise motor 42BLY3A78-24110 or the Linix 45ZWN24-40 motor, and use the following parameter file, for example:
In case you change the motor, the appropriate electrical parameters must be entered and tune the parameters of the different control schemes.
I recommend you to take as reference the following training to learn how to use our MCAT Tool:
Motor Control Application Tuning (MCAT) Tool – PMSM Servo Tuning
I hope this information is helpful.