Multi Source Translation Content

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multi Source Translation Content

Discussions

Sort by:
S32K146 - MBDT - Runtime data store & retention during power cycle. Dear NXP Support Team, I hope this message finds you well. I’m currently working on a project involving the S32K146 MCU, and I’m using Simulink to handle EEPROM operations. I’ve encountered some issues with data retention that I haven’t been able to resolve, and I’d really appreciate your guidance. In my setup, I’m trying to store values to EEPROM using the "Flash_EEEWrite" block. I’m rotating values from a Repeating Sequence block and writing them after initializing the "Flash_Config". To ensure proper initialization, I’ve also added a 100ms delay before performing any write operations. However, after a power cycle, the values I’ve written are not retained. Here’s what I’ve observed: When the data type of the FLASH_EEEWrite block is set to  uint32_t, the value read back is consistently 7fff(Hex) When set to uint8_t, the value returned is 82(hex). These values are constant regardless of the input, and do not reflect the values I’m writing. I’m not sure if the issue lies in the configuration of EEPROM, the way I’m using the Simulink blocks, or perhaps a misunderstanding of how the FLASH_EEEWrite block works in this context. I’ve attached the Simulink model I’m working with, in case it helps illustrate the setup more clearly. Would you be able to provide any insight into what might be going wrong, or any recommended steps I should follow to ensure reliable EEPROM writes and retention across power cycles? Thank you very much in advance for your time and support. I really appreciate any help or suggestions you can provide.
View full article
ボディ図に関する問題点の指摘 lv_drivers\display\monitor.c 作成本体の関数window_create 中の有段代コード iconSurface = SDL_CreateRGBSurfaceFrom(simulator_icon, 32, 32, 16, 32 * 2, 0xf000, 0x0f00, 0x00f0, 0x000f); SDL_SetWindowIcon(m->window, iconSurface); SDL_FreeSurface(アイコンサーフェス); これらの機能は SDL ボディのピクチャを表示することですが、パッケージ全体ではこのピクチャが配置される場所にも到達せず、許可が固定されているかどうかもわかりません。 これは修正できますか? 追伸:私たちの仕事は、GuiGuider を使用して、Linux 上で実行可能なプログラムを構築することです。 Re: 提问关于窗体图标的问题 こんにちは、 @water spinach 、 ご投稿ありがとうございます。このコードは、GuiGuiderのデフォルトロゴであるSDLウィンドウアイコンの設定に使用されています。関連する画像データはソースコードに直接書き込まれています。コンパイルされたソフトウェアは変更できません。 ソフトウェアのソースコードは提供されていないため、ユーザーは変更できません。コードエディターで表示できるのは、ソフトウェアによって生成されたアプリケーションコードのみです。 これが役に立つことを願います。 BR、 セレステ
View full article
Facing issues with HSE Firmware on nxp s32k312 We are using the NXP S32K312 MCU and currently facing issues with the HSE firmware: 1.The HSE status register value appears corrupted (0x4038C107). 2.Unable to access HSE APIs due to this status corruption. 3.Attempts to erase or reflash the HSE firmware have failed. 4.Writing to MU0_TR1 register or memory to trigger erase/reset commands does not work. 5.Observed multiple software resets during a single external reset when debugger is connected. Request for Assistance: 1.Could you please provide the correct and recommended procedure to erase and reflash the HSE firmware on the S32K312? 2.If reflashing the HSE firmware is not possible due to the current corrupted state, what steps can be taken to recover the HSE or resolve the status register corruption? 3.Any known issues or workarounds for the multiple resets observed during hard reset with debugger attached? 4.How can I resolve the corrupted HSE status register issue and regain access to the HSE APIs? Process we followed HSE firmware flashing. step 1:We flashed the provided PINK file without IVT along with the demo application and the secure boot application ELF files. step2:Reset done Step3:Observed ?? marks at HSE locations 0x005d4000 and DCM registers Step4: We reflashed our bootloader at address 0x00400000 and the application at address 0x00442000 Step5:When performing a hard reset with the debugger connected, we observed multiple resets triggered from the software side, despite issuing only a single external reset command  Please find Screenshots for reference @lukaszadrapa Please help me to resolve these issues Re: Facing issues with HSE Firmware on nxp s32k312 Well, this is not supposed to happen. I have a couple of questions: What is version of your SBAF? You can read it at 0x4039_C020. Description can be found in Table 141 in HSE FW reference manual rev. 2.5. Which version of HSE FW did you installed? And was that AB_SWAP or FULL_MEM version? Which installation method did you use? Is there any application loaded in the flash? If so, how are the clocks configured? And notice that once HSE feature flag in UTEST is programmed, corresponding area in flash for HSE firmware is removed from memory map permanently. If HSE firmware is erased, this area won't be accessible again. The same is valid when AB_SWAP version is installed - in this case, there are two areas reserved for HSE firmware, one in active block, one in passive block. When AB_SWAP is installed, HSE OTA flag is programmed in UTEST, so both areas will be reserved for HSE firmware forever. Facing issues with HSE Firmware on nxp s32k312 Hi, I attempted to reinstall the HSE firmware on a new hardware platform. Initially, the HSE status register shows the bit '0' (indicating the presence of HSE firmware) correctly set. However, after performing a functional reset, this bit is cleared, and I am no longer able to access the HSE firmware — even though the memory allocated for it appears to be intact. Could you please clarify the expected behavior of the HSE status register after a functional reset? Additionally, what are the recommended reset handling steps to ensure the HSE firmware remains accessible post-reset? Re: Facing issues with HSE Firmware on nxp s32k312 The HSE firmware reference manual can be downloaded from this page from Documentation -> Secure files section: https://www.nxp.com/products/S32K3#documentation If it is not visible for your, it may be necessary to request the access rights: https://www.nxp.com/support/support/secure-access-rights:SEC-ACCESS Based on content of MU FSR register (0x4038C107), the HSE firmware is not present. That means you cannot run any HSE services. As I wrote in my first response, check HSE GPR register at 0x4039_C028. If bit 0 is cleared, there's no HSE firmware installed.  There are three methods how to install the firmware - by default location, via IVT or via MU. All of them are described in the HSE firmware reference manual.  Regards, Lukas Re: Facing issues with HSE Firmware on nxp s32k312 Hi, Thanks for the reply. I am currently unable to erase the HSE firmware. I attempted the method suggested previously—writing 0x57 into RAM and using the TR[1] mechanism—but it did not succeed in erasing the memory. Additionally, the HSE firmware APIs are not responding or functioning as expected. I am facing HSE firmware reinstallation issue as shown in figure. Could you please provide an alternative or updated method to forcefully erase or reset the HSE firmware? How to download HSE Firmware Reference Manual Re: Facing issues with HSE Firmware on nxp s32k312 Hi, Thanks for the reply. I am currently unable to erase the HSE firmware. I attempted the method suggested previously—writing 0x57 into RAM and using the TR[1] mechanism—but it did not succeed in erasing the memory. Additionally, the HSE firmware APIs are not responding or functioning as expected. I am facing HSE firmware reinstallation issue. Could you please provide an alternative or updated method to forcefully erase or reset the HSE firmware? Re: Facing issues with HSE Firmware on nxp s32k312 Hi @Anitha7  This seems to be the key point: "step 1:We flashed the provided PINK file without IVT along with the demo application and the secure boot application ELF files." Installation method via "default application NVM location" (no pointer to the pink file is defined in IVT) works only when there's no valid IVT in the flash. If you loaded the pink file to 0x400000 and some other applications with valid IVT to the flash, HSE firmware will not be installed.  According to your screenshots, HSE feature flag at 0x1B00_0000 has been already programmed because area at 0x5D_4000 is reserved for HSE firmware. Easiest solution - erase whole flash (including data flash) and load only the pink file at 0x40_0000. Reset the device and HSE firmware will be installed.  Then you can check HSE GRP register at 0x4039_C028. If bit 0 is set, HSE firmware is installed.  Regards, Lukas
View full article
K32W0xx 电压纹波问题 我们现在遇到了两个与 K32W041 有关的问题: Vbat 时的电压纹波 Vbat 时的电压纹波 我们根据 AN12893(使用 DC-DC 功能)跟进了 K21W041 的电源设计。因此,正确的去耦电容,PCB设计规则。在这一点上没有让步。 我们在 Vbat 上测量到高达 40mVpp 的纹波。 这是芯片的 DCDC 造成的。 我们需要额外的信息来减少这种涟漪。 使用哪种类型的 DCDC 稳压器? 开关电流的值是多少? 如何控制开关电流? 使用哪种类型的反馈控制器? 提供 DCDC 的方框图/结构图 我们需要降低纹波和开关电流 HW-开源 Re: K32W0xx voltage ripple problems 你好 能否请您帮助我们检查一下 EVK 是否也存在这个问题? 让我知道你的发现。 顺祝商祺! 安娜-索菲亚 Re: K32W0xx voltage ripple problems 你好,索菲亚,感谢您的回复。 你给出的提示,我已经研究过了。 这就是我写这篇文章的原因。 很抱歉,这些信息并没有回答我在本帖中提出的任何问题。 我需要专家信息来优化 DCDC 的实施,以改进我们的应用。 对第一个问题的回答将对此有所帮助。 🙂 Re: K32W0xx voltage ripple problems 你好 希望你一切顺利。 K32W061/41 中的内部直流/直流模块是一个降压变流器,可将输入电源电压转换为固定输出电压。 我建议查看 K32W 硬件设计用户指南,该指南可在 K32W061/41 产品页面 > 设计资源 > K32W061 制造代码包,软件包下找到 DC-DC 负载电流配置取决于参考设计中的电感值,可以进行优化以适应应用的负载电流,基于 K32W041A/AM 的示意图的 DC-DC 电感器为 2.2 μH,参见 K32W 硬件设计用户指南第 4.1 节原理图设计。 你也可以查看第 4.9 节 " DC-DC 元器件 " 和 4.11.2 " VDD(电台)、FB、VDD_PMU、VDD_PMU、VDDE 和 VBAT 解耦 ",其中包含相关信息。 在《用户手册》第 4.2.1 节中,您可以找到 DCDC 系统图。在数据表第 9.2 节的原理图中,您可以找到应用图 - 电池供电解决方案。 你能帮我们根据这些建议审查你的板的原理图吗?使用 K32W061、QN9090 或 JN5189 首次版本 PCB 的最佳方式 顺祝商祺! 索菲亚
View full article
LS1017 - XSPI_B 读取错误 您好,恩智浦支持团队、 我在 LS1017 设备的 XSPI_B 接口上遇到了读取问题 。 硬件信息/设置: CPU XSPI_B 连接到 microsemi FPGA CPU 平台频率 = 400 MHz,CPU 速度 = 1500 MHz --> XSPI 勘误表 A-050568 不适用 单点对单点连接(线长约 70 毫米,匹配度 +-2 毫米) DDR 模式 50 MHz(100Mbit) LS1017 仅使用 IP 模式命令 DQS 由 FPGA 驱动 - 提供读取选通(MCR0[RXCLKSRC]==3) DQS 采样点的 DLL 设置为:slvdlyTarget=0xF;dllen=0x1;ovrden=0x0;dllxCR 中的其他字段保留为 RESET 值(全部为零) 只有 CS 信号有一个 4.75k 上拉电阻器 印刷电路板上的模拟信号完整性看起来很好 错误/测试信号: 首先,在 LS1017(VxWorks 操作系统)上进行测试,生成一个随机图案,并将其写入 FPGA 内的测试存储器一次。 写入事务完成后,该函数定期从 FPGA 测试存储器读取图案,并将其与原始值(每个读取循环 512 字节)进行比较。 请参阅附件中显示错误的测试功能控制台输出示例。 我尝试读取和验证测试内存内容 5000 次。在这种情况下,前 1207 次运行没有出现错误。运行 1208 包含错误。 错误模式具有明显的特征: 错误发生在 64 字节对齐(=IP 命令长度)-->(随附示例:偏移量 384/64=6) 错误正好是 64 字节长(=IP 命令长度)-->(随附示例:偏移量 448-384=63) 在 64 个错误字节内只有每一个字节都有错误——--> > DQS 的下降边缘? 看来整个 64 字节的第二个字节被转移了 预计偏移 384-391: 0x d5 7923 8052 565e 4d 实际偏移 384-391: 0x d5 8a 23 7952 805e 56 在其他测试运行中,误差具有相同的特征,但运行和偏移量不同。 我的问题 您过去是否遇到过类似的阅读问题 在参考手册中,图 187。DQS 与 A_SCLK/B_SCLK 相位一致,但实际上 DQS 的上升/下降沿会受到往返时间 + FPGA 前置时间的影响。(我们的情况是 8 至 10 毫微秒)。能否提供更多信息,说明内部 DQS 采样机制/DLL 延迟线是如何工作的?(例如,DLL 的时基) 数据表 49.包含CS 输出保持时间/CS 输出延迟的公式,参数为 T/2。同表中提到的前 FSCK 周期是多少?FSCK = 串行根时钟?--> 在我们的情况下,T=10ns? 图 32:FlexSPI DDR 模式 2 = (MCR0[RXCLKSRC]=0x3)?表 48 中的 TFSIDVW 值也适用于 MCR0[RXCLKSRC]=0x3 的 DDR 模式 顺祝商祺! SL QorIQ LS1设备 Re: LS1017 - XSPI_B read errors 你好@Stefan_L 希望这封邮件能给你带来好运、 这可能是同步问题、 我想问你几个问题、 你是否考虑过该科的说明? 18.5.14.4 DLL 采样配置: 如果串行根时钟低于 100 MHz,DLL 就无法锁定串行根时钟的半周期,因为延迟链中的延迟 单元数量有限。那么 DLL 的配置应改为: - OVRDEN=0x1 - OVRDVAL=N;DLL 中的每个延迟单元约为 75 ps~225 ps。DLL 延迟链的延迟为 (N * Delay_cell_delay),N 应根据最大值设置。当前项目支持的 DDR 频率,N = 17,请注意这是推荐值。如果遇到故障,可能需要在实际应用中进行调整。 — DllxCR 中的其他字段应保留为 RESET 值(全部为零) 能否提供 LS1017 的根时钟信号波形? 你是否考虑过 QorIQ LS1028A 参考手册 2019 年 12 月 0 修订版 " 18.6.6 FPGA 设备上的应用程序 " 部分中的信息? 祝您有美好的一天。 BR、 赫克托五世
View full article
IMX8M MiniのMIPI-CSIプレスリリース、製品ニュースパイプラインが動作しない こんにちは、チームの皆さん メディア パイプラインを構成しようとしたときに、どうしても /dev/media0 ノードをユーザー空間に表示できません。私たちのユース CASEでは、Yoctoビルドを備えたカスタム統合ボードで Compulab IMX8M Mini SOM を使用しています。Allied ビジョン カメラを同社の Alvium CSI2 ドライバと統合しようとしています。 主な基本的な質問: カーネルとデバイス ツリーが正しく設定されていれば、パイプラインが正しく構成されていれば /dev/media0 ノードは引き続き表示されますか?または、パイプラインを正常に開始するには、ドライバをロードする必要がありますか?いずれにしても、何をしても media0 ノードは表示されCANません。 起動時には、ボードのセットアップによりカメラがまだ使用可能になっていません。ユーザー空間に入ったら(電源レギュレータが設定され、カメラの準備が整った後)、ドライバをこの出力に再バインドします。 root@b2qt-imx8mm-lpddr4-evk:/usr/share/BoardSetup-scripts# ./RebindCamera.sh AVT カメラ ドライバを再バインドしています... ./RebindCamera.sh:7行目: echo: 書き込みエラー: そのようなデバイスはありません [ 43.335322] avt_csi2 0-003c: avt_probe[5107]: /usr/src/debug/avt-csi2/1.2.0+git/avt-csi2.c [ 43.344799] avt_csi2 0-003c: avt_probe[5147]: パワーダウンGPIOが定義されていません [ 43.351676] avt_csi2 0-003c: avt_probe[5164]: devm_gpiod_get_optional(dev, "reset-gpios" が成功しました [ 43.360713] avt_csi2 0-003c: avt_probe[5171]: fwnode_property_present が mipi_csi を見つけられませんでした [ 43.369373] avt_csi2 0-003c: avt_probe[5188]: bcrm_wait_timeoutが見つかりません。デフォルト値を使用してください [ 43.377842] avt_csi2 0-003c: avt_probe[5191]: bcrm_wait_timeout が 3000ms に設定されました [ 43.385046] avt_csi2 0-003c: avt_csi2_check_mipicfg[4586]: ep_cfg.bus.mipi_csi2.num_data_lanes1 [ 43.393965] avt_csi2 0-003c: avt_csi2_check_mipicfg[4588]: v4l2_fwnode_ep.nr_of_link_frequencies2 [ 43.402965] avt_csi2 0-003c: avt_csi2_check_mipicfg[4593]: v4l2_fwnode_ep.link-frequencies0 値 445500000 [ 43.412824] avt_csi2 0-003c: avt_csi2_check_mipicfg[4593]: v4l2_fwnode_ep.link-frequencies 1 値 891000000 [ 43.422688] avt_csi2 0-003c: avt_probe[5213]: powerdown-gpios powerdownが定義されていません [ 43.430332] avt_csi2 0-003c: avt_probe[5228]: reset-gpios が定義されていません [ 43.436726] avt_csi2 0-003c: avt_reset[2080] [ 43.443043] avt_csi2 0-003c: wait_camera_available[2025]: カメラのシャットダウンを待機しています... [ 44.648643] avt_csi2 0-003c: wait_camera_available[2033]: カメラがI2C転送に応答するのを待っています... [ 45.269281] kauditd_printk_skb: 15 個のコールバックが抑制されました [ 45.269292] 監査: タイプ=1334 監査(1723754849.880:26):プログラムID=21 オペレーション=UNLOAD [ 46.664540] avt_csi2 0-003c: wait_camera_available[2054]: ハートビートがサポートされています。ハートビートがアクティブになるのを待っています。 [ 49.878985] avt_csi2 0-003c: wait_camera_available[2064]: ハートビートがアクティブ [ 49.949573] avt_csi2 0-003c: read_cci_registers[748]: regmap_bulk_read(camera->regmap8, cci_cmd_tbl[CCI_REGISTER_LAYOUT_VERSION ].アドレス ret 540 [ 49.969505] avt_csi2 0-003c: cciレイアウトバージョンb: 0x00000100 [ 49.975362] avt_csi2 0-003c: cciレイアウトバージョンa: 0x00010000 [ 49.981170] avt_csi2 0-003c: avt_probe[5285]: read_cci_registers が成功しました [ 49.989267] avt_csi2 0-003c: avt_probe[5302]: bcrm_version_check が成功しました [ 49.996951] avt_csi2 0-003c: bcrm_get_write_handshake_availibility[704]: BCRM書き込みハンドシェイクがサポートされました! [ 49.996975] avt_csi2 0-003c: カメラALVIUM 1500 C-501c NIRを発見 [ 50.014014] avt_csi2 0-003c: avt_probe[5315]: ファームウェアバージョン: 0.6.0.8c98 ret = 0 [ 50.024773] avt_csi2 0-003c: gcprmのバージョンを修正 [ 50.029887] avt_csi2 0-003c: avt_probe[5353]: INIT_WORK(&camera->bcrm_wrhs_work, bcrm_wrhs_work_func); [ 50.046953] avt_csi2 0-003c: avt_get_sensor_capabilities[4409]: csiクロック [ 50.046953] カメラ範囲: 40000000:750000000 Hz [ 50.046953] dts リンク周波数数 2 [ 50.046953] dts link_frequencies[0] 445500000 Hz [ 50.103673] avt_csi2 0-003c: avt_get_sensor_capabilities[4450]: カメラから読み取ったCSIクロック: 443750000 Hz [ 50.113207] avt_csi2 0-003c: avt_get_sensor_capabilities[4454]: 最小解像度と最大解像度を取得する [ 50.128752] avt_csi2 0-003c: avt_init_avail_formats[1840]: MEDIA_BUS_FMT_UYVY8_2X8/V4L2_PIX_FMT_UYVY/MIPI_CSI2_DT_YUV422_8Bを追加 利用可能な形式のリスト -1 - 1 [ 50.152546] avt_csi2 0-003c: avt_init_avail_formats[1841]: MEDIA_BUS_FMT_UYVY8_1X16/V4L2_PIX_FMT_UYVY/MIPI_CSI2_DT_YUV422_8を追加 B 利用可能な形式のリスト -1 - 1 [ 50.167322] avt_csi2 0-003c: avt_init_avail_formats[1842]: MEDIA_BUS_FMT_YUYV8_1X16/V4L2_PIX_FMT_YUV422P/MIPI_CSI2_DT_YUV42を追加 2_8B 利用可能な形式のリスト -1 - 1 [ 50.182333] avt_csi2 0-003c: avt_init_avail_formats[1843]: MEDIA_BUS_FMT_YUYV8_2X8/V4L2_PIX_FMT_YUYV/MIPI_CSI2_DT_YUV422_8Bを追加 利用可能な形式のリスト -1 - 1 [ 50.197003] avt_csi2 0-003c: avt_init_avail_formats[1844]: MEDIA_BUS_FMT_VYUY8_2X8/V4L2_PIX_FMT_VYUY/MIPI_CSI2_DT_YUV422_8Bを追加 利用可能な形式のリスト -1 - 1 [ 50.211670] avt_csi2 0-003c: avt_init_avail_formats[1849]: MEDIA_BUS_FMT_RGB888_1X24/V4L2_PIX_FMT_RGB24/MIPI_CSI2_DT_RGB888を追加 利用可能な形式のリスト -1 - 1 [ 50.226343] avt_csi2 0-003c: avt_init_avail_formats[1850]: MEDIA_BUS_FMT_RBG888_1X24/V4L2_PIX_FMT_RGB24/MIPI_CSI2_DT_RGB888を追加 利用可能な形式のリスト -1 - 1 [ 50.241008] avt_csi2 0-003c: avt_init_avail_formats[1851]: MEDIA_BUS_FMT_BGR888_1X24/V4L2_PIX_FMT_RGB24/MIPI_CSI2_DT_RGB888を追加 利用可能な形式のリスト -1 - 1 [ 50.255682] avt_csi2 0-003c: avt_init_avail_formats[1852]: MEDIA_BUS_FMT_RGB888_3X8/V4L2_PIX_FMT_RGB24/MIPI_CSI2_DT_RGB888を追加 利用可能な形式のリスト -1 - 1 [ 50.270271] avt_csi2 0-003c: avt_init_avail_formats[1856]: MEDIA_BUS_FMT_SGRBG8_1X8/V4L2_PIX_FMT_SGRBG8/MIPI_CSI2_DT_RAW8 t を追加 o 利用可能な形式のリスト 1 - 1 [ 50.284685] avt_csi2 0-003c: avt_init_avail_formats[1863]: MEDIA_BUS_FMT_SGRBG10_1X10/V4L2_PIX_FMT_SGRBG10/MIPI_CSI2_DT_RAWを追加 10 利用可能な形式のリスト 1 - 1 [ 50.320636] avt_csi2 0-003c: avt_init_controls[3359]: コントラストコントロール (0x980901) はカメラでサポートされていません [ 50.357183] avt_csi2 0-003c: avt_init_controls[3359]: シャープネスコントロール (0x98091b) はカメラでサポートされていません [ 50.367712] avt_csi2 0-003c: avt_update_sw_ctrl_state[2840]: ソフトウェアトリガーコントロールが見つかりません! [ 50.369213] avt_csi2 0-003c: avt_update_sw_ctrl_state[2840]: ソフトウェアトリガーコントロールが見つかりません! [ 50.378025] avt_csi2 0-003c: avt_update_sw_ctrl_state[2840]: ソフトウェアトリガーコントロールが見つかりません! [ 50.412857] mxc_mipi-csi 32e30000.mipi_csi:登録されたセンササブデバイス: avt_csi2 0-003c [ 50.429900] avt_csi2 0-003c: カメラ avt_csi2 0-003c が登録されました [ 50.435940] avt_csi2 0-003c: -> avt_probe[5420]: sysfsグループが作成されました!(0) [ 50.446676] avt_csi2 0-003c: avt_probe[5442]: プローブ成功! [ 50.378025] avt_csi2 0-003c: avt_update_sw_ctrl_state[2840]: ソフトウェアトリガーコントロールが見つかりません! [ 50.412857] mxc_mipi-csi 32e30000.mipi_csi:登録されたセンササブデバイス: avt_csi2 0-003c [ 50.429900] avt_csi2 0-003c: カメラ avt_csi2 0-003c が登録されました [ 50.435940] avt_csi2 0-003c: -> avt_probe[5420]: sysfsグループが作成されました!(0) [ 50.446676] avt_csi2 0-003c: avt_probe[5442]: プローブ成功! root@b2qt-imx8mm-lpddr4-evk:/usr/share/BoardSetup-scripts# この時点では、カメラはセットアップされ、ストリーミングの準備ができていると想定されますが、フレームやデータをユーザー空間に取り込むことはできません。添付の TestStream.sh スクリプトを使用します。 root@b2qt-imx8mm-lpddr4-evk:/usr/share/BoardSetup-scripts# ./TestStream.sh ./TestStream.sh:1行目: amera: コマンドが見つかりません === カメラストリーミングコントロール === 1. 現在のカメラの状態を確認します。 [ 76.502724] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 ビデオキャプチャのフォーマット:[ 76.511315] mxc_mipi-csi 32e30000.mipi_csi:フォーマットが一致しません 幅/高さ: 0/0 [ 76.519017] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 ピクセル形式: '' 分野: 任意 1行あたりのバイト数: 0 画像サイズ: 0 カラースペース: デフォルト Tra[ 76.537857] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 nsfer関数: デフォルト([76.548706] avt_csi2 0-003cにマップ: avt_core_ops_s_power[2156]+: on 0、camera->power_count 1 記録。709) YCbCr/HSVエンコーディング: デフォルト(ITU-R 601にマップ) 量子化: デフォルト (フルレンジにマップ) フラグ: 2. 利用可能なco[ 76.570719] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 1, camera->power_count 0をリストします コントロール: 3. 利用可能なフォームをリストします[ 76.581151] mxc_mipi-csi 32e30000.mipi_csi:フォーマットが一致しません ats: ioctl: VIDIOC_ENUM_FMT Ty[ 76.589396] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 pe: ビデオキャプチャ 4. 基本的なフォーマットを設定する: [ 76.611180] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.619262] mxc_mipi-csi 32e30000.mipi_csi:フォーマットが一致しません ピクセルフォーマット「UYVY」が無効です[76.625042] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 0、camera->power_count 1 5. ストリーミング コントロールがあるかどうかを確認します。 [ 76.647122] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.655283] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 6. ストリーミングを有効にしてみます(コントロールが存在する場合)。 [ 76.672441] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.682040] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 ストリーミング V4L2 コントロールが見つかりません [ 76.699454] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.708214] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 stream_enable コントロールが見つかりません 7. 取得開始を試みます(AVT 固有): [ 76.724226] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.733618] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 取得開始コントロールが見つかりません 8. 露出とゲインをチェックします(適切であることを確認します)。 [ 76.749702] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.759271] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 露出制御なし [ 76.775975] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.784748] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 ゲインコントロールなし 9. コントロールが存在する場合は、適切な露出/ゲインを設定します。 [ 76.801835] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.810768] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 露出を設定できません [ 76.827415] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.837494] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 ゲインを設定できません 10. 設定後にフレームをキャプチャしてみます。 ./TestStream.sh:47行目: タイムアウト: コマンドが見つかりません ❌ ストリーミング設定後もデータがありません 11. カーネル メッセージでストリーミング ステータスを確認します。 [ 76.784748] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 [ 76.801835] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.810768] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 [ 76.827415] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン1、カメラ->power_count 0 [ 76.837494] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: オン0、カメラ->power_count 1 root@b2qt-imx8mm-lpddr4-evk:/usr/share/BoardSetup-scripts# 現在、フォーマットが一致しないため、/dev/media0 ノードのプレスリリース、製品ニュース-ctl を介してリセットして変更するつもりです。しかし、それは表示されません。 以下は、DTS の関連する中核部分です。 // I2Cバス上でカメラを定義する &i2c1 { /* * I2C アドレス 0x21 に PCAL6416A GPIO エクスパンダーを定義します。 * 参照できるように、「gpio_expander」というラベルを付けます。 */ gpio_expander: pcal6416a@21 { 互換性 = "nxp、pcal6416"; <0x21> レジスタ <2> = !; gpio コントローラ; #gpioセル =; }; アルビウム: アルビウム@3c { 互換性 = "alliedvision、avt_csi2"; レジスタ =<0x3c> �; ステータス = "正常"; pinctrl-names = "デフォルト"; pinctrl-0 = <&pinctrl_alvium_clk>、<&pinctrl_alvium_gpio>; // Attollo デイカメラ用ハードウェア設定 電源 = <&dayCam_step2>; リセットgpios = <&gpio1 15 GPIO_ACTIVE_LOW>; クロック = <&clk IMX8MM_CLK_CLKO1>; クロック名 = "csi_mclk"; 割り当てられたクロック = <&clk IMX8MM_CLK_CLKO1>; 割り当てられたクロックの親 = <&clk IMX8MM_CLK_24M>; 割り当てられたクロックレート = <24000000>; ポート { レジスタ = <0>; alvium_mipi_ep: エンドポイント { リモートエンドポイント = <&mipi1_sensor_ep>; データレーン = <2>; リンク周波数 = /ビット/ 64 <445500000 891000000>; mipi-csi; }; }; }; }; &mipi_csi_1 { ステータス = "正常"; /delete-node/ ポート; ポート { mipi1_sensor_ep: エンドポイント@1 { レジスタ = <1>; リモートエンドポイント = <&alvium_mipi_ep>; データレーン = <2>; csis-hs-settle = <13>; csis-clk-settle = <2>; csis-wclk; }; csi1_mipi_ep: エンドポイント@2 { レジスタ = <2>; リモートエンドポイント = <&csi1_bridge_in>; }; }; }; &csi1_bridge { ステータス = "正常"; fsl、mipi モード; /delete-node/ ポート; ポート { csi1_bridge_in: エンドポイント { リモートエンドポイント = <&csi1_mipi_ep>; }; }; }; / { dayCam_step1: camPowerEnable { compatible = "レギュレータ固定"; レギュレータ名 = "dayCam-Power-Enable"; gpio = <&gpio_expander 5 GPIO_ACTIVE_HIGH>; アクティブハイを有効にする; レギュレータ常時オン; }; dayCam_step2: dayCamI2cEnable { compatible = "レギュレータ固定"; レギュレータ名 = "dayCam-i2c-Power-Enable"; vin-supply = <&dayCam_step1>; gpio = <&gpio4 26 GPIO_ACTIVE_HIGH>; アクティブハイを有効にする; レギュレータ常時オン; // startup-delay-us = <2600000>; // 100ms待つ }; }; ご協力やアイデアをいただければ大変助かります。
View full article
S32K3xx UART Baud Rate Tolerance We are using an S32K310 with an external 16MHz crystal. Crystal is feeding the PLL for 120MHz out to CORE_CLK. The AIPS_PLAT_CLK is running at 60MHz. I'm trying to determine how much tolerance the UART (for LIN) baud rate will have from this arrangement. I have 50ppm of error from the crystal. I need to add jitter from the PLL to get full tolerance of the 60MHz AIP_PLAT_CLK. How do we include jitter in this AIPS_PLAT_CLK tolerance?  From there, do I use the equation below to find a baud rate tolerance % for my UART? I see in the UART section of the S32K3xx RM how to calculate baud error using SBR and OSR values. Would I simply use this equation for both Fmin / Fmax of the module clock to find my min / max baud rate?   Re: S32K3xx UART Baud Rate Tolerance Hi @jmnemer, 1. The formulas in 77.3.1 should be used to calculate actual baud rate, and chapter 77.3.3 should be used to estimate tolerance to baud rate mismatch. SLOW refers to when the receiver is slower than the transmitter and FAST refers to the opposite. 2. This 840ps represents the worst-case (max) jitter value. I think it is better to use the RMS value, rather than pk-pk jitter value, unless you are designing for the absolute worst-case scenario. The RMS jitter value can be calculated as such (with +/- 7 sigma considered): 840ps/14 = 60ps.  Now, the clock at 120MHz gives a period of 8.333ns or 8333ps; meaning the jitter % can be calculated: 60ps/8333ps = 0.72%. Adding the 50ppm tolerance (0.005%, or in your case, calculated 0.0068) gives us of 0.7268% of total tolerance, which can be used to calculate Fmin and Fmax for the AIPS_PLAT_CLK (60 MHz). However, I don't know if this can be considered as the PLL overall tolerance, so I'm going to raise a support ticket to the SW to confirm this. I will get back with a response as soon as I get some information from the internal team. Best regards, Julián Re: S32K3xx UART Baud Rate Tolerance Hello Julián,  Thank you for your support! I do have a few follow up questions: 1. When are the equations in 77.3.1 vs 77.3.3 expected to be used? I get quite a different value when I calculate using all 3 equations. What is significance of FAST vs SLOW?  2. How do you properly add the PLL jitter into the AIPS_PLAT_CLK tolerance? I see in the S32K3xx DS that for integer mode at 120MHz we have 353ps cycle jitter and 840ps accumulated jitter. DS states that these figures are 7sigma from RMS. How do I use these to find my actual Fmin / Fmax. I have the crystal's ~50ppm calculated to about +/-0.0068%. How do I add the jitter into this? If I simply add/subtract the 840ps to the period, I end up with poor tolerance error (> 10%). That doesn't seem correct to me. Are we expected to use the RMS value on this parameter?  Thanks! Re: S32K3xx UART Baud Rate Tolerance Hi @jmnemer, Yes. I believe your implementation is correct. Since chapter 77.3.2 & 77.3.3 does not include clock uncertainty or jitter from the clock source, you can use the baud rate formula with Fmin and Fmax values to determine the range of your baud rate, and from that, calculate the baud error %. You must estimate the total frequency variation of the clock with crystal tolerance + PLL jitter. However, keep in mind that in the LIN driver, calculations are performed automatically assuming a fixed OSR = 16U by default. Best regards, Julián
View full article
S32K3xx UART 波特率公差 我们使用的是带有外置 16MHz 晶振的 S32K310。晶体为 PLL 供电,120MHz 输出至 CORE_CLK。AIPS_PLAT_CLK 的运行频率为 60MHz。我正试图确定 UART(用于 LIN)波特率对这种安排的容差有多大。晶体的误差为 50ppm。我需要增加 PLL 的抖动,以获得 60MHz AIP_PLAT_CLK 的完全容差。如何将抖动纳入 AIPS_PLAT_CLK 容差? 在此基础上,我是否要使用下面的公式找出 UART 的波特率容差% ?我在 S32K3xx RM 的 UART 部分看到如何使用 SBR 和 OSR 值计算波特误差。我是否只需将此公式用于模块时钟的 Fmin / Fmax,就能找到最小/最大波特率? Re: S32K3xx UART Baud Rate Tolerance 嗨,@jmnemer、 1.应使用77.3.1中的公式计算实际波特率,并使用77.3.3章估算波特率不匹配的容差。慢速是指接收机比发射器慢时,FAST 指的是相反的情况。 2.840ps 代表最坏情况下的最大抖动值。我认为最好使用有效值,而不是 pk-pk 抖动值,除非您在设计时考虑到绝对最坏的情况。 均方根抖动值可以这样计算(考虑 +/- 7 sigma):840ps/14 = 60ps。 现在,120MHz 的时钟周期为 8.333ns 或 8333ps,这意味着可以计算出抖动% :60ps/8333ps = 0.72% 。 加上 50ppm 的公差(0.005% ,或在您的情况下计算出的 0.0068),我们就得到了 0.7268% 的总公差,可用来计算 AIPS_PLAT_CLK (60 MHz) 的 Fmin 和 Fmax。 不过,我不知道这是否可以被视为 PLL 的总体容差,所以我打算向 SW 提出支持票据,以确认这一点。 一旦我从内部团队获得一些信息,我将尽快回复。 致以最诚挚的问候, Julián Re: S32K3xx UART Baud Rate Tolerance 你好,胡利安 、 感谢您的支持!我有几个后续问题: 1.77.3.1 与 77.3.3 中的公式预计何时使用?当我使用所有 3 个等式进行计算时,得到的数值大相径庭。快与慢的意义何在? 2.如何将 PLL 抖动正确加入 AIPS_PLAT_CLK 容差?我在 S32K3xx DS 中看到,在 120MHz 的整数模式下,周期抖动为 353ps,累积抖动为 840ps。DS 指出,这些数字与 RMS 相差 7sigma。如何使用这些数据来找到实际的 Fmin / Fmax?我计算出晶体的 ~50ppm 值约为 +/-0.0068% 。如何将抖动加入其中?如果我简单地将 840ps 加/减去周期,最终会产生较差的公差误差 (> 10%)。我觉得这不对。我们是否应该使用该参数的有效值? 谢谢您! Re: S32K3xx UART Baud Rate Tolerance 嗨,@jmnemer、 是的。我相信你的实施是正确的。由于第77.3.2 & 77.3.3章不包括来自时钟源的时钟不确定性或抖动,因此可以使用波特率公式中的 Fmin 和 Fmax 值来确定波特率范围,并由此计算波特误差% 。 您必须估算出晶体容差 + PLL 抖动的时钟总频率变化。不过,请记住,在 LIN 驱动程序中,计算是自动进行的,默认情况下假定固定 OSR = 16U。 致以最诚挚的问候, Julián
View full article
s32k3 uart 你好,亲爱的恩智浦团队...... ,我已经为 s32k311 配置了 UART0 中断接收......,我正试图在回调函数中接收数据,但我没有接收到任何数据。我不知道问题出在哪里....,请解决这个问题....,我已将我的项目上传到下面。 Re: s32k3 uart 你好,@leoCR7、 AsyncReceive 功能启用接收功能,并立即离开功能。 应用程序必须获取接收状态,才能知道接收何时完成。您可以反复调用 GetReceiveStatus 或使用中断回调函数,并在其中使用回调事件。接收完成后(已定义的接收字节数),您需要再次调用 AsyncreCeive 以开始新的接收。 不过,在回调内部,不要再次调用 AsyncReceive,而是使用 Lpuart_Uart_Ip_SetRxBuffer 函数进行连续接收。您可以在传输结束事件中使用 AsyncReceive。 您可以参考此示例例程:[RTD600 IP] S32K312-EVB Lpuart 中断回声 - NXP Community.它以 S32K312 为基础,但只需复制其配置即可。 致以最诚挚的问候, Julián
View full article
在 nxp s32k312 上遇到 HSE 固件问题 我们使用的是 NXP S32K312 MCU,目前在 HSE 固件方面遇到了问题: 1.HSE 状态寄存器值出现损坏 (0x4038C107)。 2.由于状态损坏,无法访问 HSE API。 3.尝试清除或重新刷新 HSE 固件失败。 4. 写入 MU0_TR1 寄存器或内存以触发擦除/RESET 命令不起作用。 5. 连接调试器后,观察到在一次外部 RESET 期间进行了多次软件 RESET。 请求援助: 1.请提供在 S32K312 上清除和重新刷新 HSE 固件的正确和推荐程序? 2.如果由于当前损坏状态而无法重新刷新 HSE 固件,可以采取哪些步骤恢复 HSE 或解决状态寄存器损坏问题? 3.在连接调试器的情况下进行硬 RESET 时观察到的多次 RESET 是否有任何已知问题或变通方法? 4.如何解决 HSE 状态寄存器损坏问题,并重新获得对 HSE API 的访问权限? 我们遵循了 HSE 固件闪存的流程。 第 1 步:我们刷新了提供的没有 IVT 的 PINK 文件以及演示应用程序和安全启动应用程序 ELF 文件。 第 2 步:RESET 完成第 3 步:观察到?在 HSE 位置 0x005d4000 和 DCM 寄存器处进行标记 第 4 步:我们在地址 0x00400000 处重新刷新了引导加载程序,在地址为 0x00442000 步骤5:在连接调试器的情况下执行硬 RESET 时,尽管只发出一个外部 RESET 命令,但我们观察到从软件端触发了多次 RESET 请查找屏幕截图以供参考 @lukaszadrapa请帮我解决这些问题 Re: Facing issues with HSE Firmware on nxp s32k312 这是不应该发生的。我有几个问题: 你们的 SBAF 是什么版本?您可以在 0x4039_C020 读取它。描述可以在 HSE FW 参考手册修订版的表 141 中找到。2.5. 您安装的是哪个版本的 HSE FW?是 AB_SWAP 还是 FULL_MEM 版本? 您使用了哪种安装方法?闪存中是否加载了任何应用程序?如果是,时钟是如何配置的? 请注意,一旦UTEST 中的 HSE 功能标志被编程,闪存中用于 HSE 固件的相应区域就会从内存映射中永久删除。如果删除了 HSE 固件,就无法再访问该区域。安装 AB_SWAP 版本时也是如此 - 在这种情况下,为 HSE 固件预留了两个区域,一个在活动块中,另一个在被动块中。安装 AB_SWAP 后,HSE OTA 标志被编程到 UTEST 中,因此这两个区域将永远保留给 HSE 固件。 Facing issues with HSE Firmware on nxp s32k312 您好, 我尝试在新的硬件平台上重新安装 HSE 固件。最初,HSE 状态寄存器正确设置了位 "0"(表示存在 HSE 固件)。但是,在执行功能RESET后,该位被清除,我无法再访问 HSE 固件——尽管分配给它的内存似乎完好无损。 能否请您澄清一下功能 RESET 后 HSE 状态寄存器的预期行为?此外,为确保 HSE 固件在 RESET 后仍可访问,推荐的 RESET 处理步骤有哪些? Re: Facing issues with HSE Firmware on nxp s32k312 HSE 固件参考手册可从此页面的 “文档-> 安全文件” 部分下载: https://www.nxp.com/products/S32K3#documentation 如果您看不到,可能需要申请访问权限: https://www.nxp.com/support/support/secure-access-rights:SEC-ACCESS 根据 MU FSR 寄存器(0x4038C107)的内容,HSE 固件不存在。这意味着您不能运行任何 HSE 服务。正如我在第一个回复中所写,请检查 0x4039_C028 的 HSE GPR 寄存器。如果第 0 位清零,则没有安装 HSE 固件。 安装固件有三种方法:默认位置、通过 IVT 或通过 MU。所有这些都在 HSE 固件参考手册中进行了描述。 此致, Lukas Re: Facing issues with HSE Firmware on nxp s32k312 你好、 感谢您的回复。 我目前无法擦除 HSE 固件。我尝试了之前建议的方法--将 0x57 写入 RAM 并使用 TR[1] 机制--但未能成功擦除内存。此外,HSE 固件 API 也未按预期响应或运行。如图所示,我遇到了重新安装 HSE 固件的问题。 你能否提供一种替代或更新的方法来强制删除或 RESET HSE 固件? 如何下载 HSE 固件参考手册 Re: Facing issues with HSE Firmware on nxp s32k312 你好, 感谢您的答复。 我目前无法清除 HSE 固件。我尝试了之前建议的方法--将 0x57 写入 RAM 并使用 TR[1] 机制--但没有成功擦除内存。此外,HSE 固件应用程序接口未按预期响应或运行。我遇到了重新安装 HSE 固件的问题。 你能否提供一种替代或更新的方法来强制删除或 RESET HSE 固件? Re: Facing issues with HSE Firmware on nxp s32k312 你好@Anitha7 这似乎是关键所在: " 步骤 1:我们刷新了提供的没有 IVT 的 PINK 文件以及演示应用程序和安全启动应用程序 ELF 文件。" 通过"默认应用程序 NVM 位置" (IVT 中没有定义指向粉色文件的指针)的安装方法仅在闪存中没有有效的 IVT 时有效。如果将粉色文件加载到 0x400000,并将其他具有有效 IVT 的应用程序加载到闪存,则无法安装 HSE 固件。 根据您的截图,0x1B00_0000 位置的 HSE 功能标志已被编程,因为 0x5D_4000 位置的区域为 HSE 固件预留。最简单的解决方案是擦除整个闪存(包括数据闪存),只加载 0x40_0000 位置的粉色文件。RESET 设备,将安装 HSE 固件。 然后检查 HSE GRP 寄存器 0x4039_C028。如果第 0 位被设置,则安装了 HSE 固件。 此致, Lukas
View full article
S32K3xx UARTボーレート許容範囲 外部 16MHz 水晶を備えた S32K310 を使用しています。クリスタルは 120 MHz の PLL を CORE_CLK に供給しています。AIPS_PLAT_CLK は 60MHz で動作しています。この配置から、UART (LIN 用) ボー レートの許容範囲がどの程度になるかを判断しようとしています。水晶からの誤差は 50ppm です。60MHz AIP_PLAT_CLK の許容範囲を完全に得るには、PLL からジッターを追加する必要があります。この AIPS_PLAT_CLK 許容値にジッターを含めるにはどうすればよいでしょうか? そこから、以下の式を使用して UART のボーレート許容値 % を見つければよいのでしょうか?S32K3xx RM の UART セクションで、SBR と OSR 値を使用してボー エラーを計算する方法を確認します。最小/最大ボーレートを見つけるには、モジュール クロックの Fmin / Fmax の両方にこの式を使用するだけでよいのでしょうか? Re: S32K3xx UART Baud Rate Tolerance こんにちは@jmnemerさん、 1.実際のボー レートを計算するには77.3.1の式を使用し、ボー レートの不一致に対する許容範囲を見積もるには77.3.3章を使用する必要があります。SLOW はレシーバがトランスミッタより遅い場合を指し、 FAST はその逆の場合を指します。 2. この 840ps は最悪 CASE (最大) のジッタ値を表します。絶対的に最悪のCASEを想定して設計している場合を除き、pk-pk ジッター値ではなく RMS 値を使用する方が良いと思います。 RMS ジッタ値は次のようにCAN計算されます (+/- 7 シグマを考慮):840ps/14 = 60ps。 ここで、120MHz のクロックは 8.333ns または 8333ps の周期を示します。つまり、ジッター % は 60ps/8333ps = 0.72% と CAN 計算できます。 50ppm の許容誤差 (0.005%、またはこのCASE、計算された0.0068) を追加すると、合計許容誤差の 0.7268% が得られ、これを使用して AIPS_PLAT_CLK (60 MHz) の Fmin と Fmax を計算CAN。ただし、これが PLL 全体の許容範囲と見なせるかどうかはわかりませんので、これを確認するため、ソフトウェアにサポートチケットを発行します。 社内チームから情報が入り次第、返答させていただきます。 よろしくお願いします、 ジュリアン Re: S32K3xx UART Baud Rate Tolerance こんにちは、ジュリアン。 サポートありがとうございます!いくつか追加の質問があります。 1.77.3.1 と 77.3.3 の式はいつ使用される予定ですか?3 つの方程式すべてを使用して計算すると、まったく異なる値が得られます。FAST と SLOW の違いは何ですか? 2. PLL ジッターを AIPS_PLAT_CLK 許容値に適切に追加するにはどうすればよいですか?S32K3xx DS では、120MHz の整数モードで 353ps のサイクル ジッタと 840ps の累積ジッタがあることがわかります。DS は、これらの数値は RMS からの 7 シグマであると述べています。これらを使用して実際の Fmin / Fmax を見つけるにはどうすればよいですか。水晶の約 50 ppm を約 +/- 0.0068% と計算しました。これにジッターを追加するにはどうすればいいでしょうか?単純に 840 ps を周期に加算/減算すると、許容誤差が小さくなってしまいます (> 10%)。それは正しいとは思えません。このパラメータでは RMS 値を使用する必要があるのでしょうか? よろしくお願いします! Re: S32K3xx UART Baud Rate Tolerance こんにちは@jmnemerさん、 はい。あなたの実装は正しいと思います。77.3.2章と77.3.3章にはクロックの不確実性やクロック ソースからのジッターは含まれていないため、Fmin 値と Fmax 値を使用したボー レートの式を使用してボー レートの範囲を決定し、そこからボー エラー % を計算できます。 水晶の許容誤差 + PLL ジッタを考慮してクロックの合計周波数変動を見積もる必要があります。ただし、 LIN ドライバでは、デフォルトで OSR = 16U が固定であると想定して計算が自動的に実行されることに注意してください。 よろしくお願いします、 ジュリアン
View full article
MC9S12 MEMORY QUESTION I’m working with firmware designed for the MC9S12GC16CPBE and encountered usage of address 0x0F1C in control logic. I noticed this address isn’t documented in the datasheet or reference manual. Can anybody clarify if this is tied to the mask set 1M34C, or if there’s supplemental documentation available detailing special diagnostic or status registers for this variant? THANKS   Re: MC9S12 MEMORY QUESTION Hi,  the memory map says... After reset the map is: 0x0000–0x03FF: Register Space    ...... 1K Register Space mappable to any 2K Boundary 0x0C00–0x0FFF: 1K RAM          ...... 1K Bytes RAM Space mappable to any 2K Boundary So, your address is defined as RAM after reset by default. Best regards, Ladislav
View full article
S32DS_PPC_eqADCデモの質問 こんにちはチーム S32DS PA 2.1 を使用した MPC5777C eQADC デモについてお聞きしてもよろしいでしょうか? DS の例を使用しようとしましたが、ADC 変換トリガー中に「DEVASSERT」が表示されます。 SO、S32DS PA による MPC5777C eQADC プロジェクトの動作例を探したいと思います。 よろしくお願いします。 S32DS Re: Asking S32DS_PPC_eqADC demo こんにちは、ダン 以下を使用しましたが、説明には文言がほとんどありません。 ありがとう。 Re: Asking S32DS_PPC_eqADC demo こんにちは@Luke_Chun 、 どのMPC5777Cパッケージ バージョンを使用しましたか?例の Readme ファイルで詳細を確認しましたか? よろしくお願いいたします。 ダン
View full article
TJA1465 如何确定当前唤醒原因是特定帧唤醒? 我想请教专家,TJA1465 只配置了 WUF。执行特定帧唤醒时,如何确定当前的唤醒原因?我可以肯定 CW 位将设置为 1,但总线上还会发送其他消息,CW 也将设置为 1,这会造成干扰。是否有其他方法或寄存器来确定唤醒原因? Re: How can TJA1465 determine that the current wake-up cause is a specific frame wake-up 设置这两个唤醒区分是通过CPNC / PNCOK 提前设置的,他还有一个wake pin 是 local唤醒用的 The TJA1465 supports remote wake-up via a CAN wake-up pattern (WUP) or selective wake-up via a CAN wake-up frame (WUF). --- 所以就是有wake pin的唤醒,配置了CPNC / PNCOK那就是被选择唤醒,不配置CPNC / PNCOK被唤醒就是WUP唤醒,解释清楚了吗? Re: How can TJA1465 determine that the current wake-up cause is a specific frame wake-up 非常感谢你的回答。也许我没有描述清楚。我已经实现了特定帧唤醒 (WUF)。当 ECU 被唤醒时,我想知道是否有办法通过寄存器设置或其他方法来确定唤醒的原因是由于该特定帧,因为整个网络中还有其他唤醒源需要加以区分 Re: How can TJA1465 determine that the current wake-up cause is a specific frame wake-up 这两个唤醒还是有本质区别的看下面的介绍,以及唤醒之前的设置: CAN wake-up pattern (WUP) The CAN wake-up pattern (WUP) is used for two purposes: To activate CAN biasing in CAN Offline mode (transition from CAN offline to CAN OfflineBias) To trigger a CAN wake-up event The following conditions must be met to trigger a wake-up event via a CAN WUP: The CAN transceiver is in CAN Offline or CAN OfflineBias mode CAN wake-up enabled (CWE = 1) CAN wake-up frame detection (WUF) deactivated (CPNC = 0 or PNCOK = 0)   CAN wake-up frame (WUF) CAN partial networking through selective wake-up detection allows a device in a CAN network to be selectively woken up in response to a wake-up frame (WUF) on the CAN bus. Selective wake-up detection uses one of two filtering methods: Identifier-only filtering (PNDM = 0) Identifier + data length code + data mask filtering (PNDM = 1) The following conditions must be met to enable CAN WUF functionality: CAN biasing needs to be activated (CAN OfflineBias, CAN ListenOnly or CAN Active mode) CAN wake-up enabled (CWE = 1) CAN partial networking configuration completed (PNCOK = 1) CAN partial networking enabled (CPNC = 1) No CAN partial networking error detected (CPNERRS = 0)
View full article
No Serial Output from Example Apps in Matter Hi, I’m working with the FRDM-MCXW71 board and trying to run the Matter examples based on NXP's GitHub repo, like light-switch-combo-app, Lock-app, contact-sensor-app. I've carefully followed all the setup steps from the READ.md. I have flashed the latest NBU .sb3 image to the CM3 core using blhost and .srec file to the CM33 core using J-Link. Everything including power, USB connections, serial settings are checked, they are all fine. Despite all that, my serial monitor shows no output at all. It just sits there quietly even I pressed all the switches once. Besides, the LED 2 isn't blinking also. To rule out hardware issues, I’ve also flashed a simple Hello World demo and LED blinky demo, and it prints correctly to serial, so UART is definitely working, LEDs are all fine also. Has anyone run into the same issue? Any suggestions would be massively appreciated! Thanks! FRDM-Training Protocol: Matter Re: No Serial Output from Example Apps in Matter Thank you so much for your support! I’ve tried the latest version, and I successfully run the program on the MCXW71 board now, and everything seems to be working as expected. In addition, I was following the example in the following links originally: https://github.com/nxp-appcodehub/ap-frdm-mcxw71-light-switch-combo-app/tree/main/examples/light-switch-combo-app/nxp/mcxw71 and https://github.com/NXP/matter/tree/release/v1.4.0/examples/light-switch-combo-app/nxp/mcxw71 Re: No Serial Output from Example Apps in Matter Hello. Can you please provide a link to the exact NXP Matter Github release you are using? The default branch is release/v1.4.0. One of our latest releases is v1.4.0.2: https://github.com/NXP/matter/tree/v1.4.0.2/examples/contact-sensor-app/nxp Can you please try with this one? Until we can reproduce on our side, one thing you can do is try to debug the issue using VS Code. Details about how to setup the environment can be found in the release notes in the Development Tools section: https://github.com/NXP/matter/releases/tag/v1.4.0.2 BR, Mihai
View full article
如何在 imx8mplus 上连接两台 PCIe 设备? 您好, 我是 PICe 的新手,正在研究 imx8mplus。我需要在 PCIe 上连接 Muarata 无线模块和 Hailo8 模块。如何将这两个接口都与单个可用的 PCIe 接口连接起来? 请大家帮忙! i.MX 8 系列 | i.MX 8QuadMax (8QM) | 8QuadPlus i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: How to connect two PCIe devices on imx8mplus? 嗨,@vivek338! 感谢您联系恩智浦支持中心! 遗憾的是,我们不支持您想要的配置。不过,您可以考虑使用 SDIO 接口连接 Wi-Fi 模块,以替代 PCIe。 致以最崇高的敬意, Chavira
View full article
IMX8M Mini 上的 MIPI-CSI 媒体管道无法工作 队员们好 在尝试配置媒体管道时,我一生都无法让 /dev/media0 节点出现在用户空间中。我正在自定义集成板上使用 Compulab IMX8M Mini SOM,我们的用例是 YOCTO 版本。我正在尝试将 Allied Vision 摄像机与他们的 Alvium CSI2 驱动程序集成。 一个主要的基线问题:如果内核和设备树安装正确,如果管道配置正确,/dev/media0 节点仍会显示吗?还是需要加载驱动程序才能成功启动管道?因为无论如何,我都无法让 media0 节点显示出来。 在启动时,由于某些板设置,相机尚未准备就绪。一旦进入用户空间,我(在电源调节器设置完毕、摄像机准备就绪后)就会将驱动程序重新绑定到该输出: root@b2qt-imx8mm-lpddr4-evk:/usr/share/BoardSetup-scripts# ./RebindCamera.sh 重新绑定 AVT 摄像机驱动程序... ./RebindCamera.sh:第 7 行:echo:写入错误:没有这样的设备 [43.335322] avt_csi2 0-003c:avt_probe [5107]:/usr/src/debug/avt-csi2/1.2.0+git/avt-csi2.c [43.344799] avt_csi2 0-003c:avt_probe [5147]:未定义关机-gpios [43.351676] avt_csi2 0-003c:avt_probe [5164]:devm_gpiod_get_optional (dev," reset-gpios " 成功 [43.360713] avt_csi2 0-003c:avt_gpios 成功 [43.360713] avt_csi2 0-003c:avt_gpios 成功 [43.360713] avt_csi2 0-003probe [5171]:fwnode_probe_present 找不到 mipi_csi [43.369373] avt_csi2 0-003c:avt_probe [5188]:找不到 bcrm_wait_timeout,使用默认值 [43.377842] avt_csi2 0-003c:avt_probe [5191]:bcrm_wait_timeout 设置为 3000ms [43.385046] avt_csi2 0-003c: avt_csi2_check_mipicfg [4586]:ep_cfg.bus.mipi_csi2.num_data_lanes1 [ 43.393965] avt_csi2 0-003c: avt_csi2_check_mipicfg[4588]: v4l2_fwnode_ep.nr_of_link_frequencies2 [ 43.402965] avt_csi2 0-003c: avt_csi2_check_mipicfg[4593]: v4l2_fwnode_ep.link-frequencies0 值 445500000 [43.412824] avt_csi2 0-003c:avt_csi2_check_mipicfg [4593]:v4l2_fwnode_ep.link-fwlink-frequencys 1 值 891000000 [43.42688] avt_csi2 0-003c:avt_probe [5213]:未定义断电-gpios 关机 [43.42688] 30332] avt_csi2 0-003c:avt_probe [5228]:未定义RESET gpios [43.436726] avt_csi2 0-003c:avt_reset [2080] [43.443043] avt_csi2 0-003c:等待摄像机关闭... [44.648643] avt_csi2 0-003c:wait_camera_available [2033]:等待摄像机响应 I2C 传输... [45.269281] kauditd_printk_skb:已抑制 15 个回调 [45.269292] 审计:type=1334 audit (1723754849. 880:26):prog-id=21 op=UNLOAD [ 46.664540] avt_csi2 0-003c: wait_camera_available[2054]:支持心跳,等待心跳激活 [ 49.878985] avt_csi2 0-003c: wait_camera_available[2064]:心跳激活 [ 49.949573] avt_csi2 0-003c: read_cci_registers[748]: regmap_bulk_read(camera->regmap8, cci_cmd_tbl[CCI_REGISTER_LAYOUT_VERSION ]。address ret 540 [ 49.969505] avt_csi2 0-003c: cci layout version b: 0x00000100 [ 49.975362] avt_csi2 0-003c: cci layout version a:0x00010000 [ 49.981170] avt_csi2 0-003c: avt_probe[5285]: read_cci_registers succeeded [ 49.989267] avt_csi2 0-003c: avt_probe[5302]: bcrm_version_check succeeded [ 49.996951] avt_csi2 0-003c: bcrm_get_write_handshake_availibility[704]:支持 BCRM 写握手! [49.996975] avt_csi2 0-003c:找到相机 ALVIUM 1500 c-501c NIR [50.014014] avt_csi2 0-003c:avt_probe [5315]:固件版本:0.6.0.8c98 ret = 0 [50.024773] avt_csi2 0-003c:正确的 gcprm 版本 [50.029887] avt_csi2 0-003c:正确的 gcprm 版本 [50.029887] avt_csi7 si2 0-003c:avt_probe [5353]:INIT_WORK(& camera-> bcrm_wrhs_work,bcrm_wrhs_work_func); [50.046953] avt_csi2 0-003c:avt_get_sensor_capabilities [4409]:CSI 时钟 [50.046953] 摄像机范围:40000000:750000000 Hz [50.046953] dts nr_of_link_ 频率 2 [50.046953] dts link_frequencys [0] 445500000 Hz [50.103673] avt_csi2 0-003c:avt_get_sensor_capabilities [4450]:从摄像机读取 csi 时钟:443750000 Hz [50.113207] avt_csi2 0-003c:获取最小和最大分辨率 [4454] [50.128752] avt_csi2 0-003c:avt_init_avail_formats [1840]:将 MEDIA_BUS_FMT_UYVY8_2X8/V4L2_PIX_FMT_UYVY/MIPI_CSI2_DT_YUV422_8B 添加到可用格式列表 -1 [50.152546] avt_csi2 0-0046 3c:avt_init_avail_formats [1841]:添加 MEDIA_BUS_FMT_UYVY8_1X16/V4L2_PIX_FMT_ UYVY/MIPI_CSI2_DT_YUV422_8 B 到可用格式列表 -1 [50.167322] avt_csi2 0-003c:avt_init_avail_formats [1842]:添加 MEDIA_BUS_FMT_FMT_1842P/MIPI_CSI2_DT_1X16/V4L2_PIX_FMT_YUV422P/MIPI_CSI2_DT__YUV42 2_8B 到可用格式列表 -1 [50.182333] avt_csi2 0-003c:avt_init_avail_formats [1843]:将 MEDIA_BUS_FMT_YUYV8_2X8/V4L2_PIX_FMT_YUYV_MIPI_CSI2_DT_YUV422_8B 添加到可用格式列表中 -1 [50.197003] avt_csi2 0-003c:avt_init_avail_formats [1844]:将 MEDIA_BUS_FMT_VYUY8_2X8/V4L2_PIX_FMT_VYUY/MIPI_CSI2_DT_YUV 422_8B 添加到 可用格式列表 -1 [50.211670] avt_csi2 0-003c:avt_init_avail_formats [1849]:将 MEDIA_BUS_FMT_RGB888_1X24/V4L2_PIX_FMT_RGB24/MIPI_CSI2_DT_RGB888 添加到可用格式列表 -1 [50.226343] avt_v4L2_PIX_FMT_RGB24/MIPI_CSI2_DT_RGB888 csi2 0-003c:avt_init_avail_formats [1850]:添加 MEDIA_BUS_FMT_RBG888_ 1X24/ V4L2_PIX_FMT_RGB24/MIPI_CSI2_DT_RGB888 到可用格式列表 -1 [50.241008] avt_csi2 0-003c:avt_init_avail_formats [1851]:添加 MEDIA_BUS_FMT_BGR888_1X24/V4L2_PIX_FMT_RGB24/MIPI_CMT_RGB24/MIPI_CMT_RGB24/MIPI_CMT_RGB24/MIPI_CMT SI2_DT_RGB888 到可用格式列表 -1 [50.255682] avt_csi2 0-003c:avt_init_avail_formats [1852]:将 MEDIA_BUS_FMT_RGB888_3X8/V4L2_PIX_FMT_RGB24/MIPI_CSI2_DT_RGB888 添加到可用格式列表中 -1 [50.270271] avt_csi2 0-003c:avt_init_avail_formats [1856]:添加 MEDIA_BUS _FMT_SGRBG8_1X8/V4L2_PIX_FMT_SGRBG8/MIPI_CSI2_DT_RAW8 可用格式列表 1-1 [50.284685] avt_csi2 0-003c:avt_init_avail_formats [1863]:将 MEDIA_BUS_FMT_SGRBG10_1X10/V4L2_PIX_FMT_SGRBG10/MIPI_CSI2_DT_RAW 10 添加到可用格式列表 1-1 [50.320636] t_csi2 0-003c:avt_init_controls [3359]:相机不支持控制对比度 (0x980901) [50.357183] avt_csi2 0-003c:avt_init_csi2 [3359]:相机不支持控制清晰度 (0x98091b) [50.367712] avt_csi2 0-003c:avt_update_sw_ctrl_state [2840]:找不到软件触发器控件! [50.369213] avt_csi2 0-003c:avt_update_sw_ctrl_state [2840]:找不到软件触发信号控件! [50.378025] avt_csi2 0-003c:avt_update_sw_ctrl_state [2840]:找不到软件触发信号控件! [ 50.412857] mxc_mipi-csi 32e30000.mipi_csi:已注册传感器子设备: avt_csi2 0-003c [ 50.429900] avt_csi2 0-003c: 摄像头 avt_csi2 0-003c 已注册 [ 50.435940] avt_csi2 0-003c: -> avt_probe[5420]: sysfs 组已创建!(0) [50.446676] avt_csi2 0-003c:avt_probe [5442]:探测成功! [50.378025] avt_csi2 0-003c:avt_update_sw_ctrl_state [2840]:找不到软件触发信号控件! [ 50.412857] mxc_mipi-csi 32e30000.mipi_csi:已注册传感器子设备: avt_csi2 0-003c [ 50.429900] avt_csi2 0-003c: 摄像头 avt_csi2 0-003c 已注册 [ 50.435940] avt_csi2 0-003c: -> avt_probe[5420]: sysfs 组已创建!(0) [ 50.446676] avt_csi2 0-003c: avt_probe[5442]: 探测成功 ! root@b2qt-imx8mm-lpddr4-evk:/usr/share/BoardSetup-scripts# 此时我假设摄像机已经安装好可以直播了,但我无法将任何帧或数据传入用户空间。我使用了所附的 TestStream.sh 脚本: root@b2qt-imx8mm-lpddr4-evk:/usr/share/BoardSetup-scripts# ./TestStream.sh ./TestStream.sh:第 1 行:amera:未找到命令 === 摄像机直播控制 == = 1.查看当前摄像机状态: [76.502724] avt_csi2 0-003c:avt_core_ops_s_power [2156] +:在 1 上,摄像头-> power_count 0 格式视频捕获:[76.511315] mxc_mipi-csi 32e30000.mipi_csi: 格式不匹配 宽度/高度:0/0 [76.519017] avt_csi2 0-003c:avt_core_ops_power [2156] +:开启 0,摄像头-> power_count 1 像素格式:” 字 段:每行任意 字节:0 大小图片:0 颜色空间:默认 T ra [76.537857] avt_csi2 0-003c:avt_core_ops_power [2t_csi2 0-003c:avt_core_ops_power [2t_csi_power [2core_ops_power [2core_ops_power] 156] +:在 1 上,摄像头-> power_count 0 nsfer 函数:默认(映射到 [76.548706] avt_csi2 0-003c:avt_core_ops_power [2156] +:开启 0,摄像头-> power_count 1 Rec. 709) YCbCr/HSV 编码:默认(映射到 ITU-R 601) 量化 :默认(映射到全范围) 标志 : 2.List available co[ 76.570719] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 1, camera->power_count 0 ntrols: 3.列出可用表格[ 76.581151] mxc_mipi-csi 32e30000.mipi_csi:格式不匹配 ats: ioctl:VIDIOC_ENUM_FMT T y [76.589396] avt_csi2 0-003c:avt_core_ops_s_power [2156] +:开启 0,摄像头-> power_count 1 pe:视频捕获 4.设置基本格式: [ 76.611180] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 1, camera->power_count 0 [ 76.619262] mxc_mipi-csi 32e30000.mipi_csi:格式不匹配 像素格式'UYVY'无效[ 76.625042] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 0, camera->power_count 1 5.检查是否有流媒体控制: [ 76.647122] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 1, camera->power_count 0 [ 76.655283] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 0, camera->power_count 1 6.尝试启用流媒体(如果存在控制): [ 76.672441] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 1, camera->power_count 0 [ 76.682040] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 0, camera->power_count 1 未找到流媒体 V4L2 控制 [ 76.699454] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 1, camera->power_count 0 [ 76.708214] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 0, camera->power_count 1 未找到流媒体启用控件 7.尝试启动采集(AVT 专用): [ 76.724226] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 1, camera->power_count 0 [ 76.733618] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 0, camera->power_count 1 未找到采集启动控制。 8.检查曝光和增益(确保合理): [ 76.749702] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 1, camera->power_count 0 [ 76.759271] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 0, camera->power_count 1 无曝光控制 [ 76.775975] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 1, camera->power_count 0 [ 76.784748] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 0, camera->power_count 1 无增益控制 9.设置合理的曝光/增益(如果存在控制): [ 76.801835] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 1, camera->power_count 0 [ 76.810768] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 0, camera->power_count 1 无法设置曝光 [ 76.827415] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 1, camera->power_count 0 [ 76.837494] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 0, camera->power_count 1 无法设置增益 10。尝试在配置后捕获一帧: ./TestStream.sh:第 47 行:超时:未找到命令 ❌ 流式配置后仍无数据 11.检查流状态的内核信息: [ 76.784748] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 0, camera->power_count 1 [ 76.801835] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 1, camera->power_count 0 [ 76.810768] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 0, camera->power_count 1 [ 76.827415] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 1, camera->power_count 0 [ 76.837494] avt_csi2 0-003c: avt_core_ops_s_power[2156]+: on 0, camera->power_count 1 root@b2qt-imx8mm-lpddr4-evk:/usr/share/BoardSetup-scripts# 现在由于格式不匹配,我打算通过/dev/media0节点上的media-ctl对其进行RESET更改。但这并没有显示出来。 以下是 DTS 的核心相关部分。 //在 I2C 总线上定义你的摄像头 & i2c1 { /* * 在 I2C 地址 0x21 处定义 PCAL6416A GPIO 扩展器。 * 我们给它一个标签 “gpio_expander”,这样我们就可以参考它。 */ gpio_expander: pcal6416a@21 { compatible ="nxp,pcal6416"; reg =<0x21>; gpio-controller; #gpio-cells =<2>; }; alvium: alvium@3c { compatible ="alliedvision,avt_csi2"; reg =<0x3c>; status ="okay" ; pinctrl-names ="默认"; pinctrl-0 =<& pinctrl_alvium_clk>,<& pinctrl_alvium_gpio> ; //Atollo 日间摄像 机电源的特定硬件设置 = < & daycam_step2 >; reset-gpios = < & gpio1 15 GPIO_ACTIVE_LOW >; clocks =<& clk IMX8MM_CLK_CLKO1>; clock-names ="csi_mclk"; assigned-clocks =<& clk IMX8MM_CLK_CLKO1>; assigned-clock-parents =<& clk IMX8MM_CLK_24M>; assigned-clock-rate =<24000000> ; 端口 { reg =<0>; alvium_mipi_ep:端点 { remote-endpoint =<& mipi1_sensor_ep>; data-lanes =<2>; link-frequencies = /bits/ 64<445500000 891000000>; mipi-csi; }; }; }; }; &mipi_csi_1 { status ="okay" ; /delete-node/ 端口; 端口 { mipi1_sensor_ep:endpoint@1 { reg =<1>; remote-endpoint =<& alvium_mipi_ep>; data-lanes =<2>; csis-hs-settle =<13>; csis-clk-settle =<2>; csis-wclk; }; csi1_mipi_ep:endpoint@2 { reg =<2>; remote-endpoint =<& csi1_bridge_in>; }; }; }; &csi1_bridge { status ="okay"; fsl,mipi-mode; /delete-node/ 端口; 端口 { csi1_bridge_in:端点 { remote-endpoint =<& csi1_mipi_ep>; }; }; }; / { dayCam_step1: camPowerEnable { compatible ="regulator-fixed"; regulator-name ="dayCam-Power-Enable"; gpio =<& gpio_expander 5 GPIO_ACTIVE_HIGH>; enable-active-high; regulator-always-on; }; dayCam_step2:dayCamI2cEnable { compatible ="regulator-fixed"; regulator-name ="dayCam-i2c-Power-Enable"; vin-supply =<& dayCam_step1> ; gpio =<& gpio4 26 GPIO_ACTIVE_HIGH>; enable-active-high; regulator-always-on; // startup-delay-us =<2600000>; // Wait 100ms }; }; 如能提供帮助或想法,将不胜感激。
View full article
提问关于窗体图标的问题 lv_drivers\ display\ monitor.ccreate.comunitor.create_create中有一段代码 iconSurface = SDL_CreateRGBSurfaceFrom(simulator_icon, 32, 32, 16, 32 * 2, 0xf000, 0x0f00, 0x00f0, 0x000f); SDL_SetWindowIcon(m->window, iconSurface); SDL_FreeSurface(iconSurface); 它们的作用应该是显示sdl窗体的图标,但是整个软件找下来也没找到设置这个图标的地方,请问是否固化为 这个图标了?能否修改? 怎么修改? PS:我的工作是使用GuiGuider设计在图形化Linux下的可执行程序。 Re: 提问关于窗体图标的问题 Hello @空心菜 , 感谢您的帖子。这段代码确实是用于设置 SDL 窗口图标的,该图标是 GuiGuider 的默认 logo,相关图像数据已直接编写在源代码中。编译出来的软件不能修改。 软件源代码不提供,所以不支持用户进行修改。只是软件生成的应用代码在代码编辑里可以查看。 希望到帮到您。 BRs, Celeste
View full article
S32K146 - MBDT - 電源サイクル中のランタイム データの保存と保持。 NXPサポートチーム様 このメッセージがお役に立てば幸いです。 現在、S32K146 MCU を使用するプロジェクトに取り組んでおり、Simulink を使用して EEPROM 操作を処理しています。データ保持に関して解決できない問題がいくつか発生しましたので、ご指導いただければ幸いです。 私の設定では、「Flash_EEEWrite」ブロックを使用して EEPROM に値を保存しようとしています。繰り返しシーケンス ブロックから値を回転し、「Flash_Config」を初期化した後に書き込みます。適切な初期化を確実に行うために、書き込み操作を実行する前に 100 ミリ秒の遅延も追加しました。 しかし、電源を入れ直すと、書き込んだ値は保持されません。私が観察したことは次のとおりです。 FLASH_EEEWriteブロックのデータ型がuint32_tに設定されている場合、読み戻される値は常に7fff(Hex)になります。 uint8_t に設定すると、返される値は 82 (16 進数) になります。 これらの値は入力に関係なく一定であり、書き込んでいる値を反映しません。 問題が EEPROM の構成にあるか、Simulink ブロックの使用方法にあるか、あるいはこのコンテキストでの FLASH_EEEWrite ブロックの動作に関する誤解にあるかはわかりません。 セットアップをより明確に説明するために、作業中の Simulink モデルを添付しました。 何が問題なのかについての洞察や、電源サイクル全体で信頼性の高い EEPROM 書き込みと保持を確保するために実行する必要がある推奨手順について教えていただけますか? 皆様のお時間とサポートに心より感謝申し上げます。皆様からのご助力やご提案に心から感謝いたします。
View full article
Asking S32DS_PPC_eqADC demo Hello Team May I ask about the MPC5777C eQADC demo using S32DS PA 2.1? I tried to use the example of DS, it is showing "DEVASSERT" during ADC conversion trigger.  So I wish to seek the working example of MPC5777C eQADC project by S32DS PA. Thank you. S32DS Re: Asking S32DS_PPC_eqADC demo Hi Dan I used below and the description is showing few wording.. Thank you.  Re: Asking S32DS_PPC_eqADC demo Hello @Luke_Chun, What MPC5777C package version did you use? Did you check details in the Readme file of the example? Best regards, Dan
View full article