2141215_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2141215_en-US

2141215_en-US

MC9S12 MEMORY QUESTION

I’m working with firmware designed for the MC9S12GC16CPBE and encountered usage of address 0x0F1C in control logic. I noticed this address isn’t documented in the datasheet or reference manual. Can anybody clarify if this is tied to the mask set 1M34C, or if there’s supplemental documentation available detailing special diagnostic or status registers for this variant?

THANKS

 
Re: MC9S12 MEMORY QUESTION

Hi,

 the memory map says...

After reset the map is:
0x0000–0x03FF: Register Space    ...... 1K Register Space mappable to any 2K Boundary
0x0C00–0x0FFF: 1K RAM          ...... 1K Bytes RAM Space mappable to any 2K Boundary


So, your address is defined as RAM after reset by default.


Best regards,

Ladislav

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 06:19 PM
更新者: