Multi Source Translation Content

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multi Source Translation Content

讨论

排序依据:
Reading i.MX8MM register values with sdphost I am trying to find a way to read register values from a i.MX8MM over USB. The tool sdphost should be able to do it, but I am not able to get it to work and I cannot find sufficient instructions anywhere. For example, I want to try and read OCOTP_HW_OCOTP_BOOT_CFG0 which should be at memory address 3035_0470: ./sdphost -u 0x1fc9,0x0134 read-register 0x30350470 33 22 33 00 Status (HAB mode) = 305411090 (0x12343412) HAB enabled. But the bytes (33 22 33 00) are not correct. In fact, no matter what address I give sdphost, it always returns the same four bytes. I know the device is connected and in Serial Download Mode, because I can for example use uuu. What is the correct command to read register values with sdphost? Bonus question: is there any way to read registers with uuu? We already use uuu to flash the device and write fuses, it would be handy to use the same tool for reading registers as well. But I looked at sdphost because it did not seem to be possible with uuu. i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Re: Reading i.MX8MM register values with sdphost Is there any tool available for reading register values over USB? Re: Reading i.MX8MM register values with sdphost Hello, According to the documentation: Serial Download Protocol is a set of commands supported by NXP i.MX RT devices in the Boot ROM application’s serial download mode. I tried on our EVK and also is giving faulty readings. So, I think this tool is not intended to be used on i.MX families as is on i.MX RT families. Also, in the case of UUU, there is no documented a command to read registers on the board. Best regards.
查看全文
i.MX 8M Plus docker 无法正常工作“无效主机头” 你好, 对于我们的 i.MX 8M Plus EVK 板,我们从链接https://github.com/nxp-imx/meta-imx/tree/mickledore-6.1.55-2.2.0中的 mickledore 分支“mickledore-6.1.55-2.2.0”构建 yocto 源。 在 EVK 板上构建并刷新图像后,我们发现 docker 不起作用。以下命令如下。 root@imx8mpevk:~# uname -a Linux imx8mpevk 6.1.55+g770c5fe2c1d1#1 SMP PREEMPT 11 月 21 日星期二 23:45:58 UTC 2023 aarch64 GNU/Linux root@imx8mpevk:~# root@imx8mpevk:~# systemctl 启动docker root@imx8mpevk:~# root@imx8mpevk:~#docker pull hello-world 使用默认标签:最新 最新:从 library/hello-world 中提取 摘要:sha256:a26bff933ddc26d5cdf7faa98b4ae1e3ec20c4985e6f87ac0973052224d24302 状态:图像已针对 hello-world:latest 更新 docker.io/library/hello-world:latest root@imx8mpevk:~# root@imx8mpevk:~#docker运行hello-world http:无效的主机头 root@imx8mpevk:~# 另请参阅下面的 docker journalctl 日志。 root@imx8mpevk:~# journalctl -xefu docker 4月24日 12:23:20 imx8mpevk systemd[1]:正在启动 Docker 应用程序容器引擎... -- 主题:docker.service 单元的启动作业已开始执行 -- 定义者:systemd -- 支持: https://lists.freedesktop.org/mailman/listinfo/systemd-devel -- -- 单元 docker.service 的启动作业已开始执行。 -- -- 作业标识符为 1630。 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.465195235Z”level=info msg="正在启动" 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.471783509Z”level=info msg="[core] [Channel #1] 频道已创建" module=grpc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.471879134Z”level=info msg="[core] [通道#1] 原始拨号目标是:\"unix:///run/containerd/coc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.472032885Z”level=info msg="[core] [Channel #1] 解析的拨号目标是:{Scheme:unix Authority: Endpoc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.472097885Z”level=info msg="[core] [频道 #1] 频道权限设置为 \"localhost\"" module=grpc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.472945263Z”level=info msg="[核心] [通道 #1] 解析器状态已更新: {\n \"地址\": [\n {c 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.476382650Z”level=info msg="[core] [频道 #1] 频道切换到新的 LB 策略 \"pick_first\"" moc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.479532287Z”level=info msg="[core] [频道 #1 子频道 #2] 子频道已创建" module=grpc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.479762788Z”level=info msg="[core] [Channel #1 SubChannel #2] 子通道连接更改为 CONNc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.479931288Z”level=info msg="[core] [通道 #1 子通道 #2] 子通道选择一个新地址 \"/run/c 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.480056039Z”level=info msg="[core] [通道 #1] 通道连接状态更改为 CONNECTING" module=grc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.488533820Z”level=info msg="[core] [Channel #1 SubChannel #2] 子通道连接更改为 READc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.488714945Z”level=info msg="[core] [Channel #1] 通道连接更改为 READY" module=grpc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.496465474Z”level=info msg="[core] [Channel #4] 频道已创建" module=grpc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.496565849Z”level=info msg="[core] [通道#4] 原始拨号目标是:\"unix:///run/containerd/coc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.496669974Z”level=info msg="[core] [Channel #4] 解析的拨号目标是: {Scheme:unix Authority: Endpoc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.496746725Z”level=info msg="[core] [频道 #4] 频道权限设置为 \"localhost\"" module=grpc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.496911225Z”level=info msg="[核心] [通道 #4] 解析器状态已更新: {\n \"地址\": [\n {c 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.497074476Z”level=info msg="[core] [频道 #4] 频道切换到新的 LB 策略 \"pick_first\"" moc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.497270102Z”level=info msg="[core] [频道 #4 子频道 #5] 子频道已创建" module=grpc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.497479852Z”level=info msg="[core] [Channel #4 SubChannel #5] 子通道连接更改为 CONNc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.497737228Z”level=info msg="[core] [通道 #4 子通道 #5] 子通道选择一个新地址 \"/run/c 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.497770104Z”level=info msg="[core] [通道 #4] 通道连接更改为 CONNECTING" module=grc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.498877358Z”level=info msg="[core] [Channel #4 SubChannel #5] 子通道连接更改为 READc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.499128733Z”level=info msg="[core] [Channel #4] 通道连接更改为 READY" module=grpc 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.597137716Z”level=info msg="正在装载容器:开始。" 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.881553755Z”level=warning msg="无法加载 IPSEC 规则所需的模块:协议不支持" 4月24日 12:23:21 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:21.893731300Z”level=info msg="默认网桥(docker0)分配了IP地址172.17.0.0/16。D” 4月24日 12:23:22 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:22.029149067Z”level=info msg="装载容器:完成。" 4月24日 12:23:22 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:22.246174432Z”level=warning msg="警告:不支持 CPU CFS 配额" 4月24日 12:23:22 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:22.246261186Z”level=warning msg="警告:不支持 CPU CFS 周期" 4月24日 12:23:22 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:22.246296437Z”level=warning msg="警告:没有 blkio throttle.read_bps_device支持” 4月24日 12:23:22 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:22.246344064Z”level=warning msg="警告:没有 blkio throttle.write_bps_device支持” 4月24日 12:23:22 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:22.246379941Z”level=warning msg="警告:没有 blkio throttle.read_iops_device支持” 4月24日 12:23:22 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:22.246413692Z”level=warning msg="警告:没有 blkio throttle.write_iops_device支持” 4月24日 12:23:22 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:22.246501321Z”级别=信息消息=“Docker守护进程”提交=219f21bf07502b447095649b5a2764661737f164 graphdrive 4月24日 12:23:22 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:22.247150101Z”level=info msg="守护进程已完成初始化" 4月24日 12:23:22 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:22.323320938Z”level=info msg="[core] [Server #7] 服务器已创建" module=grpc 4 月 24 日 12:23:22 imx8mpevk systemd[1]:已启动 Docker 应用程序容器引擎。 -- 主题:docker.service 单元的启动作业已成功完成 -- 定义者:systemd -- 支持: https://lists.freedesktop.org/mailman/listinfo/systemd-devel -- -- 单元 docker.service 的启动作业已成功完成。 -- -- 作业标识符为 1630。 4月24日 12:23:22 imx8mpevk dockerd[1393]:时间=“2024-04-24T12:23:22.347791050Z”level=info msg="API 监听 /run/docker.sock" ^C root@imx8mpevk:~# 请分享您的意见 谢谢 回复:i.MX 8M Plus docker 无法正常工作“无效的主机头” 你好 降级 go 包后。docker 工作正常。 参考链接: https ://github.com/moby/moby/issues/46614#issuecomment-1757751921 谢谢
查看全文
How to use GUI Guider to generate bin file fonts? Hello, may I ask if you could help me: In GUI Guider,I found that only fonts can be generated as C files,Can you add an option to generate bin file fonts?  At present, BIN files can be generated on the LVGL official website, but when ported to the project generated by GUI Guider, there may be inconsistent font height display issues,May I ask if there is a solution. I hope to add a tool for generating bin file fonts in the next version! Thanks! Re: How to use GUI Guider to generate bin file fonts? Thanks for your answer. If this feature is implemented in future versions, I will be able to store the fonts binary like images binary in XIP FLASH and not have to update the binary every time when updating software code, which will greatly save program update time. Re: How to use GUI Guider to generate bin file fonts? Hi @White1, This is a great suggestion. I will share this idea internally with the GUI Guider team. In the end, it is up to them to see if this feature is worth implementing on future releases of GUI Guider, but I believe it would be a great addition to the tool! Thanks for your suggestions. BR, Edwin.
查看全文
如何使用GUI Guider生成bin文件字体? 你好, 请问您是否可以帮助我:在 GUI Guider 中,我发现只有字体可以生成为 C 文件,您能添加一个选项来生成 bin 文件字体吗? 目前在LVGL官网可以生成BIN文件,但是移植到GUI Guider生成的项目中可能会出现字体高度显示不一致的问题,请问有没有什么解决办法。 希望下个版本能增加生成bin文件字体的工具! 谢谢! 回复:如何使用 GUI Guider 生成 bin 文件字体? 谢谢你的回答。 如果在未来的版本中实现这个功能,我将能够将字体二进制文件像图像二进制文件一样存储在XIP FLASH中,而不必在每次更新软件代码时更新二进制文件,这将大大节省程序更新时间。
查看全文
K32L2A SWD 引脚 - 除非连接调试器,否则 MCU 无法正常运行 我有一个使用 K32L2A 的新设计,这是旧 Coldfirev1 MCF51QE32 部件的未分级设计。使用原型 PCB,软件在连接 PEMicro Cyclone 的情况下按预期运行,即使不使用该设备进行调试,只需启动设备,MCU 即可按预期运行我们的软件。 然而,当 Cyclone 与电路板断开连接时,MCU 似乎会短暂启动,然后自行关闭(不会按预期运行我们的软件,不确定它是否只是停止,或者是什么,因为我无法将 Cyclone 连接到调试,因为这会立即修复它!)。我们的设计在 SWDIO/SWCLK 线路上没有外部电阻,因为数据表提到这些电阻是由 K32L2A 内部提供的(MCF51QE 在 PCB 上有 10K 上拉电阻)。 尝试过的事情: - 在这两条线路上添加 10K 上拉电阻 - 问题仍然存在 - 将一根电线从 PCB 上取下,这样我就可以将导线接触到引脚,这样就可以解决问题,也就是说,当我用手指捏住连接到 SWDIO 引脚的导线并启动电路板时,MCU 可以正确启动并且我们的软件可以运行。它会一直运行,直到我移开手指。这与任一 SWD 引脚均可兼容。电容?我不知道!?! 在这些行上加一个小写字母似乎是一种黑客行为,显然我忽略了一些东西。 复位线上也没有外部电阻(疏忽)但这似乎不是问题,因为当我握住其中一个 SWD 引脚时 MCU 就会运行,而当我离开一个引脚时 MCU 就会失败。 想法、希望还是抱负?欢迎大家 🙂 干杯! 回复:K32L2A SWD 引脚 - 除非连接调试器,否则 MCU 无法正常运行 “在两条线路上都添加 10K 上拉电阻 - 问题仍然存在” SWD_DIO 具有内部上拉电阻。SWD_CLK 具有内部下拉。 猜测,重置时将两者都拉高可能看起来像是调试器时钟脉冲。手指等会拉下足够长的时间。 内部电阻相当高 Z 并且随温度而变化(20k 至 50k)。 我通常会添加自己的低 Z。 来自 K32L2A 的电气数据表: “虽然不需要上拉或下拉电阻 (SWD_DIO 具有内部上拉电阻,SWD_CLK 具有内部下拉电阻),建议使用外部 10 kΩ 上拉电阻以确保系统稳健性。这 还必须考虑上面提到的 RESET_b 引脚建议。”
查看全文
HID(W):LIBUSB_ERROR_PIPE ----i.mx9352 A1 Hi, We am using i.mx9352 A1 model. we are unable to port the BSP file due to some error is coming as given below ======================================================= Success 0 Failure 1 1:2 1/ 1 [HID(W):LIBUSB_ERROR_PIPE ] SDPS: boot -f imx-boot-imx93evk-sd.bin-flash_singleboot ============================================================================= Could you provide solution for that error Thanks, Vivek Re: HID(W):LIBUSB_ERROR_PIPE ----i.mx9352 A1 Hi @Binh_Hoang  Kindly check the voltage as per Table 29 of NXP hardware design guide and check  the VDD_SOC_0V8 at SOC end. Thanks Re: HID(W):LIBUSB_ERROR_PIPE ----i.mx9352 A1 Hi @vivek5676, I'm facing the same issue. Could you please let me know which change is needed for this case? Please give me more details.  Thank you in advance, Binh Re: HID(W):LIBUSB_ERROR_PIPE ----i.mx9352 A1 My problem get resolved after changes done in hardware.  
查看全文
i.MX8M Plus: IOMUX CTS/RTS directions are reversed Hello, We are having some issues related to the UART4 in a i.MX8M Plus After some investigation, it seems that the IOMUX CTS/RTS directions are reversed (in DCE and DTE mode). In the figure below: TX/RX in both cases are output/input and matches the diagram in the center-right. However, CTS/RTS in both cases are input/output but that doesn't match the diagram. Contrast this with the second image below based on a i.MX6. CTS/RTS are output/input as expected. Is this analysis correct? Where are we wrong? What can we do to correct this? Thank you. Best regards, Adriano Carvalho Re: i.MX8M Plus: IOMUX CTS/RTS directions are reversed Hello, It is an issue with the tool, is not showing the correct signals direction. Best regards. Re: i.MX8M Plus: IOMUX CTS/RTS directions are reversed Hello, Is this just an issue with the tool where it display "input" when it should display "output" and vice versa? Or are the dts files affected as well? Are the values in "imx8mp-pinfunc.h" correct? Best regards, Adriano Carvalho Re: i.MX8M Plus: IOMUX CTS/RTS directions are reversed Hello, This is an issue in the tool that is already reported, it will be fixed in next release. Best regards.
查看全文
K32L2A SWD ピン - デバッガが接続されていないと MCU が正常に動作しない 私はK32L2Aを使用して新しいデザインを持っています、古いColdfirev1 MCF51QE32パーツからの未評価のデザイン。プロトタイプのPCBでは、デバッグにデバイスを使用していないときでも、PEMicro Cycloneを接続した状態でソフトウェアが期待どおりに動作し、電源を入れるだけで、MCUが期待どおりにソフトウェアを実行します。 ただし、Cycloneがボードから切断されると、MCUは非常に短時間起動し、その後自動的に動作するように見えます(ソフトウェアが期待どおりに実行されず、単に停止するのか、それともデバッグ用にCycloneをアタッチできないため、すぐに修正されるため、ソフトウェアが停止するのかわかりません)。この設計では、SWDIO/SWCLK ラインに外部抵抗はありませんが、データシートには K32L2A によって内部で供給されていると記載されています (MCF51QE、これらの PCB には 10K のプルアップがありました)。 試したこと: - これらのラインに10Kプルアップを追加する - 問題は残っています - PCBからワイヤーを離してリード線をピンに触れると、SWDIOピンに接続されているリード線を指で挟んでボードの電源を入れると、MCUが正しく起動し、ソフトウェアが実行されます。指を離すまで走り続けます。これは、どちらの SWD ピンでも機能しました。静電容量。わからない!。! これらの行に小さなキャップを付けることはハックのように思えますが、明らかに私は何かを見落としています。 リセットラインにも外部抵抗はありません(見落とし)が、MCUはSWDピンのいずれかを保持した状態で動作し、1つのピンを離すとすぐに故障するため、これは問題ではないようです。 考え、希望、それとも憂慮?どなたでも大歓迎です 🙂よろしくお願いします。 日時: K32L2A SWD ピン - デバッガーが接続されていないと MCU が正常に動作しない 「これらの両方のラインに10Kプルアップを追加すると、問題は残ります」 SWD_DIOには内部プルアップがあります。SWD_CLKには内部プルダウンがあります。 リセット時に両方をプルアップすると、おそらく推測としてデバッガーのクロックパルスのように見えます。指などは十分に長く引き下げられます。 内部抵抗器はかなり高インピーダンスで、温度(20k〜50k)によって異なります。 私は通常、lower-Zの自分のものを追加します。 K32L2Aの電気データシートから: 「プルアップまたはプルダウン抵抗は必要ありませんが (SWD_DIOには内部プルアップがあり、SWD_CLKには内部プルダウンがあります)、システムの堅牢性のために外部10kΩプル抵抗が推奨されます。ザ 上記のRESET_bピンの推奨事項も考慮する必要があります。」
查看全文
K32L2A SWD pins - MCU fails to run properly unless debugger is attached I have a new design using the K32L2A, ungraded design from old Coldfirev1 MCF51QE32 part. With the prototype PCB, software runs as expected with a PEMicro Cyclone connected, even when not using the device for debug, just powering things up and the MCU runs our software as expected.  However, when the Cyclone is disconnected from the board, the MCU seems to start very briefly then go off on it's own (does not run our software as expected, unsure if it simply stops, or what, since I cannot attached the Cyclone to debug, as that immediately fixes it!). Our design has no external resistors on the SWDIO/SWCLK lines, as the datasheet mentioned these are provided internally by the K32L2A (MCF51QE had 10K pullups on the PCB for these).  Things tried: - Adding 10K pullup to both these lines - problem remains - Putting a wire off the PCB so I could touch the lead to the pins DOES FIX IT, that is, it I pinch the lead connected to the SWDIO pin between my fingers and power up the board, the MCU starts correctly and our software runs. It continues to run until I remove my fingers. This worked with either SWD pin. Capacitance? I dunno!?!  Putting a small cap on these lines seems like a hack, clearly I am overlooking something. No external Resistor on the Reset line either (an oversight) but this didn't seem to be the problem, as the MCU runs with me holding either one of the SWD pins, and fails as soon as I left go of the one pin. Thoughts, hope or asperations? All are welcome 🙂 Cheers! Re: K32L2A SWD pins - MCU fails to run properly unless debugger is attached Hi, As you know that the K32L2 has flash configuration area, after the chip starts up, the core will copy the data in flash configuration area to the FTFA_FOPT register automatically. The PTA4 is multiplexed with PTA4, pls connect PTA4 to a pull-up resistor. Secondly, pls clear NMI_DIS bit in the FTFA_FOPT register. In the case, NMI_b pin will not fire interrupt. Hope it can help you BR XiangJun Rong Re: K32L2A SWD pins - MCU fails to run properly unless debugger is attached "Adding 10K pullup to both these lines - problem remains" SWD_DIO has internal Pull-Up. SWD_CLK has internal Pull-Down. Pulling both up at reset probably looks like a debugger clock pulse as a guess. Fingers and such would pull down long enough. The internal resisters are rather high-Z and vary with temperature (20k to 50k). I usually add my own of lower-Z. From the electrical data sheet for the K32L2A: "While pull-up or pull-down resistors are not required (SWD_DIO has an internal pull-up and SWD_CLK has an internal pull-down), external 10 kΩ pull resistors are recommended for system robustness. The RESET_b pin recommendations mentioned above must also be considered."
查看全文
将 S32K144 项目从 ARM 的 S32 设计工作室迁移到 S32 平台的 S32 设计工作室 您好,NXP团队: 我们从 NXP 网站上获得了 MC33771C 和 MC33772C 的 BCC SW 驱动程序包。 我们正在尝试将这些示例项目迁移到 S32 平台的 S32 设计工作室(版本:3.5)。 我们按照以下链接中的迁移程序进行操作: https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/Video-Migrating-S32K1-projects-from-S32DS-for-ARM-and-SDK-3-0-x/ta-p/1296239 。 但是,代码没有正确迁移,我们无法确定原因。 请帮助我解决这个问题。 顺祝商祺! 哈里什 回复:将 S32K144 项目从 ARM 的 S32 设计工作室迁移到 S32 平台的 S32 设计工作室 你好@Hareesh 恐怕 S32DS v3.5 的迁移功能不如 S32DS v3.4 那样全面。我们建议迁移到 S32DS v3.4。 我会将这个问题告知相应的团队。带来不便敬请谅解。 回复:将 S32K144 项目从 ARM 的 S32 设计工作室迁移到 S32 平台的 S32 设计工作室 你好@Hareesh 正如我在之前的回复中提到的。所采取的步骤与所分享的视频中提供的步骤相同。完成代码迁移步骤后,出现的错误与库包含有关,可以使用我上一篇文章中提供的信息来解决。
查看全文
hantro_VC8000E_enc源代码 NXP技术支持您好 感谢一直以来的帮助和支持。 最近在i.MX8MP开发中,发现连续开关视频压缩,会有一定概率异常停止,经过跟踪调查发现,问题出在imx-gst1.0-plugin的VPUENC插件中,再进一步调查发现,问题可能出现在libhantro_vc8000e.so里面,但是因为工程中没有源代码,只有这个.so文件以及.h文件,无法进一步调查,所以想知道是否有libhantro_vc8000e.so的源代码,如果有,是否可以提供参考一下? feiyu Re: hantro_VC8000E_enc源代码 VC8000e 有许可限制,所有源代码都放入私人仓库( https://bitbucket.sw.nxp.com/projects/IMXPRIV/repos/imx-vpu-hantro-vc/ )。 也许你可以参考下面的链接 https://bitbucket.sw.nxp.com/projects/MMCSH/repos/imx-vpu-hantro-daemon/browse/v4l2_vsi_daemon/src/vsi_enc_video_h2.c https://bitbucket.sw.nxp.com/projects/MMCSH/repos/vpu_wrapper/browse/vpu_wrapper_hantro_VCencoder.c Re: hantro_VC8000E_enc源代码 你好,joanxie: 无法访问您提供的网站。还有其他网站吗?或者是否可以直接将代码作为附件添加? 飞宇 Re: hantro_VC8000E_enc源代码 你好,joanxie: 非常感谢您的帮助! 飞宇 Re: hantro_VC8000E_enc源代码 你好,joanxie: 很抱歉再次打扰您,我无法访问您提供的连接。错误如下: 此站点上的连接不安全。比特桶。sw.nxp.com 不接受您的登录证书,或者可能尚未提供。 请尝试联系您的组织。 SSL 客户端身份验证证书错误 飞宇
查看全文
Migrating S32K144 project from S32 design studio for ARM to S32 design studio for S32 platform Hi NXP team, From the NXP website, we obtained the BCC SW Driver Package for MC33771C and MC33772C. We are trying to migrate the those example projects into S32 design studio for S32 platform (Version: 3.5). We followed the migration procedure from the following link: https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/Video-Migrating-S32K1-projects-from-S32DS-for-ARM-and-SDK-3-0-x/ta-p/1296239 . However, the code is not migrating correctly, and we are unable to determine why. Please assist me in fixing this problem. Best regards, Hareesh Re: Migrating S32K144 project from S32 design studio for ARM to S32 design studio for S32 platform Hi @VaneB , Thanks for the assistance; everything is operating smoothly now. Best regards, Hareesh Re: Migrating S32K144 project from S32 design studio for ARM to S32 design studio for S32 platform Hi @Hareesh  For the S32SDK S32K1XX RTM 4.0.2, you need to install a service pack, this can be downloaded from S32 Design Studio 3.4 S32K1xx Service Pack 1 > S32 Design Studio IDE >  S32 Design Studio for S32 Platform v.3.4.  Re: Migrating S32K144 project from S32 design studio for ARM to S32 design studio for S32 platform Hi @VaneB , Following your advice, I installed S32DS v3.4. However, as you can see in the attached image below, when I attempted to migrate the project into S32DS, no project names were displayed. I can see several possibilities mentioned there after expanding the migration filter option. However, the files were associated with SDK S32K1xx 4.0.2 (see to the attached image below). However, all I see in my IDE is SDK S32K1xx 4.0.3 (see attached image below). There is no SDK S32K1xx 4.0.2 listed here. How can it be installed if SDK S32k1xx 4.0.2 is the only version that supports it? Could you please help me to address this problem? Best regards, Hareesh Re: Migrating S32K144 project from S32 design studio for ARM to S32 design studio for S32 platform Hi @Hareesh  I am afraid that looks like the migration feature of S32DS v3.5 is not as fully functional as S32DS v3.4. We recommend to move to S32DS v3.4.  I will inform the corresponding team of this issue. Sorry for the inconvenience.  Re: Migrating S32K144 project from S32 design studio for ARM to S32 design studio for S32 platform Hi @VaneB , Yes, there are no mistakes during the code's compilation. However, I am not receiving the project pins and drivers configurations (see screenshots attached), which ought to be provided as they appear in the linked video. Regards, Hareesh Re: Migrating S32K144 project from S32 design studio for ARM to S32 design studio for S32 platform Hi @Hareesh  As I mentioned in my previous response. The steps made were the ones provided in the video shared. Once the steps of code migration were done the errors presented were related to library inclusion, which can be solved with the information provided in my previous post.  Re: Migrating S32K144 project from S32 design studio for ARM to S32 design studio for S32 platform Hi @VaneB , Thanks for the update. Despite my following your instructions, it is not migrating. A snapshot of the migration window is attached. Also, for your reference I attached the project which need to be migrated into S32 design studio 3.5. Regards, Hareesh Re: Migrating S32K144 project from S32 design studio for ARM to S32 design studio for S32 platform Hi @Hareesh  I reproduced the steps of the video and the problems I faced were related to libraries inclusion.  These libraries are located in the Generated_Code file. To solve this problem you need to Rename the ".c" and the ".h", you need to delete the ".bak" of each. You also need to "Exclude from build" the Generated_Code file.  And need to include the file path at project properties.  B.R. VaneB
查看全文
Doubt about GPT in i.MX8MP Reading the IMX8MPRM document, I see that the there are 6 GPTs available. In Chapter 12, the GPT is described and it says that it has two inputs GPT_CAPTURE1 and GPT_CAPTURE2 that can be used to trigger a capture of the timer counter. In Chapter 8, Chip IO and Pinmux, I can only find 2 capture inputs named GPT1_CAPTURE1 and GPT1_CAPTURE2. Does it means that from the 6 GPTs, only the GPT1 has the ability to use the capture feature? Thanks and regards Re: Doubt about GPT in i.MX8MP Yes, right.
查看全文
对 i.MX8MP 中的 GPT 的疑问 阅读 IMX8MPRM 文档,我发现有 6 个可用的 GPT。 第 12 章描述了 GPT,并说它有两个输入 GPT_CAPTURE1 和 GPT_CAPTURE2,可用于触发定时器计数器的捕获。 在第 8 章“芯片 IO 和 Pinmux”中,我只能找到 2 个名为 GPT1_CAPTURE1 和 GPT1_CAPTURE2 的捕获输入。 这是否意味着在 6 个 GPT 中,只有 GPT1 具有使用捕获功能的能力? 感谢并致意 回复:对 i.MX8MP 中的 GPT 的疑问 是的,对。
查看全文
ARM 用 S32 デザイン スタジオから S32 プラットフォーム用 S32 デザイン スタジオへの S32K144 プロジェクト移行 こんにちは、NXPチームの皆様、 NXPのWebサイトから、MC33771CおよびMC33772C用のBCC SWドライバーパッケージを入手しました。 これらのサンプルプロジェクトをS32プラットフォーム用のS32デザインスタジオ(バージョン:3.5)に移行しようとしています。 次のリンクから移行手順に従いました:https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/Video-Migrating-S32K1-projects-from-S32DS-for-ARM-and-SDK-3-0-x/ta-p/1296239。 ただし、コードが正しく移行されておらず、その理由を特定できません。 この問題を解決するのを手伝ってください。 よろしくお願いいたします。 ハリーシュ Re:ARM用のS32デザインスタジオからS32プラットフォーム用のS32デザインスタジオへのS32K144プロジェクトの移行 こんにちは@Hareesh  残念ながら、S32DS v3.5の移行機能はS32DS v3.4ほど完全には機能していないようです。S32DS v3.4への移行を推奨します。 この問題については、対応するチームに通知します。ご不便をおかけして申し訳ございません。 Re:ARM用のS32デザインスタジオからS32プラットフォーム用のS32デザインスタジオへのS32K144プロジェクトの移行 こんにちは@Hareesh  前の回答で述べたように。行われた手順は、共有されたビデオで提供されたものです。コード移行の手順が完了すると、提示されたエラーはライブラリのインクルードに関連していましたが、これは以前の投稿で提供した情報で解決できます。
查看全文
i.MX8MPのGPTに対する疑問 IMX8MPRMのドキュメントを読むと、利用可能なGPTが6つあることがわかります。 第12章では、GPTについて説明し、タイマーカウンターのキャプチャをトリガーするために使用できる2つの入力GPT_CAPTURE1とGPT_CAPTURE2があると述べています。 第8章「チップIOとPinmux」では、GPT1_CAPTURE1とGPT1_CAPTURE2という名前の2つのキャプチャ入力しか見つかりません。 6つのGPTのうち、GPT1だけがキャプチャ機能を使用できるということですか? ありがとうございます。よろしくお願いします。 Re:i.MX8MPのGPTについての疑問 はいそうです。
查看全文
A2T27S020NR1 S パラメータ こんにちは、私はA2T27S020NR1 LDMOSトランジスタを使用しています。どなたかこのデバイスのSパラメータデータを共有していただけますか?2.4GHzで動作するパワーアンプを設計するために必要です。                      
查看全文
S32K312 スリープウェイクアップ 背景情報 現在、S32k312を使用してスリープおよびウェイクアップ機能を開発しています。以下の点についてご質問があります。ご助言をお願いいたします。 1. 高速スタンバイではなく通常ウェイクアップを使用しています。通常ウェイクアップモードでは、ウェイクアップソースをスタンバイRAMに保存できますか?現在、WISRレジスタから有効なウェイクアップソースを読み出すことができません。 2. オシロスコープで観察したところ、スリープ状態でウェイクアップソースを受信すると、K3はまずリセットしてからICU割り込みに入ることが分かりました。ウェイクアップはまずリセットされてからICU割り込みに入るのか、それともICU割り込みに入ってからリセットされるのかを知りたいです。 3. スリープ解除後、レベルエッジ割り込みによるウェイクアップを1回だけトリガーしました。ウェイクアップ後、WISRレジスタの値を見ると、ICUウェイクアップ機能で設定されたすべての割り込みが1回トリガーされたことがわかります。そのため、ウェイクアップソースA〜Bが2つ存在するのではないかと疑っています。方法AでMCUをウェイクアップすると、WISRはA〜Bの両方のウェイクアップイベントを同時に記録します。この問題の解決方法をご教示ください。 Re: S32K312 スリープウェイクアップ はい、おっしゃる通り、私のプログラムも同じように設計しています。例えば、同じウェイクアップソースとしてCANウェイクアップを使用しています。ウェイクアップメッセージを1回だけ送信すると、プログラムはウェイクアップしてからスリープ状態に戻ります。しかし、ウェイクアップメッセージを2回または3回送信すると、ソフトウェアは有効なウェイクアップソースを認識し、ウェイクアップ状態を維持できます。なぜでしょうか?ありがとうございます。 Re: S32K312 スリープウェイクアップ 1. 私のソフトウェアは有効なウェイクアップソースを検出すると、ウェイクアップ状態を維持します。この場合、MCUがスリープ状態になった後にウェイクアップイベントを1回だけトリガーすると、MCUはウェイクアップした後すぐに再びスリープ状態になります。これは、有効なウェイクアップソースが認識されていないためと考えられます。MCUがスリープ状態になった後に2回または3回トリガーされれば、有効なウェイクアップソースを認識し、ウェイクアップ状態を維持できます。したがって、K3プラットフォームでは、ウェイクアップイベントを1回だけトリガーすると、MCUをウェイクアップしてリセットすることしかできないと考えられます。2回目または3回目のウェイクアップイベントがない場合、MCUはリセット後すぐに再びスリープ状態になります。私の結論は正しいでしょうか?ありがとうございます。
查看全文
FXLS8967AF Datasheet error: SENS_CONFIG1 default value descriptions The current datasheet listed on the website is Rev 1.5 of Mar 11, 2022: https://www.nxp.com/products/sensors/accelerometers/2g-4g-8g-16g-low-power-12-bit-digital-accelerometer:FXLS8967AF Table 47 shows that the SENS_CONFIG1 register default value depends on the BT_MODE pin: This affects the FSR and ACTIVE fields. The Table 48 descriptions fail to mention this, and use inconsistent options for the 2 fields: The description of FSR uses the BT_MODE=VDD default value, 01; The description of ACTIVE uses the BT_MODE=GND default value, 0 Re: FXLS8967AF Datasheet error: SENS_CONFIG1 default value descriptions Hello andrewneil, I hope all is great with you. Thank you for using the NXP communities. Correct, I also think that Table 48 doesn't mention this. It is not clear. I just wanted to let you know that I have already shared your feedback with the corresponding team. Thank you very much for your comments. Regards, David
查看全文
What difference between Connectivty_test and HCI black box FW? Hi NXP,    We are testing SRRC for kw45 bluetooth boards and it designed by us.    When we test RF test, is accour different result by using different FW, connectivity_test and HCI black box.     like below:    When test Frenquency range, signal send by LE_transmitter_cmd is lower than connectivty test cmd send by LE_transmitter_cmd:01 1E 20 03 00 25 00, result=-36.953dBm/MHz: send by connectivty test cmd:"Mode TX, Rate BLE 1Mbps, Whiten Fixed, Channel 42, Power 31, Payload 37, XtalTrim 26> Mod PN", result=-39.23dBm/MHz:      It is higher 2dB in connectivity test.  Why and how it can occured? and we use the same sounding only different FW.     Here is we use:      SDK example: KW45B14ZEVK 2.12.7      FW: connectivity test / HCI black box from, which only I change is Xtaltrim=26.      MXUXpresso IDE: V11.8.0_1165    If you have any ideas about the commands and how to pass certification, please let us know, thanks.    Best Regards,    Annie Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  For the spec mentioned by you, we also have test result please see below pic: And would you mind to speak Chinese for better understanding each other? 您是要测带外杂散信号吗? 可以将您的问题详细描述一下发到我的邮箱:[email protected] 我把您原始的邮件转发给我们的内部专家团队帮忙看看,避免因translate引起误解。 Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? hey Christine,        We are not talking the same thing.We are testing Freq Range not Emission in Band. It is not a good solution for us.        The specification files we are refering is as attach. I am sure the limit is 30dBm/KHz as below SRRC limit .       It meas When we are sending signal in 2402MHz or 2480Mhz, It request power in 2400MHz&2483.5MHz need to less than -80dBm/Hz. And we need to calculate, Power dBm= -80dBm/hz+10*log(100000)= -80+50= -30dBm/KHz, So its limit should be -30dBm/KHz, it is talking clearly in ETSI EN 300 328 V1.7.1 (2006-10).pdf and SRRC number 129. Our SA setting when we are testing Freq Range in 2400 Center Freq=2400MHz Span=10MHz RBW=100KHz VBW=100KHz Sweep time =60s offset=cable loss+Antenna Gain Detector=RMS Max hold You can try and talk to me. Best Regards, Annie Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  Do you have any chance to read my previous comment? Please let me know whether you have any other queries. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  Our internal team's test result is similar with you. Please see below: But after checked the AN13228, we found the BT limit is -20dBm, not -30dBm. It means, according to the AN13228's BT limit, we can pass for sure. Can you please help to confirm SRRC certification limit requirement? If you have any specification files, can also share us to check together. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  I found our test result, it seems different with yours. There is no these 2 little peak in our test results as shown in the below screen shot. For details, you can also refer to our test report on KW45-EVK. AN13228-KW45B41Z-EVK RF System Evaluation Report for Bluetooth Low Energy Applications I have request our AE team help to test again, and at the same time, please share me your detailed test steps, so that we can compare and find whether have any different steps during test. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi Christine_Li,     I have tried your suggestion. But the signal is not what we want. it behaves like umodulation signal. Continuous Modulated Transmission 1's:  Continuous Modulated Transmission 0's:   Best Regards, Annie Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  It's my pleasure!  You are welcome anytime. I receive our internal team's suggestion, can you please have a try and let me know your result? Could you please try the transmitter test command with the pattern of all 0 bits or 1 bits? Thank you. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi Christine_Li,      We got the 2M-Freq Range from KW45- EVK. It also behaves less margin in 2400MHz, Like below pictrue, and its power is about 9.8dBm in 2402MHz: The test Way we get from ETSI EN 300 328 V1.7.1 (2006-10) as the attach file. Now we have tunned a matching and the result in 2M-Freq Range is similiar to KW45-EVK. If you have better ideas about the test Way or how to get more margin, please talk to us. Thank you very much. Best Regards, Annie Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  Thanks for your reply. Sure, please take your time. And also I have created an internal case to our expertise team. Hope we can resolve this issue ASAP. If I need any other info from your side, I will leave message to you. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  Thanks for your reply and your efforts on this issue. Sorry, I am not good at this Power related to certification,. I need to check with our internal team. But as you know, we will have a public holiday from May 1st to May 5th in China, totally 5 days, and I will be back to office 6th of May. I could not reply you in time during this period. I sincerely apologize for the inconvenience. Have a nice holiday~   Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  Thanks for creating case to us and hope you are doing well. I will check it and reply to you once have any updates. Have a nice weekend. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  These two is built for different examples. For the details inside of these two FWs, I need to confirm with our internal team. But before that, may I ask what kind of issue do you meet during your certification? Which FW can pass the certification? and what is the standard of the certification? Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi Christine,     Thanks for your reply.     Now we are going to get pass the China Ble standard named SRRC. And the issue I meet in certification is 2M-Frequency range fail.     When I use Connetivity_test FW, I get the 2M-Frequency range result as below, it is so close to the limit.The Frenquency of Power 30dBm/100Khz is 2.40000GHz=2.4GHz. We do not have enough value to pass the certification: cmd:  Mode TX, Rate      BLE 2Mbps, Whiten Fixed, Channel 42, Power 31, Payload 37, XtalTrim 26> Mod PN When I use HCI black box FW, I get the result as below, Power 30dBm/100Khz is 2.40065GHz>2.4GHz, Pass : cmd: 01 34 20 04 00 25 00 02 And also, The 2M-suprious emission of 2390-2400 is so close to the limit as below Picture: For connectivity test FW, Power in 2.4GHZ is -30.68dBm, we have no more margin to pass: cmd: Mode TX, Rate      BLE 2Mbps, Whiten Fixed, Channel 42, Power 31, Payload 37, XtalTrim 26> Mod PN For HCI black box FW, Power in 2.4GHZ is -33.750dBm, we still have 3dB margin to pass: cmd: 01 34 20 04 00 25 00 02 Our Surrounding: SDK: KW45 V2.12.7 IDE: V11.8.0_1165 FW: connectivity_test &HCI black box      thanks      Best Regards,      Annie Re: What difference between Connectivty_test and HCI black box FW? And, This Afternoon, I try to change Connectivity test cmd and it can get a better result. Cmd- Burst Transmission using random-payload packets: Mode RX, Rate BLE 2Mbps, Whiten Fixed, Channel 42, Power 31, Payload 37, XtalTrim 26> Packet Mode PRBS started. Press [SPACE] to stop test and 2M-Frenquency Range result as below, there is 70KHz margin: and 2M-Suprous Emisson in 2390-2400Mhz result as below, there is 6dBm margin: And if we can use Burst Transmission using random-payload packets cmd to test certification? What different in Burst Transmission using random-payload packets cmd and Continuous Modulated Transmission pseudo-random cmd and HCI_LE cmd?  connectivity test FW cmd as below: If you have any ideas about it, please let us know. Thanks. Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  I found this guide in our SDK: Generic FSK Link Layer Quick Start Guide.pdf  which is located in SDK_2_12_7_KW45B41Z-EVK\docs\wireless\GENFSK\ path. Please see section:  4.3.1 Continuous tests  So I think we just provide some examples and different modes to customer to choose according customer's preference. About SRRC certification, I think you can choose any modes from them.  Do you know SSRC has any special rules to limit the test modes? If there is no such kind of limitations, then you can pass it with Cmd- Burst Transmission using random-payload packets. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi Christine,    SRRC may request the duty cycle, but I did not get the specific limit about it. Duty cycle of an old SRRC report in 2008 is demanded more than 10%.    I try to send cmd-Burst Transmission using random-payload packets to DUT, it pass. But its duty cycle is less than 10%.    So if you have better Ideas about below: 1. HCI black box can support HCIExt_ModemTestTxCmd & HCIExt_EnhancedModemTestTxCmd HCIExt_ModemTestTxCmd: 1Mbps 2402MHz UNMoudulation: Send->01 08 FC 02 01 00 recieve>>04 FF 05 08 04 00 08 FC HCIExt_EnhancedModemTestTxCmd: 1Mbps 2402MHz UNMoudulation: Send->01 27 FC 03 01 00 00 >>04 FF 05 27 04 00 27 FC those cmd we got From other chip platform, if you have similar solution about unmodulation signal in KW45? 2. How to get 2M-Phy Frenquency Range in 2400 lower down? We really need your help, if you have any ideas, please share us, Thank you so much. Best regards, annie Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  Thanks for your reply. 1.For the unmodulated signal in KW45, can you please help to try with mode [6]? 2. How to get 2M-Phy Frenquency Range in 2400 lower down? ==>Sorry, can you give me more details for better understanding? I didn't get your point. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  I haven't received your feedback in 5 days, do my above comments help you? Please let me know whether still need our support on this thread. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi Christine,     Sorry, I'm late for your reponse.     What I talk may not so clear. 1. I hope to use HCI black box image to send unmodulation signal, not connectivity test image to send. 2.For sencond question, you can know taht 2M-Frenquency range of KW45 fail in China SRRC test. Like below picture, I send 2M signal in 2402Mhz by connectivity test, and its Frenquency Range is more than 30dBm in 2400Mhz. SRRC request in 2400Mhz, power need less than 30dBm. But HCI black box image to test 2M Freq Range, it is easily to pass this SRRC item. But it can not sopport Ummodulation signal. We need a image which can pass SRRC and send unmodulation signal&modulatuion signal. And if you have better idea? And sorry for late again and Thank you so much for your reply. Best Regards, Annie Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  Sorry for my late reply. Do you have our KW45-EVK? Have you tested with our KW45-EVK? I am suspect whether it is a hardware issue. I am not so familiar with hardware, if you have our KW45-EVK, please help to test with it and let me know the result. At the same time, I will create an internal ticket to our expertise team to ask help. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi Christine_Li,     We have KW45-EVK, and I will use KW45-EVK to test its 2M Freq Range with Connectivity test image this afternoon or tomorrow and give a feedback for you.      Thanks for your help and reply. Best Regards, Annie Re: What difference between Connectivty_test and HCI black box FW? Hi Christine_Li,      KW45-EVK 2M-Freq Range test result is as below: There is also less margin to the limit(-30dBm) in 2400Mhz. And test way I got from ETSI EN 300 328 V1.7.1 (2006-10) as attach. We have tunned a RF matching and got similiar result as KW45-EVK in SRRC 2M Freq Range. If you have better ideas about the test way or how to get better one, please talk to us, Thank you very much. Best Regards, Annie Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  Thanks for your results. I have forwarded the test result on both your board and our KW45-EVK to our expertise team. Once receive any feedback, I will share with you. I apologize again for my poor RF knowledge. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi Christine_Li,     Thanks you so much. You take much of you time to help us.     You can check the test way of Freq Range and if you have any ideas about the 2M Freq Range, you can share with us.     And if you have any updates, you can send mail to me or leave massege in this post. My Email is [email protected]. Best Regards, Annie Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  Did you get any chance to test with our internal team's suggestion? Please let me know whether it works for you. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  Thanks for your reply. I have forwarded your result to our internal team. Hope we can get more suggestions to support you. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  Thanks for your patience. I received our internal team's reply as below: ========  Yes, the HCI commands can not generate the pure continuous wave. The frequency of transmitting 1 or 0 has a positive or negative deviation than the pure continuous wave. We can consider it as an unmodulated signal while ignoring the frequency. ========= Please let me know anything else I can do for you. If you still have any other concerns, please do not hesitate to reply me. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  Anything else I can do for you on this case? Or do you have any other questions or queries? Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi Christine_Li,     Thanks for your attention in this post!     But the report that you posted the picture, the power it set is 0 dBm and it is uppper bandege which signal is 2480MHz not 2400MHz. And I do not know the reason it set the minium power. But when we go to do the SRRC certification, we need set the max power 10 dBm. And SA setting is different from SRRC requested. SRRC request       Now we found to decrease the power to 9dBm-9.5dBm, we can pass 2M Freq Range in the certification, But there is a little margin, it is stiil dangerous for us.      Thank you again. Best Regards, Annie             Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  Thanks for your reply, and you are welcome, it is my job to support you. I have forwarded your feedback to our internal team, our expertise will test today, hope they can share some good news or ideas to us. Once have any updates, I will let you know. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  Do you have any chance to read my previous comment? Please let me know whether you have any other queries. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  The test result of TX power in band is normal. And it complies with the BLE specification.  Please let me know whether you have any other concerns on this case. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  Thanks for your reply. Sure, I will forward your feedback to our internal team and request to continue to support this case. Any updates I will let you know. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  Regarding the first question, I would like to add: Are you measuring the radiation mode? Or the maximum equivalent isotropic radiated power? Is it a conducted test? For the second question, let me add one more thing. As shown in the figure below, are you testing the out-of-band emission band or the spurious emission band? Because we see that you are testing: The spurious domain is outside 2.5 times the channel bandwidth And what you tested is: 2M PHY: 2390-2400MHz. Combined with the figure below, it looks like it is in the out-of-band emission domain rather than the spurious domain? So please confirm. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi Christine_Li, Let me give you a brief reply here. The problem we encountered when testing the KW45 SRRC report was that the Ble 2M PHY-2400MHZ sideband power was too close to the limit. There are two limit requirements related to 2M PHY-2400MHz 2400 in SRRC No. 129: 1. The defined operating frequency range is 2400-2483.5MHz, and the equivalent isotropic radiated power at the upper and lower limits of the operating frequency is specified to be no greater than -80dBm/Hz. This test can also be understood as a frequency edge test. The conversion formula is: -80dBm/hz+10*log(100000)= -80+50= -30dBm/KHz. 2. Special frequency band spurious test 2M PHY-2390-2400MHz, the limit requirement is also -30dBm. The test specifications and methods we refer to are as follows: Frequency range test requirements, reference document: ETSI EN 300 328 V1.7.1 (2006-10) Frequency range test requirements and test methods, refer to the document: Bluetooth RF indicators and detection methods The results of our board test are as follows: The firmware is kw45b41zevk_connectivity_test_bm, SDK: 2.12.7 测试时,频谱仪需补的Offset应为cable loss+Antenna Gain 1. 2M PHY 2400MHz 频率边带测试 The KW45 test result of 2M PHY frequency edge 2400MHz is: -30.446dBm<-30dBm, the margin is only 0.446dBm The KW45 test result of 2M PHY frequency edge 2400MHz is: -30.383dBm<-30dBm, the margin is only 0.383dBm At present, the sideband of our 2M PHY 2400MHz is very close to the Limit -30dBm. The KW45 EVK test also has similar results. You can test it according to the method I posted in the post. At present, it is found that adjusting the RF matching cannot solve the problem well. Only by reducing the power can a better effect be achieved. I uploaded the documents used to Attach. Best Regads, Annie Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he Sorry for not replying to you for so long. We just received a reply from our internal team. We still have some questions about your test: You mainly test two parameters, one is the out-of-band transmission power, which is the maximum equivalent isotropic radiated power tested. This should not be a conducted test, right? The spurious signal of the second test should be outside 2.5 times the channel bandwidth of the center frequency, that is, 2.4G+-50M? SRRC Certification: Standards and specific requirements for Bluetooth and WI-FI product model approval testing! _Sichuan Chengdu Third-Party Testing and Certification Agency (wanttest.com) SRRC certification: standards and specific requirements for Bluetooth and WI-FI product model approval testing! SRRC certification: Standards and specific requirements for model approval testing of Bluetooth and WI-FI products! "Radio Transmitter Equipment Model Approval Certificate", the model approval code must be indicated on the label of the factory equipment. Your test document also mentions that you need to test in the spurious domain. Please help answer the above questions, thank you. Best regards, Christine. Re: What difference between Connectivty_test and HCI black box FW? Hi, @Annie_he  Thanks for the detailed information. Our internal AE team colleagues have been a bit busy recently and haven't replied to me yet. I will continue to follow up and inform you as soon as there is any progress. Best regards, Christine.
查看全文