Reading the IMX8MPRM document, I see that the there are 6 GPTs available.
In Chapter 12, the GPT is described and it says that it has two inputs GPT_CAPTURE1 and GPT_CAPTURE2 that can be used to trigger a capture of the timer counter.
In Chapter 8, Chip IO and Pinmux, I can only find 2 capture inputs named GPT1_CAPTURE1 and GPT1_CAPTURE2.
Does it means that from the 6 GPTs, only the GPT1 has the ability to use the capture feature?
Thanks and regards
Yes, right.