Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
ホストインターフェース(I2C)を備えたPN7642にファームウェアを書き込むことはできません。 こんにちは、 LPC55S16コンパニオンボードを使用して、I2C経由でPN7642にカスタムファームウェアを書き込もうとしています。 Host Crypto Scripts (01.03) を使用してesfwuファイルを生成しました。トランスポートキーにはC101チップ用のものを使用しました(EVKボードを改造して新しいC101チップをはんだ付けしました)。 PN7642のホストインターフェースを介してユーザーファームウェアを更新するためのステップバイステップガイド カスタム(セキュリティ保護されていない)アップデートがエラー0x01で失敗します。 NXP FW(セキュア版)、バージョン03.00をフラッシュすると、正常に動作します。 HostScriptの設定ファイルが、お客様のファイアウォールには適していないのではないかと疑っています。 私が変更したのは、aes_keyをC100トランスポートキーからC101トランスポートキーに変更しただけです。 手伝ってもらえますか? よろしくお願いいたします。 Re: Cannot flash a PN7642 with Host Interface (I2C) こんにちは、 @V_Palacio さん。 それとも、あなたのFWファイルを共有して、私のサイトで試させていただけますか? Re: Cannot flash a PN7642 with Host Interface (I2C) こんにちは、 @V_Palacio さん。 C101については、以下のプロジェクトを選択してください。 KaiLi_0-1781878068922.png カスタマイズしたファームウェアを更新するには、カスタマイズしたファームウェアを正しいパスに配置し、「6」を選択してください。 Re: Cannot flash a PN7642 with Host Interface (I2C) こんにちは、 @KaiLi さん。 接続は正常にできていますし、I2C経由でLPCを使ってNXPのセキュアファームウェアをアップデートする際にも問題はなかったので、これが問題の原因ではないと思います。 よろしくお願いいたします。 Re: Cannot flash a PN7642 with Host Interface (I2C) こんにちは、 添付ファイルに私のファームウェアファイルがあります。esfwuとして生成されますが、ここに添付できるように名前が変更されました。 私のtomlファイルと元の.binファイルも添付しました。FW。 そちら側でうまくいくかどうか教えてください。 よろしくお願いいたします。 Re: Cannot flash a PN7642 with Host Interface (I2C) こんにちは、 この問題について何か考えはありますか? よろしくお願いいたします。
記事全体を表示
Simultaneous Ethernet Camera Streaming Solution We are developing a custom i.MX8MP-based board for an automotive camera system. We have a working single-camera H.264 RTP streaming pipeline using the VPU hardware decoder on our 5.15.71 NXP Yocto BSP. We are now planning to scale to 4 simultaneous camera streams via an Ethernet switch.  The switch will aggregate 4x 100BASE-T1 camera ports and connect to the i.MX8MP EQOS MAC via a gigabit RGMII uplink, with each camera isolated on its own VLAN. Our display is 1280x800. For 4-stream simultaneous view each stream only needs to fill a quarter of the display (~640x400 or lower @30 fps), so we can scale camera resolution down as needed. 1. Is there an NXP i.MX8MP reference design or application note covering multi-channel video decode that we can use as a starting point? 2. Can the H.264 VPU decoder handle multiple independent instances from separate sources, or is a pre-decode composition step required to reduce the number of processes and context switches? If composition is required, what is the recommended approach on i.MX8MP? 3. What is the overall recommended software architecture for this use case from NXP's perspective? Our future application is surround view, so scalability and low latency are key requirements. Thanks! Re: Simultaneous Ethernet Camera Streaming Solution Hi @Wobaffet  The i.MX8MP can serve as a candidate platform for this 4-channel Ethernet H.264 camera quad-view application; however, only the i.MX8QM and i.MX95 have reference designs for surround view. The recommended architecture is for the four RTP/H.264 streams to enter separate GStreamer pipelines, be decoded individually by VPU hardware decoders, and then undergo hardware-assisted scaling and composition after decoding, with the output displayed on a 1280×800 display. It is not recommended to attempt composition before H.264 decoding, as separate H.264 streams cannot be directly composited into a single display frame in the compressed domain unless decoding and re-encoding have already been completed at the upstream switch or camera. For a display requirement of 4 streams at approximately 640×400@30fps, a rough estimate based on pixel rate indicates that the load is significantly lower than that of 1080p60 decoding, so this approach is reasonable. However, whether this ultimately meets the low-latency and stability requirements for surround view will require system-level verification, taking into account actual camera bitrate, profile, GOP, RTP jitter, DDR bandwidth, the GStreamer zero-copy path, and the composition method. Best Regards, Zhiming Re: Simultaneous Ethernet Camera Streaming Solution Hello, Thank you for the answer! As a follow up,  1. We are planning to run 4 independent GStreamer pipelines simultaneously, each decoding its own H.264 stream using the VPU hardware. We want to confirm that the VPU driver in the 5.15.71 BSP supports 4 truly concurrent decode instances. Is there any known configuration or limitation in this BSP that would prevent all four pipelines from decoding in parallel, or is a scheduling method required? If so, are any examples available? 2. Our setup has an Ethernet switch connecting 4 cameras to the i.MX8MP via a single RGMII uplink, with each camera on its own VLAN. On the Linux side we plan to create VLAN subinterfaces on the EQOS port and have each GStreamer pipeline receive UDP/RTP from its own subinterface. Two questions on this: Does the EQOS driver in the 5.15.71 BSP support 802.1Q VLAN tagged frames correctly out of the box, or is there any additional configuration needed? And are there any known receive-path tuning recommendations for running 4 simultaneous UDP streams on this interface in this BSP? Thanks!  
記事全体を表示
S32k328 HSE DomainID Hello, NXP Technical Team I am writing to inquire about accurately verifying the S32k328 Domain ID. I am currently using an S32k328 board and HSE Firmware.  - Setup Environment:      I am using the HSE Firmware image s32k358_hse_fw_1.14.0_2.40.0_pb230807.bin.      I am currently in a multi-core state and using RM module(only use XRDC).  - Question:     In the HSE FW RM, the S32k328 Domain ID is set to 2 as shown in the attachment. dpsdprtmvl_1-1781577003974.png However, in the S32k328 Block Diagram within the S32k3xx RM, the HSE is set to MDAC3, and the DID (Domain ID) of MDAC3 is output as 3. dpsdprtmvl_2-1781577150058.png    (1) Register Verification Code:             uint32_t mda[8];             mda[0] = IP_XRDC->MDA_W0_0_DFMT0;             mda[1] = IP_XRDC->MDA_W0_1_DFMT1;             mda[2] = IP_XRDC->MDA_W0_2_DFMT1;             mda[3] = IP_XRDC->MDA_W0_3_DFMT0;             mda[4] = IP_XRDC->MDA_W0_4_DFMT0;             mda[5] = IP_XRDC->MDA_W0_5_DFMT1;             mda[6] = IP_XRDC->MDA_W0_6_DFMT0;             mda[7] = IP_XRDC->MDA_W0_7_DFMT1;             UART_Print("--- MDA Locks ---\n");             for (uint32_t i = 0; i < 8; i++)             {                 uint32_t vld = (mda[i] >> 31) & 1U;                 uint32_t lk1 = (mda[i] >> 30) & 1U;                 uint32_t did = mda[i] & 0x3U;                 UART_Print("MDA%lu=0x%lx VLD=%lu DID=%lu LK1=%lu %s\n",(unsigned long)i, (unsigned long)mda[i],(unsigned long)vld, (unsigned long)did, (unsigned long)lk1,lk1 ? "(LOCKED)" : "");             }    (2) Register Value:            MDA0=0x80000000 VLD=1 DID=0 LK1=0            MDA1=0x20000000 VLD=0 DID=0 LK1=0            MDA2=0x20000000 VLD=0 DID=0 LK1=0            MDA3=0xc0000003 VLD=1 DID=3 LK1=1 (LOCKED)            MDA4=0x80000001 VLD=1 DID=1 LK1=0            MDA5=0x20000000 VLD=0 DID=0 LK1=0 What is the correct S32k328 Domain ID? Re: S32k328 HSE DomainID Hi @dpsdprtmvl  S32K328 has four domains 0-3 and HSE is always assigned to highest available domain – to domain 3 in this case: lukaszadrapa_0-1781608491449.png This is hardwired and it cannot be changed. The Table 136 is little bit confusing because it shows only main derivatives, not all sub-derivatives. That means: S32K32x in the second row stands for S32K322 and S32K324. S32K35x in the third row stands for S32K358, S32K356, S32K348, S32K338, S32K328 and S32K37x and S32K39x derivatives. Regards, Lukas
記事全体を表示
S32k328 HSE 域标识符 您好,恩智浦技术团队 我写这封信是为了询问如何准确验证 S32k328 功能域 ID。 我目前正在使用 S32k328 板和 HSE 固件。  - 环境设置:      我正在使用 HSE 固件镜像 s32k358_hse_fw_1.14.0_2.40.0_pb230807.bin。      我目前处于多核状态,并正在使用 RM 模块(仅使用 XRDC)。  - 问题: 在 HSE FW RM 中,S32k328 功能域 ID 设置为 2,如附件所示。 dpsdprtmvl_1-1781577003974.png 但是,在 S32K3xx RM 中的 S32K328 方框图中,HSE 设置为 MDAC3,MDAC3 的 DID(功能域 ID)输出为 3。 dpsdprtmvl_2-1781577150058.png    (1) 注册验证码:             uint32_t mda[8];             mda[0] = IP_XRDC->MDA_W0_0_DFMT0;             mda[1] = IP_XRDC->MDA_W0_1_DFMT1;             mda[2] = IP_XRDC->MDA_W0_2_DFMT1;             mda[3] = IP_XRDC->MDA_W0_3_DFMT0;             mda[4] = IP_XRDC->MDA_W0_4_DFMT0;             mda[5] = IP_XRDC->MDA_W0_5_DFMT1;             mda[6] = IP_XRDC->MDA_W0_6_DFMT0;             mda[7] = IP_XRDC->MDA_W0_7_DFMT1;             UART_Print("--- MDA 锁 ---\n");             用于 (uint32_t i = 0; i < 8; i++)             {                 uint32_t vld = (mda[i]>> 31)& 1U;                 uint32_t lk1 = (mda[i]>> 30)& 1U;                 uint32_t did = mda[i]& 0x3U;                 UART_Print("MDA%lu=0x%lx VLD=%lu DID=%lu LK1=%lu %s\n",(无符号 long)i, (无符号 long)mda[i],(无符号 long)vld, (无符号 long)did, (无符号 long)lk1,lk1 ? "(已锁定)" : "");             } (2) 寄存器值:            MDA0=0x80000000 VLD=1 DID=0 LK1=0 MDA1=0x20000000 VLD=0 DID=0 LK1=0 MDA2=0x20000000 VLD=0 DID=0 LK1=0 MDA3=0xc0000003 VLD=1 DID=3 LK1=1 (已锁定) MDA4=0x80000001 VLD=1 DID=1 LK1=0 MDA5=0x20000000 VLD=0 DID=0 LK1=0 正确的 s32k328 功能域 ID 是什么? Re: S32k328 HSE DomainID 你好@dpsdprtmvl  S32K328 有四个功能域 0-3,HSE 始终分配给最高可用功能域,在本例中分配给功能域 3: lukaszadrapa_0-1781608491449.png 这是固有的,无法更改。 表 136 有些令人困惑,因为它只列出了主要导数,而没有列出所有次导数。这意味着: 第二行中的“S32K32x”代表 S32K322 和 S32K324。 第三行中的 S32K35x 代表 S32K358、S32K356、S32K348、S32K338、S32K328 以及 S32K37x 和 S32K39x 的衍生型号。 此致, Lukas
記事全体を表示
PN7462AU FreeRTOS:无法从 heap_3 切换到 heap_4,系统卡死 + 堆内存使用情况可见性 大家好,我正在使用搭载 FreeRTOS 的 PN7462AU 平台,SDK 示例已配置为使用 heap_3.c。我目前遇到了内存溢出问题,想更深入地了解堆的配置。 由于 heap_3 使用标准库中的 malloc()/free(),因此无法使用 xPortGetFreeHeapSize() 等函数以及堆统计信息。为了了解堆的使用情况,并可能增加可用堆空间,我尝试通过禁用 heap_3.c 来切换到 heap_4.c并启用 heap_4.c。然而,进行此项更改后,应用程序在启动时会卡住。 我有以下几个问题: 在 PN7462AU 上将 heap_3 切换为 heap_4 是否安全且值得推荐? 如何确定 heap_3 当前可用的内存量? 由于 heap_3 不支持 xportgetFreeHeapSize (),因此推荐使用哪些方法来监测堆使用情况和检测内存耗尽? 从 heap_3 迁移到 heap_4 时,还需要进行哪些额外的配置更改(例如 configTOTAL_HEAP_SIZE、链接器脚本更改、内存区域等)? 如果能提供关于 PN7462AU 和 FreeRTOS 的具体指导或示例,将不胜感激。 谢谢 核心与内存 Re: PN7462AU FreeRTOS: Unable to switch from heap_3 to heap_4, system stuck + heap usage visibility 你好@uday_gowda , NFC读取器库提供了示例,展示了如何使用 PN7462 实现 FreeRTOS,这可能会有所帮助。另外,我建议参阅AN11784 ,它提供了有关将 RTOS 与 PN7462 集成的指导,您可以参考该文档。 MCUXpresso IDE 还包含多个用于 FreeRTOS 应用程序的调试功能。特别是,“堆使用情况视图”可以帮到你。更多详情请参阅MCUXpresso IDE 25.06 FreeRTOS 调试指南第 3.6 章。 最后,请注意PN7462只有12k的SRAM。 BR 哈比卜
記事全体を表示
イーサネットカメラ同時ストリーミングソリューション 当社は、車載カメラシステム向けに、i.MX8MPをベースとしたカスタム基板を開発しています。当社では、NXP Yocto BSP 5.15.71上でVPUハードウェアデコーダーを使用した、シングルカメラH.264 RTPストリーミングパイプラインが正常に動作しています。現在、イーサネット・スイッチを介して4台のカメラの映像ストリームを同時に受信できるように拡張する計画を立てています。このスイッチは4つの100BASE-T1カメラポートを集約し、ギガビットRGMIIアップリンクを介してi.MX8MP EQOS MACに接続します。各カメラはそれぞれ独自のVLANに分離されます。 当社のディスプレイの解像度は1280×800です。4ストリーム同時表示の場合、各ストリームはディスプレイの4分の1(約640x400以下、30fps)を占めるだけでよいので、必要に応じてカメラの解像度を下げることができます。 1.NXP i.MX8MPのマルチチャネルビデオデコードに関するリファレンス・デザインやアプリケーションノートで、参考になるものはありますか? 2. H.264 VPUデコーダは、複数の独立したインスタンスを別々のソースから処理できますか?それとも、プロセス数とコンテキストスイッチ数を減らすために、デコード前の合成ステップが必要ですか?合成が必要な場合、i.MX8MPではどのような方法が推奨されますか? 3. NXPの視点から見て、このユースケースにおける推奨されるソフトウェアアーキテクチャはどのようなものですか? 将来のアプリケーションはサラウンドビューなので、拡張性と低レイテンシが重要な要件となります。 ありがとう! Re: Simultaneous Ethernet Camera Streaming Solution こんにちは、 ご回答ありがとうございます! 続報として、 1. 4つの独立したGStreamerパイプラインを同時に実行し、それぞれがVPUハードウェアを使用して独自のH.264ストリームをデコードすることを計画しています。5.15.71 BSPのVPUドライバーが4つの真の同時デコードインスタンスをサポートしていることを確認したいです。このBSPには、4本すべてのパイプラインが並列にデコードできない既知の設定や制限はありますか?それともスケジューリング方式が必要ですか?もしそうなら、何か例はありますか? 2. 私たちのセットアップでは、イーサネット・スイッチで4台のカメラをi.MX8MPに1台のRGMIIアップリンクで接続し、それぞれのカメラが独立したVLANに接続しています。Linux側ではEQOSポートにVLANサブインターフェースを作成し、各GStreamerパイプラインが独自のサブインターフェースからUDP/RTPを受け取るようにする予定です。この件について2つ質問があります:5.15.71 BSPのEQOSドライバーは、802.1QのVLANタグ付きフレームを箱から正しくサポートしていますか?それとも追加の設定が必要ですか?また、このBSPでこのインターフェース上で4つの同時UDPストリームを実行する場合の受信経路チューニングの推奨はありますか? よろしくお願いします!   Re: Simultaneous Ethernet Camera Streaming Solution こんにちは、 @Wobaffet さん i.MX8MPは、この4チャンネルイーサネットH.264カメラクアッドビューアプリケーションの候補プラットフォームとして機能します。ただし、サラウンドビュー用のリファレンスデザインを持つのはi.MX8QMとi.MX95のみです。 推奨されるアーキテクチャは、4つのRTP/H.264ストリームは個別のGStreamerパイプラインに入力され、VPUハードウェアデコーダによって個別にデコードされ、デコード後にハードウェア支援によるスケーリングと合成が行われ、出力は1280×800のディスプレイに表示されます。H.264デコード前にコンポジションを試みることは推奨されません。なぜなら、別々のH.264ストリームを圧縮ドメイン内の単一の表示フレームに直接合成することは、デコードと再エンコードが上流スイッチやカメラで既に完了している場合のみです。 約640×400@30fpsで4ストリームの表示要件がある場合、ピクセルレートに基づく大まかな推定では負荷は1080p60デコードよりもかなり低いため、このアプローチは妥当です。しかし、これが最終的にサラウンドビューの低レイテンシかつ安定性の要件を満たすかどうかは、実際のカメラのビットレート、プロファイル、GOP、RTPジッター、DDR帯域幅、GStreamerのゼロコピーパス、そして構図方法を考慮したシステムレベルの検証が必要です。 よろしくお願いします、 志明
記事全体を表示
Cannot flash a PN7642 with Host Interface (I2C) Hello, I'm trying to flash a customized FW in a PN7642 via I2c with the LPC55S16 companion board. I've generated the esfwu file with Host Crypto Scripts (01.03), using as Transport Key the one for C101 chip (We have reworked our EVK board to solder a new C101 chip) Step by Step Guide to update user firmware through host interface for PN7642  Custom (not secure) update fails with error 0x01.  If I flash the NXP FW (secure), version 03.00, works OK. I suspect the HostScript configuration file is not OK for a customer FW. I only modified it to change the aes_key from C100 transport key to C101 transport key. Can I get some help? Regards, Re: Cannot flash a PN7642 with Host Interface (I2C) Hello @V_Palacio  For C101, you should select the project: KaiLi_0-1781878068922.png For updating customized FW, you should put your customized FW in the correct path and  select "6". Re: Cannot flash a PN7642 with Host Interface (I2C) Hello @V_Palacio  Or could you share your FW file with us and let me try it on my site? Re: Cannot flash a PN7642 with Host Interface (I2C) HI, Find attached my FW file. Is generated as esfwu, but renamed so I can attach it here. Also attached my toml file and the original .bin FW. Let me know if works in your side. Regards, Re: Cannot flash a PN7642 with Host Interface (I2C) Hi @KaiLi , I assume this is not the problem, because it connects ok, and I had no problem updating the NXP secure firmware with the LPC via I2C. Regards, Re: Cannot flash a PN7642 with Host Interface (I2C) Hi, Some thoughts on this problem?. Regards,
記事全体を表示
PN7462AU FreeRTOS: heap_3からheap_4への切り替えに失敗し、システムが停止しました + ヒープ使用状況の可視化 チームの皆さん、こんにちは。私はFreeRTOSを搭載したPN7462AUプラットフォームを使用しており、SDKのサンプルはheap_3.cを使用するように構成されています。メモリオーバーフローの問題に直面しており、ヒープ構成についてより深く理解したいと考えています。 heap_3は標準ライブラリのmalloc()/free()を使用するため、xPortGetFreeHeapSize()やヒープ統計などの関数は利用できません。ヒープの使用状況を可視化し、利用可能なヒープを増やすために、heap_3.c を無効にして heap_3.c から heap_4.c に切り替えてみました。そしてheap_4.cを有効にする。しかし、この変更を加えた後、アプリケーションが起動中にフリーズしてしまう。 私には以下の質問があります。 PN7462AUでheap_3からheap_4に切り替えるのは安全で推奨されることでしょうか? heap_3に現在利用可能なメモリ量をどのように確認できますか? heap_3 は xPortGetFreeHeapSize() をサポートしていないため、ヒープの使用状況を監視し、メモリ不足を検出するための推奨される方法は何ですか? heap_3からheap_4に移行する際に、他にどのような構成変更が必要ですか(例:configTOTAL_HEAP_SIZE、リンカースクリプトの変更、メモリ領域など)? PN7462AUとFreeRTOSに特化したガイダンスや事例があれば、ぜひ教えていただきたいです。 ありがとう コアとメモリ Re: PN7462AU FreeRTOS: Unable to switch from heap_3 to heap_4, system stuck + heap usage visibility こんにちは、 @uday_gowda さん、 NFCリーダライブラリには、PN7462でFreeRTOSを実装した例が掲載されており、参考になるかもしれません。また、 AN11784を見ることをお勧めします。PN7462にRTOSを統合するためのガイダンスが載っており、参考にして参考にできます。 MCUXpresso IDEにはFreeRTOSベースのアプリケーション向けのデバッグ機能もいくつか含まれています。特に「ヒープ使用ビュー」がこのCASEに役立ちます。詳細は MCUXpresso IDE 25.06 FreeRTOSデバッグガイドの第3.6章に記載されています。 最後に、PN7462のSRAM容量は12KBのみであることにご注意ください。 BR ハビブ
記事全体を表示
S32k328 HSEドメインID こんにちは、NXPテクニカルチームの皆様 S32k328ドメインIDの正確な検証方法についてお問い合わせいたします。 現在、S32k328ボードとHSEファームウェアを使用しています。 - 環境設定: 私はHSEファームウェアイメージs32k358_hse_fw_1.14.0_2.40.0_pb230807.binを使用しています。 現在、マルチコア環境でRMモジュールを使用しています(XRDCのみ使用)。 - 質問: HSE FW RMでは、添付ファイルに示すように、S32k328ドメインIDは2に設定されています。 dpsdprtmvl_1-1781577003974.png しかし、S32k3xx RM 内の S32k328 ブロック図では、HSE は MDAC3 に設定されており、MDAC3 の DID (ドメイン ID) は 3 として出力されます。 dpsdprtmvl_2-1781577150058.png (1)登録確認コード:             uint32_t mda [ 8 ];             mda [ 0 ] = IP_XRDC -> MDA_W0_0_DFMT0 ;             mda [ 1 ] = IP_XRDC -> MDA_W0_1_DFMT1 ;             mda [ 2 ] = IP_XRDC -> MDA_W0_2_DFMT1 ;             mda [ 3 ] = IP_XRDC -> MDA_W0_3_DFMT0 ;             mda [ 4 ] = IP_XRDC -> MDA_W0_4_DFMT0 ;             mda [ 5 ] = IP_XRDC -> MDA_W0_5_DFMT1 ;             mda [ 6 ] = IP_XRDC -> MDA_W0_6_DFMT0 ;             mda [ 7 ] = IP_XRDC -> MDA_W0_7_DFMT1 ;             UART_Print ( "--- MDA ロック --- \n " );             for ( uint32_t i = 0 ; i < 8 ; i ++) ヤージュ                 uint32_t vld = ( mda [ i ] >> 31 ) & 1U ;                 uint32_t lk1 = ( mda [ i ] >> 30 ) & 1U ;                 uint32_t did = mda [ i ] & 0x3U ;                 UART_Print ( "MDA %lu=0x% lx VLD= %lu DID= %lu LK1= %lu %s \n " ,( unsigned long ) i , ( unsigned long ) mda [ i ],( unsigned long ) vld , ( unsigned long ) did , ( unsigned long ) lk1 , lk1 ? "(LOCKED)" : "" ); } (2)レジスタ値: MDA0=0x80000000 VLD=1 DID=0 LK1=0 MDA1=0x20000000 VLD=0 DID=0 LK1=0 MDA2=0x20000000 VLD=0 DID=0 LK1=0 MDA3=0xc0000003 VLD=1 DID=3 LK1=1 (ロック済み) MDA4=0x80000001 VLD=1 DID=1 LK1=0 MDA5=0x20000000 VLD=0 DID=0 LK1=0 S32k328の正しいドメインIDは何ですか? Re: S32k328 HSE DomainID こんにちは、 @dpsdprtmvl S32K328には0~3の4つのドメインがあり、HSEは常に利用可能な最高位のドメイン(この場合はドメイン3)に割り当てられます。 lukaszadrapa_0-1781608491449.png これは固定設定であり、変更できません。 表136は、主要な導関数のみを示しており、すべての副導関数を示していないため、少し分かりにくい。つまり、次のようになるということです。 2行目のS32K32xは、S32K322とS32K324を表します。 3行目のS32K35xは、S32K358、S32K356、S32K348、S32K338、S32K328、およびS32K37xとS32K39xの派生型を表します。 よろしくお願いいたします。 ルーカス
記事全体を表示
S32K344の受信割り込みは機能しません こんにちは、 私はS32K344のUARTについて研究しています。このチップのUART0/UART1/UART8を使用し、各UARTはRS485チップに接続され、A/Bピンを外部回路に引き出します。UART1のRS485のA端子をUART8のRS485のA端子に、UART1のRS485のB端子をUART8のRS485のB端子に接続します。UART1のRS485のDE/REを1、UART8のRS485のDE/REを0に設定します。UART1からUART8へデータを送信しようとしたところ、スコープ内でLPUART1_TXとLPUART8_RXに波形が観測されました。つまり、UART1からUART8へデータが送信されたということです。しかし、UART8には受信割り込みがないため、UART8の受信処理は実行できません。デバッグ中、UART8 CTRL の RE=1/RIE=1 は確認できますが、STAT の RDRF=0 となっています。UART8を送信、UART1を受信に切り替えてみましたが、現象は同じです。問題箇所を確認するのを手伝っていただけますか?プロジェクトファイルを添付します。ありがとう。 通信および制御(I3C | I2C | SPI | FlexCAN | イーサネット | FlexIO) S32K344's rx interrupt can't work こんにちは、ジュリアンさん、 お返事ありがとうございます。はい、CANやPITなどの他の割り込みは問題ありません。コールバック内のすべてのコードをコメントアウトしました(つまり、tx および rx 割り込みではコールバック内の rx 関数は実行されません)が、それでもコードは受信機ステータスチェックループから抜け出せず、RDRF フラグを設定することができません(interrupt.png の赤い四角を参照)。私はRx FIFOを使用していないので、データを受信するとRDRFは1になるはずです。しかし、そうではない。UART1から文字「R」(ASCII=0x01010010)と「Q」(ASCII=0x01010001)を送信し、UART1のTXDとUART8のRXDを測定したところ、波形は正しいようです。この問題を引き起こす可能性のある他の原因はありますか? SDKのバージョンも添付します。 Re: S32K344's rx interrupt can't work こんにちは、 @Jimmybai さん。 他の割り込みも問題なく動作すると思いますか?(PIT、CANなど)割り込みが発生しているかどうかを確認するために、コールバック関数内にブレークポイントを設定していますか? コードを見ると、 Lpuart_Uart_Ip_SyncReceive とLpuart_Uart_Ip_AsyncReceive の両方を使用していることがわかります。SyncReceive はポーリングを使用しますが、 AsyncReceive 関数は受信を開始したらすぐに処理を終了します。アプリケーションは受信完了のタイミングを知るために、受信ステータスを取得する必要があります。受信が完了したら(指定されたバイト数を受信したら)、 AsyncReceive を再度呼び出して新しい受信を開始する必要があります。 ただし、コールバック内では、AsyncReceive を再度呼び出す代わりに、Lpuart_Uart_Ip_SyncReceive 関数を使用して受信をブロックします。UARTの受信機能を再度有効にしてはいけません。 私たちのコミュニティには、参考になる事例がいくつかあります。 [RTD600 IP] S32K312-EVB Lpuart割り込みエコー - NXPコミュニティ S32K344 LPUART RX/TX ISR FreeRTOS S32DS36 RTD600 の例 - NXPコミュニティ よろしくお願いします、 ジュリアン Re: S32K344's rx interrupt can't work 添付ファイルが見つからないのはなぜだろう。再び取り付けてください。 S32K344's LPUART rx interrupt can't work こんにちは、ジュリアンさん。 根本原因を突き止めました。以下のコードでは、非同期受信コードを非同期送信コードの前に配置する必要があります。なぜなら、uartの送信は非常に高速で、送信が完了するとデータは受信バスに送信されているからです。この時点でレシーバの受信手順を開始し、データ信号はバス内で消えています。つまり、レシーバを有効にする必要があります。データ信号が入ったらレシーバは動作します。必要なのはレシーバの割り込み信号を確認するだけです。コードの分析にご協力いただき、ありがとうございました。 Jimmybai_0-1781766992780.png
記事全体を表示
以太网摄像头同步流媒体传输解决方案 我们正在为汽车摄像头系统开发基于i.MX8MP的定制主板。我们在5.15.71恩智浦Yocto BSP上使用VPU硬件解码器,有一条有效的单摄像机H.264 RTP直播流水线。我们目前计划通过以太网交换机将系统扩展至支持4路同时传输的摄像头流。 该交换机将聚合4个100BASE-T1摄像头端口,并通过千兆RGMII上行链路连接至i.MX8MP EQOS MAC,每个摄像头均隔离在各自的VLAN中。 我们的显示屏分辨率为1280x800。要实现4路视频同时显示,每路视频只需占据屏幕的四分之一(约640×400或更低分辨率,30帧/秒),因此我们可以根据需要降低摄像头的分辨率。 1.是否有涵盖多通道视频解码的恩智浦i.MX8MP参考设计或应用说明可以作为起点? 2。H.264 VPU 解码器能否处理来自不同来源的多个独立实例,还是需要预解码组合步骤来减少进程和上下文切换的数量?如果需要进行图像合成,在 i.MX8MP 上推荐采用什么方法? 3. 从恩智浦的角度来看,针对此用例,总体推荐的软件架构是什么? 我们未来的应用是全景视图,因此可扩展性和低延迟是关键要求。 谢谢! Re: Simultaneous Ethernet Camera Streaming Solution 嗨@Wobaffet i.MX8MP 可以作为此 4 通道以太网 H.264 摄像机四视图应用的候选平台;然而,只有 i.MX8QM 和 i.MX95 具有环视参考设计。 推荐的架构适用于四个 RTP/H.264流进入单独的 GStreamer 管道,由 VPU 硬件解码器分别解码,解码后进行硬件辅助缩放和合成,输出显示在 1280×800 显示器上。不建议在 H.264 解码之前尝试合成,因为除非上游交换机或摄像机已经完成解码和重新编码,否则无法将单独的 H.264 流直接合成到压缩功能域中的单个显示帧中。 对于 4 路 640×400@30fps 的显示要求,根据像素速率的粗略估计,负载明显低于 1080p60 解码,因此这种方法是合理的。然而,这是否最终满足环视的低延迟和稳定性要求,还需要进行系统级验证,考虑实际的摄像机比特率、配置文件、GOP、RTP抖动、DDR带宽、GStreamer零拷贝路径和合成方法。 此致, 志明 Re: Simultaneous Ethernet Camera Streaming Solution 你好, 谢谢你的回答! 作为后续, 1. 我们计划同时运行 4 个独立的 GStreamer 流水线,每个流水线使用 VPU 硬件解码自己的 H.264 流。我们想确认 5.15.71 BSP 中的 VPU 驱动程序是否支持 4 个真正并发的解码实例。该电路板支持包中是否存在任何已知的配置或限制,会阻止所有四个流水线并行解码,或者是否需要调度方法?如果有,能否提供一些例子? 2. 我们的设置中,有一个以太网交换机,通过单个 RGMII 上行链路将 4 个摄像头连接到 i.MX8MP,每个摄像头都有自己的 VLAN。在 Linux 端,我们计划在 EQOS 端口上创建 VLAN 子接口,并让每个 GStreamer 管道从其自己的子接口接收 UDP/RTP。关于这一点有两个问题:5.15.71 电路板支持包。中的 EQOS 驱动程序是否开箱即用地正确支持 802.1Q VLAN 标记帧,还是需要任何额外的配置?对于在此 电路板支持包。 中在此接口上同时运行 4 个 UDP 流,是否有已知的接收路径调优建议? 谢谢您!  
記事全体を表示
S32K344 的接收中断无法工作 您好,     我目前正在研究 S32K344 的 UART。我们使用该芯片的UART0/UART1/UART8,每个UART都连接到一个RS485芯片,并将A/B引脚引出至外部电路。我将UART1的RS485接口的A引脚连接到UART8的RS485接口的A引脚,并将UART1的RS485接口的B引脚连接到UART8的RS485接口的B引脚。 我将UART1 RS485的DE/RE设置为1,将UART8 RS485的DE/RE设置为0。我尝试将数据从 UART1 发送至 UART8,并在示波器上观察到 LPUART1_TX 和 LPUART8_RX 信号线上有波形。这意味着,数据已从UART1发送至UART8。但 UART8 中没有 rx 中断,因此 uart8 的 rx 处理程序无法运行。在调试过程中,我可以看到 UART8 CTRL 的 RE=1/RIE=1,但 STAT 的 RDRF=0。我将发送端口切换为UART8,接收端口切换为UART1,但现象依然如故。您能帮忙查一下问题出在哪里吗?我将该项目附上。谢谢。 通信& 控制(I3C | I2C | SPI | FlexCAN | 以太网 | FlexIO) S32K344's rx interrupt can't work 嗨,胡利安, 谢谢您的答复。是的,其他中断,例如 CAN、PIT 都没有问题。现在我已将回调函数中的所有代码注释掉(这意味着发送和接收中断都不会在回调中执行接收函数),但代码仍然无法脱离检查接收器状态的循环,也无法使 RDRF 标志被设置(参见 interrupt.png 中的红色矩形)。我没有使用 Rx FIFO,因此,当接收到数据时,RDRF 应该变为 1。但事实并非如此。我通过UART1发送字符'R'(ASCII=0x01010010)和'Q'(ASCII=0x01010001),并测量了UART1的TXD和UART8的RXD,波形看起来是正确的。还有其他可能导致此问题的原因吗? 我同时附上了我的 SDK 版本。 Re: S32K344's rx interrupt can't work 嗨,@Jimmybai, 我想其他中断应该都能正常工作吧?(PIT、CAN 等)。你是否在回调函数中设置了断点,以确认中断是否触发?  从你的代码中我可以看出你同时使用了 LPUART_UART_IP_SyncreCeive & LPUART_UART_IP_Asyncreceiv e lpuart_UART_IP_ Asyncreceive。SyncreCeive 使用轮询,而 AsyncreCeive 功能则支持接收并立即退出功能。应用程序必须获得接收状态才能知道何时完成接收。接收完成后(已定义的接收字节数), 您需要再次调用 AsyncreCeive 以开始 新的接收。 不过,在回调函数内部,不要再次调用 AsyncReceive,而应使用 Lpuart_Uart_Ip_SyncReceive 函数进行阻塞式接收。你永远不会重新布防 UART 的接收。 我们社区里有一些例子,你可以参考一下:  [RTD600 IP] S32K312-EVB Lpuart 中断回显 - NXP 社区 示例 S32K344 LPUART 接收/发送中断处理程序 FreeRTOS S32DS36 RTD600 - NXP 社区 致以最诚挚的问候, Julián Re: S32K344's rx interrupt can't work 我不知道为什么我的附件不见了。将其重新安装。 S32K344's LPUART rx interrupt can't work 嗨,朱利安, 我找到了根本原因。下面的代码中,异步接收代码应该放在异步发送代码之前。因为UART传输速度非常快,发送完成后,数据就已经发送到接收总线了。此时,当您开始接收器接收程序时,总线上的数据信号已经消失。所以,我们需要启用接收器,当数据信号到来时,接收器才能工作。我们只需要检查接收器的接收中断信号即可。感谢您帮忙分析我的代码。 Jimmybai_0-1781766992780.png
記事全体を表示
P1013 为确保散热和通信稳定性而对 CPU/CCB/DDR 进行降频 我的开发板上有旧的 P1013NSE2MHB 元器件。 我想降低它们的时钟以降低元器件的热负荷,并使用 P1013NSE2LFB 元器件的 PCIe 和 SPI 标准的通信时钟,这是我最熟悉的。 简而言之,我希望让 P1013NSE2MHB 采用 P1013NXE2LFB 的 PLL 时钟配置,即 P1013NSE2MHB 的 CPU/CCB/DDR 最终时钟频率应为 1067/533/533 MHz。  根据 AN4343 第 6 节,两个元器件都应该能够支持 1067/533/533 的时钟速度。 我唯一担心的是,P1013NSE2MHB的CCB限制据说为480MHz。除了只有 CCB 时钟 400 和 480 MHz 才能使用内置的 PLL 设置来达到最大值 1200MHz 之外,我找不到任何理由。(参见AN4343第6.2.1节表16) 我只想让CPU的核心频率达到1067MHz。  P1013NSE2MHB 和 P1013NXE2LFB 均来自同一产品线,应采用相同的架构;因此,即使 CPU 最大时钟频率提升至 1200MHz,也不应妨碍使用先前已实现的 CCB 架构来实现较低的 CPU 时钟频率。除非重新设计CCB总线以支持新的CPU,尽管没有根本的不同,但这将是资源的巨大浪费。 感谢大家提供的见解。 QorIQ P1 设备 Re: P1013 CPU/CCB/DDR Underclocking for Thermal and Communication Stability 根据以下数据,架构似乎有所不同,CPU/CCB/DDR可能不会有相同的趋势 CPU/CCB/D DR 频率 (MHz) LF=1067/533/667 MH=1200/480/800 但这是旧设备,因此可能需要向恩智浦内部团队查询解释 Re: P1013 CPU/CCB/DDR Underclocking for Thermal and Communication Stability 你好, 是的——文档支持您的观察,即 CPU/核心、平台/CCB 和 DDR 在 T2080/T2081 上不必遵循相同的扩展趋势,因为它们是由不同的 PLL 功能域生成的,并且内存总线明确地由其自身的 PLL 决定。核心时钟和平台时钟由不同的 PLL 生成,T2080/T2081 时钟映射为核心集群 PLL、平台 PLL 和 DDR PLL 公开了单独的状态/控制点( Clocking_PLLCnGSR 、 Clocking_PLLPGSR 、 Clocking_PLLDGSR )。硬件规格还直接指出,内存总线时钟速度由其自身的 PLL 决定。 因此,从建筑学角度解释如下: CPU/核心频率来自核心集群PLL,根据配置的不同,可能以PLL/1、/2或/4运行。 平台/CCB 频率是一个独立的平台时钟域,具有其自身允许的 SYSCLK 比率。 DDR频率是独立于DDR的,内存总线时钟频率是DDR数据速率的一半,并由其自身的PLL控制。 这就是为什么像以下这种看起来非单调的数对: LF = 1067 / 533 / 667 MH = 1200 / 480 / 800 从建筑学的角度来看,这在原则上是合理的:这三个功能域不需要同时上升和下降。然而,我在现有的 T2080/T2081 资料中找不到记录的那两个 T2080 频率三元组。   此致 Re: P1013 CPU/CCB/DDR Underclocking for Thermal and Communication Stability 我问的不是T2080/T2081处理器。 我正在考虑P1013/P1022处理器。
記事全体を表示
ECU Core Configuration Clarification on S32K311 Hi @danielmartynek and Team We have one question regarding core configuration. On S32K311 (single-core), the generated code defines: DET_NO_ECU_CORES = 4 NUMBER_OF_CORES = 4 Since we are facing RAM constraints: Can we safely reduce these to 1? Any side effects in MCAL/DET? Also, is there a way to configure this in the NXP config tool or any configuration instead of manually editing generated files? Thanks & Regards, Yusup Khan S32K3  S32DS-ARM S32K31XEVB-Q100 Re: ECU Core Configuration Clarification on S32K311 Hi @yusupkhan241, Refer to this answer provided by the RTD SW development team: https://community.nxp.com/t5/S32K/RTD-memory-occupation/td-p/2148479 This parameter cannot be configured via the configuration tool, and there are currently no plans to support such functionality. Regards, Daniel
記事全体を表示
GD3160 SPI 配置 根据数据手册,如果我要配置 GD3160,需要先将 MODE_2 中的 CONFIG_EN 位设置为 1。既然如此,MODE_2 的第一位(Rb/W)应该是 0 还是 1? Re: GD3160 SPI 配置 了解后请看下面: 正确的解释确实是: 0 = 读取 1 = 写入   Re: GD3160 SPI 配置 是的,另外除了下图中说的 CONFIG1 to 7 registers, the MODE1 and 2 registers, the RMSK1 and RMSK2 registers, and the MSK1 and 2 registers ,这些寄存器的写受MODE_2的CONFIG_EN控制,其余寄存器只要bit23为1的情况就会进行配置吗? henh_0-1781578575329.png Re: GD3160 SPI 配置 guoweisun_0-1781578136768.png 你说的是bit23吗?
記事全体を表示
P1013 CPU/CCB/DDR Underclocking for Thermal and Communication Stability I have old P1013NSE2MHB components on dev boards.  I want to work to under clock them to reduce the thermal load on the component and use the communication clock for PCIe and SPI standard from the P1013NSE2LFB component, It is what I am most familiar with. Essentially, I want to have the P1013NSE2MHB use the P1013NXE2LFB PLL clocking setup, i.e, CPU/CCB/DDR final clock rates of the P1013NSE2MHB to be 1067/533/533 MHz.  Based on the AN4343 Section 6 both components should be able to support the 1067/533/533 clock speeds.  The only concern that I have is that the CCB limit of the P1013NSE2MHB is supposedly 480MHz. I can find no reasoning for this besides that only CCB clocks 400 and 480 MHz can use the built in PLL settings to get to the maximum of 1200MHz. (See AN4343 Section 6.2.1 Table 16) I just want the CPU to have a core clock of 1067MHz.  Both the P1013NSE2MHB use the P1013NXE2LFB are from the exact same line and should share the same architecture, the improvement in the CPU maximum clock to 1200MHz should not prevent the previously implemented CCB architecture from being used to reach a lower CPU clock speed. Unless the CCB bus was redesigned, which would be a massive waste of resources, to support the new CPU even though it isn't radically different.  Thanks for any insights. QorIQ P1 Devices Re: P1013 CPU/CCB/DDR Underclocking for Thermal and Communication Stability It seems the architecture may be different according to the data below, the CPU/CCB/DDR may not share the same trend CPU/CCB/DDR frequency (MHz) LF=1067/533/667    MH=1200/480/800 But this is old device so may need to check with NXP internal team for the explaination Re: P1013 CPU/CCB/DDR Underclocking for Thermal and Communication Stability The T2080/T2081 are not the processors I am asking about. I am looking at the P1013/P1022 processors. Re: P1013 CPU/CCB/DDR Underclocking for Thermal and Communication Stability Hello, Yes — the documentation supports your observation that CPU/core, platform/CCB, and DDR do not have to follow the same scaling trend on T2080/T2081, because they are generated by different PLL domains and the memory bus is explicitly dictated by its own PLL . Core and platform clocks are generated by different PLLs , and the T2080/T2081 clocking map exposes separate status/control points for core-cluster PLLs, the platform PLL, and the DDR PLL ( Clocking_PLLCnGSR , Clocking_PLLPGSR , Clocking_PLLDGSR ) The hardware specs also state directly that the memory bus clock speed is dictated by its own PLL. So the architectural explanation is: CPU/core frequency comes from the core cluster PLL(s) and may run at PLL/1, /2, or /4 depending on configuration. Platform/CCB frequency is a separate platform clock domain with its own allowed SYSCLK ratios. DDR frequency is separate again, and the memory bus clock is half the DDR data rate and is controlled by its own PLL That is why a non-monotonic-looking pair such as: LF = 1067 / 533 / 667 MH = 1200 / 480 / 800 is architecturally plausible in principle: the three domains are not required to rise and fall together. However, I could not find those exact two T2080 frequency triplets documented in the available T2080/T2081 material.   Regards
記事全体を表示
GD3160 SPI 構成 データシートによると、GD3160を設定するには、まずMODE_2のCONFIG_ENビットを1に設定する必要があります。その場合、MODE_2の最初のビットであるRb/Wは0であるべきか、それとも1であるべきか? Re: GD3160 SPI 配置 理解済み请次を参照: 正しい解釈は確かに次の通りです。 0 = 読み取り 1 = 書く   Re: GD3160 SPI 配置 はい、下の図に示されているCONFIG1~7レジスタ、MODE1およびMODE2レジスタ、RMSK1およびRMSK2レジスタ、MSK1およびMSK2レジスタ(これらの書き込みはMODE_2のCONFIG_ENによって制御されます)に加えて、ビット23が1である限り、他のレジスタも設定されますか? henh_0-1781578575329.png Re: GD3160 SPI 配置 guoweisun_0-1781578136768.png 23番目のビットのことですか?
記事全体を表示
S32K311におけるECUコア構成の明確化 こんにちは、 @danielmartynek さん、そしてチームの皆さん。 コア構成に関して質問が1つあります。S32K311(シングルコア)では、生成されたコードで以下のように定義されます。 DET_NO_ECU_CORES = 4 コア数 = 4 RAMの制約に直面しているため: これらを安全に1に減らすことは可能でしょうか? MCAL/DETに副作用はありますか? また、生成されたファイルを手動で編集するのではなく、NXPの設定ツールやその他の設定ツールでこれを設定する方法はありますか? よろしくお願いいたします。 ユスプ・カーンS32K3 S32DS-ARM S32K31XEVB-Q100 Re: ECU Core Configuration Clarification on S32K311 こんにちは、@yusupkhan241 さん。 RTDソフトウェア開発チームが提供したこちらの回答を参照してください。 https://community.nxp.com/t5/S32K/RTD-memory-occupation/td-p/2148479 このパラメータは設定ツールでは設定できず、現時点ではそのような機能をサポートする予定もありません。 よろしくお願いいたします。 ダニエル
記事全体を表示
无法通过主机接口(I2C)对 PN7642 进行烧录 你好 我正在尝试使用 LPC55S16 配套主板通过 i2C 在 PN7642 中刷新自定义固件。 我已经使用 Host Crypto Scripts (01.03) 生成了 esfwu 文件,将 C101 芯片的文件用作传输密钥(我们已经重新设计了 EVK 板来焊接新的 C101 芯片) PN7642通过主机接口更新用户固件的分步指南  自定义(不安全)更新因错误代码 0x01 而失败。  如果我刷入 NXP 固件(安全版),版本 03.00,就能正常工作。 我怀疑HostScript配置文件对某位客户的防火墙来说有问题。 我只是将其修改了一下,将 aes_key 从 C100 传输密钥改成了 C101 传输密钥。 能帮我一下吗? 此致, Re: Cannot flash a PN7642 with Host Interface (I2C) 你好@V_Palacio 对于 C101,您应该选择项目: KaiLi_0-1781878068922.png 要更新自定义固件,您应该将自定义固件放在正确的路径中,然后选择“6”。 Re: Cannot flash a PN7642 with Host Interface (I2C) 你好@V_Palacio 或者您能否将您的固件文件分享给我们,让我在我的网站上测试一下? Re: Cannot flash a PN7642 with Host Interface (I2C) 您好, 附件是我的固件文件。生成的文件名为esfwu,但为了方便上传,我已将其重命名。 我还附上了我的 toml 文件和原始的 .bin 文件。FW。 如果你们那边运行正常,请告诉我。 此致, Re: Cannot flash a PN7642 with Host Interface (I2C) 嗨@KaiLi , 我估计这不是问题所在,因为它连接正常,而且我通过 I2C 使用 LPC 更新 NXP 安全固件也没有遇到任何问题。 此致, Re: Cannot flash a PN7642 with Host Interface (I2C) 你好, 关于这个问题,大家有什么想法吗? 问候,
記事全体を表示
GD3160 SPI 配置 According to the data sheet, if I want to configure the GD3160, I need to first set the CONFIG_EN bit in MODE_2 to 1. In that case, should the first bit of MODE_2, Rb/W, be 0 or 1? Re: GD3160 SPI 配置 了解了请看下面: The correct interpretation is indeed: 0 = Read 1 = Write   Re: GD3160 SPI 配置 Yes, and in addition to the CONFIG1 through 7 registers, the MODE1 and 2 registers, the RMSK1 and RMSK2 registers, and the MSK1 and 2 registers shown in the figure below—writing to these registers is controlled by CONFIG_EN in MODE_2—will the remaining registers be configured whenever bit 23 is set to 1? henh_0-1781578575329.png Re: GD3160 SPI 配置 guoweisun_0-1781578136768.png Are you talking about bit23?
記事全体を表示